2381953_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2381953_en-US

2381953_en-US

ECU Core Configuration Clarification on S32K311

Hi @danielmartynek and Team

We have one question regarding core configuration. On S32K311 (single-core), the generated code defines:

  • DET_NO_ECU_CORES = 4
  • NUMBER_OF_CORES = 4

Since we are facing RAM constraints:

  • Can we safely reduce these to 1?
  • Any side effects in MCAL/DET?

Also, is there a way to configure this in the NXP config tool or any configuration instead of manually editing generated files?

Thanks & Regards,
Yusup Khan S32K3  S32DS-ARM S32K31XEVB-Q100

Re: ECU Core Configuration Clarification on S32K311

Hi @yusupkhan241,

Refer to this answer provided by the RTD SW development team:
https://community.nxp.com/t5/S32K/RTD-memory-occupation/td-p/2148479


This parameter cannot be configured via the configuration tool, and there are currently no plans to support such functionality.


Regards,

Daniel



Tags (1)
No ratings
Version history
Last update:
‎06-17-2026 03:27 AM
Updated by: