Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
RDDRONE-BMS772开发板 我想了解关于RDDRONE-BMS772这个型号的板子,板子上包含有外部温度传感器的引脚,配件里也有热敏电阻,这个板子能用来测量电池的温度吗?但是板子的配件里只写了热敏电阻,没写温度传感器,如果板子可以用来可以测量温度的话温度传感器需要自己买吗?温度传感器又应该安装在什么地方? Re: RDDRONE-BMS772开发板 你好 fan007 再会! 我想了解更多关于RDDRONE-BMS772板的信息。 它包含用于外部温度传感器的引脚,配件中还包含一个热敏电阻。这个板可以用来测量电池温度吗?但是,配件清单上只列出了热敏电阻,没有列出温度传感器。如果该电路板可以用来测量温度,我是否需要单独购买温度传感器?温度传感器应该安装在哪里? 在《RDDRONE-BMS772 参考设计入门指南》中,您可以找到一个章节,其中描述了购买此板所包含的所有内容。 是的,它包含一个带电缆的外部热敏电阻,可以用作温度传感器。不过,您也可以使用您认为更可靠的其他传感器。电路板上确实有一个专用的端口用于连接此传感器。有关其连接和使用的更多详细信息,请参阅我们网站上提供的文档。 请查看: UM11421,RDDRONE-BMS772 参考设计 - 用户指南(您需要注册账号才能访问此文档) RDDRONE-BMS772 可以选配外部温度传感器。 使用连接器 J1 的电路板。该外部传感器的应用示例是: 监测电池组内部各电芯的温度。 希望这些信息对您有所帮助,如果您还需要其他帮助,请告诉我。 祝你今天过得愉快,一切顺利。
View full article
Zephyr:支持 RW61X 的压缩固件 CONFIG_NXP_COMPRESS_WIFI_NB_FW 默认在https://github.com/nxp-zephyr/nxp-zephyr/commit/e64f39fa2a05edec7bd8a2b24d9f1236c43d6c35中启用 如果没有 rw61x_sb_wifi_a2_compressed.bin 文件,Cmake 将失败。是否缺少压缩步骤?支持哪些压缩方法? 我没有看到加载器有任何变化。它能自动处理压缩固件吗? Re: zephyr: support compressed FW for RW61X 我现在看到有NXP Zephyr论坛。应该把它移到那里吗? Re: zephyr: support compressed FW for RW61X 我使用的是 nxp-v4.4-branchzephyr/samples/net/wifi/shell 在 frdm_rw612 上。 我明白发生了什么。我忽略了这个西部更新错误: === 正在更新 wifi_nb_fw (modules/hal/nxp/zephyr/blobs): 致命错误:目标路径“modules/hal/nxp/zephyr/blobs”已存在且不是空目录。 然后,为了获取固件,我按照https://docs.zephyrproject.org/latest/boards/nxp/frdm_rw612/doc/index.html#wireless-connectivity-support中的说明,使用了“west blobs fetch hal_nxp”命令。 这样就无法下载压缩图像,导致我在设置 CONFIG_NXP_COMPRESSED_WIFI_NB_FW 时看到错误。 blobs 目录中已经包含来自以下位置的文件: https://github.com/nxp-zephyr/hal_nxp/tree/nxp-v4.4-branch/zephyr/blobs/license/ 我使用的是来自 .mcuxpressotools/.mcux-venv-3.12/bin/west 的 west。版本号为 v1.5.0。 我尝试了一个旧版本(v1.3.0),west 只是将仓库添加到现有的非空目录中,并没有报错。 Re: zephyr: support compressed FW for RW61X 你好, 希望你一切都好。请问您具体在测试什么? 您是在参考具体的例子吗? 你做了任何修改吗? 顺祝商祺! 里卡多
View full article
S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault Hello NXP team,   We are using S32K328 with RTD 7.x.   Software setup: - CM7_0 runs a bootloader. - CM7_1 is used by a second application. - CM7_2 is not intended to execute application code. - We are evaluating whether CM7_0 can use CM7_2 DTCM as system memory through the TCM backdoor/AHBS path.   Reference Manual context: Chapter “Memory Map” says ITCM/DTCM can be accessed through the 32-bit AHBS interface by other masters, including other Cortex-M7 cores and eDMA. The “TCM as system memory” section says an enabled core can use TCM of a disabled/waiting core after: 1. Enabling the target core TCM controller clock:    MC_ME PRTN2_COFB2_CLKEN[REQ64] for Cortex-M7_2 2. Setting target core CPUWAIT:    DCM_GPR DCMRWF4[CM7_2_CPUWAIT] 3. Enabling target core clock/access path:    MC_ME PRTN0_CORE4_PCONF[CCE]   What we tried: 1. Set DCM_GPR DCMRWF4[CM7_2_CPUWAIT]. 2. Set MC_ME PRTN2_COFB2_CLKEN[REQ64]. 3. Set MC_ME PRTN2_PUPD[PCUD]. 4. Applied MC_ME CTL_KEY sequence. 5. Waited for PRTN2_PUPD[PCUD] to clear. 6. Read PRTN2_COFB2_STAT and observed bit0/BLOCK64 active. 7. Set MC_ME PRTN0_CORE4_PCONF[CCE]. 8. Set MC_ME PRTN0_CORE4_PUPD[CCUPD]. 9. Applied MC_ME CTL_KEY sequence. 10. Waited for PRTN0_CORE4_STAT[CCS] to become 1. 11. Disabled MPU temporarily for the experiment. 12. Tried a single 32-bit write to the CM7_2 DTCM backdoor address.   Observed result: - PRTN2_COFB2_STAT indicates the TCM controller clock request is active. - PRTN0_CORE4_STAT[CCS] becomes 1. - The first 32-bit write to the CM7_2 DTCM backdoor region causes an imprecise BusFault escalated to HardFault.   Questions: 1. For S32K328, what is the correct CM7_2 DTCM backdoor/system address range accessible from CM7_0? 2. Is CM7_2 DTCM backdoor access from CM7_0 supported while CM7_2 remains in CPUWAIT? 3. Besides MC_ME and DCM_GPR setup, is any XRDC configuration required to allow CM7_0 to write to CM7_2 DTCM backdoor? 4. Is any MPU region required even if MPU is temporarily disabled for the test? 5. Is any MSCM/MCM/XBIC/ENEDC setting required before using the TCM backdoor path? 6. Is PRTN2_COFB2_STAT[BLOCK64] the correct status bit to confirm CM7_2 TCM controller clock is active? 7. Is PRTN0_CORE4_STAT[CCS] the correct status bit to confirm CM7_2 clock/access path is active? 8. For DTCM ECC initialization through backdoor access, is a 32-bit write from CM7_0 sufficient? 9. If the first backdoor write causes an imprecise BusFault, which fault/XRDC registers should be checked to identify whether the failure is due to XRDC, interconnect, or unmapped address?   Current goal: We only want to validate a minimal smoke test: - one 32-bit write to CM7_2 DTCM backdoor, - then readback, - before considering any production use.   Thank you. Re: S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault Hello @krishna_Bugudi, 1. Refer to the S32K3xx_memory_map.xlsx, DTCM_2 backdoor at 0x21800000 2. Yes 3. No 4. No 5. No 6. Yes, refer to RM, Section 3.4 TCM as system memory 7. Yes 8. Yes, refer to RM, Table 102. Memory ECC initialization summary 9. You wrote that XRDC is disabled. So, it won't be reported by XRDC.  What address do you write? Regards, Daniel Re: S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault Hello Daniel,   Thank you for the confirmation.   We updated the test to follow the RM/NXP sequence exactly and are still seeing the store hang.   Confirmed address: We are writing to:   0x21800000   This matches S32K3xx_memory_map.xlsx:   DTCM_2 Backdoor: - Start address: 0x21800000 - End address:   0x2181FFFF - S32K328 implemented size: 128 KB   The memory map also shows PRAM2_TCM_XBIC is present on S32K328 at: 0x40408000 - 0x4040BFFF   and describes it as: "Crossbar Integrity Checker (PRAM2 & TCM backdoor AHB Splitter"   while TCM_XBIC at 0x40400000 is marked Reserved for S32K328.   Latest test sequence:   1. Set MC_ME PRTN2_COFB2_CLKEN[REQ64]. 2. Set MC_ME PRTN2_PUPD[PCUD]. 3. Apply MC_ME CTL_KEY sequence. 4. Wait for PRTN2_PUPD[PCUD] to clear. 5. Read PRTN2_COFB2_STAT.   Observed: PRTN2_COFB2_STAT = 0x00000039   6. Set DCM_GPR DCMRWF4[CM7_2_CPUWAIT].    Readback confirms:    DCMRWF4 = 0x00080000   7. Set MC_ME PRTN0_CORE4_ADDR to a safe loop address.    Readback:    PRTN0_CORE4_ADDR = 0x00402408   8. Set MC_ME PRTN0_CORE4_PCONF[CCE]. 9. Set MC_ME PRTN0_CORE4_PUPD[CCUPD]. 10. Apply MC_ME CTL_KEY sequence. 11. Wait for PRTN0_CORE4_STAT[CCS] to become 1.   Observed: PRTN0_CORE4_STAT = 0x00000001   12. Disable CM7_0 MPU temporarily for isolation.    MPU_CTRL before disable = 0x00000003   13. Attempt one single 32-bit write:      *(volatile uint32_t *)0x21800000 = 0u;   Latest breadcrumb log:   [CORE2_DTCM_SMOKE] S4B: WORD0 WRITE START addr=0x21800000   The next breadcrumb after the store is not reached:   [CORE2_DTCM_SMOKE] S4B1: WORD0 STORE ISSUED BEFORE DSB   So the store itself appears to stall or not complete before reaching the following instruction. The DSB is not reached in this latest test.   Question: Since you confirmed that: - 0x21800000 is the correct DTCM_2 Backdoor address, - CM7_0 access is supported while CM7_2 is in CPUWAIT, - no additional XRDC/MPU/MSCM/MCM/XBIC/ENEDC setup is required, - PRTN2_COFB2_STAT[BLOCK64] is the correct status bit, - PRTN0_CORE4_STAT[CCS] is the correct status bit, - 32-bit writes are valid for DTCM ECC initialization,   what could cause the first 32-bit store to 0x21800000 to stall before completion?   Should we inspect PRAM2_TCM_XBIC at 0x40408000 for TCM backdoor AHB splitter errors on S32K328?   If yes, could you please point us to: 1. The PRAM2_TCM_XBIC status/error registers to read. 2. The expected error indication for a failed DTCM_2 backdoor transaction. 3. Whether any error-clear sequence is required before retrying the access. 4. Any other MC_ME/DCM/MSCM/XBIC/fault registers that should be captured when the store does not complete.   Regards, Krishna Re: S32K328: CM7_0 access to CM7_2 DTCM backdoor causes imprecise BusFault Hi Krishna,  Copilot said: I have tested it and was able to reproduce this error only when the default MPU is enabled in the project (configured in system.c generated by the S32DS RTD project). Could you dump the MPU registers to verify whether the MPU is disabled in your project? Regards, Daniel
View full article
EB 错误 大家好: 激活 EB Tresos 时出现错误: 错误:flxActAppActivationSend (50040,41147,10248) 指定的数量超过了允许的最大数量(0)。 连接 FlexNet Operations Server 失败。 我的代码是 7416-E905-5CC2-F20A,有效期至 2026 年 9 月 30 日。 请问有人知道如何解决这个问题吗?非常感谢您的帮助。 Re: EB ERROR 你好, 这意味着我们从 EB 获得的所有免费许可证都已用完。 通常需要几天时间,新的内容才会出现在 NXP 网站上。 顺祝商祺! Peter
View full article
FRDM-RW612 EVKで外部U.FLアンテナを有効にする方法 こんにちは、NXP チームの皆様、 私はFRDM-RW612 EVKをSDKのwifi_cli例で使っています。ロードされたWi-Fiファームウェアはrw61x_sb_wifi_a2.binです。 EVKのUFLコネクタ(J11)にMolex 1461539050外部アンテナを接続しました。しかし、オンボードPCBアンテナと比較して、RSSIの改善は見られませんでした。場合によってはRSSIがさらにわずかに低いこともあります。 Prathyush_27_0-1783428299975.png FRDM-RW612の回路図とユーザーガイドから、RFスイッチ(U16 - RTC7608U)はオンボードPCBアンテナと外部UFLコネクタのどちらかを選択し、RF_CNTL_3がこのスイッチの制御信号であることを理解しています: RF_CNTL_3 = 0 -> PCBアンテナ(デフォルト) RF_CNTL_3 = 1 -> 外部UFLアンテナ RF_CNTL_3を制御する方法は? RF_CNTL_3はWi-Fiファームウェアによって自動的に駆動されますか?はいの場合、そのデフォルト値は何ですか?その値を変更するにはどうすればよいですか? EVKの外部アンテナを有効にするには、ハードウェアまたはファームウェアの設定が必要ですか? 何かご指導やサンプルコードがあれば大変助かります。 よろしくお願いします。 Re: How to enable the external U.FL antenna on FRDM-RW612 EVK こんにちは、 確認させてください。 よろしくお願いいたします。 ダニエル。 Re: How to enable the external U.FL antenna on FRDM-RW612 EVK こんにちは、 @DanielRuvalcaba さん。この件について確認していただけましたでしょうか?何か進展がありましたらお知らせください。 よろしくお願いいたします。 プラティシュ Re: How to enable the external U.FL antenna on FRDM-RW612 EVK こんにちは、 プライベートメッセージを送りました。 よろしくお願いいたします。 ダニエル。 Re: How to enable the external U.FL antenna on FRDM-RW612 EVK こんにちは @DanielRuvalcaba また、FRDM-RW612のUFLコネクタ(J11)にアンテナを交換したいとも思っています。 どうやってやるのか、教えていただけますか? フロントエンドモジュール(FEM)の設定でアンテナを切り替えているのでしょうか? よろしくお願いいたします マルチン Re: How to enable the external U.FL antenna on FRDM-RW612 EVK こんにちは、 プライベートメッセージでご連絡いたしました。 よろしくお願いいたします。 ダニエル。 Re: How to enable the external U.FL antenna on FRDM-RW612 EVK どうやって直したのですか? Re: How to enable the external U.FL antenna on FRDM-RW612 EVK こんにちは、 @Tusisima さん。u.FLアンテナを有効にするには、特別なキャリブレーションファイルが必要です。アンテナの選択はこのキャリブレーションデータによって制御されるためです。キャリブレーションファイルを取得するにはNXPのサポート担当者に連絡してください。
View full article
S32K312: WKUP Interrupt Not Triggering DiaDev_0-1783418064066.png DiaDev_1-1783418072029.png DiaDev_2-1783418089747.png I have configured PTB2 as the WKUP input pin, and WKUP Channel 8 is mapped to PTB2. The WKUP module configuration appears to be correct; however, the WKUP interrupt is not being triggered. Previously, I configured the same pin as an EIRQ input, and the interrupt was triggered successfully, confirming that the pin and external signal are functioning correctly. Issue: PTB2 configured as WKUP input. WKUP Channel 8 mapped to PTB2. No WKUP interrupt is received. The same hardware setup works correctly with EIRQ configuration. Please help identify if there are any additional WKUP configuration requirements, dependencies, or known limitations that could prevent the interrupt from being generated.     Wkpu_Ip_Init(0U, &Wkpu_Ip_Config_PB);     /* INT2: Wakeup Trigger. */     Wkpu_Ip_EnableInterrupt(0,    Wkpu_Ip_ChannelConfig_PB[2U].hwChannel);     Wkpu_Ip_EnableNotification(Wkpu_Ip_ChannelConfig_PB[2U].hwChannel); Re: S32K312: WKUP Interrupt Not Triggering Hi @DiaDev, S32K3, added to the ~60 external wake-ups, also provides 4 internal wake-up sources, which must be taken into consideration when configuring a channel; this means, adding +4 as offset: Julin_AragnM_0-1783443817593.png PTB2 is the wake-up pad [8], plus the four internal sources, it will be the channel 12. Please change this configuration and test out if WKPU is triggered or not. Best regards, Julián
View full article
FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly Hello NXP Community, I am mechanical and electrical engineering background, and this is my first time diving deep into complex System-on-Chips (SoCs) and embedded Operating Systems. For my project, I am using the FRDM-IMX95 development board. My ultimate goal is to run two operating systems in parallel using an IPC (Inter-Process Communication) framework. The board arrived with a pre-installed Linux image on the internal eMMC. This works flawlessly out of the box, and I get full serial output logs in my terminal monitor program. Now, I am trying to follow the official Getting Started Guide to flash the standard Linux BSP image onto a microSD card using UUU (Universal Update Utility) on a Windows host machine. According to the Windows command prompt, the UUU flashing process completes with a "SUCCESS" status. I used the following standard command layout: ".\uuu.exe -b sd_all imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all imx-image-full-imx95evk.wic" The Problem: After successful flashing, I turn off the board and configure the physical boot switches for SD Boot Mode by setting SW1 [1:2] to 11 (ON / ON). When I power the board back on, the serial monitor remains completely blank. There is absolutely no text output or hardware initialization visible. 1. Do I have a fundamental misunderstanding of how the boot chain works here? According to the i.MX Linux User's Guide, the .wic image contains all four essential pieces, including the bootloader image (U-Boot). Shouldn't I at least see the initial U-Boot SPL sequence appearing on my serial monitor, since the basic hardware configuration blocks should be read from the card? Any insights, common pitfalls for beginners on this specific FRDM variant, or hidden switch requirements would be highly appreciated! Best regards FRDM-Training Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly Hello,  I'm testing on my side to share the exact steps for you, I will update soon.  Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly Thank you for looking into this and testing it on your end! I appreciate the help and look forward to your update. Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly You have the issue because you are trying to flash to the SD card with the uuu tool, it is made to flash the emmc, if you want to flash the sd card you have to perform the following command in a linux host machine.  $ sudo dd if= .wic of=/dev/sdx bs=1M && sync To identify the device node assigned to the SD/MMC card, carry out the following command: $ cat /proc/partitions major minor #blocks name 8 0 78125000 sda 8 1 75095811 sda1 8 2 1 sda2 8 5 3028221 sda5 8 32 488386584 sdc 8 33 488386552 sdc1 8 16 3921920 sdb 8 18 3905535 sdb1
View full article
S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hello, Following up on the CRS domain Secure Debug authentication issue discussed in the earlier post ("S32N55 HSE2 CRS domain authentication does not complete"), I'd like to report a new, more specific finding that I believe points to the root cause. Posting this separately as suggested. Setup: - S32N55, HSE2, CRS domain (APP_CHALLENGE), Lauterbach TRACE32 / SDC-600 - Auth flow: COMM_START -> AUTH_MODE_REQ -> APP_CHALLENGE (StartCmd) -> receive challenge -> send ProofProvCmd (debugSignalMap(4B) + appChallengeAuth(16B) via AES-CMAC) Finding: After sending debugSignalMap(4B) + appChallengeAuth(16B) = 20 bytes total via the ProofProvCmd packet, the host's SDC-600 TX FIFO status register (bit[7:0] at MU base+0xD2C) never reports free space again. In other words, HSE2 appears to stop draining the SDC-600 channel at exactly this 20-byte boundary. The host's low-level Send() routine polls this status register in a busy-wait loop with no timeout, so it blocks indefinitely at this point. This behavior is consistent regardless of what follows the 16-byte appChallengeAuth: - Whether we append additional padding bytes (to fill out the debugAuthProof union to 32 bytes) or send nothing further and go straight to FLAG_END, the FIFO stops draining at the same 20-byte point. This suggests the issue is not a packet-length/framing mismatch, but that HSE2 stops servicing the channel right after receiving the 16-byte appChallengeAuth. Question: Is this expected behavior for the APP_CHALLENGE flow (e.g., does HSE2 pause here awaiting some other action from the host before it will continue draining the channel), or does this indicate that the packet content received up to this point (debugSignalMap or appChallengeAuth) was rejected/malformed on the HSE2 side? For reference: - FSS domain (FSS_CHALLENGE) authentication with the equivalent flow completes successfully (AUTHSTATUS=0xBBB) using the same Send() routine and SDC-600 base, sending 4B signal map + 32B response with no issue. - CRS domain (APP_CHALLENGE) target = HSE_DEBUG_DOMAIN_APP (0x1B), confirmed against hse_srv_debug_auth_protocol.h. Any guidance on what HSE2 expects at this point in the APP_CHALLENGE flow would be greatly appreciated. Thanks, Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hi Chenyin, Thank you for the guidance and for reviewing the script. We'll wait for your detailed feedback on the script issues and will apply the fixes as soon as it's ready. To clarify where we currently stand relative to the two-phase approach you suggested: the hang we reported (SDC-600 TX FIFO no longer draining after debugSignalMap + appChallengeAuth) occurs right at the end of Phase 1 — specifically right after sending hseDebugAuthorizeProofProvCmd_t, before we are able to proceed to hseDebugCardCmd_t at all. So we have not yet confirmed that Phase 1 completes successfully end-to-end; the sequence currently stalls at this exact point, before Phase 2 (CardCmd) is even reached. Once we receive your feedback, we will: 1. Apply the corrections to the script. 2. Re-test following your phased approach — logging the response of each command from hseDebugCommStartCmd_t through hseDebugAuthorizeProofProvCmd_t individually, and confirming expected values at each step before proceeding further. 3. Only move on to validating hseDebugCardCmd_t once Phase 1 is confirmed to complete successfully. 4. Report back with the updated logs. Thanks again for your continued support. Best regards, Eddie Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hello, @EddiePark  Thanks for your post. 1. We have reviewed the original script shared, and found that there are some issues, I will send you the feedback soon.  During the review, we identified some issues that do not seem to align with the documented procedure. Therefore, I would recommend carefully comparing the actual packet exchange with the requirements described in the comments of HSE FW Interface. 2. Once fixed the issues found in the script, test and check the log. 3. If still issues,  I would recommend breaking the debugging procedure into two phases to help isolate the issue. As a first step, verify that the authorization sequence from hseDebugCommStartCmd_t through hseDebugAuthorizeProofProvCmd_t completes successfully. And log the response of each command and confirm that the returned values are as expected before proceeding to the next stage. In the second stage, focus on hseDebugCardCmd_t. Based on the comments provided in the HSE FW Interface documentation, I would suggest strictly validating all packets involved in this step and confirming that their contents and sequence match the documented requirements. BR Chenyin Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hello, @EddiePark  I've also sent it last week via the messages since the previous script you shared is via the private message. You may check it there in your message box. Sorry for any inconvenience. BR Chenyin Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hello Chenyin, Thank you for your previous response regarding the CRS APP domain script review. We sincerely appreciate your guidance on the two-phase debugging approach. Since we have not yet received the detailed script feedback you mentioned ("I will send you the feedback soon"), we wanted to follow up and check on the status. To prepare for your feedback, we have already: 1. Enhanced logging in our crs_auth.cmm script to support the two-phase approach you recommended: - Phase 1 (CommStart → ProofProv): Added step-by-step response logging with PASS/FAIL validation for each command (AUTH_MODE_REQ, APP_CHALLENGE, ProofProv) - Phase 2 (CardCmd): Ready to validate packet contents and sequence per HSE FW Interface documentation 2. Prepared detailed execution logs capturing: - Each command's response bytes - Lifecycle state decoding (OEM_OPEN vs OEM_CLOSED) - Authentication mode confirmation - Challenge reception validation - ProofProv response status (currently observing HSE2 remains silent after ProofProv, unlike FSS domain which returns 0x4A4A4A4A) Given that our customer (42dot) delivery schedule is approaching, could you please advise on: 1. Approximate timing for the detailed script feedback? 2. Are there any specific aspects of the packet structure or command sequence we should focus on while awaiting your feedback? We remain committed to resolving this and would greatly appreciate any additional guidance. Thank you for your continued support. Best regards, Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hi, Platform: S32N55 (HSE2), Secure Debug via SDC600 / TRACE32 CMM Domain: APP (CRS) Auth mode: Challenge (AuthMode = 0) I am implementing the debug card authentication flow. The challenge -> ProofProv phase works: after APP_CHALLENGE I receive a 32-byte challenge and compute appChallengeAuth = AES256-CMAC(key, challenge) // 16 bytes and send it in hseDebugAuthorizeProofProvCmd_t. My question is about the CARD_REQUEST phase (hseDebugCardCmd_t / hseDebugCardInfo_t). In my current script the AuthTag field is filled with the SAME value as appChallengeAuth above (i.e. the CMAC computed over the received challenge). The card authentication is rejected. I would like to confirm what the AuthTag in the card request must actually be signed over: 1. Is the card AuthTag simply the same value as appChallengeAuth (CMAC over the received challenge)? OR 2. Must the AuthTag be a separate CMAC computed over the hseDebugCardInfo_t structure (the card info being sent in the same request)? If it is (2), could you please confirm: - the exact byte range that goes into the CMAC (whole struct incl. authKeyRef/reserved, or a specific subset), - whether uidList is included when numOfAllowedUids = 0, - the authScheme value to use for AES-CMAC and whether it is part of the signed data, - packing / endianness assumptions for the serialized struct. For reference, the structure I am populating: typedef struct { uint8_t authKeyRef; uint8_t reserved0[3U]; hseOid_t ownerId; // 16 bytes hseDebugCardAuthScheme_t authScheme; uint64_t enabledDebugDomainMap; // CRS = bits 22..26 -> 0x0000000007C00000 union { hseDebugSignal_t debugDomainSignalList[HSE_MAX_NUM_OF_DEBUG_DOMAINS]; uint8_t reserved1[64U]; } debugDomainSignalList; uint8_t numOfAllowedUids; uint8_t reserved2[3U]; uint8_t uidList[HSE_MAX_UID_LIST_SIZE][HSE_UID_SIZE]; } hseDebugCardInfo_t; The HSE FW API RM does not seem to state explicitly which data the debug card AuthTag is computed over, so I would appreciate a definitive answer. Thank you. Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hello, @EddiePark  Thanks for your reply. Regarding to your previous questions: 1. Confirm whether ProofProv should be transmitted for APP domain? - Do NOT send ProofProv at all for APP (skip the tx_response call entirely)? - or Send ProofProv but don't wait for response (currently attempted)? [Comments]: The ProofProv in phase 1 must be sent for APP domain. 2. What may be causing the script stall after ProofProv? (If it is still needed) [Comments]:  After sending the ProofProv in phase 1, you should read the response from HSE FW to check if debug process  worked fine(hseDebugAuthorizeProofProvResponse_t). Please check if the response is expected.  BR Chenyin Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes Hi, Platform: S32N55 (HSE2), Secure Debug over SDC600 (APBCOM @ DP:0x5BFF8000), driven from TRACE32 CMM. I have Secure Debug authentication working for the FSS domain (AUTHSTATUS = 0xBBB). I am now bringing up the APP (CRS) domain using the exact same SDC600 base address and the same host-side SEND routine, but I hit a transmit problem. Observation: - FSS domain: I can transmit a 32-byte payload through SDC600 without any stall. - APP (CRS) domain: transmission stalls after exactly 16 bytes. My SEND routine writes each byte to the TX data register (base+0xD20) and, before each write, waits on the TX status register (base+0xD2C, lower byte) for FIFO free space: WHILE (Data.Long(&base+0xD2C) & 0x000000FF) == 0x00000000 ( ) ; wait for TX FIFO space On the APP domain, after 16 bytes this status stays 0 (no free space) indefinitely, i.e. the HSE2 side does not appear to consume the TX FIFO beyond 16 bytes. On the FSS domain the same code streams 32 bytes without stalling. Because the base address and SEND code are identical for both domains, this looks like a difference in when/whether HSE2 drains the SDC600 RX (host TX) FIFO depending on the target debug domain. Questions: 1. What determines when HSE2 begins consuming the SDC600 TX FIFO for the APP(CRS) domain? Is there a required condition/handshake (e.g. reading back the ProofProv response, a status bit, or an RX-enable) that must be satisfied before HSE2 will drain more than 16 bytes on APP? 2. Is there a per-domain difference in the SDC600 flow-control / FIFO consumption behavior between FSS and APP? 3. What is the actual SDC600 TX FIFO depth on this device, and is 0xD2C[7:0] the correct field to poll for "TX FIFO free space"? Which exact bit should be used? 4. For a payload larger than the FIFO depth on the APP domain, what is the intended host transmit sequence? Additional context that may be relevant: - After sending ProofProv (hseDebugAuthorizeProofProvCmd_t) in NOBLOCK mode, HSE2 does return a response and I can now read it back (hseDebugAuthorizeProofProvResponse_t). The 4-byte result I read is 0x7A 0xB3 0x08 0x00 - I would also appreciate confirmation of whether this indicates ProofProv success for the APP domain. Thank you.
View full article
MIMXRT1052CVL5B和MIMXRT1062CVL5B BGA196封装的是PIN TO PIN的吗? MIMXRT1052CVL5B和MIMXRT1062CVL5B BGA196封装的是PIN TO PIN的吗? 我现在用的是MIMXRT1052CVL5B,BGA196. 我可以直接不改PCB,直接把芯片换成MIMXRT1062CVL5B BGA196封装的吗? MIMXRT1052CVL5B SRAM不够用。 i.MXRT 105x i.MXRT 106x Re: MIMXRT1052CVL5B和MIMXRT1062CVL5B BGA196封装的是PIN TO PIN的吗? 你好@SDFDSFSF , 根据AN12240增强功能中的 i.MX RT1060,i.MX RT1060 将片上 SRAM 容量翻倍至 1 MB,同时保持与 i.MX RT1050 的引脚兼容性。 我建议您检查固件以及应用程序中使用的任何外围设备映射,以确保兼容性。 此致, 巴勃罗
View full article
Are the MIMXRT1052CVL5B and MIMXRT1062CVL5B BGA196 packages pin-to-pin? Are the MIMXRT1052CVL5B and MIMXRT1062CVL5B BGA196 packages pin-to-pin? I'm currently using a MIMXRT1052CVL5B with a BGA196. Can I replace the chip with a MIMXRT1062CVL5B BGA196 package without modifying the PCB? The MIMXRT1052CVL5B SRAM is insufficient. i.MXRT 105x i.MXRT 106x Re: MIMXRT1052CVL5B和MIMXRT1062CVL5B BGA196封装的是PIN TO PIN的吗? Hi @SDFDSFSF, According to AN12240 Enhanced Features in the i.MX RT1060, the i.MX RT1060 doubles the on-chip SRAM to 1 MB while maintaining pin-to-pin compatibility with the i.MX RT1050. I would recommend reviewing the firmware and any peripheral mappings used in your application to ensure compatibility. Best Regards, Pablo
View full article
S32N55 HSE2 CRS セキュアデバッグ: SDC-600 TX FIFO が 20 バイト後に停止する こんにちは、 CRSドメインのSecure Debug認証の問題についてのフォローアップ 前回の投稿(「S32N55 HSE2 CRSドメイン認証」で議論されています 「未完了」)、より具体的な新発見を報告したい 私はそれが根本原因を示していると信じています。これを別々に投稿します 提案した。 セットアップ: - S32N55、HSE2、CRSドメイン(APP_CHALLENGE)、ラウターバッハTRACE32 / SDC-600 - 認証フロー:COMM_START -> AUTH_MODE_REQ -> APP_CHALLENGE(StartCmd) -> チャレンジを受信 -> ProofProvCmd (debugSignalMap(4B) + を送信 appChallengeAuth(16B) via AES-CMAC) 調査結果: debugSignalMap(4B) + appChallengeAuth(16B) = 20バイトを送信後 ProofProvCmdパケットを介した合計、ホストのSDC-600 TX FIFOステータス レジスタ(MU ベース +0xD2C のビット [7:0])は、二度と空き領域を報告しません。 言い換えれば、HSE2はSDC-600チャネルの排水を停止しているように見えます。 まさにこの20バイトの境界線です。ホストの低レベルのSend()ルーチン このステータスレジスタはタイムアウトなしでビジーウェイトループでポーリングしますので、 この時点で無期限にブロックされています。 この動作は、16バイトの後に何が続くかに関わらず一貫しています。 appChallengeAuth: - 追加のパディングバイトを追加するかどうか( debugAuthProof を 32 バイトに結合して、またはそれ以上何も送信せずに FLAG_ENDに直接到達すると、FIFOは同じ20バイトでドレインを停止します。 ポイント。これは問題がパケット長やフレーミングではないことを示唆しています 不一致ですが、そのHSE2はすぐにチャネルのサービスを停止します 16バイトのappChallengeAuthを受け取りました。 質問: これはAPP_CHALLENGEフローに対して期待される挙動でしょうか(例:HSE2は ホストの他の動きを待つためにここで一旦一旦止めてください チャネルの排水を続けているのか、それとも この時点で受信したパケット内容(debugSignalMapまたは appChallengeAuth)がHSE2側で却下・誤った形で通知されたのでしょうか? 参考までに: - FSSドメイン(FSS_CHALLENGE)認証と同等のフロー 同じSend()を用いて(AUTHSTATUS=0xBBB)正常に完了します。 ルーチンおよびSDC-600ベースで、4B信号マップ+32B応答を送信します。 子供はない。 - CRSドメイン(APP_CHALLENGE)ターゲット = HSE_DEBUG_DOMAIN_APP(0x1B)、 hse_srv_debug_auth_protocol.h に対して確認済み。 APP_CHALLENGEのこの段階でHSE2が何を期待しているかについてのガイダンスはありますか? フローを教えていただけると大変ありがたいです。 ありがとう、 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、チェンインさん ご指導と脚本の校閲、ありがとうございました。 スクリプトの問題に関する詳細なフィードバックをお待ちしています。 修正プログラムの準備が整い次第、適用してください。 二段階アプローチに関して、我々が現在どのような立場にあるのかを明確にするために あなたが提案した: 我々が報告したハング (SDC-600 TX FIFO がもはや debugSignalMap + appChallengeAuth の後にドレインが発生すると、 フェーズ1の終了時、具体的には送信直後 hseDebugAuthorizeProofProvCmd_t に進む前に hseDebugCardCmd_t は全くありません。ですので、フェーズ1はまだ確認されていません エンドツーエンドで成功裏に完了します。現在、この数列は で停止しています。 このまさにフェーズ2(CardCmd)に到達する前の段階です。 お客様からのフィードバックを受け取り次第、以下の対応をいたします。 1. スクリプトに修正を適用する。 2. 段階的アプローチに従って再テストし、応答を記録します。 hseDebugCommStartCmd_t から各コマンドまで hseDebugAuthorizeProofProvCmd_t を個別に確認し、 次のステップに進む前に、各ステップにおける期待値を算出する。 3.フェーズ 1 が完了したら、hseDebugCardCmd_t の検証に進んでください。 正常に完了したことが確認されました。 4. 更新されたログを報告してください。 改めて、皆様のサポートに感謝します。 よろしくお願いします、 エディ Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、 @EddiePark 投稿ありがとうございます。 1. ご提供いただいた元のスクリプトを確認したところ、いくつか問題点が見つかりました。近日中にフィードバックをお送りいたします。 レビューの過程で、文書化された手順と一致しないと思われるいくつかの問題点が判明しました。したがって、実際のパケット交換とHSE FW インターフェースのコメントで説明されている要件を慎重に比較することをお勧めします。 2. スクリプトで見つかった問題を修正したら、テストを行い、ログを確認します。 3. それでも問題が解決しない場合は、デバッグ手順を2つのフェーズに分けて、問題を特定することをお勧めします。 まず最初に、hseDebugCommStartCmd_t から hseDebugAuthorizeProofProvCmd_t までの認証シーケンスが正常に完了することを確認してください。そして、各コマンドの応答をログに記録し、次の段階に進む前に、返された値が期待どおりであることを確認します。 第2段階では、hseDebugCardCmd_tに注目してください。HSE FW Interfaceドキュメントに記載されたコメントに基づき、このステップに関わるすべてのパケットを厳格に検証し、その内容と順序が文書化された要件に合致しているかを確認することをお勧めします。 BR チェイン Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、 @EddiePark 先週、メッセージ機能を使って送信しました。以前あなたが共有してくれたスクリプトはプライベートメッセージ経由だったので。メッセージボックスで確認できます。 ご迷惑をおかけして申し訳ございません。 BR チェイン Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、陳音さん、 CRS APPドメインスクリプトのレビューに関する以前のご回答、ありがとうございました。2段階デバッグ手法に関するご指導に心より感謝申し上げます。 ご指摘いただいた詳細なスクリプトに関するフィードバック(「近日中にフィードバックをお送りします」とのことでした)をまだ受け取っていないため、状況を確認するためにご連絡いたしました。 皆様からのフィードバックに備えるため、すでに以下の準備を進めております。 1. ご提案の2段階アプローチをサポートするためのcrs_auth.cmmスクリプトでの強化ログ機能: - フェーズ1(CommStart → ProofProv):各コマンド(AUTH_MODE_REQ、APP_CHALLENGE、ProofProv)に対してPASS/FAIL検証付きの段階的な応答ログを追加 - フェーズ2(CardCmd):HSE FW Interfaceドキュメントに基づくパケット内容および順序の検証準備完了 2. 詳細な実行ログの作成: - 各コマンドの応答バイト - ライフサイクル状態復号(OEM_OPEN vs OEM_CLOSED) - 認証モード確認 - チャレンジ受容の検証 - ProofProv応答状態(現在、HSE2はProofProv後に沈黙のままであり、FSSドメインは0x4A4A4A4Aを返すのとは対照的です) お客様(42dot)の配送スケジュールが近づいている中で、以下の点についてアドバイスいただけますか: 1. 詳細な脚本フィードバックのおおよその所要時間は? 2. フィードバックをお待ちいただく間、パケット構造やコマンドシーケンスに関して、特に注意すべき点はありますか? 私たちはこの問題の解決に引き続き尽力しており、さらなるご助言をいただければ大変ありがたく存じます。 引き続きご支援いただきありがとうございます。 よろしくお願いします、 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、 プラットフォーム:S32N55(HSE2)、SDC600 / TRACE32 CMMによるセキュアデバッグ ドメイン:APP(CRS) 認証モード:チャレンジ(認証モード=0) 私はデバッグカード認証フローを実装しています。チャレンジ -> ProofProv フェーズは正常に動作します: APP_CHALLENGE の後、32 バイトのチャレンジを受け取り、計算します appChallengeAuth = AES256-CMAC(key, challenge) // 16バイト そしてそれをhseDebugAuthorizeProofProvCmd_tで送信します。 私の質問は、CARD_REQUESTフェーズ(hseDebugCardCmd_t / hseDebugCardInfo_t)についてです。現在のスクリプトでは、AuthTagフィールドには上記のappChallengeAuthと同じ値(つまり、受信したチャレンジに基づいて計算されたCMAC)が入力されます。カード認証は拒否されました。 カードリクエスト内のAuthTagに実際に署名する必要があるのはどのようなものなのか確認したいです。 1. カードのAuthTagは、appChallengeAuth(受信したチャレンジに対するCMAC)と同じ値ですか? または 2. AuthTagは、hseDebugCardInfo_t構造体(同じリクエストで送信されるカード情報)に基づいて計算された、別のCMACである必要がありますか? もし(2)なら、確認していただけますか: - CMACに入力される正確なバイト範囲(全体の構造体を含む)authKeyRef/reserved、または特定のサブセット)、 - numOfAllowedUids = 0の場合にuidListが含まれているかどうか - AES-CMACで使用するauthSchemeの値と、それが署名データの一部であるかどうか、 - 直列化された構造体のパッキング/エンディアンの仮定。 参考までに、私がデータを書き込んでいる構造体は以下のとおりです。 typedef struct ヤージュ uint8_t authKeyRef; uint8_t reserved0[3U]; hseOid_t ownerId; // 16バイト hseDebugCardAuthScheme_t authScheme; uint64_t enabledDebugDomainMap; // CRS = ビット 22~26 -> 0x0000000007C00000 組合 { hseDebugSignal_t debugDomainSignalList[HSE_MAX_NUM_OF_DEBUG_DOMAINS]; uint8_t reserved1[64U]; } debugDomainSignalList; uint8_t numOfAllowedUids; uint8_t reserved2[3U]; uint8_t uidList[HSE_MAX_UID_LIST_SIZE][HSE_UID_SIZE]; } hseDebugCardInfo_t; HSE FW API RMには、デバッグカードのAuthTagがどのデータから計算されるか明示されていないようなので、明確な回答をいただけると助かります。 よろしくお願いします。 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、 プラットフォーム:S32N55(HSE2)、SDC600(APBCOM @ DP:0x5BFF8000)によるSecure Debug、TRACE32 CMMから駆動。 FSSドメインではSecure Debug認証(AUTHSTATUS = 0xBBB)が動作しています。現在、まったく同じSDC600ベースアドレスとホスト側のSENDルーチンを使用してAPP(CRS)ドメインを起動していますが、送信時に問題が発生しました。 観察: - FSSドメイン:32バイトのペイロードをSDC600経由でストールなく送信できます。 - APP (CRS) ドメイン: 送信がちょうど 16 バイト後に停止します。 私のSENDルーチンは、各バイトをTXデータレジスタ(ベース+0xD20)に書き込み、書き込みの前に、TXステータスレジスタ(ベース+0xD2C、下位バイト)でFIFOの空き領域を待機します。 WHILE (Data.Long(&base+0xD2C) & 0x000000FF) == 0x00000000 ( ) ; TX FIFO スペースが空くのを待つ APPドメインでは、16バイトを超えるとこのステータスは0(空き領域なし)のまま無期限に維持されます。つまり、HSE2側はTX FIFOを16バイトを超えて消費しないようです。FSSドメインでは、同じコードが停止することなく32バイトをストリーミングします。 ベースアドレスとSENDコードは両方のドメインで同じであるため、これはターゲットのデバッグドメインに応じて、HSE2がSDC600 RX(ホストTX)FIFOをドレインするタイミングやそのかどうかが異なることを示しているようです。 質問: 1.HSE2がAPP(CRS)ドメインのためにSDC600 TX FIFOの使用を開始するタイミングは何によって決まるのでしょうか?必須条件/握手はありますか(例:HSE2がAPP上で16バイト以上を消費する前に満たされなければならない条件(ProofProv応答の読み取り、ステータスビット、またはRX有効化)は何ですか? 2. SDC600のフロー制御/FIFO消費動作において、FSSとAPP間でドメインごとの違いはありますか? 3. このデバイスにおける実際のSDC600 TX FIFOの深さはどれくらいですか?また、0xD2C[7:0]は「TX FIFOの空き容量」をポーリングするための正しいフィールドですか?具体的にどの部分を使用すべきですか? 4. APPドメイン上のFIFO深度よりも大きいペイロードの場合、ホストの送信シーケンスはどのようになりますか? 関連するかもしれない追加の背景情報: - NOBLOCKモードでProofProv(hseDebugAuthorizeProofProvCmd_t)を送信した後、HSE2は応答を返し、それを読み返すことができる(hseDebugAuthorizeProofProvResponse_t)。私が読み取った4バイトの結果は0x7A 0xB3 0x08 0x00です。これがAPPドメインのProofProvの成功を示しているかどうかについても確認していただけると幸いです。 よろしくお願いします。 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes こんにちは、 @EddiePark ご返信ありがとうございます。 以前のご質問について: 1. ProofProvをAPPドメインに送信する必要があるかどうかを確認してください。 - APPに対してProofProvを一切送信しない(tx_response呼び出しを完全にスキップする)? - または、ProofProvを送信するが、応答を待たない(現在試行中)? [コメント]: フェーズ 1 のProofProvは APP ドメインに対して送信する必要があります。 2. ProofProv の後にスクリプトが停止する原因は何でしょうか?(もし必要であれば) [コメント]: フェーズ 1 で ProofProv を送信した後、HSE FW からの応答を読み取って、デバッグ プロセスが正常に動作したかどうかを確認する必要があります (hseDebugAuthorizeProofProvResponse_t)。その応答が想定どおりのものかどうか確認してください。 BR チェイン
View full article
MIMXRT1052CVL5BとMIMXRT1062CVL5BのBGA196パッケージは、ピン接続が一致していますか? MIMXRT1052CVL5BとMIMXRT1062CVL5BのBGA196パッケージは、ピン接続が一致していますか? 現在、BGA196パッケージのMIMXRT1052CVL5Bを使用しています。 基板を改造せずに、チップをMIMXRT1062CVL5B BGA196パッケージのものに交換することはできますか? MIMXRT1052CVL5B SRAMは容量不足です。 i.MXRT 105x i.MXRT 106x Re: MIMXRT1052CVL5B和MIMXRT1062CVL5B BGA196封装的是PIN TO PIN的吗? こんにちは@SDFDSFSF。 i.MX RT1060の AN12240 Enhanced Features によると、i.MX RT1060はオンチップSRAMを1 MBに倍増させつつ、i.MX RT1050とのピン間互換性を維持しています。 互換性を確認するために、ファームウェアやアプリケーションで使われているペリフェラルのマッピングを確認することをお勧めします。 よろしくお願いします、 パブロ
View full article
FRDM-IMX95:从 SD 卡启动时无串口输出(预装 eMMC 启动完全正常) NXP社区的各位朋友,大家好! 我拥有机械和电气工程背景,这是我第一次深入研究复杂的片上系统 (SoC) 和嵌入式操作系统。 我的项目使用的是 FRDM-IMX95 开发板。我的最终目标是使用 IPC(进程间通信)框架并行运行两个操作系统。 主板到货时,其内部 eMMC 上预装了 Linux 镜像。它开箱即用,完美运行,我的终端监测程序中可以获取完整的串行输出日志。 现在,我正在尝试按照官方入门指南,使用 Windows 主机上的 UUU(通用更新实用程序)将标准 Linux 电路板支持包映像刷写到 microSD 卡上。 根据 Windows 命令提示符显示,UUU 刷新过程以“成功”状态完成。我使用了以下标准命令布局: “.\uuu.exe -b sd_all imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all imx-image-full-imx95evk.wic” 问题:成功刷写固件后,我关闭电路板,并将物理启动开关配置为 SD 启动模式,方法是将 SW1 [1:2] 设置为 11(ON / ON)。当我重新启动电路板时,串口监视器完全空白。完全没有任何文本输出或硬件初始化信息可见。 1. 我是否对这里的启动链的工作原理存在根本性的误解?根据i.MX Linux 用户指南,.wic镜像包含所有四个基本部分,包括引导加载程序镜像(U-Boot)。既然基本的硬件配置块应该从卡上读取,那么我的串口监视器上至少应该能看到初始的 U-Boot SPL 序列吧? 任何关于此特定 FRDM 变体的见解、初学者常犯的错误或隐藏的开关要求都将不胜感激! 顺祝商祺! FRDM 培训 Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly 你好, 我这边正在进行测试,稍后会把具体步骤分享给你,稍后会更新。 Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly 感谢您调查并进行了测试!感谢您的帮助,期待您的最新消息。 Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly 你遇到这个问题是因为你试图使用 uuu 工具将固件刷入 SD 卡,而 uuu 工具是用来刷写 eMMC 的。如果你想将固件刷写到 SD 卡上,你需要在 Linux 主机上执行以下命令。 $ sudo dd if= .wicof=/dev/sdx bs=1M && 同步 要确定分配给SD/MMC卡的设备节点,执行以下命令: $ cat /proc/partitions 主次 #块名称 8 0 78125000 sda 8 1 75095811 sda1 8 2 1 sda2 8 5 3028221 sda5 8 32 488386584 sdc 8 33 488386552 sdc1 8 16 3921920 sdb 8 18 3905535 sdb1
View full article
S32K312:WKUP中断未触发 DiaDev_0-1783418064066.png DiaDev_1-1783418072029.png DiaDev_2-1783418089747.png 我已将PTB2配置为WKUP输入引脚,并将WKUP 通道 8映射到 PTB2。WKUP 模块配置看起来正确;但是,WKUP 中断没有被触发。 之前,我将同一引脚配置为EIRQ输入,并且中断已成功触发,证实该引脚和外部信号功能正常。 问题: PTB2 配置为 WKUP 输入。 WKUP 8频道映射到PTB2。 未收到 WKUP 中断。 同样的硬件配置在 EIRQ 配置下可以正常工作。 请帮忙确定是否存在任何额外的 WKUP 配置要求、依赖项或已知限制,这些都可能导致无法生成中断。 Wkpu_Ip_Init(0U, &Wkpu_Ip_Config_PB); /* INT2:唤醒触发器。*/ Wkpu_Ip_EnableInterrupt(0, Wkpu_Ip_ChannelConfig_PB[2U].hwChannel); Wkpu_Ip_EnableNotification(Wkpu_Ip_ChannelConfig_PB[2U].hwChannel); Re: S32K312: WKUP Interrupt Not Triggering 嗨@DiaDev , S32K3 除了提供约 60 个外部唤醒源外,还提供了 4 个内部唤醒源,在配置通道时必须考虑这些内部唤醒源;这意味着,偏移量需增加 4: Julin_AragnM_0-1783443817593.png PTB2 是唤醒垫 [8],加上四个内部源,它将是通道 12。请更改此配置并测试 WKPU 是否被触发。 此致, 朱利安
View full article
S32N55 HSE2 CRS 安全调试:SDC-600 TX FIFO 在传输 20 字节后停止 你好, 关于 CRS 功能域安全调试身份验证问题的后续讨论 之前的帖子中讨论过(“S32N55 HSE2 CRS 功能域身份验证”) “尚未完成”,我想报告一项新的、更具体的发现。 我认为这指出了问题的根源。单独发布此内容 建议。 设置: - S32N55、HSE2、CRS 功能域 (APP_CHALLENGE)、劳特巴赫 TRACE32 / SDC-600 - 认证流程:COMM_START -> AUTH_MODE_REQ -> APP_CHALLENGE (StartCmd) -> 接收挑战 -> 发送 ProofProvCmd (debugSignalMap(4B) + appChallengeAuth(16B) 通过 AES-CMAC) 发现: 发送 debugSignalMap(4B) + appChallengeAuth(16B) = 20 字节后 通过 ProofProvCmd 数据包获取主机 SDC-600 TX FIFO 状态的总数 寄存器(MU 基址 + 0xD2C 处的 bit[7:0])不再报告可用空间。 换句话说,HSE2 似乎停止消耗 SDC-600 通道的电量。 正好是这 20 字节的边界。主机的底层 Send() 例程 它在一个没有超时的忙等待循环中轮询此状态寄存器,因此 此处无限期封锁。 无论 16 字节之后是什么,这种行为都保持一致。 appChallengeAuth: - 是否添加额外的填充字节(以填充) debugAuthProof 联合体(转换为 32 字节)或者不再发送任何内容并继续 直接跳转到 FLAG_END,FIFO 停止在相同的 20 字节处进行数据清空。 观点。这表明问题不在于数据包长度/帧结构。 不匹配,但 HSE2 在以下情况下立即停止为该通道提供服务: 收到 16 字节的 appChallengeAuth。 问题: 这是 APP_CHALLENGE 流程的预期行为吗(例如,HSE2 是否如此) 在此处暂停,等待主机执行其他操作,然后才会继续。 继续排干河道),还是说这表明 到目前为止接收到的数据包内容(debugSignalMap 或 appChallengeAuth)在 HSE2 端被拒绝/格式错误? 供参考: - FSS 功能域 (FSS_CHALLENGE) 身份验证具有等效流程 使用相同的 Send() 函数成功完成(AUTHSTATUS=0xBBB)。 例行程序和 SDC-600 基座,发送 4B 信号映射 + 32B 响应 没问题。 - CRS 功能域 (APP_CHALLENGE) 目标 = HSE_DEBUG_DOMAIN_APP (0x1B), 已根据 hse_srv_debug_auth_protocol.h 进行确认。 能否提供一些关于 HSE2 在 APP_CHALLENGE 阶段的期望方面的指导? 非常感谢您的反馈。 谢谢, Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 陈银你好, 感谢您的指导和对剧本的审阅。 我们将等待您就剧本问题提供的详细反馈,并会 一旦修复程序准备就绪,请立即应用。 为了阐明我们目前相对于两阶段方法的立场。 您建议:我们报告的挂起问题(SDC-600 TX FIFO 不再存在) debugSignalMap + appChallengeAuth) 之后的排水操作恰好发生在 第一阶段结束——具体来说,就是在发送之后。 在能够继续之前,我们需要 hseDebugAuthorizeProofProvCmd_t hseDebugCardCmd_t 完全不存在。因此,我们尚未确认第一阶段。 端到端执行成功;序列目前停滞在 正是这一点,甚至在达到第二阶段(CardCmd)之前。 收到您的反馈后,我们将: 1. 将修改后的剧本应用到剧本中。 2. 按照分阶段的方法进行重新测试——记录响应 从 hseDebugCommStartCmd_t 到每个命令 单独检查 hseDebugAuthorizeProofProvCmd_t,并确认 在继续进行下一步之前,需要计算每一步的预期值。 3.只有在第一阶段完成后才能继续验证 hseDebugCardCmd_t。 已确认完成。 4. 请汇报更新后的日志。 再次感谢您一直以来的支持。 此致, 埃迪 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 你好, @EddiePark 感谢你的帖子。 1. 我们已经审阅了您分享的原始剧本,发现存在一些问题,我会尽快将反馈意见发送给您。 在审查过程中,我们发现了一些问题,这些问题似乎与已记录的程序不符。因此,我建议仔细比较实际数据包交换与 HSE FW 接口注释中描述的要求。 2. 修复脚本中发现的问题后,进行测试并检查日志。 3. 如果问题仍然存在,我建议将调试过程分为两个阶段,以帮助隔离问题。 首先,验证从 hseDebugCommStartCmd_t 到 hseDebugAuthorizeProofProvCmd_t 的授权序列是否成功完成。记录每个命令的响应,并在进行下一阶段之前确认返回值是否符合预期。 第二阶段,重点关注 hseDebugCardCmd_t。根据 HSE FW 接口文档中提供的评论,我建议严格验证此步骤中涉及的所有数据包,并确认其内容和顺序与文档中规定的要求相符。 BR 陈银 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 你好, @EddiePark 上周我也通过消息发送了它,因为你之前分享的剧本是通过私信发送的。您可以在消息框中查看。 给您带来的不便,敬请谅解。 BR 陈银 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 陈音你好 感谢您之前对 CRS APP 功能域脚本审查的回复。我们衷心感谢您对两阶段调试方法的指导。 由于我们尚未收到您提到的详细剧本反馈(“我会尽快把反馈发给您”),因此我们想跟进并确认一下进度。 为了准备接收您的反馈,我们已经: 1. 我们增强了 crs_auth.cmm 脚本中的日志记录功能,以支持您建议的两阶段方法: - 第一阶段(CommStart → ProofProv):添加了逐步响应日志记录,并对每个命令(AUTH_MODE_REQ、APP_CHALLENGE、ProofProv)进行 PASS/FAIL 验证。 - 第二阶段(CardCmd):准备根据 HSE FW 接口文档验证数据包内容和顺序 2. 准备详细的执行日志,捕获以下内容: - 每个命令的响应字节 - 生命周期状态解码(OEM_OPEN 与 OEM_CLOSED) - 身份验证模式确认 - 挑战接收验证 - ProofProv 响应状态(目前观察到 HSE2 在 ProofProv 后保持静默,这与返回 0x4A4A4A4A 的 FSS 功能域不同) 鉴于我方客户(42dot)的交货日期临近,请问您能否就以下方面提供建议: 1. 详细剧本反馈的大概时间是什么时候? 2. 在等待您的反馈期间,我们应该重点关注数据包结构或命令序列的哪些具体方面? 我们仍致力于解决此事,并非常感谢任何进一步的指导。 感谢您一直以来的支持。 此致, Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 你好, @EddiePark 感谢您的回复。 关于您之前的问题: 1. 确认是否需要为APP功能域传输ProofProv? - 完全不要为 APP 发送 ProofProv(完全跳过 tx_response 调用)? - 或者发送证明文件但不等待回复(目前尝试过)? [备注]:第一阶段的ProofProv必须针对 APP 功能域发送。 2. ProofProv 之后脚本卡住的原因可能是什么?(如果仍然需要的话) [注释]: 在第 1 阶段发送 ProofProv 后,您应该读取 HSE FW 的响应,以检查调试过程是否正常工作(hseDebugAuthorizeProofProvResponse_t)。请确认该回复是否在预期之内。 BR 陈银 Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 您好, 平台:S32N55 (HSE2),通过 SDC600 / TRACE32 CMM 进行安全调试 功能域:APP(CRS) 认证模式:质询(AuthMode = 0) 我正在实现调试卡认证流程。挑战 -> 证明阶段正常工作:在 APP_CHALLENGE 之后,我收到一个 32 字节的挑战并进行计算。 appChallengeAuth = AES256-CMAC(key, challenge) // 16 字节 并将其发送到 hseDebugAuthorizeProofProvCmd_t。 我的问题与 CARD_REQUEST 阶段(hseDebugCardCmd_t / hseDebugCardInfo_t)有关。在我当前的脚本中,AuthTag 字段填充了与上面的 appChallengeAuth 相同的值(即根据接收到的挑战计算出的 CMAC)。信用卡验证失败。 我想确认一下信用卡请求中的 AuthTag 究竟需要签署的是什么: 1. 卡片 AuthTag 是否与 appChallengeAuth(对接收到的质询进行 CMAC 验证)的值相同? 或者 2. AuthTag 是否必须是基于 hseDebugCardInfo_t 结构(在同一请求中发送的卡信息)计算的单独 CMAC? 如果是(2),请您确认一下: - 进入 CMAC 的确切字节范围(包括整个结构体)。authKeyRef/保留密钥,或特定子集), - 当 numOfAllowedUids = 0 时,是否包含 uidList, - 用于 AES-CMAC 的 authScheme 值,以及它是否是签名数据的一部分, - 序列化结构的打包/字节序假设。 作为参考,我正在填充的结构如下: typedef struct { uint8_t authKeyRef; uint8_t reserved0[3U]; hseOid_t ownerId; // 16 字节 hseDebugCardAuthScheme_t authScheme; uint64_t enabledDebugDomainMap; // CRS = 位 22..26 -> 0x0000000007C00000 联盟 { hseDebugSignal_t debugDomainSignalList[HSE_MAX_NUM_OF_DEBUG_DOMAINS]; uint8_t reserved1[64U]; } debugDomainSignalList; uint8_t numOfAllowedUids; uint8_t reserved2[3U]; uint8_t uidList[HSE_MAX_UID_LIST_SIZE][HSE_UID_SIZE]; } hseDebugCardInfo_t; HSE FW API RM 似乎没有明确说明调试卡 AuthTag 是基于哪些数据计算的,所以我希望得到一个明确的答案。 谢谢! Re: S32N55 HSE2 CRS Secure Debug: SDC-600 TX FIFO stalls after 20 bytes 您好, 平台:S32N55 (HSE2),通过 SDC600 进行安全调试 (APBCOM @ DP:0x5BFF8000),由 TRACE32 CMM 驱动。 我已经为 FSS 功能域启用了安全调试身份验证(AUTHSTATUS = 0xBBB)。我现在使用完全相同的 SDC600 基本地址和相同的主机端 SEND 例程来启动 APP (CRS) 功能域,但我遇到了传输问题。 观察: - FSS 功能域:我可以通过 SDC600 传输 32 字节的有效载荷而不会出现任何停顿。 - APP(CRS)功能域:传输在正好 16 个字节后停止。 我的 SEND 例程将每个字节写入 TX 数据寄存器(基址+0xD20),并且在每次写入之前,都会等待 TX 状态寄存器(基址+0xD2C,低字节)的 FIFO 空闲空间: WHILE (Data.Long(&base+0xD2C) & 0x000000FF) == 0x00000000 ();等待 TX FIFO 空间 在 APP 功能域中,16 字节后,此状态将无限期地保持为 0(没有可用空间),即 HSE2 端似乎不会在 16 字节之后继续使用 TX FIFO。在 FSS 域上,相同的代码可以无停顿地传输 32 字节。 由于两个功能域的基本地址和 SEND 代码相同,因此这看起来像是 HSE2 何时/是否根据目标调试功能域清空 SDC600 RX(主机 TX)FIFO 存在差异。 问题: 1.什么因素决定了 HSE2 何时开始使用 APP(CRS) 功能域 的 SDC600 TX FIFO?是否存在必要的条件/握手(例如)读取 ProofProv 响应、状态位或 RX 使能)必须满足哪些条件,HSE2 才能在 APP 上消耗超过 16 字节? 2. FSS 和 APP 之间 SDC600 流控制/FIFO 消耗行为是否存在功能域差异? 3. 此设备上的 SDC600 TX FIFO 实际深度是多少?0xD2C[7:0] 是否是轮询“TX FIFO 空闲空间”的正确字段?应该使用哪一位? 4. 对于大于 APP 功能域 FIFO 深度的有效载荷,预期的主机发送序列是什么? 其他可能相关的背景信息: - 在 NOBLOCK 模式下发送 ProofProv (hseDebugAuthorizeProofProvCmd_t) 后,HSE2 确实返回了一个响应,我现在可以将其读取回来 (hseDebugAuthorizeProofProvResponse_t)。我读取到的 4 字节结果是 0x7A 0xB3 0x08 0x00 - 我也希望确认这是否表示 APP 功能域的 ProofProv 成功。 谢谢!
View full article
FRDM-IMX95: SDカードから起動するとシリアル出力がない (プリインストールされたeMMCブートは正常に動作します) こんにちは、NXPコミュニティの皆さん、 私は機械工学と電気工学のバックグラウンドを持っていますが、複雑なシステムオンチップ(SoC)や組み込みオペレーティングシステムに深く取り組むのは今回が初めてです。 私のプロジェクトではFRDM-IMX95の開発ボードを使用しています。私の最終目標は、IPC(プロセス間通信)フレームワークを使用して、2つのオペレーティングシステムを並行して実行することです。 ボードは内部eMMCにプリインストールされたLinuxイメージを同梱していました。これは箱から出してすぐに完璧に動作し、ターミナルモニタープログラムでシリアル出力ログを完全に取得できます。 現在、公式の Starting Guide に従って、Windowsホストマシン上でUUU(Universal Update Utility)を使って標準のLinux BSPイメージをmicroSDカードにフラッシュしようとしています。 Windowsのコマンドプロンプトによると、UUUのフラッシュ処理は「SUCCESS」ステータスで完了します。私は以下の標準コマンドレイアウトを使用しました: ".\uuu.exe -b sd_all imx-boot-imx95-15x15-lpddr4x-frdm-sd.bin-flash_all imx-image-full-imx95evk.wic" 問題点:フラッシュに成功した後、ボードを電源を切り、物理的なブートスイッチをSDブートモードに設定し、SW1 [1:2]を11(オン/オン)に設定します。ボードの電源を入れ直しても、シリアルモニターは完全に空白のままです。テキスト出力やハードウェアの初期化は一切表示されません。 1. ブートチェーンの仕組みについて、私は根本的な誤解をしているのでしょうか?i.MX Linux ユーザーガイドによると、.wicはこのイメージには、ブートローダーイメージ(U-Boot)を含む、4つの必須要素すべてが含まれています。基本的なハードウェア構成ブロックはカードから読み込まれるはずなので、少なくとも最初のU-Boot SPLシーケンスがシリアルモニターに表示されるべきではないでしょうか? この特定のFRDMバリアントで初心者がよく注意する落とし穴、あるいは隠れたスイッチの要件について、何かアドバイスがあればぜひ教えてください! よろしくお願いいたします。 FRDMトレーニング Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly こんにちは、 現在、こちらでテストを行い、正確な手順をお伝えします。近日中に更新いたします。 Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly 調査していただき、またそちらでテストしていただき、ありがとうございます!ご協力ありがとうございます。今後のご報告をお待ちしております。 Re: FRDM-IMX95: No Serial Output when Booting from SD Card (Pre-installed eMMC Boot Works Perfectly 問題は、uuuツールでSDカードにフラッシュしようとしているからです。emmCはemmcをフラッシュするために作られています。SDカードをフラッシュしたい場合は、Linuxホストマシンで以下のコマンドを実行する必要があります。 $ sudo dd if= .wicof=/dev/sdx bs=1M && sync SD/MMCカードに割り当てられたデバイスノードを確認するには次のコマンドを実行します。 $ cat /proc/partitions メジャーマイナー #ブロック名 8 0 78125000 sda 8 1 75095811 sda1 8 2 1 sda2 8 5 3028221 sda5 8 32 488386584 sdc 8 33 488386552 sdc1 8 16 3921920 sdb 8 18 3905535 sdb1
View full article
CLI/ヘッドレス こんにちは!GUI Guider 2.0.0には、プロジェクトのCIビルドを自動化するためのCLI/ヘッドレスビルド機能はありますか?生成されたCファイルを自分のリポジトリで追跡したくはありません。 Re: CLI/Headless 私も知りたいです。 Re: CLI/Headless こんにちは、@nbarrett さん、 @znickerson さん、 GUI Guiderは、CIパイプラインから呼び出せるCLIやヘッドレスコード生成をネイティブにサポートしていません。 とはいえ、GUI Guider 2.0.0はCMakeとNinjaを利用して、GUI Guiderプロジェクトから生成されたコードをビルドおよびコンパイルし、フラッシュ可能な.binファイルを作成します。または.elfイメージを使えば、これらのツールを使ったスクリプトを作成すれば、このプロセスを自動化できるはずです。現時点では、これがどのように行われるのかのガイドやスクリプトの例はありませんが、GUI Guiderツールのビルド&コンパイルログを参照すると、GUI Guider 2.0.0がARMGCCベースのプロジェクトでどのように処理しているかを詳しく確認できます。 BR、 エドウィン。
View full article
S32K312: WKUP割り込みがトリガーされない DiaDev_0-1783418064066.png DiaDev_1-1783418072029.png DiaDev_2-1783418089747.png I have configured PTB2 as the WKUP input pin, and WKUP チャネル 8 はPTB2にマッピングされます。WKUPのモジュール構成は正しいようです。しかし、WKUPの割り込みはトリガーされていません。 以前、同じピンをEIRQ入力として設定したところ、割り込みが正常にトリガーされたため、ピンと外部信号が正しく機能していることが確認できました。 問題: PTB2はWKUPの入力として設定されています。 WKUPチャネル8はPTB2に割り当てられていました。 WKUP割り込みは受信されませんでした。 同じハードウェア構成で、EIRQ構成でも正しく動作します。 割り込みが生成されないようにする追加のWKUP設定要件、依存関係、または既知の制限があるかどうか、ご協力ください。 Wkpu_Ip_Init(0U, &Wkpu_Ip_Config_PB); /* INT2: ウェイクアップトリガー。*/ Wkpu_Ip_EnableInterrupt(0, Wkpu_Ip_ChannelConfig_PB[2U].hwChannel); Wkpu_Ip_EnableNotification(Wkpu_Ip_ChannelConfig_PB[2U].hwChannel); Re: S32K312: WKUP Interrupt Not Triggering こんにちは、 @DiaDev さん。 S32K3は~60の外部ウェイクアップに加え、4つの内部ウェイクアップソースも提供しており、チャネル設定時にこれらを考慮しなければなりません。これは、+4をオフセットとして加えることを意味します: Julin_AragnM_0-1783443817593.png PTB2はウェイクアップパッド[8]で、4つの内部ソースがチャネル 12となります。 この設定を変更して、WKPUがトリガーされるかどうかテストしてください。 よろしくお願いします、 ジュリアン
View full article
CLI/Headless Hello! Does GUI Guider 2.0.0 have any CLI / Headless build features for automating some CI builds of my project? I'd rather not track generated c files in my repo. Re: CLI/Headless I would also like to know this please. Re: CLI/Headless Hi @nbarrett , @znickerson , GUI Guider does not natively support CLI or headless code generation that you could invoke from a CI pipeline. That said, GUI Guider 2.0.0 leverages CMake and Ninja to build and compile the code generated from the GUI Guider project into a flashable .bin or .elf image, so automating this process should be achievable by creating a script that uses these tools. We don't currently have any documented guide or script example of how this would be done, but you can reference the build and compile log from the GUI Guider tool to see in detail the process that GUI Guider 2.0.0 does on an ARMGCC based project. BR, Edwin.
View full article
CLI/无头模式 您好!GUI Guider 2.0.0 是否有任何 CLI / 无头构建功能,可以用于自动化我项目中的一些 CI 版本?我不想在我的代码仓库中跟踪生成的 C 文件。 Re: CLI/Headless 我也想知道这一点。 Re: CLI/Headless 嗨@nbarrett , @znickerson , GUI Guider 本身并不支持 CLI 或无头代码生成,因此无法从 CI 管道中调用这些代码。 也就是说,GUI Guider 2.0.0 利用 CMake 和 Ninja 将 GUI Guider 项目生成的代码构建并编译成可刷写的 .bin 文件。或 .elf因此,通过创建使用这些工具的脚本,应该可以实现此过程的自动化。我们目前没有任何关于如何完成此操作的文档指南或脚本示例,但您可以参考 GUI Guider 工具的构建和编译日志,详细了解 GUI Guider 2.0.0 在基于 ARMGCC 的项目上执行的过程。 BR, 埃德温。
View full article