2391703_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2391703_en-US

2391703_en-US

Are the MIMXRT1052CVL5B and MIMXRT1062CVL5B BGA196 packages pin-to-pin?

Are the MIMXRT1052CVL5B and MIMXRT1062CVL5B BGA196 packages pin-to-pin?

I'm currently using a MIMXRT1052CVL5B with a BGA196.

Can I replace the chip with a MIMXRT1062CVL5B BGA196 package without modifying the PCB?

The MIMXRT1052CVL5B SRAM is insufficient.

i.MXRT 105xi.MXRT 106xRe: MIMXRT1052CVL5B和MIMXRT1062CVL5B BGA196封装的是PIN TO PIN的吗?

Hi @SDFDSFSF,

According to AN12240 Enhanced Features in the i.MX RT1060, the i.MX RT1060 doubles the on-chip SRAM to 1 MB while maintaining pin-to-pin compatibility with the i.MX RT1050.

I would recommend reviewing the firmware and any peripheral mappings used in your application to ensure compatibility.

Best Regards,
Pablo

Tags (1)
No ratings
Version history
Last update:
‎07-08-2026 02:36 AM
Updated by: