Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32K388 power supplies Hello S32K388, I am using the S32K388 for one of my applications. The V11 is meant to be supplied by a last mile regulator NMOS from V15. However I would like to supply this 1.5V from a external DC/DC converter. Is that feasible? Best regards, Jules Re: S32K388 power supplies Hello @JulesW , Based on the S32K388 power architecture, V11 must be generated using the external NMOS last-mile regulator from the V15 rail, as described in the Hardware Design Guidelines. However, if your question is whether the 1.5 V V15 rail itself can be supplied from an external DC/DC converter, then this is feasible. This is also the approach used on the S32K388 EVB, where one jumper option is that the 1.5 V rail is generated externally by the PMIC. Best regards, Pavel
記事全体を表示
OV5640 Interfacing with i.MX RT1170 (Without Display) Image Capture and Streaming to Desktop Hello, I am using the i.MX RT1170-EVKB board, and my goal is to capture images from the OV5640 camera and view either the captured image or a live video stream on my desktop PC without using an LCD display. I have tried the MIPI CSI SDK examples and was able to capture image data in RAW format. However, I am facing several issues. The captured output is in RAW format, and I could not find any documentation explaining how to properly convert or view these images. The captured images appear to have incorrect colors or filter-like artifacts, making it difficult to verify whether the camera output is correct. I could not find any official documentation, application notes, or video tutorials describing the complete workflow for capturing images from the OV5640 and viewing them on a desktop PC. There is no clear reference explaining how to stream the camera output over Ethernet or USB without using the onboard display. I also tried the sd_jpeg example, but I encountered multiple problems. During integration, the project reported missing JPEG library configuration files such as jconfig.h. After resolving some build issues, I continued to encounter compilation and integration errors while combining the JPEG encoder with the MIPI CSI camera example. I was unable to generate a valid JPEG image from the captured camera frame. My objective is to: Interface the OV5640 camera with the i.MX RT1170-EVKB board without using an LCD display. Capture images and transfer them to my desktop PC for viewing. Stream live video from the camera to my desktop PC over Ethernet, if supported. I would appreciate your guidance on the following questions: Is there an official SDK example or reference project for this use case? Is there any documentation explaining the complete image capture pipeline from the OV5640 through MIPI CSI, memory, JPEG or RAW processing, and Ethernet or USB transfer to a desktop PC? Is live streaming over Ethernet supported on the RT1170-EVKB? If yes, could you recommend the appropriate SDK example or middleware? Are there any known issues with the sd jpeg example or any additional configuration steps required to integrate it with the MIPI CSI camera examples? Any guidance, documentation, or reference projects would be greatly appreciated. Thank you for your support. Re: OV5640 Interfacing with i.MX RT1170 (Without Display) Image Capture and Streaming to Desktop HI @Sureshk123, We don't have an official example project or reference design for your application. That said, from my understanding, I would recommend you tackle the complete application as follows: Camera capture path (OV5640 > MIPI CSI > cameraBuffer) This part we do have an example application, which are the aforementioned MIPI CSI SDK examples. Keep in mind that, as per ERR051248: "Video Mux Controller (VIDEO_MUX), raw data and YUV422 (10 bit) formats to the MIPI_CSI2 block are not supported." Using the parallel CSI is an optional workaround, either that or a video decoder. Once you have the adequate data on your cameraBuffer, you can integrate example projects from our SDK based on USB or lwIP to transport this data to your PC. I would recommend looking into JPEG encoding only after the buffer is known to work. BR, Edwin.
記事全体を表示
SE050E2HQ1/Z01Z3Zに必要な熱データ こんにちは、チームの皆さん、 部品番号の熱抵抗データと動作接合部温度情報を探しています。 SE050E2HQ1/Z01Z3Z ありがとうございます。 ひどい スマート・カード Re: Thermal Data required for SE050E2HQ1/Z01Z3Z こんにちは、 @Harsh_Bhavsar さん。 詳細については、 https://www.nxp.com/docs/en/data-sheet/SE051.pdfをご参照ください。それらはほとんど同じです。 心から、 カン Re: Thermal Data required for SE050E2HQ1/Z01Z3Z こんにちは、Kan_Liさん。 ご回答ありがとうございます。データシートは大変参考になりました。 同じ接合部の最大許容温度を教えてもらえますか?それとも動作温度を考慮してもいいですか? ありがとうございます。 ひどい Re: Thermal Data required for SE050E2HQ1/Z01Z3Z こんにちは、kanさん、 それは本当に役立つ情報です。 ありがとうございます。 ひどい Re: Thermal Data required for SE050E2HQ1/Z01Z3Z こんにちは、 @Harsh_Bhavsar さん。 動作時の最大接合温度は動作時よりわずかに高く、内部温度センサーは 約110°C で作動し始めます。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
記事全体を表示
MCUX 11.0.1 - 调试器显示“中断失败”对话框 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我目前在使用 RT1050 时遇到一个问题,我尝试在某个 FreeRTOS 任务中设置断点,但是当到达断点时,调试器无法自行暂停,而是在我之后尝试手动暂停调试器时弹出一个对话框,提示“中断失败”。 我的应用程序启动正常。如果我手动暂停程序,就能获得有效的调试器上下文: 这正是我想要执行的任务,所以我在消息队列接收调用返回后的 switch() 语句处设置了一个断点。我在 NetIfInit() 方法中也设置了第二个断点,就在下面;我希望调试器能够命中这两个断点,或者至少命中其中一个。 我还在测试函数中设置了一个断点,该断点将启动消息队列发送。当我按下串口控制台上的按键时,调试器会到达该断点并停止运行。 然后我进入 NetInit() 函数,该函数最终会调用 xQueueSend(),经过一段漫长的停顿后,调试器会进入该函数。然后我逐步执行 xQueueGenericSend() 函数体,直到执行到这里: 当我尝试单步执行第 846 行时,调试器会暂停一段时间,然后失去上下文。请注意,我的“全部恢复”、“全部暂停”、“全部终止”按钮以及左侧的线程列表都消失了。本次会话仅提供“暂停”和“终止”按钮。如果我点击“暂停”,IDE 会停顿几秒钟,然后弹出以下对话框: 就这样,调试器的工作结束了。与此同时,我的串口控制台卡住了,只显示了一些未写入的 UART 输出。你可能会想,糟了,我把钱都花光了,目标肯定完蛋了……不,并非如此。剩下的唯一按钮是红色的“终止(停止)”按钮,如果我点击它,调试会话就会终止,执行就会恢复……我的任务一切正常。 Initialize eth0. #DA4 12.996 | eth: netif init #DA4 12.999 | eth: NV MAC = 00-07-F0-00-56-03 #DA4 12.999 | eth: NV cfg: address = 192.168.1.180, netmask = 255.255.252.0, gateway = 192.168.1.1, static #DA4 13.000 | eth: netif add: MAC 00-07-F0-00-56-03, PHY address 3 Returning to main menu. #BB4 17.572 | No Handle Base Curr HiWByte State Name #BB4 17.575 | 10 80010db8 19 19 824 Blocked Tmr Svc #BB4 17.575 | 05 20206b68 12 12 1396 Suspended led_act #BB4 17.576 | 04 20206500 12 12 1388 Blocked led_cpu #BB4 17.576 | 08 2020ba18 8 8 7216 Blocked tcpip_thread #BB4 17.576 | 07 20209868 7 7 6900 Blocked eth_mgr #BB4 17.577 | 06 20207818 4 4 1912 Blocked gui #BB4 17.577 | 01 20203538 3 3 2812 Suspended debug_mgr #BB4 17.577 | 02 20204a68 2 2 4248 Running test #BB4 17.577 | 03 20205e88 1 1 3948 Blocked backgrnd #BB4 17.579 | 09 80010d40 0 0 748 Ready IDLE‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 看来程序确实在我设置的断点处停止了,只是调试器出了问题。 有人知道为什么调试器会突然失灵吗? (编辑:已添加控制台输出附件,以防有用。) 大卫·罗杰斯 Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog 我遇到过类似的情况,调试器在 main() 处没有停止,也无法暂停,而是显示“中断失败”。我通过替换工作区目录“.mcuxpressoide_packages_support”解决了我的问题。和“.metadata”我用的是备份文件。 或许可以从另一台电脑的安装系统中获取这些目录。 或许重新导入项目也能解决问题。 Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog 我还想知道这个问题最终是否得到了解决。我遇到了完全相同的问题——我使用的是 MCUXpresso (v11.4),我的 FreeRTOS 应用程序可以正常运行数小时。我可以手动暂停调试器并单步执行代码。但是,我的程序最终会崩溃,调试器(通过 Segger JLink)只会报告“中断失败”——我失去了所有调试功能。 Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog 大家好, 我们目前也遇到了同样的问题。 我们想调试一个问题,但是 J-Link 调试器在命中断点后显示“中断失败”。 既然这个帖子最后只提到了寻求支持,那么问题是否已经解决了呢? 此致 大卫 Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,埃里希, 等等……你们还在用票务系统?我以为恩智浦半导体几年前就关闭了这条支持渠道,当时他们告诉大家去论坛寻求帮助。(当时我并不太高兴,因为我认为这是客户服务水平的下降,即“不要来找我们,去向公众寻求帮助”。)不过,恩智浦的工程师们似乎很积极地参与论坛讨论,而且通常来说,获得第三方意见是很有帮助的。) 请问是否有提交支持工单的快捷链接?如果我这周能抽出点时间(哈哈),我会看看能不能把我的项目整理成一个版本,至少在 EVKB 上能正常运行,并且仍然能重现断点失败的问题。谢谢。 大卫·R. Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,大卫, 您可以通过提交常规支持工单的方式来提交您的项目。我认为如果能在 EVK 上运行,对 IDE 工程师来说只有好处,因为他们有这种硬件可用,而且项目越小越好。 感谢您的帮助! 埃里希 Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我目前还有很多其他事情要处理,但我会在接下来的几天里尽量给你提供一些额外的信息。你说得对,我肯定不会把我的项目发布到论坛上,但如果你有一个秘密渠道,让我可以直接把我的项目发送给你或者恩智浦的工程师,那我就没问题了。是的,就目前项目的形式而言,它是 100% 可复现的。所以,如果可以的话,请私下把我的项目发给你,这样我就可以尝试做一个修改版本,让它能在 EVKB 上运行,并且仍然能重现这个问题。 大卫·R. Re: MCUX 11.0.1 - Debugger gives "Interrupt failed" dialog <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,大卫, 我偶尔也会遇到这种情况,但始终无法重现该问题,而且我猜你也无法分享你的项目(否则:请务必分享)。 我注意到或认为这可能是 SEGGER FreeRTOS 感知实现中的一个问题:我注意到它进行了大量数据读取,导致视图频繁刷新。针对此事,SEGGER 方面已收到待处理的工单。 禁用调试器中的 SEGGER FreeRTOS 感知功能确实很有帮助(但我承认,这使得调试 FreeRTOS 应用程序变得不太方便)。 我做的另一件事是尽可能关闭更多视图(尤其是反汇编视图),以减少流量。 我知道这并不理想,如果您能为 IDE 工程团队提供其他任何信息,那就太好了。 或许 GDB 跟踪信息会有所帮助,请参阅“Eclipse 中的板级启动技巧、GDB 日志和跟踪信息 | MCU on Eclipse”一文。 希望这能帮到您, 埃里希
記事全体を表示
LS-CGTツール(zipファイル)のインストール こんにちは、LS-CGTツールのダウンロード方法やアクセスをリクエストする場所を知りたいです。 スマート・カード
記事全体を表示
クールコーブレビュー 個人の快適さのためのコンパクトデザイン クールコーブ 気温が上がるにつれて、快適な室内環境の作り込みは生産性とリラクゼーションの両方にとってますます重要になります。在宅勤務でも勉強中でも、単に屋内で過ごす場合でも、良い空気の流れがあれば周囲がより爽やかで快適に感じられます。クールコーブは、パーソナルスペースの空気の流れを高めるとともに、コンパクトで携帯性の高いデザインの利便性を提供することで、室内の快適さを向上させるよう設計されています。 クールコーブ の最も魅力的な点の一つ は、そのシンプルさです。このデバイスはセットアップが簡単で、使用開始にほとんど手間がかかりません。複雑な設置や恒久的な設置が必要な大型冷却システムとは異なり、クールコーブは迅速かつ手間のない操作を目的に設計されています。ユーザーは安定した面に置き、電源を入れ、直感的な操作で設定を調整できます。このシンプルなデザインにより、あらゆる年齢層や経験レベルのユーザーがアクセスしやすいです。 コンパクトな サイズのため 、 さまざまな屋内空間に快適に収まります。机、ベッドサイドテーブル、キッチンカウンター、オフィスワークステーションなどに置いても、ほとんどスペースを取らず、周囲の環境と調和します。モダンな外観はさまざまなインテリアスタイルとよく調和し、住宅、アパート、寮、オフィスのあらゆる環境に適しています。
記事全体を表示
设置智能卡……我该从哪里开始? 这是我第一次在这里发帖,非常喜欢这个资源,我经常会参考它!我有一个关于为终端用户设置双因素认证智能卡的问题。 我们目前使用 HID 1386 非接触式卡进行大楼门禁(125Khz...?),我也希望能够将它们用于 PC。我不知道这是否可行,因为这些卡片是预先编程的,而且我甚至不知道它是否符合 NIST 800-171 指南。我收到了 HID 卡 1597 型号的报价,该卡包含智能芯片,并符合我们用于进入大楼的非接触式标准。 我的问题是,这些方法可以用于Windows身份验证吗?我的意思是,这些卡可以用于门禁吗?芯片是否兼容Windows AD?或者说,这些芯片必须符合某种标准才能正常工作?我看到的标准一直是 ISO 7816。 另外,部署这项技术在成本方面大概需要多少?我得到的报价是,100 张上述卡片的价格约为 1100 美元。我愿意考虑这个方案,因为这意味着我们只需要携带一张卡,但如果购买新的智能卡并携带一张备用卡会便宜得多,我也愿意考虑这个方案。 提前感谢! 汽车智能卡 Re: Setting up Smart Cards...where do I begin? 你好@ichiha68 希望你一切都好。 非常抱歉,我对 Windows AD 的要求以及您正在使用的免接触式卡的规格并不完全了解(请考虑联系制造商以获取更多支持)。 经过一番快速研究,HID 1386 卡似乎是 125 kHz 低频近距离凭证,用于物理访问控制。单靠 LF 近距离技术不足以实现 Windows/Active Directory 的原生智能卡登录,因为 Windows 智能卡登录似乎需要一个受支持的智能卡接口/中间件,Windows 可以通过该接口/中间件枚举用户证书并使用相应的私钥进行身份验证。 问候, 爱德华多。
記事全体を表示
S32 Design Studio for Power Architecture® 2017.R1 - License activation issue Hello, I would like to kindly request assistance regarding my license activation. My previous request was processed, but the wrong version was reactivated. I now have access to S32 Design Studio for Power Architecture v2.1, whereas I actually need to use S32 Design Studio for Power Architecture 2017.R1 (S32DS-PA v2.0) for my current projects. Could you please correct the activation and restore the proper version of the license? Thank you very much for your support. Best regards, Alessandro Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue Hello, I have requested it for you, Once it is done I will inform you. Best regards, Peter Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue Hello Peter, Thank you for your help. I just wanted to let you know that I have not received any update yet, and my license is still expired. As a result, I am currently unable to use S32 Design Studio for Power Architecture 2017.R1 (v2.0), and I am unable to continue my work. Best regards, Alessandro Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue Hello, All should be set at this time. Best regards, Peter Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue Thank you very much, Alessandro
記事全体を表示
aft05ms004nt1 i have a problem guys help me  i have an ic aft05ms004nt1 but i want it to transmit it with freq 30-45 mhz could someone help me with zload and zsource value guys please see table in attachment Re: aft05ms004nt1 Hello arkazains Good day! You're way outside the operating range of this transistor. Unfortunately, we don't have a replacement for this PN transistor due to the voltage levels it handles, but if you're willing to integrate level translators into your design, you might find other PN transistors that could help, for example: MRFE6VP61K25H Another option could be the AFT05MS003N; it's already marked as discontinued and is no longer in production, but you could check with our distributors to see if they still have any. I wish you the best of luck with your project. Have a great day and best of luck.
記事全体を表示
aft05ms004nt1 困ったことがあるんです、皆さん助けてください 私はAFT05MS004NT1というICを持っていますが、30~45MHzの周波数で送信したいと思っています。 どなたかZloadとZsourceの価値について助けていただけますか? 添付ファイルの表をご覧ください。 Re: aft05ms004nt1 こんにちは、arkazainsの皆さん。 良い一日! このトランジスタの動作範囲を大きく超えています。残念ながら、このPNトランジスタの代わりは電圧レベルの問題でありませんが、設計にレベルトランスレーターを組み込むことを検討すれば、例えば以下の通りの他のPNトランジスタが見つかるかもしれません。 MRFE6VP61K25H もう一つの選択肢は AFT05MS003N;すでに生産終了と表示されていますが、販売代理店にまだ在庫があるか確認すると良いでしょう。 プロジェクトの成功を心からお祈りしています。 良い一日をお過ごしください。幸運を祈ります。
記事全体を表示
OV5640とi.MX RT1170(ディスプレイなし)のインターフェース接続による画像キャプチャとデスクトップへのストリーミング こんにちは、 私はi.MX RT1170-EVKBボードを使用しており、OV5640カメラから画像をキャプチャし、LCDディスプレイを使用せずに、キャプチャした画像またはライブビデオストリームをデスクトップPCで表示することを目標としています。 MIPI CSI SDKの例を試してみて、RAW形式の画像データを取得できました。しかし、私はいくつかの問題に直面しています。 キャプチャされた出力はRAW形式で、これらの画像を正しく変換したり閲覧したりする方法を説明するドキュメントは見つかりませんでした。 撮影された画像には、色が不正確であったり、フィルターのようなアーティファクトが見られるため、カメラの出力が正しいかどうかを確認するのが難しい。 OV5640から画像をキャプチャしてデスクトップPCで閲覧するための完全なワークフローを説明する公式ドキュメントやアプリケーションノート、動画チュートリアルは見つかりませんでした。 オンボードディスプレイを使わずにイーサネットやUSB経由でカメラ出力をストリーミングする方法について明確な説明はありません。 私もsd_jpegのサンプルを試してみましたが、複数の問題に遭遇しました。 統合中に、プロジェクトはjconfig.hなどのJPEGライブラリ設定ファイルが不足していることを報告しました。 ビルドに関するいくつかの問題を解決した後も、JPEGエンコーダーとMIPI CSIカメラのサンプルを組み合わせる際に、コンパイルエラーと統合エラーが引き続き発生しました。 撮影したカメラ画像から有効なJPEG画像を生成することができませんでした。 私の目標は: LCDディスプレイを使わずに i.MX RT1170-EVKBボードでOV5640カメラをインターフェースしてください。 画像をキャプチャして、閲覧するためにデスクトップPCに転送します。 もし対応していれば、カメラからデスクトップPCへのライブ映像をイーサネット経由でストリーミングできます。 以下の質問について、ご助言いただければ幸いです。 このユースケースの公式SDK例や参考プロジェクトはありますか? OV5640からMIPI CSI、メモリ、JPEGまたはRAWプロセッシング、イーサネットやUSBからのデスクトップPCへの転送など、画像キャプチャパイプライン全体を説明するドキュメントはありますか? RT1170-EVKBでイーサネットを使ったライブストリーミングはサポートされていますか?もしそうなら、適切なSDKの例やミドルウェアをおすすめしてもらえますか? SD jpegの例に既知の問題や、MIPI CSIカメラの例と統合するために必要な追加設定はありますか? 何かアドバイスやドキュメント、参考プロジェクトがあれば大変ありがたいです。 再開まで今しばらくお待ちください。 Re: OV5640 Interfacing with i.MX RT1170 (Without Display) Image Capture and Streaming to Desktop こんにちは、 @Sureshk123 さん。 当事務所には、あなたの申請のための公式なプロジェクト例やリファレンスデザインはありません。とはいえ、私の理解では、以下の方法でアプリケーション全体を進めることをお勧めします。 カメラキャプチャパス(OV5640 > MIPI CSI > cameraBuffer)この部分には、前述のMIPI CSI SDKの例としてアプリケーションがあります。ERR051248によると「Video Mux コントローラ(VIDEO_MUX)、生データおよびMIPI_CSI2ブロックへのYUV422(10ビット)フォーマットはサポートされていません。」パラレルCSIの使用はオプションの回避策で、それかビデオデコーダーを使うこともできます。 カメラバッファに十分なデータが揃ったら、USBやlwIPを使ったSDKのサンプルプロジェクトを統合して、そのデータをPCに転送できます。バッファが正常に動作することが確認できてから、JPEGエンコードについて検討することをお勧めします。 BR、 エドウィン。
記事全体を表示
LS-CGT tool (zip) installtion Hello , i WOULD like to know how can i download  LS-CGT TOOL, or WHERE can i   REQUEST ACCESS to IT .  Smart Cards
記事全体を表示
スマートカードの設定…どこから始めればいいですか? 初めてここに投稿します。このリソースが利用できるのは本当にありがたいですし、頻繁に参考にしています!エンドユーザーの2段階認証スマートカードの設定について質問があります。 現在、建物(125kHz...?)にHID 1386の非接触カードを使っていますが、PCにも使えるようにしたいと思っています。しかし、カードにはあらかじめプログラムが施されているため、これが実現可能かどうかは分かりませんし、NIST 800-171のガイドラインを満たすかどうかも分かりません。スマートチップと建物に入る際に使う非接触型の標準を含むHIDカード1597のモデルの見積もりをもらいました。 私の質問は、これらはWindowsの認証に使えるかどうかです。つまり、これらのカードを使って入門できるのか、そしてそのチップはWindows ADと互換性があるのか、ということです。それとも、これらのチップが正常に動作するために満たさなければならない標準があるのでしょうか?私がよく目にした規格はISO 7816でした。 また、これを導入するにあたって、費用面ではどのような点を考慮すべきでしょうか?私が受け取った見積もりは、前述のカード100枚で約1100ドルでした。この案は、持ち歩くカードが1枚で済むので検討する価値があると思いますが、新しいスマートカードを購入して予備のカードを1枚持ち歩く方がはるかに安上がりであれば、そちらも検討します。 よろしくお願いいたします! オートモーティブ スマートカード Re: Setting up Smart Cards...where do I begin? こんにちは、@ichiha68さん あなたの調子が良いといいのですが。 申し訳ありませんが、Windows ADの要件や使用されている非接触カードの仕様を完全には把握していません(さらなるサポートについてはメーカーにお問い合わせください)。 簡単な調査の結果、HID 1386カードは物理的なアクセス制御を目的とした125 kHz LF近接認証情報のようです。このLF近接技術だけでは、Windows/Active Directoryのスマートカードログインには十分ではありません。なぜなら、Windowsスマートカードサインインは、Windowsがユーザー証明書を列挙し、対応する秘密鍵を認証できるスマートカードインターフェース/ミドルウェアを期待しているからです。 よろしくお願いいたします。 エドゥアルド。
記事全体を表示
S32 Design Studio for Power Architecture® 2017.R1 - ライセンス有効化の問題 こんにちは、 ライセンスの有効化に関して、ご支援をお願いしたいのですが。 以前のリクエストは処理されましたが、誤ったバージョンが再有効化されました。現在はPower Architecture v2.1用のS32 Design Studio にアクセスできるようになりましたが、現在のプロジェクトでは実際にはS32 Design Studio for Power Architecture 2017.R1(S32DS-PA v2.0)を使う必要があります。 アクティベーションを修正して、正しいライセンスのバージョンを復元してもらえますか? サポートありがとうございます。 よろしくお願いします、 アレッサンドロ Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue こんにちは、 あなたのためにリクエストしました。 完了次第、ご連絡いたします。 よろしくお願いいたします。 ピーター Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue こんにちは、ピーターさん。 ご協力ありがとうございます。 まだ何のアップデートも受け取っておらず、ライセンスも期限切れのままであることをお知らせしたかったのです。その結果、現在はS32 Design Studio for Power Architecture 2017.R1(v2.0)を使用できず、作業を継続することもできません。 よろしくお願いいたします。 アレッサンドロ Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue こんにちは、 現時点で全て準備が整っているはずです。 よろしくお願いいたします。 ピーター Re: S32 Design Studio for Power Architecture® 2017.R1 - License activation issue どうもありがとうございます、 アレッサンドロ
記事全体を表示
Cool Cove Review Compact Design for Personal Comfort Cool Cove As temperatures climb, creating a comfortable indoor environment becomes increasingly important for both productivity and relaxation. Whether you're working from home, studying, or simply spending time indoors, having good airflow can make your surroundings feel fresher and more pleasant. Cool Cove is designed to help improve indoor comfort by enhancing airflow in personal spaces while offering the convenience of a compact and portable design. One of the most appealing aspects of Cool Cove is its simplicity. The device is easy to set up and requires minimal effort to begin using. Unlike larger cooling systems that may involve complicated installation or permanent placement, Cool Cove is designed for quick and hassle-free operation. Users can simply position it on a stable surface, switch it on, and adjust the settings using the intuitive controls. This straightforward design makes it accessible for users of all ages and experience levels. The compact size of Cool Cove allows it to fit comfortably into a variety of indoor spaces. Whether placed on a desk, bedside table, kitchen counter, or office workstation, it occupies very little space while complementing the surrounding environment. Its modern appearance blends well with different interior styles, making it suitable for homes, apartments, dorm rooms, and office settings alike.
記事全体を表示
Thermal Data required for SE050E2HQ1/Z01Z3Z Hello Team,  I am looking for the thermal resistance data and operating junction temperature information for the part number:  SE050E2HQ1/Z01Z3Z Thanks and Regards Harsh Smart Cards Re: Thermal Data required for SE050E2HQ1/Z01Z3Z Hi @Harsh_Bhavsar , You may refer to https://www.nxp.com/docs/en/data-sheet/SE051.pdf for details. They are almost the same. Sincerely, Kan Re: Thermal Data required for SE050E2HQ1/Z01Z3Z Hello Kan_Li, Thank you for the response, the datasheet is very helpful. can you help me to get the maximum allowable junction temperature for the same OR can i consider the operating for it. Thanks and Regards Harsh Re: Thermal Data required for SE050E2HQ1/Z01Z3Z Hello kan, That is really helpful information. thanks and regards Harsh Re: Thermal Data required for SE050E2HQ1/Z01Z3Z Hi @Harsh_Bhavsar , The maximum junction temp for operation is only slightly higher than operation, as internal temp sensors start to trigger around 110°C .  Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
33FS45xx - overvoltage capability of VAUX I am using 33FS4500 and currently applying the VAUX supply as tracker to act as an external sensor supply. The use case includes short to battery level (32/40V) in error cases. The 33FS* data sheet states max. 40V for all pins the of chip itself, but does not state the consequences for the external pnp transistor in case of an overvoltage and whether there is a reverse current protection between VAUX and the Buck. - Is external sensor supply an intended use case of VAUX? - do I need an extra protection for VAUX?    and if - how does the circuit look like?   a first idea might be a schottky diode between transistor and VAUX (and its feedback). Re: 33FS45xx - overvoltage capability of VAUX Dear HajoV, using VAUX as an external/off-board sensor supply is an intended use case of the FS4500. VAUX can also operate in tracking mode to follow VCCA for ratiometric sensor applications.    For a potential short-to-battery condition (32 V to 40 V), the FS4500 documentation specifies that the VAUX-related pins are rated up to 40 V absolute maximum and explicitly mentions that VAUX is suitable for off-board supplies. It is also recommended to use an output capacitor rated above 40 V.   We could not find any statement in the datasheet, Safety Manual, or FAQ that confirms internal reverse-current protection between VAUX and the Buck/VPRE regulator. Therefore, for robust automotive designs, we recommend considering external protection, such as a Schottky blocking diode and/or a TVS clamp, to prevent back-feeding and improve robustness against fault conditions and transients.   With Best Regards, Jozef Re: 33FS45xx - overvoltage capability of VAUX Mhhh.. This information is not helping much and it is a bit disappointing as it only repeats the gaps in the data sheet. Short to battery (and GND) is somehow the class 1 error condition, every mobile eletronics is expected to survive. If designing an SBC/sensor tracker supply , I would expect, that not only the chip but the required peripherals safely survive usual overvoltages. External protection devices like (not so powerful) TVS diodes may act only above usual battery voltages😐. So they do not protect the critical range this question is about  (8.. 32V). Just to have a solution I am going to test a circuit with additional schottky diode in series to the pnp hoping that the linearity of the diode is sufficient to keep VAUX stable and test the circuit. (I added some default load to enshure that the diode is always conducting.) As I need << 100mA on VAUX I expect the diode drop to be tolerable.
記事全体を表示
SE050E2HQ1/Z01Z3Z所需的热数据 各位同事好, 我正在寻找以下零件编号的热阻数据和工作结温信息: SE050E2HQ1/Z01Z3Z 谢谢,此致敬礼。 残酷的 Smart Card Re: Thermal Data required for SE050E2HQ1/Z01Z3Z 你好@Harsh_Bhavsar , 详情请参阅https://www.nxp.com/docs/en/data-sheet/SE051.pdf 。它们几乎相同。 真挚地, 坎 Re: Thermal Data required for SE050E2HQ1/Z01Z3Z 你好 Kan_Li, 感谢您的回复,数据手册很有帮助。 你能帮我查一下这个器件的最大允许结温吗?或者我可以考虑一下它的工作温度吗? 谢谢,此致敬礼。 残酷的 Re: Thermal Data required for SE050E2HQ1/Z01Z3Z 你好 kan, 这真是非常有用的信息。 谢谢,此致敬礼。 残酷的 Re: Thermal Data required for SE050E2HQ1/Z01Z3Z 你好@Harsh_Bhavsar , 工作时的最大结温仅比工作温度略高,因为内部温度传感器在110°C左右开始触发信号。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
記事全体を表示
33FS45xx - VAUX 过压能力 我正在使用 33FS4500,目前将 VAUX 电源用作跟踪器,作为外部传感器电源。该用例包括故障情况下对电池电平(32/40V)短路。 33FS* 数据表显示最大值。芯片本身所有引脚的电压为 40V,但没有说明过压情况下外部 pnp 晶体管的后果,也没有说明 VAUX 和 Buck 之间是否有反向电流保护。 - VAUX 的预期用途之一是为外部传感器供电吗? - 我的 VAUX 接口需要额外的保护吗? 如果电路是这样的——它的结构是怎样的? 第一个想法可能是在晶体管和 VAUX(及其反馈)之间使用肖特基二极管。 Re: 33FS45xx - overvoltage capability of VAUX 亲爱的HajoV, 使用 VAUX 作为外部/板外传感器电源是 FS4500 的一个预期用途。VAUX 还可以以跟踪模式运行,以跟踪 VCCA,用于比率传感器应用。   对于可能发生的电池短路情况(32 V 至 40 V),FS4500 文档规定,VAUX 相关引脚的额定绝对最大值为 40 V,并明确指出 VAUX 适用于板外电源。建议使用额定电压高于 40V 的输出电容。   我们在数据表、安全手册或常见问题解答中找不到任何声明来确认 VAUX 和 Buck/VPRE 稳压器之间是否存在内部反向电流保护。因此,对于稳健的汽车设计,我们建议考虑外部保护,例如肖特基阻断二极管和/或 TVS 钳位电路,以防止反向馈电并提高对故障条件和瞬态的鲁棒性。   最诚挚的问候, 约瑟夫 Re: 33FS45xx - overvoltage capability of VAUX 嗯…… 这些信息帮助不大,而且有点令人失望,因为它只是重复了数据表中的不足之处。 对电池(和地线)短路属于一级错误状态,所有移动电子产品都应该能够承受。如果设计 SBC/传感器跟踪器电源,我希望不仅芯片本身,而且所需的外部设备也能安全地承受常见的过电压。 像(功率较小的)TVS二极管这样的外部保护装置可能只有在电池电压高于正常值时才会起作用。😐。 所以它们无法保护这个问题所涉及的关键范围(8.. 32V)。 为了找到解决方案,我打算测试一个在 pnp 晶体管上串联一个额外的肖特基二极管的电路,希望二极管的线性度足以保持 VAUX 稳定并测试该电路。 (我增加了一些默认负载,以确保二极管始终导通。) 由于我需要 VAUX 引脚上的电流小于 100mA,因此我预计二极管压降是可以接受的。
記事全体を表示
33FS45xx - VAUXの過電圧耐性 私は33FS4500を使っており、現在はVAUX電源をトラッカーとして外部センサ電源として使っています。ユースケースには、エラーCASEでバッテリーレベル(32/40V)までの短絡が含まれます。 33FS* データシートには最大値が記載されています。チップ本体のすべてのピンに対して40Vですが、過電圧が発生した場合の外部pnpトランジスタへの影響や、VAUXとバックスの間に逆流保護があるかどうかは明記されていません。 - 外部センサ供給はVAUXの意図されたユースケースか? - VAUXに追加の保護が必要か? もしそうなら、回路はどのような形ですか? 最初のアイデアとしては、トランジスタとVAUX(およびそのフィードバック)の間にショットキーダイオードを設置するのが考えられます。 Re: 33FS45xx - overvoltage capability of VAUX HajoV様、 VAUXを外部/オフボードのセンサ電源として使用することは、FS4500の意図された用途です。VAUXはまた、比率測定センサー用途向けにVCCAに従う追跡モードで動作することも可能です。   バッテリーへのショート(32Vから40V)の可能性がある場合、FS4500のドキュメントにはVAUX関連ピンは最大40Vまで定格されており、VAUXはオフボード電源にも適していることが明記されています。出力コンデンサは40V以上の定格のものを使用することをお勧めします。   データシート、セーフティマニュアル、FAQには、VAUXとバック/VPREレギュレーター間の内部逆流保護を肯定する記述は見つかりませんでした。したがって、堅牢なオートモーティブ設計には、逆流防止や故障状況や過渡現象に対する堅強性を高めるために、ショットキーブロッキングダイオードやTVSクランプなどの外部保護を検討することを推奨します。   敬具、 ヨゼフ Re: 33FS45xx - overvoltage capability of VAUX うーん… この情報はあまり役に立たず、データシートの欠落部分を繰り返しているだけなので、少し残念です。 バッテリー(およびGND)へのショートは、なぜかクラス1のエラー条件であり、すべての移動式エレトロニクスは生き残ることが期待されます。SBC/センサートラッカー電源を設計するなら、チップだけでなく必要なペリフェラルも通常の過電圧に安全に耐えられると期待します。 (それほど強力ではない)テレビダイオードのような外部保護装置は、通常のバッテリー電圧以上でのみ動作することがあります😐. したがって、この質問が関わる臨界範囲(8.. 32V)は保護しません。 解決策を見つけるために、pnpトランジスタにショットキーダイオードを直列に追加した回路をテストしてみようと思います。ダイオードの直線性によってVAUXが安定し、回路がテストできることを期待しています。 (ダイオードが常に導通するように、初期負荷を追加しました。) VAUXに必要な電流は100mA未満なので、ダイオードの電圧降下は許容範囲内だと考えています。
記事全体を表示