2390286_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2390286_en-US

2390286_en-US

S32K388 power supplies

Hello S32K388,

I am using the S32K388 for one of my applications. The V11 is meant to be supplied by a last mile regulator NMOS from V15. However I would like to supply this 1.5V from a external DC/DC converter. Is that feasible?

Best regards,

Jules

Re: S32K388 power supplies

Hello @JulesW ,

Based on the S32K388 power architecture, V11 must be generated using the external NMOS last-mile regulator from the V15 rail, as described in the Hardware Design Guidelines.

However, if your question is whether the 1.5 V V15 rail itself can be supplied from an external DC/DC converter, then this is feasible. This is also the approach used on the S32K388 EVB, where one jumper option is that the 1.5 V rail is generated externally by the PMIC.

Best regards,

Pavel

Tags (1)
No ratings
Version history
Last update:
‎07-04-2026 02:25 AM
Updated by: