2389767_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2389767_en-US

2389767_en-US

Thermal Data required for SE050E2HQ1/Z01Z3Z

Hello Team, 

I am looking for the thermal resistance data and operating junction temperature information for the part number: 


SE050E2HQ1/Z01Z3Z

Thanks and Regards
Harsh

Smart CardsRe: Thermal Data required for SE050E2HQ1/Z01Z3Z

Hi @Harsh_Bhavsar ,


You may refer to https://www.nxp.com/docs/en/data-sheet/SE051.pdf for details. They are almost the same.


Sincerely,

Kan

Re: Thermal Data required for SE050E2HQ1/Z01Z3Z

Hello Kan_Li,

Thank you for the response, the datasheet is very helpful.

can you help me to get the maximum allowable junction temperature for the same OR can i consider the operating for it.


Thanks and Regards
Harsh

Re: Thermal Data required for SE050E2HQ1/Z01Z3ZHello kan,

That is really helpful information.

thanks and regards
Harsh
Re: Thermal Data required for SE050E2HQ1/Z01Z3Z

Hi @Harsh_Bhavsar ,


The maximum junction temp for operation is only slightly higher than operation, as internal temp sensors start to trigger around 110°C


Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-15-2026 04:33 AM
更新者: