Create a .MEX File in S32 DS Hi, I'm using S32 Design Studio 3.4 for my project activities. Actually, I saw that .mex file is present in example projects. That .mex file helps me to understand the peripherals, clocks and pins connections. Now, as per my requirement I created a new project with Makefile and it is builded successfully. But in that project, I'm not having .mex file. So, I'm planning to create a .mex file as per my requirements. But I don't know, how to create .mex file for my project. So, could you please tell me the procedure to create .mex file for my project? & Please Let me know, if you need any other information. Note: I'm having S32K344 Development Board. Re: Create a .MEX File in S32 DS My list is EMPTY !!? : ... even already installed `S32SDK_S32K1xx_RTM_4.0.2.exe` : CY9_0-1787711160177.png -- BTW, S32 Design Studio for S32 Platform Version: 3.6.10 Build id: 260720 Re: Create a .MEX File in S32 DS Hello Ajay,
There's a couple of ways that a .mex file is created:
During project creation. When you use the New Application Project Wizard and select the Platform SDK, it will create a .mex file within the resulting project. image.png
If you have an existing project and would like to add a .mex file, then first attach the SDK.
Right-click on the project name in 'Project Explorer' view and select 'SDKs'.
Next, select the SDK from the list and click 'Attach/Detach', select all, then OK, Apply and Close.
If prompted for Check conflicted files, leave 'Replace all files' and 'Backup project files' boxes checked and click OK.
Now you will have a .mex file
Hope that helps,
Mike
查看全文