2407243_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2407243_en-US

2407243_en-US

FRDM-i.MX95: FRAMOS IMX900 and H.264 1080p120 Support

Hello,

I would like to confirm the following for the FRDM-i.MX95:

  1. Is the FRAMOS FSM:GO-IMX900C-M12-L102B-PM-A1Q1 (Sony IMX900 Color) currently supported on FRDM-i.MX95?

  2. If supported, are the required sensor driver, Device Tree configuration and NEO-ISP tuning files available? Which BSP/SDK version provides this support?

  3. Can this camera operate at 1920×1080 color at 120 FPS or higher through the i.MX95 CSI/ISP pipeline?

  4. Which adapter board and cable are required to connect this exact camera module to FRDM-i.MX95?

  5. Does the i.MX95 hardware VPU support single-stream H.264 encoding at 1920×1080 @ 120 FPS?

  6. With B-frames disabled and low-latency settings, what is the expected input-to-bitstream latency or minimum internal buffering?

  7. Is DMA-BUF zero-copy supported from the camera/ISP pipeline to the H.264 hardware encoder?

If the FRAMOS IMX900 module is not currently supported, could you recommend a supported color, global-shutter MIPI CSI-2 camera capable of 1920×1080 @ 120 FPS or higher on FRDM-i.MX95?

Thank you.

Graphics & DisplayLinuxMultimediaRe: FRDM-i.MX95: FRAMOS IMX900 and H.264 1080p120 SupportHello,

1> It is one of our partners supported sensors, so it is not completely supported by NXP, I would suggest to reach out Framos for this.

2> Same as above for this information please contact Framos

3> 2k@120FPS hits the limit of the ISP bandwidth, 1080p should not have issues but again please check with Framos for the supported features.

4> Please check with Framos for available resource for this.

5> The maximum throughput is 4K@60fps, so it should be doable for 1080p@120fps.

6> We do not provide specific input-to-bitstream latency figures for the i.MX95 VPU in low-latency mode. This must be measured on hardware with the target software configuration.

7> Yes, it is supported.

Best regards/Saludos,
Aldo.
Tags (1)
No ratings
Version history
Last update:
‎08-27-2026 04:29 AM
Updated by: