Layerscape ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layerscape Knowledge Base

ディスカッション

ソート順:
The VPP platform is an extensible framework that provides out-of-the-box production quality switch/router functionality. This document introduces Vector Packet Processing(VPP), creating VPP IPsec configuration scripts, building VPP v20.05 in LSDK 20.12, executing VPP IPsec on LS1046ARDB and LS2088ARDB platforms
記事全体を表示
This topic explains steps to compile and execute Hello World program (in C) on a Layerscape board. Similarly, you can execute other custom applications on your board. Create a Hello World program in C.  Copy this file (.c) on a Ubuntu machine (using WinSCP). Run the following command to convert the .c file into a binary file. $ aarch64-linux-gnu-gcc <.c file> -o <binary file> For example: $ aarch64-linux-gnu-gcc Hello_World.c -o Hello_World Note: You can use this command in the same directory in which .c file is present or provide path of this file. Connect to the board console on which you want to execute the custom application via terminal and boot the board with LITB. Note: It is suggested to boot the board with Tiny Linux for executing custom application.  => tftp 0xa0000000 lsdk2004_yocto_tiny_LS_arm64.itb Using e1000#0 device TFTP from server 192.168.3.1; our IP address is 192.168.3.142 Filename 'lsdk2004_yocto_tiny_LS_arm64.itb'. Load address: 0xa0000000 Loading: ################################################################# ################################################################# ##################################################### 4.3 MiB/s done Bytes transferred = 37030212 (2350944 hex) => bootm 0xa0000000#lx2160ardb ## Loading kernel from FIT Image at a0000000 ... Using 'lx2160ardb' configuration Trying 'kernel' kernel subimage Description: ARM64 Kernel Created: 2021-02-03 6:01:29 UTC Type: Kernel Image Compression: gzip compressed Data Start: 0xa00000d0 Data Size: 14086432 Bytes = 13.4 MiB When Tiny Linux boots, enable Ethernet to download the HelloWorld program on the board. To see the available networks. root@TinyLinux:~# ifconfig -a eth0 Link encap:Ethernet HWaddr 68:05:ca:2b:2c:ca BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Interrupt:114 Memory:90460c0000-90460e0000 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) sit0 Link encap:UNSPEC HWaddr 00-00-00-00-31-00-6C-6F-00-00-00-00-00-00-00-00 NOARP MTU:1480 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Enable the Ethernet connection. # ifconfig <eth interface> <IP address> netmask <netmask> up For example: root@TinyLinux:~# ifconfig eth0 192.168.3.121 netmask 255.255.255.0 up Set the gateway IP and ping the server to test the connection. # route add default gw <gateway IP> # ping <server IP> For example: root@TinyLinux:~# route add default gw 192.168.3.1 root@TinyLinux:~# ping 192.168.3.1 PING 192.168.3.1 (192.168.3.1): 56 data bytes 64 bytes from 192.168.3.1: seq=0 ttl=64 time=0.479 ms 64 bytes from 192.168.3.1: seq=1 ttl=64 time=0.204 ms Download the HelloWorld binary file on your board. For example: root@TinyLinux:~# scp [email protected]:/tftpboot/LX2160ARDB/HelloWorld . Execute the HelloWorld application. root@TinyLinux:~# ./HelloWorld Hello, World!    
記事全体を表示
To boot a Layerscape board with an empty DPL file: Create an empty DPL file, content.dts. For example: /dts-v1/; / { dpl-version = <0x0000000a>; containers { dprc@1 { compatible = "fsl,dprc"; parent = "none"; options = "DPRC_CFG_OPT_SPAWN_ALLOWED", "DPRC_CFG_OPT_ALLOC_ALLOWED", "DPRC_CFG_OPT_IRQ_CFG_ALLOWED"; objects { obj_set@dpmcp { type = "dpmcp"; ids = <0x1 0x2 0x3 0x4 0x5 0x6 0x7 0x8 0x9 0xa 0xb 0xc 0xd>; }; }; }; }; objects { dpmcp@1 { compatible = "fsl,dpmcp"; }; dpmcp@2 { compatible = "fsl,dpmcp"; }; dpmcp@3 { compatible = "fsl,dpmcp"; }; dpmcp@4 { compatible = "fsl,dpmcp"; }; dpmcp@5 { compatible = "fsl,dpmcp"; }; dpmcp@6 { compatible = "fsl,dpmcp"; }; dpmcp@7 { compatible = "fsl,dpmcp"; }; dpmcp@8 { compatible = "fsl,dpmcp"; }; dpmcp@9 { compatible = "fsl,dpmcp"; }; dpmcp@10 { compatible = "fsl,dpmcp"; }; dpmcp@11 { compatible = "fsl,dpmcp"; }; dpmcp@12 { compatible = "fsl,dpmcp"; }; dpmcp@13 { compatible = "fsl,dpmcp"; }; dpmcp@14 { compatible = "fsl,dpmcp"; }; dpmcp@15 { compatible = "fsl,dpmcp"; }; dpmcp@16 { compatible = "fsl,dpmcp"; }; dpmcp@17 { compatible = "fsl,dpmcp"; }; dpmcp@18 { compatible = "fsl,dpmcp"; }; dpmcp@19 { compatible = "fsl,dpmcp"; }; }; }; ​ Note: There is no network object capable of receiving Ethernet frames in the DPL file. You can create more dpmcps if the number of objects that will be created dynamically is high. Generate the DPL file using content.dts. dtc -I dts -O dtb -o dpl.dtb content.dts​ Flash the DPL file, dpl.dtb to the alternate bank.  tftp 0x80000000 dpl.dtb; i2c mw 66 50 20;sf probe; sf erase 0x00D00000 +$filesize && sf write 0x80000000 0x00D00000 $filesize​ Boot the board. After the board boots, create a dpmac. (Make sure you create a DPMAC that is valid based on the selected SERDES protocol configured by the RCW). restool dpmac create --mac-id=3​ Probe the dpmac driver. restool dprc assign dprc.1 --object=dpmac.3 --plugged=1​ Create a network interface. ls-addni dpmac.3​ Save contents as content_new.dts. restool dprc generate-dpl dprc.1 > content_new.dts​    
記事全体を表示
  Note: MCFBA{L/H} that is used to dump the MC log buffer is valid only after the following command is executed: fsl_mc start mc  ${mc_addr} ${dpc_addr} Run the above command first, then MCFBA contents will be valid. To display the MC log buffer in U-Boot for debug purpose, when MC console is not available: Determine the MC firmware base. At the U-Boot prompt, perform md at 0x8340020 (this is MCFBA{L/H}) => md 0x8340020 10 08340020: e0000006 00000027 00060000 00000000 ....'........... 08340030: 00000000 00000000 00000000 00000000 ................ 08340040: 00000000 00000000 00000000 00000000 ................ 08340050: 00000000 00000000 00000000 00000000 ................ The value at 08340024 is the MCFBAH address. In this case, it is 00000027. The value at 08340020 is the MCFBAL address. In this case, it is e0000000. So you can build the MCFBA base address as:  0x27e0000000. Run the following command to start the MC if it is not booted already. run mcinitcmd Dump the log buffer structure at offset 0x01000000 into the MC firmware base 0x27e1000000 (as per the example). md 27e1000000 27e1000000: 4d430100 00000000 01400000 00300000 [email protected]. 27e1000010: 000000b1 00000000 00000000 00000000 ................ 27e1000020: 00000000 00000000 00000000 00000000 ................ 27e1000030: 00000000 00000000 00000000 00000000 ................ 4d430100 = magic number, 400000 = log buffer offset, 00300000 = log buffer length Dump the content of the log buffer. md 27e1400000   The output size can be increased by specifying the number of objects.  md 27e1400000 <num> For example: md 27e1400000 20 In case that the log buffer has more information, you can extend the output of md by replacing 20 with a greater value.          
記事全体を表示
Prerequisites: The board should be running Linux and connected to terminal console. Note: For log level debug support, the restool version should be LSDK-2003-RC1 or above and MC version should be 10.20.0 or above. To check restool version: $ root@localhost:~# restool -v restool LSDK-20.04 To check MC version: root@localhost:~# restool -m MC firmware version: 10.24.0 For debugging, use the ls-debug script available in the LSDK rootfs. There is no need to create the debug object. ls-debug -h ls-debug options -h, --help ls-debug help information -ts, --timestamp=X Enable/Disable timestamp printing, X is ON or OFF -c, --console=X Enable/Disable printing in UART console, X is ON or OFF -l, --log=X Enable/Disable printing in DDR log, X is ON or OF -u, --uart=X Set UART ID of the console, X = [0 - 4], 0 = OFF -ll, --level=X Set logging level, X = [0 - 5] 0: Global 1: Debug 2: Info 3: Warning 4: Error 5: Critical -m, mem, --memory Dump information about memory modules available dpxy.z Dump information about MC respective object   For example, to enable logging in console with log level INFO: $ ls-debug --log=on --console=on --level=2 dpdbg.0 created DDR log printing ON UART console printing ON Log level set to 2 $ root@localhost:~# ls-debug --memory Memory dumped information available in MC log/console $ root@localhost:~# cat `find /dev/ -name "*mc_console"` [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dpdbg_open on DPDBG [I, RESMAN] Handling command: dpdbg_dump on DPDBG [I, DPNI] Memory info: [I, DPNI] MC DDR #1 cacheable memory [I, DPNI] Total: 134217728 bytes [I, DPNI] Used: 14802708 bytes [I, DPNI] Free: 119415020 bytes [I, DPNI] MC DDR #1 non-cacheable memory [I, DPNI] Total: 50331648 bytes [I, DPNI] Used: 27680 bytes [I, DPNI] Free: 50303968 bytes [I, DPNI] DMEM1 memory [I, DPNI] Total: 81920 bytes [I, DPNI] Used: 27168 bytes [I, DPNI] Free: 54752 bytes [I, DPNI] DMEM2 memory [I, DPNI] Total: 81920 bytes [I, DPNI] Used: 27168 bytes [I, DPNI] Free: 54752 bytes [I, DPNI] DDR #1 memory [I, DPNI] Total: 1610612736 bytes [I, DPNI] Used: 143163392 bytes [I, DPNI] Free: 1467449344 bytes [I, DPNI] PEB memory [I, DPNI] Total: 2097152 bytes [I, DPNI] Used: 524288 bytes [I, DPNI] Free: 1572864 bytes [I, DPNI] DP-DDR memory [I, DPNI] Total: 4294967296 bytes [I, DPNI] Used: 0 bytes [I, DPNI] Free: 4294967296 bytes [I, RESMAN] Handling command: dpdbg_close on DPDBG [I, RESMAN] Handling command: dprc_close for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_set_irq_mask for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_set_irq_enable for DPRC 1 on portal id 0 root@localhost:~#
記事全体を表示
This topic shows steps to customize LITB by using a different kernel image instead of the existing kernel image. Browse to the FlexBuild installation directory. Modify the kernel image in linux_arm64_LS.its. $ vi configs/linux/linux_arm64_LS.its Save the changes done in the file. Generate LITB using flex-builder. $ source setup.env $ flex-builder -i mkitb -r <distro_type>:<distro_scale> -a <arch> For example: $ source setup.env $ flex-builder -i mkitb -r ubuntu:main -a arm64 INSTRUCTION: mkitb DISTRO TYPE: ubuntu DISTRO SCALE: main .... .... /home/flexbuild_lsdk2004/build/images/lsdk2004_ubuntu_main_LS_arm64.itb [Done]   Note: To create .itb file directly from .its file, run this command: mkimage -f <xyz.its> <xyz.itb> Connect to the board console via terminal and run following commands at U-boot to boot the board with customized LITB. => ping $serverip Using e1000#0 device host 192.168.3.1 is alive => Using e1000#0 device host 192.168.3.1 is alive => tftp 0xa0000000 lsdk2004_ubuntu_main_LS_arm64.itb Using e1000#0 device TFTP from server 192.168.3.1; our IP address is 192.168.3.49 Filename 'lsdk2004_ubuntu_main_LS_arm64.itb'. Load address: 0xa0000000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# #################################### 9.8 MiB/s done Bytes transferred = 683506200 (28bd7a18 hex) => bootm 0xa0000000#lx2160ardb ## Loading kernel from FIT Image at a0000000 ... Using 'lx2160ardb' configuration Trying 'kernel' kernel subimage Description: ARM64 Kernel Created: 2021-02-03 6:01:29 UTC Type: Kernel Image Compression: gzip compressed Data Start: 0xa00000d0 Data Size: 14086432 Bytes = 13.4 MiB   Check timestamp in boot log to ensure that the board is booted with the updated kernel image in the customized LITB.   Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd083] [ 0.000000] Linux version 5.4.3 (test@Ubuntu-18) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)) #1 SMP PREEMPT Wed Feb 3 00:04:09 IST 2021 [ 0.000000] Machine model: NXP Layerscape LX2160ARDB [ 0.000000] earlycon: pl11 at MMIO32 0x00000000021c0000 (options '') [ 0.000000] printk: bootconsole [pl11] enabled [ 0.000000] efi: Getting EFI parameters from FDT:  
記事全体を表示
To extract kernel, rootfs, and dtb images from the Linux ITB (LITB) image: Browse to the folder containing LITB. For example: $ cd flexbuild_lsdk2004/build/images/ To list the header information of LITB, use the following command: $ dumpimage -l <name of the image> $ dumpimage -l lsdk2004_ubuntu_main_LS_arm64.itb FIT description: arm64 kernel, ramdisk and FDT blob Created: Tue Feb 2 18:54:19 2021 Image 0 (kernel) Description: ARM64 Kernel Created: Tue Feb 2 18:54:19 2021 Type: Kernel Image Compression: gzip compressed Data Size: 14086432 Bytes = 13756.28 kB = 13.43 MB Architecture: AArch64 OS: Linux Load Address: 0x84080000 Entry Point: 0x84080000 Hash algo: crc32 Hash value: 1980d6fd Image 1 (initrd) Description: initrd for arm64 Created: Tue Feb 2 18:54:19 2021 Type: RAMDisk Image Compression: uncompressed Data Size: 668988861 Bytes = 653309.43 kB = 638.00 MB Architecture: AArch64 OS: Linux Load Address: 0x00000000 Entry Point: 0x00000000 Hash algo: crc32 Hash value: 24aa3c08 Image 2 (ls1012ardb-dtb) Description: ls1012ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 14335 Bytes = 14.00 kB = 0.01 MB Architecture: AArch64 Hash algo: crc32 Hash value: 383a8118 Image 3 (ls1012aqds-dtb) Description: ls1012aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 15972 Bytes = 15.60 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: 7d133305 Image 4 (ls1012afrwy-dtb) Description: ls1012afrwy-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 15316 Bytes = 14.96 kB = 0.01 MB Architecture: AArch64 Hash algo: crc32 Hash value: 7c456ca3 Image 5 (ls1028ardb-dtb) Description: ls1028ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 19767 Bytes = 19.30 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: db86fa4f Image 6 (ls1028aqds-dtb) Description: ls1028aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 24733 Bytes = 24.15 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: e0b7a722 Image 7 (ls1043ardb-dtb) Description: ls1043ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 41085 Bytes = 40.12 kB = 0.04 MB Architecture: AArch64 Hash algo: crc32 Hash value: fcc6502c Image 8 (ls1043aqds-dtb) Description: ls1043aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 34544 Bytes = 33.73 kB = 0.03 MB Architecture: AArch64 Hash algo: crc32 Hash value: 45f82fba Image 9 (ls1046ardb-dtb) Description: ls1046ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 40270 Bytes = 39.33 kB = 0.04 MB Architecture: AArch64 Hash algo: crc32 Hash value: 013f5024 Image 10 (ls1046aqds-dtb) Description: ls1046aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 34317 Bytes = 33.51 kB = 0.03 MB Architecture: AArch64 Hash algo: crc32 Hash value: be066013 Image 11 (ls1046afrwy-dtb) Description: ls1046afrwy-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 31528 Bytes = 30.79 kB = 0.03 MB Architecture: AArch64 Hash algo: crc32 Hash value: d872df6c Image 12 (ls1088ardb-dtb) Description: ls1088ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 19523 Bytes = 19.07 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: 403066bc Image 13 (ls1088aqds-dtb) Description: ls1088aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 19415 Bytes = 18.96 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: a2bf2786 Image 14 (ls2088ardb-dtb) Description: ls2088ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 29838 Bytes = 29.14 kB = 0.03 MB Architecture: AArch64 Hash algo: crc32 Hash value: 0069fe03 Image 15 (ls2088aqds-dtb) Description: ls2088aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 23557 Bytes = 23.00 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: e8e9dfa7 Image 16 (lx2160ardb-dtb) Description: lx2160ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 32643 Bytes = 31.88 kB = 0.03 MB Architecture: AArch64 Hash algo: crc32 Hash value: e5859b31 Image 17 (lx2160aqds-dtb) Description: lx2160aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 27740 Bytes = 27.09 kB = 0.03 MB Architecture: AArch64 Hash algo: crc32 Hash value: f644de1e To extract a particular image from LITB, use the following command:  $ dumpimage -i <name of the image> -T <type> [-p position] [-o outfile] data_file For example: To extract the kernel image: $ dumpimage -T flat_dt -i lsdk2004_ubuntu_main_LS_arm64.itb -p 0 kernel Extracted: Image 0 (kernel) Description: ARM64 Kernel Created: Tue Feb 2 18:54:19 2021 Type: Kernel Image Compression: gzip compressed Data Size: 14086432 Bytes = 13756.28 kB = 13.43 MB Architecture: AArch64 OS: Linux Load Address: 0x84080000 Entry Point: 0x84080000 Hash algo: crc32 Hash value: 1980d6fd To extract the rootfs image: $ dumpimage -T flat_dt -i lsdk2004_ubuntu_main_LS_arm64.itb -p 1 rootfs Extracted: Image 1 (initrd) Description: initrd for arm64 Created: Tue Feb 2 18:54:19 2021 Type: RAMDisk Image Compression: uncompressed Data Size: 668988861 Bytes = 653309.43 kB = 638.00 MB Architecture: AArch64 OS: Linux Load Address: 0x00000000 Entry Point: 0x00000000 Hash algo: crc32 Hash value: 24aa3c08 To extract ls1012ardb-dtb (at position 2) and ls1012aqds-dtb (at position 3): $ dumpimage -T flat_dt -i lsdk2004_ubuntu_main_LS_arm64.itb -p 2 dtb1 Extracted: Image 2 (ls1012ardb-dtb) Description: ls1012ardb-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 14335 Bytes = 14.00 kB = 0.01 MB Architecture: AArch64 Hash algo: crc32 Hash value: 383a8118 $ dumpimage -T flat_dt -i lsdk2004_ubuntu_main_LS_arm64.itb -p 3 dtb2 Extracted: Image 3 (ls1012aqds-dtb) Description: ls1012aqds-dtb Created: Tue Feb 2 18:54:19 2021 Type: Flat Device Tree Compression: uncompressed Data Size: 15972 Bytes = 15.60 kB = 0.02 MB Architecture: AArch64 Hash algo: crc32 Hash value: 7d133305      
記事全体を表示
The below steps describe how to measure CPU temperature and how to stress individual cores of CPU. Steps are explained with an example of LX2160A SoC. However, these steps are applicable to all Layerscape devices. Download Flexbuild and add packages in Yocto tiny Generate Yocto tiny userland Enable thermal monitoring unit and build kernel Generate .itb image Load .itb image from TFTP server to Layerscape board Validate stress package and measure CPU temperature before and after stress Step 1: Download Flexbuild and add packages in Yocto tiny On a Linux machine, download Layerscape Software Development Kit - <version>. Go to Download tabs at http://www.nxp.com/lsdk. Enter login details, accept the agreement to download the Flexbuild source tarball in the name format flexbuild_<version>.tgz. Run the following commands to extract Flexbuild files from tar archived file. $ tar xvzf flexbuild_<version>.tgz $ cd flexbuild_<verison> $ source setup.env $ flex-builder -h Add “stress” package to "IMAGE_INSTALL_append" parameter of local_arm64_tiny.conf file available in flexbuild_<version>/configs/yocto/ folder. Save and exit the file. Step 2 – Generate Yocto tiny userland Change directory to flexbuild_<version>. Clean obsolete cache data. This step is needed in case source/config has changed. $ source setup.env $ flex-builder -i clean-rfs -r yocto Run the following commands to generate Yocto-based tiny userland: $ flex-builder -i mkrfs -r yocto:tiny $flex-builder -i mklinux -r yocto:tiny $ flex-builder -i mkfw -m <machine_name> -b sd This generates the following images: rootfs_lsdk<version>_yocto_tiny_arm64.cpio.gz (~22M), lsdk<version>_yocto_tiny_LS_arm64.itb, and firmware_<machine_name>_uboot_sdboot.img. For example: rootfs_lsdk2004_yocto_tiny_arm64.cpio.gz (~22M), lsdk2004_yocto_tiny_LS_arm64.itb, and firmware_lx2160ardb_rev2_uboot_sdboot.img Step 3 Enable system monitoring unit and build kernel Change directory to flexbuild_<version>/packages/linux/linux. Enable environmental setting for cross-compiling. The following setting is applicable when you configure and build kernel on a different architecture from the target. For example, compiling an Armv8 kernel on an X86 computer. Run the following commands on Ubuntu Linux: $ export CROSS_COMPILE=aarch64-linux-gnu- $ export ARCH=arm64 Run make menuconfig command to configure settings to enable thermal monitoring unit. $ make menuconfig The command opens the kernel configuration [tree-view structure] prompt. Use the Arrow keys to navigate the menu and Enter to select the submenu. Navigate to Device Drivers --> <*> Generic Thermal sysfs driver --> [ ] Generic CPU cooling support option. Press Y key to include the option. [*] symbol indicates the option is included (shown in below figure). Similarly, include the following options to enable thermal management framework. After you include all options as mentioned in the above table, save the configuration with a file name. For example,  save the configuration file as thermal.config. Exit to come out of the Kernel Configuration prompt. Copy the configuration file to arch/arm64/configs folder. $ cp <config filename> arch/arm64/configs/ For example, $ cp thermal.config arch/arm64/configs/ Configure the kernel. Load the changed configuration for Layerscape Armv8 platform in 64-bit mode for LSDK. $ export CROSS_COMPILE=aarch64-linux-gnu- $ export ARCH=arm64 $ make distclean $ make defconfig <config filename> Build kernel image and device tree image. $ make -j8 Step 4 - Generate .itb file Generate .itb file, which includes stress package and thermal monitoring unit installed, for kernel booting. Copy the Image and Image.gz files from the /flexbuild_<version>/packages/linux/linux/arch/arm64/boot folder and to the /flexbuild_<version>/build/linux/kernel/arm64/LS folder. Change directory to flexbuild_<version>. Generate .itb image using flex-builder. $ source setup.env $ flex-builder -i mkitb -r yocto:tiny This generates lsdk2<version>_yocto_tiny_LS_arm64.itb file. For example, lsdk2004_yocto_tiny_LS_arm64.itb file. Copy the .itb image to the TFTP server. Step 5 - Load .itb image from TFTP server to Layerscape board Set up Ethernet connection between the board (for example, LX2160ARDB) and host machine on which you have configured the TFTP server. Boot the board to U-Boot prompt. U-Boot prints a list of enabled Ethernet interfaces. For example, LX2160ARDB U-Boot prints following Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id  Set server IP address to the IP address of the host machine on which you have configured the TFTP server. => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LX2160ARDB Ethernet Port Mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.2.1 is alive Load the .itb image from TFTP server to DDR memory of the board. => tftp 0xa0000000 <itb_file_name> For example: => tftp 0xa0000000 lsdk2004_yocto_tiny_LS_arm64.itb Boot the kernel with .itb image as follows: => bootm 0xa0000000#<board_name> For example: => bootm 0xa0000000#lx2160ardb Let the board boots to Tiny Linux. Step 6 – Validate stress package and measure CPU temperature before and after stress Check stress-ng package using which stress-ng command: # which stress-ng /usr/bin/stress-ng Check scaling_current_frequency of the cores. # cat /sys/devices/system/cpu/cpu*/cpufreq/scaling_cur_freq  For example: Check frequency of 16 cores of LX2160ARDB as follows: Check the temperature of the CPU before applying stress. # cat /sys/class/thermal/thermal_zone*/temp Apply stress by executing following command: # stress-ng -c 8 -i 1 -m 1 --vm-bytes 128M -t 60s & The command applies stress for 60 seconds. For more information on stress-ng command, run stress-ng -h command for help. Check the temperature of the CPU after applying stress. # cat /sys/class/thermal/thermal_zone*/temp For example:
記事全体を表示
The below steps describe how to measure the CPU power using sensors and also describe how to stress individual cores of CPU. Steps are explained with an example of LX2160A SoC. However, these steps are applicable to all Layerscape devices. Download Flexbuild and add packages in Ubuntu:Lite Generate Ubuntu-based Lite userland (Ubuntu:Lite) Enable system monitoring unit and build kernel Generate .itb image Load .itb image from TFTP server to Layerscape board Validate stress package and measure CPU power using sensors Step 1: Download Flexbuild and add packages in Ubuntu:lite On a Linux machine, download Layerscape Software Development Kit - <version>. Go to Download tabs at http://www.nxp.com/lsdk. Enter login details, accept the agreement to download the Flexbuild source tarball in the name format flexbuild_<version>.tgz. Run the following commands to extract Flexbuild files from tar archived file. $ tar xvzf flexbuild_<version>.tgz $ cd flexbuild_<verison> $ source setup.env $ flex-builder -h Add packages for stress and power sensors in the additional_lite_packages_list file available in the flexbuild_<version>/configs/ubuntu/ folder. Add ‘stress’ and ‘lm-sensors’ packages for Ubuntu Lite as shown below: Save and exit the file. Step 2 – Generate Ubuntu:Lite image Change directory to flexbuild_<version>. Clean obsolete cache data. This step is needed in case the source/configuration has changed. $ source setup.env $ flex-builder -i clean-rfs -r ubuntu:lite Generate Ubuntu-based Lite userland using the following command: $ flex-builder -i mkrfs -r ubuntu:lite This generates rootfs_lsdk<version>_ubuntu_lite_arm64 file. For example: rootfs_lsdk2004_ubuntu_lite_arm64 file. Pack userland in tgz format (Optional step). $ flex-builder -i packrfs -r ubuntu:lite For example: rootfs_lsdk2004_ubuntu_lite_arm64.tgz (~180 M)   Step 3 Enable system monitoring unit and build kernel Change directory to flexbuild_<version>/packages/linux/linux. Enable environmental setting for cross-compiling. The following setting is applicable when you configure and build kernel on a different architecture from the target. For example, compiling an Armv8 kernel on an X86 computer. Run the following commands on Ubuntu Linux: $ export CROSS_COMPILE=aarch64-linux-gnu- $ export ARCH=arm64 Run make menuconfig command to configure settings to enable system monitoring unit for sensing power. $ make menuconfig The command opens the kernel configuration [tree-view structure] prompt. Use the Arrow keys to navigate the menu and Enter to select the submenu. Navigate to Device Drivers --> <*> Hardware Monitoring Support --> [M] Texas Instruments INA219 and compatibles option. Device Drivers-->Hardware Monitoring Support Press Y key to include the option. [*] symbol indicates the option is included (shown in below figure). This enables INA220. Texas Instruments INA219 and Compatibles option included Similarly, include the following options to enable I2C block device driver support and I2C bus multiplexing PC9547. Kernel Configure Tree View Option After you include all options as mentioned in the above table, save the configuration with a file name. For example,  save the configuration file as power.config. Exit to come out of the Kernel Configuration prompt. Copy the configuration file to arch/arm64/configs folder. $ cp <config filename> arch/arm64/configs/ For example, $ cp power.config arch/arm64/configs/ Configure the kernel. Load the changed configuration for Layerscape Armv8 platform in 64-bit mode for LSDK. $ export CROSS_COMPILE=aarch64-linux-gnu- $ export ARCH=arm64 $ make distclean $ make defconfig <config filename> Build kernel image and device tree image. $ make -j8 Step 4 - Generate .itb file Generate .itb file, which includes stress package and thermal monitoring unit installed, for kernel booting. Copy the Image and Image.gz files from the /flexbuild_<version>/packages/linux/linux/arch/arm64/boot folder and to the /flexbuild_<version>/build/linux/kernel/arm64/LS folder. Change directory to flexbuild_<version>. Generate .itb image using flex-builder. $ source setup.env $ flex-builder -i mkitb -r ubuntu:lite This generates lsdk<version>_ubuntu_lite_LS_arm64.itb file. For example, lsdk2004_ubuntu_lite_LS_arm64.itb Copy the .itb image to the TFTP server. Step 5 - Load .itb image from TFTP server to Layerscape board Set up Ethernet connection between the board (for example, LX2160ARDB) and host machine on which you have configured the TFTP server. Boot the board to U-Boot prompt. U-Boot prints a list of enabled Ethernet interfaces. For example, LX2160ARDB U-Boot prints following Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id  Set server IP address to the IP address of the host machine on which you have configured the TFTP server. => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LX2160ARDB Ethernet Port Mapping  for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.2.1 is alive Load the .itb image from TFTP server to DDR memory of the board. => tftp 0xa0000000 <itb_file_name> For example: => tftp 0xa0000000 sdk2004_ubuntu_lite_LS_arm64.itb Boot the kernel with .itb image as follows: => bootm 0xa0000000#<board_name> For example: => bootm 0xa0000000#lx2160ardb Board boots to Linux prompt. Step 6 – Validate stress package and measure CPU power using sensors Validate if stress and sensors packages have been installed properly. $ which stress ./usr/bin/stress  $ which sensors ./usr/bin/sensors Measure CPU power before applying stress to the cores. $ sensors CPU power before stress Apply stress to CPU cores using the following command. # stress -c <number of cores> -i <number of IO> -m <number of vm> --vm-bytes 128M -t <time in seconds> & For example: The command applies stress for 60 seconds. For more information on stress command, run stress-h command for help. Measure CPU power after applying stress in given time interval. $ sensors
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Note: Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.   To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For FlexSPI NOR flash boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_flexspi_nor.pbl BL2 binary: Platform initialization binary RCW binary for FlexSPI NOR flash fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image   Follow these steps to compile and deploy TF-A  binaries (bl2_flexspi_nor.pbl and fip.bin) in FlexSPI NOR flash. Compile PBL binary from RCW source file Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_flexspi_nor.pbl and fip.bin) for FlexSPI NOR flash Program TF-A binaries to FlexSPI NOR flash Step 1: Compile RCW binary  You need to compile the RCW binary to build the bl2_flexspi_nor.pbl binary. Clone the  rcw  repository and compile the RCW binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04  Compile the RCW binary for Rev 1 or Rev 2 board. For LX2160ARDB Rev 1: $ cd lx2160ardb For LX2160ARDB Rev 2: $ cd lx2160ardb_rev2 If required, make changes to the rcw files. $ make   The compiled PBL binary for FlexSPI NOR flash on LX2160ARDB for core frequency 2000 MHz, platform frequency 700 MHz and DDR memory data rate 2900 MT/s, with serdes1 = 19 serdes2 = 5 serdes3 = 2, rcw_2000_700_2900_19_5_2.bin is available at: rcw/lx2160ardb/XGGFF_PP_HHHH_RR_19_5_2 (For LX2160ARDB Rev 1) rcw/lx2160ardb_rev2/XGGFF_PP_HHHH_RR_19_5_2 (For LX2160ARDB Rev 2) Note: See the rcw/lx2160ardb/README or rcw/lx2160ardb_rev2/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make lx2160ardb_tfa_defconfig $ make Note: If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.12 and above U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OP-TEE binary You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-lx2160ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for FlexSPI NOR flash Clone the atf repository and compile the TF-A binaries, bl2_flexspi_nor.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=lx2160ardb bl2 SPD=opteed BOOT_MODE=flexspi_nor BL32=<path_to_optee_binary>/tee.bin pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin   The compiled BL2 binaries, bl2.bin and bl2_flexspi_nor.pbl are available at atf/build/lx2160ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_flexspi_nor.pbl binary needs to be recompiled.   To compile the BL2 binary without OPTEE: make PLAT=lx2160ardb bl2 BOOT_MODE=flexspi_nor pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=lx2160ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/lx2160ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: make PLAT=lx2160ardb fip BOOT_MODE=flexspi_nor BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT Step 5: Program TF-A binaries to FlexSPI NOR flash Boot LX2160ARDB from FlexSPI. Ensure that the switches are set to boot the board from FlexSPI. For booting from FlexSPI: SW1[1:8] = 1111 100X [X is 0 for FlexSPI NOR flash0 and X is 1 for FlexSPI NOR flash1] SW2[1:8] = 0000 0110 SW3[1:8] = 1111 1100 SW4[1:8] = 1011 1000 Boot from FlexSPI NOR flash0: => qixis_reset   For LX2160ARDB Rev 1, in boot log, you'll see: Board: LX2160ACE Rev1.0-RDB, Board version: B, boot from FlexSPI DEV#0   For LX2160ARDB Rev 2, in boot log, you'll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii [PRIME], DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id, e1000#0  Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. Note: SeeLX2160ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask>   => setenv gatewayIP <gateway IP> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.1.1 is alive Load TF-A binaries from the TFTP server Note: For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Program FlexSPI NOR flash1: => sf probe 0:1 Flash bl2_flexspi_nor.pbl: => tftp 0xa0000000 bl2_flexspi_nor.pbl => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Flash fip.bin: => tftp 0xa0000000 fip.bin => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Boot from FlexSPI NOR flash1: => qixis_reset altbank LX2160ARDB will boot with TF-A. In the boot log, you will see: => NOTICE: BL2: v1.5(release):LSDK-20.04 NOTICE: BL2: Built : 22:01:10, Aug 20 2020 NOTICE: UDIMM 18ADF2G72AZ-3G2E1 NOTICE: DDR4 UDIMM with 2-rank 64-bit bus (x8) NOTICE: 32 GB DDR4, 64-bit, CL=22, ECC on, 256B, CS0+CS1 NOTICE: BL2: Booting BL31 NOTICE: BL31: v1.5(release):LSDK-20.04 NOTICE: BL31: Built : 22:02:07, Aug 20 2020 NOTICE: Welc U-Boot 2019.10 (Aug 14 2020 - 17:43:28 +0530) SoC: LX2160ACE Rev2.0 (0x87360020) Clock Configuration: CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz CPU6(A72):2000 MHz CPU7(A72):2000 MHz CPU8(A72):2000 MHz CPU9(A72):2000 MHz CPU10(A72):2000 MHz CPU11(A72):2000 MHz CPU12(A72):2000 MHz CPU13(A72):2000 MHz CPU14(A72):2000 MHz CPU15(A72):2000 MHz Bus: 700 MHz DDR: 2900 MT/s Reset Configuration Word (RCW): 00000000: 50777738 24500050 00000000 00000000 00000010: 00000000 0c010000 00000000 00000000 00000020: 02e001a0 00002580 00000000 00000096 00000030: 00000000 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027000 00000000 00000070: 08b30010 00150020 Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#1      
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Note: Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.                                                                 To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For SD/eMMC boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_sd.pbl/bl2_emmc.pbl BL2 binary: Platform initialization binary RCW binary for SD/emmc boot  fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image   Follow these steps to compile and deploy TF-A  binaries (bl2_sd.pbl/bl2_emmc.pbl and fip.bin) on the SD/eMMC card. Compile RCW binary Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_sd.pbl/bl2_emmc.pbl and fip.bin) for SD/eMMC boot Program TF-A binaries to the SD/eMMC card Step 1: Compile RCW binary You need to compile the RCW binary to build the bl2_sd.pbl/bl2_emmc.pbl binary. Clone the  rcw repository and compile the RCW binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $  git checkout -b LSDK-20.04 LSDK-20.04 Compile RCW for Rev 1 or Rev 2 board. For LX2160ARDB Rev1: $ cd lx2160ardb For LX2160ARDB Rev2: $ cd lx2160ardb_rev2 If required, make changes to the rcw files. $ make The compiled RCW binary for SD/eMMC boot on LX2160ARDB for core frequency 2000 MHz, platform frequency 700 MHz and DDR memory data rate 2900 MT/s, with serdes1 = 19 serdes2 = 5 serdes3 = 2, rcw_2000_700_2900_19_5_2.bin is available at: rcw/lx2160ardb/XGGFF_PP_HHHH_RR_19_5_2 (For LX2160ARDB Rev 1) rcw/lx2160ardb_rev2/XGGFF_PP_HHHH_RR_19_5_2 (For LX2160ARDB Rev 2) Note: See the rcw/lx2160ardb/README or rcw/lx2160ardb_rev2/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make lx2160ardb_tfa_defconfig $ make Note: If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building the LSDK 18.12 and above U-Boot binary.             The compiled U-Boot binary, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OPTEE binary  You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-lx2160ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for SD/eMMC boot Clone the atf repository and compile the TF-A binaries, bl2_sd.pbl/bl2_emmc.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. For SD boot: $ make PLAT=lx2160ardb bl2 SPD=opteed BOOT_MODE=sd BL32=<path_to_optee_binary>/tee.bin pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin For eMMC boot: $ make PLAT=lx2160ardb bl2 SPD=opteed BOOT_MODE=emmc BL32=<path_to_optee_binary>/tee.bin pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin   The compiled BL2 images, bl2.bin and bl2_sd.pbl/bl2_emmc.pbl are available at atf/build/lx2160ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_sd.pbl/bl2_emmc.pbl binary needs to be recompiled.   To compile the BL2 binary without OPTEE: For SD boot: $ make PLAT=lx2160ardb bl2 BOOT_MODE=sd pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin    For emmc boot: $ make PLAT=lx2160ardb bl2 BOOT_MODE=emmc pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin  Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=lx2160ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/lx2160ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled.   To compile the FIP binary without OPTEE and without trusted board boot: For SD boot: $ make PLAT=lx2160ardb fip BOOT_MODE=sd BL33=<path_to_u-boot_binary>/u-boot.bin   For eMMC boot: $ make PLAT=lx2160ardb fip BOOT_MODE=emmc BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOO Step 5: Program TF-A binaries to SD/eMMC card Boot LX2160ARDB from FlexSPI. Ensure that the switches are set to boot the board from FlexSPI. For booting from FlexSPI: SW1[1:8] = 1111 100X [X is 0 for FlexSPI NOR flash0 and X is 1 for FlexSPI NOR flash1] SW2[1:8] = 0000 0110 SW3[1:8] = 1111 1100 SW4[1:8] = 1011 1000 Boot from FlexSPI NOR flash0: => qixis_reset For LX2160ARDB Rev 1, in boot log, you'll see: Board: LX2160ACE Rev1.0-RDB, Board version: B, boot from FlexSPI DEV#0 For LX2160ARDB Rev 2, in boot log, you'll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii [PRIME], DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id, e1000#0 Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. Note: See LX2160ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                                => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> => setenv gatewayIP <gateway IP> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.1.1 is alive Load TF-A binaries for SD boot from the TFTP server Note: For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Flash bl2_sd.pbl: => tftp 82000000 bl2_sd.pbl => mmc dev 0; mmc write 82000000 8 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load bl2_sd.pbl from the TFTP server, if the bytes transferred is 103353 (193b9 hex), then blk_cnt is calculated as "103353/512 = 201 (C9 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 10 (A hex) sectors, for this example, mmc write command will be: => mmc write 82000000 8 D3 Flash fip.bin: => tftp 82000000 fip.bin => mmc dev 0;  mmc write 82000000 800 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load fip.bin from the TFTP server, if the bytes transferred is 1178967 (11fd57 hex), then blk_cnt is calculated as "1178967/512 = 2302 (8FE hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 10 (A hex) sectors, for this example, mmc write command will be: =>  mmc write 82000000 800 908 Boot from SD card: => qixis_reset sd LX2160ARDB will boot with TF-A. In the boot log, you will see: => NOTICE: BL2: v1.5(release):LSDK-20.04 NOTICE: BL2: Built : 22:01:10, Aug 20 2020 NOTICE: UDIMM 18ADF2G72AZ-3G2E1 NOTICE: DDR4 UDIMM with 2-rank 64-bit bus (x8) NOTICE: 32 GB DDR4, 64-bit, CL=22, ECC on, 256B, CS0+CS1 NOTICE: BL2: Booting BL31 NOTICE: BL31: v1.5(release):LSDK-20.04 NOTICE: BL31: Built : 22:02:07, Aug 20 2020 NOTICE: Welc U-Boot 2019.10 (Aug 14 2020 - 17:43:28 +0530) SoC: LX2160ACE Rev2.0 (0x87360020) Clock Configuration: CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz CPU6(A72):2000 MHz CPU7(A72):2000 MHz CPU8(A72):2000 MHz CPU9(A72):2000 MHz CPU10(A72):2000 MHz CPU11(A72):2000 MHz CPU12(A72):2000 MHz CPU13(A72):2000 MHz CPU14(A72):2000 MHz CPU15(A72):2000 MHz Bus: 700 MHz DDR: 2900 MT/s Reset Configuration Word (RCW): 00000000: 50777738 24500050 00000000 00000000 00000010: 00000000 0c010000 00000000 00000000 00000020: 02e001a0 00002580 00000000 00000096 00000030: 00000000 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027000 00000000 00000070: 08b30010 00150020 Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from SD Load TF-A binaries for eMMC boot from the TFTP server Note: For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Flash bl2_emmc.pbl: => tftp 82000000 bl2_emmc.pbl => mmc dev 1; mmc write 82000000 8 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load bl2_emmc.pbl from the TFTP server, if the bytes transferred is 103353 (193b9 hex), then blk_cnt is calculated as "103353/512 = 201 (C9 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 10 (A hex) sectors, for this example, mmc write command will be: => mmc write 82000000 8 D3 Flash fip.bin: => tftp 82000000 fip.bin => mmc dev 1; mmc write 82000000 800 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load fip.bin from the TFTP server, if the bytes transferred is 1178967 (11fd57 hex), then blk_cnt is calculated as "1178967/512 = 2302 (8FE hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 10 (A hex) sectors, for this example, mmc write command will be: =>  mmc write 82000000 800 908 Boot from eMMC card: => qixis_reset emmc LX2160ARDB will boot with TF-A. In the boot log, you will see:   => NOTICE: BL2: v1.5(release):LSDK-20.04 NOTICE: BL2: Built : 22:01:10, Aug 20 2020 NOTICE: UDIMM 18ADF2G72AZ-3G2E1 NOTICE: DDR4 UDIMM with 2-rank 64-bit bus (x8) NOTICE: 32 GB DDR4, 64-bit, CL=22, ECC on, 256B, CS0+CS1 NOTICE: BL2: Booting BL31 NOTICE: BL31: v1.5(release):LSDK-20.04 NOTICE: BL31: Built : 22:02:07, Aug 20 2020 NOTICE: Welc U-Boot 2019.10 (Aug 14 2020 - 17:43:28 +0530) SoC: LX2160ACE Rev2.0 (0x87360020) Clock Configuration: CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz CPU6(A72):2000 MHz CPU7(A72):2000 MHz CPU8(A72):2000 MHz CPU9(A72):2000 MHz CPU10(A72):2000 MHz CPU11(A72):2000 MHz CPU12(A72):2000 MHz CPU13(A72):2000 MHz CPU14(A72):2000 MHz CPU15(A72):2000 MHz Bus: 700 MHz DDR: 2900 MT/s Reset Configuration Word (RCW): 00000000: 50777738 24500050 00000000 00000000 00000010: 00000000 0c010000 00000000 00000000 00000020: 02e001a0 00002580 00000000 00000096 00000030: 00000000 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027000 00000000 00000070: 08b30010 00150020 Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from eMMC  
記事全体を表示
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images for the LX2160ARDB on the SD/eMMC card.  Below steps are valid for both LX2160ARDB Rev 1.0 and Rev 2.0 revisions. Compiling MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/lx2160a/ $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-20.04 The prebuilt MC firmware image, mc_10.20.4_lx2160a.itb, is available at qoriq-mc-binary/lx2160a/. Note: The exact name of the MC firmware image may vary depending on the LSDK release version used.                  Compiling DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils/ $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-20.04 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc-usxgmii.dtb and dpl-eth.19.dtb images are available at /mc-utils/config/lx2160a/RDB/. Note: The exact name of the DPL and DPC images may vary depending on the LSDK release version used.             SD/eMMC card start block number for MC, DPL, and DPC images Image  SD/eMMC card start block number DPAA2 MC firmware 0x05000 = 20480 DPAA2 DPL  0x06800 = 26624 DPAA2 DPC 0x07000 = 28672   Refer the LSDK firmware and SD card start block number for complete listing of the SD card start block numbers for all LSDK firmware images.    Programming MC, DPC, and DPL images to SD/eMMC card Boot LX2160ARDB from FlexSPI. Ensure that the switches are set to boot the board from FlexSPI. SW1[1:8] = 1111 1000 SW2[1:8] = 0000 0110 SW3[1:8] = 1111 1100 SW4[1:8] = 1011 1000 Boot from FlexSPI NOR flash0: => qixis_reset For example: For LX2160ARDB, in U-Boot log, you’ll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id    Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. NOTE: See LX2160ARDB Ethernet Port Mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii  => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii  Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings.       => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.2.1 is alive  Load images from TFTP server Flash MC firmware (mc_10.20.4_lx2160a.itb): => tftp 82000000 mc_10.20.4_lx2160a.itb  Flash MC firmware to SD card: => mmc dev 0; mmc write 8200000 5000 <blk_cnt>  Flash MC firmware to eMMC card: => mmc dev 1; mmc write 8200000 5000 <blk_cnt> Here, blk_cnt refers to number of blocks in SD/eMMC card that need to be written as per the file size. For example, when you load mc_10.20.4_lx2160a.itb from the TFTP server, if the bytes transferred is 1092272 (10aab0 hex), then blk_cnt is calculated as "1092272 /512 = 2133 (855 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 10 (A hex) sectors, for this example, mmc write command will be:  => mmc write 82000000 5000 85F Flash DPAA2 DPL image. => tftp 82000000 dpl-eth.19.dtb Flash DPL image to SD card: => mmc dev 0; mmc write 8200000 6800 <blk_cnt>    Flash DPL image to eMMC card: => mmc dev 1; mmc write 8200000 6800 <blk_cnt> Here, blk_cnt refers to number of blocks in SD/eMMC card that need to be written as per the file size. For example, when you load dpl-eth.19.dtb from the TFTP server, if the bytes transferred is 4583 (11e7 hex), then blk_cnt is calculated as "4583/512 = 8 (8 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 18 (12 hex) sectors, for this example, mmc write command will be:  => mmc write 82000000 6800 12 Flash DPAA2 DPC image.    => tftp 82000000 dpc-usxgmii.dtb  Flash DPC image to SD card: => mmc dev 0; mmc write 8200000 7000 <blk_cnt> Flash DPC image to eMMC card: => mmc dev 1; mmc write 8200000 7000 <blk_cnt> Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load dpc-usxgmii.dtb from the TFTP server, if the bytes transferred is 736 (2e0 hex), then blk_cnt is calculated as "736/512 = 1 (1 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 11 (B hex) sectors, for this example, mmc write command will be:  => mmc write 82000000 7000 B Boot the board. Boot from SD card: => qixis_reset sd Boot from eMMC card: => qixis_reset emmc LX2160ARDB will boot with updated MC firmware and DPC and DPL images. In the U-Boot log, you will see:   Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from SD ... ... fsl-mc: Booting Management Complex ... SUCCESS fsl-mc: Management Complex booted (version: 10.20.4, boot status: 0x1) Hit any key to stop autoboot:  0 =>   OR   Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from eMMC ... ... fsl-mc: Booting Management Complex ... SUCCESS fsl-mc: Management Complex booted (version: 10.20.4, boot status: 0x1) Hit any key to stop autoboot:  0 =>
記事全体を表示
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images in FlexSPI NOR flash of LX2160ARDB. NOTE: Below steps are valid for both LX2160ARDB Rev 1.0 and Rev 2.0 revisions. NOTE: qixis_reset boots the board from FlexSPI NOR flash0 and qixis_reset altbank boots the board from FlexSPI NOR flash1. NOTE: sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from FlexSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program FlexSPI NOR flash1. Obtaining MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/lx2160a/ $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 The prebuilt MC firmware image, mc_10.20.4_lx2160a.itb, is available at /qoriq-mc-binary/lx2160a/. NOTE: The name of the MC firmware image may vary depending on the LSDK release version used.  Obtaining DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc-usxgmii.dtb and dpl-eth.19.dtb images are available at /mc-utils/config/lx2160a/RDB/. NOTE: The name of the DPC and DPL images may vary depending on the LSDK release version used.  Flashing MC firmware, DPC, and DPL images to FlexSPI NOR flash Boot LX2160ARDB from FlexSPI. Ensure that the switches are set to boot the board from FlexSPI. SW1[1:8] = 1111 1000 SW2[1:8] = 0000 0110 SW3[1:8] = 1111 1100 SW4[1:8] = 1011 1000 Boot from FlexSPI NOR flash0: => qixis_reset For example: For LX2160ARDB, in U-Boot log, you’ll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0   The images can be loaded to the LX2160ARB from a TFTP server or from a mass storage device (SD, USB, or SATA).   Option 1: Load image from the TFTP server   Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id  Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LX2160ARDB Ethernet Port Mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings.    => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.2.1 is alive   Load images from a TFTP server to FlexSPI NOR flash1 NOTE: Ensure that the board boots from FlexSPI NOR flash1 before programming updated MC firmware and DPL and DPC images to FlexSPI NOR flash1. If board fails to boot successfully from FlexSPI NOR flash1, you can program composite firmware image to FlexSPI NOR flash1 by following the steps available in section "LSDK Quick Start Guide or LX2160ARDB" in LSDK User Guide. Program FlexSPI NOR flash1: sf probe 0:1 Flash MC firmware: => tftp 0x80000000 mc_10.20.4_lx2160a.itb => print filesize => sf erase 0xa00000 +$filesize && sf write 0x80000000 0xa00000 $filesize Address 0xa00000 is the location of MC firmware in FlexSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image: => tftp 0x80000000 dpc-usxgmii.dtb => print filesize  => sf erase 0xe00000 +$filesize && sf write 0x80000000 0xe00000 $filesize Address 0xe00000 is the location of DPC image in FlexSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: => tftp 0x80000000 dpl-eth.19.dtb => print filesize  => sf erase 0xd00000 +$filesize && sf write 0x80000000 0xd00000 $filesize Address 0xd00000 is the location of DPL image in FlexSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1: => qixis_reset altbank In U-Boot log, you’ll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#1   Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in FlexSPI NOR flash.   Option 2: Load images from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on the storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 Program QSPI NOR flash1: => sf probe 0:1 Flash MC firmware: Load MC firmware image from the storage device => load mmc 0:2 80000000 <mc firmware> For example: => load mmc 0:2 80000000 mc_10.20.4_lx2160a.itb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize   Program MC firmware image to FlexSPI NOR flash: => sf erase 0xa00000 +$filesize && sf write 0x80000000 0xa00000 $filesize  Address 0xa00000 is the location of MC firmware in FlexSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: Load DPL image from the storage device => load mmc 0:2 80000000 <dpl image> For example: => load mmc 0:2 80000000 dpl-eth.19.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize   Program DPL image to FlexSPI NOR flash: => sf erase 0xd00000 +$filesize && sf write 0x80000000 0xd00000 $filesize  Address 0xd00000 is the location of DPL image in FlexSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout.   Flash DPC image: Load DPC image from the storage device => load mmc 0:2 80000000 <dpc image> For example: => load mmc 0:2 80000000 dpc-usxgmii.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize   Program DPC image to FlexSPI NOR flash: => sf erase 0xe00000 +$filesize && sf write 0x80000000 0xe00000 $filesize Address 0xe00000 is the location of DPC image in FlexSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from FlexSPI NOR flash1: => qixis_reset altbank In U-Boot log, you’ll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#1   Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in FlexSPI NOR flash.  
記事全体を表示
Follow these steps to update the Linux kernel image and device tree for LX2160ARDB on an SD card.  NOTE: Below steps are valid for both LX2160ARDB Rev 1.0 and Rev 2.0 revisions. STEP 1: Compiling Linux kernel images and device tree On Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-20.04-V5.4 LSDK-20.04-V5.4 where LSDK-20.04-V5.4 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to the device tree, open and edit arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-lx2160a-rdb.dtb is in arch/arm64/boot/dts/freescale/. STEP2: Copying the compiled kernel images and device tree to the SD card   Plug the SD card into the Linux host machine. sudo fdisk -l to list the disks that are accessible to the computer. Mount the SD card partition that contains Linux kernel images and device tree. sudo mkdir <mount_location> sudo mount /dev/sdX <mount_location> For example: $ sudo mkdir /carddata $ sudo mount /dev/mmcblk0p2 /carddata   NOTE: Use the command cat /proc/partitions to see the list of devices, their partitions along with their sizes to make sure that the correct device and partition name have been chosen. The eMMC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SD card directly without an extra SD card reader device, the device name of SD card is typically mmcblk0. In general, the Linux kernel images and device tree are stored in the second partition of the SD device (mmcblk0p2). For detail on storage layout on SD/eMMC/USB/SATA for LSDK images deployment, refer to section "LSDK memory layout and Userland" in Layerscape Software Development Kit User Guide. Replace Image, Image.gz, and fsl-lx2160a-rdb.dtb on the SD card with the new files compiled in the steps above. $ sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dtb <mount_location> For example: $sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dtb /carddata Unmount the card. For example: sudo umount /dev/mmcblk0p2 Plug the SD card into LX2160ARDB and boot the board. At U-Boot, run the following command to boot the board to LSDK distro using the SD card. => run bootcmd_mmc0 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
記事全体を表示
In the U-Boot log, the names of the Ethernet interfaces are printed in the format <name>@<interface type>, for example, DPMAC3@xgmii. DPMAC is a DPAA2 object that identifies the physical interface.    Interface name is not fixed in LX2160ARDB, depending upon which interface is active, name will be assigned  in TinyDistro as well as in Ubuntu distribution. Interface names can be checked using ls-listni command. root@TinyDistro:~# ls-listni dprc.1/dpni.1 (interface: eth0, end point: dpmac.2) dprc.1/dpni.0 (interface: eth1, end point: dpmac.17)   For details regarding creation of a DPAA2 network interface (DPNI) in Linux, see "LSDK Quick Start Guide for LX2160ARDB -> Bringing up DPAA2 network interfaces" in Layerscape Software Development Kit User Guide.   The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LX2160ARDB.    Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro) Port name in Linux (Ubuntu userland) Description 40G MAC2 DPMAC2@xlaui4 Interface name will be ethn, for example eth0, eth1. Eth0: If PCIe is connected, else it is any connected DPAA2 interface. PCIe: enp1s0   DPAA: ethx 40G MAC2 QSFP+ port 10G MAC3 DPMAC3@xgmii 10G MAC3 USXGMII port 10G MAC4 DPMAC4@xgmii 10G MAC4 USXGMII port 25G MAC5 DPMAC5@25g-aui 25G MAC5 SFP port 25G MAC6 DPMAC6@25g-aui 25G MAC6 SFP port 1G MAC17 DPMAC17@rgmii-id 1G MAC17 RGMII port 1G MAC18 DPMAC18@rgmii-id 1G MAC18 RGMII port  
記事全体を表示
On successful probing of the DSA Felix switch, each available front panel switch port should have a network device interface attached with the swpX name format. The ip link show command uses the swpX@enoY name format to also indicate the associated master Ethernet interface for the DSA switch port, which corresponds to an internal ENETC interface, usually the eno2 (Port2) for the LS1028A SoC. LS1028 Interface naming in Linux Single port mode Bridge mode
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344564 
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344236 
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343865 
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343717 
記事全体を表示