This how-to topic is applicable only for LSDK 18.09 and older releases.   For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries in QSPI NOR flash.   Follow these steps to update the U-Boot binary in QSPI NOR flash.   Prerequisites    Ubuntu 18.04 64-bit should be installed on the Linux host machine for building LSDK 18.06 or LSDK 18.09 U-Boot binary.     qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1.      sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1.       Compiling U-Boot binary  Clone the u-boot repository compile the U-Boot binary for QSPI boot.   $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git  $ cd u-boot  $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09   $ export ARCH=arm64  $ export CROSS_COMPILE=aarch64-linux-gnu-  $ make distclean  Run either of following depending on the board you are using:   For LS1088ARDB: $ make ls1088ardb_qspi_defconfig  For LS1088ARDB-PB: make ls1088ardb_pb_qspi_defconfig    If required, make changes to the U-Boot files.  $ make    If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.06 or LSDK 18.09 U-Boot binary.    The compiled U-Boot image, u-boot.bin, is available at u-boot/.    Flashing U-Boot binary to QSPI NOR flash   Boot LS1088ARDB/LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from the QSPI, SW1[1:8] + SW2[1] = 0011_0001_X  Boot from QSPI NOR flash0: => qixis_reset   For example:  For LS1088ARDB, in boot log, you’ll see:  Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0  For LS1088ARDB-PB, in boot log, you'll see:  Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0    U-Boot image can be loaded to LS1088ARDB/LS1088ARDB-PB from a TFTP server or from a mass storage device (SD, USB, or SATA).    Option 1: Load image from the TFTP server    Set up Ethernet connection  When board boots up, U-Boot prints a list of enabled Ethernet interfaces.  DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii   Set server IP to the IP of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1>    Set ethact and ethprime as the Ethernet interface connected to the TFTP server.   See LS1088ARDB/LS1088RDB-PB Ethernet port mapping  for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.   => setenv ethprime <name of interface connected to TFTP server>   For example:  => setenv ethprime DPMAC3@qsgmii  => setenv ethact <name of interface connected to TFTP server>  For example:  => setenv ethact DPMAC3@qsgmii   Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command. Static IP address assignment:  => setenv ipaddr <ipaddress2>  => setenv netmask <subnet mask>  Dynamic IP address assignment:  => dhcp   Save the settings. => saveenv  Check the connection between the board and the TFTP server.   => ping $serverip  Using DPMAC3@qsgmii device  host 192.168.1.1 is alive    Load U-Boot image from the TFTP server   Program QSPI NOR flash1: => sf probe 0:1   Flash U-Boot image:   => tftp 0xa0000000 u-boot.bin  => print filesize   filesize=aa4b4     Program U-Boot image to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize.  Address 0x100000 is the location of U-Boot in QSPI NOR flash. For the complete flash memory layout for the PPA boot flow, refer Flash layout for old boot flow with PPA.   Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see:  Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1  For LS1088ARDB-PB, in boot log, you'll see:  Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1  Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.    Option 2: Load image from partition on mass storage device (SD, USB, or SATA)   Select mass storage device to use. => mmc rescan  => mmc info  Or  => usb start
=> usb info  Or  => scsi scan  => scsi info    Optional – List files on storage device => ls mmc <device:partition>  For example:  => ls mmc 0:2  Or  => ls usb <device:partition>  For example:  => ls usb 0:1  Or  => ls scsi <device:partition>  For example:  => ls scsi 0:2   Program QSPI NOR flash1: => sf probe 0:1  Load U-Boot image from the storage device => load mmc 0:2 a0000000 <image name>  => print filesize  For example:  => load mmc 0:2 a0000000 u-boot.bin  => print filesize  filesize=aaa34  Or  => load usb 0:2 a0000000 <image name>  => print filesize  Or  => load scsi 0:2 a0000000 <image name>  => print filesize    Program image to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize  Address 0x100000 is the location of U-Boot in QSPI NOR flash. For the complete flash memory layout for the PPA boot flow, refer Flash layout for old boot flow with PPA.   Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see:  Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1  For LS1088ARDB-PB, in boot log, you'll see:  Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1  Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.       
        
        記事全体を表示