Layerscape ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layerscape Knowledge Base

ディスカッション

ソート順:
This document introduces porting TDM Linux driver working in internal loopback mode to do verification during custom boards bringing up and verification stage. 1. TDM Interface Configuration to Support Internal Loopback Mode 2. Modify Linux Kernel Driver to Make TDM Working in Internal Loopback Mode 3. Build TDM Driver into Linux Kernel and do verification on the target board
記事全体を表示
This how-to topic is applicable for only LSDK 18.09 and older releases. Follow these steps to update the U-Boot binary in QSPI NOR flash.  Prerequisites  Ubuntu 18.04 64-bit should be installed on the Linux host machine for building LSDK 18.06 or LSDK 18.09 U-Boot binary. cpld reset boots the board from QSPI NOR flash0 and cpld reset altbank boots the board from QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1.   Compiling U-Boot binary Clone the u-boot repository. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make ls1046ardb_qspi_defconfig If required, make changes to the U-Boot files. $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.06 or LSDK 18.09 U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available in the directory u-boot/. Flashing U-Boot binary to QSPI NOR flash U-Boot image can be loaded to LS1046ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Boot LS1046ARDB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI, SW5[1:8] = 00100010 Boot from QSPI NOR flash0: => cpld reset In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 0 Set up Ethernet connection When the board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1, FM1@TGEC2 Set server IP to the IP of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1046ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command. Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive Load U-Boot image from the TFTP server Program QSPI NOR flash1: => sf probe 0:1 Flash U-Boot image: => tftp 0xa0000000 u-boot.bin => print filesize filesize=ae84a Program U-Boot image to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Address 0x100000 is the location of U-Boot in QSPI NOR flash.  Refer Flash layout for boot flow with PPA – LSDK 18.09 and older releases for the complete flash memory layout. Boot from QSPI NOR flash1: => cpld reset altbank In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 4 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Boot LS1046ARDB from QSPI NOR flash. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI, SW5[1:8] = 00100010 Boot from QSPI NOR flash0: => cpld reset In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 0 Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:3 System Volume Information/ 714826 u-boot.bin 1 file(s), 1 dir(s) Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in QSPI NOR flash0 supports the command by typing ls at the U-Boot prompt: => ls ls - Lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in QSPI NOR flash0. For steps to update composite firmware image in QSPI NOR flash, see LS1046ARDB - How to update composite firmware image in QSPI NOR flash. Program QSPI NOR flash1: => sf probe 0:1 Load U-Boot image from the storage device. => load mmc <device:partition> a0000000 <image name> => print filesize For example: => load mmc 0:3 a0000000 u-boot.bin 714826 bytes read in 52 ms (13.1 MiB/s) => print filesize filesize=ae84a Or => load usb <device:partition> a0000000 <image name> => print filesize Or => load scsi <device:partition> a0000000 <image name> => print filesize Program U-Boot image to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Address 0x100000 is the location of U-Boot in QSPI NOR flash.  Refer Flash layout for boot flow with PPA – LSDK 18.09 and older releases for the complete flash memory layout. Boot from QSPI NOR flash1: => cpld reset altbank In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 4 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
記事全体を表示
OpenWrt is a highly extensible GNU/Linux distribution for embedded devices (typically wireless routers), OpenWrt is built from the ground up to be a full-featured, easily modifiable operating system for your router. LEDE is based on OpenWrt, targeting a wide range of wireless SOHO routers and non-network device. This document introduces how to porting and running OpenWrt/LEDE on QorIQ LS1012/LS1043 platform. 1. Porting OpenWrt/LEDE Source on QorIQ Layerscape Platforms 2. Deploy OpenWrt/LEDE Images to Boot up the System 3. Verify VLAN Interface and PFE in LEDE System
記事全体を表示
The integrated flash controller (IFC) is used to interface with external asynchronous/synchronous NAND flash, asynchronous NOR flash, SRAM, generic ASIC memory and EPROM. This document introduces how to configure IFC controller on QorIQ LS, T and P series custom boards, uses LS1043 custom board integrating NAND Flash MT29F64G08CBCBBH1 as an example to demonstrate IFC flash timing parameters calculation and control registers configuration, CodeWarrior initialization file customization and u-boot source code porting. 1. IFC Memory Mapped Registers Introduction 2. Calculate IFC Flash Timing Values and Configure Control Registers 3. Customize CodeWarrior Initialization File with the Calculated IFC Timing 4. Porting U-BOOT Source with the Calculated IFC Timing
記事全体を表示
The attached patch is to support DDR3L in LS1043A. The SDK version is Linux-LS1043A-SDK-V0.5-SOURCE-20151223-yocto.iso. Not SDK2.0. The DDR3L part number is two Winbond W632GU6KB(16M x 8 banks x 16 bits DDR3L SDRAM).
記事全体を表示
The attached patch is to support Aquantia AQR107 in LS1043A.
記事全体を表示
This document introduces basic concept of Power Management, LS1028 RCW configuration to enable GPIO, Linux Kernel source and device tree modification to support GPIO wakeup, Kernel configuration to enable sleep feature and GPIO wakeup driver, export GPIO pin and enable interrupt, Order system to sleep and trigger GPIO interrupt to wake up the system.
記事全体を表示
QorIQ LSDK is NXP new generation of SDK for Layerscape productions, consists of a set of disaggregated components based on Linux distributions, meets market demand to more Linux distributions of more types, and satisfy the requirement from a wide variety of customers. In LSDK we use Flexbuild to build all packages from LSDK, make root filesystem and generate the installer. This document introduces the basic concept of LSDK, comparison between LSDK and Yocto SDK, how to use LSDK, plan and roadmap of LSDK. 1. Basic Concept of LSDK 1.1 LSDK Specific features 1.2 LSDK Components 1.3 LSDK Images Memory Map 2. Comparison Between Layerscape SDK and QorIQ Yocto SDK 3. How to Usage LSDK 3.1 LSDK Flexbuild Utility 3.2 Build LSDK using Flexbuild 3.3 Deploy LSDK Images on the Target Board 3.4 Add a Package using Flexbuild 4. Layerscape SDK Roadmap
記事全体を表示
This how-to topic is applicable only to LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer Deploying TF-A binaries in Layerscape Software Development Kit <version> Documentation. Follow these steps to update the PBL/RCW binary on the SD card.  Compiling PBL binary from RCW source file (optional) If the user already has a PBL binary, this step can be skipped.   Clone the  rcw  repository and compile the PBL binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09  $ cd ls1046ardb If required, make changes to the rcw files. $ make   The default PBL binary for LS1046ARDB is RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin.swapped. By default, the QSPI controller on LS1046A reads/writes in 64-bit big endian (BE) mode. This makes it necessary to use a byte swapped PBL binary image, for example, rcw_1800_qspiboot.bin.swapped. The last PBI command in rcw_1800_qspiboot.bin.swapped is a write to the QPSI_MCR register that changes the endianness of QSPI controller to 64-bit little endian (LE). With this change, subsequent accesses are made in little endian format. See the rcw/ls1046ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. SD card start block number for PBL/RCW binary Image  SD card start block number PBL/RCW binary 0x00008 = 8 Refer the Flash layout for boot flow with PPA – LSDK 18.09 and older releases for a complete listing of the SD card start block numbers for all LSDK firmware images.   Programming PBL/RCW binary to SD card Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=rcw_1800_qspiboot.bin.swapped of=/dev/sdX bs=512 seek=8 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.                     Remove the SD card from the Linux host machine. Plug the SD card into LS1046ARDB and boot the board to Ubuntu using the SD card. You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 01001110 and SW5 [1:8] = 00100000, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1046ARDB, boot from SD If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
記事全体を表示
On the LX2160ARDB, there are 2 25G SFP interfaces, but no 10G SFP interface. When customer want to test the 10G SFPs to evaluate the performance, they have to change the 25G SFP interfaces into 10G by reconfiguration the SW configuration. In this document, it will give details of configuring the LX2160ARDB to support the customer’s 10G SFP interfaces requirement with LSDK2108. At the end, an image will be generated to deployed into the SD card. Because SD card is a convenient way boot up LX2160ARDB, if one wrong move could brick the system, the customer could unplug the SD card to repeat the steps below.
記事全体を表示
The BareMetal framework targets to support the scenarios that need low latency, real-time response, and high-performance. There is no OS running on the cores and customer-specific application runs on that directly. This document describes how to develop customer-specific application based on BareMetal framework. The directory “app” stored in u-boot repository includes the use cases for testing GPIO, I2C, IRQ init, QSPI, Ethernet, USB, PCIe, CAN, ENETC and SAI features. 1. GPIO use case 2. I2C use case 3. IRQ use case 4. QSPI Use case 5. Ethernet use case 6. USB Use case 7. PCIe use case 8. CAN Use Case 9. ENETC Use Case 10. SAI Use Case 11. Build and Run the Baremetal Application
記事全体を表示
PCI-Express introduction PCIe Device Type And Topology PCIe system architecture          2.1 Transaction Layer          2.2 Data link layer          2.3 Physical Layer Interrupts Mechanism PCIe enumeration and resource assignment
記事全体を表示
On successful probing of the DSA Felix switch, each available front panel switch port should have a network device interface attached with the swpX name format. The ip link show command uses the swpX@enoY name format to also indicate the associated master Ethernet interface for the DSA switch port, which corresponds to an internal ENETC interface, usually the eno2 (Port2) for the LS1028A SoC. LS1028 Interface naming in Linux Single port mode Bridge mode
記事全体を表示
  The below steps are used to update composite firmware image in FlexSPI NOR flash and SD/eMMC card using an SD card. Load composite firmware image on SD card Option 1: Using HxD editor on Windows system Option 2: Using Linux system Program updated composite firmware in SD card Program updated composite firmware in FlexSPI NOR flash (DEV#0 and DEV#1) Program updated composite firmware in eMMC card NOTE: Examples shown below use the LX2160ARDB Rev 2 image names. The same examples are applicable for LX2160ARDB Rev 1 also by replacing the Rev 2 image name with the corresponding Rev 1 image name. Step 1: Load composite firmware image in SD card Option 1: Using HxD editor on Windows system The below steps describe how to use an HxD editor on a Windows machine to program firmware image on SD card without partitioning the card. NOTE: Use the following link to download the HxD editor for Windows: https://mh-nexus.de/en/hxd/. Download composite firmware image on Windows machine using the following links: For LX2160ARDB Rev1: For SD boot: https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_uboot_sdboot.img For FlexSPI boot: https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_uboot_xspiboot.img For eMMC boot: https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_uboot_emmcboot.img For LX2160ARDB Rev 2: For SD boot: https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_sdboot.img For FlexSPI boot: https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_xspiboot.img For eMMC boot: https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_emmcboot.img Format SD card. Open HxD editor and run as administrator. Open firmware_lx2160ardb_rev2_uboot_sdboot.img binary file in HxD editor. Copy the binary file (CTRL + A and CTRL + C). Plug the SD card either directly into the slot available on your Windows machine or using a memory card adapter/reader. Open disk (SHIFT + CTRL +D). Open disk NOTE: Uncheck the 'Open as Readonly' option while opening the disk. Go to SD block (or sector) 8 (0x1000). HxD Editor - Sector 8 Paste the copied binary image content (CTRL + B). Make sure to copy the image at SD block no. 8. Save the content. Repeat above steps to load firmware_lx2160ardb_rev2_uboot_xspiboot.img and firmware_lx2160ardb_rev2_uboot_emmcboot.img binary image in SD card. For example: Load firmware_lx2160ardb_rev2_uboot_xspiboot.img image in SD card at block no. 150500 and firmware_lx2160ardb_rev2_uboot_emmcboot.img image in SD card at block no. 300500. NOTE: Make sure that you load these images in SD blocks so that the images do not get overwrite. Eject the SD card. Option 2: Using Linux system Download composite firmware image on Linux machine using the following links: For LX2160ARDB Rev1: For SD boot: $ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_uboot_sdboot.img For FlexSPI boot: $ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_uboot_xspiboot.img For eMMC boot: $ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_uboot_emmcboot.img For LX2160ARDB Rev 2: For SD boot: $ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_sdboot.img For FlexSPI boot: $ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_xspiboot.img For eMMC boot: $ wget https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_emmcboot.img Format SD card (optional, required if the card already has some data so to ensure that images have been loaded to card without conflicting with the existing data). Load composite firmware image to SD card. For SD boot: dd if=firmware_lx2160ardb_rev2_uboot_sdboot.img of=/dev/sdb bs=512 seek=8 For FlexSPI boot: dd if=firmware_lx2160ardb_rev2_uboot_xspiboot.img of=/dev/sdb bs=512 seek=150500 For eMMC boot: dd if=firmware_lx2160ardb_rev2_uboot_emmcboot.img of=/dev/sdb bs=512 seek=300500 Eject the SD card. Step 2: Program updated composite firmware in SD card NOTE: Since the updated composite firmware is now available at required block (SD start block no. 😎 in SD card, therefore, you can boot the board using SD card using following steps. Insert the SD card in SD slot of LX2160ARDB. Set switch settings to boot from SD card : SW1[1:4] = 1000  Restart the board. The board boots from updated composite firmware (SD boot) image loaded in the SD card. The U-Boot log displays: Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from SD Step 3: Program updated composite firmware in FlexSPI NOR flash (DEV#0 and DEV#1) Insert the SD card in SD slot of LX2160ARDB. Set switch settings to boot from SD card=> SW1[1:4] = 1000 Restart the board and stop at U-Boot prompt. Load firmware_lx2160ardb_rev2_uboot_xspiboot.img at 0xa0000000 (DDR address) using the following command: => mmc read 0xa0000000 <start_block_number> <block_count> where, <start_block_number> - start block number in SD card where you have loaded the firmware. For example, if you have loaded firmware at SD card block 150500, start_block_number in hex is 24be4 <block_count> - number of blocks in SD card that needs to be read as per the file size. It is calculated as ‘file size /512’ + ‘few sectors for rounding up so that last block is not missed’. If firmware file size is 52158124 (31bdeac hex), block_count is 52158124/512 = 101871 (18DEF hex) + 10 (A hex) = 101881 (18DF9 hex). For example: => mmc read 0xa0000000 24be4 18DF9 Program default FlexSPI NOR flash: =>sf probe 0:0 =>sf update 0xa0000000 0x0 <firmware_lx2160ardb_rev2_uboot_xspiboot.img _filesize_in_hex> For example: => sf update 0xa0000000 0x0 31BDEAC    Program alternate FlexSPI NOR flash: => sf probe 0:1 => sf update 0xa0000000 0x0 <firmware_lx2160ardb_rev2_uboot_xspiboot.img _filesize_in_hex>  Restart the board to boot from FlexSPI NOR flash 0 (DEV#0). Switch settings to boot from DEV#0: SW1[1:8] = 1111 1000 The U-Boot log shows the following message: Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0 Restart the board to boot from FlexSPI NOR flash 1 (DEV#1) as well. Switch settings to boot from DEV#1 SW1[1:4] = 1111 1001  The U-Boot log shows the following message: Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#1 Step 4: Program updated composite firmware in eMMC card Insert the SD card in SD slot of LX2160ARDB. Set switch settings to boot from SD card: SW1[1:4] = 1000 Restart the board and stop at U-Boot prompt. Load firmware_lx2160ardb_rev2_uboot_emmcboot.img at 0xa0000000 (DDR address) using the following command: => mmc dev 0; mmc read 0xa0000000 <start_block_number> <block_count> where, <start_block_number> - start block number in SD card where you have loaded the firmware. For example, if you have loaded firmware at SD card block 300500, start_block_number in hex is 495D4 <block_count> - number of blocks in SD card that needs to be read as per the file size. It is calculated as ‘file size /512’ + ‘few sectors for rounding up so that last block is not missed’. If firmware file size is 52158124 (31bdeac hex), block_count is 52158124/512 = 101871 (18DEF hex) + 10 (A hex) = 101881 (18DF9 hex). For example: => mmc read 0xa000000 495D4 18DF9 Program eMMC card. => mmc dev 1; mmc write 0xa0000000 8 18DF9 Restart the board to boot from eMMC. Set switch settings to boot from eMMC card. SW1[1:8] = 1001 1000 The U-Boot log shows the following message: Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from eMMC
記事全体を表示
Getting RCW image: Getting UEFI image:                              Getting PPA image: Getting Linux kernel and DTB, and Root FS images: - Download Image , fsl-ls1043a-uefi-rdb.dtb and fsl-image-core-ls1043ardb.ext2.gz . - Copy Image and fsl-image-core-ls1043ardb.ext2.gz to the TFTP server directory. Getting GRUB2 image for AARCH64 and sample GRUB configuration: - Download grub image from this location. - Download sample grub configuration from here . Placing GRUB image on FAT formatted SD card: Install FAT32 file system on SD card - Use the DISKPART utililty on windows command prompt to format a SD card with FAT32 file system. Use the following snapshot for reference - Copy grubaa64.efi and ls1043a-grub.cfg to the SD card. Booting to UEFI prompt on LS1043a RDB Board: Boot to u-boot prompt from NOR flash bank 0 on LS1043a RDB.  Setup serial port connection on host machine, to capture logs from the target LS1043a RDB board.. Reset the board to boot u-boot on bank 0, assuming that there is a valid u-boot image flashed on the primary bank 0. Copy Images to NOR flash alternate bank using u-boot commands sete uefi 'tftp 80000000 LS1043ARDB_EFI.fd; erase 0x64400000 0x644FFFFF ; cp.b 80000000 0x64400000 $filesize' sete rcw 'tftp 80000000 rcw_uefi_1500.bin; erase 0x64000000 0x640FFFFF ; cp.b 80000000 0x64000000 $filesize' sete ppa 'tftp 80000000 ppa.itb; erase 0x64500000 0x645FFFFF ; cp.b 80000000 0x64500000 $filesize' sete dtb 'tftp 80000000 fsl-ls1043a-uefi-rdb.dtb; erase 0x65B00000 0x65BFFFFF; cp.b 80000000 65B00000 $filesize' run uefi run ppa run rcw run dtb Note: The host machine is assumed to be having tftp server running, with the relevant files in place. The rcw, uefi, dtb and ppa images can also be found at compass link shared above. Note: Make sure SD card is inserted into the SD card slot on the board. Reset RDB to boot from NOR flash bank 4 => cpld reset altbank You should get UEFI boot prompt, as shown in the image below. Enter 2 to load Shell. On the Shell prompt run the following commands Shell> FS0:   Shell> ls You should see a list of the grub executable and configurations files present on SD card. Booting Linux via PXE on LS1043a RDB: Note: atftpd or tftpd-hpa, is required as tftp server for PXE boot to work. tftpd is not supported.  Load grub by entering the name of the grub executable. Shell> grubaa64.efi On the grub prompt, setup the server and client IPs for TFTP transfer. grub> set net_default_server=<server_ip> grub> net_add_addr eno0 efinet0 <client_ip> Load the grub configuration. grub> configfile (hd3,msdos1)/ls1043a-grub.cfg Grub menu is listed. Choose the entry for liinux boot. See the snapshot below for reference. Linux boot should start in around 7-8 minutes. Data transfer speed is around 100 KB/s.
記事全体を表示
Follow these steps to update the Linux kernel image and device tree on the SD card.  Compiling Linux kernel images and device tree On Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-19.06-V4.14 LSDK-19.06-V4.14 where LSDK-19.06-V4.14 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to the device tree, open and edit arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-ls1043a-rdb.dtb is in arch/arm64/boot/dts/freescale/. Copying the compiled kernel images and device tree to the SD card Plug the SD card into the Linux host machine. Mount the SD card partition that contains Linux kernel images and device tree. sudo mkdir <mount_location> sudo mount /dev/sdX <mount_location> Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/ sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0. Replace Image, Image.gz, and fsl-ls1043a-rdb.dtb on the SD card with the new files compiled in the steps above. sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb.dtb <mount_location> sudo umount /dev/sdX Plug the SD card into LS1043ARDB and boot the board to Ubuntu using the SD card.  If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card. You can confirm that Linux kernel and device tree is updated on the SD card by running this command and checking the timestamp. root@localhost:~# uname -a Linux localhost 4.14.104 #2 SMP PREEMPT Wed Aug 21 17:14:01 IST 2019 aarch64 aarch64 aarch64 GNU/Linux
記事全体を表示
IEEE Std 1588 standard is for a precision clock synchronization protocol for networked measurement and control, define a Precision Time Protocol (PTP) designed to synchronize real-time clocks in a distributed system. This document introduces IEEE 1588 related basic concept and Precision Time Protocol, hardware assist for 1588 compliant time stamping on QorIQ  LS1021 platform, Linux Kernel PTP framework device driver implementation working with ptpd stack, IEEE 1588 test setup on LS1021ATSN platform and results. IEEE 1588 Introduction and Precision Time Protocol Hardware Assist for 1588 Compliant Time Stamping on QorIQ LS1021 Platform      2.1 Accessing Timer Registers      2.2. Time-Stamping on Ethernet Frame Reception for eTSEC      2.3. Time-Stamping on Ethernet Frame Transmission for eTSEC IEEE 1588 PTP Linux Device Driver and PTPd Application     3.1 IEEE 1588 Linux Software Structure     3.2 IEEE 1588 Linux Device Driver 3.3 PTPd Application Setup IEEE 1588 test on LS1021ATSN Platform    4.1 Build Images with OpenIL    4.2 Setup IEEE 1588 test environment on LS1021ATSN    4.3 Test result
記事全体を表示
Follow these steps to update the Linux kernel image and device tree on the SD card.  Compiling Linux kernel images and device tree On the Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-18.09-V4.14 LSDK-18.09-V4.14 where LSDK-18.09-V4.14 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to device tree, open and edit arch/arm64/boot/dts/freescale/fsl-ls1046a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-ls1046a-rdb.dtb is in arch/arm64/boot/dts/freescale/. Copying the compiled kernel images and device tree to SD card Plug the SD card into the Linux host machine. List the disks that are accessible to the computer: $ cat /proc/partitions Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen.  The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced.  If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0. Mount the SD card partition that contains Linux kernel images and device tree: $ sudo mount /dev/sdX  <mount_location> Replace Image, Image.gz, and fsl-ls1046a-rdb.dtb on the SD card with the new files compiled in the steps above. sudo cp linux/arch/arm64/boot/Image linux/arch/arm64/boot/Image.gz linux/arch/arm64/boot/dts/freescale/fsl-ls1046a-rdb.dtb <mount_location> sudo umount /dev/sdX Plug the SD card into LS1046ARDB and boot the board to Ubuntu using the SD card: => cpld reset sd In boot log, you’ll see: Board: LS1046ARDB, boot from SD If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
記事全体を表示
This how-to topic is applicable only to LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries on SD card. Follow these steps to update U-Boot binary on the SD card.  Prerequisites  Ubuntu 18.04 64-bit should be installed on the Linux host machine for building LSDK 18.06 or LSDK 18.09 U-Boot binary.   Compiling U-Boot binary Clone the u-boot repository. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean Execute appropriate defconfig file: For LS1088ARDB: $ make ls1088ardb_sdcard_qspi_defconfig For LS1088ARDB-PB: $ make ls1088ardb_pb_sdcard_qspi_defconfig If required, make changes to the U-Boot files. $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.06 or LSDK 18.09 U-Boot binary.  The compiled U-Boot image, u-boot-with-spl.bin, is available at u-boot/. SD card start block number for U-Boot binary Image  SD card start block number U-Boot binary 0x00800 = 2048 Refer the Flash layout for boot flow with PPA – LSDK 18.09 and older releases for a complete listing of the SD card start block numbers for all LSDK firmware images.     Programming U-Boot binary to SD card Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=u-boot-with-spl.bin of=/dev/sdX bs=512 seek=2048 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/ sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.    Remove the SD card from the Linux host machine. On the LS1088ARDB/LS1088ARDB-PB, ensure that the switches are set to boot the board from SD card.  For booting from SD card, SW1[1:8] + SW2[1] = 0010_0000_0  Plug the SD card into the board and boot the board to Ubuntu. If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
記事全体を表示
Follow these steps to update the DPAA1 FMan ucode image on the SD card.  Obtaining DPAA1 FMan ucode image Clone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/qoriq-fm-ucode.git $ cd qoriq-fm-ucode $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-19.06 The prebuilt FMan ucode images, fsl_fman_ucode_ls1043_r1.1_<microcode version>.bin, are at qoriq-fm-ucode/. In the binary file, ls1043_r1.1 refers to the LS1043A silicon revision 1.1. See qoriq-fm-ucode/readme for a description of the ucode version numbers. SD card start block number for DPAA1 FMan ucode image Image  SD card start block number DPAA1 FMan ucode image 0x04800 = 18432 Refer Flash layout for new boot flow with TF-A for complete listing of the SD card start block numbers for all LSDK firmware images. Programming DPAA1 FMan ucode image to SD card Option 1: Load image on SD card plugged into Linux host via dd command Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin of=/dev/sdX bs=512 seek=18432 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.                                                   Remove the SD card from the Linux host machine. Plug the SD card into LS1043ARDB and boot the board to Ubuntu using the SD card. You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 10110011, SW4 [1:8] =00100000 , SW5 [1:8] = 00100010, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1043ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card. Option 2: Load image on SD card plugged into board from the TFTP server Boot LS1043ARDB from NOR flash. Ensure that the switches are set to boot the board from NOR bank 0. For booting from NOR bank 0, switch settings are as follows: SW3[1:8] = 10110011 SW4[1:8] = 00010010 SW5[1:8] = 10100010 Boot from NOR bank 0: => cpld reset For LS1043ARDB, in boot log, you'll see: Board: LS1043ARDB, boot from vBank 0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5 Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1043ARDB Ethernet and FMC port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                        => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive Load FMan ucode image from the TFTP server Flash the FMan ucode image: => tftp 0xa0000000 fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin Program the FMan ucode image to SD card: => mmc write 0xa0000000 0x04800 <blk_cnt> Address  0x04800 is the SD card block number for the FMan ucode image.  ReferFlash layout for new boot flow with TF-A for the complete flash memory layout. Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load FMan ucode from the TFTP server, if the bytes transferred is 37560 (92b8 hex), then blk_cnt is calculated as "37560/512 = 73 (49 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 5 (5 hex) sectors, for this example, mmc write command will be: => mmc write 0xa0000000 0x04800 4E You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 10110011, SW4 [1:8] =00100000 , SW5 [1:8] = 00100010, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1043ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card.
記事全体を表示