On the LX2160ARDB, there are 2 25G SFP interfaces, but no 10G SFP interface. When customer want to test the 10G SFPs to evaluate the performance, they have to change the 25G SFP interfaces into 10G by reconfiguration the SW configuration.
In this document, it will give details of configuring the LX2160ARDB to support the customer’s 10G SFP interfaces requirement with LSDK2108. At the end, an image will be generated to deployed into the SD card. Because SD card is a convenient way boot up LX2160ARDB, if one wrong move could brick the system, the customer could unplug the SD card to repeat the steps below.