Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
This is a presentation used to explain the Low Power Timer adapted by Vicente Gómez, Freescale TIC. LPTMR Module Explanation. Connection Diagram. Operation Modes Hands-On Configure a timer so that it generates an interruption every x time.  Explicación del Low Power Timer presentado por Vicente Gómez, Freescale TIC.- Explicación de los Modulos LPTMR . Diagrama de conexiones. Modos de operación Hands-on Configurar un timer para que genere una interrupción cada X tiempo.
記事全体を表示
Ezportdl:programming Kinetis EZport by MCU-Link Pro NXP launched MCU-Link Pro at the end of 2021. This is a new debugger probe that has been significantly upgraded based on mcu-link. The focus of the upgrade is to add current measurement, analog signal monitoring, USB to SPI and I2C bridge working modes, and on-board lpc804 for peripheral simulation. Among these upgrades, USB to SPI and I2C are more interesting and practical. Combining Kinetis EZport and flashloader, MCU-Link Pro can directly download programs to the target chip, instead of bridge through another board as before. This project uses the USB to SPI function of MCU-Link Pro to download programs to kinetis K series chips through EZport. In addition to the Kinetis series, many ColdFire chips of NXP also support EZport. In addition, since EZport interface protocol is compatible with SPI NOR flash, this project can also directly burn SPI NOR flash chip. This can also be used when debugging or producing i.mxRT500 and i.mxRT600. MCU Link Pro can easily use USB to SPI and I2C interfaces because NXP provides LIBUSBSIO library. Readers can download this library and related documents from NXP's official website. Here is a brief introduction. The SUB to SIO function is only an optional additional function for lpclink2 and MCU-Link Pro devices. Its main function is to provide CMSIS-DAP debugging interface for the target microcontroller, and provide virtual serial communication using USB VCOM class. The following figure is the process framework of LIBUSBSIO. As shown in the figure, LIBUSBSIO library can support SPI, I2C and GPIO. jingpan_0-1664530783351.png   The core of LIBUSBSIO communication is SPI_Transfer (lpc_handle hspi, spi_xfer_t * xfer) function. This function can send and receive 1024 bytes at most at one time. In addition, LIBUSBSIO library can set baud rate, clock polarity, sampling edge, and frame length. The following figure shows the output waveform captured by the logic analyzer. jingpan_1-1664530783624.jpeg   Command Description WREN Write Enable WRDI Write Disable RDSR Read Status Register READ Flash Read Data SP Flash Section Program SE Flash Sector Erase BE Flash Bulk Erase RESET Reset Chip WRFCCOB Write FCCOB Registers dl Image download fw Write/read any sequence to SPI port   This project has been tested on FRDM-K64F. jingpan_2-1664530783652.png    Hardware connection: MCU-Link pro            FRDM-K64F J19-2        ---       R75-1(flying a line is needed) J19-3        ---       J1-8 J19-4        ---       J11-1 J19-5        ---       J1-12    Connect ground together.   Operation steps: Before power on, R75-1 should be connected to ground, then connect openSDA USB. Thus, K64 will enter EZport status. Read memory ezportdl read [address] [number] jingpan_3-1664530783697.png   Write enable ezportdl wren Write flash, which can write up to 1000 byte. ezportdl sp [length] [data] jingpan_4-1664530783725.png   Program a binary file into flash Ezportdl dl [address] [file name] [flag]  address means start address flag=0 means erase flash before programming, flag=1 means don’t erase the flash.     Project download address: https://github.com/jophpan/ezportdl/tree/master  
記事全体を表示
Explore the Features of MCU-Link Pro MCU-Link Pro is the latest ARM Cortex-M series core debugger tool from NXP. Some of its features are inherited from the past LPC-LINK2. But overall it was redesigned and introduced and many new features. These additional functions make the MCU-Link Pro a very powerful debugging tool. This article will explore these features and highlight interesting and useful ones. These functions mainly include the following aspects. SWD+SWO Measurement of current and power consumption MCU-Link pro is supported by new blhost LIBUSBSIO library for windows, Ubuntu Linux and MacOS A secondary chip LPC804 on the board   SWD+SWO MCU-Link Pro support SWD only. It doesn’t support JTAG. The main controller in the board is LPC55S69. There is level shifter circuit between the port and LPC55S69. It makes the board can debug the target board work at 1.2V to 5V. It has reference voltage trace circuit which is use to trace the target board voltage. It can trace the port automatically, needn’t any settings. The MCU-Link Pro also can supply 1.8V/3.3V to target board. The maximum current is 350mA. This is done by connecting J6 and selecting by J5. The maximum speed of SWO is 9.6Mbit/s. Same as <PC-Link, MCU-Link Pro support CMSIS-DAP and Jlink firmware. These firmware are kept updating. The latest firmware of CMSIS-DAP is 2.25. If the firmware version is old, there will be a message jump out telling customer to update it when connecting to computer. We can see that the new version gives two VCOM while the original version only have one. The new VCOM use J26-4 and J26-5. jingpan_0-1664529871686.png   Measurement of current and power consumption MCU-Link pro provides a very interesting real-time function of current and voltage measurement. It can capture a burst of samples of target current usage, the target supply voltage, the shield current, the analog input, the debug interface reference voltage, or target power consumption at up to 100ksps. This information is displayed in a graph and can also be exported for further analysis. The average value of the collected data can also be displayed. And based on the current and voltage data, the power consumption can also be calculated and displayed in the graph. The place where the red line is drawn in the figure below is the real-time voltage at the time point of the mouse. jingpan_1-1664529871909.png     What's more interesting is that the energy measurement function does not need to activate the debug to capture the data, it is offline and has a separate data channel. But it can also be linked to a session if such a debug session exists. This is very useful in debugging various low-power applications. Not only can you see the power consumption change under each step of the command, but you can also check the power change rule for a long period of time when the system is running. Since there is a separate data channel, you can even debug the program in KEIL and watch the current change in MCUXpresso. The MCU Link Pro has two current measurement configurations, each with a maximum measurable current. This is to achieve maximum measurement accuracy for a variety of different objectives. There are two automatically controlled ranges in each configuration to provide greater precision. The automatic switching from low current measurement to high current measurement is completely controlled by hardware. jingpan_2-1664529871937.png   Each time the MCU Link Pro is powered up, the measurement circuit calibrates itself. There is no need to disconnect/reconnect the MCU Link Pro before calibration due to transistors are used to isolate the sensing circuit from the target power supply to avoid contention and to ensure a known voltage is applied to the system during calibration. At high sample rates, the MCUXpresso IDE may not capture all data, so the sample rate may need to be adjusted using the configuration options in the energy measurement configuration settings in the tool. If the target current exceeds the maximum current in the selected range, the measurement will saturate and cut off and will therefore be inaccurate. Blhost and MCU-Link Pro The most noteworthy feature of MCU Link Pro is its USB to SPI and I2C bridge functions. This enables the computer to send I2C and SPI signals directly through USB. This powerful function is not ignored by blhost. The new version of blhost can support this function and adds a new command parameter '- L'. Specifically, '- L SPI' refers to the SPI interface and '- L I2C' refers to the I2C interface. The following figure shows the test results on frdm-k64f. It can be clearly seen in the figure that the SPI interface of MCU Link Pro can communicate with mcuboot firmware on k64 and download the encryption program to flash. jingpan_3-1664529872017.png     In addition to KINETIS, this function is most suitable for i.mxrt600 and I mxRT500。 These two chips have serial ISP mode. User can download the program to ram through SPI or I2C port, and then directly let it run. Many users have this usage. In the previous examples in SDK, a board of twr-kv46 or twr-k65 or frdm-kl25 was required to receive command and data from UART and translate them to SPI and I2C command. Since there is no direct interface on these boards, flying wires are required, which is very troublesome. Moreover, NXP only provides firmware for these three boards. If you want to use other chips or boards, you must also transplant firmware. It's also very troublesome. But with MCU Link Pro, it's all very easy and pleasant.   LIBUSBSIO library In order to better expand the use of bridge functions, NXP has provided libusbsio library. By calling this library, you can realize the USB to SPI \ I2C \ GPIO function in your own application. I also made the upper computer tools for writing kinetis ezport and flash according to the libusbsio library provided by NXP. I introduced this point in detail in my last article. Interested friends can read my article. It is not enough to provide libraries based on windows and Linux. NXP also provides a python library. This library is based on python3 and can be installed through the following command >pip install libusbsio Its usage is not described in detail in the libusbsio documentation. Here is a general introduction. The following is an initialization procedure of libusbsio. import logging import logging.config from libusbsio import * # enable basic console logging logging.basicConfig() # load DLL from default directory sio = LIBUSBSIO(loglevel=logging.DEBUG) # the main code # calling GetNumPorts is mandatory as it also scans for all connected USBSIO devices numports = sio.GetNumPorts() print("SIO ports = %d" % numports) if numports > 0 and sio.Open(0): print("LIB version = '%s'" % sio.GetVersion()) print("SPI ports = %d" % sio.GetNumSPIPorts()) print("Max data size = %d" % sio.GetMaxDataSize()) if(sio.GetNumSPIPorts() > 0): spi = sio.SPI_Open(1000000, portNum=0, dataSize=8, preDelay=100) if spi: data, ret = spi.Transfer(spi_ssel[0], spi_ssel[1], b"Hello World") sio.Close() else: print("No USBSIO device found") ​ Line 9 is to open an instance of libusbsio library; Line 14: get the number of usbsio ports of all USB bridges; Lines 18, 19 and 20 are the read version information, the number of SPI ports and the maximum size of SPI cache; Line 22: open an SPI interface; Line 24, start transmitting data. It can be seen from the above that the use process is relatively simple. And these commands are very similar to those of the C language library.   A secondary controller LPC804 on the board There is also an lpc804 on the MCU Link Pro board. This chip is confusing here. What is it for? Its UART, SPI and I2C ports are all connected for external use. But what's the use? One conceivable application is that the UART port is connected to the newly added vcom2, and then the SPI or I2C works in the slave mode. As a listener, it monitors the SPI or I2C bus to be debugged and displays it on the computer terminal. The LPC804 debug interface is the same as the debugging port of MCU Link Pro. Maybe the board itself is a development board, so that users can develop lpc804 programs? In addition, its UART-ISP port is connected to a UART port of LPC55S69. It seems that in the future, it can communicate with each other through the new version of CMSIS-DAP firmware. Let's look forward to new ways of playing in the future.
記事全体を表示
A vulnerability (CVE-2022-22819) has been identified on select NXP processors by which a malformed SB2 file header sent to the device as part of an update or recovery boot can be used to create a buffer overflow. The buffer overflow can then be used to launch various exploits. Refer to the attached bulletin for more information.   09/26/2022 - Bulletin updated to include fix datecode information. 11/01/2022 - Bulletin updated with clarification that mixed datecodes are RT600 only.    
記事全体を表示
RNN on FRDM_K64 to denoise 1 Introduction Ordinary MCUs are limited by resources, and it is difficult to do some complex deep learning. But although it is difficult, it can still be done. Last time we used CNN for handwritten recognition. This time ,we use RNN for audio noise reduction. This audio noise reduction uses fixed-point noise reduction. MFCC and gain are used as input parameters for training. MFCC, Mel frequency cepstrum, is often used for audio feature extraction. RNN achieves the effect of noise reduction by adjusting the gain of different frequencies.        2 Experiment 2.1 Required tools: frdm-k64, python 3.7, Pip, IAR   2.2 Download the source code of deep learning framework, https://github.com/majianjia/nnom This is a pure C framework that does not   rely on hardware structure. Transplantation is very convenient     2.3 we select the example ‘bubble’ to add the Inc, port and Src folders in NNoM to the project, as shown in the figure nxf56274_0-1615450961299.png                        Figure 1 Open the file ‘port.h’ . The definitation of NNOM_LOG is changed to PRINTF (__ VA_ ARGS__ ), Open the ICF file, and change the heap size to 0x5000, define symbol__ size_ heap__ = 0x5000; Malloc, which is used in this library, allocates memory from here. If it is small, it can't run the network   2.4 Transplant fatfs file system to bubble project nxf56274_1-1615450975431.png   Figure 2   2.5 In the bubble.c file, add the following header file        #include "nnom_port.h" #include "nnom.h" #include "weights.h" #include "denoise_weights.h" #include "mfcc.h" #include "wav.h" #include "equalizer_coeff.h"   2.6 Find main.c under ‘examples\rnn-denoise’ in the framework, ‘main_arm.c’ is used for stm32. Main.c is provided for windows running routines. This code is used to open the audio file, then run the network, and finally generate noise reduction. Use this code to facilitate experiments. The APIs for file operations in this file need to be manually changed to MCU APIs. I added a progress bar display. You can refer the attachment.   2.7 This example also uses DSP, so DSP support needs to be turned on, as shown in the figure nxf56274_2-1615450986521.png                                                           Figure 3 2.8 Add macro nxf56274_3-1615450994191.png                                             Figure 4   2.9 After the compilation is passed, download the program. The tested wav needs to be named ‘sample.wav’, and the mcu will reduce noise for it. Finnally mcu will generate ‘filtered_sample.wav’. Plug the SD card into the computer to listen to the noise-reduced audio. This is serial message. nxf56274_4-1615451004815.png     Figure 5 This is the audio analyzed by the audio analysis software. The upper part is the noise reduced, and the lower part is the original sound. You can see that a lot of noise has been suppressed. nxf56274_5-1615451012178.png                                                    Figure 6 3 training Through the above steps, we have achieved audio noise reduction, so how is this data trained? You need to install tensorflow, and keras. How to train is written in the README_CN.md file. This tensorflow needs to install the gpu version, and needs to install cuda. Please check the installation yourself. 3.1 Download the voice data https://github.com/microsoft/MS-SNSD and put it under the MS-SNSD folder 3.2 Use pip3 to install the tools in requirements.txt 3.3 Run ‘noisyspeech_synthesizer.py’ directly, this will report an error. You need to change the 15-line float to int type. 3.4 Run the script gen_dataset.py to generate mfcc and gain 3.5 Run main.py, this will generate the noise file of the sample, which can be used for testing and also generated ‘weights.h,denoise_weights.h,equalizer_coeff.h’ PS: Put the code in directory 'boards/frdmk64f/demo_app'. 'sample.zip' has the noise wave.
記事全体を表示
Symptoms As we know: Flash must be programmed after an erase operation. Violation of this rule will cause programming fail and even hardfault(when AHB reading) on Kinetis K64 parts. Customer accidently uses SDK’s API programming same sector twice(over-programming) without an erase operation. Then when perform AHB reading of this sector(include using JFLash to read this sector), an Hardfault occurs. Diagnosis K64 flash has internal ECC on each sector. When over-programming happens, ECC will be crushed and trigger Hardfault when AHB reading of this sector. Solution Using SDK API FLASH_VerifyErase to check if this sector is erased. Call FLASH_VerifyErase every time before you want to program the flash. This problem will impact all Kinetis device which has FTFE flash module.   Thanks for Alex Yang provide the material.
記事全体を表示
  CNN on FRDM_K64 1 Introduction Limited by resources, ordinary MCU is difficult to do some complex deep learning. However, although it is difficult, it can still be done. CNN, convolutional neural network, is a kind of deep learning algorithm, which can be used to solve the classification task. After the implementation of CNN, ordinary MCU can also be used as edge computing device. Next, we introduce how to run CNN on frdm-k64 to recognize handwritten numbers. The size of digital image is 28x28. 28x28 image as input for CNN will output a 1x10 matrix. There are few deep learning libraries written for MCU on the Internet. Even if there are, there will be various problems. NNoM framework is easy to transplant and apply, so we use it     2 Experiment 2.1 Required tools: frdm-k64, python 3.7, Pip, IAR, tcp232   2.2 Download the source code of deep learning framework, https://github.com/majianjia/nnom This is a pure C framework that does not rely on hardware structure. Transplantation is very convenient   2.3  we select the example ‘bubble’ to add the Inc, port and Src folders in NNoM to the project, as shown in the figure nxf56274_0-1611022952076.png          Figure 1 Open the file ‘port.h’ . The definitation of NNOM_LOG is changed to PRINTF (__ VA_ ARGS__ ), Open the ICF file, and change the heap size to 0x5000, define symbol__ size_ heap__ = 0x5000; Malloc, which is used in this library, allocates memory from here. If it is small, it can't run the network   2.4 From the download framework, go into ‘mnist-simple/mcu’, which has trained file ‘weights.h’, and randomly generated handwritten image file, ‘image.h’. Add these two files to the project   2.5 Add headfile to ‘bubble.c’        #include "nnom_port.h" #include "nnom.h" #include "weights.h" #include "image.h"   2.6 Delete the original code, add the following code   nnom_model_t *model; const char codeLib[] = "@B%8&WM#*oahkbdpqwmZO0QLCJUYXzcvunxrjft/\\|()1{}[]?-_+~<>i!lI;:,\"^`'.   "; /*******************************************************************************  * Code  ******************************************************************************/ void print_img(int8_t * buf) {     for(int y = 0; y < 28; y++)        {         for (int x = 0; x < 28; x++)               {             int index =  69 / 127.0 * (127 - buf[y*28+x]);                      if(index > 69) index =69;                      if(index < 0) index = 0;             PRINTF("%c",codeLib[index]);                      PRINTF("%c",codeLib[index]);         }         PRINTF("\r\n");     } }   // Do simple test using image in "image.h" with model created previously. void mnist(char num) {        uint32_t predic_label;        float prob;        int32_t index = num;        PRINTF("\nprediction start.. \r\n");               // copy data and do prediction        memcpy(nnom_input_data, (int8_t*)&img[index][0], 784);        nnom_predict(model, &predic_label, &prob);          //print original image to console        print_img((int8_t*)&img[index][0]);               PRINTF("\r\nTruth label: %d\n", label[index]);        PRINTF("\r\nPredicted label: %d\n", predic_label);        PRINTF("\r\nProbability: %d%%\n", (int)(prob*100)); }   int main(void) {     uint8_t ch;     /* Board pin, clock, debug console init */     BOARD_InitPins();     BOARD_BootClockRUN();     BOARD_InitDebugConsole();     /* Print a note to terminal */     model = nnom_model_create();        // dummy run        model_run(model);     PRINTF("\r\nwhich image to distinguish? 0-9 \r\n");     for(uint8_t i=0; i<10; i++)     {         print_img((int8_t*)&img[i][0]);     }     while(1)     {         PRINTF("\r\nwhich image to distinguish? 0-9 \r\n");         ch = GETCHAR();         if((ch >'9') || ch < '0')         {             continue;         }         PRINTF("\r\n");         mnist(ch-'0');     } }   An error will be reported when compiling ‘weights.h’, due to lack of few parameters. In layer [1], layer [4], layer [7], you need to add ‘division (1,1)’ after ‘stride (1,1)’. In this way, the compilation passes.   2.7 As a result, open the serial port software. At the beginning, the terminal will print out a variety of handwritten digital pictures, and then enter a number, The corresponded picture will be recognized. nxf56274_1-1611022952200.png                                                    Figure 2 When we input ‘8’, the recognition is the handwriting '9' nxf56274_2-1611022952340.png                        Figure 3   The ‘Truth label’ corresponds to IMG9_LABLE in ‘image.h’ and ‘Predicted label’ is the prediction results   3 training Through the above steps, we have realized a simple handwritten numeral recognition. Next, we will introduce ‘weights.h’. How to generate the weight model here? The image data here are all from MNIST digital set. How can we make a handwritten number for MCU to recognize?   3.1 Under ‘nnom-master\examples\mnist-simple’, there is a ‘mnist_ simple.py’. You need to run it to generate ‘weights.h’ and ‘image.h’. To run this, you need to install tensorflow, keras and so on. When you run it, you can use pip to install what is missing The network operation process is as shown in the figure nxf56274_3-1611022952397.png                               Figure 4 Conv2d-> convolution operation, Maxpool-> pooling. The meaning of convolution operation is to extract the features of the image. Pooling is a bit like compressing data, which can reduce the running space. 28x28 input and output a 1x10 matrix, representing the possibility of 0-9   3.2 We can use the ‘Paint’ program of WIN to adjust the canvas to 28x28, write numbers on it and save it in PNG format. I wrote a ‘4’   nxf56274_4-1611022952398.png   Figure 5   Change the code as following.   nnom_model_t *model; uint8_t temp[28*28]={0}; const char codeLib[] = "@B%8&WM#*oahkbdpqwmZO0QLCJUYXzcvunxrjft/\\|()1{}[]?-_+~<>i!lI;:,\"^`'.   "; /*******************************************************************************  * Code  ******************************************************************************/ void print_img(int8_t * buf) {     for(int y = 0; y < 28; y++)        {         for (int x = 0; x < 28; x++)               {             int index =  69 / 127.0 * (127 - buf[y*28+x]);                      if(index > 69) index =69;                      if(index < 0) index = 0;             PRINTF("%c",codeLib[index]);                      PRINTF("%c",codeLib[index]);         }         PRINTF("\r\n");     } }     void mnist_pic(uint8_t *temp) {        float prob;     uint32_t predic_label;        PRINTF("\nprediction start.. \r\n");          // copy data and do prediction        memcpy(nnom_input_data, (int8_t*)temp, 784);        nnom_predict(model, &predic_label, &prob);          //print original image to console        print_img((int8_t *)temp);        PRINTF("\r\nPredicted label: %d\n", predic_label);        PRINTF("\r\nProbability: %d%%\n", (int)(prob*100)); }   int main(void) {     /* Board pin, clock, debug console init */     BOARD_InitPins();     BOARD_BootClockRUN();     BOARD_InitDebugConsole();     /* Print a note to terminal */     model = nnom_model_create();        // dummy run        model_run(model);     while(1)     {         PRINTF("\r\n Send picture by serial\r\n");            DbgConsole_ReadLine(temp,784);         PRINTF("\r\n Got picture\r\n");           mnist_pic(temp);     } }   3.3 Then use pic2mnist.py(see the attachment), run this script with CMD and enter 'Python pic2mnist.py 1. PNG ', 1. PNG is the image to be parsed, and then ‘content.txt’ will be generated. The file contains the data of the picture. Send the data to the MCU through the serial port. Note that ‘Send as Hex’ should be checked. Similarly, the handwritten picture will be displayed first, and then the picture will be recognized. nxf56274_5-1611022952440.png                                                           Figure 6   We can see that '4' was identified
記事全体を表示
Introduction: User can modify the value of internal reference clock (IRC) by using the Trimming capability of programmers. There are two registers (ICS_C3 & ICS_C4) which contains the trim and fine trim value of the clock respectively. By default, devices comes with a factory programmed trim value which is automatically passed into these registers during reset initialization when not in debug mode. These registers needs to be passed with appropriate value to get the required clock value. This is where programmers come into picture, they generally have this capability to find the accurate trim and fine trim values corresponding to required clock. Now the catch here is that the customized trim value calculated by programmers is stored at reserved flash location (eg-0x000003ff and 0x000003fe for Ke02) and have to be copied to trim registers( ICS_C3 &C4) manually by user during code initialization. Using this process to trim the clock will give accurate desired clock without any deviation between samples. Process:  There is an option in programmers( like I am using PEmicro Multilink universal ) for enabling and setting the trimming feature in the configuration settings as below:   nxf58908_0-1609673451703.jpeg       After enabling this option, the programmer will find the best trim value and store at internal memory location:   0x03ff for trim internal reference value 0x03fe for fine trim internal reference value   Below snapshot from console shows this process:   nxf58908_1-1609673451775.jpeg     Next step is to copy these value from above locations and pass it to ICS_C3 and ICS_C4 manually in our application code. You can use below code lines:       ICS->C3 = *((uint8_t*) 0x03FF); // trim internal reference clock     ICS->C4 |= ICS_C4_SCFTRIM(*((uint8_t*) 0x03FE)); // fine trim internal reference clock   What the above logic does is – it copies the trimmed value from the factory programmer into your ICS register – not dependent on a constant value but dynamically update the register as per the tuning happening by the programmer. Similar option is there in production programmers also to take care of the trimming process. Note: Above steps are with reference to KE series, for other series user has to check the device reference manual for specific address and register. Also attaching a code with the above mentioned things added into it for ease of understanding. Thanks Madhur
記事全体を表示
Making and Downloading Security Image for Kinetis Device   Introduction KINETIS devices have Flash base bootloader or ROM bootloader. They have same structure and same download tools. MCUBOOT shows supported device. The bootloader not only support plaintext image, but also encrypted image which is encrypted by AES. This can protect user’s application code from unauthorized using. Due to different internal Flash structure, security image making, key download and image download flow is a bit different to each Kinetis devices. This hands-on will introduce Flash base bootloader and ROM base bootloader security image making and downloading.   2 Security image to Flash bootloader Many NXP Kinetis device SDK have integrated bootloader. Take FRDM-K64F as example, the bootloader project is in SDK_2.8.0_FRDM-K64F\boards\frdmk64f\bootloader_examples\freedom_bootloader The bootloader support security format image by default. User can download security format image via UART and USB interface. In K64 bootloader, the key is stored in 0xb000. But the application code is start from 0xa000. That means each time the application is upgraded, key file need to be download again.   2.1 Generate key The elftosb tool can generate a key. But of course, you can take any string as key. jingpan_0-1609396818676.png     2.2 Image encryption Use the key to encrypt application image. Here is the bd file. options {  flags = 0x4; // 0x8 encrypted + signed, 0x4 encrypted  buildNumber = 0x1;  productVersion = "1.00.00";  componentVersion = "1.00.00";  keyCount = 1; }   sources {  inputFile = extern(0);  sbkey = extern(1); }   section (0) {  erase 0xa000..0xF6000; load inputFile > 0xa000; }   jingpan_1-1609396818771.png     2.3 Download key and image Connect FRDM-K64F openSDA usb port. Then download key and image. jingpan_2-1609396819004.png     2.4 Download key with KinetisFlashTool Use keyboard to input key is really annoying. There is a GUI tool named KinetisFlashTool which can download image same as blhost.exe. To download encrypted image by this tool, we can make a sb file to download key first. Here is the bd file.   sources { } section (0) {        erase 0xb000..0xc000;        load {{E0BAA2C8231283CAF1D327CEDB82AFF9}} > 0xb000; }   Using elftosb to generate the sb file. The elftosb command line is as below \>Elftosb -V -c program_key.bd -o program_key.sb   This sb file should be download at first, then download the encrypted application image. When customer want to download security image via USB MSC or HID, this is the only way to download key. There is a limitation in those bootloader which version is lower or equal to v2.7.0. MSC function and HID function can’t be enabled together. Otherwise bootloader will fail when copy encrypted sb file to MSC disk.   2.5 About the key But it is really strange that key file should always come with encrypted file. It is reasonable to keep the key in secure status, for example, an untouched place in flash. K64 has a program once field which is located in program flash IFR. This is a standalone space different from main space. It’s address is from 0x3C0 to 0x3FF. MCU core can read or write this area by special flash command. We can put the AES key here. Again, we can use sb file to download this key. sources { } section (0) {        load ifr 0xE0BAA2C8 > 0x3c0;        load ifr 0x231283CA > 0x3c1;        load ifr 0xF1D327CE > 0x3c2;        load ifr 0xDB82AFF9 > 0x3c3; } Then we should modify sbloader_init() in sbloader.c. The source code only read key form 0xb000. We should have it read key from IFR.   Security image to ROM bootloader Some Kinetis device has ROM bootloader. They are different with flash base bootloader. This document use FRDM-K32L2A as example.   3.1 Generate AES key and download the key The key can be set as 0x112233445566778899aabbccddeeff00. Besides sb file, it can also be programmed to IFR by blhost command. \>blhost -p COM9 – flash-program-once 0x30 4 11223344 msb \>blhost -p COM9 – flash-program-once 0x31 4 55667788 msb \>blhost -p COM9 – flash-program-once 0x32 4 99aabbcc msb \>blhost -p COM9 – flash-program-once 0x33 4 ddeeff00 msb If you do not write anything to IFR, the ROM bootloader will use all-zero key. Here I use all-zero key.   3.2 Encryption algorithm The ROM bootloader hasn’t encryption algorithm. Application should include algorithm code and assign the address to bootloader, or preprogram BCA table and MMCAU code into flash. You can find MMCAU code (mmcau_cm0p.bin) and BCA(BCA_mmcau_cm0p.bin) table in MCUBoot2.0.0 package. Before you program these code into flash, new address must be written into it. For example, we put MMCAU code into 0x7f800, then we should modify the BCA table as below jingpan_3-1609396819033.png     And then, according this new address, modify the MMCAU_function_info structure in mmcau_cm0p.bin. jingpan_4-1609396819123.png   After that, download BCA to 0x3c0 and mmcau_cm0p.bin to 0x7f800. jingpan_5-1609396819231.png   In order to avoid using manual operation in production, above steps can be integrate in a single sb file.   3.3 Encrypt the image and download The bd file in K64 example can be reused, just need to change the image address to 0x00. jingpan_6-1609396819344.png   Press the reset button, after 5 second, the led will blink.   References: Kinetis Bootloader v2.0.0 Reference Manual Kinetis Elftosb User's Guide Kinetis Bootloader QuadSPI User's Guide Kinetis blhost User's Guide
記事全体を表示
Hey All, Check out the unboxing video for UAV Drone designed using Kinetis V series MCUs to be showcased in Freescale Technology Forum 2015 at booth 249. The Kinetis V series 32-bit MCUs are based on ARM Cortex M cores and specially designed to enable motor control and power conversion applications. Please visit Kinetis V Series Webpage for more information. This drone is powered by Kinetis KV5x MCU (First Kinetis MCU with the latest ARM Cortex M7 Core). The Kinetis KV5x is used in Electronic Speed Control (ESC) unit and a single Kinetis KV5x MCU chip is used to control 4 Brushless DC motors which typically is controlled by four 8 bit MCUs. Along with controlling four motors, the KV5x MCU has enough performance and peripheral headroom so that it can be used as a flight controller and communication interface with connectivity features such as CAN and Ethernet. Kinetis KV5x is ideal solution for industrial IOT with the applications such high performance motor control and power conversion and real time control. Please visit Kinetis KV5x Series Webpage for more information. There is another drone in the Analog section at Freescale Technology Forum based on Kinetis KV4x MCU (based on ARM Cortex M4 core) and Freescale GD3000 3-Phase Brushless DC Gate driver. The Kinetis KV4x MCU is used to control 4 Brushless DC motors and is the cost optimized version of Kinetis KV5x MCUs. Please check out the Kinetis based drone demo as well as other cool demos at Freescale Technology Forum. PS: I apologize for the quality of the video. Working on the better video and editing skills.  Thanks, Mohit Kedia
記事全体を表示
Reference Solution being developed with Kinetis V (also can be done with a Kinetis K device) of a Class-D audio amplifier. 16-bit ADC sampling the audio input FlexTimer doing the PWM's for the Class-D amplifier DC/DC switched power supply with input of 12V and output of 130V to 180V (generates the power you need for making some good noise - 1kW) being controlled by the Kinetis MCU also. Capabiltiy of Audio processing/filtering using the Cortex-M4 DSP capabilities. Solution originally designed for cost-effective Automotive aftermarket sound systems. But can be adapted for implementing other audio amplifier applications also in the consumer space! Can you thing of cool applications/markets that this solution can be also quickly adapted? Soon, plan to make the reference solution design files available in the community. Stay tunned. Cheers! PK
記事全体を表示
Overview The Sub-GHz Remote Control Dimmer is a reference design which demonstrates the functionality of the MKW01Z128 MCU working in a custom IEEE 802.15.4 star network.   This reference design is focused on a home automation application where the user is able to control various RGB bulbs connected into a network using the KW01-RCD-RD board as a remote control. Controlled devices are USB-KW019032 boards, and each board simulates an RGB bulb in a GUI.   Sub-GHz technology has some advantages over other wireless technologies such less data traffic in its respective ISM band.   Features: Documentation: Quick start guide Application users guide Board users guide Software user guide Schematics, Software, GUI and BSP: Link Best regards, Luis Burgos.
記事全体を表示
Hi All, all presentations were included in this archive file.
記事全体を表示
Freescale's Jeff Bock highlights the awesome features of the Kinetis 32-bit microcontrollers based on the ARM Cortex-M4 core
記事全体を表示
      In the practical KE KEA usage, a lot of customers meet the watchdog can’t reset problems. Some customers find when they want to enable the watchdog, but can’t really enable the watchdog by set the EN bit in register WDOG_CS1; Some customers find when in debug mode, the EN bit WDOG_S1 register always be clear, but from the reference manual, this bit should be set after reset, even they check their code, and make sure they didn’t disable the watchdog;  There also have some customers find when they use the KEXX_DRIVERS_V1.2.1_DEVD code, and set the timeout value register by themselves, but the watchdog can’t reset in the timeout value. Now according to these problems, this document will analyze it and give the recommendation to avoid these problems.      From the above problem description, we can get that there actually mainly 2 reasons caused these problems: 1, software configuration; 2, debugger usage 1.  Software configuration   1) Start code disable the watchdog In the KE KEA sample code, after reset, the chip will enter in the start code at first, the start code always disable the watchdog at first, if the watchdog is disabled, the watchdog can’t be enable just by set the EN bit in register WDOG_CS1, because bit EN in register WDOG_CS1 is the write-once bit after reset. It only can be modified when the UPDATE bit is set and with 128 bus clocks after performing the unlock write sequence. Now how to find the disable code in the start code? Take KEXX_DRIVERS_V1.2.1_DEVD sample code as an example IAR: from crt0.s, will find the watchdog disable code WDOG_DisableWDOGEnableUpdate();  in the start function. The above IAR start picture is for KE, but in the KEA start file, you can’t see the start function in the KEA sample code which download from the freescale web, just find the __iar_program_start in cstartup_M_KEA128.s after the reset happens, but where is the __iar_program_start function, it can’t be searched in the whole project. Actually __iar_program_start is the default program entry function, it include the following function: You can find it will enter __low_level_init function, the watchdog disable code is just in  __low_level_init function. MDK:  From startup_MK0XZ4.s will find the watchdog disable code in the SystemInit function. Codewarrior: From __arm_start.c file, will find the watchdog disable code in __init_hardware function. 2) Codewarrior script init_kinetis.tcl disable the watchdog      To the Codewarrior, just comment the disable watchdog code in the __arm_start.c file is not enough to check the watchdog enable after reset, because in the codewarrior connect script init_kinetis.tcl, there also have the watchdog disable code.      If you want to find the state of EN bit in register WDOG_S1 after reset, you must disable all these watchdog disable code.   3) Timeout register configuration incorrect From the header file MKE02Z2.h, we can find the time out register define like this:   union {                                          /* offset: 0x4 */     __IO uint16_t TOVAL;                             /**< WDOG_TOVAL register., offset: 0x4 */     struct {                                         /* offset: 0x4 */       __IO uint8_t TOVALH;                             /**< Watchdog Timeout Value Register: High, offset: 0x4 */       __IO uint8_t TOVALL;                             /**< Watchdog Timeout Value Register: Low, offset: 0x5 */     } TOVAL8B; This structure means that customer can define the watchdog timeout value by separated unit8 TOVALH, TOVALL or just defined it with unint16 TOVAL. But actually in the IAR project usage, take an example, use 1khz as the clock source for watchdog, then want to set the timeout value as 1s, it means the timeout value should be 1000=0x03e8, so one of the customers configure it like this:    You can find, we need the TOVALL= 0XE8, TOVALH=0X03, but from the test result, the register is TOVALL= 0X03, TOVALH=0Xe8, this will cause the timeout value is much larger than 1000, that is why customer can’t reset the mcu after 1s, because the register configuration is not correct. It is caused by the IAR int16 store endian mode, the default IAR endian mode is little endian mode. So in the practical usage, it is recommended to use the separated time out value definition. 2. debugger usage When in debug mode with IDE, some customers find even they comment all the watchdog disable code, they still can’t reset the MCU by the watchdog. After check the register WDOG_S1, bit EN is 0, it means the watchdog is disabled. But from the reference manual, we get that after reset, the EN bit should be 1. What caused this? After test, we find this actually caused by the debugger, the debugger hardware which you are using. Eg, in the same project which already comment all the watchdog disable code, SEGGER JLINK will still disable the watchdog, but the PE opensda or PE multilink won’t do this, the EN bit is enabled by default, the following is the test picture, take codewarrior as an example: 1) JLINK 2) PE Opensda or PE multilink    So, if you want to test the watchdog in debug mode, and want the EN is set after reset, you can choose PE debugger tool instead of JLINK, but this JLINK feature is just influence the debug mode, after you download the code to the chip flash, and after reset, the EN bit in WDOG_S1 will still be set. Wish this document will help you get out the problem of watchdog can’t be reset.
記事全体を表示
My customer wanted to use K60 in his design but he only has the Keil IDE, so I helped to port some examples in KINETIS_SC for him as a starting point. The attachment is my porting work, which also includes a exe file to create new keil project. You may refer to "keil\build\uv4\make_new_project_keil.exe" for details. Hope that helps, B.R Kan
記事全体を表示
Hi: Kinetis's ADC have no multi channels sequence sampling function, compared with LPC's ADC. But we could use DMA for such case, attached are two demos: 1.multi_channels_edma_ADC_DMA_SW_TRIG Description: use SW trigger DMA transfer for 6 ADC channels, DMA ch0 is for ADC channels transfer, DMA ch1 is for ADC sample result transfer in DMA ch1 ISR, report ADC sample are done; 2.multi_channels_edma_ADC_DMA_LPIT_HW_TRIG Description: use LPIT timely trigger DMA transfer for 6 ADC channels, DMA ch0 is for ADC channels transfer, DMA ch1 is for ADC sample result transfer in DMA ch1 ISR, report ADC sample are done; but LPIT could trigger continuously without SW engage.
記事全体を表示
I2C (Inter-Integrated Circuit) Module by Alejandro Lozano, Freescale TIC. i2C Protocol Explanation. Connection Diagram. How to configure the registers. Hands-On. Presentación del módulo de I2C (Inter-Integrated Circuit) por Alejandro Lozano, Freescale TIC. Explicación del Protocolo I2C. Diagrama de conexión. Explicación de cómo configurar los registros. Hands-On
記事全体を表示