Kinetis Rock 'n' Roll! 1kW Class-D Audio Amplifier

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Rock 'n' Roll! 1kW Class-D Audio Amplifier

Kinetis Rock 'n' Roll! 1kW Class-D Audio Amplifier

Reference Solution being developed with Kinetis V (also can be done with a Kinetis K device) of a Class-D audio amplifier.

  • 16-bit ADC sampling the audio input
  • FlexTimer doing the PWM's for the Class-D amplifier
  • DC/DC switched power supply with input of 12V and output of 130V to 180V (generates the power you need for making some good noise - 1kW) being controlled by the Kinetis MCU also.
  • Capabiltiy of Audio processing/filtering using the Cortex-M4 DSP capabilities.

Solution originally designed for cost-effective Automotive aftermarket sound systems. But can be adapted for implementing other audio amplifier applications also in the consumer space!

Can you thing of cool applications/markets that this solution can be also quickly adapted?

Soon, plan to make the reference solution design files available in the community. Stay tunned.

Cheers!

PK

(view in My Videos)
No ratings
Version history
Last update:
‎06-15-2015 04:07 PM
Updated by: