Connects - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

讨论

排序依据:
Explore how to build secure CAN connections by using data encryption or CMAC, while taking the best performance on S32K144.
查看全文
Adoption of Passive Keyless Entry / Go is growing rapidly, and adding such functionality in the car key introduces challenges for battery life and security. As such, a new class of motion sensor has been developed to address these challenges. In this class, the newest NXP motion sensor, FXLS8962AF, which boasts benchmark power consumption, EMC Class III compliance and full AEC-Q100 qualification is introduced. The sensor has been specifically designed for compatibility with NXP’s all-in-one IC for passive entry keys (i.e. TOKEN), and this class will explain how the two devices are being used together to improve battery life and enhance security in the passive entry system implementation.
查看全文
ADAS roadmaps, value proposition, current and future plans for tools and reference designs.
查看全文
DDR tools overview. Part 1, DDR test tool features and capabilities. Part 2, DDR configuration tool features and capabilities, benefits of each for the end users.
查看全文
This presentation will present a simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC. New research presented on the impact of discrete components on radiated and conducted emissions, with an emphasis on cost analysis. Results of recent research on various power supply PCB topology will be discussed.
查看全文
This session will cover NXP's complete voice and audio solutions for IoT market. This includes solutions for voice calling, AI voice recognition and music playback. NXP brings complete and optimized audio framework on NXP's MCU and MPU products, which provides ready and easy to use voice and audio functions to IoT developers.  In the applications such as AI speakers, home electrical equipment and voice control nodes.
查看全文
Market and application trends in automotive radar, supporting NCAP and autonomous architectures.
查看全文
A guide to using the Vision SDK for S32V. Learn how to leverage S32V design tools to work with APEX and ISP on the S32V family.  
查看全文
How to build an automotive application using the S32 SDK, integration with design studio, tips & tricks, FreeRTOS, communication stacks; focus on S32K144 and S32K148.
查看全文
Overview of S32K, MagniV and other GPIS products.
查看全文
The session includes the overview of S32K Automotive MCU product family for general purpose automotive applications, as well as industrial applications which require automotive quality and reliability. It will cover the introduction of S32K solutions – touch sense, motor control, secured car access, CAN-FD communication, etc.
查看全文
In this workshop you will learn about UJA1196 capabilities for HS-CAN communications focused on low-power applications, using its great features for supply voltage, wake-up capabilities, etc. All of this in a very small package.
查看全文
This class will cover basic operation and the internal mechanisms of DDR devices. The class will also cover available tools to enable and simplify bring-up and validation of a DDR subsystem.
查看全文
Introduction to the MCU Alexa Voice solution describing the features, architecture, and presenting the cost and ease of use benefits. We will be also showing the Out-of-Box Experience of on-boarding Alexa using Wi-Fi as well as interacting with Alexa by using a cost effective far-field Implementation.  
查看全文
In Automotive, the need for communication between various ECUs has grown as the number of ECU’s have grown as well. Implementing a software solution which is scalable, portable, open and easy to program is key to offering a complete software enablement to our customers. This session will present our software solution for communication between multiple SOCs with different operating systems across  multiple physical areas.
查看全文
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
查看全文
Safety by Software (SBSW) is a new way of achieving ASIL-D with high-level measures, supported by NXP S32X hardware. The SBSW hardware module together with SBSW firmware enables to check the user application flow, compare results of main and redundant algorithms and detect faulty behavior with high degree of independence. This session makes you familiar with SBSW usage, configuration, tools, etc.
查看全文
S32 Design Studio 3.0 S32V234 focus on configuration tools pin wizard, clocks config, with SDK configuration, FreeRTOS configuration and use building and running a project showing debug with S32 debugger on the m4 with code on target. Configuration tools suite formed from pins, clocks, peripherals, DCD, IVT are offering a complete view of the platform with complete access to all the details directly from the tool and possibility to generate, build and debug the applications.
查看全文
A deep dive into the pixel processing pipeline of the i.MX 8. Attendees will get a detailed insight into the available accelerators for 2D, 3D, Video, Vision, AI, Capture and Display and how they enable the multimedia and safety features of the eCockpit.
查看全文
I2C master and slave devices are used in many system for various reasons. NXP offers the widest portfolio of I2C devices. This class will introduce the I2C-Bus interface, address some common pitfalls when designing with I2C-Bus, and present solutions to these challenges.
查看全文