コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
The session will introduce an upcoming xEV traction motor power inverter platform system-play solution featuring a new MCU, new IGBT gate driver, and new safe SBC bound together with system enablement software and ASIL-D compliant safety support. A fully functional traction motor reference design being designed by partner Vepco will also be introduced based on a Power IGBT Module from Fuji Electric. The session will describe the platform’s components, software structure, value proposition, enablement support and go-to-market approach to help enhance understanding of the application and NXP solution as well as how to sell the system platform.
記事全体を表示
This hands-on session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs based on the ARM® Cortex®-M core. Using either Kinetis or LPC development hardware, attendees will build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application.
記事全体を表示
In this class, you will learn to use NXP’s FreeMASTER debug tool to aid in system development and debug. Although it is has many uses in various applications, we will demonstrate the features and use of FreeMASTER to simplify the development process with a motor control example based on our MagniV MC9S12ZVMRM microcontroller. Participants will see how useful and easy it is to use and configure so that system variables can be adjusted on the fly or watch system parameters real time.
記事全体を表示
This session will present the advantages of H-bridge based window lifters against relay based ones, new functionalities that can be implemented and how NXP MagniV S12ZVMB64 microcontroller provides a well-integrated solution for a window lifter end node. With integrated functionalities like: internal regulator, GDU, PMF, ADC, current sensing, input capture and LIN physical layer.
記事全体を表示
This session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs. Using either Kinetis, LPC or i.MX RT development hardware, attendees will watch how to build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application, as well as the advanced debugging capabilities of the MCUXpresso IDE, including trace, profiling, coverage, watch points and more.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers and a variety of home appliances like fridges, washing machines, air purifiers, coffee machines, blenders all have one thing in common: Near Field Communication (NFC) allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be authenticated and configured without any user interaction, and without power supply. And commissioning an IOT node into a wireless network has never been as easy as it is now with NFC. We will share the latest status of NFC support in iOS and present the brand new NFC Tandem module.
記事全体を表示
In electronic systems, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems or the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators and GPIO expanders are often used to bridge between the interconnects on the board. In this session, we will explore the application of these interface devices from NXP and discuss their applications in various customer systems.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
記事全体を表示
This session will go into the detail of the software enablement around the BlueBox v2.0, aka “Blue Box Min”. From an engineering perspective, topics will include: The SoCs in the platform and it’s layout; Booting the individual SoCs; Linux options between and inter-communication between them; Discussion of middleware options (including ROS versions, Polysync and others); How ADAS vision perception is accomplished with Neusoft ADAS perception; Combined to achieve level 2/3 ADAS with AutonomouStuff; Extra topics: OpenCV, OpenSSL security between subsystems and more. Please expect a non-marketing lecture explaining the internals of this enablement.
記事全体を表示
This session will introduce NXP differentiated GaN technology for cellular band high power applications, including full cellular portfolio RF Power products.
記事全体を表示
This session will focus on tire localization: Dual axis sensors enable rotation rate detection and determination of drivers / passenger side in seconds. NogaroE: Enhanced features added to a proven volume production TPMS sensor. Gen 4x4: Next-generation of ultra-low power TPMS sensors in smallest package features increased accuracy and processing power.
記事全体を表示
The i.MX processors have features for advanced key management techniques. This session examines these feature in depth.
記事全体を表示
Join us to learn how to develop PCBs of all kinds and the complexity to perform well in harsh environments.
記事全体を表示
As IC geometries continue to shrink and switching speeds increase, designing electromagnetic systems and printed circuit boards to meet the required signal integrity and EMC specifications has become even more challenging. A new design methodology is required. Specifically, the utilization of an electromagnetic physics-based design methodology to control the field energy in your design will be discussed. This training module will walk through the development process and provide you with guidelines for building successful, cost effective printed circuit boards.
記事全体を表示
This session will introduce the NXP mature and widely accepted solutions of RF products serve the DAS and small cell applications from 0.5W, 10W to 20W and 40W.
記事全体を表示
Extend your logistics track and trace with condition insights. NTAG SmartSensor enables sensing and logging with NFC readout. NTAG SmartSensor enables your IoT application for smart logistics, smart healthcare, drug delivery and smart packaging.
記事全体を表示
Learn about NXP's secured IoT Gateway platform with sensor fusion, local and cloud analytic. IoT data aggregation, sensor fusion and analytic processes are run in VMs providing VM isolation advantage. IoT processes can also run in Virtualized Network Functions (VnF) that can run as service chains across end-to-end virtualized network equipment
記事全体を表示
The material presented will be focused on the physics of electromagnetic energy basic principles, presented in easy to understand language with plenty of diagrams. Attendees will discover how understanding the behavior of EM fields can help to design PCBs that will be more robust and have better EMC performance. This is not rocket science, but an easy to understand application of PCB geometry.
記事全体を表示