i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
  Background : Some customer want to test the LPDDR4/X ECC feature based on the i.MX93 chip, But, for now, Our DDR Config Tool do not release this test chosen. And our ECC guide only tell the ECC feature function, does not tell the customer how to test it. So in this article, Will show you more details about ECC feature and how to run the ECC test use uboot command. But I won't put the source code of the test here, You can download the binary run the test on the i.MX93 EVK board.   HW : i.MX93 EVK board with 2GB LPDDR4 SW : 6.1.1-1.0.0   ECC Introduce what is ECC?       ECC is the abbreviation of Error Correction Code. Its function is to automatically detect and repair some minor errors in the memory to prevent data errors. How does ECC work? We can think of it as an "automatic proofreader", and its workflow is roughly as follows:  When writing data: The memory controller generates a "check code" (similar to the fingerprint of the data) for each piece of data. This check code will be stored together with the data. When reading data: The memory controller will recalculate the "fingerprint". Then compare the previously stored check code to see if there is any difference. If a difference is found: If it is just a 1-bit error, ECC can automatically correct it. But, If there are multiple errors, ECC can at least detect them and issue a warning.   ECC test step: 1. Flash the attachment file to the imx93 board. 2. Enter the uboot, run the "ecc --help" command, you will see the below help output message   3. For example : ecc 0x80000000 0x90000000, it will test the ecc feature with on bit error detect and correct , 2 bits errors detect with 256MB DRM size.   if you need this ECC_ test binary file, please contact me, i will share it to you        
記事全体を表示
Our default BSP code can support below resolution:       https://github.com/nxp-imx/linux-imx/blob/cbfe1a744dc4a794e79396c7079339a54f89c8f2/drivers/phy/freescale/phy-fsl-samsung-hdmi.c If customer want to add new pixel clock about their  panel, they can ask our support to generate the new parameters about it, and then add the result to below struct: const struct phy_config samsung_phy_pll_cfg[] = {}. After add the result to the struct, you need to re-compile the kernel and boot your board, then run the "modetest -c" command Check whether the changes are effective when you run the modetest -c command, the following code show as below, You can see all the resolutions currently supported by your monitor.   How to change the panel display resolution: 1) Run the below command at the uboot period: setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:1920x1080-32@30' video=HDMI-A-1:3840x2160-32@30: Set video output parameters: HDMI-A-1: Specifies the use of the HDMI interface. 3840x2160: The resolution is 3840x2160 (4K). -32: The color depth is 32 bits. @30: The refresh rate is 30Hz. saveenv boot 2) Change the westom.ini file at the /etc/xdg/weston location, Change the resolution you want in [output] part. [output] #name=HDMI-A-1 #mode=640x480@60 #transform=rotate-90 3)Reboot the board, and run the "modetest -p" command see if your change is effective
記事全体を表示
  This article is an example for users to change the DDR clock on i.MX6ULL board Environment: Hardware : i.MX6ULL EVK board Concept of MMDC controller clock source on i.MX6ull Consult Chapter 18 Clock Controller Module(CCM) in the I.MX 6ull reference manual. The MMDC clock source is shown in Figure 23.3.3.1:   Figure 23.3.3.1 MMDC Clock Source Figure 23.3.3.1 shows the clock source path diagram of MMDC, which is mainly divided into three parts. 1. CBCMR[PRE_PERIPH2_CLK_SEL] : The pre_periph2 clock selector, which is the pre-selector of periph2_clkd, is controlled by the PRE_PERIPH2_CLK_SEL bit (bit22:21) of the CBCMR register. 2. CBCDR[PERIPH2_CLK_SEL] : periph2_clk clock selector, controlled by the PERIPH2_CLK_SEL bit (bit26) of the CBCDR register,When it is 0, pll2_main_clk is selected as the clock source of periph2_clk. When it is 1, periph2_clk2_clk is selected as the clock source of periph2_clk. 3. CBCDR[FABRIC_MMDC_PODF] : It is a frequency divider. The frequency division value is set by the FABRIC_MMDC_PODF bit (bit5:3) of the CBCDR register. It can be set to 0~7, corresponding to 1~8 frequency divisions respectively. To configure the clock source of the MMDC to 396MHz, it must be set to 1 here, so FABRIC_MMDC_PODF=0. The above is the clock source setting of MMDC. Implementation Step 1 : git clone the uboot code from NXP github web $ git clone https://github.com/nxp-imx/uboot-imx.git Step 2 : Modify the different frequencies of DDR by modifying the following files : uboot-imx/board/freescale/mx6ullevk/imximage.cfg As default BSP code, our DDR run frequency is 400MHz (Actually, it's 396MHz), If you want DDR to boot at 132MHz, we need to configurate the CCM_CBCDR[FABRIC_MMDC_PODF] bit,  from this bit content, we need to set it to 010. The frequency division value is 3 based on 396MHz   Change code as following: DATA 4 0x020c4014 0x00018910, Add this code in imximage.cfg file. Step 3 : Re-compile the uboot and flash the uboot to the board. Result Now, We can see that DDR is running at successfully at 132MHz. Before modification:   After modification:      
記事全体を表示
Hello everyone, in this post we will control one (or more) WS2812 LEDs from a Linux UserSpace application, communicating with Cortex M33 through RPMSG.  Required materials: FRDM-IMX93 WS2812 LED/Strip Attached wsled.c (userspace application) Attached ws2812_m33_project (Source code of firmware for M33)   Environment: Linux Kernel 6.6 arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-eabi SDK 24.12.00   This is the block diagram of the application:        CORTEX M33 SIDE.  From WS2812  LED datasheet, we can see the timing must be precise, that is the reason we will use the Cortex M33 (Real time applications):    As we can see, the timing just accept tolerance of 150ns, that is the reason is preferred to use the Cortex M33 instead of control with Linux that is in charge of other tasks.    The function that we will implement to send Zero and One is:  void WS2812B_send_bit(uint8_t bit) { if (bit) { // Send "1" RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 1); for (int i = 0; i < HIGH_ONE_CYCLES; i++) __asm__("NOP"); RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 0); for (int i = 0; i < LOW_ONE_CYCLES; i++) __asm__("NOP"); } else { // Send "0" RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 1); for (int i = 0; i < HIGH_ZERO_CYCLES; i++) __asm__("NOP"); RGPIO_PinWrite(WS2812B_LED_RGPIO, WS2812B_LED_RGPIO_PIN, 0); for (int i = 0; i < LOW_ZERO_CYCLES; i++) __asm__("NOP"); } }     Testing and measuring the toggle timing with the RGPIO driver of Cortex M33, we could find the best number of NOP instructions to adjust with the required timing according to datasheet, and the results with core running at 200MHz are:    Parameter  Number of NOP times  HIGH_ONE_CYCLES  22  (T1H: 700 ns)  LOW_ONE_CYCLES  12  (T1L: 600 ns)  LOW_ZERO_CYCLES  20  (T0L: 800 ns)  HIGH_ZERO_CYCLES  6    (T0H: 350 ns)      Zero:   One:   Taking in mind this information, we can start to develop our application. From Cortex M33, we created a little protocol, that will wait for instructions to do.    For example, the expected string to fill the RPMSG buffer is:    Index  Purpose  Example  app_buf[0]  Command ('c' or 't')  'c' = store color in buffer  't' = show colors on LEDs  app_buf[1]  Red component (0–255)  0xFF  app_buf[2]  Green component (0–255)  0x00  app_buf[3]  Blue component (0–255)  0x80  app_buf[4]  LED index (target LED position)  e.g. 0, 1, 2    Commands:    'c'  "Color store"  This command stores the RGB color value into a local buffer, targeting a specific LED (app_buf[4]).  It doesn't update the LED strip immediately, it just prepares the data.  Example of RPMSG received buffer from Cortex A (Linux):   app_buf = { 'c', 0xFF, 0x00, 0x00, 2 };  // Store red color for LED 2     't'  "Transfer"  This command sends the full color buffer to the WS2812 strip, updating the LED colors.  The RGB values in the buffer are ignored, it simply triggers an update based on previously stored data.  Example of RPMSG received buffer from Cortex A (Linux):  app_buf = { 't', 0, 0, 0, 0 };  // Transfer the buffered colors to the LED strip     You can modify the code to add your custom commands like change number of LEDs on the strip, or change the GPIO, etc. Currently, the number of WS2812 LEDs supported is defined in software by NUM_RGB_LEDS. As default is 8 LEDs.    I will attach the full code for Cortex M33 firmware, it was tested with arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-eabi and SDK 2_15, SDK 2_16 and SDK 24.    In this example, the EXP_GPIO_IO24 of FRDM-IMX93 was used to control the LED Strip.   CORTEX A55 SIDE.  For Cortex A55 (Linux side), we developed an userspace application, that will create the structure for the buffer to send to the Cortex M33 and send through RPMSG using the imx_rpmsg_tty included on the NXP BSP. You can find the userspace application attached.    As we know, the imx_rpmsg_tty creates the tty channel called ttyRPMSG31 under /dev. So, this userspace application communicates directly with the device /dev/ttyRPMSG31 to send the buffer with the required structure for Cortex M33.    EXAMPLE OF USAGE.    STEP 1. Compile firmware for Cortex M33 and store in FRDM-IMX93 under /lib/firmware to use with remoteproc:   STEP 2.  Compile or cross-compile the userspace application (attached.)  To compile on the platform:  root@imx93evk:~# gcc wsled.c -o wsled root@imx93evk:~# ls wsled wsled.c Also, we can copy the wsled under /bin to practicity. root@imx93evk:~# wsled Error: -c <red> <green> <blue> is required. WS2812 Usage: wsled -c <red> <green> <blue> [-n <led_position>] Load the color of exact LED to the buffer wsled -t Shows the colors to the LEDs   STEP 3. To run the entire example: boot the board and load the firmware for cortex M33 with remoteproc: root@imx93evk:~# cd /sys/class/remoteproc/remoteproc0 root@imx93evk:/sys/class/remoteproc/remoteproc0# echo ws2812_m33.elf > firmware root@imx93evk:/sys/class/remoteproc/remoteproc0# echo start > state  Then, we will receive this from Cortex M33 terminal: RPMSG String Communication Channel FreeRTOS RTOS M33 clock is at: 200000000 Hz Nameservice sent, ready for incoming messages from Cortex-A55! WSLED   Load the imx_rpmsg_tty module in Linux to initialize RPMSG: root@imx93evk:~# modprobe imx_rpmsg_tty   Then, we will have the hello world message from Cortex A (Linux side), but with our buffer format in Cortex M33 console: CMD: h [1]:0x65 [2]:0x6c [3]:0x6c [4]: 111 LEN = 12   Finally, we are ready change colors of the LEDs: Load the buffer (LED 1 = RED, LED 2 = Green, LED 3 = Blue). root@imx93evk:~# wsled -c 0x55 0x00 0x00 -n 1 root@imx93evk:~# wsled -c 0x00 0x55 0x00 -n 2 root@imx93evk:~# wsled -c 0x00 0x00 0x55 -n 3   Show colors on LEDs. root@imx93evk:~# wsled -t    
記事全体を表示
The use case from one customer we are supporting requires to run i.MX93 M33 code with a combination of DRAM and on chip TCM.  However, the examples in the official MCUXpresso SDK release support to run M33 code in TCM only. So we did some customization to achieve that. User can refer to the the attached slides and patches for the details.
記事全体を表示
current bsp fixed the lvds pixel clock up to 74.25Mhz for single channel and 148.5Mhz for dual channel, if customer wants to know why and how to change it, maybe can refer to the enclosed file, hope helpful for you
記事全体を表示
NETC is a TSN capable Ethernet IP, which enables a comprehensive portfolio of Ethernet solutions. One of the major capabilities offered by NETC is the support of Time Sensitive Networking (TSN). TSN is a set of standards developed by IEEE that enables Ethernet to handle time sensitive traffic in addition to best effort traffic. TSN allows time sensitive traffic and best effort traffic to co-exist on the same network, makes Ethernet deterministic with bounded low latency, and with improved reliability and resiliency. This document introduces I.MX95 NETC functional view and capabilities; Analyze IMX95 supported TSN protocols such as 802.1Qbv, 802.1Qav, 802.1Qci, IEEE1588 and stream identifying; Provide Procedures to implement the Qbv use case scenario on I.MX95.
記事全体を表示
Platform: i.MX8MP EVK, SDK 2.16   The rpmsg debug will stuck at rpmsg_queue_recv/rpmsg_lite_send when we use Step Over debug with JLink. The error log on Linux side: [ 42.422658] remoteproc remoteproc0: kicking vq index: 1 [ 42.524256] imx-rproc imx8mp-cm7: imx_rproc_kick: failed (1, err:-62) [ 42.524286] remoteproc remoteproc0: kicking vq index: 0 [ 42.628566] imx-rproc imx8mp-cm7: imx_rproc_kick: failed (0, err:-62)   The demo source code of rpmsg in SDK uses  RL_BLOCK, this flag will cause communication stuck during debug. while (msg.DATA <= 100U) { (void)PRINTF("Waiting for ping...\r\n"); (void)rpmsg_queue_recv(my_rpmsg, my_queue, (uint32_t *)&remote_addr, (char *)&msg, sizeof(THE_MESSAGE), ((void *)0), RL_BLOCK); msg.DATA++; (void)PRINTF("Sending pong...\r\n"); (void)rpmsg_lite_send(my_rpmsg, my_ept, remote_addr, (char *)&msg, sizeof(THE_MESSAGE), RL_BLOCK); }   The solution for rpmsg step over debug is that we need to use RL_DONT_BLOCK in sdk.    
記事全体を表示
Introduction There are some cases where it is needed to flash the image from a removable boot source (e.g. an SD card) to another boot source (e.g. eMMC), according to our documentation this can be done via dd but this does not work in the case you would like to do all the process in the board caused by the eMMC partition structure. Required equipment. i.MX93 FRDM board (this is the selected board for this post, it works for others). Debug USB-C cable. Data USB-C cable. Micro SD (64GB memory used in this test). Personal computer. The default partition configuration for an eMMC device is as follows: Where: - Boot areas are used for bootloader and environment configurations. - Replay-protected memory-block area (RPMB) is used to store secure data. - User area used for application data such as file system, usually divided in two or more partitions. In the case of an image, the eMMC is organized according to the next diagram: - Boot area 1 is used to store SPL and U-boot with no file system in a fixed offset according to each processor as mentioned in i.MX Linux User's Guide section 4.3 Preparing an SD/MMC card to boot. - User area partition 1 uses a FAT format where Kernel and Device Tree files are stored. - User area partition 2 is used for root file system with Ext3/Ext4 format. Exception Our documentation has a method to flash .wic image which contains all the mentioned above or each part manually using an SD card connected to a host Linux machine via dd command: sudo dd if=<image name>.wic of=/dev/sdx bs=1M && sync Or set up the partitions manually such as bootloader: sudo dd if=<U-Boot image> of=/dev/sdx bs=1k seek=<offset> conv=fsync Also, copying the kernel image and DTB file and the root file system as mentioned in i.MX Linux User's Guide. This method works for SD card since the data is stored in user area and the offset changes to burn the bootloader. This fails when we try to flash the image from SD card to eMMC. How to reproduce the issue? First, we need to erase the eMMC, here a post to achieve this task. Format boot partition of eMMC from U-boot - NXP Community How to flash image from SD card to eMMC? With the eMMC erased, we need a boot source to store and flash the image, in this case the SD card. Once the image is flashed into the Micro SD, we need to copy the necessary files such as bootloader and image. By default, our BSP has a User Area space of <>GB and we need to increase it to save the bootloader and the image, here the steps: Verify the device and partition numeration: lsblk The command to increase the size of the partition is the next: parted /dev/<storage unit> unit MiB resizepart <partition> <size in bytes> And the command to apply the changes is: resize2fs /dev/<storage and partition unit>  In this case, the device and partition we need to change is mmcblk0p2 so, the command is as follows: parted /dev/mmcblk0 unit MiB resizepart 2 10000 I increased the partition size by 10000 MB; this will be enough to store the required files. And now, we need to apply the changes: resize2fs /dev/mmcblk0p2 In the board will look like this: Now, let's copy the bootloader and root file system in SD. In this post we will use SCP: Now, we need to boot from SD card and run the next commands: As is mentioned in Linux User's guide, we need to flash the .wic image. This contains all the necessary data to flash the entire image but when flashing from SD card to eMMC we need to follow additional steps to unlock the partition used to store the bootloader: sudo dd if=<image name>.wic of=/dev/sdx bs=1M && sync Disable write protection: echo 0 > /sys/block/<storage and partition unit>/force_ro And flash the bootloader: dd if=<bootloader> of=/dev/<storage and partition unit> bs=1K seek=0 In the board will look like this: With this process now it is needed to reboot the board, change boot mode switches to boot from eMMC, and the board will boot normally, the user can perform an image flashing to simplify development workflow and also an alternative to update OS without external host dependencies.      
記事全体を表示
Hello, this post describes how you can add Japanese Language to the Yocto BSP. There are just a few steps to achieve. It was tested on the i.MX93-FRDM board, i.MX93-EVK and i.MX8M (Family). And Linux kernel 6.6.36.   The first step before to start your board building according to the Yocto Project User's Guide, is adding the below lines to the local.conf file: GLIBC_GENERATE_LOCALES = "en_US.UTF-8 ja_JP.UTF-8" IMAGE_LINGUAS = "en-us ja-jp" IMAGE_INSTALL:append = " \ glibc-gconv-euc-jp \ glibc-gconv-sjis \ glibc-gconv-utf-16 \ glibc-utils \ fontconfig \ ttf-bitstream-vera \ ttf-dejavu-sans \ "   Where:  glibc-gconv-*: Adds Japanese encoding conversions.   After building, flash the Image to the board and boot it. You can check if the Japanese font was installed successfully with: root@imx93frdm:~# locale -a C POSIX en_US en_US.utf8 ja_JP ja_JP.utf8   We can see it was installed successfully: ja_JP ja_JP.utf8   Then, we can change the Language at Runtime with: root@imx93frdm:~# export LANG=ja_JP.UTF-8 root@imx93frdm:~# export LC_ALL=ja_JP.UTF-8   Finally, probe with a command that supports Japanese outputs like "date": root@imx93frdm:~# date 2024年 2月 27日 火曜日 17:29:11 UTC     I hope this information can helps to you.   Best regards, Salas.
記事全体を表示
share the document for ov5640 support on imx93 evk with 6.12 bsp
記事全体を表示
We are pleased to announce that Config Tools for i.MX v25.06 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) • DDR – Support for i.MX 91 is added. – Synchronized with BSP Q2 release – Support for the i.MX 91 FRDM board is added. – Support for the i.MX 93 FRDM board is added. – Spectrum support for i.MX 95 and i.MX 943 is spread. – The Address mirroring option in the UI for all mscale devices with DDR3L and DDR4 is exposed. – DDR3L support for i.MX 8M and i.MX 8MM is added. – Linux support for code generation (beta) is added. • SerDes tool – i.MX 943 support (Beta) is added. • Clocks – Support for read-only element settings is added. – Filtering all settings of Initialization modules in the Details view is supported. • Peripherals – A wizard to export the Registers view data in the CSV format is supported. – Performance of the tool is improved. • An ability to export/import Expansion Boards and Expansion Headers is added.
記事全体を表示
This guide provides a clear overview of how different versions of GUI Guider integrate with LVGL and the supported rendering backends: DRM and Wayland. It also explains how to configure and run your application based on the selected backend. Switching between backends is straightforward—simply modify a few lines in the lv_conf.h file, located in the lvgl folder of the code generated by GUI Guider.   Default Rendering Backends by GUI Guider Version GUI Guider Version LVGL v8 LVGL v9 1.9.1 DRM WAYLAND 1.9.0 WAYLAND WAYLAND   Note: Only one configuration (DRM or Wayland) can be used at a time. Configuration Settings in lv_conf.h To use DRM, set the following: #define LV_USE_WAYLAND 0 #define LV_USE_LINUX_DRM 1   To use Wayland, set: #define LV_USE_WAYLAND 1 #define LV_USE_LINUX_DRM 0   Running LVGL with DRM Before launching the gui_guider binary in DRM mode, you must stop the Weston service: systemctl stop weston ./gui_guider Note: These steps must be executed via the debug console or over SSH, as stopping Weston will disable the desktop environment and make the local display unavailable Running LVGL with Wayland No special steps are required. Simply run the binary: ./gui_guider   You can refer to the following guides to learn how to compile GUI Guider binaries according to the version you are using: Build GUI Guider projects for iMX93 (GUI GUIDER 1.9.X)  Build GUI Guider projects for iMX93 (GUI GUIDER 1.6.x, 1.7.x, 1.8x)   
記事全体を表示
The documentation is about to present a detailed build steps to implement the verification of the integrity of the rootfs for i.MX8ULP.
記事全体を表示
the enclosed code is based on How to fuse key through nvmem on i.MX93 - NXP Community and modified for the imx8mp, this article about how to fuse mac address via fuse command in the uboot or nvmem in the kernel  ================================================================ Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design.  Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
記事全体を表示
This guide walks you through the required steps to prepare your development environment and hardware for debugging the M core on the FRDM-IMX93 board using the MCU-LINK Pro. You’ll install the necessary firmware, perform minor hardware modifications, compile and flash a binary, and finally, initiate a debug session using MCUXpresso for VS Code. Requirements: FRDM-IMX93 Board MCU-LINK Pro Debug Probe Soldering Station (for minor rework) PC Host with MCUXpresso for VS Code installed Adapter Cables   Install Segger Firmware on MCU-LINK Pro By default, the MCU-LINK Pro does not support i.MX processors. Installing the Segger firmware is essential for proper debugging. Follow the firmware update guide to update your MCU-LINK Pro.   Rework the FRDM-IMX93 Board The FRDM-IMX93 uses UART5 (shared with the BT module) for debug pins, which causes conflicts. To enable reliable debugging, remove the following resistors: R3017 R3018 Note: After this modification, the Bluetooth module will no longer function under Linux. Schematic: FRDM BOARD:   Note: After this rework we can't use the Bluetooth module in Linux   Compile the Binary for the M Core Ensure MCUXpresso for VS Code is properly installed.   Import the iMX93-EVK SDK   Import "hello world" example Ensure that we are compiling a debug binary   Build Project   Flash the Binary using UUU Tool Connect the FRDM Board to your Host PC via USB   Enter Fastboot Mode in U-Boot Terminal => fastboot 0   On your Host PC, navigate to the binary location and flash it using the next commands: $ cd <project_location>/armgcc/debug/ $ uuu -b fat_write sdk20-app.bin mmc X:1 hello_world.bin Note: replace the X with 0 if you are booting from eMMC or 1 if you are booting from SD Card   Connect MCU-LINK Pro to the Target To set up debugging, connect the FRDM-IMX93 board to your host computer using the MCU-LINK Pro and the J-LINK Adapter for Cortex-M. FRDM-IMX93 Debug connector:   Required Connections Use the following pin mapping between the J-LINK Adapter and the FRDM-IMX93 debug connector:   J-LINK ADAPTER        -->         FRMD-IMX93  V REF        -->      3.3v(RPI Connector pin 1 )  SWDIO        -->      SWDIO (P14 pin 2)  SWCLK        -->      SWCLK (P14 pin 1)  GND        -->      GND (P14 pin 3)   Make sure all connections are secure before powering on the board.   Launch the M Core from U-Boot Terminal Use the following commands in the U-Boot terminal: => fatload mmc X:1 80000000 hello_world.bin; cp.b 0x80000000 0x201e0000 0x10000; => bootaux 0x1ffe0000 0 Note: replace the X with 0 if you are booting from eMMC or 1 if you are booting from SD Card   Start the Debug Session Once the M core is launched, you can start your debug session in VS Code using MCUXpresso:        With the MCU-LINK Pro configured, the FRDM-IMX93 reworked, and the binary successfully flashed and executed, you are now ready to debug applications on the M core using MCUXpresso and VS Code. This setup enables a reliable development workflow for i.MX93-based projects.
記事全体を表示
Introduction. In some cases, such as development stages, testing, validate flash process from zero, etc. It is needed to erase the eMMC storage device, here is described the process and the required equipment: Required equipment. i.MX93 FRDM board (this is the selected board for this post, it works for others). Debug USB-C cable. Data USB-C cable. Micro SD (16GB recommended). Personal computer. How to erase the eMMC? This method will use another boot source (Micro SD) to erase the eMMC so, it is needed to flash the Micro SD with at least the bootloader (U-boot), you can use a prebuilt image for the EVK board, it can be downloaded from the following link. But, in the case of i.MX93 FRDM board, there is no pre-built image available and needs to be build: The FRDM-IMX93 BSP release is based on i.MX SW 2024 Q3 release with Yocto Project 5.0 (Scarthgap). To build FRDM-IMX93 image from source code, please first check i.MX Yocto Project User's Guide to get familiar with Yocto project and Yocto build. Then please follow below steps to build image for FRDM-IMX93. 1. Download i.MX SW 2024 Q3 BSP Release: $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml $ repo sync 2. Integrate FRDM-MX93 layer into Yocto code base: $ cd ${MY_YOCTO}/sources $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git 3. Yocto Project Setup: $ MACHINE=imx93frdm DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-setup.sh -b frdm-imx93 4. Build images: $ bitbake imx-image-full The flashing process can be consulted here. Once the board is flashed, we need to change the boot switches to boot from Micro SD and turn-on the board. To debug this process, we will use Tera Term terminal with the board connected from the Micro USB debug cable to the PC and select the next configuration: Please verify that you are selecting the corresponding COM for Cortex-A debug. After boot we need to press a key, and the board will enter to U-boot. So, then we need to select the partition of the eMMC with the next command: u-boot=> mmc dev <storage device> <partition> In the case of the eMMC, the storage device corresponds to the device "0" and if the device has an image flashed into the eMMC e.g. Linux, the device will have three partitions from 0 to 2. The next command will select the eMMC and the boot partition area: u-boot=> mmc dev 0 0 switch to partitions #0, OK mmc0(part 0) is current device Depending on the device, image, etc. This partition size can vary so, we need to know how many blocks it has. We can use the next command that will let us know the max address value that is assigned to this partition by getting an error on the address that is out of the range. u-boot=> mmc read ${loadaddr} 0x7fffffff 1 MMC read: dev # 0, block # 2147483647, count 1 ... MMC: block number 0x80000000 exceeds max(0x1d5a000) 0 blocks read: ERROR Now, with this information, we are able to erase the entire partition with the next command: u-boot=> mmc erase 0 0x1d5a000 MMC erase: dev # 0, block # 0, count 30777344 ... 30777344 blocks erased: OK As mentioned before, the device has multiple partitions so, this process needs to be done in each partition Boot area Partition. User Area 1 Partition. User Area 2 Partition. But the process is the same, let's change the partition to User Area 1: u-boot=> mmc dev 0 1 switch to partitions #1, OK mmc0(part 1) is current device  Confirm the size of the partition: u-boot=> mmc read ${loadaddr} 0x7fffffff 1 MMC read: dev # 0, block # 2147483647, count 1 ... MMC: block number 0x80000000 exceeds max(0x2000) 0 blocks read: ERROR And erase it: u-boot=> mmc erase 0 0x2000 MMC erase: dev # 0, block # 0, count 8192 ... 8192 blocks erased: OK And let's finish with User Area 2 Partition: u-boot=> mmc dev 0 2 switch to partitions #2, OK mmc0(part 2) is current device u-boot=> mmc read ${loadaddr} 0x7fffffff 1 MMC read: dev # 0, block # 2147483647, count 1 ... MMC: block number 0x80000000 exceeds max(0x2000) 0 blocks read: ERROR u-boot=> mmc erase 0 0x2000 MMC erase: dev # 0, block # 0, count 8192 ... 8192 blocks erased: OK With this done, the eMMC is completely erased and you can confirm it by turning off the board, change the boot switched to eMMC, remove the SD card and turn-on the board.  Since there is not a bootable image into the boot source, the board will jump to serial download mode and you can verify connecting the USB data cable to the board and run the next command in UUU: Conclusion. Erasing the eMMC of the board is optional step in your development stage but also helpful for testing or system recovery (e.g. test manufacture mode). By using a Micro SD you can access to the eMMC and do all the modifications in the partitions that you want without issues. With this you can go to a clean storage state into the boot device and test a new image from scratch or test recovery methods in your design.
記事全体を表示
OK-MX93 SPI2CAN/ADC Release Documentation Overview This document describes how to use the KV11Z SPI2CAN driver to implement IMX93 peripheral interface expansion. The driver connects to the KV11Z microcontroller via SPI interface, extending CAN bus and ADC acquisition capabilities for the IMX93 processor. Key Features: CAN Bus Extension: Provides 1Mbps CAN 2.0A/B communication capability ADC Acquisition Extension: Supports 8-channel 16-bit ADC with 1kHz sampling rate per channel Standard Interface: Fully compatible with Linux CAN Socket API and IIO subsystem High-Performance Transfer: Efficient data transfer architecture based on SPI+DMA+interrupt With this driver, developers can easily implement industrial-grade CAN communication and multi-channel analog signal acquisition on the IMX93 platform. System Architecture System Architecture Diagram Hardware Connection Description IMX93 and KV11Z are connected via standard SPI bus: MOSI: Master Output, Slave Input MISO: Master Input, Slave Output SCLK: SPI clock signal CS: Chip select signal (controlled by GPIO) IRQ: Interrupt signal (KV11Z to IMX93) Important Configuration Notes: Must use GPIO CS + DMA method, main controller CS method has known issues For device tree configuration, refer to the  OK-MX93-C.dts  file in the project SPI frequency recommended to be set at 7-12.5MHz, DMA configuration recommended to be enabled Data Flow Diagram Directory Structure . ├── adctest.c ├── build.sh ├── cantest.c └── OKMX93-linux-kernel-6.1.36 ├── arch │   └── arm64 │   └── boot │   └── dts │   └── freescale │   └── OK-MX93-C.dts └── drivers └── net └── can └── kv11z_spi2can.c Core Components 1. kv11z_spi2can.c - Core Driver Program Function: KV11Z SPI2CAN/ADC Linux kernel driver Implements CAN network device interface, supports standard Linux CAN Socket API Implements IIO ADC device interface, supports multi-channel ADC data acquisition Communicates with KV11Z microcontroller via SPI protocol Supports interrupt-driven high-performance data transfer Key Features: CAN Function: Supports standard and extended CAN frames, configurable baud rate and filters (under development) ADC Function: 8-channel ADC acquisition, supports triggered buffer mode and direct read mode High Performance: Multi-threaded architecture, supports concurrent CAN and ADC operations Configurable: Rich module parameters, supports runtime tuning Module Parameters: # CAN Configuration g_can_bitrate=1000000 # CAN baud rate (default 1Mbps) # ADC Configuration g_adc_mask=0xFF # ADC channel enable mask (default all channels) g_adc_sample_rate=1000 # ADC sampling rate (default 1kHz) # SPI Configuration spi_speed=7000000 # SPI bus speed (default 7MHz) transfer_time_us=30 # SPI transfer interval (default 30μs) # Debug Options debug=0 # Debug information switch (0=off, 1=on) 2. adctest.c - ADC Test Application Function: ADC data acquisition test tool Supports two ADC reading modes: direct mode and buffer mode Provides real-time data display and CSV file output Supports timestamps and performance statistics Hardware compatibility detection and channel validation Key Features: Dual Mode Support: Direct read mode (sysfs) and buffer mode (IIO buffer) Flexible Configuration: Configurable channel mask and sampling rate Data Export: Supports CSV format data export for subsequent analysis Real-time Display: Color terminal output and statistical information Usage Examples: # Compile gcc -O2 -o adctest adctest.c # Buffer mode, enable channels 0-3, with timestamps ./adctest -m 1 -c 0x0F -t # Direct mode, 500ms sampling interval ./adctest -m 0 -d 500000 # Save data to CSV file ./adctest -m 1 -f /tmp/adc_data # View help ./adctest -h 3. cantest.c - CAN Bus Test Tool Function: Comprehensive CAN bus testing and benchmarking tool Supports CAN frame generation, transmission and reception Provides MD5 verification to ensure data integrity Supports file transfer over CAN bus Real-time performance monitoring and statistical analysis Key Features: Performance Testing: Supports bulk transmission testing of large numbers of frames Data Integrity: MD5 verification ensures transmission data integrity File Transfer: Supports arbitrary file transfer over CAN bus Real-time Monitoring: Progress bar display, FPS statistics, error statistics, etc. Usage Examples: # Compile gcc -O2 -o cantest cantest.c # Transmitter: Send 1000 random CAN frames ./cantest -i can0 -t -n 1000 -d 1000 # Receiver: Receive CAN frames and verify ./cantest -i can0 -r # File transfer transmitter ./cantest -i can0 -t -f /path/to/file # File transfer receiver ./cantest -i can0 -r -f /path/to/output # View help ./cantest -h Quick Start 1. Environment Setup Ensure cross-compilation toolchain is installed: # Set cross-compilation environment source environment-setup-aarch64-toolchain 2. Build System # Complete build ./build.sh all # Or step-by-step build ./build.sh uboot ./build.sh kernel ./build.sh apps ./build.sh mkfs 3. Deploy Driver # Load driver module insmod kv11z_spi2can.ko # Configure CAN interface ip link set can0 type can bitrate 1000000 ip link set can0 up # Verify ADC device ls /sys/bus/iio/devices/ 4. Function Testing # Test ADC function ./adctest -m 1 -c 0xFF -t # Test CAN function ./cantest -i can0 -t -n 100 Technical Specifications Hardware Requirements Main Controller: OK-MX93 development board (IMX93 processor) Co-processor: KV11Z microcontroller Interface: SPI bus connection CAN: Supports CAN 2.0A/B protocol ADC: 8-channel 12-bit ADC Performance Metrics CAN Baud Rate: Up to 1Mbps ADC Sampling Rate: Up to 1kHz (per channel) SPI Speed: Up to 12.5MHz Latency: CAN frame transmission latency ≤1ms Throughput: Supports 7500 frames/second CAN transmission Software Compatibility Kernel Version: Linux 6.1.36 Architecture: ARM64 (aarch64) Compiler: GCC cross-compilation toolchain API: Standard Linux CAN Socket API, IIO subsystem API Troubleshooting Common Issues Compilation Failure Check if cross-compilation environment is correctly set Confirm all dependency packages are installed Driver Loading Failure Check if device tree configuration is correct Confirm SPI interface and GPIO configuration CAN Communication Abnormal Check CAN bus hardware connections Verify if baud rate configuration matches ADC Data Abnormal Check ADC channel mask configuration Verify if sampling rate setting is reasonable Debugging Methods # Enable driver debug information echo 1 > /sys/module/kv11z_spi2can/parameters/debug # View system logs dmesg | grep kv11z # Check device status cat /proc/interrupts | grep kv11z Technical Support For technical support, please contact the development team or refer to relevant technical documentation. Note: This software package is only applicable to OK-MX93 development board. Please ensure hardware configuration is correct before use.Other boards please porting by yourself. Disclaimer: "Any support, information, and technology ("Materials") provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction."
記事全体を表示
What we need?  USB cable Windows Host PC MCU-LINK PRO What Do You Gain? With this firmware upgrade, you will be able to debug the M core of i.MX processors (such as i.MX8 and i.MX9). Also, the cost advantage due to the MCU-LINK PRO is currently the most affordable debugger available for i.MX processors.   Firmware Upgrade Steps   Install Required Tools Install the MCUXpresso IDE, or use the MCUXpresso Installer for VS Code to install the necessary software tools.     Download Firmware Get the latest firmware from the Segger web page   Save Firmware Save the downloaded firmware in the following directory: C:\nxp\LinkServer_1.6.133\MCU-LINK_installer\probe_firmware   Backup Old Firmware Rename the existing firmware file to keep a backup.   Example: Rename firmware.s19 to old_firmware.s19   Set Jumper and Connect Place a jumper on J4 and connect the MCU-LINK PRO to the host PC via USB.   Open LinkServer CLI Launch the LinkServer CLI. If it's not installed, download it from NXP web page.   Run the Update Script Execute the following commands in the terminal: $ cd MCU-LINK_installer $ scripts\program_JLINK.cmd   Start Firmware Flash Once the MCU-LINK PRO is detected, press any key to flash the Segger firmware.     Finalize Update After a successful update, remove the jumper from J4, disconnect and reconnect the MCU-LINK PRO   Verify Installation You can confirm that the debug probe is recognized using MCUXpresso IDE, or MCUXpresso for VS Code     References: MCU-Link installation   
記事全体を表示
  Platform & BSP : i.MX8MPlus EVK , L6.12.3, uboot lf_v2024.04   The attachments enable the i.MX8MPlus pci function in uboot. lspci in Linux root@imx8mpevk:~# lspci -nn 00:00.0 PCI bridge [0604]: Synopsys, Inc. DWC_usb3 / PCIe bridge [16c3:abcd] (rev 01) 01:00.0 Ethernet controller [0200]: Marvell Technology Group Ltd. Device [1b4b:2b42] (rev 11) pci test results in uboot:  u-boot=> pci BusDevFun VendorId DeviceId Device Class Sub-Class _____________________________________________________________ 00.00.00 0x16c3 0xabcd Bridge device 0x04 01.00.00 0x1b4b 0x2b42 Network controller 0x00 u-boot=> pci bar 00.00.00 ID Base Size Width Type ---------------------------------------------------------- 0 0x0000000018000000 0x0000000000100000 32 MEM u-boot=> pci regions 00 Buses 00-01 # Bus start Phys start Size Flags 0 0x0000000000000000 0x000000001ff80000 0x0000000000010000 io 1 0x0000000018000000 0x0000000018000000 0x0000000007f00000 mem 2 0x0000000040000000 0x0000000040000000 0x0000000016000000 mem sysmem 3 0x0000000058000000 0x0000000058000000 0x00000000a8000000 mem sysmem 4 0x0000000100000000 0x0000000100000000 0x00000000c0000000 mem sysmem u-boot=> pci header 00.00.00 vendor ID = 0x16c3 device ID = 0xabcd command register ID = 0x0007 status register = 0x0010 revision ID = 0x01 class code = 0x06 (Bridge device) sub class code = 0x04 programming interface = 0x00 cache line = 0x08 latency time = 0x00 header type = 0x01 BIST = 0x00 base address 0 = 0x18000000 base address 1 = 0x00000000 primary bus number = 0x00 secondary bus number = 0x01 subordinate bus number = 0x01 secondary latency timer = 0x00 IO base = 0x10 IO limit = 0x00 secondary status = 0x0000 memory base = 0x1820 memory limit = 0x1810 prefetch memory base = 0xfff0 prefetch memory limit = 0x0000 prefetch memory base upper = 0x00000000 prefetch memory limit upper = 0x00000000 IO base upper 16 bits = 0x0000 IO limit upper 16 bits = 0x0000 expansion ROM base address = 0x18100000 interrupt line = 0xff interrupt pin = 0x01 bridge control = 0x0000 u-boot=> pci header 01.00.00 vendor ID = 0x1b4b device ID = 0x2b42 command register ID = 0x0006 status register = 0x0010 revision ID = 0x11 class code = 0x02 (Network controller) sub class code = 0x00 programming interface = 0x00 cache line = 0x08 latency time = 0x00 header type = 0x00 BIST = 0x00 base address 0 = 0x1810000c base address 1 = 0x00000000 base address 2 = 0x1820000c base address 3 = 0x00000000 base address 4 = 0x00000000 base address 5 = 0x00000000 cardBus CIS pointer = 0x00000000 sub system vendor ID = 0x0000 sub system ID = 0x0000 expansion ROM base address = 0x00000000 interrupt line = 0xff interrupt pin = 0x01 min Grant = 0x00 max Latency = 0x00
記事全体を表示