i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
View full article
Installing the new release (Ubuntu 22.04) was detected some NXP boards as iMX8MNEVK, iMX8MM-EVK, iMX8MP-EVK and iMX8ULP-EVK had an issue with the WIFI module that basically it does not initialize at boot. Remember, the supported WIFI modules in Ubuntu 22.04 in the EVKs are the following:       • NXP 88W8987       • NXP 88W9098       • NXP 88W8997       • NXP IW416       • NXP 88W8801       • NXP IW612 To initialize the WIFI module of NXP EVKs in Ubuntu 22.04 you can set the following command in console:   sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   That command find the correct driver for our WIFI module and then initialize it, but this only works when Ubuntu is working and if you reset the EVK you need to set the command again.   The definitive solution is create a custom startup script as a service:   Step 1: Go to etc/systemd/system   cd etc/systemd/system   Step 2: In this directory create a new file with the name of your preference but the extension must be .service. You can do it with nano or vim: sudo nano or sudo vim   The file must contain: [Unit] Description=”Wifi Start” [Service] ExecStart=sudo modprobe moal mod_para=nxp/wifi_mod_para.conf [Install] WantedBy=multi-user.target   Now save the file, in my case the name was wifi_start.service.   Step 3: Now we need to enable the script in the startup/boot sequence following the command: sudo systemctl enable wifi_start.service   Remember in wifi_start.service is the name as you saved your file.   Finally, each time you boot your board, the WIFI module will initialize automatically.   Boards tested: iMX8MN (With WIFI module NXP 88W8987) iMX8MM (With WIFI module NXP 88W8987) iMX8MP (With WIFI module NXP 88W8997) iMX8ULP (With WIFI module NXP IW416)  
View full article
Hello everyone! In this quick example its focused on how to customize uboot code to generate an uboot image with a silent console so its speed up the flash and boot time, this may provide helpful for customers who have a bigger images or just want to have a silent console. Note: this should not be enabled if the image is still being under test, since this will disable all communication with the debug terminal and there won't be boot messages. Requirements: I.MX 8M Nano DDR4 EVK i.MX 8M Nano EVK Prebuilt image (6.1.1-1.0.0) UUU tool First clone the code from the uboot repository: $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.1.1-1.0.0 $ cd uboot-imx After we get the code, then proceed to enable the silent console in the uboot defconfig: $ nano configs/imx8mn_ddr4_evk_defconfig CONFIG_SILENT_CONSOLE=y CONFIG_SILENT_U_BOOT_ONLY=y For this to actually work we need to create the silent environmental variable and give it a value different from "0": $ nano include/configs/imx8mn_evk.h "silent=1\0"      \ As specified in our Linux porting guide: Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command, set Target-Machine to the machine you are building for. See Section "Build configurations" in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG) Set up the host terminal window toolchain environment: $ source/opt/fsl-imx-xwayland/6.1.1/environment-setup-aarch64-poky-linux $ export ARCH=arm64 Build uboot binary: $ make distclean $ make imx8mn_ddr4_evk_defconfig $ make Build ARM Trusted Firmware (ATF) $ cd .. $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.1.1-1.0.0 $ cd imx-atf/ $ make PLAT=imx8mn bl31 In case you get the error aarch64-poky-linux-ld.bfd: unrecognized option '-Wl,-O1' $ unset LDFLAGS Download the DDR training & HDMI binaries $ cd .. $ mkdir firmware-imx $ cd firmware-imx $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.19.bin $ chmod a+x firmware-imx-8.19.bin $ ./firmware-imx-8.19.bin Accept EULA and the firmware will be deployed. Download imx-mkimage and build the boot image $ cd .. $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.1.1-1.0.0 $ cd imx-mkimage $ cp ../uboot-imx/spl/u-boot-spl.bin iMX8M/ $ cp ../uboot-imx/u-boot-nodtb.bin iMX8M/ $ cp ../uboot-imx/arch/arm/dts/imx8mn-ddr4-evk.dtb iMX8M/ $ cp ../imx-atf/build/imx8mn/release/bl31.bin iMX8M/ $ cp ../firmware-imx/firmware-imx-8.19/firmware/ddr/synopsys/ddr4_* iMX8M/ $ cp ../uboot-imx/tools/mkimage iMX8M/mkimage_uboot $ make SOC=iMX8MN flash_ddr4_evk After this we can download our uboot image to our board, we can either use the uboot image for boot or for flashing purpose only. We can compare the time it takes using UUU with a standard pre-built image uuu -V -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-full-imx8mnevk.wic It takes 485.5 seconds using normal uboot with debug console enabled. uuu -V -b emmc_all flash.bin imx-image-full-imx8mnevk.wic It takes 477.5 seconds using silent uboot console. Even if the speed is not greatly improved (~8 seconds), in larger files it could help to speed up flashing, even if wants to have the console silent is a good option. Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
View full article
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there.  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
View full article
Customer is asking high-capacity external storage(for example >64GB) support on i.MX BSP, ext4 is ok for HC storage, but it can’t be supported by Windows. Pls find NFTS and exFAT support status on Linux BSP below: Updated test result on L5.4.70.2.3.0 and L6.1.22: L5.4.70.2.3.0 1.You can enable ntfs support in kernel config as below,  ntfs can be mounted normally, but you can only modify existing file content in disk, you can’t create/delete/rename file on disk. > File systems > DOS/FAT/NT Filesystems   Log: root@imx8mpevk:~# mount -t ntfs /dev/sda1 /mnt/fat/ [  662.732869] ntfs: volume version 3.1. root@imx8mpevk:~# cp ntfs-3g /mnt/fat/ cp: cannot create regular file '/mnt/fat/ntfs-3g': Permission denied root@imx8mpevk:~# ls /mnt/fat/ 111.png  Image_org  System Volume Information  gpuinfo.sh root@imx8mpevk:~# vi /mnt/fat/gpuinfo.sh root@imx8mpevk:~# umount /mnt/fat/ root@imx8mpevk:~# ntfs file system can be accessed via ntfs-3g in user space as below //build: wget https://tuxera.com/opensource/ntfs-3g_ntfsprogs-2017.3.23.tgz tar zxvf ntfs-3g_ntfsprogs-2017.3.23.tgz cd ntfs-3g_ntfsprogs-2017.3.23/ source ../../sdk/environment-setup-aarch64-poky-linux   ./configure --host=aarch64-linux --build=aarch64-poky-linux --disable-shared --enable-static   make   ls /src/ntfs-3g   //put it into rootfs cp ntfs-3g /bin   //test log: root@imx8mpevk:/# [ 1058.724471] usb 1-1: USB disconnect, device number 4 [ 1062.058613] usb 1-1: new high-speed USB device number 5 using xhci-hcd [ 1062.214029] usb-storage 1-1:1.0: USB Mass Storage device detected [ 1062.220986] scsi host0: usb-storage 1-1:1.0 [ 1063.235871] scsi 0:0:0:0: Direct-Access     VendorCo ProductCode      2.00 PQ: 0 ANSI: 4 [ 1063.246185] sd 0:0:0:0: [sda] 15728640 512-byte logical blocks: (8.05 GB/7.50 GiB) [ 1063.254023] sd 0:0:0:0: [sda] Write Protect is off [ 1063.259164] sd 0:0:0:0: [sda] No Caching mode page found [ 1063.264540] sd 0:0:0:0: [sda] Assuming drive cache: write through [ 1063.296946]  sda: sda1 [ 1063.300860] sd 0:0:0:0: [sda] Attached SCSI removable disk   root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh root@imx8mpevk:/# cp /unit_tests/memtool /mnt/fat/ root@imx8mpevk:/# umount /mnt/fat/ root@imx8mpevk:/# ntfs-3g /dev/sda1 /mnt/fat/ root@imx8mpevk:/# ls /mnt/fat/ README  System Volume Information  gpu.sh  gpuinfo.sh  memtool root@imx8mpevk:/#   3.exFAT is not supported on this BSP..   L6.1.22(you can check it on L5.15 and above, should be the same) You can enable ntfs support in kernel config as below, full features can be supported. > File systems > DOS/FAT/EXFAT/NT Filesystems   Pls use ‘-t ntfs3’ during mounting, otherwise it will be mounted as ‘read-only’ Log: root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information' root@imx8ulpevk:~# root@imx8ulpevk:~# cp gpuinfo.sh /mnt/fat/ root@imx8ulpevk:~# umount /mnt/fat/ root@imx8ulpevk:~# root@imx8ulpevk:~# mount -t ntfs3 /dev/sda1 /mnt/fat/ root@imx8ulpevk:~# ls /mnt/fat/ 111.png   Image_org  'System Volume Information'   gpuinfo.sh root@imx8ulpevk:~#   exFAT has been supported in L6.1.22. > File systems > DOS/FAT/EXFAT/NT Filesystems   /dev/sda1 on /run/media/sda1 type exfat (rw,relatime,fmask=0022,dmask=0022,iocharset=utf8,errors=remount-ro) root@imx8ulpevk:~# ls /run/media/sda1 'Certificate of Completion.pdf'             carlife.MP4 Image_org                                  example.tflite L5.4.70_2.3.0                              mx8mp_vpu.txt NXP-5G.mp4                                 sd.mp4 'System Volume Information'                 vela.ini android_p9.0.0_2.1.0-auto-ga_image_8qmek root@imx8ulpevk:~# ls Image_org  gpuinfo.sh root@imx8ulpevk:~# cp gpuinfo.sh /run/media/sda1/ root@imx8ulpevk:~# umount /run/media/sda1 root@imx8ulpevk:~#
View full article
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU   This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. On new window select download SDK Select on new pop-up window download both SDK and documentation Read and accept EULA so the download start Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
View full article
Dynamic debug is designed to allow you to dynamically at runtime  enable/disable  kernel code to obtain additional kernel information. Currently, if ``CONFIG_DYNAMIC_DEBUG`` is set, then all ``pr_debug()``/``dev_dbg()`` and ``print_hex_dump_debug()``/``print_hex_dump_bytes()`` calls can be dynamically enabled per-callsite.    
View full article
This article is rather short that only mentions the script that is needed to make an iMX93EVK act as a USB mass storage device so that whenever you connect your iMX device to a windows/linux system via USB, it should get enumerated something like a usb drive.  The storage that is used in this example is mmc so the expectation is that you have inserted a mmc card in the slot. Below is the script:- #!/bin/sh   # This composite gadget include function: # - MASS STORAGE     # # Exit status is 0 for PASS, nonzero for FAIL # STATUS=0   # Check if there is udc available, if not, return fail UDC_DIR=/sys/class/udc if test "$(ls -A "$UDC_DIR")"; then echo "The available udc:" for entry in "$UDC_DIR"/* do echo "$entry" done else STATUS=1 echo "No udc available!" exit $STATUS; fi   id=1; udc_name=ci_hdrc.0 #back_file=/dev/mmcblk1 back_file=/tmp/lun0.img   mkdir /sys/kernel/config/usb_gadget/g$id cd /sys/kernel/config/usb_gadget/g$id   # Use NXP VID, i.MX8QXP PID echo 0x1fc9 > idVendor echo 0x12cf > idProduct   mkdir strings/0x409 echo 123456ABCDEF > strings/0x409/serialnumber echo NXP > strings/0x409/manufacturer echo "NXP iMX USB Composite Gadget" > strings/0x409/product   mkdir configs/c.1 mkdir configs/c.1/strings/0x409   echo 5 > configs/c.1/MaxPower echo 0xc0 > configs/c.1/bmAttributes   mkdir functions/mass_storage.1 echo $back_file > functions/mass_storage.1/lun.0/file ln -s functions/mass_storage.1 configs/c.1/   echo $udc_name > UDC First execute the script. After that insert the g_mass_storage module in the kernel by executing :- modprobe g_mass_storage file=/dev/mmcblk1 removable=1 In the dmesg output, you will see something like below:-   After that you can connect a C type USB cable to the USB1 port of imx93evk and the other end to any USB ports of a laptop. The moment it is connected, you would be able to see a USB drive similar to what you get when we connect a pen-drive. 
View full article
The HSM Coding-Signing is new. When we follow the instructions in Code-Signing Tool User’s Guide , still has something to overcome, most of them are related to the OS. Actually, Code-Signing Tool User’s Guide  can not give detail every “obvious” step. The purpose of this document is to share the experiences on my system. Hope those experience can give you some clues on your system.     25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt  
View full article
Sometime need standalone compile device tree. Only Linux headers and device tree directory are needed.         
View full article
The table below contains notable updates to the current release of the Reference Manual. The information provided here is preliminary and subject to change without notice. Affected Modules Issue Summary Description Date - - No issues noted -
View full article