i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
The following document contains a list of document, questions and discussions that are relevant in the community based on amount of views. If you are having a problem, doubt or getting started in i.MX processors, you should check the following links to see if your doubt is in there. Yocto Project Freescale Yocto Project main page‌ Yocto Training - HOME‌ i.MX Yocto Project: Frequently Asked Questions‌ Useful bitbake commands‌ Yocto Project Package Management - smart  How to add a new layer and a new recipe in Yocto  Setting up the Eclipse IDE for Yocto Application Development Guide to the .sdcard format  Yocto NFS & TFTP boot  YOCTO project clean  Yocto with a package manager (ex: apt-get)  Yocto Setting the Default Ethernet address and disable DHCP on boot.  i.MX x Building QT for i.MX6  i.MX6/7 DDR Stress Test Tool V3.00  i.MX6DQSDL DDR3 Script Aid  Installing Ubuntu Rootfs on NXP i.MX6 boards  iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP i.MX Design&Tool Lists  Simple GPIO Example - quandry  i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines  Streaming USB Webcam over Network  Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53  Linux / Kernel Copying Files Between Windows and Linux using PuTTY  Building Linux Kernel  Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)  load kernel from SD card in U-boot  Changing the Kernel configuration for i.MX6 SABRE  Android  The Android Booting process  What is inside the init.rc and what is it used for.  Others How to use qtmultimedia(QML) with Gstreamer 1.0
記事全体を表示
This guide is about how to use EVIS to create user nodes and kernels in OpenVX to implement image processing on NPU(i.MX8MP)/GPU(i.MX8QM). Take gaussian filter as an example. It is tested on i.MX8QM and i.MX8MP. User Node Creation from User Kernel 1. Define a user node Register a user kernel by its ID or name For example, #define VX_KERNEL_NAME_GAUSSIAN "com.nxp.extension.gaussian" #define VX_KERNEL_ENUM_GAUSSIAN 100 Get the kernel reference by the ID or name For example, vx_kernel kernel = vxGetKernelByName(context, VX_KERNEL_NAME_GAUSSIAN); vx_kernel kernel = vxGetKernelByEnum(context, VX_KERNEL_ENUM_GAUSSIAN ); Create a user node vx_node node = vxCreateGenericNode(graph, kernel); Set input/output node parameters For example, vx_status status = vxSetParameterByIndex(node, index++, (vx_reference)in_image); status |= vxSetParameterByIndex(node, index++, (vx_reference)out_image); 2. Create InputValidator/OutputValidator functions for the node The validators are only used for graph verification. For example, static vx_status VX_CALLBACK vxGaussianInputValidator(vx_node node, vx_uint32 index) static vx_status VX_CALLBACK vxGaussianOutputValidator(vx_node node, vx_uint32 index, vx_meta_format metaObj) ToDo: a. InputValidator: Get the reference to the parameter object   vx_parameter paramObj = NULL; vx_image imgObj = NULL; paramObj=vxGetParameterByIndex(node, index); vxQueryParameter(paramObj, VX_PARAMETER_REF, &imgObj, sizeof(vx_image)); Check meta-data restriction vxQueryImage(imgObj, VX_IMAGE_FORMAT, &imgFmt, sizeof(imgFmt)); Check consistency with other parameters if (VX_DF_IMAGE_U8==imgFmt) status = VX_SUCCESS; else status = VX_ERROR_INVALID_VALUE; b. OutputValidator Set the meta_format object with expected meta-data for the output status |= vxSetMetaFormatAttribute(metaObj, VX_IMAGE_FORMAT, &imgFmt, sizeof(imgFmt)); status |= vxSetMetaFormatAttribute(metaObj, VX_IMAGE_WIDTH, &width, sizeof(width)); status |= vxSetMetaFormatAttribute(metaObj, VX_IMAGE_HEIGHT, &height, sizeof(height)); 3. Create Initializer function for the node. The initializer is used to specify workdim, global work size and local work size for the user kernel. These parameters are similiar to that in OpenCL. For example,                                                                                    /* workdim, globel offset, globel scale, local size, globel size */ vx_kernel_execution_parameters_t shaderParam = {2,               {0, 0, 0},        {0, 0, 0},        {0, 0, 0},   {0, 0, 0}}; vx_status VX_CALLBACK vxGaussianInitializer(vx_node nodObj, const vx_reference *paramObj, vx_uint32 paraNum) Set attribute to the node vxSetNodeAttribute(nodObj, VX_NODE_ATTRIBUTE_KERNEL_EXECUTION_PARAMETERS, &shaderParam, sizeof(vx_kernel_execution_parameters_t)); Note: The links below are guides about OpenCL on GPU, which are helpful to understand OpenVX implemented on GPU/NPU. OpenCL Work Item Ids: Global/Group/Local OpenCL Programming Guide OpenCL Resources Introduction to OpenCL 4. Create Deinitializer function for the node (Optional) It is used to de-allocate memory allocated at initializer. User Kernel on NPU/GPU Creation 1. Create description of a user kernel For example, vx_kernel_description_t vxGaussianKernelVXCInfo = { VX_KERNEL_ENUM_GAUSSIAN, VX_KERNEL_NAME_GAUSSIAN, nullptr, vxGaussianKernelParam, (sizeof(vxGaussianKernelParam)/sizeof(vxGaussianKernelParam[0])), vxGaussianValidator, nullptr, nullptr, vxGaussianInitializer, nullptr }; 2. Register the new kernel For example, static vx_kernel_description_t* kernels[] = { &vxGaussianKernelVXCInfo, }; 3. Write kernel source implemented on NPU/GPU For example, char vxcKernelSource[] = { "#include \ \n\ \n\ \n\ __kernel void gaussian\n\ ( \n\ __read_only image2d_t in_image, \n\ __write_only image2d_t out_image \n\ ) \n\ { \n\ int2 coord = (int2)(get_global_id(0), get_global_id(1)); \n\ int2 coord_out = coord; \n\ vxc_uchar16 lineA, lineB, lineC, out;\n\ int2 coord_in1 = coord + (int2)(-1, -1);\n\ VXC_OP4(img_load, lineA, in_image, coord_in1, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in2 = coord + (int2)(-1, 0);\n\ VXC_OP4(img_load, lineB, in_image, coord_in2, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int2 coord_in3 = coord + (int2)(-1, 1);\n\ VXC_OP4(img_load, lineC, in_image, coord_in3, 0, VXC_MODIFIER(0, 15, 0, VXC_RM_TowardZero, 0));\n\ int info = VXC_MODIFIER_FILTER(0, 13, 0, VXC_FM_Guassian, 0);\n\ VXC_OP4(filter, out, lineA, lineB, lineC, info); ;\n\ VXC_OP4_NoDest(img_store, out_image, coord_out, out, VXC_MODIFIER(0, 13, 0, VXC_RM_TowardZero, 0)); \n\ }\n\ " }; Note: the source is written by EVIS instructions with less latency. But the EVIS instructions are limited. These fucntions defination can be found in "cl_viv_vx_ext.h" located at "/usr/include/CL/cl_viv_vx_ext.h". Read back the processed data by GPU/NPU to check if the operations are correct. For example, status = vxCopyImagePatch(vx_out_image, &rect, 0, &addressing, data2, VX_READ_ONLY, VX_MEMORY_TYPE_HOST); 4. Build the NPU/GPU source code runtime For example, programObj = vxCreateProgramWithSource(ContextVX, 1, programSrc, &programLen); vxBuildProgram(programObj, "-cl-viv-vx-extension"); 5. Add kernel to the program For example, ... kernelObj = vxAddKernelInProgram(programObj, kernels[i]->name, kernels[i]->enumeration, kernels[i]->numParams, kernels[i]->validate, kernels[i]->initialize, kernels[i]->deinitialize ); ... for(vx_uint32 j=0; j < kernels[i]->numParams; j++) { status = vxAddParameterToKernel(kernelObj, j, kernels[i]->parameters[j].direction, kernels[i]->parameters[j].data_type, kernels[i]->parameters[j].state ); 6. Finalize the kernel creation For example, status = vxFinalizeKernel(kernelObj); Exercise The example is attached. You can build and test it on i.MX8QM or i.MX8MP. Results on i.MX8QM: References: Khronosdotorg/resources.md at master · KhronosGroup/Khronosdotorg · GitHub  Further Reading: OpenVX Vision Image Extension API Introduction - Basic API OpenVX Vision Image Extension API Introduction - DP Dot Products
記事全体を表示
1. HW Environment:     IMX8mp-evk board.     ITE6151 mipi dsi to eDP bridge board.   2. SW Environment:     IMX YOCTO 5.4.24-2.1.0 release.   3. Patch operation:     a. git clone https://source.codeaurora.org/external/imx/linux-imx.git     b. git checkout -b  imx_5.4.24_2.1.0 origin/imx_5.4.24_2.1.0     c. patch -p1 < ../ite6151_mipi2edp_linux_5.4.24_20200921.patch   4. Tested on imx8mp-evk board with DP monitor on 1080p mode: 5. Attached doc list:     IT6151 demo board user guide v1.0.pdf ------  ite6151 bridge board HW guide     it6151_qfn48_v20_20190905-01_end.pdf  ------  ite6151 bridge board SCH     imx8mp_ite6151_mipi2edp_linux_5.4.24_20200921.patch ------  Linux kernel driver patch     Image + imx8mp-evk-it6151.dtb  ------  test image and dtb  
記事全体を表示
This documents describes how to add the NFC support to i.MX8M mini evk running Android Pie. Hardware setup: The i.MX8M mini evk (see i.MX 8M Mini Evaluation Kit | NXP) featuring Raspberry Pi compliant connector, the OM5578/RPI PN7150 demo kit can be used to perform this porting (see NFC Development Kits for Arduino and more|NXP). However a small modification must be done because some of the signals required by PN7150 are not mapped to i.MX8M mini expansion connector pins. OM5578 IRQ signal must be mapped to Raspberry Pi connector pin #19 and OM5578 VEN signal must be mapped to Raspberry Pi connector pin #21. See below a picture of the modification: Then, the two boards can fit together as shown in the picture below: Quick start using demo image: The demo image including support for PN7150, is based on Android P9.0.0 Pie (P9.0.0_1.0.0, 4.14 kernel) i.MX software release (see i.MX Software | NXP). Related documentation can be downloaded from here: https://www.nxp.com/docs/en/supporting-information/android_p9.0.0_1.0.0-ga_docs.zip. Just flash the demo image (downloaded from here:https://www.nxp.com/lgfiles/updates/NFC/ANDROID_P9-0-0_PN7150_IMAGE_8MMEVK.zip) following guidelines from i.MX_Android_Quick_Start document (part of Android P9.0.0_1.0.0 Documentation package mentioned above). The NFC support is then included in the device settings, as shown in below screenshot of the device: Approaching the NFC tag, provided as reference in the OM5578 demo kit, to the NFC Antenna will trigger a sound notification: Unfortunately the Android demo image doesn't embed a web browser, so it won't be automatically open when the NFC tag content (an URL to the demo kit web page) is read. Otherwise (if a web browser is installed) you could see such page opening on the device: Adding PN7150 support to imx-android-pie release: If you wish to add PN7150 support to your imx-android-pie environment, just apply the patches (imx-p9.0.0_1.0.0-ga_pn7150_patches.tar.gz file attached) from the ${MY_ANDROID} source code root folder (refer to i.MX_Android_User_Guide document part of Android P9.0.0_1.0.0 Documentation package mentioned above).  $ patch -p1 -d device/fsl/ <device_fsl.patch  $ patch -p1 -d packages/apps/Nfc <packages_apps_Nfc.patch  $ patch -p1 -d hardware/nxp/nfc <hardware_nxp_nfc.patch  $ patch -p1 -d vendor/nxp <vendor_nxp.patch  $ patch -p1 -d vendor/nxp-opensource/kernel_imx/ <vendor_nxp-opensource_kernel_imx.patch When building, the PN7150 support will then be included to the android image, as shown in the demo image described above. Reference: This porting have been done (demo image and patches creation) following guidelines provided in AN11690_NXP-NCI_Android_Porting_Guidelines document.
記事全体を表示
Recently I published this i.MX Dev Blog post about the Gateworks plugin gst-variable-rtsp-server support for i.MX 6. Now, you can check how to use it on i.MX 8 SoCs as well. 1. Preparing the image In order to use gst-variable-rtsp-server plugin, prepare your machine and distro: Add the following line to conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gst-variable-rtsp-server" Download the attached patch and apply it by doing: $ cd <yocto_path>/sources/meta-fsl-bsp-release/ $ git am ~/Download/0001-Add-RTSP-support-for-i.MX-8-L4.14.78_ga1.0.0-or-olde.patch Note: This patch is not necessary for L4.14.98_ga2.0.0 BSP! Then, build the image with bitbake and deploy it to the SD card. 2. Video Test Source Example Server $ gst-variable-rtsp-server -p 9001 -u "videotestsrc ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client 2. Camera Example Server $ gst-variable-rtsp-server -p 9001 -u "v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client In order to use VLC or other application as the client, just enter the URL as shown in the image below:
記事全体を表示
Environment:   VMware player 15 + ubuntu 18.04 LTS Reference document: i.MX_Yocto_Project_User's_Guide.pdf 1. Software packages for the compilation # sudo apt-get install flex bison gperf build-essential zlib1g-dev # sudo apt-get install lib32ncurses5-dev x11proto-core-dev # sudo apt-get install libx11-dev lib32z1-dev libgl1-mesa-dev # sudo apt-get install tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib # sudo apt-get install subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev # sudo apt-get install liblz-dev lzop liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install python3 python3-pip python3-pexpect python3-git python3-jinja2 pylint3 # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils # sudo apt-get install openjdk-8-jdk device-tree-compiler aptitude # sudo apt-get install libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat # sudo apt-get install libncursesw5-dev libssl-dev libegl1-mesa # sudo apt-get install net-tools python libsdl1.2-dev xterm socat # sudo apt-get install icedtea-netx-common icedtea-netx 2. downloading yocto bsp (L5.4.24_2.1.0) # rm -rf ~/bin # mkdir ~/bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=~/bin:$PATH   # mkdir imx-yocto-bsp-5.4.24-2.1.0 # cd imx-yocto-bsp-5.4.24-2.1.0 # repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml # cd .repo/manifests # gedit imx-5.4.24-2.1.0.xml          Modify git to https like below:   <remote fetch="https://git.yoctoproject.org/git" name="yocto"/>   <remote fetch="https://github.com/Freescale" name="community"/>   <remote fetch="https://github.com/openembedded" name="oe"/>   <remote fetch="https://github.com/OSSystems" name="OSSystems"/>   <remote fetch="https://github.com/meta-qt5"  name="QT5"/>   <remote fetch="https://github.com/TimesysGit"  name="Timesys"/>   <remote fetch="https://github.com/meta-rust"  name="rust"/>   <remote fetch="https://git.openembedded.org"  name="python2"/>   <remote fetch="https://source.codeaurora.org/external/imx" name="CAF"/> Save it and exit. # cd ~/ imx-yocto-bsp-5.4.24-2.1.0 # repo sync          Begin to compile i.MX8MQ BSP: # DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build-wayland          If users want to use chromium, do it like below, otherwise omit the step.        Add CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" to local.conf        And use 8 thread to compile BSP # gedit ./conf/local.conf …… BB_NUMBER_THREADS =”4” PARALLEL_MAKE =”-j 4” CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" ……          Save it and exit. [comment]          If your ubuntu has 8GB DDR, BB_NUMBER_THREADS can be set to “2”, PARALLEL_MAKE can be set to “-j 2”. # bitbake chromium-ozone-wayland -c fetch # bitbake imx-image-full Use ulimit -n 4096 to solve the issue. Then continue. # bitbake imx-image-full chromium compilation error:          Compile chromium-ozone-wayland separately. # bitbake chromium-ozone-wayland -c cleansstate # bitbake chromium-ozone-wayland -c compile          Use the command to solve the problem. # gedit ../sources/meta-imx/meta-sdk/dynamic-layers/browser-layer/recipes-browser/chromium/chromium-ozone-wayland_%.bbappend DEPENDS += "\         libxkbcommon \         virtual/egl \         wayland \         wayland-native \          mesa         \ "          Add mesa to DEPENDS          Save and exit.          Continue to compile it. # bitbake chromium-ozone-wayland -c compile          done, continue to compile full image   # bitbake imx-image-full Attachment is document in pdf format, which should be clear. NXP TIC team Weidong Sun 08/21/2020
記事全体を表示
  1.overwrite the sources/meta-freescale/recipes-security/optee-imx with optee-imx.zip 2.add below code to conf/local.conf DISTRO_FEATURES_append += " systemd" DISTRO_FEATURES_BACKFILL_CONSIDERED += "sysvinit" VIRTUAL-RUNTIME_init_manager = "systemd" VIRTUAL-RUNTIME_initscripts = "systemd-compat-units" MACHINE_FEATURES_append += "optee" DISTRO_FEATURES_append += "optee" IMAGE_INSTALL_append += "optee-test optee-os optee-client optee-examples" 3.bitbake optee-examples or bitbake imx-image-xxx You can directly install optee-examples_3.11.0-r0_arm64.deb in your device.  
記事全体を表示
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
記事全体を表示
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
記事全体を表示
UPDATE: Note that this document describes eIQ Machine Learning Software for the NXP L4.14 BSP release. Beginning with the L4.19 BSP, eIQ Software is pre-integrated in the BSP release and this document is no longer necessary or being maintained. For more information on eIQ Software in these releases (L4.19, L5.4, etc), please refer to the "NXP eIQ Machine Learning" chapter in the Linux User Guide for that specific release.  Original Post: eIQ Machine Learning Software for iMX Linux 4.14.y kernel series is available now. The NXP eIQ™ Machine Learning Software Development Environment enables the use of ML algorithms on NXP MCUs, i.MX RT crossover processors, and i.MX family SoCs. eIQ software includes inference engines, neural network compilers, and optimized libraries and leverages open source technologies. eIQ is fully integrated into our MCUXpresso SDK and Yocto development environments, allowing you to develop complete system-level applications with ease. Source download, build and installation Please refer to document NXP eIQ(TM) Machine Learning Enablement (UM11226.pdf) for detailed instructions on how to download, build and install eIQ software on your platform. Sample applications To help get you started right away we've posted numerous howtos and sample applications right here in the community. Please refer to eIQ Sample Apps - Overview. Supported platforms eIQ Machine learning software for i.MX Linux 4.14.y supports the L4.14.78-1.0.0 and L4.14.98-2.0.0 GA releases running on i.MX 8 Series Applications Processors. For more information on artificial intelligence, machine learning and eIQ Software please visit AI & Machine Learning | NXP.
記事全体を表示
Summary: The i.MX 8M-Mini can boot from QSPI flash using a dedicated boot image. The boot config settings are not correctly documented in the EVK Board Hardware User's Guide Rev 0 from 02/2019. In the document i.MX_Linux_User's_Guide.pdf  in the BSP documentation 4.14.98 the settings are correctly given in Table 38 Details: To generate a bootable file for the QSPI with Yocto, you need to include the following setting into local.conf: UBOOT_CONFIG = "fspi" If you don't want/need to make a complete build, just rebuild u-boot: bitbake -c deploy u-boot-imx Alternatively the file imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi included already in the BSP demo packages will work as well Program the image into QSPI: With UUU:   uuu -b qspi imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi With u-boot: u-boot=> fatls mmc 0:1 14557696   Image    …   1446848   imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi 11 file(s), 0 dir(s) u-boot=> sf probe SF: Detected n25q256a with page size 256 Bytes, erase size 4 KiB, total 32 MiB u-boot=> fatload mmc 0:1 0x40480000 imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi 1446848 bytes read in 79 ms (17.5 MiB/s) u-boot=> sf erase 0x0 0x200000 SF: 2097152 bytes @ 0x0 Erased: OK u-boot=> sf write 0x40480000 0x0 0x200000 device 0 offset 0x0, size 0x200000 SF: 2097152 bytes @ 0x0 Written: OK u-boot=> sf read 0x50000000 0x0 0x200000 device 0 offset 0x0, size 0x200000 SF: 2097152 bytes @ 0x0 Read: OK u-boot=> cmp.b 0x40480000 0x50000000 0x200000 Total of 2097152 byte(s) were the same u-boot=> Set boot config jumpers correctly and power on the board (no SD-card in the slot) 8M-Mini Rev A and Rev B boards:  01xxxxx0 0000x001 8M-Mini Rev C boards: 0110xxxxxx 00100x0010
記事全体を表示
The Android P9.0.0_2.0.0 GA (4.14.98 kernel) is now available on IMX software landing page. Overview -> i.MX BSP Updates and Releases -> Android -> Android P9.0.0_2.0.0 (4.14.98 kernel)    Files available:   # Name Description 1 android_p9.0.0_2.0.0-ga_docs.zip Android P9.0.0_2.0.0 Documentation 2 imx-p9.0.0_2.0.0-ga.tar.gz i.MX Android proprietary surce code for Android P9.0.0_2.0.0 3 android_p9.0.0_2.0.0-ga_image_8mmevk.tar.gz Prebuilt images with NXP extended features for the i.MX 8M Mini EVK 4 android_p9.0.0_2.0.0-ga_image_8mqevk.tar.gz Prebuilt images with NXP extended features for the i.MX 8M Quad EVK 5 android_p9.0.0_2.0.0-ga_image_8qmek.tar.gz Prebuilt images with NXP extended features for the i.MX8QMax and 8QXPlus MEK 6 fsl_aacp_dec_p9.0.0_2.0.0-ga.tar.gz AAC Plus Codec for P9.0.0_2.0.0_GA   Supported boards: i.MX 8MMini MEK Board i.MX 8MQuad EVK Board i.MX 8QuadMax MEK i.MX 8QuadXPlus MEK   Features and Known issues For features and known issues, please consult the Release Notes in detail.  ======================================================================================= The Android P9.0.0_2.1.0_AUTO GA (4.14.98 kernel) is now available on IMX software landing page. Overview -> i.MX BSP Updates and Releases -> Android AUTO-> Android P9.0.0_2.1.0_AUTO   Files available:   # Name Description 1 android_p9.0.0_2.1.0-auto-ga_docs.zip Android P9.0.0_2.1.0_AUTO  Documentation 2 imx-p9.0.0_2.1.0-auto-ga.tar.gz i.MX Android Automotive proprietary source code for Android P9.0.0_2.1.0_AUTO 3 android_p9.0.0_2.1.0-auto-ga_image_8qmek.tar.gz Prebuilt images with NXP extended features with the EVS function enabled in the Cortex-M4 CPU core for the i.MX 8QuadMax/8QuadXPlus MEK 4 android_p9.0.0_2.1.0-auto-ga_image_8qmek2.tar.gz Prebuilt images with NXP extended features for the i.MX8QMax and 8QXPlus MEK, without the EVS in M4 Core.   Supported boards: i.MX 8QuadMax MEK i.MX 8QuadXPlus MEK   Features and Known issues For features and known issues, please consult the Release Notes in detail.
記事全体を表示
 This article instruct customer how to develop on i.MX8MP NPU and how to debug performance. 
記事全体を表示
Note: This guide is specifically for use with Segger software. For steps to use with the MCUXpresso extension for VSCode please refer to How to Use Segger J-Link Plus with i.MX 8M Process... - NXP Community This guide aims to be a technical reference to start using the SEGGER J-Link Plus debug probe on the i.MX 8M Family processors. The board used for this guide specifically is the i.MX 8M Nano EVK, but it also applies to all processors of the i.MX 8M Family. Here we will describe the process using the following structure: Hardware requirements Software requirements How to find, build, and download the i.MX SDK Host setup Build an example application Target setup Run an example application Hardware requirements Evaluation Kit for the i.MX8M Nano Applications Processor (i.MX 8M Nano Evaluation Kit | NXP Semiconductors) Quick Start Guide for i.MX8M Nano (I.MX 8M Nano EVK Quick Start Guide (nxp.com)) J-Link Plus JTAG/SWD debug probe with USB interface (SEGGER J-Link PLUS) Features Download speed up to 1MB/s Unlimited breakpoints in flash memory Supports direct download into RAM and flash memory Supported NXP Devices Supported Devices - Search results "nxp" (segger.com) 9 Pin Cortex-M Adapter (9-Pin Cortex-M Adapter (segger.com)) Description Adapts from the 20-pin 0.1'' JTAG connector to a 9-pin 0.05'' Samtec FTSH connector as defined by Arm. Software requirements Windows 10 OS (host) J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) i.MX 8M Nano SDK (Welcome | MCUXpresso SDK Builder (nxp.com)) MinGW CMake GNU ARM Embedded Toolchain Terminal Emulator for serial port connection (Tera Term, PuTTY, etc.)   How to find, build, and download the i.MX 8M Nano SDK Enter Welcome | MCUXpresso SDK Builder (nxp.com) Click on "Select Development Board"  Select EVK-MIMX8MN (MIMX8MN6xxxJZ) from Boards -> i.MX -> EVK-MIMX8MN Click on the Build MCUXpresso SDK button Click on Download SDK, you'll be redirected to the MCUXpresso SDK Dashboard Look for the i.MX 8M Nano SDK and click on Download SDK Click on Download SDK archive and documentation, accept the Software Terms and Conditions and the .zip file for the SDK will be downloaded.   Host Setup J-Link Software and Documentation Pack for Windows Download J-Link Software and Documentation Pack for Windows (https://www.segger.com/products/debug-probes/j-link/models/j-link-plus/) Execute .exe file downloaded and then click on "Next" Follow the installation wizard with default parameters and click on "Finish".   MinGW Download the MinGW installer from MinGW - Minimalist GNU for Windows - Browse /Installer at SourceForge.net. Follow the installer instructions leaving all options in their default values. Click on Continue when the installer finishes. A MinGW Installation Manager window will pop up, select mingw32-base and msys-base from basic setup. Click on the Installation menu and select Apply Changes. On the next window, click on Apply and wait for the package to finish downloading. Add the appropriate item to the Windows operating system path environment variable. It can be found under Control Panel->System and Security->System->Advanced System Settings in the Environment Variables... section. The path is: \bin. Assuming the default installation path, "C:\MinGW". If the path is not set correctly, the toolchain does not work. Note: If you have C:\MinGW\msys\x.x\bin in your PATH variable (as required by KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.   CMake Download CMake Windows x64 Installer from  Download CMake. Scroll down to find the latest release for the installer: Run the installer and follow the instructions. Make sure to check the Add CMake to system PATH for all users option during the installation process. Restart your PC to apply changes. GNU ARM Embedded Toolchain Download the GNU ARM Embedded Toolchain installer from Downloads | GNU Arm Embedded Toolchain Downloads – Arm Developer, scroll down to find the latest release for the installer: Follow the installer instructions and check the Add to PATH option at the end of the process. Add a new system environment variable named ARMGCC_DIR with the GNU ARM embedded Toolchain installation path as its value ARMGCC_DIR=ARMGCC_DIR=C:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10​   Build and example application Press the Windows Key and search for GCC Command Prompt and run it. Change the directory to the example application project directory (inside the armgcc folder), for example: C:\Users/<user>\Documents\8MNANO\boards\evkmimx8mn\demo_apps\hello_world\armgcc Type build_debug.bat on the command line or double click the build_debug.bat file (inside the armgcc folder of the application project) through Windows Explorer Wait for the building process to end and make sure no error messages are shown. Target Setup Connect the debug cable (USB-UART) to the board and the other end to your PC. Connect the power cable to the second USB-C port and to a wall socket. Don't turn on the board yet. Connect the JLink Plus to your PC with the USB cable. Connect the JLink Plus to the JTAG of the i.MX 8M Nano EVK board In this part we will need to identify pin number 1 from the 9 Pin Cortex-M adapter and from the i.MX 8M Nano EVK board. For the first one identify pin 7 identifiable by a "Non-connect pin". For the i.MX 8M Nano, you can identify easily with a number 1 in one corner of the connectors.    The whole setup should look similar to this: Run an example application Open a terminal application (TeraTerm, PuTTY, etc.) on your host PC and set it to the serial debug port with the lowest numbered port with the following settings: Speed: 115200 Data: 8-bit Parity: none Stop bits: 1 bit Flow Control: none Start SEGGER J-Link GDB Server. On section “Target Device” select MIMX8MN6_M7 and click “OK”. You will see the following window. Open a new instance of GCC Command Prompt. Change to the directory with the example previously compiled. Here is the path to folder that contains the files: <install_dir>/boards/<boad_name>/<example_type>/<application_name>/armgcc/debug​ Run the command: arm-none-eabi-gdb.exe <application_name>.elf.​ Example: At this point you are in the GDB Command Prompt, run the following commands: target remote localhost:2331 monitor reset monitor halt load monitor go The application will be now running and you can see the “hello world” on your terminal (PuTTY,Tera Term, etc.).  
記事全体を表示
This is a quick article focused on how to add the support of the ssh on the i.MX devices using Yocto to add that packages.   Refer to the pdf attached.
記事全体を表示
  Anyone who want to use this solution should get reference design and firmware from Lontium. Hardware Here is the block diagram of LT9611UXC Demo Board. As the MIPI port of our EVK can provide 5V, 3V3 and 1V8.We can remove useless DC-DC chips from reference design. Below is the LT9611UXC Demo Board. Software Download the firmware into LT9611UXC. In Linux side, we need to drive the MIPI to output signals with standard timings of 1080P. Panel type diff --git a/arch/arm64/boot/dts/freescale/imx8mp-evk.dts b/arch/arm64/boot/dts/freescale/imx8mp-evk.dts index 1732b5c72380..c6a829be541f 100644 --- a/arch/arm64/boot/dts/freescale/imx8mp-evk.dts +++ b/arch/arm64/boot/dts/freescale/imx8mp-evk.dts @@ -696,13 +716,17 @@ &ldb_phy { &mipi_dsi { status = "okay"; + panel@0{ + compatible = "nxp,lt9611uxc"; + reg = <0>; + status = "okay"; }; }; &snvs_pwrkey { diff --git a/drivers/gpu/drm/panel/panel-simple.c b/drivers/gpu/drm/panel/panel-simple.c index 4f78bbf63f33..90d99f12515b 100644 --- a/drivers/gpu/drm/panel/panel-simple.c +++ b/drivers/gpu/drm/panel/panel-simple.c @@ -4997,6 +4997,34 @@ struct panel_desc_dsi { unsigned int lanes; }; +static const struct drm_display_mode lt9611_panel_mode = { + .clock = 148500, + .hdisplay = 1920, + .hsync_start = 1920 + 88, + .hsync_end = 1920 + 88 + 44, + .htotal = 1920 + 88 + 44 + 148, + .vdisplay = 1080, + .vsync_start = 1080 + 4, + .vsync_end = 1080 + 4 + 5, + .vtotal = 1080 + 4 + 5 + 36, +}; + +static const struct panel_desc_dsi lt9611_panel = { + .desc = { + .modes = &lt9611_panel_mode, + .num_modes = 1, + .bpc = 8, + .size = { + .width = 62, + .height = 110, + }, + .connector_type = DRM_MODE_CONNECTOR_DSI, + }, + .flags = MIPI_DSI_MODE_VIDEO_HSE | MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_NO_EOT_PACKET | MIPI_DSI_MODE_VIDEO_SYNC_PULSE, + .format = MIPI_DSI_FMT_RGB888, + .lanes = 4, +}; + static const struct drm_display_mode auo_b080uan01_mode = { .clock = 154500, .hdisplay = 1200, @@ -5201,6 +5229,9 @@ static const struct panel_desc_dsi osd101t2045_53ts = { static const struct of_device_id dsi_of_match[] = { { + .compatible = "nxp,lt9611uxc", + .data = &lt9611_panel, + },{ .compatible = "auo,b080uan01", .data = &auo_b080uan01 }, {
記事全体を表示