i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The Guide is how to use Ubuntu filesystem with i.MX8 series platform.At present, I had try it on i.MX8QXP with 4.14.98 kernel with ubuntu16.04. The Document will be continuously updated with enable VPU, ubuntu18.04. The desktop we can chose Gnome or weston.  Because driver  support issue, gc7000 series gpu not support render Gnome destop but it can render weston destop.  Update 2019/7/31: Ubuntu-i.MX8-weston.pdf   Feature: weston + ubuntu18.04 + 4.14.98 kernel VPU (enable with gplay or gst-play)  GPU (could render desktop and run GPU demo under root privileges on Weston Desktop) I also try ubuntu with gnome desktop, ubuntu18.04 can not run gnome, need use ubuntu19.04. But Gnome Desktop just render by CPU.  ------------------------------------------------------------------------------------- Update 2020/3/6: Ubuntu-i.MX8M.pdf Just a simple guide for IMX8M series, will be  continuously updated. 
View full article
The reference code is based on L4.14.78 GA1.0.0 BSP and M4 SDK 2.5.1.  It is tested on iMX8QXP MEK board, and it should also work for iMX8QM board. In L4.14.78 GA1.0.0 BSP, MU_5 is used for RPMSG between M4 FreeRTOS and A35 Linux, SC_R_MU_5B is M4 side and SC_R_MU_5A is A35 side. In linux side, we used the "imx_rpmsg_tty.ko" for this test, this driver is built as module in default BSP. Case 1: M4 wake up A35. Apply "L4.14.78_rpmsg_wakeup.patch" to linux kernel, this patch will enable the RPMSG wake up feature. "rpmsg_lite_pingpong_rtos.tar.bz2" is the M4 side test code. After booted the board with Linux + M4 rpmsg software, run followed test commands: 1. In A35 UART side, run followed commands:     # echo enabled > /sys/bus/platform/devices/90000000.rpmsg/power/wakeup     # insmod ./imx_rpmsg_tty.ko     # /unit_tests/Remote_Processor_Messaging/mxc_mcc_tty_test.out /dev/ttyRPMSG30 115200 R 100 1000 &     # echo deadbeaf > /dev/ttyRPMSG30     # echo mem > /sys/power/state 2. M4 UART side:    After run "echo deadbeaf > /dev/ttyRPMSG30" from Linux side, it will show "Got ping..." and wait there, after run A35 suspend commane "echo mem > /sys/power/state", Linux suspends. Then from M4 UART side, press "c" key, it will send RPMSG to A35 and wake up A35 Linux. Case 2: A35 wake up M4. "power_mode_switch_rpmsg_wakeup.tar.bz2" is the M4 side test code, After booted the board with Linux + M4 rpmsg software, the M4 UART will wait for A35 RPMSG driver ready. Test commands: 1. In A35 UART side, run followed commands to make RPMSG driver ready:     # insmod ./imx_rpmsg_tty.ko     # /unit_tests/Remote_Processor_Messaging/mxc_mcc_tty_test.out /dev/ttyRPMSG30 115200 R 100 1000 &     # echo deadbeaf > /dev/ttyRPMSG30 2. Now M4 UART shows ping pong messages to make sure RPMSG is ready. Now M4 is in power switch menu, select VLLS power mode in M4 UART:      Press  H for enter: VLLS     - Very Low Leakage Stop mode     ... ...      Press R for RPMSG. After press "R" key in M4 UART, M4 will print "Send a RPMSG message to wake up" and goto suspend mode. 3. Wake up M4 from A35 side, send any data to RPMSG:     # echo deadbeaf > /dev/ttyRPMSG30 M4 resumed and goto power switch menu again. SDK folder to compile the two M4 sample code: SDK/boards/mekmimx8qx/multicore_examples/rpmsg_lite_pingpong_rtos SDK/boards/mekmimx8qx/demo_apps/power_mode_switch
View full article
adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C0 chips.   ISL79987 is the 4 virtual channel TVin chip which can input 4 CVBS cameras to iMX8QXP with MIPI CSI2 inteface, it can only work with iMX8QXP C0 chips. The iMX8QXP B0 chips have MIPI CSI2 virtual channel errata.   To test the capture to file: $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -num 300 -fmt YUYV -of   To test the preview on screen: $ killall weston $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -fmt RGBP -num 30000   Note: 1. For weaving mode de-interlace, when the ISI is doing de-interlace, it can't do CSC at the same time, so preview will get color issue, because the real output video is always YUYV format. 2. For blending mode de-interlace, it must use ISI0, so for ISL79987, only one camera can use blending mode, the other three cameras are still using weaving mode. The preview color is OK for such use case. 3. The patch is for L4.19.35 BSP.     2019-11-14 update: Add the test application "mx8_v4l2_cap_drm.tar.gz" to support YUYV render to display. Test command to render 4 weaving mode cameras:    ./mx8_v4l2_cap_drm.out -cam 0xF -fmt YUYV -num 30000     2020-04-29 update: Add "0006-isl7998x-fix-the-mipi_bps-overwrite-issue-from-set_f.patch", it fixed the issue that MIPI bps information in isl7998x_data->format.reserved[0] had been overwritten by isl7998x_set_fmt().   2021-06-11 update: Added the patches based on L5.4.70_2.3.0 GA BSP.
View full article
iMX8QXP/iMX8QM have hardware JPEG decoder: The JPEG-D-X core. This is the example code to use this hw decoder in M4 SDK to decode JPEG files. M4_JPEG_DECODER_SDK_2.5.1.7z The attached "rear_view_camera_jpegdec.tar.bz2" is the updated source code for "SDK\boards\mekmimx8qx\demo_apps\rear_view_camera". It is based on SDK 2.5.1 for iMX8QXP MEK. The "rear_view_camera_jpegdec.patch" is the modified code, it hasn't included the added "fsl_jpeg_dec.c" and "fsl_jpeg_dec.h".   The testing used two 256*256 JPEG files, they are RGB color space. We used followed commands to build them into flash.bin: ./mkimage_imx8 -soc QX -rev B0 -append ahab-container.img -c -scfw scfw_tcm.bin -m4 m4_rear_view_camera.bin 0 0x34FE0000 --data demo_rgb.jpg 0x84000000 --data demo_rgb2.jpg 0x84008000 -out flash.bin   If customer need change the JPEG resoluion, they can change them in file "fsl_jpeg_dec.h", APP_JPEG_SIZE_OF_KB is the JPEG file length in memory, aligned in KB.   #define APP_JPEG_WIDTH (256) #define APP_JPEG_HEIGHT (256) #define APP_JPEG_SIZE_OF_KB (32) #define APP_JPEG_FORMAT JPEG_RGB #define APP_JPEG_BUFFER (0x84000000)   To created RGB format JPEG file from RGB data, the customer can use linux unit test application "/unit_tests/JPEG/encoder_test.out". M4_JPEG_DECODER_WINDOW_MODE_SDK_2.5.1.7z Based on JEPG decoder, added DPU CSC support and render JEPG decoded video in overlay window. The architecture is followed: NXP logo is put in FetchLayer0 with RGB565 format, after LayerBlend0, it will be the prim layer for LayberBlend1 (FetchLayer0 can't be used as prim layer for LayerBlend), the JPEG decoder output is put to FetchDecoder0. RGB888 format, and it will be resize to 640*480, and put to x=100, y=100 of the display. (Only the sec layer of LayerBlend can be window mode). Some limitation for layer selection in LayerBlend:
View full article
Design Check Lists: HW Design Checking List for i.MX6DQSDL HW Design Checking List for i.Mx53 Hardware Design Checklist for i.MX28 HW_Design_Checking_List_for_i.MX6SoloX i.MX6UL Hardware design checklist   DDR Design Tool: I.MX53 DDR3 Script Aid imx53 DDR stress tester V0.042 i.Mx6DQSDL DDR3 Script Aid MX6DQP DDR3 Script Aid i.Mx6DQSDL LPDDR2 Script Aid i.Mx6SL LPDDR2 Script Aid i.MX6SX DDR3 Script Aid I.MX6UL DDR3 Script Aid i.MX6UL_LPDDR2_Script_Aid i.MX6ULL_DDR3_Script_Aid  i.MX6ULL_LPDDR2_Script_Aid  MX6SLL_LPDDR2_Script_Aid  MX6SLL_LPDDR3_Script_Aid  i.MX6 DDR Stress Test Tool V1.0.3 i.MX6/7 DDR Stress Test Tool V3.00 i.MX8MSCALE DDR Tool Release  i.MX8M DDR3L register programming aid  i.MX 8/8X Family DDR Tools Release   Application Notes: MX_Design_Validation_Guide I.MX6 series USB Certification Guides
View full article
This document is aimed to introduce seamless switch on rear view camera function in android P9 auto, and this can also be referenced for sharing dpu(display process unit) between A core and m4 core on imx8qxp/qm platform. OS: Android p9 auto beta. (linux needs some modifies). SDK_2.5.1_MEK-MIMX8QX for m4 core. Hardware platform: imx8qxp/qm mek board IT6263 lvds to hdmi cable. max9286 deserializer board. ov16035 camera. Hardware block:     Imx8qxp dpu block, for imx8qm there are two dpus:     Android/Linux and M4 shared dpu path:     The switch function is done by framegen0 unit in dpu, framegen unit can select 7 modes: primary src only second src only primary on second second on primary .....etc. for more details, please refer to the kernel codes at include/video/dpu.h, fgdm_t type. Seamless switch booting flow: Patches contain three main parts: Linux kernel: remove init or configure codes of dpu units and lvds used by m4 core, add ui ready rpmsg pipe. M4 code: modify dpu pipes, add ui ready rpmsg handle. AOSP init.rc scripts: add sending ui ready message scripts.
View full article
Default Ethernet feature is removed for Android Auto (both Android_Pie9.0 and Android10) Below are the patched to bring Ethernet feature back to Android Auto. Please try to apply the according patches if you want to enable Ethernet. For Android_Pie9.0_Auto(example with car2 build): --- a/arch/arm64/configs/android_car2_defconfig +++b/arch/arm64/configs/android_car2_defconfig @@ -245,7 +245,7 @@ CONFIG_DM_VERITY_FEC=y CONFIG_NETDEVICES=y CONFIG_MACVTAP=m CONFIG_TUN=y -# CONFIG_ETHERNET is not set +CONFIG_ETHERNET=y CONFIG_MDIO_BUS_MUX_MMIOREG=m CONFIG_AT803X_PHY=m CONFIG_MARVELL_PHY=m @@ -517,7 +517,7 @@ CONFIG_SQUASHFS=y CONFIG_SQUASHFS_DECOMP_MULTI=y CONFIG_SQUASHFS_XATTR=y CONFIG_SQUASHFS_LZ4=y -# CONFIG_NETWORK_FILESYSTEMS is not set +CONFIG_NETWORK_FILESYSTEMS=y   --- a/imx8q/mek_8q/mek_8q.mk +++ b/imx8q/mek_8q/mek_8q.mk @@ -46,6 +46,7 @@ PRODUCT_COPY_FILES += \      $(IMX_DEVICE_PATH)/fstab.freescale.car:$(TARGET_COPY_OUT_VENDOR)/etc/fstab.freescale \      $(IMX_DEVICE_PATH)/early.init_car.cfg:$(TARGET_COPY_OUT_VENDOR)/etc/early.init.cfg \      $(IMX_DEVICE_PATH)/required_hardware_auto.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/required_hardware.xml \ +    frameworks/native/data/etc/android.hardware.ethernet.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.ethernet.xml \      device/fsl/imx8q/init.recovery.freescale.car.rc:root/init.recovery.freescale.rc   For Android10_Auto,(example with car build): --- a/arch/arm64/configs/android_car_defconfig +++ b/arch/arm64/configs/android_car_defconfig @@ -23,6 +23,8 @@ CONFIG_SCHED_AUTOGROUP=y CONFIG_SCHED_TUNE=y CONFIG_RELAY=y CONFIG_BLK_DEV_INITRD=y +CONFIG_FEC=y +CONFIG_AT803X_PHY=y # CONFIG_RD_BZIP2 is not set # CONFIG_RD_LZMA is not set # CONFIG_RD_XZ is not set @@ -246,7 +248,6 @@ CONFIG_DM_VERITY=y CONFIG_DM_VERITY_FEC=y CONFIG_NETDEVICES=y CONFIG_TUN=y -# CONFIG_ETHERNET is not set   --- a/imx8q/mek_8q/mek_8q.mk +++ b/imx8q/mek_8q/mek_8q.mk @@ -46,6 +46,7 @@ PRODUCT_COPY_FILES += \      $(IMX_DEVICE_PATH)/fstab.freescale.car:$(TARGET_COPY_OUT_VENDOR)/etc/fstab.freescale \      $(IMX_DEVICE_PATH)/early.init_car.cfg:$(TARGET_COPY_OUT_VENDOR)/etc/early.init.cfg \      $(IMX_DEVICE_PATH)/required_hardware_auto.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/required_hardware.xml \ +    frameworks/native/data/etc/android.hardware.ethernet.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.ethernet.xml \      device/fsl/imx8q/init.recovery.freescale.car.rc:root/init.recovery.freescale.rc   Note: Please also check for below file, if fec1 is disabled, please also apply below diff. --- a/arch/arm64/boot/dts/freescale/imx8qm-mek-car2.dts +++ b/arch/arm64/boot/dts/freescale/imx8qm-mek-car2.dts @@ -147,10 +147,6 @@ status = "disabled"; }; -&fec1 { - status = "disabled"; -}; - &fec2 { status = "disabled"; };
View full article
Platform: imx8qm mek imx-yocto-L4.14.98_2.0.0_ga Building Step: Apply the nvp6324 patches.   Symbol: IMX8_NVP6324 [=y] Type : tristate Prompt: IMX8 NVP6324 Driver Location: -> Device Drivers -> Multimedia support (MEDIA_SUPPORT [=y]) -> V4L platform devices (V4L_PLATFORM_DRIVERS [=y]) -> MX8 Video For Linux Video Capture (VIDEO_MX8_CAPTURE [=y]) (1) -> IMX8 Camera ISI/MIPI Features support ‍‍‍‍‍‍‍‍‍ select nvp6324 to y in menuconfig(default is 'y') make Image -j8; make freescale/fsl-imx8qm-mek-nvp6324.dtb, to build kernel and dts, outputs are at  work/imx8qmmek-poky-linux/linux-imx/4.14.98-r0/build/arch/arm64/Image work/imx8qmmek-poky-linux/linux-imx/4.14.98-r0/build/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-nvp6324.dtb copy them to the sd boot partition. reboot the board, you can test the first camera with command: ./mx8_v4l2_cap_drm.out -cam 1 -ow 1280 -oh 720 mx8_v4l2_cap_drm.out is at /unit_tests/V4L2/mx8_v4l2_cap_drm.out The corresponding video device should be default to /dev/video0 ~ /dev/video3.
View full article
GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secure communication protocol to support the national security hardware password device , To provide in line with the national standard programming interface and command line tools, can be used to build PKI / CA, secure communication, data encryption and other standards in line with national security applications. For more information, please access GmSSL official website http://gmssl.org/english.html.   Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga cryptodev: 1.9 HW platform: i.MX6UL, i.MX7D/S, i.MX8M/MM, i.MX8QM/QXP. The patches include the following features: 1, Support SM2/SM9 encryption/decryption/sign/verify/key exchange, RSA encryption/decryption, DSA/ECDSA sign/verify, DH/ECDH key agreement, ECC & DLC & RSA key generation and big number operation and elliptic curve math by CAAM hardware accelerating. 2, run "git apply 0001-Enhance-cryptodev-and-its-engine-in-GmSSL-by-CAAM-s-.patch" under folder sources/poky, and "git apply 0001-Add-public-key-cryptography-operations-in-CAAM-drive.patch" under folder sources/meta-fsl-bsp-release for patch these codes. 3, GmSSL Build command: $ tar zxvf GmSSL-master-iMX.tgz $ cd GmSSL-master-iMX (For i.MX8M/MM, i.MX8QM/QXP) $ source /opt/arm-arch64/environment-setup-aarch64-poky-linux  $ ./Configure -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS -DHW_ENDIAN_SWAP  --prefix=~/install64 --openssldir=/etc/gmssl --libdir=/usr/lib no-saf no-sdf no-skf no-sof no-zuc -no-ssl3 shared linux-aarch64 $ make  $ make install                            /*image and config file will be installed to folder ~/install64 */   (For i.MX6UL, i.MX7D/S) $ source /opt/arm-arch32/environment-setup-cortexa7hf-neon-poky-linux-gnueabi $ ./Configure -DHAVE_CRYPTODEV -DUSE_CRYPTODEV_DIGESTS --prefix=~/install32 --openssldir=/etc/gmssl --libdir=/usr/lib no-saf no-sdf no-skf no-sof no-zuc -no-ssl3 shared linux-armv4 $ make  $ make install                            /*image and config file will be installed to folder ~/install32 */   4, How to use GmSSL: copy image gmssl to /usr/bin on i.MX board; copy gmssl libcrypto.so.1.1 and libssl.so.1.1 to /usr/lib on i.MX board; copy folder etc/gmssl to /etc/ on i.MX board. copy test examples (dhtest, dsatest, rsa_test, ecdhtest, ecdsatest, eciestest, sm3test, sms4test, sm2test, sm9test) under GmSSL-master-iMX/test  to U disk for running. You can run test examples by the following commands: #insmod /lib/modules/4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbeafb80c/extra/cryptodev.ko #/run/media/sda1/dhtest #/run/media/sda1/dsatest #/run/media/sda1/rsa_test #/run/media/sda1/ecdhtest #/run/media/sda1/ecdsatest #/run/media/sda1/eciestest #/run/media/sda1/sm3test #/run/media/sda1/sms4test #/run/media/sda1/sm2test #/run/media/sda1/sm9test and speed test commands: #gmssl speed sm2 #gmssl genrsa -rand -f4 512 #gmssl speed dsa #gmssl genrsa -rand -f4 1024 #gmssl speed rsa #gmssl genrsa -rand -f4 2048 #gmssl speed ecdsa #gmssl genrsa -rand -f4 3072 #gmssl speed ecdh #gmssl genrsa -rand -f4 4096   ++++++++++++++++++++++++++++     updating at 2019-09-10   +++++++++++++++++++++++++++++++++++++++++++++ 0001-fix-the-bug-which-hash-and-cipher-key-don-t-use-DMA-.patch fix the issue which dismatching on key buffer between crytodev and caam driver. Crytodev uses stack's buffer for key storage and caam driver use it to dma map which cause flush cache failure. The patch need to apply on cryptodev-module in Yocto build.   ++++++++++++++++++  updating at 2019-10-14 +++++++++++++++++++++++++++++++++++ This updating is for China C-V2X application. The meta-gmcrypto is Yocto layer which bases on GmSSL and Cryptodev. I add HW SM2 verification by dedicated CAAM job descriptor and enhanced SW SM2 verification by precomputed multiples of generator and ARMv8 assembler language to accelerate point  operation. Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga cryptodev: 1.9 HW platform: i.MX8M/MM/MN, i.MX8QM/QXP. How to build: 1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-4.14.98_2.0.0.  Copy meta-gmcrypto to folder (Yocto 4.14.98_2.0.0_ga dir)/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-cv2x and add BBLAYERS += " ${BSPDIR}/sources/meta-cv2x " into (Yocto 4.14.98_2.0.0_ga dir)/build-cv2x/conf/bblayers.conf and  IMAGE_INSTALL_append += " gmssl-bin "  into local.conf 3, Run bitbake fsl-image-validation-imx. 4, You can find cv2x-verify.c under (build dir)/tmp/work/aarch64-poky-linux/cryptodev-tests/1.9-r0/git/tests. It is example for using CAAM cryptdev interface to do C-V2X verification (includes SM2 p256, NIST p256 and brainpoolP256r1).  cv2x_benchmark.c under (build dir)/tmp/work/aarch64-poky-linux/gmssl/1.0-r0/gmssl-1.0/test is the benchmark test program of C-V2X verifying. It includes HW, SW and HW+SW(one CPU) verifying for SM2 p256, NIST p256 and brainpoolP256r1. 5, Run the below command on your i.MX8QXP MEK board. modprobe cryptodev ./cv2x_benchmark Note: the udpated GmSSL also support projective coordinates and affine coordinates (CAAM only support affine coordinates). Affine coordinates is used by default. You can call EC_GROUP_set_coordinates() and EC_GROUP_restore_coordinates() to change coordinates and restore default. When you hope to use some EC APIs under expected coordinates, you need to call EC_GROUP_set_coordinates() before EC APIs and EC_GROUP_restore_coordinates() after them. Like the below example: orig_coordinate = EC_GROUP_set_coordinates(EC_PROJECTIVE_COORDINATES); group = EC_GROUP_new_by_curve_name(NID_sm2p256v1); EC_GROUP_restore_coordinates(orig_coordinate);   ++++++++++++++++++++++++++++     updating at 2020-11-09   +++++++++++++++++++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.4.47_2.2.0​​. The meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release.  Software environments as the belows: Linux kernel: imx_5.4.47_2.2.0 cryptodev: 1.10 HW platform: i.MX6UL, i.MX7D/S, i.MX8M/8M Mini/8M Nano/8M Plus, i.MX8/8X. How to build: 1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.4.47-2.2.0. Copy meta-gmcrypto to folder (Yocto 5.4.47_2.2.0 dir)/sources/ 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-gmcrypto " into (Yocto 5.4.47_2.2.0 dir)/build-imx8mmevk/conf/bblayers.conf and  IMAGE_INSTALL_append += " gmssl-bin "  into local.conf 3, Run bitbake fsl-image-validation-imx. 4, You can find cv2x-verify.c under (build dir)/tmp/work/aarch64-poky-linux/cryptodev-tests/1.10caam-r0/git/tests. It is example for using CAAM cryptdev interface to do C-V2X verification (includes SM2 p256, NIST p256 and brainpoolP256r1).  cv2x_benchmark.c under (build dir)/tmp/work/aarch64-poky-linux/gmssl/1.0-r0/gmssl-1.0/test is the benchmark test program of C-V2X verifying. It includes HW, SW and HW+SW(one CPU) verifying for SM2 p256, NIST p256 and brainpoolP256r1. 5, Run the below command on your i.MX8M Mini evk board. modprobe cryptodev ./cv2x_benchmark gmssl speed sm2 gmssl speed dsa gmssl speed rsa gmssl speed ecdsa gmssl speed ecdh gmssl genrsa -rand -f4 -engine cryptodev 4096 Note: 1, the udpated GmSSL also support projective coordinates and affine coordinates (CAAM only support affine coordinates). Affine coordinates is used by default. You can call EC_GROUP_set_coordinates() and EC_GROUP_restore_coordinates() to change coordinates and restore default. When you hope to use some EC APIs under expected coordinates, you need to call EC_GROUP_set_coordinates() before EC APIs and EC_GROUP_restore_coordinates() after them. Like the below example: orig_coordinate = EC_GROUP_set_coordinates(EC_PROJECTIVE_COORDINATES); group = EC_GROUP_new_by_curve_name(NID_sm2p256v1); EC_GROUP_restore_coordinates(orig_coordinate); 2, Yocto Zeus integrates openssl 1.1.1g, so I change library name of gmssl from libcrypto to libgmcrypto and from libssl to libgmssl to avoid name confliction with openssl 1.1.1g (lib name are also libcrypto.so.1.1 and libssl.so.1.1). You should use -lgmcrypto and -lgmssl when you link gmssl library instead of -lcrypto and -lssl.   +++++++++++++++++++++++    updating at 2021-02-08  ++++++++++++++++++++++++++++ This updating is for Yocto release of Linux 5.4.70_2.3.0​​. The package meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release. You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.4.70-2.3.0.    +++++++++++++++++++++++    updating for Linux-5.10.52-2.1.0  +++++++++++++++++++++++ This updating is for Yocto release of Linux 5.10.52_2.1.0​​. The package meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release.  1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.10.52-2.1.0.  Copy meta-gmcrypto to folder (Yocto 5.10.52_2.1.0 dir)/sources/. 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-gmcrypto " into (Yocto 5.10.52_2.1.0 dir)/build-imx8mmevk/conf/bblayers.conf and  IMAGE_INSTALL_append += " gmssl-bin "  into local.conf 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev gmssl speed sm2 gmssl genrsa -rand -f4 -engine cryptodev 512 gmssl speed dsa gmssl genrsa -rand -f4 -engine cryptodev 1024 gmssl speed rsa gmssl genrsa -rand -f4 -engine cryptodev 2048 gmssl speed ecdsa gmssl genrsa -rand -f4 -engine cryptodev 3072 gmssl speed ecdh gmssl genrsa -rand -f4 -engine cryptodev 4096 gmssl speed -evp sha256 -engine cryptodev -elapsed gmssl speed -evp aes-128-cbc -engine cryptodev -elapsed gmssl speed -evp aes-128-ecb -engine cryptodev -elapsed gmssl speed -evp aes-128-cfb -engine cryptodev -elapsed gmssl speed -evp aes-128-ofb -engine cryptodev -elapsed gmssl speed -evp des-ede3 -engine cryptodev -elapsed gmssl speed -evp des-cbc -engine cryptodev -elapsed gmssl speed -evp des-ede3-cfb -engine cryptodev -elapsed +++++++++++++++++++++++    updating for Linux-5.15.71-2.2.0 +++++++++++++++++++++++ This updating is for Yocto release of Linux 5.15.71-2.2.0​​. The package meta-gmcrypto is Yocto layer which also support c-v2x feature in previous release.  1, You need to git clone https://gitee.com/zxd2021-imx/meta-gmcrypto.git, and git checkout Linux-5.15.71-2.2.0.  Copy meta-gmcrypto to folder (Yocto 5.15.71-2.2.0 dir)/sources/. 2, Run DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build-imx8mmevk and add BBLAYERS += " ${BSPDIR}/sources/meta-gmcrypto " into (Yocto 5.15.71-2.2.0 dir)/build-imx8mmevk/conf/bblayers.conf and  IMAGE_INSTALL:append = " gmssl-bin "  into local.conf 3, Run bitbake imx-image-multimedia. 4, Run the below command on your i.MX8M Mini EVK board. modprobe cryptodev gmssl speed sm2 gmssl genrsa -rand -f4 -engine cryptodev 512 gmssl speed dsa gmssl genrsa -rand -f4 -engine cryptodev 1024 gmssl speed rsa gmssl genrsa -rand -f4 -engine cryptodev 2048 gmssl speed ecdsa gmssl genrsa -rand -f4 -engine cryptodev 3072 gmssl speed ecdh gmssl genrsa -rand -f4 -engine cryptodev 4096 gmssl speed -evp sha256 -engine cryptodev -elapsed gmssl speed -evp aes-128-cbc -engine cryptodev -elapsed gmssl speed -evp aes-128-ecb -engine cryptodev -elapsed gmssl speed -evp aes-128-cfb -engine cryptodev -elapsed gmssl speed -evp aes-128-ofb -engine cryptodev -elapsed gmssl speed -evp des-ede3 -engine cryptodev -elapsed gmssl speed -evp des-cbc -engine cryptodev -elapsed gmssl speed -evp des-ede3-cfb -engine cryptodev -elapsed   +++++++++++++++++++++++    Updating for Linux-6.1.55-2.2.0 +++++++++++++++++++++++ This updating is new GmSSL 3.1.1 and Yocto release of Linux 6.1.55-2.2.0. 主要特性 超轻量:GmSSL 3 大幅度降低了内存需求和二进制代码体积,不依赖动态内存,可以用于无操作系统的低功耗嵌入式环境(MCU、SOC等),开发者也可以更容易地将国密算法和SSL协议嵌入到现有的项目中。 更合规:GmSSL 3 可以配置为仅包含国密算法和国密协议(TLCP协议),依赖GmSSL 的密码应用更容易满足密码产品型号检测的要求,避免由于混杂非国密算法、不安全算法等导致的安全问题和合规问题。 更安全:TLS 1.3在安全性和通信延迟上相对之前的TLS协议有巨大的提升,GmSSL 3 支持TLS 1.3协议和RFC 8998的国密套件。GmSSL 3 默认支持密钥的加密保护,提升了密码算法的抗侧信道攻击能力。 跨平台:GmSSL 3 更容易跨平台,构建系统不再依赖Perl,默认的CMake构建系统可以容易地和Visual Studio、Android NDK等默认编译工具配合使用,开发者也可以手工编写Makefile在特殊环境中编译、剪裁。 More information, please refer to Readme Recipe file is the attached gmssl_3.1.1.bb.tar.gz
View full article
This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards. Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
View full article
Application Note AN13872  Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini, and i.MX 93 is available on www.nxp.com    SWUpdate: Embedded Systems become more and more complex. Software for Embedded Systems have new features and fixes can be updated in a reliable way. Most of time, we need OTA(Over-The-Air) to upgrade the system. Like Android has its own update system. Linux also need an update system. SWUpdate project is thought to help to update an embedded system from a storage media or from network. However, it should be mainly considered as a framework, where further protocols or installers (in SWUpdate they are called handlers) can be easily added to the application. Mongoose daemon mode: Mongoose is a daemon mode of SWUpdate that provides a web server, web interface and web application. Mongoose is running on the target board(i.MX8MM EVK/i.MX8QXP MEK).Using Web browser to access it.   Suricatta daemon mode: Suricatta regularly polls a remote server for updates, downloads, and installs them. Thereafter, it reboots the system and reports the update status to the server. The screenshot is SWUpdate scuricatta working with hawkbit server.          
View full article
i.mx8x启动代码定制文档   目录 1    i.MX8X 板级开发包镜像结构... 2 2    创建 i.MX8QXP Linux 4.14.78_ga 板级开发包编译环境... 2 2.1  下载板级开发包... 2 2.2  创建yocto编译环境: 3 3    i.MX8X SC firmware. 11 3.1  SC firmware 目录结构... 11 3.2  SC firmware 启动流程... 12 3.3  SC firmware定制... 12 4    i.MX8X ATF. 18 5    FSL Uboot 定制... 20 5.1  FDT支持... 21 5.2  DM(driver model)支持... 27 5.3  Uboot目录 结构... 40 5.4  Uboot编译... 42 5.5  Uboot初始化流程... 43 5.6  uboot 定制... 53 5.7  uboot debug信息... 60
View full article
  Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.     杂记共享一下在开发和学习过程中的经验。    虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。   02/07/2024 Device Tree Standalone Compile under Windows https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Windows/ta-p/1855271   02/07/2024 i.MX8X security overview and AHAB deep dive i.MX8X security overview and AHAB deep dive - NXP Community   11/23/2023 “Standalone” Compile Device Tree https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Standalone-Compile-Device-Tree/ta-p/1762373     10/26/2023 Linux Dynamic Debug https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611   08/10/2023 u-boot environment preset for sdcard mirror u-boot environment preset for sdcard mirror - NXP Community   06/06/2023 all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community     09/26/2022 parseIVT - a script to help i.MX6 Code Signing parseIVT - a script to help i.MX6 Code Signing - NXP Community   Provide  run under windows   09/16/2022   create sdcard mirror under windows create sdcard mirror under windows - NXP Community     08/03/2022   i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011     02/16/2022 mx8_ddr_stress_test without UI   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/mx8-ddr-stress-test-without-UI/ta-p/1414090   12/23/2021 i.MX8 i.MX8X Board Reset https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130       12/21/2021 regulator userspace-consumer https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/1389948     11/24/2021 crypto af_alg blackkey demo crypto af_alg blackkey demo - NXP Community   09/28/2021 u-boot runtime modify Linux device tree(dtb) u-boot runtime modify Linux device tree(dtb) - NXP Community     08/17/2021 gpio-poweroff demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306         08/04/2021 How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709       07/14/2021 SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416     04/07/2021 i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45       03/25/2021 sc_misc_board_ioctl to access the M4 partition from A core side sc_misc_board_ioctl to access the M4 partition fr... - NXP Community     03/17/2021 How to Changei.MX8X MEK+Base Board  Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8X-MEK-Base-Board-Linux-Debug-UART/ba-p/1246779#M43     03/16/2021 How to Change i.MX8MM evk Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40       05/06/2020 Linux fw_printenv fw_setenv to access U-Boot's environment variables Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community     03/30/2020 i.MX6 DDR calibration/stress for Mass Production https://community.nxp.com/docs/DOC-346065     03/25/2020 parseIVT - a script to help i.MX6 Code Signing https://community.nxp.com/docs/DOC-345998     02/17/2020 Start your machine learning journey from tensorflow playground Start your machine learning journey from tensorflow playground      01/15/2020 How to add  iMX8QXP PAD(GPIO) Wakeup How to add iMX8QXP PAD(GPIO) Wakeup    01/09/2020 Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly https://community.nxp.com/docs/DOC-345359   09/29/2019 Docker On i.MX6UL With Ubuntu16.04 https://community.nxp.com/docs/DOC-344462   09/25/2019 Docker On i.MX8MM With Ubuntu https://community.nxp.com/docs/DOC-344473 Docker On i.MX8QXP With Ubuntu https://community.nxp.com/docs/DOC-344474     08/28/2019 eMMC5.0 vs eMMC5.1 https://community.nxp.com/docs/DOC-344265     05/24/2019 How to upgrade  Linux Kernel and dtb on eMMC without UUU How to upgrade Linux Kernel and dtb on eMMC without UUU     04/12/2019 eMMC RPMB Enhance and GP https://community.nxp.com/docs/DOC-343116   04/04/2019 How to Dump a GPT SDCard Mirror(Android O SDCard Mirror) https://community.nxp.com/docs/DOC-343079   04/04/2019 i.MX Create Android SDCard Mirror https://community.nxp.com/docs/DOC-343078   04/02/2019: i.MX Linux Binary_Demo Files Tips  https://community.nxp.com/docs/DOC-343075   04/02/2019:       Update Set fast boot        eMMC_RPMB_Enhance_and_GP.pdf   02/28/2019: imx_builder --- standalone build without Yocto https://community.nxp.com/docs/DOC-342702   08/10/2018: i.MX6SX M4 MPU Settings For RPMSG update    Update slide CMA Arrangement Consideration i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf   07/26/2018 Understand ML With Simplest Code https://community.nxp.com/docs/DOC-341099     04/23/2018:     i.MX8M Standalone Build     i.MX8M Standalone Build.pdf     04/13/2018:      i.MX6SX M4 MPU Settings For RPMSG  update            Add slide CMA Arrangement  Consideration     i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf   09/05/2017:       Update eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 09/01/2017:       eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 08/30/2017:     Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)     Dual LVDS for High Resolution Display.pdf 08/27/2017:  L3.14.28 Ottbox Porting Notes:         L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf MFGTool Uboot Share With the Normal Run One:        MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf Mass Production with programmer        Mass_Production_with_NAND_programmer.pdf        Mass_Production_with_emmc_programmer.pdf AndroidSDCARDMirrorCreator https://community.nxp.com/docs/DOC-329596 L3.10.53 PianoPI Porting Note        L3.10.53_PianoPI_PortingNote_151102.pdf Audio Codec WM8960 Porting L3.10.53 PianoPI        AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf TouchScreen PianoPI Porting Note         TouchScreen_PianoPI_PortingNote_151103.pdf Accessing GPIO From UserSpace        Accessing_GPIO_From_UserSpace.pdf        https://community.nxp.com/docs/DOC-343344 FreeRTOS for i.MX6SX        FreeRTOS for i.MX6SX.pdf i.MX6SX M4 fastup        i.MX6SX M4 fastup.pdf i.MX6 SDCARD Secondary Boot Demo        i.MX6_SDCARD_Secondary_Boot_Demo.pdf i.MX6SX M4 MPU Settings For RPMSG        i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf Security        Security03172017.pdf    NOT related to i.MX, only a short memo
View full article
In defaut Linux BSP, NXP implemented LVDS to HDMI(it6263) and MIPI-DSI to HDMI(adv7535) bridge chip drivers. And these drivers need read the EDID from display, then apply the timing parameters to DRM driver. But for the use case that bridge chip -> Serializer -> Deserializer -> LCD Panel use case, there is no EDID. The attached are reference patches for such use case, it combined the bridge chip to panel directly, and no EDID is needed. The patches are tested on iMX8QXP MEK with bridge chip + panel mode, both of them can see the fb0 device under /sys/class/graphics/ folder, also can see card under  /sys/class/drm/. Display works fine with DTS selected 720P panel mode. [2020-06-24]: Add patches for L4.14.98 kernel: Android_Auto_P9.0.0_GA2.1.0_Kernel_No_EDID_IT6263.patch L4.14.98-iMX8QXP-MEK-ADV7535-MIPI-DSI-to-HDMI-bridge-chip-com.patch
View full article
What is a device tree? The device tree is a data structure that is passed to the Linux kernel to describe the physical devices in a system. Before device trees came into use, the bootloader (for example, U-Boot) had to tell the kernel what machine type it was booting. Moreover, it had to pass other information such as memory size and location, kernel command line, etc. Sometimes, the device tree is confused with the Linux Kernel configuration, but the device tree specifies what devices are available and how they are accessed, not whether the hardware is used. The device tree is a structure composed of nodes and properties: Nodes: The node name is a label used to identify the node. Properties: A node may contain multiple properties arranged with a name and a value. Phandle: Property in one node that contains a pointer to another node. Aliases: The aliases node is an index of other nodes. A device tree is defined in a human-readable device tree syntax text file such as .dts or .dtsi. The machine has one or several .dts files that correspond to different hardware configurations. With these .dts files we can compile them into a device tree binary (.dtb) blobs that can either be attached to the kernel binary (for legacy compatibility) or, as is more commonly done, passed to the kernel by a bootloader like U-Boot. What is Devshell? The Devshell is a terminal shell that runs in the same context as the BitBake task engine. It is possible to run Devshell directly or it may spawn automatically. The advantage of this tool is that is automatically included when you configure and build a platform project so, you can start using it by installing the packages and following the setup of i.MX Yocto Project User's Guide on section 3 “Host Setup”. Steps: Now, let’s see how to compile your device tree files of i.MX devices using Devshell. On host machine. Modify or make your device tree on the next path: - 64 bits. ~/imx-yocto-bsp/<build directory>/tmp/work-shared/<machine>/kernel-source/arch/arm64/boot/dts/freescale - 32 bits. ~/imx-yocto-bsp/<build directory>/tmp/work-shared/<machine>/kernel-source/arch/arm/boot/dts To compile, it is needed to prepare the environment as is mentioned on i.MX Yocto Project User's Guide on section 5.1 “Build Configurations”. $ cd ~/imx-yocto-bsp $ DISTRO=fsl-imx-xwayland MACHINE=<machine> source imx-setup-release.sh -b <build directory> $ bitbake -c devshell virtual/kernel (it will open a new window) On Devshell window. $ make dtbs (after finished, close the Devshell window) On host machine. $ bitbake -c compile -f virtual/kernel $ bitbake -c deploy -f virtual/kernel This process will compile all the device tree files linked to the machine declared on setup environment and your device tree files will be deployed on the next path: ~/imx-yocto-bsp/<build directory>/tmp/deploy/images/<machine> I hope this article will be helpful. Best regards. Jorge.
View full article
i.MX8/i.MX8X/i.MX8DXL has ddr stress test tool. It is a window UI program. In some cases, i.MX devices is security closed. Need signed image to run. Such as unit fail field return analyze, switch new ddr part on existing board.  
View full article
-BACKGROUND       Since the release of i.MX8MQ and i.MX8M Mini, some customers have submitted questions about the design of USB2.0 for these two processors: due to the needs of the project, there is no need to use USB3.0 and USB TYPE-C. Therefore, these applications need to use a conventional USB2.0 interface design similar to i.MX6Q.       In order for customers with similar needs to complete the design smoothly, this document summarizes the answers to previous customer responses and draws two USB2.0 design schematics. At the same time, the i.MX expert hardware team member helped review these two drawings, and the i.MX Expert software team gave suggestions on software adjustments. -BEGIN       i.MX8MQ supports USB3.0 and is compatible with USB2.0, i.MX8M Mini only supports USB2.0, not USB3.0. In both development boards, the USB TYPE-C design scheme is used. We must remove the USB TYPE-C, PD chip and logic chip. At the same time, change the connector to MicroUSB and USB TYPE-A-F. No.1 Hardware Design 1. IOMUX list 2 、USB circuit design (1) USB Power & OC control I.MX8MM i.MX8MQ                                                 i.MX8MQ                                              i.MX8MQ [Comment] For i.MX8MQ -USB1 is configured as Dual Role Mode, USB1 OTG ID is used for detection -USB2 is configured as fixed Host mode, USB2 OTG ID is used for detection -i.MX8M Mini USB2.0                                        i.MX8M Mini                                     i.MX8M Mini [Comment] For i.MX8M Mini -USB1 is configured as Dual Role Mode, USB1 OTG ID is used for detection -USB2 is configured as fixed Host mode, USB2 OTG ID is used for detection (3) Additional description --About USB1_VBUS & USB2_VBUS of i.MX8M Mini          According to i.MX8M Mini datasheet, USB1_VBUS & USB2_VBUS allows 0~3.9V input. See below, please! Therefore, some customers have questioned the USB1_VBUS on the I.MX8M Mini-EVK. From the drawings, the external input voltage exceeds this range.          In fact, customers do not need to worry about this problem. There are internal voltage-dividing resistors on the USB1_VBUS and USB2_VBUS pins. As long as the customer refers to the design method on the I.MX8M Mini-EVK, the input voltage of these 2 pins can be guaranteed Inside. --About USBx OTG ID & USBx_ID (1) USBx_OTG_ID          USBx OTG ID is also called GPIO ID, which is the same as that of i.MX6Q. During the work process, the software changes the role between device and host according to the level of the ID pin from high to low or from low to high. (2)USBx_ID          USBx_ID is called USB PHY ID, which can also perform the same function as USBx OTG ID. (3)Using USBx_OTG_ID or USBx_ID          USBx_OTG_ID is recommended. But if customer wants to use USBx_ID, for i.MX8MQ, she can configure USB_CTL0_ADDR[utmiotg_iddig_sel] register. And for I.MX8M Mini, USBNC_n_CTRL2[DIG_ID_SEL] register. [Comment]          The configuration is got from reference manual of these 2 processors, due to no suitable board, this configuration is not validated on board. Customers can try it. (4) About Flashing Images to the Storage of Board          For an empty board or a board that requires an update image, we need to use the USB interface to program the image. At this time, we need the USB interface to work in device mode. For this, the ROM CODE inside the CPU will ensure that the USB works in device mode. No.2 Tuning Software 1.IOMUX According to the actual application, the signals to be used are multiplexed in the dts file. This step is relatively simple and will not be described here 2. Tuning USB configuration in u-boot / device tree For i.MX8M Mini & i.MX8MQ, i.MX Expert softer team gives the following suggestions, I quote their suggestions here:       Customer can try it by removing CONFIG_USB_TCPC in imx8mm_evk_defconfi and well as removing the typec_ptn5110_1/2 dependencies in the fsl-imx8mm-evk.dts. The uboot does check the state of the Type C ICs and crash or gets stuck if they are removed. --i.MX8M Mini U-BOOT:  CONFIG_USB_TCPC=n Device Tree: &usbotg1 {     status = "okay"; }; &usbotg2 {     status = "okay"; --------------------------------------------------------- --i.MX8MQ --u-boot CONFIG_USB_TCPC=n --Node of Device tree &usb_dwc3_0 {              status = "okay";              /*extcon = <&typec_ptn5100>;*/              dr_mode = "otg";              hnp-disable;              srp-disable;              adp-disable;              maximum-speed = "high-speed"; }; ---------------------------------------------- -END [Comment] If you encounter problems while using this document, please submit a ticket to me. Here are the steps to submit a ticket: 1. Open below SUPPORT site, click blue "Go to Tickets" in the middle. http://www.nxp.com/support/support:SUPPORTHOME 2.Then you will be requested to Login, if you have no an account, please first Register with your business email. 3.After login, please "Create New Cases" button in the middle, then you can submit your question. NXP TIC team Weidong Sun 2020/3/30
View full article
恩智浦BSP的内核定制 ........................................... 103 6.1 IO管脚配置与Pinctrl驱动 .................................... 103 6.2 新板bringup ........................................................ 118 6.3 更改调试串口: .................................................. 127 6.4 uSDHC设备定制(eMMC flash,SDcard, SDIOcard) 133 6.5 LVDS LCD 驱动定制 .......................................... 142 6.6 GPIO_Key 驱动定制 .......................................... 145 6.7 GPIO_LED 驱动定制 ......................................... 149 6.8 Fuse nvram驱动 ................................................. 152 6.9 SPI与SPI Slave驱动 ........................................... 153 6.10 USB 3.0 TypeC 改成 USB 3.0 TypeA(未验证) ... 160 6.11 汽车级以太网驱动定制 ....................................... 160
View full article
This doc show: on i.MX8QXP MEK board, configure ov5640 sensor(parallel interface) output 5MP(2592x1944) RAW(Bayer) data at 15fps, and Parallel Capture Subsystem and Image Sensor Interface capture RAW RGB data, and i.MX8QXP GPU debayer RAW data then display image. HW: i.MX8QXP MEK board, MEK base board (to place the parallel camera), ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc.   Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my kernel patch imx8-ov5640-raw-capture-driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code. Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/imx8/ov5640_v3.c. This register setting is come from ov5640 software application note and data sheet. Configure at i.MX8QXP side The Parallel Capture Subsystem consists of the Parallel Capture Interface (BT 656) and associated peripherals. It interfaces to the Parallel CSI sensor. This allows for up to 24 RGB data bits in parallel or for RGB components on consecutive clocks (up to 10-bit color depth). The formats supported are RGB, RAW and YUV 422. Below is Parallel Capture Subsystem diagram: For RAW format data, CSI_CTRL_REG of Parallel Capture Subsystem need configured as my patch, otherwise found cannot get correct data.   The multiple input sources (MIPI CSI, Parallel Capture) captures the pixel data and feeds it to the ISI. The ISI is responsible for capturing and pre-processing the pixel data from multiple input sources and storing them into the memory. Below is ISI diagram: For RAW format data, it should be bypass any processing pipeline of ISI, just use ISI to save it to memory.   Capture test code To capture the RAW data and save it to file, check my patch imx8_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./imx8_cap.out -of -cam 1 -fr 15 -fmt BA81 -ow 2592 -oh 1944 -num 100   Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX8QXP GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from g2d lib, it is dma-buffer also get logic/physical address of buffer, then queue it as DMABUF to v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx8_debayer-gpusdk-5.3.0.diff which apply on i.MX GPU SDK 5.3.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is, this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8QXP&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>ov5640 data sheet e>ov5640 software application note f>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
View full article