无线连接知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wireless Connectivity Knowledge Base

讨论

排序依据:
Hello, all, Bellow you can find the necessary steps to enable dual monitor mode on our Wi-Fi chip: 88W9098. This procedure is helpful for using 88W9098's dual interfaces in monitor mode to simultaneously capture Wi-Fi sniffer logs in different band . Below is my test environment: Hardware: I.MX8MQ-EVK M.2 AzureWave PCIe XM458 module Software: Linux kernel version: L6.6.52 (prebuilt image for I.MX8MQ-EVK) Device Tree: imx8mq-evk-pcie1-m2.dtb Wi-Fi/BT Driver & Firmware: Version: PCIE9098--17.92.1.p149.81-MM6X17540.p33-(FP92) Firmware: nxp/pcieuart9098_combo_v1.bin Configuration: Edit wifi_mod_para.conf and add: mon_filter=0x27 max_vir_bss=2 Example configuration: PCIE9098_0 = { cfg80211_wext=0xf max_vir_bss=2 cal_data_cfg=none ps_mode=1 auto_ds=1 host_mlme=1 mon_filter=0x27 fw_name=nxp/pcieuart9098_combo_v1.bin } PCIE9098_1 = { cfg80211_wext=0xf max_vir_bss=2 cal_data_cfg=none ps_mode=1 auto_ds=1 host_mlme=1 mon_filter=0x27 fw_name=nxp/pcieuart9098_combo_v1.bin } Compile tcpdump Compile libpcap: wget https://www.tcpdump.org/release/libpcap-1.10.4.tar.gz tar -xvf libpcap-1.10.4.tar.gz cd libpcap-1.10.4 ./configure --host=arm-linux-gnueabihf --prefix=/opt/tcpdump make Output: libpcap.so.1.10.4 Compile tcpdump: wget https://www.tcpdump.org/release/tcpdump-4.99.4.tar.gz tar -xvf tcpdump-4.99.4.tar.gz cd tcpdump-4.99.4/ ./configure --host=arm-linux-gnueabihf --prefix=/opt/tcpdump --with-pcap=/opt/tcpdump make Output: tcpdump Deploy to Board: Copy libpcap.so.1.10.4 and tcpdump to the board Add execute permission: chmod +x tcpdump Dual Monitor Mode on 88W9098 Load the Wi-Fi drivers and firmware: modprobe moal mod_para=nxp/wifi_mod_para.conf Monitor Interface Setup 5 GHz (mlan0): iw mlan0 interface add mon0 type monitor ip link set mon0 up ip link set mlan0 down iw mon0 set channel 36 ./tcpdump -i mon0 -w capture_5g.pcap & ./tcpdump -r capture_5g.pcap 2.4 GHz (mmlan0): iw mmlan0 interface add mon1 type monitor ip link set mon1 up ip link set mmlan0 down iw mon1 set channel 6 ./tcpdump -i mon1 -w capture_2g.pcap & ./tcpdump -r capture_2g.pcap Simultaneous Capture ./tcpdump -i mon0 -w capture_5g.pcap & ./tcpdump -i mon1 -w capture_2g.pcap & Stop Capture killall tcpdump Read Captures ./tcpdump -r capture_5g.pcap ./tcpdump -r capture_2g.pcap Reference link: https://docs.nxp.com/bundle/RM00297/page/connectivity-features/topics/monitor_mode.html   Best regards, Christine.
查看全文
This article shares 2 step by step methods to create P2P connections between 2 IW612 modules. One is not setting pin code, another is setting pin code. And also shares local test results and printed logs for your reference. The basic environment: Hardware: 2 IW612 modules(Murata LBES5PL2EL) + I.MX93-EVK Software: Linux 6.12.20 Wi-Fi Driver and FW version = SDIW612---w9177o-V1, SDIO, FP99, 18.99.3.p25.7-MM6X18537.p9-GPL-(FP92) As a reference, you can also test on other NXP's Wi-Fi products based on Linux OS.   Best regards, Christine.
查看全文
The slides were prepared for European School of Antennas at Carlos III University in Madrid. The contents: - About NXP and wireless controllers - About channel sounding and NXP solutions - Design of CS antennas and functional tests - CS antenna arrays and CS localization
查看全文
Matter is the industry-unifying standard from the Connectivity Standards Alliance that is delivering reliable, secure and interoperable connectivity for smart home devices, ensuring that they will work seamlessly together, today and tomorrow. From connectivity to security, processing and software, NXP offers complete end-to-end solutions for accelerating the development of Matter-enabled devices and is focused on helping our customers overcome the complexity and challenges that come with developing around this game-changing technology.   Getting Started Our investment in Matter starts with easing the development experience for adopting Matter in existing or new designs. With the breadth and scale of our portfolios, we scale to the system level to enable the autonomous edge - bringing intelligence to the edge. This approach provides developers with integrated platforms for the processing, connectivity and security requirements to go from prototype to production faster.   Matter Open-Source Protocol Compatible Products    Matter (previously known as Project CHIP) is a single, unified, application-layer connectivity standard designed to enable developers to connect and build reliable, secure IoT ecosystems and increase compatibility among Smart Home and Building devices. Backed by major brands and developed through collaboration within the Connectivity Standards Alliance (previously known as the Zigbee Alliance), Matter is an open-source royalty-free connectivity standard built with market-proven technologies using Internet Protocol (IP) and compatible with Thread and Wi-Fi network transports.   Useful Links   Getting Started with MCUXpresso for VS Code: Matter on Windows (24.12.71) MCUXpresso extension for VS Code v24.12.71 integrates the Matter toolchain for development on Windows, macOS and Linux.    Understanding Matter Terminology   Matter Is What's Cooking and NXP Has All the Right Ingredients     Matter GitHub Links    Releases Matter 
查看全文
NXP wireless solutions build upon decades of Wi-Fi, Bluetooth®, multiprotocol silicon, software and system design expertise, including 802.15.4 in the latest tri-radio architectures. NXP is committed to driving large-scale deployment across multiple markets by a broad array of power- and cost-optimized Wi-Fi, Bluetooth and 802.15.4 transceivers, enabling products with advanced Wi-Fi and multiradio capabilities including Wi-Fi 4, Wi-Fi 5 and Wi-Fi 6 chips.   Market Product Wi-Fi Spec Wi-Fi Support Summary  IoT IW623 802.11ax (Wi-Fi 6E) 2x2 Tri-band (2.4G/5/7 GHz) + 1x1 Single Band (2.4 GHz) supports Wi-Fi 6E, with a high-performance 2x2 tri-band module for fast and flexible connectivity, plus an extra 1x1 2.4 GHz module likely for compatibility or low-power tasks IoT IW693 802.11ax (Wi-Fi 6/6E) CDW 2x2 Dual Band (5-7 GHz) + 1x1 Single Band (2.4 GHz) High-speed, low-latency connectivity on modern bands (5 and 6 GHz). Compatibility with older devices via 2.4 GHz A 2x2 MIMO setup for better performance, plus a 1x1 fallback for basic connections IoT IW610 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz)   IoT IW612 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz)   IoT IW611 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz)   IoT IW620 802.11ax (Wi-Fi 6) 2x2 DB (2.4/5 GHz)   IoT IW416 802.11n (Wi-Fi 4) 1x1 DB (2.4/5 GHz)       Markets Product Wi-Fi Spec Wi-Fi Support Summary Wireless MCU Hostless RW612 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz) supports Wi-Fi 6, has a single antenna (1x1), and can connect to both 2.4 GHz and 5 GHz networks. Wireless MCU Hostless RW610 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz) supports Wi-Fi 6, has a single antenna (1x1), and can connect to both 2.4 GHz and 5 GHz networks.   Markets Product Wi-Fi Spec Wi-Fi Support Automotive AW692 802.11ax (Wi-Fi 6) 2x2 + 1x1 CDW DB (2.4/5GHz + 2.4Ghz) Automotive AW693 802.11ax (Wi-Fi 6E) 2x2 + 1x1 CDW TB (2.4/5/6Ghz + 2.4Ghz) Automotive AW611 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz) Automotive AW690 802.11ax (Wi-Fi 6) 1x1 CDW DB (2.4/5 GHz)   Wireless Module Partners Leading wireless connectivity solution providers offer NXP wireless modules in their wireless connectivity solutions. Module manufacturers develop Wi-Fi modules using NXP’s broad portfolio of Wi-Fi chips (system-on-chip (SoC)), including Wi-Fi 6 chips, Wi-Fi and Bluetooth® combo integrated circuits (ICs) and tri-radio SoCs with 802.15.4. NXP enables a broad range of wireless applications with an ecosystem of wireless module partners.   Why Use a Module Vendor? Accelerate time-to-market Avoid the complexity of RF design and testing Ensure regulatory compliance more easily (e.g. FCC, CE, ISED) Focus on the host product’s functionality while relying on the vendor for wireless performance   Useful Links Wi-Fi Basic concepts: This post provides information about the different terms used in Wi-Fi, 802.11 standards and the three types of 802.11 MAC frames. Wi-Fi Security Concepts: This post covers the security and authentication processes  Wi-Fi Connection/Disconnection process: In 802.11 standards, the connection procedure includes three major steps that shall be performed to make the device part of the Wi-Fi network and communicate in the network. Wi-Fi Software Drivers Locations: NXP Recommends using Wi-Fi source code drivers WiFi_BT_Integretation-(Linux_BSP_compilation_for_iMX_platform): This article describes how to compile the Linux BSP of the i.MX platform under ubuntu 18.04, 20.04 LTS and debian-10. This is a necessary step to integrate WIFI/BT to the I.MX platform. See the attachment for detailed steps. Enabling i.MX8MP-EVK uSDHC1 M.2 for Wi-Fi on Android-11.0.0_2.6.0: Detailed steps on enabling usdhc1 NXP Wi-Fi and Bluetooth Product:  The article will introduce how to build Wi-Fi Mass Market Driver Wi-Fi Firmware Automatic Recovery on RW61x: This article introduces the Wi-Fi automatic recovery feature as well as how to enable and verify it on RW61x SDK. Access Point Wi-Fi configuration on i.MX8 Family: This guide explains how to achieve that, using the i.MX8M Plus EVK (8MP) as the AP device and the i.MX8M Mini EVK (8MM) as the connected device. How to connect to a Wi-Fi network on i.MX8MP: this article guides you step by step how to connect to a Wi-Fi network NXP Wi-Fi/Bluetooth firmware on the i.MX8M series: steps to replace Wi-Fi/Bluetooth firmware on the i.MX8M series on Linux Enabling Wi-Fi on Zephyr projects with the FRDM-RW612: In this guide, we'll modify the mqtt_publisher example—originally designed for Ethernet—to work with Wi-Fi instead Training FRDM-iMX91 connectivity Wi-Fi Basic Hands-on FRDM-iMX91 connectivity Wi-Fi Bluetooth LE and OT COEX RW612/MCXW71 - Wi-Fi and thread border router Training FRDM-RW612 Getting Started, Wi-Fi CLI on VScode Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here 
查看全文
In modern embedded systems, precise and reliable clocking is fundamental to the correct operation of digital peripherals. Microcontrollers like NXP’s KW45 and MCXW71 rely on internal oscillators to provide timing references for peripherals such as UART, SPI, timers, and ADCs. One such oscillator is the 6 MHz Free Running Oscillator (FRO6M), which is commonly used as a default clock source. This article provides a comprehensive guide to: Selecting and configuring alternative clock sources Choosing an alternative clock source The KW45/MCXW71 microcontroller offers several alternatives, including the Free Running Osilator 192Mhz (FRO192), the RF_OSC , and external crystal oscillators. Each option has its own advantages: FRO192 is stable and available, and external oscillators provide long-term accuracy. The choice of clock source should be based on the peripheral’s timing requirements, power constraints, and the availability of the clock in the current operating mode. Reconfiguring Peripheral Clock Sources Reconfiguring a peripheral’s clock source in KW45 is straightforward using the SDK’s clock management APIs. The function CLOCK_SetIpSrc() allows developers to assign a new clock source to a specific peripheral. Example on changing a UART clocking from FRO6M to other clocksource. UART peripheral connected to FRO6M   uint32_t uartClkSrcFreq = BOARD_DEBUG_UART_CLK_FREQ; CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq);   For example, to switch a UART from FRO6M to FRO-192M, the following code can be used: //Replace kCLOCK_Lpuart1 for your peripheral for clicking CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro192M); Also in the example above we would have to set the  uint32_t uartClkSrcFreq  variable to the correct freq value corresponding to the FRO192M as it is being used as clock source, but the same logic applies to any other clock source for the peripheral.   Other clocking changes for modules can be done as shown in this examples: //Change clock source for LPIT 0 module from 6M FRO to other clocksources /* Iniital source for the LPIT module */ CLOCK_SetIpSrc(kCLOCK_Lpit0, kCLOCK_IpSrcFro6M); /* Set the new source for the LPIT 0 module */ CLOCK_SetIpSrc(kCLOCK_Lpit0, kCLOCK_IpSrcFro192M); /* Set the corresponding divider for application, need to be decided by developer*/ CLOCK_SetIpSrcDiv(kCLOCK_Lpit0, 15U); /* Set the source for the TPM 0 module */ CLOCK_SetIpSrc(kCLOCK_Tpm0, kCLOCK_IpSrcFro6M); /* Set the source for the TPM 0 module */ CLOCK_SetIpSrc(kCLOCK_Tpm0, kCLOCK_IpSrcFro192M); /* Set the corresponding divider for application, need to be decided by developer*/ CLOCK_SetIpSrcDiv(kCLOCK_Tpm0, 3U); //Change clock source for Luart 1 module from 6M FRO to other clocksources CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); /* Set the source for the Lpuart 1 module */ CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro192M); uartClkSrcFreq = CLOCK_GetIpFreq(kCLOCK_Lpuart1); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq); After changing the clock source, it is important to reinitialize the peripheral to ensure that timing parameters such as baud rate, prescaler, or sampling intervals are correctly recalculated. This step ensures that the peripheral operates reliably with the new clock configuration. Those were some examples on changing clock sources for some peripherals, but the same logic can be applied to any other module or peripheral, those examples were taken from SDK 2.16.00 as an example on how a module configured with a clock source can be switched to another.
查看全文
See the necessary steps to enable additional SDK components for a project when using GitHub SDK and Kconfig/CMake.
查看全文
Board pictures (KW47-M2) neidys_vargas_0-1753807293929.png Connectors (KW47-M2) Part Identifier Connector Type Description J3 2x5 pin header SWD DNP J8 1x6 pin header UART1 – FTDI DNP J9 1x6 pin header Power connector DNP Jumpers (KW47-M2) Part Identifier Connector Type Description JP5 2x3 pin header supply power source selection jumper: 1-2 shorted (default configuration): Use this configuration to set target MCU in DCDC mode.  3-4 shorted: Use this configuration to set target MCU in LDO/Bypass mode. All MCU power domains are supplied by P3V3_DUT.  JP4 1x2 pin header Target MCU boot configuration enable jumper: • Open (default setting): ISP mode is disabled • Shorted: ISP mode is enabled Push Buttons (KW47-M2) Part Identifier Switch name Description SW1 Reset button Resets the target MCU. This causes peripherals to reset to their default state. After this, MCU ROM bootloader will be executed. LED D1 turns on at SW1 press. SW2 User PB General purpose input. This pin supports low-power wakeup capabilities through Wake-Up Unit (WUU). LEDs (KW47-M2) Part Identifier Switch name Description D1 Reset LED Indicates a system reset event. When reset is triggered—such as by pressing the SW1 reset button—the D1 LED turns ON. D2 Led Green User indicator, indicates system activity   Power Configurations (KW47-M2) Populate J9 PWR connector. To run KW47 M2 as standalone, supply 3.3V to P3V3_DUT power rail neidys_vargas_1-1753714061544.png Figure 1 J9 M10 Configuration (KW47-M2)   To get the KW47 M2 up and running, you need to select a power configuration through JP5 jumper. For more information on KW47 power configurations, refer to RM: Part Identifier pin Description JP5 1-2 1-2 shorted (default setting): Sets target MCU to DCDC mode. This mode is the recommended configuration. JP5 3-4 3-4 shorted: Sets target MCU to LDO mode.     External power configuration (KW47-M2) Enable KW47-M2 by supplying power through J9 connector: Note: When using DCDC or LDO mode, it is recommended to supply P3V3_DUT power rail only. Part Identifier pin Description J9 5 Use this pin to supply P3V3_DUT power rail with 3.3V. To get KW47-M2 up and running, it is recommended to set KW47 to DCDC mode and supply P3V3_DUT only. J9 3 Use this pin to supply P1V8_LDO power rail with 1.8V. This power rail is intended for an accurate control of VDD_RF power domain, but it is not necessary. J9 1 Use this pin to supply P1V1_EXT power rail with 1.1V. This power rail is intended for an accurate control of VDD_CORE power domain, but it is not necessary.   neidys_vargas_2-1753714061554.png   Programming the NBU in the KW47-M2 board The following steps guide you to program the NBU software for the KW47-M2 Place a jumper on the JP4 header while holding down the reset button (SW) on the module board. Then, connect the USB cable to the J8 connector (USB-to-serial bridge) and plug it into your computer. After the USB cable is connected, release the reset button. neidys_vargas_6-1753714061702.png   Verify what COM Port was assigned to your KW47-M2 board. You can check the COM Port assigned in the Windows “Device Manager” program. Search for “Ports (COM & LPT)” and save the COM Port number. In this example the COM Port assigned was “COM19” neidys_vargas_7-1753714061704.png   Navigate to your computer to the MCU-Link installation folder. The default installation path is located at “C:\nxp\LinkServer_25.3.31\MCU-LINK_installer Locate the “bin” folder and open it. Run the script “blhost” within a windows command prompt. neidys_vargas_8-1753714061713.png   Type “blhost.exe -p COMX write-memory 0x48800000”, drag and drop the NBU binary file. When the process is ready you will see the response status "success" neidys_vargas_9-1753714061729.png  
查看全文
Hello, Starting with SDK version 24.12.00, documentation is available online at: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/index.html  To view documentation for previous releases, replace latest in the URL with the specific version number: - example: https://mcuxpresso.nxp.com/mcuxsdk/25.03.00/html/index.html    Bluetooth LE Documentation For Bluetooth LE-related resources, refer to the following sections:  Bluetooth LE Host Documentation (change log and guides): https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/bluetooth/index.html  ovidiu_usturoi_0-1752503129993.png   Connectivity Framework Documentation(change log and guides):  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/framework/index.html ovidiu_usturoi_1-1752503167217.png   Release Notes by platform To view what's new for each platform, refer to the "What is new" section in the respective release notes: KW45 - EVK:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw45b41zevk/releaseNotes/rnindex.html   KW47-EVK:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw47evk/releaseNotes/rnindex.html FRDM-MCXW23:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/MCX/frdmmcxw23/releaseNotes/rnindex.html  Regards, Ovidiu    
查看全文
Useful Links: Bluetooth Ranging Access Vehicle Enablement System - NXP Community
查看全文
Blue Ravens (Bluetooth Ranging Access Vehicle Enablement System) is a system solution developed by NXP to assist customers in designing their own BLE-based car access solutions using NXP products. It is designed to support a variety of car access use cases through a modular approach. The main objective (but not limited) is to present all the capabilities and advantages of the Channel Sounding technology and NXP BLE Handover in an automotive use case. Channel Sounding is part of the new Bluetooth Low Energy (BLE) standard (BLE 6.0) as a highly accurate distance measurement solution, and available on the NXP KW47 chip. BLE Handover is an NXP proprietary feature developed by NXP to seamlessly transfer a BLE connection from one device to another, without disconnection, using and out of band channel (e.g. CAN). This transfer does not impact the peer device so interoperability is guaranteed. This feature can also be used to enable BLE connection RSSI sniffing to increase RSSI based system security. (KW45 & KW47) Thanks to its modularity, this system can be used to address multiple use-cases, from simple BLE connection system, up to a full BLE Channel Sounding positioning system. Please, note that Channel Sounding is only supported on KW47 chip. KW45 can only be used for simple BLE system. By default, the system on KW47 covers a basic use of Channel Sounding to measure the distance between one remote device (Digital Key) and alternatively several different fixed devices (Car Anchor). At each instant in time, only one anchor is connected to the Digital Key. The other anchors (not connected) can be set in Connection RSSI Sniffing mode (based on Handover). This mode increase the system security by accessing the RSSI value of a connection instead of an advertising packet. These RSSI values can be used to estimated which anchor can be used in the round-robin or to keep the best BLE link around the Car. neidys_vargas_0-1752250251016.png     The system is composed of multiple KW4x boards, each with a specific role. On board is used as Digital Key, to be caried by the user, the other represent the Car sub-system. On this Car Sub-system, all boards are connected to each other using the CAN bus. The CAN bus fulfills the purpose to power all boards with 12V and to allow communication between the boards: neidys_vargas_1-1752250251039.png Control Unit (KW4x EVK-Board) Car Anchors (KW4x LOC-Board) Digital Key (KW4x LOC-Board) Role: Central decision-making node Functionality: - Coordinates BLE anchors. - Triggers actions based on received data   Role: BLE devices connected to the Control Unit via CAN bus Functionality: - Advertise BLE presence. - Wait for a Digital Key to connect. - Act as CS initiators during the session. Role: Acts as the remote BLE device Functionality: - Scans for BLE anchors. - Initiates connection with a Car Anchor. - Once connected, behaves as a CS reflector.     A Desktop application is used to monitor the states and monitor the measurement done by the system: neidys_vargas_8-1752250480774.png   Using the successive measurement on each anchors, the Car sub-system is able to estimate the Digital Key position (Disclaimer: this solution is not consider accurate in dynamic environments)   neidys_vargas_9-1752250744081.png     Features   BLE connection Supporting 1 connection only for now (multiple peer plan) BLE Channel Sounding (KW47 only) Yes RSSI Sniffing Yes – All not connected anchors Automatic exclusion of suboptimal anchors Yes BLE Handover with CS context (No CS repeat) Yes Trilateration algorithm Yes Measurement filtering (real time) Yes Detection area triggering action (e.g. Welcome zone) Yes Car Anchor CAN Synchronization (radio core sync) No (planned for next release) Channel Sounding Sniffing No (feasibility study ongoing)   KPIs   Number of Anchor From 2 to 8 Number of Digital Key 1 BLE Connection Interval 7.5ms – 4s (Default = 30ms) BLE Handover connection transfer time (+CS context transfer) <60ms (CI=30ms) <50ms (CI=10ms) CS start Delay (2+7)*CI CS measurement and data transfer (Real Time) <70ms (CI=30ms) CS Algo <30ms Full cycle time (CS + Handover) [Algorithm runs asynchronously on the anchor after the handover is finished] 390ms (CI=30ms) 190ms (CI=10ms) Line Of Sight CS measurement range 100m Max (at 10dBm) Back Pocket CS measurement range 10m (at 10dB)   This solution is under development and improvement will be added in the future releases. This system can also be enhanced with Ultra-Wide Band support. Videos For access, please contact [email protected]  
查看全文
As documented in the MCX W23 [ERRATA] for WLCSP packaged devices, Tx modulation quality can potentially be violated on 2 data channels
查看全文
This article introduces the Wi-Fi automatic recovery feature as well as how to enable and verify it on RW61x SDK. 1. Introduction Wi-Fi automatic recovery is a NXP proprietary feature that monitors Wi-Fi running status and recovers Wi-Fi out of exception state when running into one of the following cases: Driver fails to wakeup Wi-Fi MCU for commands/Tx Driver fails to receive command response from Wi-Fi MCU Driver detects Wi-Fi firmware is in abnormal state Once Wi-Fi automatic recovery is triggered, Wi-Fi middleware and driver will clean up the running states, reset Wi-Fi MCU power, reload Wi-Fi firmware and restart Wi-Fi initialization. It will not impact the ongoing Bluetooth LE/802.15.4 activities. Figure 1 is the Wi-Fi software architecture. Figure 1: Wi-Fi Software Architecture Figure 2 shows the work flow of Wi-Fi automatic recovery: Figure 2: Wi-Fi Automatic Recovery Work Flow Wi-Fi driver detects command timeout/wakeup card timeout/FW exception   Wi-Fi driver triggers WLAN reset to Stop Wi-Fi activities and de-initialize Wi-Fi Reset Wi-Fi power Reload the Wi-Fi only firmware and wait for the firmware to be active Send an event to notify the application before resetting it   2. SDK Configuration The Wi-Fi automatic recovery feature is not enabled by default in RW61x SDK. It needs to be enabled explicitly: Add below line in <example>/source/wifi_config.h to enable the feature  #define CONFIG_WIFI_RECOVERY 1 Besides, please also make sure the "CONFIG_WIFI_RESET" macro is defined as "1" in the SDK.   3. Automatic Recovery Verification This section introduces how to verify the Wi-Fi automatic recovery feature on RW61x SDK. wifi_cli application is used as example here together with the RW612 RD board. Refer to UM11799: NXP Wi-Fi and Bluetooth Demo Applications for RW61x for steps to flash and run Wi-Fi applications. Below are the steps to verify the Wi-Fi automatic recovery feature: Step 1: Define CONFIG_WIFI_RECOVERY in wifi_cli/source/wifi_config.h     #define CONFIG_WIFI_RECOVERY 1 Step 2: Build and flash the wifi_cli application onto RW612 RD board Step 3: Connect RW612 RD board to a serial terminal Step 4: Reset the power of RW612 RD board Step 5: Trigger Wi-Fi MCU into hung-up state with the following command to mimic a command timeout     # wlan-recovery-test Step 6: Wi-Fi recovery background task detects Wi-Fi FW hang and starts recovery process [wifi] Warn: Command response timed out. command 0x8b, len 12, seqno 0x1c timeout happends. # app_cb: WLAN: FW hang Event: 14 --- Disable WiFi --- [wifi] Warn: Recovery in progress. command 0x10 skipped [wifi] Warn: Recovery in progress. command 0x10 skipped [wifi] Warn: Recovery in progress. command 0xaa skipped [dhcp] Warn: server not dhcpd_running. --- Enable WiFi --- Initialize WLAN Driver [wifi] Warn: WiFi recovery mode done! Wi-Fi cau temperature : 31 STA MAC Address: C0:95:DA:01:1D:A6 board_type: 2, board_type mapping: 0----QFN 1----CSP 2----BGA app_cb: WLAN initialized ======================================== WLAN CLIs are initialized ======================================== ENHANCED WLAN CLIs are initialized ======================================== HOST SLEEP CLIs are initialized ======================================== CLIs Available: ======================================== help clear wlan-version wlan-mac wlan-thread-info wlan-net-stats wlan-set-mac <MAC_Address> wlan-scan wlan-scan-opt ssid <ssid> bssid ... wlan-add <profile_name> ssid <ssid> bssid... wlan-remove <profile_name> wlan-list wlan-connect <profile_name> wlan-connect-opt <profile_name> ... wlan-reassociate wlan-start-network <profile_name> wlan-stop-network wlan-disconnect wlan-stat wlan-info wlan-address wlan-uap-disconnect-sta <mac address> wlan-get-uap-channel wlan-get-uap-sta-list wlan-ieee-ps <0/1> wlan-set-ps-cfg <null_pkt_interval> wlan-deep-sleep-ps <0/1> wlan-get-beacon-interval wlan-get-ps-cfg wlan-set-max-clients-count <max clients count> wlan-get-max-clients-count wlan-rts <sta/uap> <rts threshold> wlan-frag <sta/uap> <fragment threshold> wlan-host-11k-enable <0/1> wlan-host-11k-neighbor-req [ssid <ssid>] wlan-host-11v-bss-trans-query <0..16> wlan-mbo-enable <0/1> wlan-mbo-nonprefer-ch <ch0> <Preference0: 0/1/255> <ch1> <Preference1: 0/1/255> wlan-get-log <sta/uap> <ext> wlan-roaming <0/1> <rssi_threshold> wlan-multi-mef <ping/arp/multicast/del> [<action>] wlan-wakeup-condition <mef/wowlan wake_up_conds> wlan-auto-host-sleep <enable> <mode> <rtc_timer> <periodic> wlan-send-hostcmd wlan-ext-coex-uwb wlan-set-uap-hidden-ssid <0/1/2> wlan-eu-crypto-rc4 <EncDec> wlan-eu-crypto-aes-wrap <EncDec> wlan-eu-crypto-aes-ecb <EncDec> wlan-eu-crypto-ccmp-128 <EncDec> wlan-eu-crypto-ccmp-256 <EncDec> wlan-eu-crypto-gcmp-128 <EncDec> wlan-eu-crypto-gcmp-256 <EncDec> wlan-set-antcfg <ant_mode> <evaluate_time> <evaluate_mode> wlan-get-antcfg wlan-scan-channel-gap <channel_gap_value> wlan-wmm-stat <bss_type> wlan-reset wlan-set-regioncode <region-code> wlan-get-regioncode wlan-11d-enable <sta/uap> <0/1> wlan-uap-set-ecsa-cfg <block_tx> <oper_class> <new_channel> <switch_count> <bandwidth> wlan-csi-cfg wlan-set-csi-param-header <sta/uap> <csi_enable> <head_id> <tail_id> <chip_id> <band_config> <channel> <csi_monitor_enable> <ra4us> wlan-set-csi-filter <opt> <macaddr> <pkt_type> <type> <flag> wlan-txrx-histogram <action> <enable> wlan-subscribe-event <action> <type> <value> <freq> wlan-reg-access <type> <offset> [value] wlan-uapsd-enable <uapsd_enable> wlan-uapsd-qosinfo <qos_info> wlan-uapsd-sleep-period <sleep_period> wlan-tx-ampdu-prot-mode <mode> wlan-rssi-low-threshold <threshold_value> wlan-rx-abort-cfg wlan-set-rx-abort-cfg-ext enable <enable> margin <margin> ceil <ceil_thresh> floor <floor_thresh> wlan-get-rx-abort-cfg-ext wlan-cck-desense-cfg wlan-net-monitor-cfg wlan-set-monitor-filter <opt> <macaddr> wlan-set-monitor-param <action> <monitor_activity> <filter_flags> <radio_type> <chan_number> wlan-set-tsp-cfg <enable> <backoff> <highThreshold> <lowThreshold> <dutycycstep> <dutycycmin> <highthrtemp> <lowthrtemp> wlan-get-tsp-cfg wlan-get-signal wlan-set-bandcfg wlan-get-bandcfg wlan-set-ips <option> wlan-enable-disable-htc <option> wlan-set-su <0/1> wlan-set-forceRTS <0/1> wlan-set-mmsf <enable> <Density> <MMSF> wlan-get-mmsf wlan-set-multiple-dtim <value> wlan-set-country <country_code_str> wlan-set-country-ie-ignore <0/1> wlan-single-ant-duty-cycle <enable/disable> [<Ieee154Duration> <TotalDuration>] wlan-dual-ant-duty-cycle <enable/disable> [<Ieee154Duration> <TotalDuration> <Ieee154FarRangeDuration>] wlan-external-coex-pta enable <PTA/WCI-2/WCI-2 GPIO> ExtWifiBtArb <enable/disable> PolGrantPin <high/low> PriPtaInt <enable/disable> StateFromPta <state pin/ priority pin/ state input disable> SampTiming <Sample timing> InfoSampTiming <Sample timing> TrafficPrio <enable/disable> CoexHwIntWic <enable/disable> wlan-sta-inactivityto <n> <m> <l> [k] [j] wlan-get-temperature wlan-auto-null-tx <sta/uap> <start/stop> wlan-detect-ant <detect_mode> <ant_port_count> channel <channel> ... wlan-recovery-test wlan-get-channel-load <set/get> <duration> wlan-get-txpwrlimit <subband> wlan-set-chanlist wlan-get-chanlist wlan-set-txratecfg <sta/uap> <format> <index> <nss> <rate_setting> <autoTx_set> wlan-get-txratecfg <sta/uap> wlan-get-data-rate <sta/uap> wlan-get-pmfcfg wlan-uap-get-pmfcfg wlan-set-ed-mac-mode <interface> <ed_ctrl_2g> <ed_offset_2g> <ed_ctrl_5g> <ed_offset_5g> wlan-get-ed-mac-mode <interface> wlan-set-tx-omi <interface> <tx-omi> <tx-option> <num_data_pkts> wlan-set-toltime <value> wlan-set-rutxpwrlimit wlan-11ax-cfg <11ax_cfg> wlan-11ax-bcast-twt <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-setup <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-teardown <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-report wlan-get-tsfinfo <format-type> wlan-set-clocksync <mode> <role> <gpio_pin> <gpio_level> <pulse width> wlan-suspend <power mode> ping [-s <packet_size>] [-c <packet_count>] [-W <timeout in sec>] <ipv4/ipv6 address> iperf [-s|-c <host>|-a|-h] [options] dhcp-stat ======================================== --- Done --- Step 7: Run other Wi-Fi shell commands to confirm Wi-Fi resumes to normal state  
查看全文
Using the Signal Frequency Analyzer (SFA) to Measure the FRO 6M Frequency Overview The Signal Frequency Analyzer (SFA) is a specialized hardware peripheral available in NXP’s KW45, MCXW71 microcontrollers. It is designed to provide precise, real-time measurement and analysis of digital signal characteristics, including frequency, period, and timing intervals. This makes it a valuable tool for applications requiring accurate timing diagnostics, signal validation, and system debugging. By utilizing internal 32-bit counters and configurable trigger mechanisms, the SFA enables high-resolution capture of signal transitions, supporting robust system monitoring and fault detection. Functional Capabilities of the SFA The SFA module supports the following measurements: Clock signal frequency of a Clock Under Test (CUT) Clock signal period It operates using two 32-bit counters: One for the Reference Clock (REF) One for the Clock Under Test (CUT) Measurement is performed by comparing the counts of both clocks until predefined target values are reached. FRO 6M Frequency Failure Scenarios The 6 MHz Free Running Oscillator (FRO6M) may occasionally output an incorrect frequency under certain conditions: When the device exits reset When the device wakes from low-power modes To mitigate potential issues caused by incorrect FRO6M output, it is the application developer’s responsibility to verify the oscillator’s frequency and apply corrective measures as needed. Monitoring the FRO 6M Using the SFA To monitor the FRO6M signal, the following configuration is recommended: SFA Configuration Parameters Reference Clock (REF): CPU Clock (e.g., 96 MHz) Clock Under Test (CUT): FRO6M routed via CLKOUT Interrupt Mode: Enabled for asynchronous measurement completion Code Implementation The presented functions are meant to be implemented in users application, the inner functions are part of the implementations of the SFA driver from the NXP’s SDK. It can be used on MCXW71, KW45 just make sure SFA Peripheral Initialization  void init_SFA_peripheral(void) { /* Enable SFA interrupt. */ EnableIRQ(SFA_IRQn); /* Set SFA interrupt priority. */ NVIC_SetPriority(SFA_IRQn, 1); SFA_Init(DEMO_SFA_BASEADDR); SFA_InstallCallback(DEMO_SFA_BASEADDR, EXAMPLE_SFA_CALLBACK); } SFA Callback Function void EXAMPLE_SFA_CALLBACK(status_t status) { if (status == kStatus_SFA_MeasurementCompleted) { SfaMeasureFinished = true; } sfa_callback_status = status; } Frequency Measurement Function This function sets up the measurement of the FRO6M signal using the CPU clock as the reference. uint8_t SFA_freq_measurement_6M_FRO(void) { uint8_t ratio = 0; uint32_t freq = 0UL; sfa_config_t config; CLOCK_SetClkOutSel(kClockClkoutSelSirc); //set clokout to SIRC SFA_GetDefaultConfig(&config); //Get SFA default config config.mode = kSFA_FrequencyMeasurement0; config.refSelect = kSFA_REFSelect1; //Set CPU clk as ref clk config.cutSelect = kSFA_CUTSelect1; //Set clkout as CUT config.refTarget = 0xFFFFFFUL; config.cutTarget = 0xFFFFUL; config.enableCUTPin = true; freq = get_ref_freq_value(CPU_CLK); SFA_SetMeasureConfig(DEMO_SFA_BASEADDR, &config); SFA_MeasureNonBlocking(DEMO_SFA_BASEADDR); while (1) { if (SfaMeasureFinished) { SfaMeasureFinished = false; if(kStatus_SFA_MeasurementCompleted == sfa_callback_status) { freq = SFA_CalculateFrequencyOrPeriod(DEMO_SFA_BASEADDR, freq);//Calculate the FRO freq if(FREQ_6MHZ + TOLERANCE <= freq ) { ratio = 1; } else { if(FREQ_3MHZ + TOLERANCE <= freq) { ratio = 2; } else { if(FREQ_2MHZ + TOLERANCE <= freq) { ratio = 3; } else { ratio = 4; } } } break; } } else { __WFI(); } } return ratio; } Result Interpretation and Usage To test the FRO 6M after adding the above functions the FRO can be tested after executing: init_SFA_peripheral(); SFA_freq_measurement_6M_FRO(); The measured FRO6M frequency ratio is returned by the function SFA_freq_measurement_6M_FRO(), with the ratio you can know the current frequency output of the 6M FRO, ration 1 means 6M are being output by the FRO, ratio 2 means the frequency output of the FRO it's being cut in half meaning the FRO is outputting 3 Mhz, ration 3 means the FRO output frequency is being cut by a third part, this results in 2MHz frequency output. With this information you can: Adapt peripheral clocking if the FRO6M frequency is incorrect (This can be achieve by modifying the peripheral dividers if dividers are being used). Trigger corrective actions such as  switching to an alternate clock source Steps to Reconfigure Peripheral Clocking When FRO6M output frequency is lower Detect the Faulty FRO6M Output Use the SFA measurement as described earlier to determine if the FRO6M is operating below its expected frequency (6 MHz). If the result is significantly lower, proceed to reconfigure. Choose an Alternative Clock Source Most NXP MCUs offer multiple internal and external clock sources. Common alternatives include: FRO 192M OSC RF 32M Sys OSC RTC OSC Choose one that is: Stable Available in your current power mode Compatible with the peripheral’s timing requirements You can add more clock divers if needed to make a higher frequency clock reach a certain lower frequency. Reconfigure the Peripheral Clock Source Use the SDK’s CLOCK_Set... APIs to change the clock source. You may also need to: Adjust dividers to match the required baud rate or timing Reinitialize the peripheral with the new clock settings Example Scenario: Measuring the FRO and Adjusting UART Based on Frequency Ratio Imagine your application relies on the 6 MHz Free Running Oscillator (FRO), and its accuracy directly affects UART communication. To ensure reliable operation, you can use the System Frequency Adjustment (SFA) feature to monitor the FRO output and dynamically adjust the UART configuration. After measuring the 6 MHz FRO using the recommended method, the system returns a frequency ratio value. This value ranges from 1 to 4, where: 1 indicates the frequency is within expected limits (no issues), 2 to 4 represent varying degrees of deviation from the expected frequency. Using this ratio, you can initialize and configure the UART peripheral and its driver to compensate for any frequency variation, ensuring stable and accurate communication. */ int main(void) { BOARD_InitHardware(); uint8_t ch = 0; uint8_t FRO_ratio = 0; init_SFA_peripheral(); /*Measure FRO6M output frequency*/ FRO_ratio = SFA_freq_measurment_6M_FRO(); /*Init debug console and compensate in case a different frequency is output */ if(0 == FRO_ratio) { assert(0);//this user defined return value means something went wrong while measuring 6Mz FRO } uint32_t uartClkSrcFreq = BOARD_DEBUG_UART_CLK_FREQ/FRO_ratio;//Compensate the src frequency set for uart module CLOCK_EnableClock(kCLOCK_Lpuart1); CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq); ...... } SDK 25.0.00 Enhancements for FRO6M Calibration To address known reliability issues with the 6 MHz Free Running Oscillator (FRO6M), particularly during transitions from low-power modes, SDK version 25.06.00 introduces a set of software enhancements aimed at improving oscillator validation and calibration. Key Features Introduced FRO6M Calibration API Two new functions have been added to facilitate runtime verification of the FRO6M frequency: PLATFORM_StartFro6MCalibration() Initializes the calibration process by enabling the cycle counter, capturing a timestamp, and preparing the system to measure elapsed time using both the CPU and the FRO6M-based timestamp counter. PLATFORM_EndFro6MCalibration() Completes the calibration by comparing the time measured via CPU cycles and the FRO6M timestamp counter. This comparison determines whether the oscillator is operating at the expected 6 MHz or has erroneously locked to a lower frequency (e.g., 2 MHz). The result is stored in a global ratio variable (fwk_platform_FRO6MHz_ratio) for use by the system. These functions provide a lightweight and efficient mechanism to detect and respond to oscillator misbehavior, ensuring system stability and timing accuracy. Configuration Macro gPlatformEnableFro6MCalLowpower_d This macro enables automatic FRO6M frequency verification upon exiting low-power modes. When defined, the system will invoke the calibration functions to validate the oscillator before resuming normal operation. Default Integration The calibration mechanism is enabled by default in the SDK configuration file fwk_config.h, ensuring that all applications benefit from this safeguard without requiring manual setup. Use Case and Benefits These enhancements are particularly valuable in applications where: Precise timing is critical (e.g., wireless communication, sensor sampling). The system frequently enters and exits low-power states. Clock source integrity must be guaranteed to avoid peripheral misbehavior or timing faults. By integrating these calibration routines, developers can proactively detect and correct FRO6M frequency anomalies, improving overall system robustness and reducing the risk of runtime errors due to clock instability.  
查看全文
The MCX W23 is a family of devices. All devices are Arm Cortex®-M33 based wireless microcontrollers for embedded applications supporting Bluetooth Low Energy 5.3. It can be used to develop IoT solutions. MCX W23xA supports LV_SM mode. MCX W23xB supports HV_SM and XR_SM mode. Building on NXP's strong history of providing industrial edge solutions, the MCX W series offers a wide operating temperature range from -40 °C to 125 °C. The Arm Cortex-M33 provides a security foundation, offering isolation to protect valuable IP and data with Trust Zone technology. It simplifies the design and software development of digital signal control systems with the integrated digital signal processing (DSP) instructions. To support security requirements, the MCX W23 also offers support for SHA-1, SHA2-256, AES, RSA, ECC, UUID, dynamic encryption, and decryption of the flash data using a PRINCE engine, debug authentication, and TBSA-M compliance. neidys_vargas_1-1760378278216.png   Documents Reference Manual Fact sheet Data Sheet Errata for MCX W23xUIK MCX W23 Hardware Design Guide Secure Reference manual** European Union Declaration of Conformity for FRDM-MCXW23 FRDM-MCXW23 Board User Manual Bluetooth Specifications The MCX W23 is compatible with the Bluetooth Low Energy 5.3 specification: – Bluetooth Low Energy 5.3 controller subsystem (QDID 200592) – Bluetooth Low Energy 5.3 host subsystem (QDID 226395) – Includes a 48-bit unique Bluetooth device address – Up to 4 simultaneous connections supported The MCX W23 supports the following Bluetooth Low Energy features: – Device privacy and network privacy modes (version 5.0) – Advertising extension PDUs (version 5.0) – Anonymous device address type (version 5.0) – Up to 2 Mbps data rate (version 5.0) – Long range (version 5.0) – High-duty cycle, Non connectable advertising (version 5.0) – Channel selection algorithm #2 (version 5.0) – High output power (version 5.0) – Advertising channel index (version 5.1) – Periodic advertising sync transfer (PAST) (version 5.1) – Supports LE power control feature (version 5.2) RF antenna: 50 Ω single-ended RF receiver characteristics: – Sensitivity −94 dBm in Bluetooth Low Energy 2 Mbps – Sensitivity −97 dBm in Bluetooth Low Energy 1 Mbps – Sensitivity −100 dBm in Bluetooth Low Energy 500 kbps – Sensitivity −102 dBm in Bluetooth Low Energy 125 kbps – Accurate RSSI measurement with ±3 dB accuracy Flexible RF transmitter level configurability: – TX mode 1 (TXM1): Range from −31 dBm to +2 dBm when VDD_RF exceeds 1.1 V – TX mode 2 (TXM2): Range from −28 dBm to +6 dBm when VDD_RF exceeds 1.7   Bluetooth_5.0_Feature_Overview Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview   Training MCX W Series Training - NXP Community   Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development    Application Notes Power Management: AN14660: Power Management for MCX W23: This App Note provides information about the power manager software component. The application uses this component and the operating system to achieve optimal low-power states, based on the requirements of the application. RF: AN14575: MCX W23 Health Care IoT Peripheral Software Architecture: This App Note provides an overview of the software architecture for the MCX W23 Health care IoT Peripheral application. Designed as a model implementation, this application showcases the key features of the MCX W23 platform and serves as a foundation for developing product-quality applications. AN14659: MCX W23 Bluetooth Low Energy Power Consumption Analysis: This App Note describes the power consumption of the MCX W23 Bluetooth Low Energy (LE) device and the procedure to measure the current consumption using the MCXW23_EVK_BB and MCXW236B_RDM boards. AN2731: Compact Planar Antennas for 2.4 GHz Communication: This App Note is not an exhaustive inquiry into antenna design. It is instead focused on helping the customers understand enough board layout and antenna basics to select a correct antenna type for their application, as well as avoiding typical layout mistakes that cause performance issues that lead to delays Security: AN14657: Getting Started with Secure Boot on MCX W23: This application note covers the design of the bootloader ROM code that NXP has developed on the MCX W23, and how to use all its features. Useful Links Bluetooth LE FSCI Host Application running on FRDM-MCXN947 and MCXW23B-Click Board: The Bluetooth LE FSCI Host application demonstrates a host-side implementation for the Health Thermometer use case. It is designed to work alongside the FSCI Blackbox application, which runs on platforms such as the MCXW236 Click Board, FRDM-MCXW236, or other compatible Bluetooth LE wireless MCUs. Transmitter Maximum Output Power Override Application Note   Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization):  This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47/KW43) and MCX W7x (MCX W71/W72/W70) Power Profile Tools. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery lifetime of your solution. Development Tools    VSCode: MCUXpresso for Visual Studio Code (VS Code) provides an optimized embedded developer experience for code editing and development. Zephyr RTOs  NXP Application Code Hub: Application Code Hub (ACH) repository enables engineers to easily find microcontroller software examples, code snippets, application software packs and demos developed by our in-house experts. This space provides a quick, easy and consistent way to find microcontroller applications. NXP SPSDK: Is a unified, reliable, and easy to use Python SDK library working across the NXP MCU portfolio providing a strong foundation from quick customer prototyping up to production deployment. NXP SEC Tool: The MCUXpresso Secure Provisioning Tool us a GUI-based application provided to simplify generation and provisioning of bootable executables on NCP MCU devices. NXP OTAP Tool: Is an application that helps the user to perform an over the air firmware update of an NXP development board.
查看全文
The customer wanted to update the FW of the PN7462 to an NFC cockpit. In general, we recommend that customers use MASS STORAGE MODE to update two files (including Flash and EEPROM) into memory. But there will always be customers who don’t know or how to successfully access MASS STORAGE MODE. They cannot succeed in doing so. Therefore, it is recommended to use the GUI FLASH tool to upgrade the FW to the NFC cabin. In order to clearly indicate the user how to use the GUI FLASH tool, this document describes this step by step.
查看全文
The customer submitted a case through DFAE to seek support from NXP. They designed the product using PN5180, and according to feedback, about 10% of the boards could not read the card. The specific manifestation of the problem is: after the host issues the RF_ON command, RF field seems cannot be turned on and then fails to detect the card. Therefore, it can be seen that the problem should be on TX, not RX. The customer's device does not enable DPC and LPCD.
查看全文
Generality on the Oscillation Margin Outline It is a margin to the oscillation stop and the most important item in the oscillation circuit. This margin is indicated by ratio based on the resistance of crystal, and it shows how amplification oscillation capability the circuit has. The oscillation circuit can theoretically operate if the oscillation margin is 1 or more. However, if oscillation margin is close to 1, the risk of operation failure will increase on module due to a too long oscillation start up time and so on. Such problems will be able to be solved by a larger oscillation margin. It is recommended to keep 3 times or more as oscillation margin during the startup of the oscillation. Factor of 10 is commonly requested for Automotive at startup and steady state. 5 is enough for IoT market. However, some providers accept to have 3 times as oscillation margin for steady state. Here below is an oscillation example to explain better the phenomenon: At start up, the configuration is set internally by the hardware in order to be sure to start the oscillation, the load capacitor is 0pF. After this time, it is the steady state and the load capacitor from the internal capabank is taken into account. laurent_rouzier_2-1743663107235.png   If load capacitor is not set correctly with the right oscillator gain, the oscillation will not be maintained after the start up. laurent_rouzier_3-1743663151047.png   The oscillator gain value will also depend on the resisting path on the crystal track.  A good way to evaluate it is to add a resistor on the crystal path and try to launch the oscillation. In the SDK, the gain and the load capacitor can set directly in the application code. Calculation The oscillation margin is able to be calculated as follows: The oscillation margin calculation is based on the motional resistor Rm by formula below : laurent_rouzier_5-1743663216381.png ESR: Crystal Equivalent Series Resistance C0: Shunt Capacitance Rm1: Motional resistor Cm1: Motional Capacitance Lm1: Motional Inductance fosc: oscillation frequency, measured with Rs_Max mounted fr: resonance frequency of the Rm1Lm1Cm1 of the crystal from (1) :  laurent_rouzier_6-1743663251430.png   Oscillation margin is:              laurent_rouzier_7-1743663273516.png        Example: for the EVK board’s 32kHz crystal (NX2012SE) ESR    80000,0 Ω Rm1    79978,2 Ω Lm1    3900 H Cm1   6,00E-15 F C0      1,70E-12 F CL      1,25E-08 F fr        32901,2 Hz fosc    32771 Hz Series Resistor Rsmax        7,50E+05 Ω Oscillation Margin   10,3   Measurement Requirements for measurement PCB (for the test, it is recommended to add a series resistor on the EXTAL32k trace) Crystal unit (with equivalent circuit constants data) Resistors (SMD) Measurement equipment (Oscilloscope, Frequency counter or others capable to observe oscillation) Add a resistor to the resonator in serial and check if the oscillation circuit works or not. laurent_rouzier_8-1743663470883.png   If the oscillation is confirmed by 2), change the resistor to larger. If there is no oscillation, change the resistor to smaller. Find out the maximum resistor (=Rs_max) which is the resistor just before the oscillation stops. Measure the oscillating frequency with Rs_max. Calculate the oscillation margin based on the Rs_max.   Notes The Oscillation margin is affected not only by crystal characteristics but also parts that compose the oscillation circuit (MCU, capacitor and resistor). Therefore, it is recommended to check the oscillation margin after the MCU functionality is checked on your module. The series resistor is only for evaluation. Please do not use this resistor in actual usage. It is recommended to check the functionality of your module also. It is possible that the module does not work correctly due to a frequency shift on oscillation circuit and so on. A test jig and socket could be used in measurement but stray of them will give influence for oscillation margin.   KW47/MCX W72 product oscillation margin overview 32MHz crystal NXP recommends to use the quartz NDK NX1612SA 32MHz (EXS00A-CS15781) to be compliant with the +/-50ppm required in Bluetooth LE. Using the current SDK, NXP guarantees an oscillation margin of 10 for startup and steady state commonly used by Automotive customers. Higher oscillation margin can be reached by using higher ISEL and CDAC parameters with some drawback respectively on the power consumption and the clock accuracy. ( the load capacitance bank (CDAC) and the oscillator amplifier current (ISEL)) NDK recommended / target values for oscillation margin is informed case by case. On a general basis, the requested oscillation margin has to be between the recommended value and 3 times this value. "NDK quartz provider (FR) explains this oscillation margin specification is only mandatory at the start-up phase, not at the steady state. Starting the oscillation is the phase that needs more energy. That's why the gain of the oscillator gain is at the maximum value which means not optimal consumption. When the oscillation stability is reached, the gain could be reduced to save power. The oscillation will not be affected.  Keep in mind a quartz oscillates by mechanical effect. So, when the oscillation is starting you need the highest energy to emulate it. By its own inertial, you need less energy to maintain the mechanical oscillation. NDK provides a good picture of this. Starting up a crystal into oscillation is like a train what you would like to start moving. At the beginning the train is stopped and you need a lot of energy to start running. When the train is running at its nominal speed, you need less effort to maintain that movement and a very big effort to stop it completely."   Example: for the oscillation margin 10 (Series Resistor Rs_max = 560 Ω) The CDAC/ISEL area where the oscillation starts and propagates in the internal blocks is defined (green color raws) in the table below. The frequency accuracy is indicated for some of them: laurent_rouzier_10-1743663991258.png     32kHz crystal NXP recommends to use the quartz NDK NX2012SE (EXS00A-MU01517) or NDK NX2012SA (EXS00A-MU00801) to be compliant with the +/-500ppm required in Bluetooth LE. using the current SDK, the oscillation margin with this quartz is 10 with some limitation on the Crystal load capacitance selection (Cap_Sel) and the Oscillator coarse gain amplifier (ESR_Range) values, with some drawback respectively on the power consumption and the clock accuracy. For an oscillation margin at 10 for instance, the Capacitor value from the databank (Cap_Sel) is limited (green area) as shown in the graph below: laurent_rouzier_11-1743664069050.png   Example: for an oscillation margin at 6.3, if the load cap is set at 12pF and the ESR_Range to 3, the 32kHz frequency accuracy will be around -23ppm. From this point, the oscillation margin can be enlarged to 10.3 by decreasing the load cap to 6pF but the accuracy will be degraded (110ppm).   For an Oscillation margin at 10, the graph below is showing the ESR_Range versus the load cap. The possible load cap variation range (in green) is larger when the ESR_Range increases: laurent_rouzier_12-1743664104826.png   Example: at oscillation margin 10.3, the clock accuracy can be improved from 111ppm to 21ppm by setting the ESR_range 2 to an ESR_Range 3 but the current consumption will be increased to 169.5nA. Another important point is that for a given ESR_Range value, getting higher the load cap is much more increasing the current than in the example above.   Remark: Under a high oscillation margin condition, the crystal voltage will be smaller.   Other possible ways to improve the oscillation margin exist: - Use external capacitor instead of internal capacitor banks. Oscillation margin goes up to 10. - Use the internal 32kFRO is supported for BLE (target:+/-500ppm)              
查看全文
Channel Sounding 
查看全文
Content
查看全文