ワイヤレス接続に関するナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wireless Connectivity Knowledge Base

ディスカッション

ソート順:
Hello, Starting with SDK version 24.12.00, documentation is available online at: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/index.html  To view documentation for previous releases, replace latest in the URL with the specific version number: - example: https://mcuxpresso.nxp.com/mcuxsdk/25.03.00/html/index.html    Bluetooth LE Documentation For Bluetooth LE-related resources, refer to the following sections:  Bluetooth LE Host Documentation (change log and guides): https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/bluetooth/index.html    Connectivity Framework Documentation(change log and guides):  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/framework/index.html   Release Notes by platform To view what's new for each platform, refer to the "What is new" section in the respective release notes: KW45 - EVK:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw45b41zevk/releaseNotes/rnindex.html   KW47-EVK:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw47evk/releaseNotes/rnindex.html FRDM-MCXW23:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/MCX/frdmmcxw23/releaseNotes/rnindex.html  Regards, Ovidiu    
記事全体を表示
Useful Links: Bluetooth Ranging Access Vehicle Enablement System - NXP Community
記事全体を表示
Blue Ravens (Bluetooth Ranging Access Vehicle Enablement System) is a system solution developed by NXP to assist customers in designing their own BLE-based car access solutions using NXP products. It is designed to support a variety of car access use cases through a modular approach. The main objective (but not limited) is to present all the capabilities and advantages of the Channel Sounding technology and NXP BLE Handover in an automotive use case. Channel Sounding is part of the new Bluetooth Low Energy (BLE) standard (BLE 6.0) as a highly accurate distance measurement solution, and available on the NXP KW47 chip. BLE Handover is an NXP proprietary feature developed by NXP to seamlessly transfer a BLE connection from one device to another, without disconnection, using and out of band channel (e.g. CAN). This transfer does not impact the peer device so interoperability is guaranteed. This feature can also be used to enable BLE connection RSSI sniffing to increase RSSI based system security. (KW45 & KW47) Thanks to its modularity, this system can be used to address multiple use-cases, from simple BLE connection system, up to a full BLE Channel Sounding positioning system. Please, note that Channel Sounding is only supported on KW47 chip. KW45 can only be used for simple BLE system. By default, the system on KW47 covers a basic use of Channel Sounding to measure the distance between one remote device (Digital Key) and alternatively several different fixed devices (Car Anchor). At each instant in time, only one anchor is connected to the Digital Key. The other anchors (not connected) can be set in Connection RSSI Sniffing mode (based on Handover). This mode increase the system security by accessing the RSSI value of a connection instead of an advertising packet. These RSSI values can be used to estimated which anchor can be used in the round-robin or to keep the best BLE link around the Car.     The system is composed of multiple KW4x boards, each with a specific role. On board is used as Digital Key, to be caried by the user, the other represent the Car sub-system. On this Car Sub-system, all boards are connected to each other using the CAN bus. The CAN bus fulfills the purpose to power all boards with 12V and to allow communication between the boards: Control Unit (KW4x EVK-Board) Car Anchors (KW4x LOC-Board) Digital Key (KW4x LOC-Board) Role: Central decision-making node Functionality: - Coordinates BLE anchors. - Triggers actions based on received data   Role: BLE devices connected to the Control Unit via CAN bus Functionality: - Advertise BLE presence. - Wait for a Digital Key to connect. - Act as CS initiators during the session. Role: Acts as the remote BLE device Functionality: - Scans for BLE anchors. - Initiates connection with a Car Anchor. - Once connected, behaves as a CS reflector.     A Desktop application is used to monitor the states and monitor the measurement done by the system:   Using the successive measurement on each anchors, the Car sub-system is able to estimate the Digital Key position (Disclaimer: this solution is not consider accurate in dynamic environments)       Features   BLE connection Supporting 1 connection only for now (multiple peer plan) BLE Channel Sounding (KW47 only) Yes RSSI Sniffing Yes – All not connected anchors Automatic exclusion of suboptimal anchors Yes BLE Handover with CS context (No CS repeat) Yes Trilateration algorithm Yes Measurement filtering (real time) Yes Detection area triggering action (e.g. Welcome zone) Yes Car Anchor CAN Synchronization (radio core sync) No (planned for next release) Channel Sounding Sniffing No (feasibility study ongoing)   KPIs   Number of Anchor From 2 to 8 Number of Digital Key 1 BLE Connection Interval 7.5ms – 4s (Default = 30ms) BLE Handover connection transfer time (+CS context transfer) <60ms (CI=30ms) <50ms (CI=10ms) CS start Delay (2+7)*CI CS measurement and data transfer (Real Time) <70ms (CI=30ms) CS Algo <30ms Full cycle time (CS + Handover) [Algorithm runs asynchronously on the anchor after the handover is finished] 390ms (CI=30ms) 190ms (CI=10ms) Line Of Sight CS measurement range 100m Max (at 10dBm) Back Pocket CS measurement range 10m (at 10dB)   This solution is under development and improvement will be added in the future releases. This system can also be enhanced with Ultra-Wide Band support. Videos For access, please contact [email protected]  
記事全体を表示
As documented in the MCX W23 [ERRATA] for WLCSP packaged devices, Tx modulation quality can potentially be violated on 2 data channels
記事全体を表示
This article introduces the Wi-Fi automatic recovery feature as well as how to enable and verify it on RW61x SDK. 1. Introduction Wi-Fi automatic recovery is a NXP proprietary feature that monitors Wi-Fi running status and recovers Wi-Fi out of exception state when running into one of the following cases: Driver fails to wakeup Wi-Fi MCU for commands/Tx Driver fails to receive command response from Wi-Fi MCU Driver detects Wi-Fi firmware is in abnormal state Once Wi-Fi automatic recovery is triggered, Wi-Fi middleware and driver will clean up the running states, reset Wi-Fi MCU power, reload Wi-Fi firmware and restart Wi-Fi initialization. It will not impact the ongoing Bluetooth LE/802.15.4 activities. Figure 1 is the Wi-Fi software architecture. Figure 1: Wi-Fi Software Architecture Figure 2 shows the work flow of Wi-Fi automatic recovery: Figure 2: Wi-Fi Automatic Recovery Work Flow Wi-Fi driver detects command timeout/wakeup card timeout/FW exception   Wi-Fi driver triggers WLAN reset to Stop Wi-Fi activities and de-initialize Wi-Fi Reset Wi-Fi power Reload the Wi-Fi only firmware and wait for the firmware to be active Send an event to notify the application before resetting it   2. SDK Configuration The Wi-Fi automatic recovery feature is not enabled by default in RW61x SDK. It needs to be enabled explicitly: Add below line in <example>/source/wifi_config.h to enable the feature  #define CONFIG_WIFI_RECOVERY 1 Besides, please also make sure the "CONFIG_WIFI_RESET" macro is defined as "1" in the SDK.   3. Automatic Recovery Verification This section introduces how to verify the Wi-Fi automatic recovery feature on RW61x SDK. wifi_cli application is used as example here together with the RW612 RD board. Refer to UM11799: NXP Wi-Fi and Bluetooth Demo Applications for RW61x for steps to flash and run Wi-Fi applications. Below are the steps to verify the Wi-Fi automatic recovery feature: Step 1: Define CONFIG_WIFI_RECOVERY in wifi_cli/source/wifi_config.h     #define CONFIG_WIFI_RECOVERY 1 Step 2: Build and flash the wifi_cli application onto RW612 RD board Step 3: Connect RW612 RD board to a serial terminal Step 4: Reset the power of RW612 RD board Step 5: Trigger Wi-Fi MCU into hung-up state with the following command to mimic a command timeout     # wlan-recovery-test Step 6: Wi-Fi recovery background task detects Wi-Fi FW hang and starts recovery process [wifi] Warn: Command response timed out. command 0x8b, len 12, seqno 0x1c timeout happends. # app_cb: WLAN: FW hang Event: 14 --- Disable WiFi --- [wifi] Warn: Recovery in progress. command 0x10 skipped [wifi] Warn: Recovery in progress. command 0x10 skipped [wifi] Warn: Recovery in progress. command 0xaa skipped [dhcp] Warn: server not dhcpd_running. --- Enable WiFi --- Initialize WLAN Driver [wifi] Warn: WiFi recovery mode done! Wi-Fi cau temperature : 31 STA MAC Address: C0:95:DA:01:1D:A6 board_type: 2, board_type mapping: 0----QFN 1----CSP 2----BGA app_cb: WLAN initialized ======================================== WLAN CLIs are initialized ======================================== ENHANCED WLAN CLIs are initialized ======================================== HOST SLEEP CLIs are initialized ======================================== CLIs Available: ======================================== help clear wlan-version wlan-mac wlan-thread-info wlan-net-stats wlan-set-mac <MAC_Address> wlan-scan wlan-scan-opt ssid <ssid> bssid ... wlan-add <profile_name> ssid <ssid> bssid... wlan-remove <profile_name> wlan-list wlan-connect <profile_name> wlan-connect-opt <profile_name> ... wlan-reassociate wlan-start-network <profile_name> wlan-stop-network wlan-disconnect wlan-stat wlan-info wlan-address wlan-uap-disconnect-sta <mac address> wlan-get-uap-channel wlan-get-uap-sta-list wlan-ieee-ps <0/1> wlan-set-ps-cfg <null_pkt_interval> wlan-deep-sleep-ps <0/1> wlan-get-beacon-interval wlan-get-ps-cfg wlan-set-max-clients-count <max clients count> wlan-get-max-clients-count wlan-rts <sta/uap> <rts threshold> wlan-frag <sta/uap> <fragment threshold> wlan-host-11k-enable <0/1> wlan-host-11k-neighbor-req [ssid <ssid>] wlan-host-11v-bss-trans-query <0..16> wlan-mbo-enable <0/1> wlan-mbo-nonprefer-ch <ch0> <Preference0: 0/1/255> <ch1> <Preference1: 0/1/255> wlan-get-log <sta/uap> <ext> wlan-roaming <0/1> <rssi_threshold> wlan-multi-mef <ping/arp/multicast/del> [<action>] wlan-wakeup-condition <mef/wowlan wake_up_conds> wlan-auto-host-sleep <enable> <mode> <rtc_timer> <periodic> wlan-send-hostcmd wlan-ext-coex-uwb wlan-set-uap-hidden-ssid <0/1/2> wlan-eu-crypto-rc4 <EncDec> wlan-eu-crypto-aes-wrap <EncDec> wlan-eu-crypto-aes-ecb <EncDec> wlan-eu-crypto-ccmp-128 <EncDec> wlan-eu-crypto-ccmp-256 <EncDec> wlan-eu-crypto-gcmp-128 <EncDec> wlan-eu-crypto-gcmp-256 <EncDec> wlan-set-antcfg <ant_mode> <evaluate_time> <evaluate_mode> wlan-get-antcfg wlan-scan-channel-gap <channel_gap_value> wlan-wmm-stat <bss_type> wlan-reset wlan-set-regioncode <region-code> wlan-get-regioncode wlan-11d-enable <sta/uap> <0/1> wlan-uap-set-ecsa-cfg <block_tx> <oper_class> <new_channel> <switch_count> <bandwidth> wlan-csi-cfg wlan-set-csi-param-header <sta/uap> <csi_enable> <head_id> <tail_id> <chip_id> <band_config> <channel> <csi_monitor_enable> <ra4us> wlan-set-csi-filter <opt> <macaddr> <pkt_type> <type> <flag> wlan-txrx-histogram <action> <enable> wlan-subscribe-event <action> <type> <value> <freq> wlan-reg-access <type> <offset> [value] wlan-uapsd-enable <uapsd_enable> wlan-uapsd-qosinfo <qos_info> wlan-uapsd-sleep-period <sleep_period> wlan-tx-ampdu-prot-mode <mode> wlan-rssi-low-threshold <threshold_value> wlan-rx-abort-cfg wlan-set-rx-abort-cfg-ext enable <enable> margin <margin> ceil <ceil_thresh> floor <floor_thresh> wlan-get-rx-abort-cfg-ext wlan-cck-desense-cfg wlan-net-monitor-cfg wlan-set-monitor-filter <opt> <macaddr> wlan-set-monitor-param <action> <monitor_activity> <filter_flags> <radio_type> <chan_number> wlan-set-tsp-cfg <enable> <backoff> <highThreshold> <lowThreshold> <dutycycstep> <dutycycmin> <highthrtemp> <lowthrtemp> wlan-get-tsp-cfg wlan-get-signal wlan-set-bandcfg wlan-get-bandcfg wlan-set-ips <option> wlan-enable-disable-htc <option> wlan-set-su <0/1> wlan-set-forceRTS <0/1> wlan-set-mmsf <enable> <Density> <MMSF> wlan-get-mmsf wlan-set-multiple-dtim <value> wlan-set-country <country_code_str> wlan-set-country-ie-ignore <0/1> wlan-single-ant-duty-cycle <enable/disable> [<Ieee154Duration> <TotalDuration>] wlan-dual-ant-duty-cycle <enable/disable> [<Ieee154Duration> <TotalDuration> <Ieee154FarRangeDuration>] wlan-external-coex-pta enable <PTA/WCI-2/WCI-2 GPIO> ExtWifiBtArb <enable/disable> PolGrantPin <high/low> PriPtaInt <enable/disable> StateFromPta <state pin/ priority pin/ state input disable> SampTiming <Sample timing> InfoSampTiming <Sample timing> TrafficPrio <enable/disable> CoexHwIntWic <enable/disable> wlan-sta-inactivityto <n> <m> <l> [k] [j] wlan-get-temperature wlan-auto-null-tx <sta/uap> <start/stop> wlan-detect-ant <detect_mode> <ant_port_count> channel <channel> ... wlan-recovery-test wlan-get-channel-load <set/get> <duration> wlan-get-txpwrlimit <subband> wlan-set-chanlist wlan-get-chanlist wlan-set-txratecfg <sta/uap> <format> <index> <nss> <rate_setting> <autoTx_set> wlan-get-txratecfg <sta/uap> wlan-get-data-rate <sta/uap> wlan-get-pmfcfg wlan-uap-get-pmfcfg wlan-set-ed-mac-mode <interface> <ed_ctrl_2g> <ed_offset_2g> <ed_ctrl_5g> <ed_offset_5g> wlan-get-ed-mac-mode <interface> wlan-set-tx-omi <interface> <tx-omi> <tx-option> <num_data_pkts> wlan-set-toltime <value> wlan-set-rutxpwrlimit wlan-11ax-cfg <11ax_cfg> wlan-11ax-bcast-twt <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-setup <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-teardown <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-report wlan-get-tsfinfo <format-type> wlan-set-clocksync <mode> <role> <gpio_pin> <gpio_level> <pulse width> wlan-suspend <power mode> ping [-s <packet_size>] [-c <packet_count>] [-W <timeout in sec>] <ipv4/ipv6 address> iperf [-s|-c <host>|-a|-h] [options] dhcp-stat ======================================== --- Done --- Step 7: Run other Wi-Fi shell commands to confirm Wi-Fi resumes to normal state  
記事全体を表示
Using the Signal Frequency Analyzer (SFA) to Measure the FRO 6M Frequency Overview The Signal Frequency Analyzer (SFA) is a specialized hardware peripheral available in NXP’s KW45, MCXW71 microcontrollers. It is designed to provide precise, real-time measurement and analysis of digital signal characteristics, including frequency, period, and timing intervals. This makes it a valuable tool for applications requiring accurate timing diagnostics, signal validation, and system debugging. By utilizing internal 32-bit counters and configurable trigger mechanisms, the SFA enables high-resolution capture of signal transitions, supporting robust system monitoring and fault detection. Functional Capabilities of the SFA The SFA module supports the following measurements: Clock signal frequency of a Clock Under Test (CUT) Clock signal period It operates using two 32-bit counters: One for the Reference Clock (REF) One for the Clock Under Test (CUT) Measurement is performed by comparing the counts of both clocks until predefined target values are reached. FRO 6M Frequency Failure Scenarios The 6 MHz Free Running Oscillator (FRO6M) may occasionally output an incorrect frequency under certain conditions: When the device exits reset When the device wakes from low-power modes To mitigate potential issues caused by incorrect FRO6M output, it is the application developer’s responsibility to verify the oscillator’s frequency and apply corrective measures as needed. Monitoring the FRO 6M Using the SFA To monitor the FRO6M signal, the following configuration is recommended: SFA Configuration Parameters Reference Clock (REF): CPU Clock (e.g., 96 MHz) Clock Under Test (CUT): FRO6M routed via CLKOUT Interrupt Mode: Enabled for asynchronous measurement completion Code Implementation The presented functions are meant to be implemented in users application, the inner functions are part of the implementations of the SFA driver from the NXP’s SDK. It can be used on MCXW71, KW45 just make sure SFA Peripheral Initialization  void init_SFA_peripheral(void) { /* Enable SFA interrupt. */ EnableIRQ(SFA_IRQn); /* Set SFA interrupt priority. */ NVIC_SetPriority(SFA_IRQn, 1); SFA_Init(DEMO_SFA_BASEADDR); SFA_InstallCallback(DEMO_SFA_BASEADDR, EXAMPLE_SFA_CALLBACK); } SFA Callback Function void EXAMPLE_SFA_CALLBACK(status_t status) { if (status == kStatus_SFA_MeasurementCompleted) { SfaMeasureFinished = true; } sfa_callback_status = status; } Frequency Measurement Function This function sets up the measurement of the FRO6M signal using the CPU clock as the reference. uint8_t SFA_freq_measurement_6M_FRO(void) { uint8_t ratio = 0; uint32_t freq = 0UL; sfa_config_t config; CLOCK_SetClkOutSel(kClockClkoutSelSirc); //set clokout to SIRC SFA_GetDefaultConfig(&config); //Get SFA default config config.mode = kSFA_FrequencyMeasurement0; config.refSelect = kSFA_REFSelect1; //Set CPU clk as ref clk config.cutSelect = kSFA_CUTSelect1; //Set clkout as CUT config.refTarget = 0xFFFFFFUL; config.cutTarget = 0xFFFFUL; config.enableCUTPin = true; freq = get_ref_freq_value(CPU_CLK); SFA_SetMeasureConfig(DEMO_SFA_BASEADDR, &config); SFA_MeasureNonBlocking(DEMO_SFA_BASEADDR); while (1) { if (SfaMeasureFinished) { SfaMeasureFinished = false; if(kStatus_SFA_MeasurementCompleted == sfa_callback_status) { freq = SFA_CalculateFrequencyOrPeriod(DEMO_SFA_BASEADDR, freq);//Calculate the FRO freq if(FREQ_6MHZ + TOLERANCE <= freq ) { ratio = 1; } else { if(FREQ_3MHZ + TOLERANCE <= freq) { ratio = 2; } else { if(FREQ_2MHZ + TOLERANCE <= freq) { ratio = 3; } else { ratio = 4; } } } break; } } else { __WFI(); } } return ratio; } Result Interpretation and Usage To test the FRO 6M after adding the above functions the FRO can be tested after executing: init_SFA_peripheral(); SFA_freq_measurement_6M_FRO(); The measured FRO6M frequency ratio is returned by the function SFA_freq_measurement_6M_FRO(), with the ratio you can know the current frequency output of the 6M FRO, ration 1 means 6M are being output by the FRO, ratio 2 means the frequency output of the FRO it's being cut in half meaning the FRO is outputting 3 Mhz, ration 3 means the FRO output frequency is being cut by a third part, this results in 2MHz frequency output. With this information you can: Adapt peripheral clocking if the FRO6M frequency is incorrect (This can be achieve by modifying the peripheral dividers if dividers are being used). Trigger corrective actions such as  switching to an alternate clock source Steps to Reconfigure Peripheral Clocking When FRO6M output frequency is lower Detect the Faulty FRO6M Output Use the SFA measurement as described earlier to determine if the FRO6M is operating below its expected frequency (6 MHz). If the result is significantly lower, proceed to reconfigure. Choose an Alternative Clock Source Most NXP MCUs offer multiple internal and external clock sources. Common alternatives include: FRO 192M OSC RF 32M Sys OSC RTC OSC Choose one that is: Stable Available in your current power mode Compatible with the peripheral’s timing requirements You can add more clock divers if needed to make a higher frequency clock reach a certain lower frequency. Reconfigure the Peripheral Clock Source Use the SDK’s CLOCK_Set... APIs to change the clock source. You may also need to: Adjust dividers to match the required baud rate or timing Reinitialize the peripheral with the new clock settings Example Scenario: Measuring the FRO and Adjusting UART Based on Frequency Ratio Imagine your application relies on the 6 MHz Free Running Oscillator (FRO), and its accuracy directly affects UART communication. To ensure reliable operation, you can use the System Frequency Adjustment (SFA) feature to monitor the FRO output and dynamically adjust the UART configuration. After measuring the 6 MHz FRO using the recommended method, the system returns a frequency ratio value. This value ranges from 1 to 4, where: 1 indicates the frequency is within expected limits (no issues), 2 to 4 represent varying degrees of deviation from the expected frequency. Using this ratio, you can initialize and configure the UART peripheral and its driver to compensate for any frequency variation, ensuring stable and accurate communication. */ int main(void) { BOARD_InitHardware(); uint8_t ch = 0; uint8_t FRO_ratio = 0; init_SFA_peripheral(); /*Measure FRO6M output frequency*/ FRO_ratio = SFA_freq_measurment_6M_FRO(); /*Init debug console and compensate in case a different frequency is output */ if(0 == FRO_ratio) { assert(0);//this user defined return value means something went wrong while measuring 6Mz FRO } uint32_t uartClkSrcFreq = BOARD_DEBUG_UART_CLK_FREQ/FRO_ratio;//Compensate the src frequency set for uart module CLOCK_EnableClock(kCLOCK_Lpuart1); CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq); ...... } SDK 25.0.00 Enhancements for FRO6M Calibration To address known reliability issues with the 6 MHz Free Running Oscillator (FRO6M), particularly during transitions from low-power modes, SDK version 25.06.00 introduces a set of software enhancements aimed at improving oscillator validation and calibration. Key Features Introduced FRO6M Calibration API Two new functions have been added to facilitate runtime verification of the FRO6M frequency: PLATFORM_StartFro6MCalibration() Initializes the calibration process by enabling the cycle counter, capturing a timestamp, and preparing the system to measure elapsed time using both the CPU and the FRO6M-based timestamp counter. PLATFORM_EndFro6MCalibration() Completes the calibration by comparing the time measured via CPU cycles and the FRO6M timestamp counter. This comparison determines whether the oscillator is operating at the expected 6 MHz or has erroneously locked to a lower frequency (e.g., 2 MHz). The result is stored in a global ratio variable (fwk_platform_FRO6MHz_ratio) for use by the system. These functions provide a lightweight and efficient mechanism to detect and respond to oscillator misbehavior, ensuring system stability and timing accuracy. Configuration Macro gPlatformEnableFro6MCalLowpower_d This macro enables automatic FRO6M frequency verification upon exiting low-power modes. When defined, the system will invoke the calibration functions to validate the oscillator before resuming normal operation. Default Integration The calibration mechanism is enabled by default in the SDK configuration file fwk_config.h, ensuring that all applications benefit from this safeguard without requiring manual setup. Use Case and Benefits These enhancements are particularly valuable in applications where: Precise timing is critical (e.g., wireless communication, sensor sampling). The system frequently enters and exits low-power states. Clock source integrity must be guaranteed to avoid peripheral misbehavior or timing faults. By integrating these calibration routines, developers can proactively detect and correct FRO6M frequency anomalies, improving overall system robustness and reducing the risk of runtime errors due to clock instability.  
記事全体を表示
The MCX W23 is a family of devices. All devices are Arm Cortex®-M33 based wireless microcontrollers for embedded applications supporting Bluetooth Low Energy 5.3. It can be used to develop IoT solutions. MCX W23xA supports LV_SM mode. MCX W23xB supports HV_SM and XR_SM mode. Building on NXP's strong history of providing industrial edge solutions, the MCX W series offers a wide operating temperature range from -40 °C to 125 °C. The Arm Cortex-M33 provides a security foundation, offering isolation to protect valuable IP and data with Trust Zone technology. It simplifies the design and software development of digital signal control systems with the integrated digital signal processing (DSP) instructions. To support security requirements, the MCX W23 also offers support for SHA-1, SHA2-256, AES, RSA, ECC, UUID, dynamic encryption, and decryption of the flash data using a PRINCE engine, debug authentication, and TBSA-M compliance.   Documents Reference Manual Fact sheet Data Sheet Errata for MCX W23xUIK MCX W23 Hardware Design Guide Secure Reference manual** European Union Declaration of Conformity for FRDM-MCXW23 FRDM-MCXW23 Board User Manual Bluetooth Specifications The MCX W23 is compatible with the Bluetooth Low Energy 5.3 specification: – Bluetooth Low Energy 5.3 controller subsystem (QDID 200592) – Bluetooth Low Energy 5.3 host subsystem (QDID 226395) – Includes a 48-bit unique Bluetooth device address – Up to 4 simultaneous connections supported The MCX W23 supports the following Bluetooth Low Energy features: – Device privacy and network privacy modes (version 5.0) – Advertising extension PDUs (version 5.0) – Anonymous device address type (version 5.0) – Up to 2 Mbps data rate (version 5.0) – Long range (version 5.0) – High-duty cycle, Non connectable advertising (version 5.0) – Channel selection algorithm #2 (version 5.0) – High output power (version 5.0) – Advertising channel index (version 5.1) – Periodic advertising sync transfer (PAST) (version 5.1) – Supports LE power control feature (version 5.2) RF antenna: 50 Ω single-ended RF receiver characteristics: – Sensitivity −94 dBm in Bluetooth Low Energy 2 Mbps – Sensitivity −97 dBm in Bluetooth Low Energy 1 Mbps – Sensitivity −100 dBm in Bluetooth Low Energy 500 kbps – Sensitivity −102 dBm in Bluetooth Low Energy 125 kbps – Accurate RSSI measurement with ±3 dB accuracy Flexible RF transmitter level configurability: – TX mode 1 (TXM1): Range from −31 dBm to +2 dBm when VDD_RF exceeds 1.1 V – TX mode 2 (TXM2): Range from −28 dBm to +6 dBm when VDD_RF exceeds 1.7   Bluetooth_5.0_Feature_Overview Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview   Training MCX W Series Training - NXP Community   Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development    Application Notes Power Management: AN14660: Power Management for MCX W23: This App Note provides information about the power manager software component. The application uses this component and the operating system to achieve optimal low-power states, based on the requirements of the application. RF: AN14575: MCX W23 Health Care IoT Peripheral Software Architecture: This App Note provides an overview of the software architecture for the MCX W23 Health care IoT Peripheral application. Designed as a model implementation, this application showcases the key features of the MCX W23 platform and serves as a foundation for developing product-quality applications. AN14659: MCX W23 Bluetooth Low Energy Power Consumption Analysis: This App Note describes the power consumption of the MCX W23 Bluetooth Low Energy (LE) device and the procedure to measure the current consumption using the MCXW23_EVK_BB and MCXW236B_RDM boards. AN2731: Compact Planar Antennas for 2.4 GHz Communication: This App Note is not an exhaustive inquiry into antenna design. It is instead focused on helping the customers understand enough board layout and antenna basics to select a correct antenna type for their application, as well as avoiding typical layout mistakes that cause performance issues that lead to delays Security: AN14657: Getting Started with Secure Boot on MCX W23: This application note covers the design of the bootloader ROM code that NXP has developed on the MCX W23, and how to use all its features. Useful Links Bluetooth LE FSCI Host Application running on FRDM-MCXN947 and MCXW23B-Click Board: The Bluetooth LE FSCI Host application demonstrates a host-side implementation for the Health Thermometer use case. It is designed to work alongside the FSCI Blackbox application, which runs on platforms such as the MCXW236 Click Board, FRDM-MCXW236, or other compatible Bluetooth LE wireless MCUs. Transmitter Maximum Output Power Override Application Note   Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization):  This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47/KW43) and MCX W7x (MCX W71/W72/W70) Power Profile Tools. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery lifetime of your solution. Development Tools    VSCode: MCUXpresso for Visual Studio Code (VS Code) provides an optimized embedded developer experience for code editing and development. Zephyr RTOs  NXP Application Code Hub: Application Code Hub (ACH) repository enables engineers to easily find microcontroller software examples, code snippets, application software packs and demos developed by our in-house experts. This space provides a quick, easy and consistent way to find microcontroller applications. NXP SPSDK: Is a unified, reliable, and easy to use Python SDK library working across the NXP MCU portfolio providing a strong foundation from quick customer prototyping up to production deployment. NXP SEC Tool: The MCUXpresso Secure Provisioning Tool us a GUI-based application provided to simplify generation and provisioning of bootable executables on NCP MCU devices. NXP OTAP Tool: Is an application that helps the user to perform an over the air firmware update of an NXP development board. Support If you have questions regarding MCX W23, please leave your question in our Wireless MCU Community! here
記事全体を表示
The customer wanted to update the FW of the PN7462 to an NFC cockpit. In general, we recommend that customers use MASS STORAGE MODE to update two files (including Flash and EEPROM) into memory. But there will always be customers who don’t know or how to successfully access MASS STORAGE MODE. They cannot succeed in doing so. Therefore, it is recommended to use the GUI FLASH tool to upgrade the FW to the NFC cabin. In order to clearly indicate the user how to use the GUI FLASH tool, this document describes this step by step.
記事全体を表示
The customer submitted a case through DFAE to seek support from NXP. They designed the product using PN5180, and according to feedback, about 10% of the boards could not read the card. The specific manifestation of the problem is: after the host issues the RF_ON command, RF field seems cannot be turned on and then fails to detect the card. Therefore, it can be seen that the problem should be on TX, not RX. The customer's device does not enable DPC and LPCD.
記事全体を表示
Generality on the Oscillation Margin Outline It is a margin to the oscillation stop and the most important item in the oscillation circuit. This margin is indicated by ratio based on the resistance of crystal, and it shows how amplification oscillation capability the circuit has. The oscillation circuit can theoretically operate if the oscillation margin is 1 or more. However, if oscillation margin is close to 1, the risk of operation failure will increase on module due to a too long oscillation start up time and so on. Such problems will be able to be solved by a larger oscillation margin. It is recommended to keep 3 times or more as oscillation margin during the startup of the oscillation. Factor of 10 is commonly requested for Automotive at startup and steady state. 5 is enough for IoT market. However, some providers accept to have 3 times as oscillation margin for steady state. Here below is an oscillation example to explain better the phenomenon: At start up, the configuration is set internally by the hardware in order to be sure to start the oscillation, the load capacitor is 0pF. After this time, it is the steady state and the load capacitor from the internal capabank is taken into account.   If load capacitor is not set correctly with the right oscillator gain, the oscillation will not be maintained after the start up.   The oscillator gain value will also depend on the resisting path on the crystal track.  A good way to evaluate it is to add a resistor on the crystal path and try to launch the oscillation. In the SDK, the gain and the load capacitor can set directly in the application code. Calculation The oscillation margin is able to be calculated as follows: The oscillation margin calculation is based on the motional resistor Rm by formula below : ESR: Crystal Equivalent Series Resistance C0: Shunt Capacitance Rm1: Motional resistor Cm1: Motional Capacitance Lm1: Motional Inductance fosc: oscillation frequency, measured with Rs_Max mounted fr: resonance frequency of the Rm1Lm1Cm1 of the crystal from (1) :    Oscillation margin is:                     Example: for the EVK board’s 32kHz crystal (NX2012SE) ESR    80000,0 Ω Rm1    79978,2 Ω Lm1    3900 H Cm1   6,00E-15 F C0      1,70E-12 F CL      1,25E-08 F fr        32901,2 Hz fosc    32771 Hz Series Resistor Rsmax        7,50E+05 Ω Oscillation Margin   10,3   Measurement Requirements for measurement PCB (for the test, it is recommended to add a series resistor on the EXTAL32k trace) Crystal unit (with equivalent circuit constants data) Resistors (SMD) Measurement equipment (Oscilloscope, Frequency counter or others capable to observe oscillation) Add a resistor to the resonator in serial and check if the oscillation circuit works or not.   If the oscillation is confirmed by 2), change the resistor to larger. If there is no oscillation, change the resistor to smaller. Find out the maximum resistor (=Rs_max) which is the resistor just before the oscillation stops. Measure the oscillating frequency with Rs_max. Calculate the oscillation margin based on the Rs_max.   Notes The Oscillation margin is affected not only by crystal characteristics but also parts that compose the oscillation circuit (MCU, capacitor and resistor). Therefore, it is recommended to check the oscillation margin after the MCU functionality is checked on your module. The series resistor is only for evaluation. Please do not use this resistor in actual usage. It is recommended to check the functionality of your module also. It is possible that the module does not work correctly due to a frequency shift on oscillation circuit and so on. A test jig and socket could be used in measurement but stray of them will give influence for oscillation margin.   KW47/MCX W72 product oscillation margin overview 32MHz crystal NXP recommends to use the quartz NDK NX1612SA 32MHz (EXS00A-CS15781) to be compliant with the +/-50ppm required in Bluetooth LE. Using the current SDK, NXP guarantees an oscillation margin of 10 for startup and steady state commonly used by Automotive customers. Higher oscillation margin can be reached by using higher ISEL and CDAC parameters with some drawback respectively on the power consumption and the clock accuracy. ( the load capacitance bank (CDAC) and the oscillator amplifier current (ISEL)) NDK recommended / target values for oscillation margin is informed case by case. On a general basis, the requested oscillation margin has to be between the recommended value and 3 times this value. "NDK quartz provider (FR) explains this oscillation margin specification is only mandatory at the start-up phase, not at the steady state. Starting the oscillation is the phase that needs more energy. That's why the gain of the oscillator gain is at the maximum value which means not optimal consumption. When the oscillation stability is reached, the gain could be reduced to save power. The oscillation will not be affected.  Keep in mind a quartz oscillates by mechanical effect. So, when the oscillation is starting you need the highest energy to emulate it. By its own inertial, you need less energy to maintain the mechanical oscillation. NDK provides a good picture of this. Starting up a crystal into oscillation is like a train what you would like to start moving. At the beginning the train is stopped and you need a lot of energy to start running. When the train is running at its nominal speed, you need less effort to maintain that movement and a very big effort to stop it completely."   Example: for the oscillation margin 10 (Series Resistor Rs_max = 560 Ω) The CDAC/ISEL area where the oscillation starts and propagates in the internal blocks is defined (green color raws) in the table below. The frequency accuracy is indicated for some of them:     32kHz crystal NXP recommends to use the quartz NDK NX2012SE (EXS00A-MU01517) or NDK NX2012SA (EXS00A-MU00801) to be compliant with the +/-500ppm required in Bluetooth LE. using the current SDK, the oscillation margin with this quartz is 10 with some limitation on the Crystal load capacitance selection (Cap_Sel) and the Oscillator coarse gain amplifier (ESR_Range) values, with some drawback respectively on the power consumption and the clock accuracy. For an oscillation margin at 10 for instance, the Capacitor value from the databank (Cap_Sel) is limited (green area) as shown in the graph below:   Example: for an oscillation margin at 6.3, if the load cap is set at 12pF and the ESR_Range to 3, the 32kHz frequency accuracy will be around -23ppm. From this point, the oscillation margin can be enlarged to 10.3 by decreasing the load cap to 6pF but the accuracy will be degraded (110ppm).   For an Oscillation margin at 10, the graph below is showing the ESR_Range versus the load cap. The possible load cap variation range (in green) is larger when the ESR_Range increases:   Example: at oscillation margin 10.3, the clock accuracy can be improved from 111ppm to 21ppm by setting the ESR_range 2 to an ESR_Range 3 but the current consumption will be increased to 169.5nA. Another important point is that for a given ESR_Range value, getting higher the load cap is much more increasing the current than in the example above.   Remark: Under a high oscillation margin condition, the crystal voltage will be smaller.   Other possible ways to improve the oscillation margin exist: - Use external capacitor instead of internal capacitor banks. Oscillation margin goes up to 10. - Use the internal 32kFRO is supported for BLE (target:+/-500ppm)              
記事全体を表示
Channel Sounding 
記事全体を表示
The MCX W72x family features a 96 MHz Arm® Cortex®-M33 core coupled with a multiprotocol radio subsystem supporting Matter, Thread, Zigbee and Bluetooth LE. The independent radio subsystem, with a dedicated core and memory, offloads the main CPU, preserving it for the primary application and allowing firmware updates to support future wireless standards. The MCX W72x also offers advanced security with an integrated EdgeLock® Secure Enclave Core Profile and will be supported by NXP's EdgeLock 2GO cloud services for credential sharing. The MCX W72x family includes Bluetooth Channel Sounding capabilities, with a dedicated on-chip Localization Compute Engine to reduce ranging latency. It incorporates additional memory to support application-specific code, connectivity stacks and over-the-air firmware updates. In addition, the radio subsystem can run the full Thread or Zigbee stack alongside the Bluetooth Low Energy stack. This delivers reliable wireless performance, as the real-time activities of the radio run on a separate core from the application. Building on NXP's strong history of providing industrial edge solutions, the MCX W series offers a wide operating temperature range from -40 °C to 125 °C and peripherals for industrial applications, including an optional CAN interface and will be part of NXP's 15-year Product Longevity program to support long-term industrial use. The MCX W series is supported by the MCUXpresso Developer Experience to optimize, ease and help accelerate embedded system development.   Security Certifications  PSA Certified Level 2 SESIP Level 2 Security Target  SESIP Level 2 KW47/MCXW72 SESIP certificate and ST are on TrustCB website Regulatory Certifications European Union Declaration of Conformity - FRDM MCXW72 European Union Declaration of Conformity - MCXW72-LOC Bluetooth Qualifications Qualified Products | Bluetooth® Technology Website Q360996: KW47 / MCX W72 Bluetooth LE 6.0 (Channel Sounding) Controller Q332147: KW47 / MCX W72 Bluetooth LE 6.0 (Channel Sounding) Host Documents MCX W72 Product Family Data Sheet MCX W72 Reference Manual Errata Sheet for MCX W72 MCXW72 Hardware Design Guide   Getting Started with Matter on MCX W72 platforms Getting Started with OpenThread on NXP MCX W72    FRDM-MCXW72 User Manual Getting Started with the FRDM-MCXW72   MCX W72-LOC User Manual Bluetooth Interested in Bluetooth technology? Bluetooth® Low Energy Primer – Essential reading for understanding BLE fundamentals. Bluetooth® Specifications – Full list of standards, protocols, and technical documents. Awards and Recognition - Every year, the Bluetooth Special Interest Group (SIG) celebrates the hard work and commitment of working groups, committee members, and contributors who have been recognized by their peers as making a difference in advancing Bluetooth technology.  2024: Channel Sounding 2025: Channel sounding amplitude-based attack resilience, LE test mode enhancements and Ranging profile and service.  Bluetooth Feature Overview Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview Bluetooth_6.1_Feature_Overview Bluetooth_6.2_Feature_Overview Bluetooth_6.3_Feature_Overview Application Notes Software, Hardware and Peripherals: AN14850 Boosting application performance with MCX W72: This application note describes the usage of the dual-core architecture in the MCX W72 microcontroller to improve performance in generic embedded applications. AN14937 32kHz Crystal-less mode on MCX W72: This application note provides information on the 32 kHz Crystal-less mode on the MCX W72 device. This mode allows you to reduce the cost of the system, without compromising the 32 kHz clock accuracy. The Free‑Running Oscillator (FRO32K) is used as the 32 kHz clock source and is calibrated against the 32 MHz RF oscillator through the Signal Frequency Analyzer (SFA) module of MCX W72 AN14745 Features, Usage, and Capabilities of Smart Power Switch on the MCX W72: This application note describes the use of the smart power switch in the MCX W72microcontroller. The MCX W72 integrates a programmable solid-state switch that turns connected components on or off, including MCX W72 power domains. AN14747 Loadpull test Report for MCX W72: This document explains the purpose of measuring the supply current, the transmit power, and the harmonics level. These measurements are monitored while the complex output load seen by the device under test (DUT) is tuned in amplitude and phase. Power Management:  AN14739 MCX W72 Bluetooth Low Energy Power Consumption Analysis: This document provides the power consumption analysis of the MCX W72 (IIOT) wireless MCU using the MCXW72-EVK board AN14745 Features Usage and Capabilities of Smart Power Switch on MCX W72 Microcontroller:  This application note describes the use of the smart power switch in the MCX W72 microcontroller. The MCX W72 integrates a programmable solid-state switch that turns connected components on or off, including MCX W72 power domains. AN14841 802.15.4 Matter and Zigbee Power Consumption Analysis for MCX W72: This document provides the power consumption analysis of the Kinetis MCX W72 (IIoT) wireless MCUs. AN14742 Power Management Hardware for the MCX W72: This application note describes the usage of the different modules dedicated to power management in the MCX W72microcontroller AN14664 Coincell Hardware Recommendations for Kinetis BLE Applications: his document describes some hardware and software solutions to minimize the peaks of current at the coin cell level AN14889: FRDM-MCXW72 Radio Frequency System Evaluation Report for Bluetooth Low Energy and for IEEE 802.15.4 This document provides the radio frequency (RF) evaluation test results of the FRDM-MCXW72 board for Bluetooth Low Energy (2FSK modulation) and IEEE 802.15.4 (OQPSK modulation) applications.  RF: AN14865 Channel Sounding Fundamentals for the KW47 and MCX W72: This document provides an overview of the fundamentals for CS technology and how it can be used for custom solutions and applications. AN14779 Printed Channel Sounding Antennas for the KW47 and MCX W72: his application note is focused on printed antennas implemented on printed-circuit boards (PCB), designed by NXP for the KW47 and MCX W72 controllers AN14832 Fundamental Steps to Design a Channel Sounding Board - Creating a Simple PCB without Diversity: In this document, an example of a minimalistic CS subsystem is presented. Attention is paid to the Radio-Frequency (RF) path, since RF circuitry strongly influences the properties of the whole CS application. AN14747 Loadpull Test Report for MCX W72: This document explains the purpose of measuring the supply current, the transmit power, and the harmonics level. These measurements are monitored while the complex output load seen by the device under test (DUT) is tuned in amplitude and phase. AN14868 RF Modeling of Channel Sounding in ANSYS: focuses on techniques for simulating and analyzing channel sounding in wireless communication systems using ANSYS tools AN14855 Channel Sounding Tests in Different Environments: This application note is about Bluetooth Channel Sounding (CS), a technique for measuring the distance between two devices in the Bluetooth frequency band. It explains key factors affecting accuracy AN14869 Fundamental Steps to Design a Complex Channel Sounding Board:  It focuses on creating hardware that supports advanced CS features, including antenna diversity and optimized RF paths, to improve accuracy and mitigate issues like multipath propagation. AN2731 Compact Planar Antennas for 2.4GHz Communication: This document is not an exhaustive inquiry into antenna design. It is instead focused on helping the customers understand enough board layout and antenna basics to select a correct antenna type for their application, as well as avoiding typical layout mistakes that cause performance issues that lead to delays Security: AN14648 MCX W72 In-System Programming Utility: The document provides steps to boot the MCX W72 MCU in ISP mode and establish various serial connections to communicate with the MCU AN14613 MCX W72 Secure Boot using SEC tool: The MCX W72 is a low-power, highly secure, single-chip wireless MCU, the contents of flash memory can be saved as encrypted data, which can be decrypted instantly. It helps in protecting the sensitive data and algorithms. AN14646 Debug Authentication on MCX W72: This application note describes the steps for debug authentication using the MCUXpresso Secure Provisioning Tool (SEC). AN14728 MCX W72 Flash Encryption using NPX: There is an increasing requirement to protect the application code and data stored in flash memories in an encrypted form due to security reasons. The NVM PRINCE XEX (NPX) is a module inside the Flash Memory Controller (FMC) that allows customers to protect the contents of flash regions (up to four regions). It performs on-the-fly, low-latency encryption and decryption of flash contents, and it is transparent to the developer and to the Cortex-M33 platform. No special handle is needed from the perspective of the developer. AN14644 MCX W72 Managing Lifecycles: This document describes the following: Lifecycle stages that are available to the user, how to access the lifecycles, limitations of the lifecycles, how to transition to the next lifecycle AN14670 EdgeLock 2GO Provisioning via SPSDK for MCUs: EdgeLock 2GO is a fully managed cloud platform operated by NXP that provides secure provisioning services for easy deployment and maintenance of IoT devices that integrate NXP MCU, MPU, and EdgeLock SE05x secure elements. AN14624 EdgeLock 2GO PRovisioning via Secure Provisioning Tool (SEC) for MCUs: EdgeLock 2GO is a fully managed cloud platform operated by NXP that provides secure provisioning services for easy deployment and maintenance of IoT devices that integrate NXP MCU, MPU, and EdgeLock SE05x secure elements. AN14544 EdgeLock 2Go Services for MPU and MCU: EdgeLock 2GO is the service platform of NXP for provisioning and managing IoT devices. It lets you securely install keys and certificates into your devices, either during manufacturing or in the field, and then keep credentials up to date during the device life cycle. EdgeLock 2GO uses the security capability of each device, for optimal levels of security across your entire IoT fleet. Bluetooth Training Bluetooth Low Energy 6.0 NXP Training MCX W Series Training - NXP Community   RF Switch Comparison Absorptive/Reflective Standards Comparison ETSI / FCC / ARIB requirements BLE Channel Sounding  - Overview BLE Channel Sounding - RF Hardware BLE Channel Sounding - ANSYS Modeling Tools  BLE Channel Sounding - Antenna Prototypes Validation Measurements Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development  Useful Links Debug probe firmware installation for the KW47-EVK and FRDM-MCXW72 This post will cover how to install the CMSIS-DAP/SEGGER J-link firmware for the KW47-EVK and FRDM-MCXW72 using NXP’s MCU-LINK installer. Updating NBU for Wireless Examples on KW47/MCXW72This post will cover how to update the NBU firmware How to import and run demo examples with MCUXpresso for Visual Studio Code: This article gives information on how to import and run demo examples from the new SDK with ARM GCC toolchain, in MCUXpresso for Visual Studio Code. [MCUXSDK] How to use GitHub SDK for KW4x, MCXW7x, MCXW2x - NXP Community this community post provides step by step how to use GitHub SDK [MCUXSDK] GitHub SDK - Documentation for Bluetooth LE platforms - NXP Community this community post provides the documentation for BLE platforms.  The best way to build a PCB first time right with KW47 (Automotive) or MCXW72 (IoT/Industrial): In this community provides the important link to build a PCB using a KW45 or K32W148 and MCXW71 and all concerning the radio performances, low power and radio certification (CE/FCC/ICC) Workaround implementation for DCDC failure during drive strength change a DCDC failure can occur infrequently during a drive strength change to low, and the DCDC output voltage becomes greater than or equal to the current output voltage. How to use the HCI_bb on Kinetis family products and get access to the DTM mode:  This article is presenting two parts: How to flash the HCI_bb binary into the Kinetis product. Perform RF measurement using the R&S CMW270 BLE HCI Application to set transmitter/receiver test commands: This article provides the steps to show how user could send serial commands to the device. Bluetooth LE HCI Black Box Quick Start Guide : This article describes a simple process for enabling the user controls the radio through serial commands. Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization):  This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47/KW43) and MCX W7x (MCX W71/W72/W70) Power Profile Tools. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery lifetime of your solution. KW47/MCXW72 32MHz & 32kHz Oscillation margins: this article provides the properly configuration for the Oscillation margins for the circuit. Videos NXP Channel Sounding technology interfacing with Google Pixel 10 This is a demo showing the MCX W72 LOC board interacting with Google Pixel 10 phone using channel sounding Exploring Bluetooth Channel Sounding on FRDM-MCXW72 - Part 1: In this video, you will see step‑by‑step how Bluetooth® Channel Sounding works using NXP’s Rate2 distance‑estimation solution. Performing the demonstration includes a computer with VS Code, the MCUXpresso extension and toolchains installed, a FRDM‑MCXW72 development board and a smartphone running the BLE Hero application. Exploring Bluetooth Channel Sounding on FRM-MCXW72 - Part 2:  Concluding the demonstration of Bluetooth® Channel Sounding, part two of this presentation continues with a brief review of the testing setup and walks you through running board‑to‑board measurements Support If you have questions regarding MCX W72, please leave your question in our Wireless MCU Community! here
記事全体を表示
KW47 family features a 96 MHz Arm® Cortex®-M33 core coupled with a Bluetooth LE subsystem. The independent radio subsystem, with a dedicated core and memory, offloads the main CPU, preserving it for the primary application and allowing firmware updates to support future wireless standards. The KW47 also offers advanced security with an integrated EdgeLock® Secure Enclave Core Profile and will be supported by NXP's EdgeLock 2GO cloud services for credential sharing. The KW47 family includes Bluetooth Channel Sounding capabilities, with a dedicated on-chip Localization Compute Engine to reduce ranging latency. It incorporates additional memory to support application-specific code, connectivity stacks and over-the-air firmware updates. This delivers reliable wireless performance, as the real-time activities of the radio run on a separate core from the application. Building on NXP's strong history of providing automotive solutions, the KW47 family offers a wide operating temperature range from -40 °C to 125 °C and peripherals for automotive applications, KW47 will be part of NXP's 15-year Product Longevity program to support long-term use. The KW47 series is supported by the MCUXpresso Developer Experience to optimize, ease and help accelerate embedded system development.   KW47 boards KW47-EVK Getting Started with the KW47 EVK KW47-EVK Board User Manual KW47-M2 Board User Manual  KW47-EVK Quick Start Guide KW47-M2 Quick Start Guide   KW47-LOC Getting Started with the KW47-LOC KW47-LOC Board User Manual KW47-LOC Quick Start Guide KW47: Bluetooth Channel Sounding MCU with On-Chip Localization Compute Engine the KW47 Security Certifications  PSA Certified Level 2 SESIP Level 2 Security Target  SESIP Level 2 KW47/MCXW72 SESIP certificate and ST are on TrustCB website  Regulatory Certifications European Union Declaration of Conformity - KW47-EVK European Union Declaration of Conformity - KW47-LOC Bluetooth Qualifications Qualified Products | Bluetooth® Technology Website Q360996: KW47 / MCX W72 Bluetooth LE 6.0 (Channel Sounding) Controller Q332147: KW47 / MCX W72 Bluetooth LE 6.0 (Channel Sounding) Host Documents  KW47 Product Family Data Sheet KW47 Reference Manual Errata for KW47 KW47 Hardware Design Guide Bluetooth Interested in Bluetooth technology? Bluetooth® Low Energy Primer – Essential reading for understanding BLE fundamentals. Bluetooth® Specifications – Full list of standards, protocols, and technical documents. Awards and Recognition - Every year, the Bluetooth Special Interest Group (SIG) celebrates the hard work and commitment of working groups, committee members, and contributors who have been recognized by their peers as making a difference in advancing Bluetooth technology, like NXP! 2024: Channel Sounding 2025: Channel sounding amplitude-based attack resilience, LE test mode enhancements and Ranging profile and service.  Bluetooth Feature Overview Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview Bluetooth_6.1_Feature_Overview Bluetooth_6.2_Feature_Overview Bluetooth_6.3_Feature_Overview Application Notes Software, Hardware and Peripherals: AN14884 32kHz Cristal-less mode on KW47: This application note provides information on the 32 kHz Crystal-less mode on the KW47 device. This mode allows you to reduce the cost of the system, without compromising the 32 kHz clock accuracy.  AN14846 Boosting Application Performance with the KW47 Dual-Core Architecture: This application note describes how to use the dual-core architecture in the KW47 microcontroller to improve performance in generic embedded applications AN14796 Migration Guide from the KW45 to the KW47:  This document describes the procedure to migrate from KW45B41Z to KW47 with emphasis on the connectivity software. The document is intended for software engineers, software testers, software integrators, and customers designing their own hardware. Power Management: AN14709 Power Management Hardware for the KW47: This application note describes the usage of the different modules dedicated to power management in the KW47microcontroller. TheKW47integrates a DC-DC buck converter, a couple of low-dropout regulators, and a programmable solid-state switch to turn on/off theKW47power domains AN14684 Features, Usage, and Capabilities of Smart Power Switch on the KW47 Microcontroller: This application note describes the use of the smart power switch in the KW47 microcontroller. The KW47 integrates a programmable solid-state switch that turns connected components on or off, including KW47 power domains AN14664 Coincell Hardware Recommendations for Kinetis BLE Applications: his document describes some hardware and software solutions to minimize the peaks of current at the coin cell level AN14554 KW47 Bluetooth Low Energy Power Consumption Analysis:  This document provides the power consumption analysis of the Kinetis KW47 (automotive) wireless MCU using the KW47-EVK board RF: AN14940 KW47 Coexistence with RF System Evaluation Report for the Bluetooth LE Applications: This document provides the coexistence RF evaluation test results of the KW47-EVK for Bluetooth LE applications (2FSK modulation). It includes the test setup description and the tools used to perform the tests on your own. For the KW47 radio parameters AN14461 KW47-EVK RF System Evaluation Report for Bluetooth LE Applications: This document provides the RF evaluation test results of the KW47-EVK board for Bluetooth LE (2FSK modulation) applications. It includes the test setup description and the tools used to perform the tests. AN14826 KW47-LOC System Evaluation Report for BLE Applications: This document provides the RF evaluation test results of the KW47 Localization board (KW47-LOC) for Bluetooth LE (2FSK modulation) applications. It includes the test setup description, and the tools used to perform the tests on your own. AN14696 Loadpull Test Report for KW47: This document explains the purpose of measuring the supply current, the transmit power, and the harmonics level. These measurements are monitored while the complex output load seen by the device under test (DUT) is tuned in amplitude and phase. AN14628 KW47 CCC Channel Sounding Power Profile Analysis:  this document explains power consumption measurement at each step of the full distance measurement procedure, changing of the code to set the different option in the SDK software, and usage of the associated power profile estimator tool. AN14865 Channel Sounding Fundamentals for the KW47 and MCX W72: This document provides an overview of the fundamentals for CS technology and how it can be used for custom solutions and applications. AN14832 Fundamental Steps to Design a Channel Sounding Board - Creating a Simple PCB without Diversity: In this document, an example of a minimalistic CS subsystem is presented. Attention is paid to the Radio-Frequency (RF) path, since RF circuitry strongly influences the properties of the whole CS application. AN14779 Printed Channel Sounding Antennas for the KW47 and MCX W72: his application note is focused on printed antennas implemented on printed-circuit boards (PCB), designed by NXP for the KW47 and MCX W72 controllers AN14720 Creation of Firmware Update Image for KW47 using Over the Air Programming Tool: This document outlines the steps to create and upgrade the image on the KW47–EVK board AN14868 RF Modeling of Channel Sounding in ANSYS: focuses on techniques for simulating and analyzing channel sounding in wireless communication systems using ANSYS tools AN14855 Channel Sounding Tests in Different Environments: This application note is about Bluetooth Channel Sounding (CS), a technique for measuring the distance between two devices in the Bluetooth frequency band. It explains key factors affecting accuracy AN14869 Fundamental Steps to Design a Complex Channel Sounding Board:  It focuses on creating hardware that supports advanced CS features, including antenna diversity and optimized RF paths, to improve accuracy and mitigate issues like multipath propagation. AN2731 Compact Planar Antennas for 2.4 GHz Communication: This document is not an exhaustive inquiry into antenna design. It is instead focused on helping the customers understand enough board layout and antenna basics to select a correct antenna type for their application, as well as avoiding typical layout mistakes that cause performance issues that lead to delays Security: AN14727 KW47 Flash Encryption using NPX: There is an increasing requirement to protect the application code and data stored in flash memories in an encrypted form due to security reasons. The NVM PRINCE XEX (NPX) is a module inside the Flash Memory Controller (FMC) that allows customers to protect the contents of flash regions (up to four regions). It performs on-the-fly, low-latency encryption and decryption of flash contents, and it is transparent to the developer and to the Cortex-M33 platform. No special handle is needed from the perspective of the developer. AN14607 KW47 Secure Boot using SEC tool: The KW47 is a low-power, highly secure, single-chip wireless MCU, the contents of flash memory can be saved as encrypted data, which can be decrypted instantly. It helps in protecting the sensitive data and algorithms. AN14647 KW47-LOC In-System Programming Utility: The document provides steps to boot the KW47 MCU in ISP mode and establish various serial connections to communicate with the MCU AN14653 Debug Authentication on KW47: This application note describes the steps for debug authentication using the MCUXpresso Secure Provisioning Tool (SEC). AN14649 KW47-EVK In-System Programming Utility: This document provides steps to boot the KW47 MCU into ISP mode and establish various serial connections to communicate with the MCU. AN14643 KW47 Managing Lifecycles: This document describes the following: Lifecycle stages that are available to the user, how to access the lifecycles, limitations of the lifecycles, how to transition to the next lifecycle Training Bluetooth Low energy 6.0 NXP Introduction KW4x: Automotive Bluetooth Low Energy MCUs for Secure Car Access RF Switch Comparison Absorptive/Reflective Standards Comparison ETSI / FCC / ARIB requirements BLE Channel Sounding  - Overview BLE Channel Sounding - RF Hardware BLE Channel Sounding - ANSYS Modeling Tools  BLE Channel Sounding - Antenna Prototypes Validation Measurements   Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development  Useful Links How to run KW47-M2 standalone - NXP Community Debug probe firmware installation for the KW47-EVK and FRDM-MCXW72 This post will cover how to install the CMSIS-DAP/SEGGER J-link firmware for the KW47-EVK and FRDM-MCXW72 using NXP’s MCU-LINK installer. Updating NBU for Wireless Examples on KW47/MCXW72This post will cover how to update the NBU firmware How to import and run demo examples with MCUXpresso for Visual Studio Code: This article gives information on how to import and run demo examples from the new SDK with ARM GCC toolchain, in MCUXpresso for Visual Studio Code. [MCUXSDK] How to use GitHub SDK for KW4x, MCXW7x, MCXW2x - NXP Community this community post provides step by step how to use GitHub SDK [MCUXSDK] GitHub SDK - Documentation for Bluetooth LE platforms - NXP Community this community post provides the documentation for BLE platforms.  The best way to build a PCB first time right with KW47 (Automotive) or MCX W72 (IoT/Industrial) - NXP Community : In this community provides the important link to build a PCB using a KW47 and MCX W72 and all concerning the radio performances, low power and radio certification (CE/FCC/ICC). Workaround implementation for DCDC failure during drive strength change a DCDC failure can occur infrequently during a drive strength change to low, and the DCDC output voltage becomes greater than or equal to the current output voltage. How to use the HCI_bb on Kinetis family products and get access to the DTM mode:  This article is presenting two parts: How to flash the HCI_bb binary into the Kinetis product. Perform RF measurement using the R&S CMW270 BLE HCI Application to set transmitter/receiver test commands: This article provides the steps to show how user could send serial commands to the device. Bluetooth LE HCI Black Box Quick Start Guide : This article describes a simple process for enabling the user controls the radio through serial commands. Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization):  This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47/KW43) and MCX W7x (MCX W71/W72/W70) Power Profile Tools. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery lifetime of your solution. KW47/MCXW72 32MHz & 32kHz Oscillation margins: this article provides the properly configuration for the Oscillation margins for the circuit. Changing CAN interface configuration on KW47-EVK while using serial terminal:Most available example applications use UART as the serial interface for terminal communication. This approach is commonly chosen because a terminal provides a simple and efficient method for interacting with the application during development and debugging. Reference Designs Bluetooth Ranging Access Vehicle Enablement System - NXP Community Blue Ravens (Bluetooth Ranging Access Vehicle Enablement System) is a system solution developed by NXP to assist customers in designing their own BLE-based car access solutions using NXP products. Videos NXP Channel Sounding technology interfacing with Google Pixel 10 This is a demo showing the MCX W72 LOC board interacting with Google Pixel 10 phone using channel sounding Support If you have questions regarding KW47, please leave your question in our Wireless MCU Community! here
記事全体を表示
Wireless Equipment: Ellisys:  Ellisys is a leading worldwide supplier of advanced protocol test solutions for Bluetooth®, Wi-Fi, WPAN, USB 2.0, SuperSpeed USB 3.1, USB Power Delivery, USB Type-C, DisplayPort and Thunderbolt technologies.  USB, Bluetooth and WiFi Protocol Test Solutions  Bluetooth Vanguard - Advanced Bluetooth Analysis System Bluetooth Qualifier - Bluetooth Qualification System   RFcreations:     RFcreations is a core team of highly skilled and knowledgeable, professional engineers with decades of experience across the design and development of both RF and digital hardware, embedded, protocol stacks and UI software mini-moreph morephCS   Teledyne Lecroy:    offers an extensive range of test solutions to help with design, development, and deployment of devices and systems frontline-x240 Wireless Protocol Analyzer  frontline-x500e Wireless Protocol Analyzer  Rohde&Schwarz:        is a global technology group striving for a safer and connected world. Offers Test & Measurement, Technology Systems and Networks & Cybersecurity Divisions R&S CMW270 wireless connectivity tester Useful links:  Top Online Bluetooth LE learning Resource Ellisys Bluetooth Video Series RFcreations Bluetooth Sniffers and Test Tools Learn Bluetooth Low Energy in a single weekend
記事全体を表示
The wireless examples feature many common Bluetooth, zigbee and thread configurations. This article describes each SDK example.  MCUs: KW45 K32W1 KW47 MXCW71/72 Category SDK Example Name Description comments BLE Controller hci_bb the HCI black box demo gives access to the BLE controller via serial interface using commands and events.    Bluetooth adv_ext_central the adv_ext_central implements a custom GATT based temperature Profile. After pairing with the peripheral, it configures notifications and displays temperature values on a terminal.  Board to Board Bluetooth adv_ext_peripheral the adv_ext_peripheral implements a custom GATT based temperature Profile. it begins with a general discoverable mode and waits for the central node to connect and configure notifications for the temperature value.  Board to Board Bluetooth ancs_c the demo acts as a peripheral that advertises a service solicitation for custom ANCS service. Also, can acts as a client once connected to the device offering the ANCS service. The application displays information about ANCS notifications received from the mobile. this service is available on iOS mobile devices.   Bluetooth beacon the demo has non-connectable advertising packets that are sent on the three advertising channels. From the info sent by the beacon we can see: company identifier.  beacon identifier.  UUID, by default this value is a random value based on the UI of the board.  some beacon application data  RSSI IoT toolbox app Bluetooth ble_fscibb implements a custom GATT based wireless UART profile. it can be possible to interact with the device through a serial terminal.    Serial Terminal  Bluetooth ble_shell implements a console application that allows the user to interact with a full feature BLE stack library. implements GAP roles and both client and server, to enabling these roles can be done using some commands. this demo allows the user to add, erase or modify services.  Serial Terminal Bluetooth eatt_central the application behaves as a GAP central node. It scans for an EATT peripheral to connect to. Once connected it performs service discovery, initiates an EATT connection and configures indications on the peripheral for services A and B.  The central reports the received service data and steps taken during the setup on a serial terminal.  Board to Board Bluetooth eatt_peripheral the application behaves as a GAP peripheral node. it works a as general discoverable mode and waits for a GAP central node to connect. This application implements two services, Service A and Service B. After the EATT connection in completed, the peer must enable indications for the two services to periodically receive profile data over EATT.   Board to Board Bluetooth hid_device (Mouse) the demo moves the cursor in a square pattern between a min and max axis. this demo behaves as a GAP peripheral node with a general discoverable mode that waits for a GAP central node to connect.    Bluetooth hid_host the application behaves as a GAP central node. it works as a GAP limited discovery Procedure and searches for HID devices to connect to. After connecting with the peripheral node, it configures notifications and displays the received HID reports on a serial terminal.  Serial Terminal Bluetooth loc_reader the application behaves as a GAP peripheral node. This application has the RASP profile implemented; it advertises for compatible devices, once it connected begins to send ranging data to the central device.  Board to Board Bluetooth loc_user_device the application behaves as a GAP central node. it scans for compatible devices, once it connected begins to send ranging commands to the peripheral device and calculates the distance estimation based on the information received.  Board to Board Bluetooth otac_att the over the air programming client is a GAP peripheral which advertising the BLE OTAP service and waits for a connection from an OTAP server. After an OTAP server connects, the OTAP client waits for it to write the OTAP control point CCCD and then starts sending commands via ATT indications.  over the air programming tool //IoT toolbox app Bluetooth otac_I2cap (different transfer method) The over the air programming client is a GAP peripheral which advertising the BLE OTAP service and waits for a connection from an OTAP server. After an OTAP server connects, the OTAP client waits for it to write the OTAP control point CCCD and then starts sending commands via ATT indications.  over the air programming tool // IoT toolbox app Bluetooth otas the Over the air programming server application is a GAP central which scans for devices advertising the BLE OTAP service. After it finds one, it connects to it and configures the OTAP control point CCC descriptor to receive ATT indications from the device then it waits fir OTAP commands from the device.  over the air programming tool // IoT toolbox app Bluetooth temp_coll the application behaves as a GAP central node, it enters GAP limited discovery procedure and searches for sensor devices to pair with. After pairing with the peripheral, it configures notifications and displays temperature values on a serial terminal.  Board to Board Bluetooth temp_sens the application behaves as a GAP peripheral node. it enters GAP general discoverable mode and waits for a GAP central node to connect and configure notifications for the temperature value.  Board to Board Bluetooth w_uart implements a custom GATT based wireless UART profile. it can be possible to interact with the device through a serial terminal.  IoT toolbox app Bluetooth wireless_ranging Is used to perform secure and highly accurate distance estimation between two BLE device.  the application is made of two parts: The embedded firmware, that can be controlled manually via serial connection. the host application (python) running on a PC and controlling the firmware using serial link. Wireless Ranging application allows to: Configure most of the parameters required for measurement. Select what type of measurement to be performed.  Trigger CS measurements using range or test command. Log system debug information but also raw IQ data information in MatLab. Board to Board  genfsk connectivity_test   Board to Board ieee_802.15.4 connectivity_test   Board to Board reference design bluetooth this application is based on a GATT temperature Service and demonstrates power consumption optimization in BLE. The power consumption is optimized during advertising, connected and no activity states.   
記事全体を表示
The MCX W71 is a secure and ultra‑low‑power wireless microcontroller designed for Bluetooth® Low Energy 5.3 applications alongside Matter, Thread and Zigbee connectivity.  MCX W71 targets Bluetooth® LE 5.3 designs with basic connectivity requirements. Applications requiring greater scalability, advanced Bluetooth features, or long‑term feature expansion should use MCX W72 MCX W71 Block Diagram Evaluation boards FRDM-MCXW71 Page FRDM-MCXW71 User Manual FRDM-MCXW71 Getting Started   Bluetooth For the latest Bluetooth LE 6.x features please refer to MCX W72 Knowledge Hub   Support If you have questions regarding MCX W71, please leave your question in our Wireless MCU Community! here
記事全体を表示
Aiming to increase the reach of card and mobile payment, Europay, Mastercard and Visa (EMV) point of sale (POS) terminals are getting more lightweight, replacing hardware security with software and back-end security. Off-the-shelf mobile devices, like your smart phone, can become an acceptance point for payment cards, a so-called SoftPOS.
記事全体を表示
MIFARE DESFire EV1 supports the APDU message structure according to ISO/IEC 7816-4 for an optional wrapping of the native MIFARE DESFire EV1 APDU format and for the additionally implemented 7816-4 commands from a practical point of view.
記事全体を表示
 Introduction The KW45-EVK & FRDM-MCX W71 include an RSIM (Radio System Integration Module) module with an external 32 MHz crystal oscillator and 32kHz external oscillator. 32MHz clock source reference is mainly intended to supply the Bluetooth LE Radio peripheral, but it can be used as the main clock source of the MCU as well. This oscillator includes a set of programmable capacitors to support crystals with different load capacitance needs. Changing the value of these capacitors can modify the frequency the oscillator provides, that way, the central frequency can be tuned to meet the wireless protocol standards. This configurable capacitance range is from C: 3.74pF to C: 10.67pF and it is configured through the RFMC Register XO_Test field at the CDAC. The KW45 comes preprogrammed with a default load capacitance value (0x1Eh). However, since there is variance in devices due to tolerances and parasite effects, the correct load capacitance should be checked by verifying that the optimal central frequency is attained.  You will need a spectrum analyzer to measure the central frequency. To find the most accurate value for the load capacitance, it is recommended to use the Connectivity Test demo application. 32kHz clock source reference is mainly intended to run in low power when the 32MHz clock is switched off. This 32kHz clock enable to leave the low power mode and enter in Bluetooth LE events. Adjusting 32MHz Frequency Example   Program the KW45 /MCX W71 Connectivity Test software on the device. This example can be found in SDK_2_15_000_KW45B41Z-EVK_MR5\boards\kw45b41zevk\wireless_examples\genfsk\connectivity_test folder from your SDK package. Baremetal and FreeRTOS versions are available. In case that KW45-EVK board is being used to perform the test, you should move the 15pF capacitor populated in C3 to C4, to direct the RF signal on the SMA connector.                                   3. Connect the board to a serial terminal software. When you start the application,              you will be greeted by the NXP logo screen: Press the enter key to start the test. Then press "1" to select "Continuous tests":          5. Finally, select "6" to start a continuous unmodulated RF test. At this point, you should be able to measure the signal in the spectrum analyzer. You can change the RF channel from 0 to 127 ("q" Ch+ and "w" Ch- keys), which represents the bandwidth from 2.360GHz to 2.487GHz, stepping of 1MHz between two consecutive channels. To demonstrate the trimming procedure, this document will make use of channel 42 (2.402GHz) which corresponds to the Bluetooth LE channel 37. In this case, with the default capacitance value, our oscillator is not exactly placed at the center of the 2.402GHz, instead, it is slightly deflected to 2.40200155 GHz, as depicted in the following figure:         6. The capacitance can be adjusted with the "d" XtalTrim+ and "f" XtalTrim- keys. Increasing the capacitance bank means a lower frequency. In our case, we need to increase the capacitance to decrease the frequency. The nearest frequency of 2.402 GHz was 2.40199940 GHz        7. Once the appropriate XTAL trim value has been found, it can be programmed as default in any Bluetooth LE example, changing the BOARD_32MHZ_XTAL_CDAC_VALUE constant located in the board_platform.h file:   Adjusting 32kHz Frequency Example   You could adjust the capacitor bank on the 32kHz oscillator. You need to observe the 32kHz frequency at pin 45 (PTC7) using an spectrum analyzer or a frequency meter. Inserting this below code in the main(void) in your application: Hello_world application in this example. 32kHz frequency is not active by default on pin45(PTC7). You need to configure the OSC32K_RDY at 1 in the CCM32K register Status Register (STATUS) field to observe the 32kHz frequency at pin 45 (PTC7). Configure the CAP_SEL, XTAL_CAP_SEL and EXTAL_CAP_SEL field available in the CCM32K register 32kHz Oscillator Control Register (OSC32K_CTRL).       XTAL_CAP_SEL and EXTAL_CAP_SEL values are from 0pF (0x00h) to 30pF (0x0Fh). You could configure those 2 registers in the clock_config.c file. Default values are 8pF for both registers.        
記事全体を表示