无线连接知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wireless Connectivity Knowledge Base

讨论

排序依据:
       My customer asks if QN9080 can be tested with MT887x. We co-work with Anritsu Taiwan to integrate QN9080 and MT887x to perform 1M bps, 2M bps and Frame error rate test. This document will address the QN9080 setup and MT887x connection setup. We show the 1M bps, 2M bps and frame error rate results. The Anritsu equipment is applied to MT8870, MT8872 model name.        If you would like to perform the same test environment. You may contact Anritsu to get the latest "Auto-test tool " released by Anritsu and follow their SOP document to install "Auto-test tool" into PC to perform this RF validation test. 
查看全文
Hello community, This time I bring to you a document which explains what are the ZigBee Test Client commands and how to use it. Before to read this guide, I widely recommend to take a look into the document Running a demo with BeeKit (802.15.4 MAC, SMAC and ZigBee BeeStack). This guide requires the BeeKit Wireless Connectivity Toolkit​ and the Test Tool for Connectivity Products applications.     I hope you find this guide useful. Enjoy this guide! Any feedback is welcome. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
查看全文
MyWirelessAPP Demo Beacon(End device) code for RTS development
查看全文
Hello everyone, Over The Air Programming (OTAP) NXP's custom Bluetooth LE service provides the developer a solution to upgrade the software that the MCU contains. It removes the need for cables and a physical link between the OTAP client (the device that is reprogrammed) and the OTAP server (the device that contains the software update). This post explains how to run the OTAP Client Software that comes within the FRDM-KW36 package: Reprogramming a KW36 device using the OTAP Client Software. As it is mentioned in the last post, the OTAP Client can reprogram the KW36 while it is running, with new software using Bluetooth LE. However, this implementation for most of the applications is not enough since once you have reprogrammed the new image, the KW36 can not be reprogramed a second time using this method. For these applications that require to be updated many times using Bluetooth LE during run-time, we have created the following application note, that comes with a functional example of how to implement the OTAP Client software, taking advantage of this service. You can download the software clicking on the link in blue and the documentation is in the link in green. Please visit the following link: DOCUMENTS and Application Notes for KW36 In the "DOCUMENTS" section, you can found more information of the KW36. In the "Application Note" section, you can found more software and documentation of interesting topics like this.        Best Regards.
查看全文
Introduction This document describes the hardware considerations for the schematic and layout of the MKW36A512VFT4 device. This MCU is packaged into a 48-pin HVQFN - 7x7 mm, dissimilar to MKW36Z512VHT4 which comes packaged into a 48-pin LQFN - 7x7 mm (the last one takes part of FRDM-KW36).   Pin Layout  The MKW36A512VFT4 MCU is pin to pin compatible with the MKW36Z512VHT4 (FRDM-KW36) MCU, except for the DCDC pins. The following figure shows the distribution of the pins in the MKW36A512VFT4 MCU (left), compared with the MKW36Z512VHT4 (FRDM-KW36 MCU, right). Surely, this is the most important consideration for MKW36A512VFT4, since you can not simply move the FRDM-KW36 layout on your design. Minimum BOM The following figures show the minimum BOM necessary for each DCDC mode in KW36. For more information about DCDC modes and hardware guidelines, please visit: MKW4xZ/3xZ/3xA/2xZ DC-DC Power Management Bypass Mode   Buck Auto-Start Mode   Buck Manual-Start Mode     Layout Recommendations The footprint and layout are critical for RF performance, hence if the recommended design is followed exactly in the RF region of the PCB, sensitivity, output power, harmonic and spurious radiation, and range, you will succeed. For more information of layout recommendations, please visit Hardware Design Considerations for MKW35A/36A/35Z/36Z Bluetooth Low Energy Devices. The footprint recommended for the MKW36A512VFT4 is shown in the figure below. NXP prefers to use a top layer thickness of no less than 8-10 mils. The use of a correct substrate like the FR4 with a dielectric constant of 4.3 will assist you in achieving a good RF design. Other recommendations during EMC certification stages are: - Specific attention must be taken on 4 pins PTC1, 2, 3 & 4 if they are used on the application. - 4 decoupling capacitors of 3pF are mandatory on those pins and be positioned as close as possible. - Wires from those 4 pins must be underlayer. - NXP recommends putting the vias under the package in case the customer HW design rules allow it. Some recommendations for a good Vdd_RF supply layout are: - Vdd_RF1 and Vdd_RF2 lines must have the same length as possible, linked to pointA (‘Y’ connection). - 12pF decoupling capacitor from Vdd_RF wire must be connected to the Ground Antenna. The purpose is to get the path as short as possible from Vdd_RF1/Vdd_RF2 to the ground antenna. - 12pF decoupling capacitor from the Vdd_RF3 pin must be as close as possible. Return to ground must be as short as possible. So vias (2 in this below picture) must be placed near to the decoupling capacitor to get close connection to the ground layer. The recommended RF stage is shown in the following figure. The MKW36A512VFT4 has a single-ended RF output with a 2 components matching network composed of a shunt capacitor and a series inductor. Both elements transform the device impedance to 50 ohms. The value of these components may vary depending on your board layout. Avoid routing traces near or parallel to RF transmission lines or crystal signals. Maintain a continuous ground under an RF trace is critical to keep unaltered the characteristic impedance of the transmission line. Avoid routing on the ground layer that will result in disrupting the ground under RF traces. For more information about RF considerations please visit: Freescale IEEE 802.15.4 / ZigBee Package and Hardware Layout Considerations.
查看全文
Introduction In some applications, is it necessary to keep updated the software running in many MCU's that take part in the system, fortunately, Over The Air Programming, it's a custom Bluetooth LE service developed to send "over the air" software updates for the KW MCU series. FRDM-KW36 SDK already provides the "otap_client" software, that can be used together with the "otap_bootloader" such as it is described in the following community post: Reprogramming a KW36 device using the OTAP Client Software to reprogram the KW36. This example can be modified to store code for another MCU and later send the software update to this device as depicted in the figure below. This post guides you on modifying the OTAP client software to support software updates for other MCU's. Preparing the OTAP client software The starting point of the following modifications is supposing that there is no need to perform over the air updates for the KW36 MCU, so the use of the "otap_bootloader" is obsolete and will be removed in this example. In other words, KW36 will be programmed only with the "otap_client" code. Open the MCUXpresso settings window (Project->Properties->"C/C++ Build->MCU settings") and configure the following fields. Save the changes. For external storage: For internal storage: Locate the "app_preinclude.h" file, and set the storage method, as follows: For external storage: #define gEepromType_d       gEepromDevice_AT45DB041E_c For internal storage: #define gEepromType_d        gEepromDevice_InternalFlash_c Locate the "main_text_section.ldt" linker script into the "linkscripts" folder, and delete it from the project.  Search in the project for "OTA_SetNewImageFlag();" and "ResetMCU();" functions in the "otap_client.c" file (source->common->otap_client->otap_client.c) and delete or comment. (For reference, there are 4 in total). Locate the following code in "OtaSupport.h" (framework->OtaSupport->Interface) and delete or comment. extern uint16_t gBootFlagsSectorBitNo;‍‍‍‍‍‍ void OTA_SetNewImageFlag(void);‍‍‍‍‍‍‍ Locate the following code in "OtaSupport.c" (framework->OtaSupport->Source) and delete or comment. extern uint32_t __BootFlags_Start__[]; #define gBootImageFlagsAddress_c ((uint32_t)__BootFlags_Start__)‍‍‍‍‍‍‍‍‍‍‍‍ #if !gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d) /*! Variables used by the Bootloader */ #if defined(__IAR_SYSTEMS_ICC__) #pragma location = "BootloaderFlags" const bootInfo_t gBootFlags = #elif defined(__GNUC__) const bootInfo_t gBootFlags __attribute__ ((section(".BootloaderFlags"))) = #elif defined(__CC_ARM) volatile const bootInfo_t gBootFlags __attribute__ ((section(".BootloaderFlags"))) = #else #error "Compiler unknown!" #endif { {gBootFlagUnprogrammed_c}, {gBootValueForTRUE_c}, {0x00, 0x02}, {gBootFlagUnprogrammed_c}, #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) {PLACEHOLDER_SBKEK}, {BOOT_MAGIC_WORD} #endif }; #endif /* !gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d) */‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ uint16_t gBootFlagsSectorBitNo; gBootFlagsSectorBitNo = gBootImageFlagsAddress_c/(uint32_t)((uint8_t*)FSL_FEATURE_FLASH_PFLASH_BLOCK_SECTOR_SIZE);‍‍‍‍ gBootFlagsSectorBitNo = gBootImageFlagsAddress_c/(uint32_t)((uint8_t*)FSL_FEATURE_FLASH_PAGE_SIZE_BYTES);‍‍‍‍ void OTA_SetNewImageFlag(void) { #if (gEepromType_d != gEepromDevice_None_c) && (!gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d)) /* OTA image successfully written into the non-volatile storage. Set the boot flag to trigger the Bootloader at the next CPU Reset. */ union{ uint32_t value; uint8_t aValue[FSL_FEATURE_FLASH_PFLASH_BLOCK_WRITE_UNIT_SIZE]; }bootFlag; #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) uint8_t defaultSBKEK[SBKEK_SIZE] = {DEFAULT_DEMO_SBKEK}; #endif uint32_t status; if( mNewImageReady ) { NV_Init(); bootFlag.value = gBootValueForTRUE_c; status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.newBootImageAvailable, sizeof(bootFlag), bootFlag.aValue); if( (status == kStatus_FLASH_Success) && FLib_MemCmpToVal(gBootFlags.internalStorageAddr, 0xFF, sizeof(gBootFlags.internalStorageAddr)) ) { bootFlag.value = gEepromParams_StartOffset_c + gBootData_ImageLength_Offset_c; status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.internalStorageAddr, sizeof(bootFlag), bootFlag.aValue); } #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) if( status == kStatus_FLASH_Success ) { /* Write the default SBKEK for secured OTA */ status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.sbkek, SBKEK_SIZE, defaultSBKEK); } #endif if( status == kStatus_FLASH_Success ) { mNewImageReady = FALSE; } } #endif }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   At this point, the FRDM-KW36 can receive and store any image for any MCU and can request a further software update from the OTAP server device.    Adding API's to reprogram the "MCU X" on OTAP client software Once the software update has been downloaded from the OTAP Server into the OTAP Client, the developer should request the software update from the OTAP Client to the "MCU X" through a serial protocol such as UART, SPI, CAN, etc. You should develop the API's and the protocol according to the requirements for your system to send the software update to the "MCU X" (as well as the bootloader for the MCU X). The handling your protocol can be integrated into the OTAP client code replacing "ResetMCU()" (The same code removed in step 4) in the code by "APISendSoftwareUpdateToMCUX()" for instance, since at this point the image was successfully sent over the air and stored in the memory of the KW36. 
查看全文
Introduction The FRDM-KW36 includes an RSIM (Radio System Integration Module) module with an external 32 MHz crystal oscillator. This clock source reference is mainly intended to supply the Bluetooth LE Radio peripheral, but it can be used as the main clock source of the MCU as well. This oscillator includes a set of programmable capacitors to support crystals with different load capacitance needs. Changing the value of these capacitors can modify the frequency the oscillator provides, that way, the central frequency can be tuned to meet the wireless protocol standards. This configurable capacitance range is from C1: 5.7pF - C2: 7.1pF to C1: 22.6pF - C2: 28.2pF and it is configured through the BB_XTAL_TRIM field at the ANA_TRIM. The KW36 comes preprogrammed with a default load capacitance value. However, since there is variance in devices due to tolerances and parasite effects, the correct load capacitance should be checked by verifying that the optimal central frequency is attained.  You will need a spectrum analyzer to measure the central frequency. To find the most accurate value for the load capacitance, it is recommended to use the Connectivity Test demo application. Adjusting Frequency Example Program the KW36 Connectivity Test software on the device. This example can be found in wireless_examples -> genfsk -> conn_test folder from your SDK package. Baremetal and FreeRTOS versions are available. In case that FRDM-KW36 board is being used to perform the test, you should move the 10pF capacitor populated in C55 to C57, to direct the RF signal on the SMA connector. Connect the board to a serial terminal software. When you start the application, you will be greeted by the NXP logo screen:  Press the enter key to start the test. Then press "1" to select "Continuous tests": Finally, select "6" to start a continuous unmodulated RF test. At this point, you should be able to measure the signal in the spectrum analyzer. You can change the RF channel from 0 to 127 ("q" Ch+ and "w" Ch- keys), which represents the bandwidth from 2.360GHz to 2.487GHz, stepping of 1MHz between two consecutive channels. To demonstrate the trimming procedure, this document will make use of channel 42 (2.402GHz) which corresponds to the Bluetooth LE channel 37. In this case, with the default capacitance value, our oscillator is not exactly placed at the center of the 2.402GHz, instead, it is slightly deflected to 2.40200155 GHz, as depicted in the following figure: The capacitance can be adjusted with the "d" XtalTrim+ and "f" XtalTrim- keys. Increasing the capacitance bank means a lower frequency. In our case, we need to increase the capacitance to decrease the frequency. The nearest frequency of 2.402 GHz was 2.40199940 GHz  Once the appropriate XTAL trim value has been found, it can be programmed as default in any Bluetooth LE example, changing the mXtalTrimDefault constant located in the board.c file: static const uint8_t mXtalTrimDefault‍ = 0x36;‍‍‍
查看全文
This document provides the calculation of the Bluetooth Low Power consumption linked to the setting of the Kinetis.   The Power Profile Calculator is build to provide the power consumption of your application. It's a mix between real measurements in voltage and temperature. The process is not taken into account which may create some variation.   DISCLAIMER: This excel workbook is provided as an estimation tool for NXP customers and is based on power profile measurements done on a set of randomly selected parts. A specific part may exhibit deviation from the nominal measurements used on this tool.   This document is the summary of all the information available in the AN12180 Power Consumption Analysis - FRDM-KW36 available in the NXP web page.   Several parameters could be fill-in: Buck or bypass mode (DCDC) Supply Voltage (2.4V to 3.6V) Temperature (-40°C to +105°C) Processor configuration (20MHz, 32MHz or 48MHz) 2 different deep sleep modes (LLS3 or VLLS2) Different Tx output power (0dBm, +3.5dBm or +5dBm) Possibility to set the Advertising interval, connection interval, scan interval and active scan windows duration Fix the Bluetooth Packet sizes in Advertising and Connection  Tx/Rx payload.   One optional information is to provide an idea of the duration life time on typical batteries.
查看全文
Regarding to the "Reprogramming a KW36 device using the OTAP Client Software" and "Reprogramming a KW35 device using the OTAP Client Software" documents, there are some additional steps to debug the OTAP client software in the specific case when you use MCUXpresso together with a P&E micro debug probe. Just before to program the OTAP client project (the second software), the user must do the following: Open the "Debug Configurations" view clicking on the green bug as depicted below. Go to the "Debugger" perspective and search the "Advanced Options" button. Enable the "Preserve this range (Memory Range 0)" checkbox, and edit the textbox "From: 0" To: 1fff" for the KW36 device or "From: 0 To: 3fff" for the KW35 device. After to flash the device, disconnect and connect again. If everything it's OK, the RGB LED must blink (If you are using an FRDM board). Then, test the demo as described in the document.
查看全文
Hi RF High Power Model Kit 2020 Rev2.1 Installation Questions URL: nxp.com/products/rf/rf-high-power-models/models-for-ads-keysight-advanced-design-system:RF_HIGH_POWER_MODELS_KEYSIGHT file name: RF-POWER-ADS2020v2p1-DK.zip I installed it but the library does not contain anything as shown below. Please help with this. Thank you!
查看全文
In addition of the Design Guideline, PCB hardware package find here the design in check list to build sucessfully your own PCB
查看全文
Introduction When a Bluetooth LE Central and Peripheral devices are in connection, data within the payload can be encrypted. Encryption of the channel can be achieved through pairing with others. Once the communication has been encrypted, the Bluetooth LE devices could distribute the keys to save it for future connections. The last is better known as bonding. When two Bluetooth LE devices are bonded, in a future connection, they do not need to exchange the keys since they already know the shared secret, thus, they can encrypt the channel directly, saving time and power. However, if an attacker is listening to the first time that both (Central and Peripheral) Bluetooth LE devices enter into a connection state, the security of the link could be vulnerated, since the attacker could decipher the original message. Fortunately, Out Of Band (OOB) provides the ability (obviously, if both devices support it) to share the keys on an unknown medium for an attacker listening Bluetooth LE (for instance, NFC, SPI, UART, CAN, etc), increasing the security of the communication. This document explains how to enable OOB pairing on Bluetooth LE connectivity examples, basing on FRDM-KW36 SDK HID Host and HID Device examples.   Dedicated Macros and APIs for OOB Pairing The connectivity software stack contains macros and APIs that developers should implement to interact with the host stack and handle the events necessary for OOB. The following sections explain the main macros, variables, and APIs that manage OOB in our software.   Definitions and Variables gAppUsePairing_d It is used to enable or disable pairing to encrypt the link. Values Result 0 Pairing Disabled 1 Pairing Enabled   gAppUseBonding_d It is used to enable or disable bonding to request and save the keys for future connections. Values Result 0 Bonding Disabled 1 Bonding Enabled   gBleLeScOobHasMitmProtection_c This flag must be set if the application requires Man In the Middle protection, in other words, if the link must be authenticated. You can determine whether your software needs to set or clear this flag from the GAP Security Mode and Level. Red instances of the following table indicate that gBleLeScOobHasMitmProtection_c must be set to 1.   gPairingParameters This struct contains the pairing request or the pairing response (depending on the device's GAP role) payload. To enable and configure OOB pairing, oobAvailable field of the struct must be set to 1.   APIs bleResult_t Gap_ProvideOob (deviceId_t deviceId, uint8_t* aOob) This API must be implemented in response of gConnEvtOobRequest_c event in BleConnManager_GapPeripheralEvent or BleConnManager_GapCentralEvent functions (depending of the GAP role). This event only will be triggered if OOB is enabled and LE Legacy pairing is used. The gConnEvtOobRequest_c event occurs when the stack request the OOB data received from the peer device just after the gConnEvtPairingRequest_c or gConnEvtPairingResponse_c (depending of the GAP role). This API is valid only for LE Legacy pairing. Name of the Parameter Input/Output Description deviceId Input ID of the peer device aOob Input Pointer to OOB data previously received from the peer.   bleResult_t Gap_LeScGetLocalOobData (void) This API must be implemented either in response of gConnEvtPairingRequest_c or gConnEvtPairingResponse_c events  in BleConnManager_GapPeripheralEvent or BleConnManager_GapCentralEvent functions (depending of the GAP role) to get the local OOB data generated from the controller and in response of gLeScPublicKeyRegenerated_c event at BleConnManager_GenericEvent. Each time that Gap_LeScGetLocalOobData is executed in the application to obtain the OOB data, it triggers the gLeScLocalOobData_c generic event to inform that OOB data must be read from pGenericEvent->eventData.localOobData to send it to the peer device. This API is valid only for LE Secure Connections pairing.   bleResult_t Gap_LeScSetPeerOobData (deviceId_t deviceId, gapLeScOobData_t* pPeerOobData) This API must be implemented in response of gConnEvtLeScOobDataRequest_c event in BleConnManager_GapPeripheralEvent or BleConnManager_GapCentralEvent functions(depending of the GAP role). This event occurs when the stack requires the OOB data previously recieved from the peer. This API is valid only for LE Secure Connections pairing. Name of the Parameter Input/Output Description deviceId Input ID of the peer device aOob Input Pointer to gapLeScOobData_t struct that contains the OOB data received from the peer.   Enabling OOB on KW36 Bluetooth LE Peripheral Device The following example is based on the HID Device software included in the FRDM-KW36 SDK. It explains the minimum code needed to enable OOB. In the following sections, brown color indicates that such definition or API takes part in the stack and violet color indicates that such definition does not take part in the stack and its use is only for explanation purposes in this document.   Changes in app_preinclude.h file The app_preinclude.h header file contains definitions for the management of the application. To enable OOB pairing, you must ensure that gAppUseBonding_d and gAppUsePairing_d are set to 1. You can also set the value of the gBleLeScOobHasMitmProtection_c in this file, depending on the security mode and level needed in your application.  This example makes use of two custom definitions: gAppUseOob_d and gAppUseSecureConnections_d. Such definitions are used to explain how to enable/disable OOB and, if OOB is enabled, how to switch between LE Secure Connections pairing or LE Legacy paring.   /*! Enable/disable use of bonding capability */ #define gAppUseBonding_d 1 /*! Enable/disable use of pairing procedure */ #define gAppUsePairing_d 1 /*! Enable/disable use of privacy */ #define gAppUsePrivacy_d 0 #define gPasskeyValue_c 999999 /*! Enable/disable use of OOB pairing */ #define gAppUseOob_d 1 /*! Enable MITM protection when using OOB pairing */ #if (gAppUseOob_d) #define gBleLeScOobHasMitmProtection_c TRUE #endif /*! Enable/disable Secure Connections */ #define gAppUseSecureConnections_d 1‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Using the code above, you can enable or disable OOB using gAppUseOob_d, also you can decide whether to use LE Secure Connections (gAppUseSecureConnections_d = 1) or LE Legacy (gAppUseSecureConnections_d = 0)     Changes in app_config.c file The following portion fo code depicts how to fill gPairingParameters struct depending on which pairing method is used by the application.   /* SMP Data */ gapPairingParameters_t gPairingParameters = { .withBonding = (bool_t)gAppUseBonding_d, /* If Secure Connections pairing is supported, then set Security Mode 1 Level 4 */ /* If Legacy pairing is supported, then set Security Mode 1 Level 3 */ #if (gAppUseSecureConnections_d) .securityModeAndLevel = gSecurityMode_1_Level_4_c, #else .securityModeAndLevel = gSecurityMode_1_Level_3_c, #endif .maxEncryptionKeySize = mcEncryptionKeySize_c, .localIoCapabilities = gIoKeyboardDisplay_c, /* OOB Available enabled when app_preinclude.h file gAppUseOob_d macro is true */ .oobAvailable = (bool_t)gAppUseOob_d, #if (gAppUseSecureConnections_d) .centralKeys = (gapSmpKeyFlags_t) (gIrk_c), .peripheralKeys = (gapSmpKeyFlags_t) (gIrk_c), #else .centralKeys = (gapSmpKeyFlags_t) (gLtk_c | gIrk_c), .peripheralKeys = (gapSmpKeyFlags_t) (gLtk_c | gIrk_c), #endif /* Secure Connections enabled when app_preinclude.h file gAppUseSecureConnections_d macro is true */ .leSecureConnectionSupported = (bool_t)gAppUseSecureConnections_d, .useKeypressNotifications = FALSE, };‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Additionally, the serviceSecurity struct registers which are the security mode and level of each Bluetooth LE service, so if Secure Connections is selected (gAppUseSecureConnections_d = 1), mode = 1 level = 4.   static const gapServiceSecurityRequirements_t serviceSecurity[3] = { { .requirements = { #if (gAppUseSecureConnections_d) .securityModeLevel = gSecurityMode_1_Level_4_c, #else .securityModeLevel = gSecurityMode_1_Level_3_c, #endif .authorization = FALSE, .minimumEncryptionKeySize = gDefaultEncryptionKeySize_d }, .serviceHandle = (uint16_t)service_hid }, { .requirements = { #if (gAppUseSecureConnections_d) .securityModeLevel = gSecurityMode_1_Level_4_c, #else .securityModeLevel = gSecurityMode_1_Level_3_c, #endif .authorization = FALSE, .minimumEncryptionKeySize = gDefaultEncryptionKeySize_d }, .serviceHandle = (uint16_t)service_battery }, { .requirements = { #if (gAppUseSecureConnections_d) .securityModeLevel = gSecurityMode_1_Level_4_c, #else .securityModeLevel = gSecurityMode_1_Level_3_c, #endif .authorization = FALSE, .minimumEncryptionKeySize = gDefaultEncryptionKeySize_d }, .serviceHandle = (uint16_t)service_device_info } };‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     Changes in ble_conn_manager.c file LE Legacy Pairing If your application will use LE Legacy Pairing, then you have to implement Gap_ProvideOob in response to the gConnEvtOobRequest_c event at the BleConnManager_GapPeripheralEvent function. In this example, gOobReceivedTKDataFromPeer is an array that stores the data previously received OOB from the peer device (using SPI, UART, I2C, etc), therefore, the procedure to fill this array with the data received from the peer depends entirely on your application. Notice that gOobReceivedTKDataFromPeer must contain the data received from the peer before to execute Gap_ProvideOob.   static uint8_t gOobReceivedTKDataFromPeer[16]; void BleConnManager_GapPeripheralEvent(deviceId_t peerDeviceId, gapConnectionEvent_t* pConnectionEvent) { switch (pConnectionEvent->eventType) { case gConnEvtConnected_c: { ... ... ... } break; ... ... ... #if (gAppUseOob_d && !gAppUseSecureConnections_d) case gConnEvtOobRequest_c: { /* The stack has requested the LE Legacy OOB data*/ (void)Gap_ProvideOob(peerDeviceId, &gOobReceivedTKDataFromPeer[0]); } break; #endif ... ... ... } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     LE Secure Connections Pairing When using Secure Connections Pairing, the application must handle two events at the BleConnManager_GapPeripheralEvent function. In gConnEvtPairingRequest_c event, you must implement Gap_LeScGetLocalOobData API to generate the local (r, Cr) values. The gConnEvtLeScOobDataRequest_c event indicates that the application is requesting the (r, Cr) values previously received OOB from the peer device (using SPI, UART, I2C, etc). Such values are contained into gOobReceivedRandomValueFromPeer and gOobReceivedConfirmValueFromPeer buffers. You must implement Gap_LeScSetPeerOobData in response to gConnEvtLeScOobDataRequest_c, This function has two parameters, the device ID of the peer and a pointer to a gapLeScOobData_t type struct. This struct is filled with the data contained in gOobReceivedRandomValueFromPeer and gOobReceivedConfirmValueFromPeer buffers.   gapLeScOobData_t gPeerOobData; static uint8_t gOobReceivedRandomValueFromPeer[gSmpLeScRandomValueSize_c]; /*!< LE SC OOB r (Random value) */ static uint8_t gOobReceivedConfirmValueFromPeer[gSmpLeScRandomConfirmValueSize_c]; /*!< LE SC OOB Cr (Random Confirm value) */ void BleConnManager_GapPeripheralEvent(deviceId_t peerDeviceId, gapConnectionEvent_t* pConnectionEvent) { switch (pConnectionEvent->eventType) { case gConnEvtConnected_c: { ... ... ... } break; case gConnEvtPairingRequest_c: { #if (defined(gAppUsePairing_d) && (gAppUsePairing_d == 1U)) gPairingParameters.centralKeys = pConnectionEvent->eventData.pairingEvent.centralKeys; (void)Gap_AcceptPairingRequest(peerDeviceId, &gPairingParameters); #if (gAppUseOob_d && gAppUseSecureConnections_d) /* The central has requested pairing, get local LE Secure Connections OOB data */ (void)Gap_LeScGetLocalOobData(); #endif #else (void)Gap_RejectPairing(peerDeviceId, gPairingNotSupported_c); #endif } break; ... ... ... #if (gAppUseOob_d && gAppUseSecureConnections_d) case gConnEvtLeScOobDataRequest_c: { /* The stack has requested the peer LE Secure Connections OOB data. Fill the gPeerOobData struct and provide it to the stack */ FLib_MemCpy(gPeerOobData.randomValue, &gOobReceivedRandomValueFromPeer[0], gSmpLeScRandomValueSize_c); FLib_MemCpy(gPeerOobData.confirmValue, &gOobReceivedConfirmValueFromPeer[0], gSmpLeScRandomConfirmValueSize_c); Gap_LeScSetPeerOobData(peerDeviceId, &gPeerOobData); } break; #endif ... ... ... } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   The gLeScPublicKeyRegenerated_c event in the BleConnManager_GenericEvent function must be handled using the Gap_LeScGetLocalOobData API as depicted below. Each time that Gap_LeScGetLocalOobData is executed by the software, it generates, asynchronously, the gLeScLocalOobData_c event (also handled in the BleConnManager_GenericEvent function) indicating that the local (r, Cr) values were successfully generated and you can read them using the pGenericEvent->eventData.localOobData pointer to send it OOB to the peer device. In this example, Oob_SendLocalRandomValueToPeer and Oob_SendLocalConfirmValueToPeer  are custom synchronous functions that demonstrate how you can implement a custom API that sends the local (r, Cr) read from pGenericEvent->eventData.localOobData pointer to the peer device using other protocols (SPI, UART, I2C, etc).   void BleConnManager_GenericEvent(gapGenericEvent_t* pGenericEvent) { switch (pGenericEvent->eventType) { case gInitializationComplete_c: { ... ... ... } break; ... ... ... #if (defined(gAppUsePairing_d) && (gAppUsePairing_d == 1U)) case gLeScPublicKeyRegenerated_c: { /* Key pair regenerated -> reset pairing counters */ mFailedPairings = mSuccessfulPairings = 0; /* Local Secure Connections OOB data must be refreshed whenever this event occurs */ #if (gAppUseOob_d && gAppUseSecureConnections_d) (void)Gap_LeScGetLocalOobData(); #endif } break; #endif ... ... ... #if (gAppUseOob_d && gAppUseSecureConnections_d) case gLeScLocalOobData_c: { /* Get the local Secure Connections OOB data and send to the peer */ Oob_SendLocalRandomValueToPeer((uint8_t*)pGenericEvent->eventData.localOobData.randomValue); Oob_SendLocalConfirmValueToPeer((uint8_t*)pGenericEvent->eventData.localOobData.confirmValue); } break; #endif ... ... ... } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     Enabling OOB on KW36 Bluetooth LE Central Device The following example is based on the HID Host software included in the FRDM-KW36 SDK. It explains the minimum code needed to enable OOB. In the following sections, brown color indicates that such definition or API takes part in the stack and violet color indicates that such definition does not take part in the stack and its use is only for explanation purposes in this document.   Changes in app_preinclude.h file The app_preinclude.h header file contains definitions for the management of the application. To enable OOB pairing, you must ensure that gAppUseBonding_d and gAppUsePairing_d are set to 1. You can also set the value of the gBleLeScOobHasMitmProtection_c in this file, depending on the security mode and level needed in your application.  This example makes use of two custom definitions: gAppUseOob_d and gAppUseSecureConnections_d. Such definitions are used to explain how to enable/disable OOB and, if OOB is enabled, how to switch between LE Secure Connections pairing or LE Legacy paring.   /*! Enable/disable use of bonding capability */ #define gAppUseBonding_d 1 /*! Enable/disable use of pairing procedure */ #define gAppUsePairing_d 1 /*! Enable/disable use of privacy */ #define gAppUsePrivacy_d 0 #define gPasskeyValue_c 999999 /*! Enable/disable use of OOB pairing */ #define gAppUseOob_d 1 /*! Enable MITM protection when using OOB pairing */ #if (gAppUseOob_d) #define gBleLeScOobHasMitmProtection_c TRUE #endif /*! Enable/disable Secure Connections */ #define gAppUseSecureConnections_d 1‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Using the code above, you can enable or disable OOB using gAppUseOob_d, also you can decide whether to use LE Secure Connections (gAppUseSecureConnections_d = 1) or LE Legacy (gAppUseSecureConnections_d = 0)     Changes in app_config.c file The following portion fo code depicts how to fill gPairingParameters struct depending on which pairing method is used by the application.   /* SMP Data */ gapPairingParameters_t gPairingParameters = { .withBonding = (bool_t)gAppUseBonding_d, /* If Secure Connections pairing is supported, then set Security Mode 1 Level 4 */ /* If Legacy pairing is supported, then set Security Mode 1 Level 3 */ #if (gAppUseSecureConnections_d) .securityModeAndLevel = gSecurityMode_1_Level_4_c, #else .securityModeAndLevel = gSecurityMode_1_Level_3_c, #endif .maxEncryptionKeySize = mcEncryptionKeySize_c, .localIoCapabilities = gIoKeyboardDisplay_c, /* OOB Available enabled when app_preinclude.h file gAppUseOob_d macro is true */ .oobAvailable = (bool_t)gAppUseOob_d, #if (gAppUseSecureConnections_d) .centralKeys = (gapSmpKeyFlags_t) (gIrk_c), .peripheralKeys = (gapSmpKeyFlags_t) (gIrk_c), #else .centralKeys = (gapSmpKeyFlags_t) (gLtk_c | gIrk_c), .peripheralKeys = (gapSmpKeyFlags_t) (gLtk_c | gIrk_c), #endif /* Secure Connections enabled when app_preinclude.h file gAppUseSecureConnections_d macro is true */ .leSecureConnectionSupported = (bool_t)gAppUseSecureConnections_d, .useKeypressNotifications = FALSE, };‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     Changes in ble_conn_manager.c file LE Legacy Pairing If your application will use LE Legacy Pairing, then you have to implement Gap_ProvideOob in response to the gConnEvtOobRequest_c event at the BleConnManager_GapCentralEvent function. In this example, gOobOwnTKData is an array that stores the TK data which will be sent OOB to the peer device (using SPI, UART, I2C, etc)  and, at the same time, is the TK data that will be provided to the stack using Gap_ProvideOob. This data must be common on both Central and Peripheral devices, so the procedure to share the TK depends entirely on your application. Oob_SendLocalTKValueToPeer is a custom synchronous function that demonstrates how you can implement a custom API that sends the local TK to the peer device using other protocols (SPI, UART, I2C, etc).   static uint8_t gOobOwnTKData[16] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F}; void BleConnManager_GapCentralEvent(deviceId_t peerDeviceId, gapConnectionEvent_t* pConnectionEvent) { switch (pConnectionEvent->eventType) { case gConnEvtConnected_c: { ... ... ... } break; ... ... ... case gConnEvtPairingResponse_c: { /* Send Legacy OOB data to the peer */ #if (gAppUseOob_d & !gAppUseSecureConnections_d) Oob_SendLocalTKValueToPeer(&gOobOwnTKData[0]); #endif } break; ... ... ... #if (gAppUseOob_d && !gAppUseSecureConnections_d) case gConnEvtOobRequest_c: { /* The stack has requested the LE Legacy OOB data*/ (void)Gap_ProvideOob(peerDeviceId, &gOobOwnTKData[0]); } break; #endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ ... ... ... } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     LE Secure Connections Pairing When using Secure Connections Pairing, the application must handle two events at the BleConnManager_GapCentralEvent function. In gConnEvtPairingResponse_c event, you must implement Gap_LeScGetLocalOobData API to generate the local (r, Cr) values. The gConnEvtLeScOobDataRequest_c event indicates that the application is requesting the (r, Cr) values previously received OOB from the peer device (using SPI, UART, I2C, etc). Such values are contained into gOobReceivedRandomValueFromPeer and gOobReceivedConfirmValueFromPeer buffers. You must implement Gap_LeScSetPeerOobData in response to gConnEvtLeScOobDataRequest_c, This function has two parameters, the device ID of the peer and a pointer to a gapLeScOobData_t type struct. This struct is filled with the data contained in gOobReceivedRandomValueFromPeer and gOobReceivedConfirmValueFromPeer buffers.   gapLeScOobData_t gPeerOobData; static uint8_t gOobReceivedRandomValueFromPeer[gSmpLeScRandomValueSize_c]; /*!< LE SC OOB r (Random value) */ static uint8_t gOobReceivedConfirmValueFromPeer[gSmpLeScRandomConfirmValueSize_c]; /*!< LE SC OOB Cr (Random Confirm value) */ void BleConnManager_GapCentralEvent(deviceId_t peerDeviceId, gapConnectionEvent_t* pConnectionEvent) { switch (pConnectionEvent->eventType) { case gConnEvtConnected_c: { ... ... ... } break; ... ... ... case gConnEvtPairingResponse_c: { /* The peripheral has acepted pairing, get local LE Secure Connections OOB data */ #if (gAppUseOob_d && gAppUseSecureConnections_d) (void)Gap_LeScGetLocalOobData(); #endif } break; ... ... ... #if (gAppUseOob_d && gAppUseSecureConnections_d) case gConnEvtLeScOobDataRequest_c: { /* The stack has requested the peer LE Secure Connections OOB data. Fill the gPeerOobData struct and provide it to the stack */ FLib_MemCpy(gPeerOobData.randomValue, &gOobReceivedRandomValueFromPeer[0], gSmpLeScRandomValueSize_c); FLib_MemCpy(gPeerOobData.confirmValue, &gOobReceivedConfirmValueFromPeer[0], gSmpLeScRandomConfirmValueSize_c); Gap_LeScSetPeerOobData(peerDeviceId, &gPeerOobData); } break; #endif ... ... ... } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   The gLeScPublicKeyRegenerated_c event in the BleConnManager_GenericEvent function must be handled using the Gap_LeScGetLocalOobData API as depicted below. Each time that Gap_LeScGetLocalOobData is executed by the software, it generates, asynchronously, the gLeScLocalOobData_c event (also handled in the BleConnManager_GenericEvent function) indicating that the local (r, Cr) values were successfully generated and you can read them using the pGenericEvent->eventData.localOobData pointer to send it OOB to the peer device. In this example, Oob_SendLocalRandomValueToPeer and Oob_SendLocalConfirmValueToPeer  are custom synchronous functions that demonstrate how you can implement a custom API that sends the local (r, Cr) read from pGenericEvent->eventData.localOobData pointer to the peer device using other protocols (SPI, UART, I2C, etc).   void BleConnManager_GenericEvent(gapGenericEvent_t* pGenericEvent) { switch (pGenericEvent->eventType) { case gInitializationComplete_c: { ... ... ... } break; ... ... ... #if (defined(gAppUsePairing_d) && (gAppUsePairing_d == 1U)) case gLeScPublicKeyRegenerated_c: { /* Key pair regenerated -> reset pairing counters */ mFailedPairings = mSuccessfulPairings = 0; /* Local LE Secure Connections OOB data must be refreshed whenever this event occurs */ #if (gAppUseOob_d && gAppUseSecureConnections_d) (void)Gap_LeScGetLocalOobData(); #endif } break; #endif ... ... ... #if (gAppUseOob_d && gAppUseSecureConnections_d) case gLeScLocalOobData_c: { /* Get the local LE Secure Connections OOB data and send to the peer */ Oob_SendLocalRandomValueToPeer((uint8_t*)pGenericEvent->eventData.localOobData.randomValue); Oob_SendLocalConfirmValueToPeer((uint8_t*)pGenericEvent->eventData.localOobData.confirmValue); } break; #endif ... ... ... } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     Simplified Flow Diagram of OOB Central and Peripheral Events LE Legacy Pairing The following figure shows a simplified flow diagram of the LE Legacy OOB pairing example in this document. The LE Central device is the one that contains the OOB TK data that will be shared OOB using the custom Oob_SendLocalTKValueToPeer function. It must be implemented at the gConnEvtPairingResponse_c event to ensure that both devices know the OOB TK before to execute Gap_ProvideOob since this function requests this data. If the OOB data is correct on both sides, the pairing procedure ends, and it is noticed through gConnEvtPairingComplete_c. LE Secure Connections Pairing The following figure shows a simplified flow diagram of the LE Secure Connections OOB pairing example in this document. After both devices enter in connection, the data that will be shared OOB using the custom Oob_SendLocalRandomValueToPeer and Oob_SendLocalConfirmValueToPeer  functions is yielded by Gap_LeScGetLocalOobData on both sides. The last one must be implemented at gConnEvtPairingResponse_c and gConnEvtPairingRequest_c events to ensure that both devices know the Peripheral and Central (r, Cr) OOB data before to execute Gap_LeScSetPeerOobData since this function requests this data. If the OOB data is correct on both sides, the pairing procedure ends, and it is noticed through gConnEvtPairingComplete_c. This is how OOB pairing can be implemented in your project. I hope this document will be useful to you. Please, let us know any questions or comments. 
查看全文
This patch fixes some minor issues with the Connectivity Software v1.0.2 when working with the Kinetis BLE Toolbox application for smartphones. Following issues are fixed. BLE OTAP Application: Fixes application failing to download the new image when the previous image upload has been interrupted due a disconnection. BLE Wireless UART: Fixes MTU exchange issue causing some characters not bein shown in the smartphone application in iOS and Android. Hybrid BLE + Thread console: Fixes MTU exchange issue causing some characters not bein shown in the smartphone application console in iOS and Android. Make sure the Connectivity Software version 1.0.2 is installed in your computer before proceeding to install this application.
查看全文
This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prototyping and demonstration of the KW39A/38A/37A/39Z/38Z family of devices. The KW38 is an ultra-low-power, highly integrated single-chip device that enables Bluetooth Low Energy (Bluetooth LE) or Generic FSK (at 250, 500 and 1000 kbps) for portable, extremely low-power embedded systems. The KW38 integrates a radio transceiver operating in the 2.36 GHz to 2.48 GHz range supporting a range of GFSK, an ARM Cortex-M0+ CPU, up to 512 KB Flash and up to 64 KB SRAM, Bluetooth LE Link Layer hardware and peripherals optimized to meet the requirements of the target applications. MKW38 device is also available on the FRDM-KW38 Freedom Development Board. For more information about the FRDM-KW38 Freedom Development Board, see the FRDM-KW38 Freedom Development Board User's Guide (document FRDMKW38ZUG available in the NXP Connectivity website also).
查看全文
As know, FSK and OOK are the modulation types that can be configured in the radio by setting the bits 4-3 from the RegDataModul register, as shown in below picture taken from Reference Manual:                                                          A common inquire you could have is: what modulation should I use? Let's first understand how these modulations work. FSK: Frequency Shift Keying is a modulation type that uses two frequencies, for 0 and 1. In a spectrum analyzer we can see a spectrum similar to the next picture, where the frequency for 0's is separated from the central frequency with FDev, and same case for the frequency for the 1's: OOK: On Off Keying is a modulation type that represents a logic 1 with the presence of the carrier frequency and a logic 0 with the absence of it. In a spectrum analyzer we can see a spectrum similar to the next picture, where the central frequency represents a logic 1. We can not see a logic 0 in the spectrum due to it's represented as the absence of power. Then what modulation should I use? FSK is most commonly used because is more spectral efficient so has better sensitivity. In the other hand, OOK modulation is commonly used in applications where the frequency accuracy can not be guaranteed. It also helps in conserving battery power due to the power absence for the logic 0's. Regards, Luis Burgos.
查看全文
This document describes the implementation of the Connected Home Gateway for the Internet of Things (IoT) and its controller implemented in a Smart device (tablet) running Android OS. The gateway is intended to serve as a communication bridge between WiFi/Ethernet and ZigBee Protocol, making every ZigBee-enabled device accessible and controllable from any smart device with Wi-Fi capabilities such as a smart phone or tablet. This will remove the need of having a ZigBee transceiver in every mobile device attempting to control the house appliances. In general, users will be able to: Remote control of Home Appliances using ZigBee protocol Any WiFi-enabled device could control the appliances without a ZigBee transceiver Achieve bi-directional communication between users and appliances Real system implementation would require a powerful MCU to manage all WiFi/Ethernet communication and a second MCU to manage all ZigBee communications. The Kinetis K60 and KW24 were selected among the different options available.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340508
查看全文
This patch fix the issue in hdmi dongle JB4.2.2_1.1.0-GA release that wifi((STA+P2P)/AP) cann't be enabled properly. In the root directory of Android Source Code, use the following command to apply the patch: $ git apply hdmi_dongle_wifi_jb4.2.2_1.1.0.patch
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-332703
查看全文