S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
1 Abstract After learning S32K3 PWM and have written some MCAL codes, this is the first MCAL article record starts with the combination of K344 EMIOS+ICU+TRIMUX+LCU, which can involve comprehensive configurations such as PORT, DIO, EMIOS, interrupt ICU, TRIGMUX, LCU, etc. The board platform is still based on NXP official S32K344EVB, RTD400, and the function is: use two channels of EMIOS0 and one channel of EMIOS1. After one channel of EMIOS 0 outputs PWM, it connects LCU through TRIGUMX to generate a set of complementary PWM, and the other channel can realize hardware interrupt control of PWM duty cycle through SW5 PT26 button. One channel of EMIOS1 is directly connected to the PTA29 onboard red light, and the brightness is gradually changed by changing the PWM duty cycle, and then the breathing light effect is realized by directly changing the on and off cycle. At the same time, when the PWM turns off the red light, the onboard green light is turned on through DIO, and when the PWM turns on the red light, the DIO turns off the onboard green light. Text description is always less intuitive than graphic description, so here is the picture:      Fig 1 2. Function realization This article is based on porting the MCAL code to the S32DS demo. Then, on the S32DS platform, MCAL related modules are configured through EB, and then compiled and downloaded for simulation through S32DS. Of course, if you like the command line mode, you can directly use the xmd file configured by EB, and then compile with VScode. The process is also very simple. This article will not go into details about the command line method.     2.1 Hardware and software platform Board:S32K344EVB,also can use other K3 boards. IDE:S32DS3.5 RTD: K344 RTD 400 MCAL tool: EBtresos Studio 29.0 2.2 Software control process Before talking about the specific MCAL configuration, here is the software flow chart of the functions in this article:                                                                             Fig 2 Here you can see that the default situation is the one configured through MCAL, and then the PWM frequency is also modified in the code, and the PWM duty cycle is modified by keystrokes and loop delays. 2.3 Resource Allocation Overview The hardware resources and functions used in this article are listed as follows: Fig 3 The configuration of emios related buses is as follows: Fig 4 It should be noted here that for the master bus and bus mode in MCL emios, it is necessary to select the appropriate PWM mode and counter bus in the PWM module, otherwise either the configuration will be wrong or the correct PWM waveform cannot be generated. From the official S32K3 RM, you can check the clock channel and bus type: Fig 5 For example, if EMIOS_CH23 is selected in PWM0, then this bus corresponds to bus A, and this clock can be used for all channels, so PWM0 is CH12 and can use Bus A. CH22 corresponds to bus F, and this clock can also be used for all channels, so it is no problem to select Bus F for PWM1 CH4. CH0 corresponds to bus B, and this clock corresponds to channels 0-7, so it can also be used for PWM2 is CH2. When selecting the counter bus clock source for your EMIOS channel, you must consider the channel coverage of the counter bus. In addition to the selection of the counter bus, there is also the PWM mode selection, which is easier to handle. For clock counting up, select OPWMB, and for clock counting up and down, select OPWMCB center-aligned PWM.      In actual use, the mode selection is usually determined based on one's own PWM requirements, and then based on the following RM table: Fig 6 You can find the channel types that the corresponding mode can support, and then select the corresponding channel, counter bus, etc. according to the channel type in Figure 5. With these basic knowledge, we can directly enter the EB configuration. 2.4 EB configuration    Here we list all the modules used in EB tresos related to this article, and focus on the modules that require specific configuration. Fig 7 2.4.1 Dio module The DioPort interface needs to be configured. The main purpose is to configure PTA30, onboard green light, select DioPort Id=1, Dio Channel Id=14. The rules for DioPortId and Dio Channel Id are as follows:     Channel = DioChannelId + DioPortId∗16 For S32K3X4 derivatives – Port AL=0 – Port AH=1 – Port BL=2 – Port BH=3 – Port CL=4 – Port CH=5 – Port DL=6 – Port DH=7 – Port EL=8 – Port EH=9 – Port FL=10 – Port FH=11 – Port GL=12 – Port GH=13 PTA30=>30=DioChannelId(14)+DioPortId*16 2.4.2 Icu module First, configure IcuSiul2, the goal is to enable the input interrupt of onboard SW5, PTB26. PTB26 corresponds to EIRQ[13], Then, the corresponding interrupt situation is as follows: Fig 8 Fig 9 (1) Icu->IcuSiul2->IcuSiul2Channels:13 (2) Icu->IcuChannel configuration is: Fig 10 Select IcuChannelRef as the previously configured IcuSiul2Channels, and add the interrupt notification function: User_EdgeDetect, note that this function is the name of the user interrupt processing function that needs to be added in the code.    (3)Icu->IcuHwInterruptConfigList-> ICU Peripheral ISR Name: SIUL2_0_IRQ_CH_13,IcuIsrEnable enable 2.4.3 Mcl module This module is mainly used to configure emios counting clock, trgmux, and LCU configuration. (1)Mcl->Trgmux Logic Instance->Hardware Instance: TRGMUX_IP_HW_INST_0   (2) Mcl->Trgmux Logic Group: Fig 11 The main purpose is to connect PWM1 Emios0_ch4 to LCU0_IN0 through Trigmux. (3)Mcl->LCU Configuration Here is the configuration of the LCU module. The main function is to configure the logic input and logic output. There is one input IN0 and two outputs OUT0 and OUT1. Fig 12 Fig 13 Fig 14 OUTPUT0  value is 0XAAAA=43690, OUTPUT1 value is 0X5555=21845 The purpose of this is to generate a pair of complementary PWMs from the input PWM. Fig 15 (4)Mcl->Emios Common Add two Emios, EMIOS_0 and EMIOS_1, which means two EMIOS are used. EMIOS0 is configured with two master bus channels: CH_22 and CH_0, and has different mode types, counting up and down and counting up. EMIOS1 is configured with one master bus channel: CH_23, counting up Corresponding to Figure 4. Fig 16 Fig 17 Note that the channel here is not the actual PWM output channel, but the counter bus channel of the PWM channel, which has the ability to provide clocks. 2.4.4 Mcu module   This module is the basis for the entire MCU to configure the clock. When using the default setting of the original RTD PWM demo, there is only one point that needs attention Mcu->McuClockSettingConfig_0->McuClockReferencePoint->McuClockReferencePoint_0->core clock 48MHZ. This clock is the source of the EMIOS clock. With the clock source, it is not difficult to calculate the actual PWM frequency according to the set period. For example, if a 1Khz PWM is required, you can configure period=48M/1K=48000 2.4.5 Platform module Platform->Interrupt Controller->IntCtrlConfig0, enable SIUL_1_IRQn, and add Handler as: SIUL2_EXT_IRQ_8_15_ISR Note that this SIUL2_EXT_IRQ_8_15_ISR is not written randomly, but must correspond to the one in Siul2_Icu_Ip_Irq.c, otherwise an error will be reported. Fig18 Different interrupts have different interrupt service functions. You need to find the function name defined in the code and fill it into EB. EB configuration is as follows: Fig 19 2.4.6 Port module The configuration of 8 pins is as follows: Fig 20 As you can see, there are 3 main EMIOS PWMs, one input interrupt, one output GPIO, and two output LCU complementary PWMs. 2.4.7 Pwm module Mcl configures the counter clock channel of EMIOS. The PWM channels to be output need to be configured in the Pwm module and linked to the MCU clock source and the emios counter bus source in Mcl. (1) Pwm->PwmEmios Add two groups for the corresponding EMIOS modules. For example, this article uses EMIOS0 and EMIOS1, so two need to be added: Fig 21 For PwmEmios_1, there is one channel, and the configuration is as follows: Fig 22 PwmEmiosBusRef: /Mcl/Mcl/MclConfig/EmiosCommon_1/EmiosMclMasterBus_0 Fig 23 As you can see, the busRef of PwmEmios_1 here is Emios_ch_23 in Mcl, that is, BusA. That is to say, the bus reference clock used by EMIOS1_CH12 comes from EMIOS1_CH23, that is, Bus A. There are two channels configured in PwmEmios_0, and the configuration is as follows: Fig 24 Fig 25 The bus reference clock used by EMIOS0_CH4 comes from EMIOS0_CH22, which is Bus F. Another EMIOS0 channel: Fig 26 Fig 27 The bus reference clock used by EMIOS0_CH2 comes from EMIOS0_CH0, that is, Bus B, so select Bus BCDE. At this point, we can clearly understand the relationship between the real PWM output channel and the internal MCL Emios counter bus channel. (2)Pwm->PwmEmios With the specific information of PWM configured above, we can directly configure the PWM channels. There are three channels in total: PWM0, PWM1, PWM2, which are also the flags needed in the code. Fig 28 2.5 main code   #include "Pwm.h" #include "Mcu.h" #include "Port.h" #include "Mcl.h" #include "Platform.h" #include "Dio.h" #include "Icu.h" //#include "check_example.h" #define NUM_BLINK_LED (uint32)10U #define DELAY_TIMER (uint32)5000000U #define MCL_EMIOS_1_CH_23 (uint16)279U #define MCL_EMIOS_0_CH_22 (uint16)22U Mcl_LcuSyncOutputValueType PWM_OutputList[2]; volatile uint8 UserCountIrqCH0; void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer<delay) { DelayTimer++; } DelayTimer=0; } void User_EdgeDetect(void) { /* increment IRQ counter */ UserCountIrqCH0++; if(UserCountIrqCH0 % 2 == 0) { Pwm_SetDutyCycle(PwmChannel_2, 0X6000); } else { Pwm_SetDutyCycle(PwmChannel_2, 0X2000); } } int main(void) { uint8 num_blink = 0U, i = 0; uint16 duty_cnt = 0; UserCountIrqCH0 = 0U; /* Initialize the Mcu driver */ Mcu_Init(&Mcu_Config_VS_0); /* Initialize the clock tree */ Mcu_InitClock(McuClockSettingConfig_0); /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); Platform_Init(NULL_PTR); /* Initialize all pins using the Port driver */ Port_Init(&Port_Config_VS_0); /* Initialize Mcl driver */ Mcl_Init(&Mcl_Config_VS_0); /* Initialize the Icu driver */ Icu_Init(NULL_PTR); Icu_EnableEdgeDetection(IcuChannel_0); Icu_EnableNotification(IcuChannel_0); /* Initialize Pwm driver , after that Led on*/ Pwm_Init(&Pwm_Config_VS_0); /* PTA29 duty cycle is 50% */ Pwm_SetDutyCycle(PwmChannel_0, 0X4000); // PTB16,pwm1 , emios0_ch4, use trigmux LCU output 2 Complementarity PWM Mcl_LcuSyncOutputValueType lcuEnable[2U]; lcuEnable[0].LogicOutputId = 0; lcuEnable[0].Value = 1U; lcuEnable[1].LogicOutputId = 1; lcuEnable[1].Value = 1U; Mcl_SetLcuSyncOutputEnable(lcuEnable, 2U); TestDelay(DELAY_TIMER); /* Set new period for all channels used external counter bus */ Mcl_Emios_SetCounterBusPeriod(MCL_EMIOS_1_CH_23, 4800, FALSE); // pwmchannel_0 10Khz Mcl_Emios_SetCounterBusPeriod(MCL_EMIOS_0_CH_22, 1200, FALSE);// for PwmChannel_1, 20Khz // PWM0: 10kHZ //PWM1: 20KHZ //PWM2:1KHZ // PTA29 10kHZ /* PTA29 duty cycle is 50% */ Pwm_SetDutyCycle(PwmChannel_0, 0X4000); /* Setup new duty cycle to the pin*/ Pwm_SetDutyCycle(PwmChannel_1, 0x4000); for(i=0; i <= 10; i++) { duty_cnt = i * 0x800; Pwm_SetDutyCycle(PwmChannel_0, duty_cnt); TestDelay(DELAY_TIMER); } /* Using duty cycle 0% and 100% to Blink LED */ while(1) { /* pwm1 when duty cycle is 75% */ Pwm_SetDutyCycle(PwmChannel_1, 0X6000); //Led off Pwm_SetDutyCycle(PwmChannel_0, 0X0000); //red off Dio_WriteChannel(DioConf_DioChannel_Digital_ledgreenPTA30, STD_HIGH); //green on TestDelay(DELAY_TIMER); /* pwm 1 when duty cycle is 25% */ Pwm_SetDutyCycle(PwmChannel_1, 0X2000); //Led ON Dio_WriteChannel(DioConf_DioChannel_Digital_ledgreenPTA30, STD_LOW); //Green OFF Pwm_SetDutyCycle(PwmChannel_0, 0X8000); //RED ON TestDelay(DELAY_TIMER); num_blink++; } /* De-Initialize Pwm driver */ Pwm_DeInit(); //Exit_Example(TRUE); return 0U; }   3. Test Result After power-on, the onboard red light flashes, then gradually turns bright from off, and flashes alternately with the green light. Test PWM1 PTB16: EMIOS0_CH4, the waveform is 20Khz after stabilization, and the duty cycle changes alternately between 25% and 75%. PWM2 PTB14: EMIOS0_CH2, after stabilization, the frequency is 1KHZ, and as the onboard SW5 is pressed, the duty cycle changes alternately between 25% and 75%. Test PTD3, PTD2, it can be seen that it is a pair of complementary waveforms, and the frequency is the same as PTB16, and the duty cycle change rule is also the same. It can be seen that the key interrupt, 3 main PWM, and 2 LCU PWM in this article are already working. Fig 29 Fig 30  
View full article
[S32K3 Tools Part] How to use VScode to compile EB MCAL project       For EB configured MCAL code, it is usually based on RTD and then compiled using the command line. When I first started learning, I always opened the relevant files directly to modify them, and then used the window cmd method to type commands. This method is very clumsy. Therefore, this article will show how to use VScode to open and compile a RTD4.0.0 S32K344 MCAL project. Of course, for MCAL EB projects, before compiling, you need to use the EB tool to open the configuration file of the corresponding project, and then close it after the project is generated. 1 VScode tool and configuration VScode download link: https://code.visualstudio.com/Download After downloading, install it. Here are some installation plug-ins I often use:   Fig 1 Fig 2 You can search in extensions and install it directly. 2. Use VScode to compile the RTD MCAL project This article takes RTD4.0.0, SW32K3_S32M27x_RTD_R21-11_4.0.0 as an example, and the platform is the official S32K344-EVB board. The code takes Dio_TS_T40D34M40I0R0 project as an example. In order not to affect the original routine, Dio_TS_T40D34M40I0R0 is copied and saved as Dio_TS_T40D34M40I0R0_vscode 2.1 Use EB tresos generate the configuration Open EB tools, import the project in path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject Fig 3 Double-click someId, then right-click. If you do not need to make custom configurations, just click generate project. Wait for the generation to complete without errors and close the EB IDE. Fig 4 2.2 VScode  open project    First open VScode and select the project path in open Folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344 Fig 5 After opening, you can see that all the files in the path have been put in: Fig 6 You can save the workspace so you don't need to open the folder every time. File->Save workspace as, save to the path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_vscode\examples\EBT\S32K3XX\Dio_Example_S32K344   2.3 Modify mk file The project mk file needs to be modified to specify gcc, tresos paths, etc. Modify points:project_parameters.mk GCC_DIR = C:/NXP/S32DS.3.5_RTD400/S32DS/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_4.0.0/eclipse/plugins Fig 7 Modify points: check_build_params.mk Delete ifeq ("$(wildcard $(T32_DIR)/bin/windows/t32marm.exe)","") $(error Invalid path set to Trace32. \ The provided path: from project_parameters.mk T32_DIR=$(T32_DIR) is invalid!) Endif Fig 8 Then save all files:File->save all 2.4 Compile the file Terminal->New Terminal Enter the following command: >make generate >make build Fig 9 Fig 10 As you can see, after make build, an elf file has been generated in the out folder. This elf file can be directly downloaded using two methods: (1) S32DS empty project link to elf to download (2) Lauderbach directly download elf file   2.5 debug the generated elf file Since the S32K344-EVB has an onboard opensda tool, we directly use the S32DS empty project to link to the generated main.elf file to download and debug. Create a new S32DS project, and the interface is PE Multilink, then directly change the elf file to main.elf in the debug configuration, and then put the previously generated elf file into the folder of the new S32DS project:  \Debug_FLASH Fig 11 Then, enter debug mode, the results are as follows: Fig 12 As you can see, the chip has entered debug mode and can run successfully. Running at full speed, you can see the onboard red light flashing, so at this point, VSCode has compiled the MCAL code and run successfully.  
View full article
What is S32K1‘s IDLE feature: IDLE is set when the LPUART receive line becomes idle for a full character time after a period of activity.When CTRL[ILT] is cleared, the receiver starts counting idle bit times after the start bit. Why write this demo? Because the RTM driver does not support Lpuart's IDLE detect. What needs to be modified? -1.add "UART_EVENT_DMA_IDLE = 0x04U" to “callbacks.h”   -2 add "LPUART_DRV_RxIdleCallback" to ".lpuart_driver.c"   -3 Define “LPUART_DRV_RxIdleCallback” function   static void LPUART_DRV_RxIdleCallback(uint32_t instance) { DEV_ASSERT(instance < LPUART_INSTANCE_COUNT); LPUART_Type *base = s_lpuartBase[instance]; lpuart_state_t * lpuartState = (lpuart_state_t *)s_lpuartStatePtr[instance]; LPUART_ClearStatusFlag(base,LPUART_IDLE_LINE_DETECT); if(lpuartState->transferType == LPUART_USING_DMA) { lpuartState->rxSize = EDMA_DRV_GetRemainingMajorIterationsCount(lpuartState->rxDMAChannel); LPUART_DRV_StopRxDma(instance); lpuartState->rxCallback(lpuartState,UART_EVENT_DMA_IDLE,NULL);/*UART_EVENT_DMA_IDLE : 0x04*/ } }     -4 add below code to "LPUART_DRV_IRQHandler" and be sure these code must  be put before "LPUART_DRV_ErrIrqHandler(instance)" /* Handle idle line interrupt */ if (LPUART_GetIntMode(base, LPUART_INT_IDLE_LINE)) { if (LPUART_GetStatusFlag(base, LPUART_IDLE_LINE_DETECT)) { LPUART_DRV_RxIdleCallback(instance); } }   -5 configure IDLE releated register in main function. LPUART1->CTRL |= LPUART_CTRL_ILT(1); LPUART1->CTRL |= LPUART_CTRL_IDLECFG(7); LPUART1->CTRL |= LPUART_CTRL_ILIE(1);   Test environment: Hardware is base on S32K144EVB-Q100 Software is S32 Design Studio for Arm V 2.2 + RTM 3.0.X Demo Description:           The baud rate of the serial port is set to 19200, and the function implemented is to send back the received data using DMA methods .      
View full article
 ------------------------------------------------------------------------------ * Test HW: S32K3 T-BOX * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ********************************************************************************  The purpose of this demo application is to present a usage of the  SPI-HAP of S32K3xx MCU to download firmware to SJA1110. SPI using Interrupt working code :-- S32K324_SPI_DMA_SJA1110_Load_firmware__Working__SPI__Interrupt.zip SPI using DMA working code :-- S32K324_SPI_DMA_SJA1110_Load_firmware__SPI_DMA_not_working.zip Firmware image of the SJA1110 is stored inside the S32K3 flash memory.. See the linker file of S32K3, we specify the location where the firmware image is present. This this firmware attached to be loaded to SJA1110, any one of the firmware can be selected and renamed to flash_image.bin  :-- 1>  flash_image.bin  --> Green LED blink on SJA1110 2> flash_image_RED.bin  --> Green LED blink on SJA1110 If you use your proprietary SJA1110 binary firmware, then this example to work, you have to change this MACO, in SJA1110_APP.h file  :-- You can get the size of the SJA1110 image from the MAP file of the attached project. Check for this __sja1110_BIN_SIZE, Symbol in MAP file :--   Switch connection to S32K3 SPI pins :--   LED connected to these pins of SJA1110, on T-BOX hardware :---  
View full article
 ------------------------------------------------------------------------------ * Test HW: S32K3 T-BOX * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K3 T-BOX : SJA1110 Firmware update using SPI HAP : S32DS-3.5 : RTD-3.0.0 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-T-BOX-SJA1110-Firmware-update-using-SPI-HAP-S32DS-3-5-RTD/ta-p/1939324
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-6 = PTB-19 -----> PRESS to enter the STANDBY mode. SW-5 = PTB-26 = WKUP[41] --> PRESS to exit the STANDBY mode. RTC --> Wakeup source-1 The example uses PIT-0 timer, to generate the periodic interrupt. T ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************   Make following settings, SIRC enabled in Standby mode :--    
View full article
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K324 SPI Transmit & Receive, using Interrupt :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-I2C-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1818631 Example S32K324 Bootloader to Application Jump DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-Bootloader-to-Application-Jump-DS3-5-RTD300/ta-p/1832649 Example S32K324 STANDBY wake up using GPIO Switch DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-STANDBY-wake-up-using-GPIO-Switch-DS3-5-RTD300/ta-p/1892849 Example S32K324 STANDBY wake up using CAN-0-RX and GPIO Switch DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K324-STANDBY-wake-up-using-CAN-0-RX-and-GPIO-Switch/ta-p/1911972
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-5 = PTB-26  -----> PRESS to enter the STANDBY mode. SW-6 = PTB-19 = WKUP[38] --> PRESS to exit the STANDBY mode. CAN-0-RX = PTA-6 = WKUP[15] --> send CAN message to exit the STANDBY mode The example uses PIT-0 timer, to generate the periodic interrupt. The example uses FLEXCAN-0 for transmit & receive using following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** CAN BUS :--   Push Buttons :---         Wake-up source, SW-6 GPIO:--   Wake-up source, CAN-0-RX :-- According to the IOMUX table in RM, for example, PTA6 can be used as WKPU15 and CAN0_RX. It means that the WKPU15 input doesn't require specific MSCR configuration. So if its input buffer is enabled and the corresponding WKPU input channel is enabled/configured in the WKPU, it should be able to act as wake-up input.   Standby entry :--   STandby clock :--   Enter Standby mode :--   ********* If you use external BJT on your board to generate 1.5 volts *******************     I tested on Our T172 EVB, with NPN external Ballast transistor is selected to supply the V15_MCU domain. I am able to wake up from standby mode. If we select 2-3 in J31 then NPN external Ballast transistor is selected to supply the V15_MCU domain & wakeup is ok on T172 EVB You have to make following settings in code :--      
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-6 = PTB-19 -----> PRESS to enter the STANDBY mode. SW-5 = PTB-26 = WKUP[41] --> PRESS to exit the STANDBY mode. CAN-0-RX = PTA-6 = WKUP[15] --> send CAN message to exit the STANDBY mode. The example uses PIT-0 timer, to generate the periodic interrupt. The example uses FLEXCAN-0 for transmit & receive using following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Push button :--   Wake-up source, CAN-0-RX :-- According to the IOMUX table in RM, for example, PTA6 can be used as WKPU15 and CAN0_RX. It means that the WKPU15 input doesn't require specific MSCR configuration. So if its input buffer is enabled and the corresponding WKPU input channel is enabled/configured in the WKPU, it should be able to act as wake-up input. Wake-up source, SW-5 GPIO:-- Standby entry :--   STandby clock :-- Enter Standby mode :--  
View full article
Question As we know, the TPPSDK supports S32K144 MCU and various Kinetis MCUs to initialize GD3000 in NXP MC solutions. Because of the release of S32K3 and related SW RTD, it’s necessary to expand the capability of TPPSDK to support S32K3 MC based RTD LLD driver or MCAL driver. Unfortunately, the AA team will not maintain the TPPSDK anymore.  How could we configure the GD3000 chip for S32K3 platform?   Answer I took some time to finish this work. Here I'd like to share you the The Expanded TPPSDK Based on S32K3 RTD that is suitable for S32K3 MC application. You can find the Application Note, the source code of new TPPSDK (GD3000 driver), two examples in the attachment. I hope these materials can help you get start with the expanded TPPSDK on S32K3.
View full article
******************************************************************************** * Detailed Description: * The example updates th UART TX buffer for continuous transfer. * ---------------------------------------------------------------------- * Test HW: S32K344EVB-Q172 * MCU: S32K344, RTD 4.0.0 P24 * Debugger: S32DS_ARM_3.5 * Target: internal_FLASH ********************************************************************************
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-5 = PTB-26  -----> PRESS to enter the STANDBY mode. SW-6 = PTB-19 = WKUP[38] --> PRESS to exit the STANDBY mode. The example uses PIT-0 timer, to generate the periodic interrupt.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Push Buttons :---     Wake-up source, SW-6 GPIO:--     ********* If you use external BJT on your board to generate 1.5 volts *******************   I tested on Our T172 EVB, with NPN external Ballast transistor is selected to supply the V15_MCU domain. I am able to wake up from standby mode. If we select 2-3 in J31 then NPN external Ballast transistor is selected to supply the V15_MCU domain & wakeup is ok on T172 EVB You have to make following settings in code :--      
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3x1 MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x47_A000   starting of FLS_CODE_ARRAY_0_BLOCK_0_S61.  ------------------------------------------------------------------------------ * MCU: S32K310 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Flash end address = 0x480000 Size of each block = 8192 = 0x2000 Start Address of 63 block = 0x480000 - 0x2000 = 0x47E000 = 4710400 Start Address of 62 block = 0x480000 - 0x4000 = 0x47C000 = 4702208 Start Address of 61 block = 0x480000 - 0x6000 = 0x47A000 = 4694016   Ram location where FLASH writing erase code is placed :-- I placed the code at 0x256 byte below the MAX address of the RAM size 16*1024 = 16384 = 0x4000 End of RAM = 0x20400000 + 0x4000 = 0x20404000  0x20404000 - 0x256 = 0x20403DAA 0x20403DAA = 541081002   Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407b80 - 0x00407b54 = 0x2C = 44 byte  S32K3 FLASH Memory Terminology :--        
View full article
 ------------------------------------------------------------------------------ * MCU: S32K310 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K310 MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K310 MEM_InFls DS3.5 RTD300 - NXP Community
View full article
------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K31XEVB-Q100 :-- S32K31XEVB-Q100 Evaluation Board for Automotive General Purpose | NXP Semiconductors Example MCAL S32K311 MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K311 MEM_InFls DS3.5 RTD300 - NXP Community
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3x1 MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x48_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Results :--     Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20407DAA = 541097386             Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00406ff0 - 0x00406f78 = 120 bytes                S32K3 FLASH Memory Terminology :--        
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3xx MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x50_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Results :-- Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20417DAA = 541162922     Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407e64 - 0x00407e38 = 44 bytes      S32K3 FLASH Memory Terminology :--    
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU. This example read & write 4 byte FEE BLock. I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE. The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x52_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
View full article
------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300 :-- Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300 - NXP Community Example S32K344 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :-- Example S32K344 UART Transmit & Receive Using Interrupt DS3.5 RTD300 - NXP Community
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for transmit & receive five bytes using the Interrupt.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************         Putty output :--  
View full article