S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
******************************************************************************** The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - It configures FlexCAN0 module and its transceiver (TJA1153). - MB0 is used to transmit CANFD std. ID - MB1 is configured to receive any std. ID - Callback function is used as well to handle TX and RX process in MBs. Received ID is echoed back. - setupCanXCVR function is called to Init TJA1153 connected to FlexCAN0 on the board. It expects transceiver in Vanilla state and set TPL to pass all std and ext ID and do not block any message coming from bus. Finally leaving configuration mode without writing to non-volatile memory nor locking the transceiver. * * ------------------------------------------------------------------------------ * Test HW: S32K3X8EVB-Q289 rev B2 * MCU: P32K358HVS 0P14E * Compiler: S32DS.ARM.3.5 * SDK release: S32K3_RTD_4.0.0_D2311 / S32K3_RTD_5_0_0_D2408 * Debugger: Lauterbach * Target: internal_FLASH * ********************************************************************************
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the Bootloader Jump to Application.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************   Jump is decided based on the boot_header, size we use to jump to the RESET handler:-- Dinesh_Guleria_0-1708069834663.png Dinesh_Guleria_1-1708069881672.png   Cortex M-7 Interrupt vector table, RESET handler is 4 byte offset from starting of vector table :-- Dinesh_Guleria_2-1708070071946.png   Dinesh_Guleria_3-1708070172883.png // Reset_Handler+1  --> required in IVT, to avoid hard fault As per Arm®v7-M Architecture Reference Manual  --> DDI0403E_e_armv7m_arm.pdf   Dinesh_Guleria_1-1747378493457.png   Dinesh_Guleria_2-1747378510321.png     How to burn elf file of both application & bootloader code :-- Dinesh_Guleria_0-1708073268921.png  
查看全文
[RTD400 LLD]K344 Center Aligned PWM Trigger ADC BCTU 1. Abstract     Not long ago, a customer's actual project needed to implement the high-level center point of the center-aligned PWM on the S32K3XX to trigger the ADC BCTU multi-channel sampling. This function requires the use of EMIOS, ADC, and BCTU. At the beginning, the customer was always unable to achieve the trigger at the center point of the PWM, and the trigger position was wrong. Later, After we give the explanation and analysis of the principles of the K3 related modules to the customer, as well as the guidance of the actual code configuration test, and the customer also achieved the required function. For the convenience of testing, PIT and UART printf functions are also added here. So here is a summary of the specific situation of this function, so that other customers who encounter similar functional requirements in the future can have a reference and can quickly build it. The requirements are as shown in the figure below. In the up-down counting mode, the center-aligned PWM is output, and the trigger sampling of the ADC BTCU LIST is realized at the center point of the high level. This article will implement 1KHZ center-aligned PWM, 50% duty cycle, and high-level center point to achieve ADC BTCU LIST sampling on the official S32K344-EVB board, based on the RTD400 LLD version.   kerryzhou_12-1737802508258.png Fig 1 2. Center-aligned PWM center point trigger ADC principle       Regarding the principle, there is no suspense about ADC. You can directly refer to the previous article on ADC software and hardware triggering: [RTD400 LLD]K344 ADC SW+HW trigger This is the structure shown in Figure 2. After configuring ADC, BCTU and select the triggered EMIOS channel. When the relevant flag of EMIOS is generated, BCTU will be triggered. After the watermark is reached, a notification will be generated to store all LIST ADC channel values ​​in the buffer, and then the ADC value can be printed out for easy viewing according to the situation.  kerryzhou_13-1737802525461.png   Fig 2 In the current working condition, the logic that needs to be concerned about is mainly: how to generate center-aligned PWM, how to generate a flag at the high-level center point, and use this flag to trigger BTCU sampling. 2.1 How to generate center-aligned PWM      First, let’s take a look at the channel status of EMIOS and the channel status that supports center-aligned PWM. kerryzhou_14-1737802545570.png  Fig 3 The center-aligned PWM mode is: OPWMCB As shown in Figure 1, we can see that the counter count mode in this mode is up and down. Let's take a look at the channel types that support OPWMCB. We can see that there is only type G.  kerryzhou_15-1737802657145.png  Fig 4 So, what are the channels supported by Type G? See the figure below: kerryzhou_16-1737802660362.png  Fig 5 The mystery is solved. Only CH1-CH7 of eMIOS supports center-aligned PWM. Well, then a new question arises. Can this mode directly generate a trigger signal at the center point of the PWM high level to trigger the ADC BCTU sampling? Answer: No! The reason can be seen from Figure 1. In this PWM mode, there are two trigger flags generated when the up and down count comparison is completed. Therefore, if this mode channel is used to directly trigger ADC sampling, two triggers will be generated in one cycle, and both are on the edge of PWM. Since OPWMCB cannot directly generate a trigger at the center point of PWM, how to achieve it? In addition, open a dedicated channel, and the clock source is the same as OPWMCB, but that channel only counts to generate trigger flags and does not output any waveform. 2.2 How to generate PWM center point trigger flag   Key information: OPWMCB simultaneous clock source, only counting mode, or up and down MCB mode, only one channel is satisfied: ADC CH0, counter bus type also needs to be selected as counter_bus_B      kerryzhou_17-1737802664429.png  Fig 6 Let's take a look at the trigger flag of MCB: kerryzhou_18-1737802668518.png  Fig 7 As you can see, it is perfect. The trigger mark is at the top of the upward and downward counting, which is exactly the center point of the high level of the same source PWM. So, here, the specific channel arrangement has been determined in principle, two channels: EMIOS0_CH0 MCB mode pure counting and triggering the generation of flags to trigger ADC sampling; EMIOS0_CH1-CH7 is OPWMCB mode, simply outputting center-aligned PWM. 3. Software configuration and implementation       The software uses the S32K3 RTD400 version, and other versions have similar configurations! 3.1 Demo CT  module configuration First, you need to prepare a K344 demo, and then configure the pins, clocks, and peripheral modules. The following will explain the configurations. The modules used are: 2 GPIOs, ADC, BCTU, EMIOS clock, EMIOS PWM, LPUART for printing logs, PIT for timed printing, Trgmux is configured but not used in this article, so I won't talk about it!      3.1.1 Pin configuation       The pins used are as follows: kerryzhou_19-1737802674350.png  Fig 8 The two GPIOs are used to toggle in BCTU trigger notification and BCTU watermark notification respectively, to test the waveform positioning. ADC1_s10 pin is used for ADC1, but this article mainly uses BCTU to combine ADC0. ADC0 does not add specific external pins, but uses internal signals. LPUART is used for printing, and EMIOS0_CH1 is used to generate center-aligned PWM waveforms. 3.1.2 Clock configuration      The clocks that need to be paid attention to here are: ADC clock, EMIOS clock, UART clock, and PIT clock. kerryzhou_20-1737802679200.png  Fig 9 These clocks will be used later when configuring specific timing periods and baud rates. 3.1.3 Peripheral configuration       The peripherals used mainly include the following modules: kerryzhou_21-1737802684346.png  Fig 10 (1)Adc_Sar_Ip The configuration of the ADC0 module uses the one shot mode, that is, one conversion is generated after one trigger. In this way, the timer EMIOS channel can be used to generate trigger conditions to trigger a conversion. Pre-sampling is enabled to prevent the residual charge of the sampled value of the previous channel from affecting the result of the current channel and causing deviation of the ADC value. The trigger mode uses BCTU. For the configuration of Adc prescaler value and calibration prescale, the frequency division requirements in RM need to be met. The final configuration is as follows: kerryzhou_22-1737802689462.png  Fig 11  kerryzhou_23-1737802693578.png   Fig 12 (2)Bctu_Ip The configuration of Bctu_Ip needs to select the right EMIOS channel to use. From the above principle, we can know that EMIOS0_CH0 is used, and then LIST mode is adopted. For ADC0, three internal channels are currently added to the LIST: BANDGAP, VREFL, VREFH. The specific configuration is as follows: kerryzhou_24-1737802696994.png  Fig 13  kerryzhou_25-1737802702313.png  Fig 14 (3)Emios_Mcl_Ip Here we need to consider the PWM cycle that needs to be generated. The goal is to generate a 1Khz center-aligned PWM, so the EMIOS mode is the MCB up-down counting mode. The clock cycle formula for MCB is: (2 x AS1) – 2. So for the EMIOS0 clock source of 160Mhz, what is the corresponding 1KHZ counter? First do 160 divide to get 1Mhz, and then calculate according to (2 x AS1) – 2: (2 x AS1) – 2 = 1Mhz/1KHZ=>AS1=1000/2 +1= 501. The configuration is as follows: kerryzhou_26-1737802711894.png  Fig 15 (3)Emios_Pwm The previous principle analysis shows that the PWM uses the OPWMCB center-aligned mode PWM, the clock comes from the counter bus B of EMIOS CH0, then the period is 1khz, and the duty cycle is 50%. The specific configuration is as follows: kerryzhou_27-1737802722172.png  Fig 16 (4)Lpuart_Uart Configure UART6 clock baud rate to 115200.  kerryzhou_28-1737802726379.png  Fig 17 (5)Pit  kerryzhou_29-1737802729584.png  Fig 18 (6)IntCtrl_Ip The interrupt configuration is as follows, and it can actually be configured via code. kerryzhou_30-1737802734820.png  Fig 19 3.2 Main code situation After the configuration is completed, the output of the center PWM and the sampling of the ADC BCTU can be realized by calling the following code in main. #include "Clock_Ip.h" #include "IntCtrl_Ip.h" #include "Adc_Sar_Ip.h" #include "Bctu_Ip.h" #include "Siul2_Port_Ip.h" #include "Pit_Ip.h" #include "Siul2_Dio_Ip.h" #include "Trgmux_Ip.h" #include "Lpuart_Uart_Ip.h" #include "Lpuart_Uart_Ip_Irq.h" #include "string.h" #include "stdio.h" #include "retarget.h" #include "Emios_Mcl_Ip.h" #include "Emios_Pwm_Ip.h" /* PIT instance used - 0 */ #define PIT_INST_0 0U /* PIT Channel used - 0 */ #define CH_0 0U /* PIT time-out period - equivalent to 1s */ #define PIT_PERIOD 40000000 static volatile uint8 toggleLed = 0U; #ifdef ADC_3V3_VREF_SELECTED #define ADC_BANDGAP 5980U /* Vbandgap ~ 1.2V on 14 bits resolution, 3.3V VrefH */ #else #define ADC_BANDGAP 3932U /* Vbandgap ~ 1.2V on 14 bits resolution, 5V VrefH */ #endif #define ADC_SAR_USED_CH 48U /* Internal Bandgap Channel */ #define BCTU_USED_SINGLE_TRIG_IDX 0U #define BCTU_USED_FIFO_IDX 0U #define BCTU_FIFO_WATERMARK 3U #define ADC_TOLERANCE(x,y) (((x > y) ? (x - y) : (y - x)) > 200U) /* Check that the data is within tolerated range */ #define LED_Q172_PIN 13u #define LED_Q172_PORT PTA_H_HALF #define GPIO_PTA2_PIN 2u #define GPIO_PTA2_PORT PTA_L_HALF #define EMIOS_INST0 0U volatile int exit_code = 0; volatile boolean notif_triggered = FALSE; volatile boolean notif_triggered1 = FALSE; volatile uint16 data; volatile uint16 data1; volatile uint16 data_bctu[3]; #define UART_LPUART_INTERNAL_CHANNEL 6 #define WELCOME_MSG_1 "Hello, This message is sent via Uart!\r\n" volatile Lpuart_Uart_Ip_StatusType lpuartStatus = LPUART_UART_IP_STATUS_ERROR; uint32 remainingBytes; uint32 T_timeout = 0xFFFFFF; uint8* pBuffer; extern void Adc_Sar_0_Isr(void); extern void Bctu_0_Isr(void); extern void Adc_Sar_1_Isr(void); void AdcEndOfChainNotif(void) { notif_triggered = TRUE; data = Adc_Sar_Ip_GetConvData(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_USED_CH); /* Checks the measured ADC data conversion */ } void AdcEndOfChainNotif1(void) { notif_triggered1 = TRUE; data1 = Adc_Sar_Ip_GetConvData(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, 34); /* Checks the measured ADC data conversion */ } void Pit0ch0Notification(void) { toggleLed = 1U; } void BctuWatermarkNotif(void) { uint8 idx; Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 1U); notif_triggered = TRUE; for (idx = 0u; idx < BCTU_FIFO_WATERMARK; idx++) { data_bctu[idx] = Bctu_Ip_GetFifoData(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_FIFO_IDX); } Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); } void BcutTriggerNotif() { Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 1U); Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 0U); } void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } int main(void) { StatusType status; uint8 Index; Clock_Ip_StatusType clockStatus; /* Initialize and configure drivers */ clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); while (clockStatus != CLOCK_IP_SUCCESS) { clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); } Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); #if 1 Bctu_Ip_Init(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &BctuHwUnit_0_BOARD_INITPERIPHERALS); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_0_BOARD_InitPeripherals); while (status != E_OK); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_1_BOARD_InitPeripherals); while (status != E_OK); /* set PIT 0 interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(PIT0_IRQn); /* Install and enable interrupt handlers */ IntCtrl_Ip_InstallHandler(ADC0_IRQn, Adc_Sar_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(BCTU_IRQn, Bctu_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(ADC1_IRQn, Adc_Sar_1_Isr, NULL_PTR); IntCtrl_Ip_EnableIrq(ADC0_IRQn); IntCtrl_Ip_EnableIrq(BCTU_IRQn); IntCtrl_Ip_EnableIrq(ADC1_IRQn); // IntCtrl_Ip_EnableIrq(EMIOS0_5_IRQn); /* Call Calibration function multiple times, to mitigate instability of board source */ for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); /* Start a SW triggered normal conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_NORMAL); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; /* Start a SW triggered injected conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_INJECTED); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; #endif /* Initialize PIT instance 0 - Channel 0 */ Pit_Ip_Init(PIT_INST_0, &PIT_0_InitConfig_PB_BOARD_InitPeripherals); /* Initialize channel 0 */ Pit_Ip_InitChannel(PIT_INST_0, PIT_0_CH_0); /* Enable channel interrupt PIT_0 - CH_0 */ Pit_Ip_EnableChannelInterrupt(PIT_INST_0, CH_0); /* Start channel CH_0 */ Pit_Ip_StartChannel(PIT_INST_0, CH_0, PIT_PERIOD); // Trgmux_Ip_Init(&Trgmux_Ip_xTrgmuxInitPB);// Lpuart_Uart_Ip_Init(UART_LPUART_INTERNAL_CHANNEL, &Lpuart_Uart_Ip_xHwConfigPB_6_BOARD_INITPERIPHERALS); Emios_Mcl_Ip_Init(EMIOS_INST0, &Emios_Mcl_Ip_0_Config_BOARD_INITPERIPHERALS); Emios_Pwm_Ip_InitChannel(EMIOS_PWM_IP_BOARD_INITPERIPHERALS_I0_CH1_CFG, &Emios_Pwm_Ip_BOARD_InitPeripherals_I0_Ch1); printf("S32K344 PIT TRIGMUX ADC demo RTD400.\r\n"); /* Uart_AsyncSend transmit data */ lpuartStatus = Lpuart_Uart_Ip_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *) WELCOME_MSG_1, strlen(WELCOME_MSG_1)); /* Check for no on-going transmission */ do { lpuartStatus = Lpuart_Uart_Ip_GetTransmitStatus(UART_LPUART_INTERNAL_CHANNEL, &remainingBytes); } while (LPUART_UART_IP_STATUS_BUSY == lpuartStatus && 0 < T_timeout--); Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); while(1) { #if 1 if( toggleLed == 1) { toggleLed = 0; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu[0]); printf("ADC0_vrefl ch54 data_bctu = %d .\r\n", data_bctu[1]); printf("ADC0_vrefh ch55 data_bctu = %d .\r\n", data_bctu[2]); } #endif } return exit_code; } 3.3 Test result    The test results include two parts: the printed results show the ADC sampling value, and the relationship between the PWM output and the BCTU trigger position. The printed results are as follows, and you can see that the values ​​of the three different ADC channels are correct: kerryzhou_31-1737802747820.png  Fig 20 PWM wave test result is: Ch1:PTB13 PWM Ch2:PTA29 BCTU trigger notification Ch3: PTA2 BCTU watermark notification kerryzhou_33-1737802767062.png   Fig 21 From the figure, we can see that the first BCTU trigger is at the center point of the PWM high level, and the BCTU watermark notification is used to store data after the ADC sampling is triggered three times. Here is another waveform to view the PWM cycle: kerryzhou_34-1737802770654.png  Fig 22 It can be seen that the PWM period is 1Khz, the duty cycle is 50%, and the first trigger of BCTU is at the center of the PWM high pulse. 4. Summary and trip description Through the above configuration, the RTD400 LLD method was finally used on the S32K344-EVB to implement a 1Khz, 50% duty cycle center-aligned PWM, and the high pulse center position triggered the ADC BCTU LIST acquisition. The trip encountered were my own configuration problems. At the beginning, I mistakenly thought that the watermark configuration value was consistent with the number of LIST channels. In fact, the watermark trigger is triggered only when the watermark value is exceeded. Therefore, if it is a 3-channel LIST, the watermark needs to be configured as 2, not 3. If it is 3, the test waveform is as follows: kerryzhou_35-1737802774543.png Fig 23 As you can see, the watermark notification is actually generated after it is triggered 4 times. Therefore, remember to match the FIFO number of the watermark. Attachment: 1. S32K344_centerPWM1k_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip Center PWM triggered BCTU LIST   2.S32K344_CPWM1k_TRIGMUX_BCTUHWLIST_EMIOSch4_ADC_printf_RTD400.zip PWM emios0_ch4 falling edge trigger the BCTU, for the comment situation.   3. Another method of center trigger: MCB_Counter up. Emios0_CH0 as the counter bus EMIOS0_CH1 as the PWM output EMIOS0_CH2 as the center trigger, but no PWM output, OPWMB S32K344_NCPWM1k1_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip
查看全文
*********************************************************************************** * Detailed Description: * C40_Ip driver is moved to SRAM in files: C40_Ip.h, SchM_Mem_43_INFLS.h * The function that launches the C40_Ip APIs from main() is also placed in the SRAM. * Check the addresses of the APIs in the .map file. * ------------------------------------------------------------------------------ * Test HW: : S32K312EVB-Q172 * MCU: : S32K312 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : S32DS 3.5, RTD 5.0.0 * Build Version : S32K3_RTD_5_0_0_D2408_ASR_REL_4_7_REV_0000_20241002 ***********************************************************************************
查看全文
******************************************************************************************** * Test HW: S32K312 EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: Internal_FLASH ******************************************************************************************** The objective of this demo application is to generate an interrupt by comparing DAC internal reference voltage against any analog input which is connected in analog mux input channels(IN0 : IN7) and wakes the MCU from sleep(standby) mode.  In this demo code,            1)LPCMP0 is used - DAC output is  given to comparator minus (INM) and                                                      AIN2 is given to comparator plus (INP).                From S32K3 RM, highlighted the channels used for reference.                                         krshvivek_1-1741344085196.png                             Green color represents DAC, Pink color represents AIN2 which is selected from PMUX           2) From S32K RM,                "Compares two analog input voltages applied to INP and INM,                   COUT_RAW is high when the INP input voltage is greater than the INM input voltage,                   COUT_RAW is low when the INP input voltage is less than the INM input voltage"                So in this demo code,                RED LED is ON , if AIN2 Voltage > DAC Internal reference voltage(COUT is HIGH)                GREEN LED is ON, If AIN2 Voltage < DAC Internal reference voltage (COUT is LOW)   MODULES USED: Modules.png   MODIFICATIONS IN LPCMP MODULE:     CMP_Config.png CMP_Config_1.png   MODIFICATIONS IN INTCTRL_IP MODULE: krshvivek_7-1741346448044.png     MODIFICATIONS IN WKPU MODULE:   WKPU_2.png    From S32K3 RM, Analog comparator has used Channel 2 for wakeup. WKPU_4.png  Modifications in the "Cmp_Ip_IrqHandler" function in "Cmp_IP.c" source file: NOTE: Not sure how it got missed or from where to get COUT status, so added manually to get COUT status from CSR register in the Cmp_Ip_Irqhandler once code generation is completed. krshvivek_11-1741347732110.png   PIN SELECTION DETAILS: PIN_SELECTION.png HOW TO TEST?  a) Connect jumper wire at the PTC2 in the EVB as highlighted in EVB below. b) RED LED ON -> Jumper wire connects to 5V      GREEN LED ON-> Jumper wire connects to GND c) MCU enters STANDBY once SW5 is pressed and it wakes up if the jumper wire is disconnected from either 5V or GND. NOTE: In this demo, since jumper wire is used instead of button/ADC, due to high impendence state, LED will be toggling if jumper wire is not connected to GND/5V. krshvivek_12-1741348477463.png Connect male jumper wire at PTC2 Thanks & regards, Krishnakumar V
查看全文
******************************************************************************************** * Test HW: S32K312 EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************************** The objective of this demo application is to generate an interrupt by comparing DAC internal reference voltage against any analog input which is connected in analog mux input channels(IN0 : IN7). In this demo code,            1)LPCMP0 is used - DAC output is  given to comparator minus (INM) and                                                      AIN2 is given to comparator plus (INP).                From S32K3 RM, highlighted the channels used for reference.                Green color represents DAC, Pink color represents AIN2 which is selected from PMUX          2) From S32K RM,                "Compares two analog input voltages applied to INP and INM,                   COUT_RAW is high when the INP input voltage is greater than the INM input voltage,                   COUT_RAW is low when the INP input voltage is less than the INM input voltage"                So in this demo code,                RED LED is ON , if AIN2 Voltage > DAC Internal reference voltage(COUT is HIGH)                GREEN LED is ON, If AIN2 Voltage < DAC Internal reference voltage (COUT is LOW)   Modules used: LPCMP_ModulesUsed.png          Modifications in LPCMP module: LPCMP_CMP_modifications.png LPCMP_CMP_Modifications2.png   Modifications in IntCtrl_IP module: LPCMP_INTCtrl_IP_Modifcations.png Modifications in the "Cmp_Ip_IrqHandler" function in "Cmp_IP.c" source file: Note: Not sure how it got missed or from where to get COUT status, so added manually to get COUT status from CSR register in the Cmp_Ip_Irqhandler once code generation is completed. LPCMP_IRQHandler_codeChange.png GPIO selection details: LPCMP_PinSelectionDetails.png How to test ? a) Connect jumper wire at the PTC2 in the EVB as highlighted in EVB below. b) RED LED ON -> Jumper wire connects to 5V      GREEN LED ON-> Jumper wire connects to GND Connect male jumper wire at PTC2 Thanks & regards, Krishnakumar V
查看全文
*********************************************************************************** * Detailed Description: * The example locks * PFC PFCBLK2_SSPELOCK REG_PROT soft lock * and PFC REG_PROT hard lock. * ------------------------------------------------------------------------- * Test HW: : S32K344EVB-Q172 * MCU: : S32K344 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * SW Version : 5.0.0 * Build Version : S32K3_RTD_5_0_0_D2408_ASR_REL_4_7_REV_0000_20241002 ***********************************************************************************
查看全文
This article has been moved to a new location: https://community.nxp.com/t5/S32M-Knowledge-Base/S32M2xx-Motor-control-use-cases/ta-p/2039790
查看全文
This is an example project which is created to do an internal wake up from VLPS mode using LPTMR0.   From S32KRM, it tells us that internal wakeup is achievable using LPTMR0. Wakeup_info.png     What code does? ======================================= 1) LPTMR0 is configured for 5 Seconds. So for interrupt occurs for every 5 seconds 2)LPTMR0  wakes up MCU for every 5 seconds and again it goes back to sleep for next 5 seconds. This cycle repeats forever. 3) When MCU is in RUN mode, GREEN color LED will be ON and it will in OFF if it goes to VLPS.   Project Configurations: =======================================   PinConfigurations.png   Other Informations: ======================================= Design studio: S32DS3.4 SDK                    : RTM 4.0.2 EVB                     : S32K118EVB2Q048   Note:   Following symbols should be included if you are creating the project from scratch to properly put MCU to sleep and wakeup from POR. MACRO1.png Symbol2.png   Thanks & regards, Krishnakumar V
查看全文
【RTD400 MCAL 3】 K312 MCU clock system configuration 1. Abstract This document is talking about how to configure the clock system in the MCU of the K3 chip MCAL. This topic was always disdainful to talk about when I was doing LLD before, because the clock system of K3 is too simple, with internal fast and slow clock sources, external fast and slow clock sources, a PLL multiplier, and then various core peripherals to share. K3's RM even made a few options to frame the rules. From the perspective of LLD, especially the perspective of S32DS CT configuration, it is even more concise and clear. Here is a CT picture to show it: kerryzhou_0-1737807670859.png   Fig 1   kerryzhou_1-1737807677834.png   Fig 2 With such a clock system, you can generate code with just a few taps and pokes. However, LLD is too free, and MCAL often encounters problems. Therefore, I decided to spend some time to understand the entire clock system of this MCAL MCU. This article takes K312 as an example to explain. Other K3 series are similar. 2. Clock system theory and configuration 2.1 K312 clock system From the clock chapter of RM, you can see the whole system block diagram:   kerryzhou_2-1737807691162.png   Fig 3 This block diagram clearly shows the situation of each part. There are four clock sources: Internal fast clock FIRC: 48MHz, +/-5% error, maximum startup time 25us Internal slow clock SIRC: 32KHz, +/-10% error, maximum startup time 3ms External fast clock FXOSC: 8-40MHz, startup stabilization time FXOSC_CTRL[EOCV] × 128 External slow clock SXOSC: 32.768KHz, startup stabilization time SXOSC_CTRL[EOCV] x 128 One PLL: input 8-40MHZ, VOC output 640M-1280Mhz, PLL_PHIn_CLK output 25-480MHz. MUX_0: Output CORE_CLK, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK MUX_1: Output system timer STM0_CLK MUX_3: Output FLEXCAN0-2 clock MUX_4: Output FLEXCAN3-5 clock MUX_5: Output CLKOUT_STANDBY MUX_6: Output CLKOUT_RUN MUX_11: Output TRACE_CLK RTC_CLK: RTC clock 2.1.1 PLL From the PLL perspective, we need to know which values ​​the frequency multiplier is related to, which can be calculated using the following formula:   kerryzhou_3-1737807699042.png   Fig 4 If it is an integer, the red box in the above figure is the common method, and this article will also use the above method to configure. PLL_PHI is the clock output by the final PLL, which is provided to the MC corresponding to other MUXs for selection. 2.1.2 MUX_0 System The MUX_0 system with details can be seen from RM:   kerryzhou_4-1737807714498.png   Fig 5 As you can see, the clock source of MUX_0 can be two types: PLL or internal FIRC. Then the core clock can be generated later, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK. So what is the specific frequency of the generated clock? In principle, it can meet the maximum clock corresponding to each module, but the K3 series also makes some option recommendations. For example, K312 recommends using option B mode when RUN, especially the HSE clock, which usually needs to strictly meet the option recommendation. 2.1.3 MUX_6 Clock output In order to check the corresponding clock situation in the chip, the corresponding clock can be output through the CLKOUT pin. The CLKOUT pin can correspond to the selection of multiple clock sources. The specific situation is as follows:   kerryzhou_5-1737807720158.png   Fig 6 The yellow content in the figure is what K312's CLKOUT_RUN can support. After the clock is configured, the corresponding clock will be selected to test whether the output is consistent with the configuration. 2.1.4 option B Recommended Solution In this article, K312 will configure the clock of option B in EB.   kerryzhou_6-1737807735724.png   Fig 7 2.2 EB configuration        First, create a new K312 EB project. For the specific creation method, please refer to the previous article: [S32K3 Tools Part] How to port RTD's existing MCAL demo to other K3 chips This article will focus on the clock configuration corresponding to the MCU module based on RTD400 MCAL. For MCU configuration, two documents need to be consulted as reference books: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Mcu_TS_T40D34M40I0R0\doc: RTD_MCU_UM.pdf and RTD_MCU_IM.pdf If you don’t know how to configure, just follow the default values ​​recommended by the document. The following figure is an overview of the MCU. The main configured modules have the following three components: General, McuClockSettingConfig, McuModeSettingConf   kerryzhou_7-1737807749313.png   Fig 8 2.2.1 General configuration In addition to Figure 8, you need to turn on the internal and external fast and slow clock control and PLL control, and add the corresponding API, as well as the crystal oscillator frequency. If this is not turned on, the corresponding configuration later will not be able to be configured.   kerryzhou_8-1737807754646.png   Fig 9 2.2.2 McuClockSettingConfig configuration        This is the core area of ​​MCU clock configuration, which includes clock source, PLL, and various MUX conditions. First, you need to add a clock configuration:   kerryzhou_9-1737807770429.png   Fig 10 Click in and there will be detailed configuration:   kerryzhou_10-1737807778011.png   Fig 11 There are 17 items in total. You can keep the default configuration for options 1 and 6. Since the board does not connect to the external slow crystal oscillator 5, it is not configured. The rest should be configured according to the actual situation. The following explains them one by one: 2.2.2.1 McuFIRC configuration    Internal fast clock, 48MHz:   kerryzhou_11-1737807791866.png   Fig 12 2.2.2.2 McuSIRC configuration Internal slow clock 32Khz   kerryzhou_12-1737807801198.png   Fig 13 2.2.2.3 McuFXOSC configuration External crystal oscillator 16MHZ, fill in according to the actual connection situation.   kerryzhou_13-1737807813718.png   Fig 14 2.2.2.4 McuCgm0ClockMux0 configuration Mux0 configuration, here are configured core clock, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE, DCM_CLK, is to meet the optionB requirements, and the clock comes from PLL_PHI0_CLK. When actually configuring, first configure the PLL clock to output the correct PLL_PHI0_CLK, PLL_PHI1_CLK clock.   kerryzhou_14-1737807826426.png   Fig 15 2.2.2.5 McuCgm0ClockMux1 configuration   kerryzhou_15-1737807916728.png   Fig 16 It can be configured according to the clock source required by the actual module. 2.2.2.6 McuCgm0ClockMux3 configuration Configure the clock source of the FLEXCAN0-2 module:   kerryzhou_16-1737807926938.png   Fig 17 2.2.2.7 McuCgm0ClockMux4 configuration Configure the clock source of the FLEXCAN3-5 module:   kerryzhou_17-1737807941602.png   Fig 18 2.2.2.8 McuCgm0ClockMux5 configuration Configure the clock source of the CLKOUT_STANBY module:   kerryzhou_18-1737807946406.png   Fig 19 2.2.2.9 McuCgm0ClockMux6 configuration Configure the clock source of the CLKOUT_RUN module   kerryzhou_19-1737807964974.png   Fig 20 2.2.2.10 McuCgm0ClockMux11 configuration Configure the clock source of the TRACE_CLK module   kerryzhou_20-1737807973402.png   Fig 21 2.2.2.11 McuRtcClockSelect configuration Configure the clock source of the RTC module   kerryzhou_21-1737807987068.png   Fig 22 2.2.2.12 McuPLL configuration Configure the clock source of the PLL module   kerryzhou_22-1737807991862.png   Fig 23 2.2.2.13 McuClockReferencePoint configuration Configure the reference clock and the clock source selection interface of the peripheral modules.   kerryzhou_23-1737808007938.png   Fig 24 At this point, the clock configuration is complete. For verification, you can use the CLKOUT_RUN output to output the corresponding clock to pin PTD10 for viewing. 2.2.3 McuModeSettingConf  configuration In Mcu's McuModeSettingConf->McuPeripheral, you need to turn on the peripherals you want to use:   kerryzhou_24-1737808019153.png   Fig 25 2.2.4 PORT  configuration Because the internal clock needs to be output to CLKOUT_RUN, K312's PTD10 MSCR106 is checked, so the PORT pin is added as follows:   kerryzhou_25-1737808030584.png   Fig 26 3. Test Result Next, on the S32K312-EVB board, we modify the clock source of EB's CLKOUT_RUN to test whether the clock matches the configuration. Commonly used MCU-related drivers are as follows:   kerryzhou_26-1737808035339.png   Fig 27 The calling sequence of system startup MCU initialization is as follows: 1). Mcu_Init() 2). Mcu_InitClock() 3). Mcu_GetPllStatus() - Till PLL is locked. 4). Mcu_DistributePllClock() 5). Mcu_SetMode() 6). Mcu_InitRamSection() - If required The corresponding main code is as follows: #include "Mcu.h" #include "Mcu_Cfg.h" #include "Port.h" #include "Dio.h" #include "Port_Cfg.h" #include "Platform.h" void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } /** * @brief Main function of the example * @details Initialize the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { uint8 count = 0U; uint8 u8TimeOut = 100U; /* Initialize the Mcu driver */ #if (MCU_PRECOMPILE_SUPPORT == STD_ON) Mcu_Init(NULL_PTR); #elif (MCU_PRECOMPILE_SUPPORT == STD_OFF) Mcu_Init(&Mcu_Config_VS_0); #endif /* (MCU_PRECOMPILE_SUPPORT == STD_ON) */ /* Initialize the clock tree and apply PLL as system clock */ Mcu_InitClock(McuClockSettingConfig_0); #if (MCU_NO_PLL == STD_OFF) while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() ) { } Mcu_DistributePllClock(); #endif /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize Platform driver */ Platform_Init(NULL_PTR); while (count++ < 10) { Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_HIGH); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_HIGH); TestDelay(5000000); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_LOW); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_LOW); TestDelay(5000000); } // Exit_Example(TRUE); return (0U); } #ifdef __cplusplus } #endif 3.1 CLKOUT FIRC_CLK DIV2   kerryzhou_27-1737808056154.png   Fig 28 It can be seen that the original 48Mhz clock of FIRC is divided by 2 and the clock waveform of 24Mhz is obtained, which is correct! 3.2 CLKOUT SIRC_CLK DIV2   kerryzhou_28-1737808060208.png   Fig 29 It can be seen that the original 32Khz clock of SIRC is divided by 2 and the clock waveform of 16khz is obtained, which is correct! 3.3 CLKOUT FXOSC_CLK DIV10   kerryzhou_29-1737808075509.png   Fig 30 It can be seen that the original 16Mhz clock of FXOSC is divided by 10 and the clock waveform of 1.6Mhz is obtained. 3.4 CLKOUT PLLPH0 CLK DIV10   kerryzhou_30-1737808081217.png   Fig 31 It can be seen that the original 120Mhz clock of PLLPH0 is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.5 CLKOUT CORE CLK DIV10   kerryzhou_31-1737808094772.png   Fig 32 It can be seen that the original 120Mhz clock of CORE is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.6 CLKOUT PLLPH1 CLK DIV4   kerryzhou_32-1737808099268.png   Fig 33 It can be seen that the original 48Mhz clock of PLLPH1 is divided by 4 and the 12Mhz clock waveform is obtained. 3.7 CLKOUT HSE CLK DIV10   kerryzhou_33-1737808116460.png   Fig 34 It can be seen that the original 60Mhz clock of HSE is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.8 CLKOUT AIPS_PLAT CLK DIV10   kerryzhou_34-1737808124117.png   Fig 35 It can be seen that the original 60Mhz clock of AIPS_PLAT_CLK is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.9 CLKOUT AIPS_SLOW CLK DIV10   kerryzhou_35-1737808132759.png   Fig 36 It can be seen that the original 30Mhz clock of AIPS_SLOW_CLK is divided by 10 and the clock waveform of 3Mhz is obtained, which is correct.  
查看全文
Hi team, First let me explain about the code about what it does. ======================================= 1) From POR, LED  starts blinking - In this state RTC won't be initialized. 2) Once SW5 is pressed in S32K312 EVB - RTC will be initialized before MCU goes to sleep. 3) RTCCNT will be incrementing during sleep  4) Once SW6 is pressed , MCU wakes from the sleep and we could able see the updated RTC time and date. WAR(Work Around)done to keep RTC alive during sleep: ======================================= Tried to test the RTC with sleep mode, observed that RTCCNT value is getting reset once after every wakeup. So that time and date was not able to preserve the value. In order to avoid this, I have done two workarounds to solve this RTCCNT value reset issue. 1) RTC will not be initialized for if MCU wakeup from the sleep - Made the check to initialize when MCU is not from the wakeup before it goes to sleep. krshvivek_0-1736931950041.png wake_up_event will be incremented if MCU reset reason is wakeup as shown below. krshvivek_1-1736932038455.png   2) Updating "Rtc_Ip_u32ChState" array variable for "ticksPerSecond" member in "Rtc_Ip.c" file manually after the code generation is completed.  Note: With auto generated code the value of "ticksPerSecond "will be "0". krshvivek_2-1736932277658.png    Any other alternatives other than this approach is highly appreciated. Thanks in advance!  
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the DMA. This above mentioned operation is performed 10 times continuously MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** For S32K312, please use this correct clock HSE to AIPS clock should be ½. Please make these changes in the below all example code clock setting. HSE clock to 60 MHZ. Dinesh_Guleria_0-1721124304036.png   Dinesh_Guleria_0-1705047952901.png Dinesh_Guleria_1-1705047972487.png   Use this MACRO to enable disable the non cacheable region variable placement :-- Dinesh_Guleria_0-1736407682746.jpeg   Dinesh_Guleria_1-1736407682748.jpeg   Dinesh_Guleria_2-1736407682749.jpeg   Dinesh_Guleria_3-1736407682750.jpeg    
查看全文
******************************************************************************************** * Test HW: S32K311 EVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************************** The purpose of this demo application is to enter the standby mode and waking up from sleep using the user button. =============== How this DEMO works ========== 1) once the image is flashed, the application starts running and BLUE LED blinks for every one second during RUN mode 2) Once SW5 in EVB is pressed, MCU enters the SLEEP mode and it turns off BLUE LED & PIT 3) To Wakeup: Press SW4 in EVB 4) Once it returns to normal mode, BLUE LED and PIT starts running. Used pins: ========= PTC11 -> SW5 -> EnterStandby PTA8 -> SW4 -> WakeupFromSleep PTB8 -> D12   -> Blue led  
查看全文
The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD and Enhance RXFIFO using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - MB0 is configured to transmit either std. or ext ID - MB1 is configured to receive ext ID 0xFACE and MB2 to receive std ID 0x1 - Enhanced RXFIFO is enabled and 3 enhanced RXFIFO filter elements (filter + mask scheme) are defined ext ID 0xABCD with mask 0x1FFFFFFF std ID 0x123 with mask 0x7FF std ID 0x456 with mask 0x7FF - DMA is used to read enhanced RXFIFO, watermark is set to 5 - Callback function is used as well to handle TX and RX process in MBs and Enhanced RXFIFO after DMA complete 5 reading of RXFIFO  ------------------------------------------------------------------------------  Test HW: S32K3444EVB-Q172  MCU: PS32K344EHVPBS 1P55A  Compiler: S32DS.ARM.3.5  SDK release: S32K3_RTD_4_0_0_D2311  Debugger: Lauterbach  Target: internal_FLASH
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the SPI Interrupt Lpspi_Ip_AsyncTransmit() method . MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Interrupt Triggered :-- Dinesh_Guleria_0-1733909921359.png Async callback triggered at the end of transfer/reception :-- Lpspi_Ip_AsyncTransmit(&MASTER_EXTERNAL_DEVICE, txBuffer, rxBuffer, numberOfBytes, lpspi_callback_int); Dinesh_Guleria_1-1733909974233.png     Dinesh_Guleria_0-1733909770614.png  
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the SPI polling Lpspi_Ip_SyncTransmit() method. MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Dinesh_Guleria_1-1733909785035.png   Dinesh_Guleria_0-1733909770614.png  
查看全文
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K312 MEM_InFls  DS3.5 RTD300 :-- Example MCAL S32K312 MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE DS3.5 RTD300 :-- Example MCAL S32K312 FEE DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 - NXP Community Dinesh_Guleria_0-1718095365471.png Example MCAL S32K312 PWM ICU using Custom IRQ EMIOS DS3.5 RTD300 :-- Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community  Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community
查看全文
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Interrupt mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :-- Dinesh_Guleria_0-1733896956186.png Dinesh_Guleria_4-1733897197653.png   Dinesh_Guleria_5-1733897299281.jpeg   This example is tested for SAIC & IPWM mode both. You can change the mode by this setting in MEX file :-- Dinesh_Guleria_3-1733900502087.png     Difference between SAIC & IPWM,  ICU Driver User Manual :-- Dinesh_Guleria_2-1733897086528.png   These Two Macro :-- SAIC_MODE  --> this maco will enable variables to store for SAIC mode CUSTOM_IRQ  --> this MACRO will enable customized IRQ or RTD available IRQ Dinesh_Guleria_8-1733897822913.png   Result :-- Dinesh_Guleria_2-1733900446350.png     Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :-- Dinesh_Guleria_1-1733900369112.png    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Polling mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :-- Dinesh_Guleria_0-1733896956186.png Dinesh_Guleria_4-1733897197653.png   Dinesh_Guleria_5-1733897299281.jpeg   This example is tested for IPWM mode .  :-- Dinesh_Guleria_1-1733899599108.png       IPWM mode ,  ICU Driver User Manual :-- Dinesh_Guleria_2-1733897086528.png   Result :-- Dinesh_Guleria_0-1733899546647.png Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :-- Dinesh_Guleria_1-1733900303954.png      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
*******************************************************************************  The purpose of this demo application is to present a usage of the ICU & PWM MCAL Driver for the S32K3xx MCU. This example uses the custom IRQ. The example uses:-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Dinesh_Guleria_0-1733220239428.png     Dinesh_Guleria_1-1733220247864.png   Result :-- Dinesh_Guleria_2-1733220259942.png      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文