S32K ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Knowledge Base

ラベル

ディスカッション

ソート順:
******************************************************************************** * Detailed Description: * CM7_0 starts CM7_2 using Power_Ip or directly in MC_ME (macro USE_RTD_POWER_IP). * Disconnect the debugger and power-cycle the MCU. * * ------------------------------------------------------------------------------ * Test HW: S32K3x8EVB-Q289 * MCU: S32K358 * Debugger: S32DS_ARM_3.5, S32K3_RTD_4_0_0_P24_D2405 * Target: internal_FLASH ******************************************************************************** Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
記事全体を表示
S32K344 + MC33664 + MC33774 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33664-MC33774-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2028783 S32K344 + MC33665 + MC33774 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33665-MC33774-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2127108 S32K344 + MC33664 + MC33775 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33664-MC33775-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2127049 S32K344 + MC33665 + MC33775 : RTD 3.0.0 : BMS SDK 1.0.2 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33665-MC33775-RTD-3-0-0-BMS-SDK-1-0-2/ta-p/2127140 S32K144 : RTD-1.0.1 porting for : BCC_S32K144_FreeMASTER :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K144-RTD-1-0-1-porting-for-BCC-S32K144-FreeMASTER/ta-p/2130167
記事全体を表示
MCU : S32K144 AFE : MC33771 RTD : 1.0.1 As we know BCC sample software for MC33771C which is delivered is based on SDK for S32K144 , and uses S32DS-2.2 :-- BCC_S32K144_FreeMASTER I am having a setup , for this combination, using SPI :-- FRDM33771CSPEVB evaluation board  + S32K144 + 14 cell Battery EMULATOR :    S32K144 pins used :-- MOSI :  LPSPI0  : PTB-4 MISO :  LPSPI0  : PTB-3 SCK :    LPSPI0  : PTB-2 CSB :    LPSPI0  : PTB-5 RESET line of MC33771C : PTD-4 FRDM33771CSPEVB pins used :-- https://www.nxp.com/docs/en/user-guide/UM11402.pdf SI of MC33771C : Connects to MOSI of S32K144 : K2-7 SO of MC33771C : Connects to MISO of S32K144 : K2-9 SCK of MC33771C : Connects to PTD-4 of S32K144 : K2-11 CSB :    K2 -5 RESET line of MC33771C : K4 -1 Freemaster uses UART-1 on S32K144 EVB ():-- TX : PTC7 RX : PTC6 I have ported the BCC_S32K144_FreeMASTER  sample code to S32K144 using RTD-1.0.1 & is working fine. This attached code work fine for SPI.  Two sample project i have attached, both are tested and working fine :--- 1> Chip select is controlled by LPSPI. 2> Chip select is controlled manually in user software. Fremaster project is also inside the folder, name of freemaster project is :-- 1> FreeMASTER_project.pmp TPL related part i have not ported & tested because at present i am not having MC33664ATL on S32K144 EVB board & do not have FRDM33771BTPLEVB (MC33771C board with TPL on it). Regards, Dinesh
記事全体を表示
The S32K14x MCU ARM Cortex M4F core processor handles fault exceptions using four handlers.   Handlers UsageFault_Handler() Usage faults are caused by an application that incorrectly uses Cortex M4 processor trying to execute an undefined instruction execute an instruction that makes illegal use of the Execution Program Status Register (EPSR), typically, this processor support only Thumb instruction set and it requires that all branch targets should be indicated as odd numbers, having bit[0] set. perform an illegal load of EXC_RETURN to the PC access a coprocessor if the access is denied or privileged only (configurable in CPACR) make an unaligned memory access execute an SDIV or UDIV instruction with a divisor of 0   The detection of the division by zero fault is disabled by default which means that such an operation returns zero and the fault is not detected. Similarly, the Cortex-M4 processor supports unaligned access for certain instructions. The detection on both the division by zero and the unaligned access (for every instruction) faults can be enabled in Configuration and Control Register (CCR).   BusFault_Handler() Bus faults occur when a bus slave returns an error response while stacking for an exception entry unstacking for an exception return prefetching an instruction during floating-point lazy state preservation Beside these faults listed above, there are also bus faults labeled as Precise and Imprecise. Imprecise bus fault occurs when an application writes to buffered memory region and continues executing subsequent instructions before the actual bus fault is detected. Therefore, at the time the exception rises the program counter doesn’t point to the instruction that has caused the bus fault. For debugging purposes, it is necessary to have “precise” program counter value to know which instruction has caused the fault exception. Imprecise bus fault can be forced to be precise by disabling the write buffer in (ACTLR_DISDEFWBUF = 1). This however might decrease the performance.   Note: The S32K144 MCU has its own system Memory Protection Unit which is implemented on the bus. Therefore, any system MPU violation triggers bus faults.   MemManage_Handler() Typically, these exceptions rise on an attempt to access regions that are protected by the core ARM Cortex M4 Memory Protection Unit. attempt to load or store at a protected location instruction fetch from a protected location stacking/unstacking fault caused by violation of the memory protection protection violation during floating-point lazy state preservation   S32K1xx series implements its own system Memory Protection Unit on the bus and therefore an attempt to access a protected region results in a bus fault exception instead. Nevertheless, the system MPU does not protect access to peripheral registers, and as the attached example code shows, an attempt to fetch instruction from a peripheral memory region causes a MemManage fault exception.   HardFault_Handler() This handler is the only one that has a fixed priority (-1) and is always enabled. If other handlers are disabled (in the SHCSR register), all faults are escalated to this handler. The escalation take place also when a fault occurs during another fault handling execution or while the vector table is read.   Priority of exception fault handlers   The fault exception handlers’ priorities, besides the HardFault handler (fixed priority -1), are configurable in fields PRI_4, PRI_5 and PRI_6 of SHPR1 register. These fields are byte-accessible and Cortex M4 support 255 priority levels, however, S32K14x MCUs support 16 priority levels only. Therefore, priorities are configurable in the four most significant bits of PRI_4, PRI_5 and PRI_6 only, which is similar to other NVIC IPR registers as shown below.   The lower priority number is set, the higher priority. By default, all handlers have priority set to zero.   Status and address registers for fault exceptions Configurable Fault Status Register (CSFR) consists from three status bit fields for Usage Fault (UFSR), Bus Fault (BFSR), and Memory Management Fault (MMFSR) where each bit represents a fault exception.     There are also two auxiliary address registers. If BFARVALID is set in the BFSR register, Bus Fault Address Register (BFAR) holds the memory access location of a precise bus fault. Similarly, if MMARVALID bit is set in MMFSR register, Memory Manage Address Register (MMAR) holds the address of a MemManage fault.   Example code To demonstrate the debugging process, the following exceptions can be forced: attempt to access an unimplemented memory area attempt to write to a non-gated peripheral register write to read only register fetching an instruction from a protected peripheral memory region division be zero unaligned memory access execution of a non-thumb instruction execution of an undefined instruction   When the program enters an exception handler, the stack frame is pushed onto the stack including the program counter value of the fault instruction. In this example, the exception handlers are declared with __attribute__((nake_)) (fault_exceptions.h), no prologue is generated and the program counter is always offset by 6 words (0x14) from the stack pointer that can be read in the handlers using either the debugger (memory view) or a SW pointer. If an application uses Process Stack Pointer (PSP) as well, it is necessary to find out whether the stack pointer comes from Main Stack Pointer (MSP) or PSP, this information is available in the EXC_RETURN value in the link register. Having a precise program counter address, we can find the fault instruction in Disassembly. This applies to all exception except for imprecise bus faults as explained above, imprecise bus faults can be forced to be precise by disabling the Write buffer.   The CSFR register is read to determine which exception has occurred and, if available, the memory access location that has caused the exception.    References Cortex-M4 Devices Generic User Guide Cortex-M4 Technical Reference Manual   Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
記事全体を表示
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 2 AFE MC33775 board connected in TPL 3> Change following macro in mc33775_cfg.h file  to change the numbers of AFE connected in TPL.     RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33775 AFE connected in TPL mode.   =============== MCU Pins used ===========   FRDM665SPIEVB Jumper setting  :---                   K1, K2 & K4 connector of S32J344 EVB :--             K1 on MC33665 & S32K334 evb :--      K2 on MC33665 & S32K334 evb :--    K4 on MC33665 & S32K334 evb :--        ================= EVB Link ==================   https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM665SPIEVB https://www.nxp.com/design/design-center/development-boards-and-designs/RD33775ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172 ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255)   Disable Communication timeout in code :--     ================= Results for TWO AFE ===========================          
記事全体を表示
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 3 AFE MC33774 board connected in TPL 3> Change following macro in mc33774_cfg.h file  to change the numbers of AFE connected in TPL.     RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33774 AFE connected in TPL mode. FRDM665SPIEVB stackable board used for MC33665.     =============== MCU Pins used =========== FRDM665SPIEVB Jumper setting  :---     K1, K2 & K4 connector of S32J344 EVB :--       K1 on MC33665 & S32K334 evb :--  K2 on MC33665 & S32K334 evb :--  K4 on MC33665 & S32K334 evb :--    ================= EVB Link ================== https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM665SPIEVB https://www.nxp.com/design/design-center/development-boards-and-designs/mc33774ata-evaluation-board-with-isolated-daisy-chain-communication:RD33774ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172   ================== Measurement types used in example ===== Periodic measurement is done by 33774 , this is cyclic Other Two : application , sync  need send command to start Application measurement , need send app_capture command twice , and then read the result. Synchronous measurement take out the Primary adc result(VC)and secondary result(VB) .But the VC and VB result comes from different adc. Period measurement start when you send  API "MSR_StartMeasurement" and then 774 will do period measurement automatically periodically :--   Why we need to measure Vc & Vb both :-- ASIL-D ,yes we can measurement VC channel by primary ADC and measurement VB by secondary ADC from hardware VC and VB are come from same point of battery cell. Now 2 ADC compare with each other, that lead to high safety (ASIL D). Primary & Secondary Device temperature reading :-- This API is used for it MC33774_CDD_BCC_SWC_Running_Slot4(). ============= Cell Balancing =========== Cell Balancing method used :-- MC33774 balance will switch between odd channel (1,3,5,7,... 17) and even channel (2,4,6,8,..18) by 500ms period , (250ms for odd and then switch to even 250ms and then odd 250ms...)it is because of IC design and cannot change by software.   MC33774 have lots of balance method  this example uses "timer method ". How to check Balancing is enabled :-- Following function MC33774_CDD_BCC_SWC_Running_Slot5() read the : Balance status & fault registers BAL_SWITCH_STAT0, BAL_SWITCH_STAT1 represent the balancing MOSFET current status.   Measure the voltage drop across the balancing register is the best approach. You will see the voltage drop appears every 250ms if PWM is 100%.  Please check the schematic of the 33774 EVB, find the balancing resistor on which channel balancing is enabled.     ======= How much time to wait to extract the measurements results ======= 240 us is the time of one SCAN Time between each Application measurement sequence. Min App measure time for 16 sample :-- 4.08ms = (16+1) *240 Min 1 SYNC measurement time, for 16 samples = 18 cycle ≈ 18 * (16*240us) ≈ 69 ms ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255) Disable Communication timeout in code :--   ================= Results for FIRST AFE ===========================            
記事全体を表示
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 2 AFE MC33775 board connected in TPL 3> Change following macro in mc33775_cfg.h file  to change the numbers of AFE connected in TPL.   RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33775 AFE connected in TPL mode.   =============== MCU Pins used =========== TPL1-TX :-- TPL1TXCSB  --> PTC6/LPSPI0_PCS1 TPL1TXSCLK --> TPL12TXCLK --> PTE1/LPSPI0_SCK    TPL1TXDATA --> TPL12TXDATA --> PTE2/LPSPI0_SOUT    TPL1-RX :-- TPL1RXCSB  --> PTB17/LPSPI1_PCS3 TPL1RXCLK  --> PTB14/LPSPI1_SCK TPL1RXDATA --> PTB15/LPSPI1_SIN     ================= EVB Link ================== https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/evaluation-board-for-mc33664atl-isolated-network-high-speed-transceiver:FRDMDUALK3664EVB https://www.nxp.com/design/design-center/development-boards-and-designs/RD33775ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172   ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255) Disable Communication timeout in code :--   ================= Results for FIRST AFE ===========================          
記事全体を表示
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 2 AFE MC33774 board connected in TPL 3> Change following macro in mc33774_cfg.h file  to change the numbers of AFE connected in TPL. RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33774 AFE connected in TPL mode.         =============== MCU Pins used =========== TPL1-TX :-- TPL1TXCSB  --> PTC6/LPSPI0_PCS1 TPL1TXSCLK --> TPL12TXCLK --> PTE1/LPSPI0_SCK    TPL1TXDATA --> TPL12TXDATA --> PTE2/LPSPI0_SOUT    TPL1-RX :-- TPL1RXCSB  --> PTB17/LPSPI1_PCS3 TPL1RXCLK  --> PTB14/LPSPI1_SCK TPL1RXDATA --> PTB15/LPSPI1_SIN     ================= EVB Link ================== https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/evaluation-board-for-mc33664atl-isolated-network-high-speed-transceiver:FRDMDUALK3664EVB https://www.nxp.com/design/design-center/development-boards-and-designs/mc33774ata-evaluation-board-with-isolated-daisy-chain-communication:RD33774ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172   ================== Measurement types used in example ===== Periodic measurement is done by 33774 , this is cyclic Other Two : application , sync  need send command to start Application measurement , need send app_capture command twice , and then read the result. Synchronous measurement take out the Primary adc result(VC)and secondary result(VB) .But the VC and VB result comes from different adc. Period measurement start when you send  API "MSR_StartMeasurement" and then 774 will do period measurement automatically periodically :--   Why we need to measure Vc & Vb both :-- ASIL-D ,yes we can measurement VC channel by primary ADC and measurement VB by secondary ADC from hardware VC and VB are come from same point of battery cell. Now 2 ADC compare with each other, that lead to high safety (ASIL D). Primary & Secondary Device temperature reading :-- This API is used for it MC33774_CDD_BCC_SWC_Running_Slot4(). ============= Cell Balancing =========== Cell Balancing method used :-- MC33774 balance will switch between odd channel (1,3,5,7,... 17) and even channel (2,4,6,8,..18) by 500ms period , (250ms for odd and then switch to even 250ms and then odd 250ms...)it is because of IC design and cannot change by software.   MC33774 have lots of balance method  this example uses "timer method ". How to check Balancing is enabled :-- Following function MC33774_CDD_BCC_SWC_Running_Slot5() read the : Balance status & fault registers BAL_SWITCH_STAT0, BAL_SWITCH_STAT1 represent the balancing MOSFET current status.   Measure the voltage drop across the balancing register is the best approach. You will see the voltage drop appears every 250ms if PWM is 100%.  Please check the schematic of the 33774 EVB, find the balancing resistor on which channel balancing is enabled.     ======= How much time to wait to extract the measurements results ======= 240 us is the time of one SCAN Time between each Application measurement sequence. Min App measure time for 16 sample :-- 4.08ms = (16+1) *240 Min 1 SYNC measurement time, for 16 samples = 18 cycle ≈ 18 * (16*240us) ≈ 69 ms ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255) Disable Communication timeout in code :--   ================= Results for FIRST AFE =========================== Application Measurement : Cell voltage result :-- SYNC measurement : VC, VB same for both primary & Secondary  measure :--      
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the HSE IP Driver for the S32K3xx MCU. This DEMO make use of SHE based keys & the RAM keys.  Step-1> Uncomment this MACRO to program the MASTER_ECU_KEY & BOOT_MAC_KEY #define FORMAT_HSE_KEY_CATALOG (1U) Step-2> Then comment the above mentioned MACRO to test the demo. Step-3> End of the DEMO in Switch case HSE_ERASE : keys are erased. HSE_EraseKeys(); SHE based secured boot :-- This demo uses the SHE based secured boot. You can test this after performing step-1. Once SHE is enabled code will be stuck at this point, after this issue an RESET.    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
記事全体を表示
[S32K3 tool part]:How to flexibly debug elf files without source code  1.Doc Introduction When supporting customers with the MCU software technical issues, we often encounter situations where customers are unable to provide the source code of problematic projects due to company policies. At most, they can provide the elf files of problematic projects. This involves how to make good use of elf to achieve flexible debugging goals. Elf file is a binary file format that contains program code, data, symbol tables, segment tables, and other information. When debugging elf, you cannot see the source code, but you can see the function name corresponding to the assembly address. At this time, debugging can still relatively know the location. However, the problem is that it is not possible to freely modify and generate new files like modifying the source code. Is it feasible to make specific modifications to elf files to achieve the purpose of functional testing? This article will provide testing methods for skipping specific positions, erasing functions, replacing code, concatenating functions, etc. on an existing elf, to achieve skipping of code in certain positions of elf, or not executing it at any time, creating a new area to concatenate other functional functions, and then modifying the original call position to forcibly insert test function code. The testing platform for this article is S32K344 and RTD500.        Fig 1 2. Function implementation    Fig 1 is an elf file of the original function. The function is to call three functions after startup: Fun1, Fun2, and Fun3 Fun1: Flashing Red Light Fun2: Flashing green light Fun3: Flashing Blue Light The main functions that need to be implemented in this article are as follows: (1) Fun2 function skipped There are two types of function skipping here: When debugging, start from Fun2 and modify the PC to jump to Fun3 Do not run Fun2 even when powered on, simply erase the Fun2 value from the main as nop        Fig 2    (2)Add Fun4, modify Fun2 call in Main to jump to Fun4        This involves inserting Fun4 code into an empty flash address, modifying the jump asm code of Fun2 to jump to Fun4   Fig 3 2.1 Code and Tool preparation Hardware Platform: S32K344-EVB Software: RTD500, S32DS3.5, JFLASH, PE Multilink(built-in to EVB), Lauterbach  JFLASH tool download link:https://www.segger.com/downloads/jlink/  Create a simple led blinking project that can be based on RTD's existing Siul_2Dio_ip_Instance_S32K344 project, add three LED light pins, and construct three functions for flashing red, green, and blue lights respectively. Call the three functions sequentially in main. Generate elf backup when testing is working. 2.2 Implementation of elf modification function: Fun2 function skipped    Here is the specific implementation method for Figure 2: the PC crosses Fun2 and replaces Fun2 with asm nop 2.2.1 PC Crossing Fun2 In the Main function, call the assembly position breakpoint of Fun2, directly modify PC to the value of Fun3 address+1, and then run to skip Fun2. As shown in Figure 4, it has already been run to Fun2, but has not yet entered the function body of Fun2. Simply change the pointer entry that was originally intended to call Func2 to 0X4027B4+1, which is the function entry of Fun3. As can be seen, after modifying the PC, press enter and step into the Fun3 function body. If you modify the starting point of Fun2's function body to jump from PC to Fun3, both sides of Fun3 will run from the main function as a whole   Fig 4 Fig 5 2.2.2 Replace Fun2 with NOP The situation of directly using debug to jump to PC above bypasses Fun2. Although Fun2 can be skipped in testing, it should be noted that when downloading the code, it will actually run the code before entering debug. If some tests want to start from POR without running Fun2, then it is necessary to directly erase the location code of the original elf Fun2 call, and the commonly used method can be replaced with harmless nop instructions. The assembly hexadecimal value of the nop instruction is 00 BF, as shown in the following figure:       Fig 6 With the target modification value, the following is to find the call address of Fun2 in elf main and replace the corresponding 4 bytes with 00BF00BF. From the original elf file, we can see that the data location of the call Fun2 is 4 bytes starting from the absolute address 0X0040280E, use the JFLASH tool in the Segger JLINK driver to open the original elf file, modify the data of the 4 bytes starting address 0X0040280E from FFF7ABFF to 00BF00BF, save the modified data as an srec file, and then call the srec file in the temporary project to run the modified code. The following figure shows the modification process Fig 7 The modified debug result is as follows: Fig 8 As can be seen, the assembly that jumped from the 0X40280e area to Fun2 has now become a nop instruction. At this point, running at full speed will ignore fun2 and proceed in sequence. Whether debugging or after powering on, Fun2 calls have been completely erased from the overall runtime sequence. Of course, since manually modified elf cannot be directly saved as an elf file through JFLASH, choosing to save it as an Srec file will result in losing the symbol table when debugging again. When using elf in the early stage, remember the absolute addresses of several functions that need to be used. 2.3 Elf modification function implementation: Fun4 replaces Fun2 entrance     In the above content, we skip or insert nop directly at the main Fun2 call position, can we call another function body in the original Fun2 for testing, achieving the same area but with other functions? It's possible. There are also two types here: one is to destroy the original Fun2 function body position and directly replace the code content of the function body, of course, this is limited by the size of the original Fun2 function body. On the other hand, keep the original Fun2 for future use. You can start another function Fun4 at other blank addresses in flash, and then change the code that calls Fun2 in main to call Fun4 to achieve seamless docking of Fun1->Fun4->Fun3 operations.     This article mainly uses to create a new function at a specific absolute address in the flash blank space. Of course, attention should be paid to the original elf map situation to ensure that the blank area is sufficient for use. It is best for this new function to be self-contained and independent of other functions to avoid calling bias. If it is necessary to call other function bodies, it is necessary to set the addresses of other dependent functions in the sample project to be consistent when constructing this new function.     Here, we will create a S32DS project and allocate a flash area in the linkfile to store the newly created Fun4. The Fun4 function is to achieve alternating blink green and red led.      2.3.1 linkfile modification MEMORY { int_pflash : ORIGIN = 0x00400000, LENGTH = 0x00010000 /* 4096KB - 176KB (sBAF + HSE)*/ int_pflash_user : ORIGIN = 0x00410000, LENGTH = 0x003C4000 int_dflash : ORIGIN = 0x10000000, LENGTH = 0x00020000 /* 128KB */ int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00010000 /* 64KB */ int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x0001F000 /* 124KB */ int_stack_dtcm : ORIGIN = 0x2001F000, LENGTH = 0x00001000 /* 4KB */ int_sram : ORIGIN = 0x20400000, LENGTH = 0x0002FF00 /* 184KB, needs to include int_sram_fls_rsv */ int_sram_fls_rsv : ORIGIN = 0x2042FF00, LENGTH = 0x00000100 int_sram_no_cacheable : ORIGIN = 0x20430000, LENGTH = 0x0000FF00 /* 64KB, needs to include int_sram_results */ int_sram_results : ORIGIN = 0x2043FF00, LENGTH = 0x00000100 int_sram_shareable : ORIGIN = 0x20440000, LENGTH = 0x00004000 /* 16KB */ ram_rsvd2 : ORIGIN = 0x20444000, LENGTH = 0 /* End of SRAM */ } SECTIONS { .FUNC4 : { *(.func4) } > int_pflash_user … } 2.3.2 Fun4 function code The function body code is constructed as follows, purely logical, without relying on any external functions or variables. __attribute__((section (".func4"))) void Func4(void) { uint8 count1 = 0U; static volatile uint32 DelayTimer = 0; volatile uint8 *red_addr_byte = (volatile uint8 *)0x4029131e; volatile uint8 *green_addr_byte = (volatile uint8 *)0x4029131d; volatile uint8 *blue_addr_byte = (volatile uint8 *)0x4029131c; //RED: GPIO29, 0x4029131e //green: GPIO30, 0x4029131d //blue: GPIO31, 0x4029131c while (count1++ < 6) { *red_addr_byte = 1; *green_addr_byte = 0; while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; *red_addr_byte = 0; *green_addr_byte = 1; while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; /* Siul2_Dio_Ip_WritePin(LED_RED_PORT, LED_RED_PIN, 1U); Siul2_Dio_Ip_WritePin(LED_GREEN_PORT, LED_GREEN_PIN, 0U); while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; Siul2_Dio_Ip_WritePin(LED_RED_PORT, LED_RED_PIN, 0U); Siul2_Dio_Ip_WritePin(LED_GREEN_PORT, LED_GREEN_PIN, 1U); while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; */ } *red_addr_byte = 0; *green_addr_byte = 0; } Here we know, this Fun4 address starts from flash 0x00410000 and generates elf after compiling the project with the above function. 2.3.3 Separate Fun4 function body into independent files Open the elf file with newly created Fun4 using JFLASH and delete all code above 0x00410000. Method: JFLASH->Edit->Delete range:   Fig 9 After deletion, obtain a file containing only Fun4 code and save it as the ElfdebugSource_S32K344_STD500_delete.srec file. 2.3.4 Merge the Fun4 function body into the corresponding Srec of the original elf      Open the Srec corresponding to the original elf and the Fun4 Srec file that was just separated using JFLASH. Choosing to merge two files will automatically concatenate Fun4 files with different addresses into the original Srec file and save them as a separate file.   Fig 10 Fig 11 2.3.5 Modify the original Fun2 calling in main to Fun4 calling Modify code from: 0040280e: ff f7 ab ff   bl      0x402768 <Func2> To: 0040280e: 0d f0 f7 fb   bl      0x410000 Among them, 0x410000 is the absolute address of Fun4. Fig12 Modify the Srec file that has already added Fun4 to start with 0040280e with a value of 0d f0 f7 fb, then save it as a new Srec and debug it. It can be found that the running order of main has changed to Fun1->Fun4->Fun3 Skipped Fun2 while also running the newly integrated Fun4. The above image was run in the S32DS+PE Multilink environment. At this time, due to the operation of the Srec file, the symbol table information for elf was no longer included, but the functionality was successful. 2.3 Lauderbach synchronously loads the original elf symbol table Due to a series of grafting modifications on the original elf and saving it as SREC, the symbol table was lost. So if you still want to view the symbol table of unmodified areas, you can use the Laubach tool. After attaching the code, you can load the original elf file in trace32 by following the command: Data.LOAD.Elf  C:\S32DS35_RTD500\elfdebug\elftest\Debug_FLASH\Elfdebug_S32K344_RTD500.elf /nocode As can be seen, the original part with Fun2 symbol table is only missing due to modifications, but other call header symbol tables still exist. This is also convenient for code execution and reading.     Fig 13 Fig 14 Fig 15 3. Knowledge points Here we share the corresponding hexadecimal data operations for BL addr jumps. The previous one was generated directly using S32DS 0040280e: 0d f0 f7 fb   bl      0x410000 It can be known that the value corresponding to the bl 0x410000 instruction is 0d f0 f7 fb So how is the value of 0d f0 f7 fb calculated? This requires reference to ARM's architecture document: DDI0403E_d_armv7m_arm.pdf For the situation corresponding to the BL jump thumb2 instruction: Fig 16 For BL, it is a long jump, which is actually composed of two jump instructions, Thumb instructions are all 2 bytes long, and BL consists of 2 jump instructions that make up 4 bytes. The 0-11 bits represent an 11 bit address, with the following specific meanings: The 11th digit is 0, representing a high offset The 11th digit is 1, representing a low offset The calculation formula is as follows: offset = (target address- source address -4) & 0x007fffff high = offset >> 12(decimalism) low = ( offset & 0x00000fff )>>1  machineCode = ((0xF800 | low) << 16) | (0xF000 | high) Let's calculate what we use here: bl      0x410000 Offset=(Destination Address - Source Address -4)&0x007fffff = (0x410000-0x40280e-4)& 0x007fffff =D7EE High=offset>>12 (decimal)=D low = ( offset & 0x00000fff )>>1  = 3F7 machineCode = ((0xF800 | low) << 16) | (0xF000 | high) =((0xF800 | 3F7) << 16) | (0xF000 | D) =0XFBF7F00D This corresponds to a low to high: 0D 00 7F FB This is also the source of the following binary modulation instructions: 0040280e: 0d f0 f7 fb   bl      0x410000    
記事全体を表示
******************************************************************************** The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - It configures FlexCAN0 module and its transceiver (TJA1153). - MB0 is used to transmit CANFD std. ID - MB1 is configured to receive any std. ID - Callback function is used as well to handle TX and RX process in MBs. Received ID is echoed back. - setupCanXCVR function is called to Init TJA1153 connected to FlexCAN0 on the board. It expects transceiver in Vanilla state and set TPL to pass all std and ext ID and do not block any message coming from bus. Finally leaving configuration mode without writing to non-volatile memory nor locking the transceiver. * * ------------------------------------------------------------------------------ * Test HW: S32K3X8EVB-Q289 rev B2 * MCU: P32K358HVS 0P14E * Compiler: S32DS.ARM.3.5 * SDK release: S32K3_RTD_4.0.0_D2311 / S32K3_RTD_5_0_0_D2408 * Debugger: Lauterbach * Target: internal_FLASH * ********************************************************************************
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the Bootloader Jump to Application.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************   Jump is decided based on the boot_header, size we use to jump to the RESET handler:--   Cortex M-7 Interrupt vector table, RESET handler is 4 byte offset from starting of vector table :--   // Reset_Handler+1  --> required in IVT, to avoid hard fault As per Arm®v7-M Architecture Reference Manual  --> DDI0403E_e_armv7m_arm.pdf         How to burn elf file of both application & bootloader code :--  
記事全体を表示
[RTD400 LLD]K344 Center Aligned PWM Trigger ADC BCTU 1. Abstract     Not long ago, a customer's actual project needed to implement the high-level center point of the center-aligned PWM on the S32K3XX to trigger the ADC BCTU multi-channel sampling. This function requires the use of EMIOS, ADC, and BCTU. At the beginning, the customer was always unable to achieve the trigger at the center point of the PWM, and the trigger position was wrong. Later, After we give the explanation and analysis of the principles of the K3 related modules to the customer, as well as the guidance of the actual code configuration test, and the customer also achieved the required function. For the convenience of testing, PIT and UART printf functions are also added here. So here is a summary of the specific situation of this function, so that other customers who encounter similar functional requirements in the future can have a reference and can quickly build it. The requirements are as shown in the figure below. In the up-down counting mode, the center-aligned PWM is output, and the trigger sampling of the ADC BTCU LIST is realized at the center point of the high level. This article will implement 1KHZ center-aligned PWM, 50% duty cycle, and high-level center point to achieve ADC BTCU LIST sampling on the official S32K344-EVB board, based on the RTD400 LLD version.   Fig 1 2. Center-aligned PWM center point trigger ADC principle       Regarding the principle, there is no suspense about ADC. You can directly refer to the previous article on ADC software and hardware triggering: [RTD400 LLD]K344 ADC SW+HW trigger This is the structure shown in Figure 2. After configuring ADC, BCTU and select the triggered EMIOS channel. When the relevant flag of EMIOS is generated, BCTU will be triggered. After the watermark is reached, a notification will be generated to store all LIST ADC channel values ​​in the buffer, and then the ADC value can be printed out for easy viewing according to the situation.    Fig 2 In the current working condition, the logic that needs to be concerned about is mainly: how to generate center-aligned PWM, how to generate a flag at the high-level center point, and use this flag to trigger BTCU sampling. 2.1 How to generate center-aligned PWM      First, let’s take a look at the channel status of EMIOS and the channel status that supports center-aligned PWM.  Fig 3 The center-aligned PWM mode is: OPWMCB As shown in Figure 1, we can see that the counter count mode in this mode is up and down. Let's take a look at the channel types that support OPWMCB. We can see that there is only type G.   Fig 4 So, what are the channels supported by Type G? See the figure below:  Fig 5 The mystery is solved. Only CH1-CH7 of eMIOS supports center-aligned PWM. Well, then a new question arises. Can this mode directly generate a trigger signal at the center point of the PWM high level to trigger the ADC BCTU sampling? Answer: No! The reason can be seen from Figure 1. In this PWM mode, there are two trigger flags generated when the up and down count comparison is completed. Therefore, if this mode channel is used to directly trigger ADC sampling, two triggers will be generated in one cycle, and both are on the edge of PWM. Since OPWMCB cannot directly generate a trigger at the center point of PWM, how to achieve it? In addition, open a dedicated channel, and the clock source is the same as OPWMCB, but that channel only counts to generate trigger flags and does not output any waveform. 2.2 How to generate PWM center point trigger flag   Key information: OPWMCB simultaneous clock source, only counting mode, or up and down MCB mode, only one channel is satisfied: ADC CH0, counter bus type also needs to be selected as counter_bus_B       Fig 6 Let's take a look at the trigger flag of MCB:  Fig 7 As you can see, it is perfect. The trigger mark is at the top of the upward and downward counting, which is exactly the center point of the high level of the same source PWM. So, here, the specific channel arrangement has been determined in principle, two channels: EMIOS0_CH0 MCB mode pure counting and triggering the generation of flags to trigger ADC sampling; EMIOS0_CH1-CH7 is OPWMCB mode, simply outputting center-aligned PWM. 3. Software configuration and implementation       The software uses the S32K3 RTD400 version, and other versions have similar configurations! 3.1 Demo CT  module configuration First, you need to prepare a K344 demo, and then configure the pins, clocks, and peripheral modules. The following will explain the configurations. The modules used are: 2 GPIOs, ADC, BCTU, EMIOS clock, EMIOS PWM, LPUART for printing logs, PIT for timed printing, Trgmux is configured but not used in this article, so I won't talk about it!      3.1.1 Pin configuation       The pins used are as follows:  Fig 8 The two GPIOs are used to toggle in BCTU trigger notification and BCTU watermark notification respectively, to test the waveform positioning. ADC1_s10 pin is used for ADC1, but this article mainly uses BCTU to combine ADC0. ADC0 does not add specific external pins, but uses internal signals. LPUART is used for printing, and EMIOS0_CH1 is used to generate center-aligned PWM waveforms. 3.1.2 Clock configuration      The clocks that need to be paid attention to here are: ADC clock, EMIOS clock, UART clock, and PIT clock.  Fig 9 These clocks will be used later when configuring specific timing periods and baud rates. 3.1.3 Peripheral configuration       The peripherals used mainly include the following modules:  Fig 10 (1)Adc_Sar_Ip The configuration of the ADC0 module uses the one shot mode, that is, one conversion is generated after one trigger. In this way, the timer EMIOS channel can be used to generate trigger conditions to trigger a conversion. Pre-sampling is enabled to prevent the residual charge of the sampled value of the previous channel from affecting the result of the current channel and causing deviation of the ADC value. The trigger mode uses BCTU. For the configuration of Adc prescaler value and calibration prescale, the frequency division requirements in RM need to be met. The final configuration is as follows:  Fig 11    Fig 12 (2)Bctu_Ip The configuration of Bctu_Ip needs to select the right EMIOS channel to use. From the above principle, we can know that EMIOS0_CH0 is used, and then LIST mode is adopted. For ADC0, three internal channels are currently added to the LIST: BANDGAP, VREFL, VREFH. The specific configuration is as follows:  Fig 13   Fig 14 (3)Emios_Mcl_Ip Here we need to consider the PWM cycle that needs to be generated. The goal is to generate a 1Khz center-aligned PWM, so the EMIOS mode is the MCB up-down counting mode. The clock cycle formula for MCB is: (2 x AS1) – 2. So for the EMIOS0 clock source of 160Mhz, what is the corresponding 1KHZ counter? First do 160 divide to get 1Mhz, and then calculate according to (2 x AS1) – 2: (2 x AS1) – 2 = 1Mhz/1KHZ=>AS1=1000/2 +1= 501. The configuration is as follows:  Fig 15 (3)Emios_Pwm The previous principle analysis shows that the PWM uses the OPWMCB center-aligned mode PWM, the clock comes from the counter bus B of EMIOS CH0, then the period is 1khz, and the duty cycle is 50%. The specific configuration is as follows:  Fig 16 (4)Lpuart_Uart Configure UART6 clock baud rate to 115200.   Fig 17 (5)Pit   Fig 18 (6)IntCtrl_Ip The interrupt configuration is as follows, and it can actually be configured via code.  Fig 19 3.2 Main code situation After the configuration is completed, the output of the center PWM and the sampling of the ADC BCTU can be realized by calling the following code in main. #include "Clock_Ip.h" #include "IntCtrl_Ip.h" #include "Adc_Sar_Ip.h" #include "Bctu_Ip.h" #include "Siul2_Port_Ip.h" #include "Pit_Ip.h" #include "Siul2_Dio_Ip.h" #include "Trgmux_Ip.h" #include "Lpuart_Uart_Ip.h" #include "Lpuart_Uart_Ip_Irq.h" #include "string.h" #include "stdio.h" #include "retarget.h" #include "Emios_Mcl_Ip.h" #include "Emios_Pwm_Ip.h" /* PIT instance used - 0 */ #define PIT_INST_0 0U /* PIT Channel used - 0 */ #define CH_0 0U /* PIT time-out period - equivalent to 1s */ #define PIT_PERIOD 40000000 static volatile uint8 toggleLed = 0U; #ifdef ADC_3V3_VREF_SELECTED #define ADC_BANDGAP 5980U /* Vbandgap ~ 1.2V on 14 bits resolution, 3.3V VrefH */ #else #define ADC_BANDGAP 3932U /* Vbandgap ~ 1.2V on 14 bits resolution, 5V VrefH */ #endif #define ADC_SAR_USED_CH 48U /* Internal Bandgap Channel */ #define BCTU_USED_SINGLE_TRIG_IDX 0U #define BCTU_USED_FIFO_IDX 0U #define BCTU_FIFO_WATERMARK 3U #define ADC_TOLERANCE(x,y) (((x > y) ? (x - y) : (y - x)) > 200U) /* Check that the data is within tolerated range */ #define LED_Q172_PIN 13u #define LED_Q172_PORT PTA_H_HALF #define GPIO_PTA2_PIN 2u #define GPIO_PTA2_PORT PTA_L_HALF #define EMIOS_INST0 0U volatile int exit_code = 0; volatile boolean notif_triggered = FALSE; volatile boolean notif_triggered1 = FALSE; volatile uint16 data; volatile uint16 data1; volatile uint16 data_bctu[3]; #define UART_LPUART_INTERNAL_CHANNEL 6 #define WELCOME_MSG_1 "Hello, This message is sent via Uart!\r\n" volatile Lpuart_Uart_Ip_StatusType lpuartStatus = LPUART_UART_IP_STATUS_ERROR; uint32 remainingBytes; uint32 T_timeout = 0xFFFFFF; uint8* pBuffer; extern void Adc_Sar_0_Isr(void); extern void Bctu_0_Isr(void); extern void Adc_Sar_1_Isr(void); void AdcEndOfChainNotif(void) { notif_triggered = TRUE; data = Adc_Sar_Ip_GetConvData(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_USED_CH); /* Checks the measured ADC data conversion */ } void AdcEndOfChainNotif1(void) { notif_triggered1 = TRUE; data1 = Adc_Sar_Ip_GetConvData(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, 34); /* Checks the measured ADC data conversion */ } void Pit0ch0Notification(void) { toggleLed = 1U; } void BctuWatermarkNotif(void) { uint8 idx; Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 1U); notif_triggered = TRUE; for (idx = 0u; idx < BCTU_FIFO_WATERMARK; idx++) { data_bctu[idx] = Bctu_Ip_GetFifoData(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, BCTU_USED_FIFO_IDX); } Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); } void BcutTriggerNotif() { Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 1U); Siul2_Dio_Ip_WritePin(LED_Q172_PORT, LED_Q172_PIN, 0U); } void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } int main(void) { StatusType status; uint8 Index; Clock_Ip_StatusType clockStatus; /* Initialize and configure drivers */ clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); while (clockStatus != CLOCK_IP_SUCCESS) { clockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); } Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); #if 1 Bctu_Ip_Init(BCTUHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &BctuHwUnit_0_BOARD_INITPERIPHERALS); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_0_BOARD_InitPeripherals); while (status != E_OK); status = (StatusType) Adc_Sar_Ip_Init(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, &AdcHwUnit_1_BOARD_InitPeripherals); while (status != E_OK); /* set PIT 0 interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); IntCtrl_Ip_EnableIrq(PIT0_IRQn); /* Install and enable interrupt handlers */ IntCtrl_Ip_InstallHandler(ADC0_IRQn, Adc_Sar_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(BCTU_IRQn, Bctu_0_Isr, NULL_PTR); IntCtrl_Ip_InstallHandler(ADC1_IRQn, Adc_Sar_1_Isr, NULL_PTR); IntCtrl_Ip_EnableIrq(ADC0_IRQn); IntCtrl_Ip_EnableIrq(BCTU_IRQn); IntCtrl_Ip_EnableIrq(ADC1_IRQn); // IntCtrl_Ip_EnableIrq(EMIOS0_5_IRQn); /* Call Calibration function multiple times, to mitigate instability of board source */ for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } for(Index = 0; Index <= 5; Index++) { status = (StatusType) Adc_Sar_Ip_DoCalibration(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE); if(status == E_OK) { break; } } Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); Adc_Sar_Ip_EnableNotifications(ADCHWUNIT_1_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_NOTIF_FLAG_NORMAL_ENDCHAIN | ADC_SAR_IP_NOTIF_FLAG_INJECTED_ENDCHAIN); /* Start a SW triggered normal conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_NORMAL); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; /* Start a SW triggered injected conversion on ADC_SAR */ Adc_Sar_Ip_StartConversion(ADCHWUNIT_0_BOARD_INITPERIPHERALS_INSTANCE, ADC_SAR_IP_CONV_CHAIN_INJECTED); /* Wait for the notification to be triggered and read the data */ while (notif_triggered != TRUE); notif_triggered = FALSE; #endif /* Initialize PIT instance 0 - Channel 0 */ Pit_Ip_Init(PIT_INST_0, &PIT_0_InitConfig_PB_BOARD_InitPeripherals); /* Initialize channel 0 */ Pit_Ip_InitChannel(PIT_INST_0, PIT_0_CH_0); /* Enable channel interrupt PIT_0 - CH_0 */ Pit_Ip_EnableChannelInterrupt(PIT_INST_0, CH_0); /* Start channel CH_0 */ Pit_Ip_StartChannel(PIT_INST_0, CH_0, PIT_PERIOD); // Trgmux_Ip_Init(&Trgmux_Ip_xTrgmuxInitPB);// Lpuart_Uart_Ip_Init(UART_LPUART_INTERNAL_CHANNEL, &Lpuart_Uart_Ip_xHwConfigPB_6_BOARD_INITPERIPHERALS); Emios_Mcl_Ip_Init(EMIOS_INST0, &Emios_Mcl_Ip_0_Config_BOARD_INITPERIPHERALS); Emios_Pwm_Ip_InitChannel(EMIOS_PWM_IP_BOARD_INITPERIPHERALS_I0_CH1_CFG, &Emios_Pwm_Ip_BOARD_InitPeripherals_I0_Ch1); printf("S32K344 PIT TRIGMUX ADC demo RTD400.\r\n"); /* Uart_AsyncSend transmit data */ lpuartStatus = Lpuart_Uart_Ip_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *) WELCOME_MSG_1, strlen(WELCOME_MSG_1)); /* Check for no on-going transmission */ do { lpuartStatus = Lpuart_Uart_Ip_GetTransmitStatus(UART_LPUART_INTERNAL_CHANNEL, &remainingBytes); } while (LPUART_UART_IP_STATUS_BUSY == lpuartStatus && 0 < T_timeout--); Siul2_Dio_Ip_WritePin(GPIO_PTA2_PORT, GPIO_PTA2_PIN, 0U); while(1) { #if 1 if( toggleLed == 1) { toggleLed = 0; printf("ADC0_bandgap ch48 data_bctu = %d .\r\n", data_bctu[0]); printf("ADC0_vrefl ch54 data_bctu = %d .\r\n", data_bctu[1]); printf("ADC0_vrefh ch55 data_bctu = %d .\r\n", data_bctu[2]); } #endif } return exit_code; } 3.3 Test result    The test results include two parts: the printed results show the ADC sampling value, and the relationship between the PWM output and the BCTU trigger position. The printed results are as follows, and you can see that the values ​​of the three different ADC channels are correct:  Fig 20 PWM wave test result is: Ch1:PTB13 PWM Ch2:PTA29 BCTU trigger notification Ch3: PTA2 BCTU watermark notification   Fig 21 From the figure, we can see that the first BCTU trigger is at the center point of the PWM high level, and the BCTU watermark notification is used to store data after the ADC sampling is triggered three times. Here is another waveform to view the PWM cycle:  Fig 22 It can be seen that the PWM period is 1Khz, the duty cycle is 50%, and the first trigger of BCTU is at the center of the PWM high pulse. 4. Summary and trip description Through the above configuration, the RTD400 LLD method was finally used on the S32K344-EVB to implement a 1Khz, 50% duty cycle center-aligned PWM, and the high pulse center position triggered the ADC BCTU LIST acquisition. The trip encountered were my own configuration problems. At the beginning, I mistakenly thought that the watermark configuration value was consistent with the number of LIST channels. In fact, the watermark trigger is triggered only when the watermark value is exceeded. Therefore, if it is a 3-channel LIST, the watermark needs to be configured as 2, not 3. If it is 3, the test waveform is as follows: Fig 23 As you can see, the watermark notification is actually generated after it is triggered 4 times. Therefore, remember to match the FIFO number of the watermark. Attachment: 1. S32K344_centerPWM1k_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip Center PWM triggered BCTU LIST   2.S32K344_CPWM1k_TRIGMUX_BCTUHWLIST_EMIOSch4_ADC_printf_RTD400.zip PWM emios0_ch4 falling edge trigger the BCTU, for the comment situation.   3. Another method of center trigger: MCB_Counter up. Emios0_CH0 as the counter bus EMIOS0_CH1 as the PWM output EMIOS0_CH2 as the center trigger, but no PWM output, OPWMB S32K344_NCPWM1k1_TRIGMUX_BCTUHWLIST_EMIOS_ADC_printf_RTD400.zip
記事全体を表示
*********************************************************************************** * Detailed Description: * C40_Ip driver is moved to SRAM in files: C40_Ip.h, SchM_Mem_43_INFLS.h * The function that launches the C40_Ip APIs from main() is also placed in the SRAM. * Check the addresses of the APIs in the .map file. * ------------------------------------------------------------------------------ * Test HW: : S32K312EVB-Q172 * MCU: : S32K312 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * Autosar Conf.Variant : * SW Version : S32DS 3.5, RTD 5.0.0 * Build Version : S32K3_RTD_5_0_0_D2408_ASR_REL_4_7_REV_0000_20241002 ***********************************************************************************
記事全体を表示
******************************************************************************************** * Test HW: S32K312 EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: Internal_FLASH ******************************************************************************************** The objective of this demo application is to generate an interrupt by comparing DAC internal reference voltage against any analog input which is connected in analog mux input channels(IN0 : IN7) and wakes the MCU from sleep(standby) mode.  In this demo code,            1)LPCMP0 is used - DAC output is  given to comparator minus (INM) and                                                      AIN2 is given to comparator plus (INP).                From S32K3 RM, highlighted the channels used for reference.                                                                     Green color represents DAC, Pink color represents AIN2 which is selected from PMUX           2) From S32K RM,                "Compares two analog input voltages applied to INP and INM,                   COUT_RAW is high when the INP input voltage is greater than the INM input voltage,                   COUT_RAW is low when the INP input voltage is less than the INM input voltage"                So in this demo code,                RED LED is ON , if AIN2 Voltage > DAC Internal reference voltage(COUT is HIGH)                GREEN LED is ON, If AIN2 Voltage < DAC Internal reference voltage (COUT is LOW)   MODULES USED:   MODIFICATIONS IN LPCMP MODULE:       MODIFICATIONS IN INTCTRL_IP MODULE:     MODIFICATIONS IN WKPU MODULE:      From S32K3 RM, Analog comparator has used Channel 2 for wakeup.  Modifications in the "Cmp_Ip_IrqHandler" function in "Cmp_IP.c" source file: NOTE: Not sure how it got missed or from where to get COUT status, so added manually to get COUT status from CSR register in the Cmp_Ip_Irqhandler once code generation is completed.   PIN SELECTION DETAILS: HOW TO TEST?  a) Connect jumper wire at the PTC2 in the EVB as highlighted in EVB below. b) RED LED ON -> Jumper wire connects to 5V      GREEN LED ON-> Jumper wire connects to GND c) MCU enters STANDBY once SW5 is pressed and it wakes up if the jumper wire is disconnected from either 5V or GND. NOTE: In this demo, since jumper wire is used instead of button/ADC, due to high impendence state, LED will be toggling if jumper wire is not connected to GND/5V. Connect male jumper wire at PTC2 Thanks & regards, Krishnakumar V
記事全体を表示
******************************************************************************************** * Test HW: S32K312 EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************************** The objective of this demo application is to generate an interrupt by comparing DAC internal reference voltage against any analog input which is connected in analog mux input channels(IN0 : IN7). In this demo code,            1)LPCMP0 is used - DAC output is  given to comparator minus (INM) and                                                      AIN2 is given to comparator plus (INP).                From S32K3 RM, highlighted the channels used for reference.                Green color represents DAC, Pink color represents AIN2 which is selected from PMUX          2) From S32K RM,                "Compares two analog input voltages applied to INP and INM,                   COUT_RAW is high when the INP input voltage is greater than the INM input voltage,                   COUT_RAW is low when the INP input voltage is less than the INM input voltage"                So in this demo code,                RED LED is ON , if AIN2 Voltage > DAC Internal reference voltage(COUT is HIGH)                GREEN LED is ON, If AIN2 Voltage < DAC Internal reference voltage (COUT is LOW)   Modules used:           Modifications in LPCMP module:   Modifications in IntCtrl_IP module: Modifications in the "Cmp_Ip_IrqHandler" function in "Cmp_IP.c" source file: Note: Not sure how it got missed or from where to get COUT status, so added manually to get COUT status from CSR register in the Cmp_Ip_Irqhandler once code generation is completed. GPIO selection details: How to test ? a) Connect jumper wire at the PTC2 in the EVB as highlighted in EVB below. b) RED LED ON -> Jumper wire connects to 5V      GREEN LED ON-> Jumper wire connects to GND Connect male jumper wire at PTC2 Thanks & regards, Krishnakumar V
記事全体を表示
*********************************************************************************** * Detailed Description: * The example locks * PFC PFCBLK2_SSPELOCK REG_PROT soft lock * and PFC REG_PROT hard lock. * ------------------------------------------------------------------------- * Test HW: : S32K344EVB-Q172 * MCU: : S32K344 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * SW Version : 5.0.0 * Build Version : S32K3_RTD_5_0_0_D2408_ASR_REL_4_7_REV_0000_20241002 ***********************************************************************************
記事全体を表示
This article has been moved to a new location: https://community.nxp.com/t5/S32M-Knowledge-Base/S32M2xx-Motor-control-use-cases/ta-p/2039790
記事全体を表示
This is an example project which is created to do an internal wake up from VLPS mode using LPTMR0.   From S32KRM, it tells us that internal wakeup is achievable using LPTMR0.     What code does? ======================================= 1) LPTMR0 is configured for 5 Seconds. So for interrupt occurs for every 5 seconds 2)LPTMR0  wakes up MCU for every 5 seconds and again it goes back to sleep for next 5 seconds. This cycle repeats forever. 3) When MCU is in RUN mode, GREEN color LED will be ON and it will in OFF if it goes to VLPS.   Project Configurations: =======================================     Other Informations: ======================================= Design studio: S32DS3.4 SDK                    : RTM 4.0.2 EVB                     : S32K118EVB2Q048   Note:   Following symbols should be included if you are creating the project from scratch to properly put MCU to sleep and wakeup from POR.   Thanks & regards, Krishnakumar V
記事全体を表示
【RTD400 MCAL 3】 K312 MCU clock system configuration 1. Abstract This document is talking about how to configure the clock system in the MCU of the K3 chip MCAL. This topic was always disdainful to talk about when I was doing LLD before, because the clock system of K3 is too simple, with internal fast and slow clock sources, external fast and slow clock sources, a PLL multiplier, and then various core peripherals to share. K3's RM even made a few options to frame the rules. From the perspective of LLD, especially the perspective of S32DS CT configuration, it is even more concise and clear. Here is a CT picture to show it:   Fig 1     Fig 2 With such a clock system, you can generate code with just a few taps and pokes. However, LLD is too free, and MCAL often encounters problems. Therefore, I decided to spend some time to understand the entire clock system of this MCAL MCU. This article takes K312 as an example to explain. Other K3 series are similar. 2. Clock system theory and configuration 2.1 K312 clock system From the clock chapter of RM, you can see the whole system block diagram:     Fig 3 This block diagram clearly shows the situation of each part. There are four clock sources: Internal fast clock FIRC: 48MHz, +/-5% error, maximum startup time 25us Internal slow clock SIRC: 32KHz, +/-10% error, maximum startup time 3ms External fast clock FXOSC: 8-40MHz, startup stabilization time FXOSC_CTRL[EOCV] × 128 External slow clock SXOSC: 32.768KHz, startup stabilization time SXOSC_CTRL[EOCV] x 128 One PLL: input 8-40MHZ, VOC output 640M-1280Mhz, PLL_PHIn_CLK output 25-480MHz. MUX_0: Output CORE_CLK, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK MUX_1: Output system timer STM0_CLK MUX_3: Output FLEXCAN0-2 clock MUX_4: Output FLEXCAN3-5 clock MUX_5: Output CLKOUT_STANDBY MUX_6: Output CLKOUT_RUN MUX_11: Output TRACE_CLK RTC_CLK: RTC clock 2.1.1 PLL From the PLL perspective, we need to know which values ​​the frequency multiplier is related to, which can be calculated using the following formula:     Fig 4 If it is an integer, the red box in the above figure is the common method, and this article will also use the above method to configure. PLL_PHI is the clock output by the final PLL, which is provided to the MC corresponding to other MUXs for selection. 2.1.2 MUX_0 System The MUX_0 system with details can be seen from RM:     Fig 5 As you can see, the clock source of MUX_0 can be two types: PLL or internal FIRC. Then the core clock can be generated later, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK. So what is the specific frequency of the generated clock? In principle, it can meet the maximum clock corresponding to each module, but the K3 series also makes some option recommendations. For example, K312 recommends using option B mode when RUN, especially the HSE clock, which usually needs to strictly meet the option recommendation. 2.1.3 MUX_6 Clock output In order to check the corresponding clock situation in the chip, the corresponding clock can be output through the CLKOUT pin. The CLKOUT pin can correspond to the selection of multiple clock sources. The specific situation is as follows:     Fig 6 The yellow content in the figure is what K312's CLKOUT_RUN can support. After the clock is configured, the corresponding clock will be selected to test whether the output is consistent with the configuration. 2.1.4 option B Recommended Solution In this article, K312 will configure the clock of option B in EB.     Fig 7 2.2 EB configuration        First, create a new K312 EB project. For the specific creation method, please refer to the previous article: [S32K3 Tools Part] How to port RTD's existing MCAL demo to other K3 chips This article will focus on the clock configuration corresponding to the MCU module based on RTD400 MCAL. For MCU configuration, two documents need to be consulted as reference books: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Mcu_TS_T40D34M40I0R0\doc: RTD_MCU_UM.pdf and RTD_MCU_IM.pdf If you don’t know how to configure, just follow the default values ​​recommended by the document. The following figure is an overview of the MCU. The main configured modules have the following three components: General, McuClockSettingConfig, McuModeSettingConf     Fig 8 2.2.1 General configuration In addition to Figure 8, you need to turn on the internal and external fast and slow clock control and PLL control, and add the corresponding API, as well as the crystal oscillator frequency. If this is not turned on, the corresponding configuration later will not be able to be configured.     Fig 9 2.2.2 McuClockSettingConfig configuration        This is the core area of ​​MCU clock configuration, which includes clock source, PLL, and various MUX conditions. First, you need to add a clock configuration:     Fig 10 Click in and there will be detailed configuration:     Fig 11 There are 17 items in total. You can keep the default configuration for options 1 and 6. Since the board does not connect to the external slow crystal oscillator 5, it is not configured. The rest should be configured according to the actual situation. The following explains them one by one: 2.2.2.1 McuFIRC configuration    Internal fast clock, 48MHz:     Fig 12 2.2.2.2 McuSIRC configuration Internal slow clock 32Khz     Fig 13 2.2.2.3 McuFXOSC configuration External crystal oscillator 16MHZ, fill in according to the actual connection situation.     Fig 14 2.2.2.4 McuCgm0ClockMux0 configuration Mux0 configuration, here are configured core clock, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE, DCM_CLK, is to meet the optionB requirements, and the clock comes from PLL_PHI0_CLK. When actually configuring, first configure the PLL clock to output the correct PLL_PHI0_CLK, PLL_PHI1_CLK clock.     Fig 15 2.2.2.5 McuCgm0ClockMux1 configuration     Fig 16 It can be configured according to the clock source required by the actual module. 2.2.2.6 McuCgm0ClockMux3 configuration Configure the clock source of the FLEXCAN0-2 module:     Fig 17 2.2.2.7 McuCgm0ClockMux4 configuration Configure the clock source of the FLEXCAN3-5 module:     Fig 18 2.2.2.8 McuCgm0ClockMux5 configuration Configure the clock source of the CLKOUT_STANBY module:     Fig 19 2.2.2.9 McuCgm0ClockMux6 configuration Configure the clock source of the CLKOUT_RUN module     Fig 20 2.2.2.10 McuCgm0ClockMux11 configuration Configure the clock source of the TRACE_CLK module     Fig 21 2.2.2.11 McuRtcClockSelect configuration Configure the clock source of the RTC module     Fig 22 2.2.2.12 McuPLL configuration Configure the clock source of the PLL module     Fig 23 2.2.2.13 McuClockReferencePoint configuration Configure the reference clock and the clock source selection interface of the peripheral modules.     Fig 24 At this point, the clock configuration is complete. For verification, you can use the CLKOUT_RUN output to output the corresponding clock to pin PTD10 for viewing. 2.2.3 McuModeSettingConf  configuration In Mcu's McuModeSettingConf->McuPeripheral, you need to turn on the peripherals you want to use:     Fig 25 2.2.4 PORT  configuration Because the internal clock needs to be output to CLKOUT_RUN, K312's PTD10 MSCR106 is checked, so the PORT pin is added as follows:     Fig 26 3. Test Result Next, on the S32K312-EVB board, we modify the clock source of EB's CLKOUT_RUN to test whether the clock matches the configuration. Commonly used MCU-related drivers are as follows:     Fig 27 The calling sequence of system startup MCU initialization is as follows: 1). Mcu_Init() 2). Mcu_InitClock() 3). Mcu_GetPllStatus() - Till PLL is locked. 4). Mcu_DistributePllClock() 5). Mcu_SetMode() 6). Mcu_InitRamSection() - If required The corresponding main code is as follows: #include "Mcu.h" #include "Mcu_Cfg.h" #include "Port.h" #include "Dio.h" #include "Port_Cfg.h" #include "Platform.h" void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } /** * @brief Main function of the example * @details Initialize the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { uint8 count = 0U; uint8 u8TimeOut = 100U; /* Initialize the Mcu driver */ #if (MCU_PRECOMPILE_SUPPORT == STD_ON) Mcu_Init(NULL_PTR); #elif (MCU_PRECOMPILE_SUPPORT == STD_OFF) Mcu_Init(&Mcu_Config_VS_0); #endif /* (MCU_PRECOMPILE_SUPPORT == STD_ON) */ /* Initialize the clock tree and apply PLL as system clock */ Mcu_InitClock(McuClockSettingConfig_0); #if (MCU_NO_PLL == STD_OFF) while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() ) { } Mcu_DistributePllClock(); #endif /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize Platform driver */ Platform_Init(NULL_PTR); while (count++ < 10) { Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_HIGH); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_HIGH); TestDelay(5000000); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_LOW); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_LOW); TestDelay(5000000); } // Exit_Example(TRUE); return (0U); } #ifdef __cplusplus } #endif 3.1 CLKOUT FIRC_CLK DIV2     Fig 28 It can be seen that the original 48Mhz clock of FIRC is divided by 2 and the clock waveform of 24Mhz is obtained, which is correct! 3.2 CLKOUT SIRC_CLK DIV2     Fig 29 It can be seen that the original 32Khz clock of SIRC is divided by 2 and the clock waveform of 16khz is obtained, which is correct! 3.3 CLKOUT FXOSC_CLK DIV10     Fig 30 It can be seen that the original 16Mhz clock of FXOSC is divided by 10 and the clock waveform of 1.6Mhz is obtained. 3.4 CLKOUT PLLPH0 CLK DIV10     Fig 31 It can be seen that the original 120Mhz clock of PLLPH0 is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.5 CLKOUT CORE CLK DIV10     Fig 32 It can be seen that the original 120Mhz clock of CORE is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.6 CLKOUT PLLPH1 CLK DIV4     Fig 33 It can be seen that the original 48Mhz clock of PLLPH1 is divided by 4 and the 12Mhz clock waveform is obtained. 3.7 CLKOUT HSE CLK DIV10     Fig 34 It can be seen that the original 60Mhz clock of HSE is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.8 CLKOUT AIPS_PLAT CLK DIV10     Fig 35 It can be seen that the original 60Mhz clock of AIPS_PLAT_CLK is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.9 CLKOUT AIPS_SLOW CLK DIV10     Fig 36 It can be seen that the original 30Mhz clock of AIPS_SLOW_CLK is divided by 10 and the clock waveform of 3Mhz is obtained, which is correct.  
記事全体を表示