Example S32K344 TempSenser S32DS36 RTD600/500/400_p24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32K344 TempSenser S32DS36 RTD600/500/400_p24

Example S32K344 TempSenser S32DS36 RTD600/500/400_p24

********************************************************************************

The purpose of this demo application is to show you how to use the Temperature Sensor module in S32DS. It includes two methods to obtain temperature.

-The first one starts a normal software conversion with one-shot mode on temp sense channel and calculates the temperature on chip from the data conversion.

-The second one calculates the temperature based on given data (if read directly using ADC).

Note: Please adjust the ADC reference voltage according to the board you are using

* ------------------------------------------------------------------------------
* Test HW: S32K344EVB-T172
* MCU: S32K344 1P55A
* Compiler: S32DS.ARM.3.5/6
* SDK release: S32K3_RTD_6.0.0/5.0.0/4.0.0_P24
* Debugger: OpenSDA/PE&Micro
* Target: internal_FLASH

*Jumper:J18-1:2,5V used.

*********************************************************************************

Note that if you use "sprintf", you need to check the following option.
Senlent_0-1753435505415.png

 

添付
評価なし
バージョン履歴
最終更新日:
‎07-25-2025 02:27 AM
更新者: