S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
**************************************************************************************************** * Detailed Description: * * SW triggered conversion of ADC0 internal channel 50 (ANAMUX_OUT). * ANAMUX is used for internal supply monitoring. * Supply to be monitored is configured using DCMRWF1 register. * * PIT is configured to generate interrupt each second then ADC conversion for selected supply is * SW started and measured result is printed to the UART interface * * ------------------------------------------------------------------------------------------------ * Test HW: S32K3x4EVB-T172 Rev B * MCU: S32K344_172HDQFP * IDE: S32DS 3.6.0 * RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 * Debugger: Lauterbach, P&Emicro * Target: Internal_FLASH * Serial: 115200, 8N1 ***************************************************************************************************/ Terminal output PetrS_0-1771351094333.png
View full article
The procedure to restrict JTAG access on the S32K3 MCU depends on whether HSE Firmware (FW) is used: With HSE FW: This scenario is not covered in this document. Without HSE FW: WARNING: ONCE THIS PROCESS IS COMPLETED, HSE CANNOT BE INSTALLED ON THE DEVICE. Development Environment: All code snippets provided represent the essential parts of the application and were developed using: Test HW: S32K344 (not EVB) MCU: S32K344 IDE: S32DS v3.5 Debugger: PEmicro USB Multilink Universal FX (unless otherwise noted) Drivers: S32K3 Real-Time Drivers v3.0.0 (released March 31, 2023) Base Project: Modified version of C40_Ip_Example_S32K344 Step 1: Program the CUST_DB_PSWD_A Field The UTEST Sector is an OTP (One Time Programmable), meaning erase operations are not allowed. You can only append or read data. Memory Range: 0x1B00_0080 to 0x1B00_009 Only the first 16 bytes (0x1B00_0080 to 0x1B00_008F) are usable. The rest is reserved (see Table 202 in the S32K3xx Reference Manual, Rev. 11). Programming Steps: I. Unlock the UTEST sector using PFCBLKU_SPELOCK[SLCK]. II. Write the 16-byte password to address 0x1B00_0080. Code Adjustments: /*============================================================================ * LOCAL MACROS ============================================================================*/ #define FLS_MASTER_ID 0U #define FLS_BUF_SIZE 16U #define FLS_SECTOR_ADDR 0x1B000080U #define FLS_SECTOR_TEST C40_UTEST_ARRAY_0_S000 NOTE: Ensure FLS_MAX_VIRTUAL_SECTOR and C40_SECTOR_ERROR are correctly defined in C40_Ip_Cfg.h: Instead of: #define FLS_MAX_VIRTUAL_SECTOR (527U) … #define C40_SECTOR_ERROR (528U) Use: #define FLS_MAX_VIRTUAL_SECTOR (528U) … #define C40_SECTOR_ERROR (529U) /*============================================================================ * GLOBAL CONSTANTS ============================================================================*/ uint8 TxBuffer[FLS_BUF_SIZE] = {0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0A,0x0B,0x0C,0x0D,0x0E,0x0F}; /* Password */ VaneB_0-1696631634239.png You can verify the password using the Memory Viewer (not covered here). VaneB_1-1696631672308.png   Step 2: Advance the MCU Lifecycle I. Set the lifecycle configuration word address in the IVT/boot header. Refer to sections 32.5 and 32.5.3 of the Reference Manual. NOTE: Ensure the structure of the boot_header (located in Project_Settings → Startup_Code → startup_cm7.s) is defined as follows: VaneB_2-1696631885135.png #define LF_CONFIG_ADDR (0x007D2000) /* The LC word can be at any flash address, taking care that does not interfere with HSE */ II. Write the LC word to the defined address: Life cycle stage Valid Values for LC Advancement OEM_PROD DADA_DADAh IN_FIELD BABA_BABAh Code Adjustments: /*=========================================================================== * LOCAL MACROS ===========================================================================*/ #define FLS_MASTER_ID 0U #define FLS_BUF_SIZE 8U #define FLS_SECTOR_ADDR 0x007D2000U #define FLS_SECTOR_TEST C40_CODE_ARRAY_0_BLOCK_3_S489 /* Look into C40_Ip_Cfg.h file to find the corresponding sector */ /*=========================================================================== * GLOBAL CONSTANTS ===========================================================================*/ uint8 LC_TxBuffer[FLS_LC_SIZE] = {0xDA, 0xDA, 0xDA, 0xDA, 0x0, 0x0, 0x0, 0x0}; /* Minimum data length 8 bytes */ VaneB_3-1696632329064.png Confirm the LC word using the Memory Viewer. VaneB_4-1696632360649.png III. Reset the MCU using the RESET_B pin, not the debugger. If the procedure was done correctly, you should see the following message: VaneB_5-1696632423439.png Step 3: Debugger Authentication To unlock the MCU, PEmicro provides Python scripts (PEmicro support files package) to facilitate debugger authentication when the password is set. In summary: I. Ensure Python 3.5 or later is installed. II. Open Command Prompt. III. Use cd to navigate to the directory containing the file package. IV. Run the script: py authenticate_password_mode.py -hardwareid=USB1 -password=… hardwareid: Debug hardware IP, name, serial number, or port password: 16-byte hexadecimal password NOTE: This must be done every time the MCU is reset or power cycled.   VaneB_6-1696632573362.png Step 4: Secure Debugging in S32DS In S32DS, when configuring the Debug Configurations of a project, change the Target to "SECUREDEBUG". This is necessary because during debug entry, a hard reset is toggled, which clears the authentication. VaneB_7-1696632658751.png VaneB_8-1696632678698.png Once authenticated, you can securely debug the device in S32DS.  *Additional Resources iSystem: How to unlock secure debug on NXP S32G2/3xx, S32R45x, and S32K3 Segger: NXP S32K3xx - Debug Authentication   Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
******************************************************************************************************* * Detailed Description: These demos showcase how to use eMIOS in Input Capture mode with DMA, utilizing both low-level drivers (Ip) and high-level drivers (MCAL). They demonstrate how timestamp data from captured input signals is stored and how a GPIO toggle provides a simple visual confirmation that the interrupt is being triggered as expected. VaneB_0-1763760555431.png * Connections:  VaneB_0-1763761243338.png ******************************************************************************************************* * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Debugger: S32DS 3.6.2, OpenSDA * Target: internal_FLASH ******************************************************************************************************* * Important information:  eMIOS Pwm: Configures EMIOS 0 Channel 1 as OPWMB (Output Pulse Width Modulation Buffered). This channel generates a waveform that will be captured by Channel 9 eMIOS Icu with DMA: Configures EMIOS 0 Channel 9 in ICU_MODE_TIMESTAMP using SAIC (Single Action Input Capture) mode. This channel captures the timestamps of the waveform generated by Channel 1. After a predefined number of captures, a DMA interrupt is triggered. ******************************************************************************************************* Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
NXP has ported FreeRTOS SMP (V11.1.0) to the S32K389. Many customers are interested in how to enable the FreeRTOS SMP on the S32K3xx. The demo is implemented as a single project with a single linker file and a single ELF file. Demo SW/HW Environment: 1. S32DS3.6.4 2. RTD7.0 3.SW32K3_FreeRTOS_11.1.0_7.0.0_CD1_HF1_D2511_DesignStudio_updatesite 4. S32K389 EVB  Demo Code Key Features: 1.FreeRTOS SMP is running on the S32K389 with all cores active. 2.DTCM is used as the task stack. 3.The hardware semaphore (SEMA42) is enabled in FreeRTOS. 4.XRDC is enabled so that each core has a unique core ID for semaphore operations. 5.CAN0 runs on Core0, and CAN4 runs on Core2. 6.LPUART11 is used to print debug information. All cores can output their own messages via LPUART11.  Disclaimer: The code is provided as demo code. NXP makes no commitment regarding its quality.  
View full article
This is set of S32K389EVB-Q437 demo projects. S32K389_GPIO_RTD6d0_S32DS3d6d2 S32K389_LPUART_RTD6d0_S32DS3d6d2 S32K389_FlexCAN_RTD6d0_S32DS3d6d2 S32K389_PFLASH_RTD6d0_S32DS3d6d2 S32K389_ADC_RTD6d0_S32DS3d6d2 S32K389_eMIOS_GPT_RTD6d0_S32DS3d6d2 S32K389_LowPower_RTD6d0_S32DS3d6d2 Examples are based on S32K3 RTD version 6.0 and created in S32DS version 3.6.2
View full article
S32K1 vdd falling low voltage POR clear situation 1. Abstract This document primarily aims to explain the situation where the POR flag in the RCM_SSRS of the S32K1 chip is cleared, and to explain the setting status of the reset pin and the POR and LVD bits when VDD is powered down. This article is written because some customers, when using the RCM_SSRS reset flag to determine the corresponding RAM initialization conditions, have made incomplete considerations, leading to component failures in actual projects. They mistakenly believe that as long as the SSRS POR flag is not cleared by software writing a 1 after power-on, the POR bit will remain indefinitely. In reality, even after power-on, if subsequent power fluctuations cause VDD to drop to LVD/LVR and trigger a reset, the POR flag may still be automatically cleared by the chip.   2. Document content This article mainly categorizes VDD power-down scenarios into three main types: (1) VDD drops below the minimum LVR value but above VPOR, and then power is  back to normal VDD. In this case, reset flag POR=0 and LVD=1 in RCM_SSRS. (2) VDD drops below LVD, above LVR, and LVDRE=0. In this case, reset flag POR=1 and LVD=1 in RCM_SSRS. (3) VDD drops below LVD, above LVR, and LVDRE=1. In this case, reset flag POR=0 and LVD=1 in RCM_SSRS. The schematic diagram is as follows: kerryzhou_0-1769060181626.png   3. Test result on S32K116 board kerryzhou_1-1769060181995.png   kerryzhou_2-1769060182346.png   kerryzhou_3-1769060182721.png   kerryzhou_4-1769060182767.png  
View full article
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** For S32K312, please use this correct clock HSE to AIPS clock should be ½. Please make these changes in the below all example code clock setting. HSE clock to 60 MHZ. Dinesh_Guleria_0-1717149049774.png   S32K312 PIT BTCU ADC-1 BCTU_ADC_DATA_REG DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-ADC-1-BCTU-ADC-DATA-REG-DMA-DS3-5/ta-p/1787778 S32K312 UART Transmit & Receive Using DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1787799 S32K312 EIRQ Interrupt :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-EIRQ-Interrupt-DS3-5-RTD300/ta-p/1787860 S32K312 SPI Transmit & Receive Using DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SPI-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1787856 Example S32K31 SPI multiple packet Transmit & Receive : solution for DMA Cache issue :- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K31-SPI-multiple-packet-Transmit-amp-Receive-solution/ta-p/2130091 Example S32K312 SPI Transmit & Receive Using Polling DS3.5 RTD300 :-- Example S32K312 SPI Transmit & Receive Using Polling DS3.5 RTD300 - NXP Community Example S32K312 SPI Transmit & Receive Using Interrupt DS3.5 RTD300 :-- Example S32K312 SPI Transmit & Receive Using Interrupt DS3.5 RTD300 - NXP Community S32K312 CAN Transmit & Receive Using Polling mode :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-Polling-mode-DS3/ta-p/1789191 S32K312 CAN Transmit & Receive Using MB & FIFO DMA :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-amp-FIFO-DMA/ta-p/1789196 S32K312 ADC :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-ADC-DS3-5-RTD300/ta-p/1789282 S32K312 Switch Debouncing :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Switch-Debouncing-DS3-5-RTD300/ta-p/1789290 S32K312 UART Freemaster :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Freemaster-DS3-5-RTD300/ta-p/1789306 S32K312 PIT BTCU parallel ADC FIFO DMA  :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1789908 S32K312 placing variables in DTCM & code in ITCM  :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-placing-variables-in-DCTM-amp-code-in-ICTM-DS3-5/ta-p/1790101 Example S32K312 Standby mode & Standby RAM and PAD keeping DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Standby-mode-amp-Standby-RAM-and-PAD-keeping-DS3/ta-p/1797713 Example S32K312 SWT DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SWT-DS3-5-RTD300/ta-p/1800559 Example S32K312 Printf Semihosting DS3.5 RTD300 :--- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Printf-Semihosting-DS3-5-RTD300/ta-p/1801354 Example S32K312 I2C Transmit & Receive Using DMA DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-I2C-Transmit-amp-Receive-Using-DMA-DS3-5-RTD300/ta-p/1801357 Example S32K312 HARDFAULT Handling Interrupt DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-RTD300/ta-p/1806259 Example S32K312 Bootloader to Application Jump DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Bootloader-to-Application-Jump-DS3-5-RTD300/ta-p/1809810 Example S32K312 PIT timer Toggle LED DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-timer-Toggle-LED-DS3-5-RTD300/ta-p/1809932 Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Interrupt-Handling-using-a-script-DS3/ta-p/1818507 Example S32K312 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Interrupt-DS3-5/ta-p/1818775 Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-Interrupt-DS3/ta-p/1818790 Example S32K312 STANDBY wake up using CAN-0-RX and GPIO Switch DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-CAN-0-RX-and-GPIO-Switch/ta-p/1891411 Example S32K312 STANDBY wake up using RTC DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-RTC-DS3-5-RTD300/ta-p/1930115 S32K312 : ADC Clock selection :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-ADC-Clock-selection/ta-p/1997759 Example IP S32K312 PWM ICU using EMIOS Custom IRQ DS3.5 RTD300 :-- Example IP S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community Example IP S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :-- Example IP S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community Example IP S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :-- Example IP S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community Example S32K312 Continuous SPI Transmit & Receive Using DMA DS3.5 RTD300 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Continuous-SPI-Transmit-amp-Receive-Using-DMA/ta-p/2024597 S32K312 : HSE Demo project :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-HSE-Demo-project/ta-p/2112562 S32K312 : FS26 Watchdog trigger using the SBC_FS26 CDD :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K312-FS26-Watchdog-trigger-using-the-SBC-FS26-CDD/ta-p/2161357
View full article
******************************************************************************* The purpose of this demo application is to place variables in DTCM memory for the S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** ZERO table : is for bss segment variables :  contains RAM start & end address of BSS section which need to be initialized with ZER). Init_table : is for DATA segment variables : contains RAM start address of DATA section & START & end address of ROM address where the initialization values of the variables are stored.   Startup file startup_cm7.s call function init_data_bss() . Inside this function uses these section :-- Dinesh_Guleria_0-1705479264979.png Variables declared :-- Dinesh_Guleria_1-1705479293837.png Linker file changes :-- Dinesh_Guleria_3-1705486935533.png   Dinesh_Guleria_2-1705479316994.png startup_cm7.s file changes :-- Dinesh_Guleria_3-1705479347509.png Dinesh_Guleria_4-1705487006718.png   MAP file :-- Dinesh_Guleria_4-1705479364855.png   Dinesh_Guleria_0-1705486825279.png   Debug window results :-- Dinesh_Guleria_5-1705479384543.png   Dinesh_Guleria_6-1705479395572.png   Dinesh_Guleria_1-1705486885096.png Dinesh_Guleria_2-1705486897441.png     https://www.kernel.org/doc/html/v5.9/arm/tcm.html   Due to being embedded inside the CPU, the TCM has a Harvard-architecture, so there is an ITCM (instruction TCM) and a DTCM (data TCM).  The DTCM can not contain any instructions, but the ITCM can actually contain data.   TCM is used for a few things: FIQ and other interrupt handlers that need deterministic timing and cannot wait for cache misses. Idle loops where all external RAM is set to self-refresh retention mode, so only on-chip RAM is accessible by the CPU and then we hang inside ITCM waiting for an interrupt. Other operations which implies shutting off or reconfiguring the external RAM controller.  
View full article
**************************************************************************************************** * Detailed Description: * * - CMU errors cannot be injected by any means other than manipulating the CMU thresholds, * except for FXOSC_CLK, which can be physically disrupted on the PCB. * * - CMU_FC_0 (FXOSC_CLK) is configured for **synchronous interrupt** on both LFF and HFF CMU events. * - CMU_FC_3 (CORE_CLK) is configured for **asynchronous destructive reset** triggered only by the LFF event; the HFF event is ignored. * - CMU_FC_4 (CORE_CLK) is configured identically to CMU_3: **asynchronous destructive reset** on LFF only; HFF is ignored. * - CMU_FC_5 (HSE_CLK) can be configured by the HSE_B core only. * Refer to the Reference Manual rev.10, Figure 122. Frequency checking (FC) instances * * - The configuration must be identical in both the MCU MCAL driver and the Clock Configuration Tool (clock details). * - To inject a specific CMU error, define one of the following macros: `INJECT_CMU_0`, `INJECT_CMU_3`, or `INJECT_CMU_4`. * * Behavior After Destructive Reset: * - Following a destructive reset (either `MCU_CORE_CLK_FAIL_RESET` or `MCU_AIPS_PLAT_CLK_FAIL_RESET`), * execution will halt in the `while(wait)` loop. * ------------------------------------------------------------------------------------------------ * Test HW: S32K3X4EVB_Q257 * MCU: S32K344, 0P55A * SDK: RTD 6.0.0 * Debugger: PEMicro Multilink FX * Target: internal_FLASH ****************************************************************************************************
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART0 for transmit 20 packets with each packet of 21 bytes using the Interrupt in cyclic order. Also when receiving UART packet generate Idle interrupt when variable length of data is received. I used coolterm tool to send the string of data. If Data send by cool term is less than 20 bytes which is set by API call Lpuart_Uart_Ip_AsyncReceive(), then Ideal interrupt is received RTD driver modified in RTD --> Lpuart_Uart_Ip.c. Baudrate : 921600  ------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Terminal Used :-- CoolTerm User can also use following terminal :-- Hercules uart terminal Dinesh_Guleria_0-1713853153843.png Idle Interrupt received :-- Dinesh_Guleria_1-1713853788454.png    
View full article
Lauterbach FCCU_Utility plugin - S32K3xx MPC57xx_FCCU_Utility_rev0.pdf This Lauterbach debugger plugin alows user to use FCCU configurations directly from debugger interface. Such will speed up development and will not require to recompile and program project each time FCCU configuration is changed. FCCU NCF_TOE1.png  The supplied document describes how to use Lauterbach FCCU (fault collection and control unit) periphery extension for S32K3xx devices. It is expected that user has deep knowledge on FCCU mechanisms in order to effectively use this extension. In such case this debugger plugin could be of a great value for various use cases like FA or debugging in development. Best regards, Peter
View full article
***************************************************************************** *Detailed Description: *This example will show you how to configure Sbc_fs23 Driver. *It initialization of Sbc_fs23 with watchdog window disabled. The Sbc_fs23_InitDevice() must be done within the dedicated 256 ms INIT window. *It Disable regulator V2, then re-enable it again. FS0b pin is asserted due to V2 Undervoltage reaction setting configured in FailSafe Init Configuration tab. *If the example runs without errors, the D12 LED on S32K31XEVB-Q100 will light up Green; otherwise, it will light up Red. *The SPI data between FS23 and S32K311 are captured and attached to the project. *Use the analog input of a logic analyzer or an oscilloscope to monitor the signals of FS23_V2 (TP27) and FS23_FS0 (TP8) on the KITFS23SKTEVM board. *------------------------------------------------------------------------------ *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A P32K311HV 0P98C * KITFS23SKTEVM Dev-kit SCH-53096 REV B2 MFS2320BMBB1EP * My S32K31XEVB-Q100 has an onboard PFS2320A0L1W1, but Step 13/14 of AN14041 mention that A0 devices are not supported, so S32K311 communicate with the FS23 on the KITFS23SKTEVM. *Connections: KITFS23SKTEVM | S32K31XEVB-Q100 ------------------------------|-------------------- SPI_CSB J28-2 | J12-5(PTB-17) SPI_MOSI J29-2 | J12-7(PTB-16) SPI_SCK J31-2 | J12-11(PTB-14) SPI_MISO J32-2 | J12.9(PTB-15) VCC J6-1 | J40-15 GND J6-2 | J40-13 - KITFS23SKTEVM: SW1 - position 2-3 , J30 - ON, J26 5-6 ON, J26 9-10 ON . - Connect KITFS23SKTEVM Dev-kit and S32K3 MCU via on-board Arduino headers. *SDK: * S32K3 RTD 4.0.0 (SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip) * FS23 RTD 1.0.0 (S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip) *Debugger: S32DS 3.5.8, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference Documentation: * AN14041 FS23 quick start guide (Rev. 2.0 — 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 — 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 — 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Sbc_fs23_TS_T40D34M10I0R0\doc * This example is migrated from Sbc_fs23_example_HLD_S32K344. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 ***************************************************************************** * Revision History: * Ver Date Author Description of Changes * 0.0 10-26-2025 Robin Shen Initial version * 0.1 11-21-2025 Robin Shen Upgrade FS23 RTD 1.0.0 from S32K3xx_SBC_FS23_R21-11_1.0.0_DS_updatesite_D2402_updated_D250115.zip to S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip ***************************************************************************** Example_S32K311_SPI_Sbc_fs23_HLD_v0_1_S32DS358_RTD400 Connections.jpg Example_S32K311_SPI_Sbc_fs23_HLD_v0_1_S32DS358_RTD400 saleae Logic 2.png
View full article
     In fact, this topic has been written by many people before, and it is well written. However, in actual operation, you may encounter some pitfalls, so this article will not write the article steps in detail, but will provide a real and direct operation video process. The main reference article source link is: https://www.wpgdadatong.com.cn/blog/detail/74936 The method is very useful. I have tried the existing RTD4.0.0 MCAL code and also imported it into my own configured MCAL code. The method is reliable and effective. Platform:     SW32K3_S32M27x_RTD_R21-11_4.0.0 S32DS3.5 EB tresos Studio 29.0 S32K344-EVB Attach the video directly: The main steps are as follows: STEP 1. Create a new S32DS project STEP 2. S32DS project configuration Including folder deletion, addition, filter condition addition, include files, link files, optimization conditions, macro definitions, etc. STEP 3. Create a new EB project Configure a new RTD, or copy the existing RTD configuration to avoid unnecessary problems and errors. STEP 4. Compile and download The following are some related files that need to be copied: MCAL_Plugins->Link Source Resource Filters 1.png  Fig 1 Includes 2.png  Fig 2 "${ProjDirPath}/Generate/include" "${MCAL_PLUGIN_PATH}/Adc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ae${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/BaseNXP${MCAL_MODULE_NAME_SUFFIX}/header" "${MCAL_PLUGIN_PATH}/BaseNXP${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Can_43_FLEXCAN${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CanIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CanTrcv_43_AE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Crc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CryIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Crypto_43_HSE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Csm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dem${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Det${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dio${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dpga${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EcuM${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Eth_43_GMAC${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthSwt${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthTrcv${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Fee${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Gdu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Gpt${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/I2c${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/I2s${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Icu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Lin_43_LPUART_FLEXIO${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/LinIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/LinTrcv_43_AE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mcl${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mcu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_EEP${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_EXFLS${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_INFLS${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/MemAcc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/MemIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ocotp${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ocu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Os${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/startup/include" "${MCAL_PLUGIN_PATH}/Port${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Pwm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Rm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Rte${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Sent${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Spi${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Uart${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Wdg${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/WdgIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Zipwire${MCAL_MODULE_NAME_SUFFIX}/include"   Preprocessor 3.png  Fig  3 S32K3XX S32K344 GCC USE_SW_VECTOR_MODE D_CACHE_ENABLE I_CACHE_ENABLE ENABLE_FPU   Linker   4.png Fig  4 "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k344.ld" optimization   5.png Fig 5 -fno-short-enums -funsigned-char -fomit-frame-pointer -fstack-usage   main.c Comment: #include "check_example.h #Exit_Example(TRUE);   Attached code: MCAL_Dio_S32K344_S32DS363_RTD600_CP.zip: RTD MCAL copy to S32DS project MCAL_Dio_S32K312_RTD600_MCUPLL.zip: S32K312 MCU with PLL, add UART printf Others attachment all link the MCAL to RTD install path.
View full article
***************************************************************************** *Detailed Description: *This example will show you how to configure Wdg_fs23 Driver. *Sbc_fs23_InitDriver, Sbc_fs23_GoToInitState, Wdg_43_fs23_Init, Sbc_fs23_InitDevice initialize the Sbc device and external Wdg in SLOW MODE(This mode can e.g. be used during system startup/initialization phase). *Sbc_fs23_InitDevice release FS0B, according to the configuration in Sbc_fs23 WatchdogConfig tab: Release safety outputs after init *Sbc_fs23_TimeDelay delay for an amount of time, allow Gpt ISR to trigger watchdog externally. *Wdg_43_fs23_SetMode(WDGIF_FAST_MODE); switch Wdg operation mode to FAST MODE(This mode can e.g. be used during normal operations of the ECU). *Wdg_43_fs23_SetTriggerCondition(10000U); sets a new timeout value to 10 seconds, during which Wdg_fs23_Cbk_GptNotification0 continuously refresh the watchdog. *To demonstrate the watchdog timeout, Wdg_43_fs23_SetTriggerCondition was not called again to set a new timeout value, and Wdg_fs23_Cbk_GptNotification0 no longer refreshed the watchdog. *The watchdog error counter(WD_ERR_CNT) continues to increase reached its maximum value(WD_ERR_LIMIT), causing fault error counter(FLT_ERR_CNT) to increment by 1. *FS23 eventually enters fail-safe mode because FLT_ERR_CNT >= max. At this point, it was observed that LEDs V1 (D7), V2 (D8), and V3 (D9) of KITFS23SKTEVM were turned off. *The SPI data between FS23 and S32K311 are captured and attached to the project. *------------------------------------------------------------------------------ *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A P32K311HV 0P98C * KITFS23SKTEVM Dev-kit SCH-53096 REV B2 MFS2320BMBB1EP * My S32K31XEVB-Q100 has an onboard PFS2320A0L1W1, but Step 13/14 of AN14041 mention that A0 devices are not supported, so S32K311 communicate with the FS23 on the KITFS23SKTEVM. *Connections: KITFS23SKTEVM | S32K31XEVB-Q100 ------------------------------|-------------------- SPI_CSB J28-2 | J12-5(PTB-17) SPI_MOSI J29-2 | J12-7(PTB-16) SPI_SCK J31-2 | J12-11(PTB-14) SPI_MISO J32-2 | J12.9(PTB-15) VCC J6-1 | J40-15 GND J6-2 | J40-13 - KITFS23SKTEVM: SW1 - position 2-3 , J30 - ON, J26 5-6 ON, J26 9-10 ON . - Connect KITFS23SKTEVM Dev-kit and S32K3 MCU via on-board Arduino headers. *SDK: * S32K3 RTD 4.0.0 (SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip) * FS23 RTD 1.0.0 (S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip) *Debugger: S32DS 3.5.8, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference: * AN14041 FS23 quick start guide (Rev. 2.0 — 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 — 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 — 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Sbc_fs23_TS_T40D34M10I0R0\doc * RTD_WDG_43_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Wdg_43_fs23_TS_T40D34M10I0R0\doc * AUTOSAR_SWS_WatchdogDriver.pdf https://www.autosar.org/fileadmin/standards/R21-11/CP/AUTOSAR_SWS_WatchdogDriver.pdf * This example is migrated from Wdg_fs23_example_HLD_S32K344. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 ***************************************************************************** Example_S32K311_SPI_Wdg_fs23_HLD_v0_0_S32DS358_RTD400 connections.jpg Example_S32K311_SPI_Wdg_fs23_HLD_v0_0_S32DS358_RTD400 saleae Logic 2.png
View full article
[S32K3 Tools Part] How to port RTD's existing MCAL demo to other K3 chips  1. Abstract     From the release notes of NXP's RTD4.0.0, we can see that the supported chip models are very complete: 1.png Fig 1 From this point, we can know that RTD4.0.0 can cover all S32K3 series chips. But if you want a ready-made demo, such as MCAL demo, you can see it under the ready-made demo path, for example: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0\examples\EBT Just S32K344,S32K358,S32K388,S32K396,S32M276。 Therefore, if you use other S32 chips, such as K312, in actual use, although it is within the range supported by RTD, but there is no ready-made demo to use, you need to do the porting by yourself. This article will explain how to port the RTD4.0.0 K344 MCAL demo to S32K312 and configure the corresponding EB project. First, implement the execution in the command line. After success, port the working MCAL code EB project to S32DS. 2. Platform and migration steps 2.1 Platform Description This article is based on RTD4.0.0: SW32K3_S32M27x_RTD_R21-11_4.0.0 For other versions with patch or HF, the operation process is the same! Hardware platform: S32K312 mini EVB or S32K312EVB Other official EVBs, such as S32K31XEVB, or the customer's own S32K3 hardware board also have the same steps. Due to the lack of official EVB boards, this article is based on S32K312 mini EVB, combined with P&E Multilink simulator download simulation. The platform situation is as follows: 2.png Fig 2 2.2 Migration steps The reference demo can be any existing demo in RTD4.0.0. In order to simplify the process, this article takes DIO as an example: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344 2.2.1 Copy the project and configure 2.2.1.1 Copy the project In order not to affect the original RTD default demo, here we directly copy a Dio_TS_T40D34M40I0R0 and open the path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins Copy Dio_TS_T40D34M40I0R0 and save it in a folder named: Dio_TS_T40D34M40I0R0_miniK312_doc The process for other chips is similar. You only need to change the chip name and related configuration to the required chip. Open folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX Copy Dio_Example_S32K344 to Dio_Example_S32K312 3.png Fig 3    Open path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject  Modify the EB project Dio_Example_S32K344 to Dio_Example_S32K312 4.png Fig 4 2.2.1.2 Configure the project Enter the newly created Dio_Example_S32K312, open the path with VScode, and save the VScode workspace to this path. Modify project_parameters.mk: GCC_DIR = C:/NXP/S32DS.3.5_RTD400/S32DS/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_4.0.0/eclipse/plugins EXAMPLE_DERIVATIVE = S32K312 TRESO_PROJECT_NAME = Dio_Example_S32K312 ​ 5.png Fig 5 6.png Fig 6 Check_build_params.mk, delete the following code: ifeq ("$(wildcard $(T32_DIR)/bin/windows/t32marm.exe)","") $(error Invalid path set to Trace32. \ The provided path: from project_parameters.mk T32_DIR=$(T32_DIR) is invalid!) endif This part is used for lauterbach trace32. If it is not deleted, an error will be reported. 2.2.2 EB project configuration The following is the configuration of the EB project. Open the EB tresos Studio 29.0 software and import the project. File->Import->General->Existing Projects into Workspace, add the EB project path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject\Dio_Example_S32K312 Note, do not click copy projects into workspace!!! Select the project Dio_Example_S32K344, right-click the mouse, and rename it to: Dio_Example_S32K312 7.png Fig 7 Double-click someId to open the configuration module. Open the Resource module, General->ResourceSubderivative select the target chip partbumber, here select: s32k312_hdqfp172 8.png Fig 8 After saving, you will find many errors reported as follows: 9.png Fig 9 There is no need to worry too much here, because if you analyze it carefully, you will find that it is actually because there are many modules on K344 that K312 does not have. So enter the error prompt location and delete the missing K312 module. Mcu->McuModeSettingConf->McuPeripheral If you click in, you can find that if the K312 does not have a module, there is a red cross in front of the peripheral Name. 10.png Fig 10 The direct method is to delete all the error items, a total of 41. After deleting, you can find that all the problems are gone: 11.png Fig 11 Select someId in the project, right-click, and click Generate Code. You can see that the project can be generated without any errors. 12.png Fig12 Don't take it lightly here. Although the code can be generated without error, there is still a place that needs to be modified. Here, we can firstly close the EB tresos tool, then open terminal->new terminal in VScode and enter: 13.png Fig13 We can see the error content is : mcucgm0_clockMux0/McuClockMux0Divider5, McuClockMux0Divider6, McuClkMux0Div5_En, McuClkMux0Div6_En. Open S32KRM here, and you can see that K312 actually does not have MUX_0_5,6. 14.png Fig 14 At this time, when I opened the EB tresos software again, there was indeed such an error on the interface, and there was no divider 5,6 option in mcucgmClockMux0. 15.png Fig 15 Don't worry at this time, there is a way to fix this problem. Close the EB tresos tool and open the text: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject\Dio_Example_S32K312\config\ Mcu.xdm file. Directly turn off the enablement and value configuration of divider 5 and 6 in the file. Modify the following code:Modified to:The main thing is to change the enable and frequency value of Mux0Divider5,6 hidden in the file. Reopen it and you can see that the error disappears. Right-click on the EB project someId, generate project, and the code can be generated normally without error. Here is a little trick: In order to prevent the mismatch between the previously generated code and the latest EB project, you can also change: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\generate Folder:src,include clean it,then regenerate in EB tresos when generating a project. Close the EB software and enter make generate again in the terminal of the Vscode project You can see that there are no problems at this time: 16.png Fig 16  3.Command line compilation and result testing From the above steps, the code and EB configuration migration of an existing RTD K344 project to a K312 MCAL project has been completed. Now, through VScode, command line form, generate main.elf, and then download and test. Command: make generate make build the main.elf can be found in the following folder path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\out Regarding testing, because there is a main.elf file and PE Multilink, you can create a new K312 project in S32DS. The debug interface is PE Multilink. After compiling and generating the code, copy main.elf to the Debug_FLASH folder of the new project. In the S32DS debug configuration, directly replace the C/C++ application with main.elf and download it for testing.  17.png Fig 17 As you can see, you can enter the debug interface, and the LED light on the actual test board can flash successfully. This means that the MCAL code has been successfully ported to K312. 4. S32DS project migration and testing       In the previous document: https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-import-RTD-EB-project-into-S32DS/ta-p/1966207 Previously, the RTD MCAL EB project was transplanted to the K344 project of S32DS. Simply modify the project name, project chip model, ld file, driver file inclusion, etc., then clean the project and compile the project.      It is assumed here that you already have an RTD MCAL project imported into the S32DS project, and then modify it based on this. 4.1 S32DS Project Configuration     Because the folder was copied under the original RTD folder, there is a newly created folder in the S32DS project Mcal_Plugins->Link_Source. This folder needs to be excluded from compilation: Select Dio_TS_T40D34M40I0R0_minik312_doc, right-click Build path->remove from->Debug_FLASH.      18.png Fig 18 Rename the project from Mcal_Dio_S32K344_RTD400 to Mcal_Dio_S32K312_RTD400. Modify the following project configuration, project->properties: (1)preprocessor S32K344->S32K312 19.png Fig 19   (2) Sstandard S32DS C Linker->General Modify "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k344.ld" To "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k312.ld" After modification, click apply and close Now, change the main.c content to the content in path:  C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\src\main.c Add header file: #include "Port_Cfg.h" Comment code: // #include "check_example.h" // Exit_Example(TRUE);   4.2 EB project replacement Copy: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Dio_TS_T40D34M40I0R0_miniK312_doc\examples\EBT\S32K3XX\Dio_Example_S32K312\TresosProject\Dio_Example_S32K312\config All the .xdm file to the S32DS EB folder, replace the old file: Mcal_Dio_S32K312_RTD400\Tresos_Project\Mcal_Dio_S32K344_RTD400\config Use the EB tresos open the above project, then Generate project,after the code is generated, close the EB project, back to the S32DS side. 4.3 MCAL S32DS project testing clean project:project->clean project,  then build the project 20.png Fig 20 You can see that it can be compiled successfully, then RUN->debug configuration selects the downloaded code xxx_Debug_FLASH_PNE. Note that you need to change the Device from S32K344 to S32K312 21.png Fig 21 After successful configuration, click debug, download the code and simulate. The results are as follows: 22.png Fig 22 As you can see, we can successfully enter debug, and the light on the board is actually blinking, which means that the RTD MCAL project demo can be successfully ported to S32K312 S32DS. Video: 1.MCAL demo porting K344 to K312 based on RTD500     2.S32DS CT MCAL demo porting K344 to K312 based on RTD500 Attachment: Dio_Example_S32K312_MCALRTD600.zip: unzip it, get Dio_Example_S32K312, put in the RTD600 folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_xxx\examples\EBT\S32K3XX Dio_TS_T40D34M60I0R0_xxx is copy from Dio_TS_T40D34M60I0R0
View full article
**************************************************************************************************** * Detailed Description: * This code demonstrates how to inject an ECC (Error Correction Code) fault into either DTCM0 * (Data Tightly Coupled Memory) or SRAM0 using the EIM (ECC Injection Module). * * When the processor reads corrupted data from DTCM0 or SRAM0, an ECC error is detected, resulting in: * - A Bus Fault exception raised by the core. * - An error report generated by the ERM (Error Reporting Module), which can also trigger an interrupt. * * By default, the ERM interrupt has a lower priority than the Bus Fault exception. In this example, * the Bus Fault exception priority is intentionally lowered so that the ERM interrupt is serviced first. * This ensures the system can respond to the ERM interrupt before the core's Bus Fault handler executes. * * IMPORTANT: The interrupt vector table must not reside in SRAM0 or DTCM0 when injecting an * uncorrectable ECC fault into these memories. Otherwise, the ECC fault would corrupt the vector * table during a fetch, leading to unpredictable behavior. * Always check the VTOR (Vector Table Offset Register) * to confirm the vector table location before performing ECC fault injection. * * Memory Selection: * You can select which memory to inject the ECC fault into using the following macros: * #define SRAM0 * #define DTCM0 *************************************************************************************************** * ------------------------------------------------------------------------------------------------* * Test HW: S32K3X4EVB_Q257 * MCU: S32K344, 0P55A * SDK: NA * Debugger: Lauterbach Trace32 * Target: internal_FLASH ****************************************************************************************************
View full article
Hi everyone, Welcome to the NXP Tech Days 2025 training session AUT-T437: Hands - On Workshop: Explore Ethernet Integration on the S32K3 Microcontroller. My name is Alejandro Flores Triana (Alex) and I will be your guide during this conference. I am an Automotive Applications Engineer supporting different OEMs, Tier1s, Partners and other internal NXP teams on topics related to communication protocols (e.g. CAN, LIN, SPI, I2C, Ethernet, etc.). The idea of this session is for you to understand how to program the S32K3 Ethernet interface using NXP Real-Time Drivers (RTDs) – Autosar MCAL Layer. We will use a base project and together modify it to create a simple Ethernet application. Therefore, to be ready follow the steps below to get your environment up and running before the session. On your laptop, install the NXP Software environment described in the attached presentation: Hands - On Workshop: S32K3 Ethernet Prerequisites.   Once you have the NXP software environment installed, download the attached project: S32K344_ETH_MCAL_TechDays.exe.   Run the .exe project with administrator rights. Accept the license and install in the desired folder.   AlexTriana_0-1729298444699.png   AlexTriana_1-1729298444701.png   AlexTriana_2-1729298444703.png   Open the NXP Design Studio. Click File -> Import -> Existing Projects into Workspace. AlexTriana_3-1729298444705.png   Select root directory and browse the folder where you downloaded the project. AlexTriana_4-1729298444708.png   Select Copy projects into workspace. Then, click Finish. AlexTriana_5-1729298444713.png   Select the project. Click on the arrow next to the hammer. Click on Debug_FLASH. Picture1.png Then you are ready for the session! See you soon. Best Regards, Alejandro Flores Triana
View full article
Hi everyone, Welcome to the NXP Tech Days 2024 training session AUT-T4977: Hands - On Workshop: S32K3 Ethernet- How to Configure Hardware and Software. This session was initially planned for 15 attendees. But due to the popularity of the lecture, we have increased the number of available seats . Therefore, we will work in pairs during the Hands-On. My name is Alejandro Flores Triana (Alex) and I will be your guide during this conference. I am an Automotive Applications Engineer supporting different OEMs, Tier1s, Partners and other internal NXP teams on topics related to communication protocols (e.g. CAN, LIN, SPI, I2C, Ethernet, etc.). The idea of this session is for you to understand how to program the S32K3 Ethernet interface using NXP Real-Time Drivers (RTDs) – Autosar MCAL Layer. We will use a base project and together modify it to create a simple Ethernet application. Therefore, to be ready follow the steps below to get your environment up and running before the session. On your laptop, install the NXP Software environment described in the attached presentation: Hands - On Workshop: S32K3 Ethernet Prerequisites.   Once you have the NXP software environment installed, download the attached project: S32K344_ETH_MCAL_TechDays.exe   Run the .exe project with administrator rights. Accept the license and install in the desired folder   AlexTriana_0-1729298444699.png   AlexTriana_1-1729298444701.png   AlexTriana_2-1729298444703.png   Open the NXP Design Studio. Click File -> Import -> Existing Projects into Workspace AlexTriana_3-1729298444705.png   Select root directory and browse the folder where you downloaded the project AlexTriana_4-1729298444708.png   Select Copy projects into workspace AlexTriana_5-1729298444713.png   Click Finish. Select the project. Click on the arrow next to the hammer. Click on Debug_FLASH. Picture1.png Then you are ready for the session! See you soon. Best Regards, Alejandro Flores Triana
View full article
This document provides a brief explanation of the Excel-based calculator developed to assist with the computation of TX Arbitration Start Delay as described in the S32K3 reference manual. Senlent_5-1760435008352.png The tool implements the formula provided in the datasheet, allowing users to input relevant parameters and automatically calculate the delay values. It is intended to support engineers in evaluating CAN transmission timing and optimizing arbitration performance in S32K3-based applications.   1.Fill in the clock and CBT and FDCBT configuration parameters according to your requirements. For example, we fill the parameters according Case 3: Senlent_2-1760432857467.png Senlent_0-1760432107988.png  Then we can get the TASD value for non-FD frames is 24.05. Senlent_4-1760433268477.png   Please note that this summary is not officially released by NXP. It is a personal summary for reference only. If there are any errors, please contact me.
View full article
****************************************************************************************************** * Detailed Description: These demos showcase how to configure the eMIOS module on the S32K3 series, highlighting various operational modes and their implementations using the RTD high-level drivers, commonly known as MCAL drivers. The implementations demonstrated in these examples follow the approach outlined in the community thread:  S32M27x/S32K3 – eMIOS Usage. * Connections:  VaneB_0-1759773423423.png ******************************************************************************************************* * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Debugger: S32DS 3.6.2, OpenSDA/ PEmicro Multilink Universal FX  * Target: internal_FLASH ******************************************************************************************************* * Important information:  The OPWMT channel does not support the notification function. In this mode, the Sn[FLAG] bit is only set upon an AS2 match, which defines the generation of a trigger event within the PWM period. As a result, OPWMT mode cannot support notifications based on signal edges. A bus exception may occur during the execution of Mcl_Init() if the eMIOS clock is not properly enabled. To avoid this issue, ensure that the eMIOS peripheral clock is activated in the configuration settings under: MCU driver → McuModuleConfiguration → McuModeSettingConf → McuPeripheral *******************************************************************************************************
View full article