Example S32K311 eMIOS MCAL S32DS 3.6.2 RTD 6.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32K311 eMIOS MCAL S32DS 3.6.2 RTD 6.0.0

Example S32K311 eMIOS MCAL S32DS 3.6.2 RTD 6.0.0

******************************************************************************************************
* Detailed Description:
These demos showcase how to configure the eMIOS module on the S32K3 series, highlighting various operational modes and their implementations using the RTD high-level drivers, commonly known as MCAL drivers.

The implementations demonstrated in these examples follow the approach outlined in the community thread: 
S32M27x/S32K3 – eMIOS Usage.

* Connections: 

VaneB_0-1759773423423.pngVaneB_0-1759773423423.png

*******************************************************************************************************
* Test HW: S32K31XEVB-Q100
* MCU: S32K311
* Debugger: S32DS 3.6.2, OpenSDA/ PEmicro Multilink Universal FX 
* Target: internal_FLASH
*******************************************************************************************************
* Important information: 
The OPWMT channel does not support the notification function. In this mode, the Sn[FLAG] bit is only set upon an AS2 match, which defines the generation of a trigger event within the PWM period.

As a result, OPWMT mode cannot support notifications based on signal edges.

A bus exception may occur during the execution of Mcl_Init() if the eMIOS clock is not properly enabled. To avoid this issue, ensure that the eMIOS peripheral clock is activated in the configuration settings under:

MCU driver → McuModuleConfiguration → McuModeSettingConf → McuPeripheral
*******************************************************************************************************

添付
評価なし
バージョン履歴
最終更新日:
‎10-06-2025 11:26 AM
更新者: