S12 / MagniVマイクロコントローラ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12 / MagniV Microcontrollers Knowledge Base

ラベル

ディスカッション

ソート順:
I've just went through my PC and put some examples here. ( I made them "a few" days ago.) The files are presented with extension BMP because of some firewals.   AN3490.pdf DOC-XEP100-MMC-Memory_Map-Common_Map-V5_0-MSExcel.xls EEE.xls TN263-CodeWarrior IDE.pdf XEP100 - EEPROM Direct Access - CW45.zip XEP100 - Initial data in Emulated EEPROM - CW47.zip XEP100 - MPU - CW47.ZIP XEP100 - RAM addressing - CW45.zip XEP100 - SCI - XonXoff_poll - CW47.zip XEP100 - Security + Backdoor Key Access - CW47.zip XEP100-ATD wakes up from STOP - CW47.zip XEP100-ATD-ATDandXGATEandSharedRAM-CW50.zip XEP100-ATD-CH1toCH4-CW47.ZIP XEP100-ATD-CH1toCH8-CW47.ZIP XEP100-ATD-Cntnuos_SingleCh-v1_0-CW47_Data.zip XEP100-ATD-Tmprture_bandgapV-v1_0-CW47_Data.zip XEP100-BDM-BDMcommExample-CW50.zip XEP100-BufferRAMasOneArray-CW51.zip XEP100-BufferRAMasRAMonly-CW51.zip XEP100-CAN-CAN0-RxTxIsrLoopback-CW47.zip XEP100-CAN-CAN0-TxAtXGATE-CW51.zip XEP100-CAN-CAN0CAN1 - CW45.ZIP XEP100-CAN-CAN2CAN2-Identifiers SandX-loopback-CW51.zip XEP100-CAN-CAN2CAN3-CW47.ZIP XEP100-CAN-CAN2CAN3-FILTER-CW51.ZIP XEP100-CAN-CAN2CAN3-Identifiers SandX-CW51.zip XEP100-CAN-LoopbackInterrupt-CW51.zip XEP100-CAN.ZIP XEP100-CAN0 - CAN1 - CW45.ZIP XEP100-CAN0-RxTxIsrLoopback-CW47.zip XEP100-CAN0-RxTxIsrLoopbackXGATE-CW51.zip XEP100-CAN0-TxAtXGATE-CW51.zip XEP100-CRG-COP-CW47.ZIP XEP100-CRG-PLL-Setup-CW47.zip XEP100-EBI-MRAM256x16-CS0-CW51.zip XEP100-EBI-MRAM256x16-CS2-CW51.zip XEP100-ECT-ECTasPWM-CW47.zip XEP100-ECT-FreqMeasurement-CW51.zip XEP100-ECT-InputCapture-CW51.zip XEP100-ECT-TIM.ZIP XEP100-EEEPROM-Addressing-Lukas-CW46.zip XEP100-EEEPROM-DataPlacement-CW51.zip XEP100-EEEPROM-plusMPU-CW51.zip XEP100-EEPROM-DirectAccess-CW51.zip XEP100-EXBUS-EXRAM256x16-CS1-CW47.zip XEP100-EXBUS-ExRam_MR2A16ACYS35-CS1-CW51.ZIP XEP100-FLASH-PFLASH-CW47.ZIP XEP100-FLASH-PFLASH-CW51.ZIP XEP100-FLASH-PFLASH-PFlashInitData.zip XEP100-FLASH-PFLASH_reading-CW47.zip XEP100-GPIO-PJ2isr-CW47.zip XEP100-GPIO-PortPisrXgate-CW51.zip XEP100-ID-readPartID-CW47.zip XEP100-IIC-Master4Flash24C16-CW51.zip XEP100-INT-INTERRUPTNUMBER-CW51.ZIP XEP100-INT-TRAPPROC-CW51.ZIP XEP100-MDDC-delay generator-v1_0-CW47.zip XEP100-MPU-MPU-CW47.ZIP XEP100-PFLASH-CW47.ZIP XEP100-PFLASH-CW51.ZIP XEP100-PIM-PTPfunctions1-CW47.zip XEP100-PIT-FLOATING PERIOD-CW51.ZIP XEP100-PIT-SERIAL_DATA_OUT-CW45.ZIP XEP100-PIT-XGATE-SEMAPHORES-CW51.ZIP XEP100-PWM-dutyatXGATE-CW47.zip XEP100-RAM-addressing-v1_0-CW51.zip XEP100-RAM-RAMaddressing-CW45.zip XEP100-SCI_PIT-CW47.zip XEP100-SCI-ECHO-isr.zip XEP100-SCI-ECHOatCPU-CW47.zip XEP100-SCI-ECHOatCPUisr-CW47.zip XEP100-SCI-ECHOatXGATEisr-CW47.zip XEP100-SCI-Sci0transmitterOnXGATE-CW45.zip XEP100-SCI-SciTx-CW45.zip XEP100-SCI-SCI_PIT-CW47.zip XEP100-SCI-XonXoff_poll-CW47.zip XEP100-SciTx-CW45.zip XEP100-SECURITY-BackdoorKeyAccess-CW47.zip XEP100-STOP-ATDwakesUp-CW47.zip XEP100-STOP-RTIwakesUp-CW51.zip XEP100-STOP-WakeUp-CW47.zip XEP100-STOP_and_ API_and_PLL-CW47.zip XEP100-STOP_and_XIRQ_and_PLL-CW47.zip XEP100-TIM-10msIsr-CW47.zip XEP100-TIM-FreqMeasurement-CW51.zip XEP100-UnionInPages.zip XEP100-UnionInPagesAndECT.zip XEP100-XGATE-SharedVars-CW51.zip XEP100PWM-PWM8bit-CW45.zip XEP100_SPI_master_w_25AA256.zip XEQ384EXBUS-EXRAM256x16-CS2-4000-7FFF-CW47.zip XEQ512-PWM-10kHz8bit100point-CW51.zip XEQ512-RAM-addressing-v1_0-CW51.zip XEQ512-SWtrigger-CPU_XGATE-CW47.zip XET256-ECT-asPWM-CW47.zip XET256-ECT-OC-CW47.ZIP XET256-EXBUS-ExROM2ExRAM-CW46.zip XET256-RTI-RTIdec and COP-v1_0-CW47.zip XET256-SCI-Tx_Poll-CW51.zip XF256-SCI-ECHOatCPUisr-CW47.zip XF256-SCI-ECHOatXGATEisr-CW47.zip XF256-SCI-ECHOatXGATEisr-CW47.zip
記事全体を表示
The DEVKIT platform The NXP released new board platform for automotive products – DEVKIT. The DEVKIT is a low-cost development platform with Arduino UNO/Mega pin compatibility. In my review, I will focus mainly on DEVKIT-ZVL128 board.                                          The DEVKIT boards are similar to FRDM boards, but they are slightly wider (58mm versus 53mm) due to moving MCU specific pins to external rows of Arduino pin compatible connectors. So, we should be able to access MCU specific pins even when we connect any Arduino shield on top of this board.     The other currently or soon available DEVKIT boards are: DEVKIT-S12ZVL DEVKIT-S12ZVC DEVKIT-S12G128 DEVKIT-S12XE DEVKIT-S12VR64 DEVKIT-MPC5748G DEVKIT-MPC5744P FRDM-KEA128 FRDM-KEA64 FRDM-KEA32 DEVKIT-COMM - 6 LIN and 4 CAN transceivers shield DEVKIT-MOTORGD – three-phase motor control shield with GD3000 N-channel MOSFETs driver and power stage Note: The FRDM-KEA boards belongs also into the DEVKIT platform despite on the “FRDM” in the board name.     The Content What you will get for US$35 (current price on NXP web pages): Antistatic paper box DEVKIT-ZVL128 board short micro-USB cable       The sticker on the box points to the NXP web pages for downloading more documents such as the quick start guide, schematic, PCB BOM and design files, code examples or buy the same board again ;-). Unfortunately, the board User Guide is not available yet.   This web page is also offering “Getting Started” tab with the interactive quick start guide – quite useless feature since the page forgets on necessary 12V power supply for MCU powering and it proposes old CW5.1 (Classic IDE) for S12(X) instead of CW10 (Eclipse IDE).   What else you will need: The IDE – for example, the NXP CodeWarrior or Cosmic ZAP 12V DC power supply (3.8V~40V) with barrel connector (6mm outside diameter x 2mm inside diameter) MCU code   The Board DEVKIT-ZVL128 board is assembled by: S12ZVLA128 MCU (Big Knox) in 48-pin LQFP package 8MHz crystal Standard 2mm DC power jack connector for 12V power supply On-board OSBDM debugger trough micro-USB connector Standard BDM connector Arduino UNO pin compatible connectors with extended connectivity (the internal rows of the connectors are arranged to fulfill Arduino™ shields compatibility) RGB LED and 2 x push button switches LIN and CAN connectors CAN transceiver MC33901 5k potentiometer and RESET switch 3V/150mA and 5V/150mA LDO voltage regulators     The great thing is that the board has connector pins named from the bottom side of the PCB = less tracking on schematic.     On another side, some of the MCU pins may be routed to Arduino connectors trough zero Ohm resistors. Since these resistors are very small (size 0402), the potential re-routing will need a solid hand.     It is great that loop type test points arrived finally also on low-cost development boards – now in surface mount version. The small loops may be simply locked by test hooks and measured by laboratory equipment.       The MCU The S12ZVLA128 is one of MagniV family MCUs using the 180nm NVM + UHV technology that offers the capability to integrate 40V analog components. It integrates S12Z core, features from the existing S12 portfolio together with “high-voltage” analog modules, including the voltage regulator (VREG) and a Local Interconnect Network (LIN) physical layer (LIN PHY). The S12ZVL(A)128/96/64 derivatives introduces several unique enhancements in comparison with older S12ZVL32/S12ZVL16 derivatives: Significantly bigger memories (64/96/128kB flash, 1/2kB EEPROM, and 4/8kB RAM) The VDDX voltage regulator is capable of providing 5V or 3.3V MsCAN module The S12ZVLA derivatives additional features/improvements: 2% VDDX regulator tolerance improvements 10/6 channel 12bit ADC 8bit DAC module the rail-to-rail analog comparator (ACMP) the Programmable Gain Amplifier (PGA) I am going to use the PGA for thermocouple measurement in the near future.   Software The Software Integration Guide guides us through CW 10.6.4 installation and creating a new project with Processor Expert (PE) tool. Unfortunately, while following that guide, I discovered that the CW10.6.4 does not offer PE as an option (only project without PE) when I tried to create an S12ZVL128 project. But this option is available in newer CW10.7 version. Note: If S12ZVL(A)128 derivative is missing in your CW10.6.4 IDE, please update your CW IDE via menu-Help-Install New Software-FSL MCU Eclipse Update Site and focus mainly on “S12Z Support” and “MCU 10.6.4 Updates” folders.   The code examples contains three primitive example projects: DEVKIT-ZVL128_Lab1GPIO – configure GPIO pins DEVKIT-ZVL128_Lab2ADC – initialize and measure ADC value DEVKIT-ZVL128_Lab3PWM – configure voltage regulator, initialize CLOCK, initialize and measure ADC value, generate PWM   Note: The zip file contains already built projects. The loading it into MCU does not work due to different paths. We have to clean it and build again in our workspace prior loading into the MCU.   These projects are really simple, but they omit some specific potential issues. For example: I would like to recommend to configure CPMUVREGCTL_VREG5VEN bit also in GPIO example since this bit influences output pin voltage levels. The value of the CPMUVREGCTL_VREG5VEN bit is not influenced by any MCU reset. So, we have to be careful especially when we are starting a new project with new peripherals connected to the S12ZVL128 GPIO pins. The ADC command lists (adc0_cmdlist) and ADC result lists (adc0_results) are not aligned in these example codes. It may be fixed by simple modification: volatile unsigned char adc0_cmdlist[1][4] __attribute__ ((aligned (4))) = {0xC0,0xD0,0xA0,0x00}; volatile unsigned short adc0_results[1] __attribute__ ((aligned (4)));‍‍‍‍ The NXP offers for this MCU also LIN2.x and SAE J2602 Stack and S12Z NVM Standard Software Driver (Flash/EEPROM driver).   There are also well-documented example codes at Community from Technical support team which may be used for an inspiration. For example: S12ZVM clock module and PLL configuration - SW examples S12Z Interrupt catcher for unexpected interrupts S12Z voltage measurement A Library of Functions for HD44780 Based LCD Modules (no R/W) for S12Z devices S12ZVL-TIM-FrequencyMeasurement S12Z Flash example code S12Z EEPROM example code …   The next source of information may be NXP application notes. For example: AN4723 S12Z MagniV Bootloader with SW, AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers, AN4841 S12ZVL LIN Enabled Ultrasonic Distance Measurement with SW, AN4842 S12ZVL LIN Enabled RGB LED Lighting Application with SW, AN5084 Hardware Design Guidelines for S12ZVL Microcontrollers, AN5122 Using Freescale’s LIN Driver with the MagniV Family with SW   Summary One of the best advantages of DEVKIT platform is the price. When we compare DEVKIT board prices with alternative evaluation boards (if any exist), we may save between 40 and 95 % EVB price depending on target MCU family. For example, the older TRK-S12ZVL board (assembled by S12ZVL32) is bigger, additionally offers 9 user switches, buzzer, HVI potentiometer, switchable LIN_OUT connector and header ring with all MCU pins. But the price is also almost three times higher than the price of DEVKIT-ZVL128. Also, the connectors with standard 100mils pitch are definitely plus in comparison with previously used TWRPI/PCI EXPRESS connectors and the board allows using plenty of available Arduino shields without complex hardware interconnections. You may look for it for example at Arduino pages, shieldlist.org, Adafruit, …   From my side - thumbs up :smileycheck:.
記事全体を表示
AN12086 Simple Serial Bootloader for S12Z AN12086 SW     AN5330 Migration Guide for S12ZVM Devices AN5330       AN5327 Three-phase Sensorless Single-Shunt Current-Sensing PMSM Motor Control Application with MagniV MC9S12ZVM AN5327       AN5264 Emulating I2C Master Mode AN5264 SW     AN5207 Hardware Design Guidelines for S12ZVM Microcontrollers AN5207       AN5190 S12ZVM Derivatives Configuring PMF Module AN5190 SW     AN5168 Using the ADC Module in S12ZVM AN5168 SW     AN5135 3-phase Sensorless PMSM Motor Control Kit with MagniV MC9S12ZVM AN5135       AN5122 Using Freescale’s LIN Driver with the MagniV Family AN5122 SW     AN5084 Hardware Design Guidelines for S12ZVL Microcontrollers AN5084       AN5082 MagniV in 24V Applications AN5082       AN4975 Using MSCAN on the MagniV Family AN4975 SW     AN4912 Tuning 3-Phase PMSM Sensorless Control Application Using MCAT Tool AN4912       AN4867 Hardware Design Guide lines for S12ZVC AN4867       AN4852 Using the SENT Transmitter Module in S12ZVC Devices AN4852 SW     AN4842 S12ZVL LIN Enabled RGB LED Lighting Application AN4842 SW     AN4841 S12ZVL LIN Enabled Ultrasonic Distance Measurement AN4841 SW     AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers AN4731       AN4723 S12Z MagniV Bootloader AN4723 SW     AN4722 Real Time Counter (RTC) on the S12ZVH Family AN4722       AN4721 S12ZVH: Hardware Design Guidelines AN4721       AN4718 3-Phase BLDC Hall Sensor Application Using S12ZVM AN4718 SW     AN4704 3-phase Sensorless BLDC Motor Control Kit with the S12 MagniV MC9S12ZVM AN4704       AN4680 PMSM Electrical Parameters Measurement AN4680       AN4643 S12VR - Hardware Design Guidelines AN4643       AN4642 Motor Control Application Tuning (MCAT) Tool for 3-Phase PMSM AN4642       AN4618 Sensorless BLDC Motor Control Using S12G240 Based on HVAC Platform AN4618       AN4617 HMI Design Using HVAC Platform AN4617       AN4616 Flap Motor Control Based On HVAC Platform AN4616       AN4558 3-phase Sensorless BLDC Motor Control Development Kit with MC9S12G128 MCU AN4558 SW     AN4540 Comparison Between the MC9S12VR and MM912_634 AN4540       AN4506 Software Analysis in CodeWarrior for MCU AN4506       AN4505 Safety Considerations S12G-Family AN4505       AN4483 Emulated EEPROM Routines for the S12P Family AN4483 SW     AN4455 MC9S12G128_A240 Demonstration Lab Training AN4455 SW     AN4448 MC9S12VR Family Demonstration Lab Training AN4448 SW     AN4418 MC9S12G64 Demonstration Lab Training AN4418 SW     AN4388 Quad Flat Package (QFP) AN4388       AN4364 Glucose Meter Fundamentals and Design AN4364 SW     AN4320 Introduction to the 16-bit Tower Boards Using the MC9S12GN32 AN4320       AN4303 Light control and diagnostics using a MC9S12GN32 MCU AN4303 SW     AN4302 Introduction to the S12G Family EEPROM AN4302 SW     AN4283 Migrating Software Applications from the S12 (XEXSP) and S08 to S12G Microcontrollers AN4283       AN4268 Three-phase Sensorless BLDC Motor Control Kit with the Qorivva MPC5604P AN4268       AN4263 Modification of the eGUI (D4D) Driver for char Displays (D4CD) AN4263 SW     AN4258 Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Technology AN4258 SW     AN4236 MC9S12XHY-Family Demonstration Lab Training AN4236 SW     AN4143 Migrating from the 16-bit S12XE to 32-bit MPC5604B Family of Microcontrollers AN4143       AN4058 BLDC Motor Control with Hall Effect Sensors Using the 9S08MP AN4058       AN4024 High Speed Stall Detection on the S12HY Family AN4024 SW     AN4021 MC9S12HY-Family Demonstration Lab Training AN4021 SW     AN3961 EEPROM Emulation for the MC9S12XS and MC9S12P Families Using AN2302 as a Reference AN3961 SW     AN3937 MC9S12P-Family Demonstration Lab Training AN3937 SW     AN3936 How to install and run Classic CodeWarrior products on 64-bit Windows 7 PC AN3936       AN3832 Sensorless BLDC Motor Control Using MC9S08AC16 AN3832 SW     AN3784 Understanding the Memory Scheme in the S12(X) Architecture AN3784       AN3743 Emulated EEPROM Quick Start Guide AN3743       AN3624 S12X Temperature Sensor AN3624       AN3622 Comparison of the S12XS CRG Module with S12P CPMU Module AN3622       AN3613 Using the MC9S12XS Family as a Development Platform for MC9S12P Family AN3613       AN3589 Optically-Isolated Multilink BDM Interface for the S08-S12 Microcontrollers AN3589       AN3555 Investigating XGATE Software Errors AN3555       AN3510 S12HZ and S12XHZ Family Compatibility AN3510       AN3497 S12XS Family Compatibility Considerations AN3497       AN3493 TFT display AN3493 SW     AN3490 Overview of the MC9S12XE Emulated EEPROM AN3490       AN3469 S12 and S12XE Family Compatibility AN3469       AN3458 Debugging XGATE Code AN3458       AN3419 System Integrity Techniques for the S12XE AN3419       AN3391 LFAE Bootloader Example and Interface for use with AN2546 (CAN bootloader for S12XE) AN3391       AN3333 Implementing CAN and LIN Signal Level Gateway AN3333 SW     AN3330 Introduction to the Stepper Stall Detector Module AN3330 SW     AN3328 HCS12XD Family Compatibility Considerations AN3328       AN3327 Using the S12XE-Family as a Development Platform for the S12XS-Family AN3327       AN3300 General Soldering Temperature Process Guidelines AN3300       AN3298 Solder Joint Temperature and Package Peak Temperature AN3298       AN3292 XGATE Library SCI Emulation AN3292 SW     AN3291 How to Use IIC Module on M68HC08, HCS08, and HCS12 MCUs AN3291       AN3289 Low-Power Techniques for the S12X Family AN3289       AN3275 S12 All-Access Bootloader for the HCS12 Microcontroller Family AN3275 SW     AN3262 Designing Hardware for the HCS12X D-Family AN3262       AN3257 Meeting IEC 60730 Class B Compliance with the MC9S08AW60 AN3257       AN3253 XGATE Library Load Measurement AN3253 SW     AN3242 S12XD and S12XE Family Compatibility AN3242       AN3226 XGATE Library ATD Average AN3226 SW     AN3225 XGATE Library PWM Driver AN3225 SW     AN3224 Tutorial Introducing the XGATE Module to Consumer and Industrial Application Developers AN3224       AN3219 XGATE Library TN STN LCD Driver AN3219 SW     AN3208 Crystal guide AN3208       AN3153 USB - HID - ZSTAR AN3153 SW     AN3145 XGATE Library Using the Freescale XGATE Software Library AN3145       AN3144 Using XGATE to Implement a Simple Buffered SCI AN3144 SW     AN3034 Using MSCAN on the HCS12 Family AN3034 SW     AN3031 Temperature Sensor for the HCS08 Microcontroller Family AN3031 SW     AN3015 Using the XGATE for Manchester Decoding AN3015 SW     AN2974 Quick Start for Beginners to Drive a Stepper Motor AN2974       AN2881 Mapping Memory Resources on HCS12 Microcontrollers AN2881       AN2880 Using Backdoor Access Capability to Unsecure HCS12 MCUs AN2880 SW     AN2836 Web Server Development with MC9S12NE64 and OpenTCP AN2836 SW SW2 SW3 AN2764 Improving the Transient Immunity Performance of MCU-based Applications AN2764       AN2759 Implementing an Ethernet Interface with the MC9S12NE64 AN2759 SW     AN2734 HCS12X Family Memory Organization AN2734       AN2732 Using XGATE to Implement LIN Communication on HCS12X AN2732       AN2727 Designing Hardware for the HCS12 D-Family AN2727       AN2726 XGATE Library CAN Driver AN2726 SW     AN2724 Using the HCS12X PIT as a 24-bit Elapsed Timer AN2724       AN2720 A Utility for Programming Single FLASH Array HCS12 MCUs, with Minimum RAM Overhead AN2720 SW SW2   AN2708 An Introduction to the External Bus Interface on the HCS12X AN2708       AN2700 Basic Web Server Development with MC9S12NE64 and CMX-MicroNetT TCP-IP Stack AN2700 SW     AN2692 MC9S12NE64 Integrated Ethernet Controller AN2692       AN2685 How to Configure and Use the XGATE on S12X Devices AN2685       AN2678 Using the HCS12 NVM Standard Software Drivers with the Cosmic Compiler AN2678       AN2624 Basic Web Server Development with the CMX-MicroNet TCP-IP Stack AN2624 SW     AN2617 A Software Piority Interrupt Scheme on HCS12 Microcontrollers AN2617 SW     AN2615 HCS12 and S12X Family Compatibility AN2615       AN2612 PWM Generation Using HCS12 Timer Channels AN2612 SW     AN2597 Using the MC9S12E128 to Implement an IrDA Interface AN2597 SW     AN2573 LINkits LIN Evaluation Boards AN2573       AN2554 Clearing and Disabling Interrupt Flags AN2554       AN2552 Configuring the System and Peripheral Clocks in the MC9C12E128 AN2552 SW     AN2548 Serial Monitor Program for HCS12 MCUs AN2548 SW     AN2546 HCS12 Load RAM and Execute Bootloader User Guide AN2546 SW     AN2485 HCS12 Software Stationery AN2485 SW     AN2461 Low Power Management using HCS12 and SBC devices AN2461       AN2438 ADC Definitions and Specifications AN2438       AN2434 Input-Output Pin Drivers on HCS12 Family MCUs AN2434       AN2433 5V to 3V Design Considerations AN2433       AN2429 Interfacing to the HCS12 ATD Module AN2429       AN2428 An Overview of the HCS12 ATD Module AN2428       AN2408 Examples of HCS12 External Bus Design AN2408       AN2400 HCS12 NVM Guidelines AN2400       AN2396 Servo Motor Control Application on a LIN AN2396 SW     AN2342 Opto Isolation Circuits For In Circuit Debugging of 68HC9(S)12 and 68HC908 Microcontrollers AN2342       AN2321 Designing for Board Level Electromagnetic Compatibility AN2321       AN2318 Using the I2C Bus with HCS12 Microcontrollers AN2318 SW     AN2304 Implementation of a UDP-IP (User Datagram Protocol) Stack on HCS12 Microcontrollers AN2304 SW     AN2302 EEPROM Emulation for the MC9S12C32 AN2302 SW     AN2295 Developer's Serial Bootloader for M68HC08 abd HCS08 MCUs AN2295       AN2287 HCS12 External Bus Design AN2287       AN2283 Scalable Controller Area Network (MSCAN) Interrupts AN2283       AN2263 PC Master Software: Creation of Advanced Control Pages AN2263       AN2255 MSCAN Low-Power Applications AN2255       AN2250 Audio Reproduction on HCS12 Microcontrollers AN2250 SW SW2 SW3 AN2221 MI Bus Software Driver for the MC9S12DP256 AN2221 SW     AN2216 MC9S12DP256 Software Development Using Metrowerk's Codewarrior AN2216       AN2213 Using Cosmic Software's M68HC12 Compiler for MC9S12DP256 Software Development AN2213       AN2204 Fast NVM Programming for the MC9S12DP256 AN2204 SW     AN2201 Low Battery Cranking Pulse in Automotive Applications AN2201       AN2189 Using the Clock Generation Module on the HC12 D Family AN2189       AN2153 A Serial Bootloader for reprogramming the MC9S12DP256 FLASH Memory AN2153 SW     AN2104 Using Background Debug Mode for the M68HC12 Family AN2104       AN2103 Local Interconnect Network (LIN) Demonstration AN2103       AN2011 The MSCAN on the MC9S12DP256 compared with the MSCAN on the HC12 family AN2011       AN1954 MPXY8000 Series Tire Pressure Monitoring Sensor AN1954       AN1837 Non-Volatile Memory Technology Overview AN1837       AN1798 CAN Bit Timing Requirements AN1798       AN1783 Determining MCU Oscillator Start-up Parameters AN1783       AN1775 Expanding Digital Input with an AD converter AN1775       AN1771 Precision Sine-Wave Tone Synthesis Using 8-Bit MCUs AN1771       AN1716 Using M68HC12 Indexed Indirect Addressing AN1716       AN1705 Noise Reduction Techniques for Microcontroller-Based Systems AN1705       AN1284 Transporting M68HC11 Code to M68HC12 Devices AN1284       AN1280 Using and Extending D-Bug12 Routines AN1280       AN1263 System Design and Layout Techniques with Single-Chip Microcontrollers AN1263       AN1259 System Design and Layout Techniques for Noise Reduction in MCU-Based Systems AN1259       AN1058 Reducing A_D Errors in Microcontroller Applications AN1058       AN1051 Transmission Line Effects in PCB Applications AN1051       AN1050 Designing for Electromagnetic Compatibility (EMC) with HCMOS Microcontrollers AN1050       AN5389 S12Z MagniV LIN Bootloader AN5389 SW     AN11967 S12ZVM Family in 48 V Applications AN11967      
記事全体を表示
Officially we offer two S12ZVM motor control kits: MTRCKTSBNZVM128: 3-phase Sensorless BLDC Development Kit with S12 MagniV S12ZVM MTRCKTSPNZVM128: 3-phase Sensorless PMSM Development Kit with S12 MagniV® MC9S12ZVML128 MCU     In fact, the kit contents are the same - S12ZVML12EVBLIN board and LINIX 45ZVN24-90 motor. The LINIX motor is BLDC type, but their characteristics are rather close to the PMSM type. So, the difference is just in used software and jumper settings.   Since the current web pages are slightly confused, I would like to place here links for the main 4 types of software for MTRCKTSBNZVM128 and MTRCKTSPNZVM128 kits.   3-Phase Sensorless BLDC S12ZVM Application – six step driving https://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVM128QSG.pdf https://www.nxp.com/docs/en/application-note/AN4704.pdf https://www.nxp.com/webapp/Download?colCode=MTRCKTSBNZVM128_SW&appType=license    3-Phase Hall Sensor BLDC S12ZVM Application – six step driving https://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVMHQSG.pdf https://www.nxp.com/docs/en/application-note/AN4718.pdf https://www.nxp.com/docs/en/application-note-software/AN4718SW.zip   3-phase Sensorless Dual-Shunt PMSM S12ZVM Application – FOC driving https://www.nxp.com/docs/en/user-guide/MTRCKTSPNZVM128QSG.pdf https://www.nxp.com/docs/en/application-note/AN5135.pdf https://www.nxp.com/webapp/Download?colCode=MTRCKTSPNZVM128-SW&appType=license    3-phase Sensorless Single-Shunt PMSM S12ZVM Application – FOC driving https://www.nxp.com/docs/en/user-guide/AN5327-QSG.pdf Note: please be aware that there is still typo error in this document (already reported) – the jumpers J57 and J60 should be in position 2-3. https://www.nxp.com/docs/en/application-note/AN5327.pdf https://www.nxp.com/docs/en/application-note-software/AN5327SW.zip   EDIT: Additionally, we may use a cost-effective S12ZVM Mini Board or Mini Kit evaluation platform. The software refers to the above mentioned, but with small modification for S12ZVML-MINBRD board.    I hope it helps you.
記事全体を表示
Since there isn't a CAN based bootloader developed for S12X device family, here are some useful documents that might be of help for creating such bootloader:   - The AN3312 is an application note of a BootLoader that uses CAN but it is targetted for our DSC family of devices. These devices have the FlexCAN module (the silicon that handles CAN Communications is different to the one in the MC9S08DZ60). However this document can be used as a reference on how to build a loader. https://www.nxp.com/docs/en/application-note/AN3312.pdf    - Following document explains how to use the msCAN module for communications. It provides basic examples on how to send and receive data through the port. https://www.nxp.com/docs/en/application-note/AN3034.pdf    - Next document provides the source code and documentation for an assembly-written Bootloader. This software loads the code through the serial port and burns it into flash. This document can help you understand the specific details of the bootloader implementation. This code is available for a lot of S08 families included the MC9S08DZ60 device. https://www.nxp.com/docs/en/application-note/AN2295.pdf  - Serial booloader for S12(X) family: https://www.nxp.com/docs/en/application-note/AN4258.pdf    With the information in these documents you can design your loader and plan how to solve the 5 main challenges of a loader application:   ++Memory Protection++ The Boot Loader handles the non-volatile memory of the microcontroller. The developer must plan how much memory is needed for the loader and protect it. Memory protection provides a guideline of the final system memory organization. A section of memory is used for the loader and another section for the application. Applications that will be executed with a loader are affected by how the loader manages memory and interrupt vectors.   ++Burning Flash++ Programming and Erasing non-volatile memory requires special attention as the procedure must be executed in RAM. The process of handling NVM may vary between devices. We have source code that provides routines to write Flash and that solves the problem of executing in RAM.   ++Vector Redirection+ Interrupt vectors should be shared between the application and the users code. Hardware vector redirection is supported by the microcontrollers but with some limitations. It is necessary to decide how vector redirection will be implemented. Software and hardware methods can be used to redirect vectors.   ++Data Interface++ Different applications required different interfaces to receive s-record information. Serial Ports are used widely for this purpose although the bootloader implementation should allow exchanging interfaces in a simple way. For your case you want CAN interface. CAN frames support up to 8 bytes of data per frame. This requires the developer to fully design a protocol or a data structure mounted over the CAN frames to be able to send the complete frames to the device that will be reprogrammed.   ++Mode Selection++ The Boot Loader is the owner of the reset vector. Upon startup the Boot Loader should select if the User code will be executed or if the Boot Loader mode should execute. The applicaton determines the best way to select between User/Loader mode. It might be a simple GPIO or a CAN frame or any input that can be recognized by the application and Loader to be able to set the loader mode when needed. Developing a loader is not easy, but hopefully this information will be of a great help.
記事全体を表示
S12(X) MCU Secure: There’s a security byte in the flash memory at address 0xFF0F that should be programmed appropriately. Datasheet says: “The contents of the Flash Protection/Options byte at $FF0F in the Flash Protection/Options Field must be changed directly by programming $FF0F when the device is unsecured and the higher address sector is unprotected. If the Flash Protection/Options byte is left in the secure state, any reset will cause the MCU to return to the secure operating mode.”   If you use CodeWarrior then you can use the syntax as follows: const unsigned char secure @0xFF0F = 0xFC;   If the security is enabled then: - internal flash memory cannot be read via BDM device. - debug features are disabled. For more information see the description of FSEC register in datasheet.   I would like also recommend our application note AN2400 HCS12 NVM Guidelines: http://www.freescale.com/files/microcontrollers/doc/app_note/AN2400.pdf AN2880 Using the Backdoor Access Capability to Unsecure HCS12 MCUs: http://www.freescale.com/files/microcontrollers/doc/app_note/AN2880.pdf http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2880SW     Security at S12(X) MCUs with 180nm Flash: This is related to all S12(X) MCUs with 180nm Flash with ECC (S12G, S12HY, S12P, S12XE, S12XF, S12XHY,  S12XS, MM912G634, MM912H634, MM912J637 and S12VR):   If we load the flash security byte together with other code, ****************** c code example: //set backdoor key and secure the flash (set flash security byte to 0xBD): const unsigned char flash_array[] @0xFF00 = {0xAA,0xAA,0xAA,0xAA,0xAA,0xAA,0xAA,0xAA,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xBD}; ****************** then we have to add following command to preload command file (P&E_Multilink_USB_Preload.cmd if you use PE Multilink):   FLASH NOUNSECURE   This command will ensure that the burner will not change security byte to unsecured state prior to programming. That's normal way: the MCU is erased, flash security byte is programmed to default unsecure state (0xFE) and then the code is loaded. We just have to turn off the programming of security byte.   Why: The cumulative bits within the phrase is not allowed. If the flash security byte at address 0xFF0F is not erased prior to programming of the new value then the ECC checksum of this phrase is corrupted and the MCU will be left in secured state and the flash will be fully protected after next reset.   Datasheet says: "If a double bit fault is detected while reading the P-Flash phrase containing the P-Flash protection byte during the reset sequence, the FPOPEN bit will be cleared and remaining bits in the FPROT register will be set to leave the P-Flash memory fully protected."   "If a double bit fault is detected while reading the P-Flash phrase containing the Flash security byte during the reset sequence, all bits in the FSEC register will be set to leave the Flash module in a secured state with backdoor key access disabled."   The same for D-Flash...   S12(X) unsecure: Unsecure is possible by three ways: 1. Backdoor key access(temporary) 2. Reprogramming the security bits 3. Complete memory erase (special modes) Ad1) For secure and backdoor key you set 16bytes on address 0xFF00. The backdoor key access method allows debugging of a secured microcontroller without having to erase the Flash. This is particularly useful for failure analysis. For unsecure by backdoor key you use special flash command 0C (caption Verify Backdoor Access Key Command in reference manual). No word of the backdoor key is allowed to have the value 0x0000 or 0xFFFF. Unsecure is valid only till reset. If an invalid attempt is made to verify the Backdoor Keys the command will be locked out until a power down occurs.  Ad2) In normal single chip mode (NS), security can also be disabled by erasing and reprogramming the security bits within Flash options/security byte to the unsecured value. Because the erase operation will erase the entire sector from 0xFE00–0xFFFF, the backdoor key and the interrupt vectors will also be erased; this method is not recommended for normal single chip mode. Ad3) Complete mass erase by BDM device(in special mode). In Code Warior debugger menu ->MultilinkCyclonePro->Unsecure… If not work you can use unsecure12 from P&E: http://www.pemicro.com/downloads/download_file.cfm?download_id=16 Unsecure_12 Help Files: http://www.pemicro.com/downloads/download_file.cfm?download_id=14 Note: For downloading is necessary registration.
記事全体を表示
Example code pack for S12G contains simple code examples how to initialize and how to use MCU module/feature. List of examples: G128-API_wakeup_from_Stop_Mode G128-Clock and COP examples G128-Interrupt_catcher-CW51 G128-LIN-CW51 G128-PLL_PEEmode-CW51 G128-Security-CW51 G240-API+STOP-CW51 G240-API-CW51 G240-ATD+GPIO-CW51 G240-ATD-Continuous_conversion_with_interrupt-CW51 G240-ATD-Multichannel_single_conversion-CW51 G240-ATD-Single_conversion-CW51 G240-Checksum-CW51 G240-Flash-CW51 G240-PLL-PBE_mode-CW51 G240-PLL-PEE_mode-CW51 G240-PLL-PEI_mode-CW51 G240-TIM_50us_interval-CW51 G240-TIM_50us_period-CW51 GN32-EEPROM-EW-CW51 GN32-LIN-CW51 GN32-PWM16b_GPIO GN32-PWM_8bit-CW51 GN32-SCI_SPI_Gateway-CW51 GN32-SCI_wake_up_from_stop-CW51   Oct-22-2013 Update: I added G128-CAN-CW51, G240-SPI-MC33810-CW51, G240-SPI-Slave examples. I added PLL calculator. I fixed error in GN32-EEPROM-EW-CW51 example code.   Aug-21-2015 Update: Updated G240-Flash-CW51 example code. Removed image files and object code from projects (9MB->2MB size)
記事全体を表示
This application note was already officially released. Please, download it from: AN12086 Simple Serial Bootloader for S12Z AN12086SW software package    1.  Introduction This application note covers the operation and use of a simple serial Bootloader for the S12Z microcontroller families. The Bootloader can be a convenient way to support programming during production or “in-system”, where support for the dedicated HCS12 Background Debug interface (BDM) may not be available. Users must pre-program the S12Z MCU with the Bootloader during production or at a programming vendor. The Bootloader should reside in the MCU for further use. This Bootloader implementation allows User Application software to be downloaded into the MCU flash and EEPROM memory using the SCI serial interface. The Bootloader may be also configured for self-update similar way as a User Application software update. This Bootloader is originally based on AN4258 Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Technology with several modifications and improvements. The Bootloader described in this document is only an example and comes with no guarantees and no direct support.   2. Bootloader Overview The software architecture consists of two independent software projects: Bootloader Project User Application Project For avoiding compatibility issues between these projects, the minimum interface points must be kept. The switching between Bootloader and User Application codes is managed through MCU reset. So, the Bootloader and application are not limited by write-once registers. The Bootloader Project itself contain small user-defined dispatcher code which is executed directly after MCU reset and decide whether Bootloader or User Application will be executed as next. Figure 1 Software Architecture   2.1.     Hardware Compatibility The Bootloader is written for S12Z derivatives (S12ZVM, S12ZVMB, S12ZVMA, S12ZVC, S12ZVL, S12ZVH, S12ZVHY and S12ZVFP). The Bootloader for S12Z microcontrollers is not optimized for the smallest derivatives. Therefore, S12ZVL8 derivative (only 512B RAM) is not supported and only some of derivatives (with 4kB or more RAM) supports Bootloader self-update feature (rewritable).   2.2.     Dispatcher code The Dispatcher code is executed right after MCU reset. It just temporary initializes stack (write stack pointer) and directly executes user code for testing conditions whether Bootloader code should be executed or not. The most typical testing conditions for Bootloader presents: pushed button some specific value in the EEPROM memory waiting loop for command via the communication interface If User Application code is already loaded and Bootloader was not selected, the User Application is automatically started.   2.3.     Serial interface All S12Z microcontrollers include an on-chip serial communication interface. Notice that the RS-232 or USB to TTL level shifter is necessary to communicate with PC. Optionally, the virtual COM port at OSBDM interface may be used. By default, the serial communication is set to format: 8-data bit one start bit one stop bit no parity Xon / Xoff flow control Default baud rate is configured in Config.h file. The baud rate can be changed via the Bootloader’s menu to 38400, 57600, or 115200 bps. The Bootloader implementation currently assumes using just one of SCI channels. However, this may be changed by Bootloader code modification. The same approach may be used for a different type of channel implementation like CAN or LIN.   2.4.     PC software interface A general terminal emulation program like Microsoft HyperTerminal, Tera Term, RealTerm or similar software can be used on a PC to communicate with a microcontroller. A terminal emulation program must support communications over serial COM ports, Xon / Xoff flow control, and it must be able to send a text file.   3.  Functional Description The operation of the Bootloader is straightforward. This section describes only the most important and specific points. Figure 2 Memory map 3.1.     Bootloader Project Folders The C language codes and appropriate header files are located in Sources and Project_Header folders. The exception is Dispatcher.c and start12z.c files located in Project_Settings\Startup_Code folder. The linker file is located in Project_Settings\Linker_Files folder. The FLASH folder contain generated files like elf, map or s19 files. The SRecCvt folder contains a SRecCvt.exe tool for re-formating generated S-record file. The content of Documentation folder should help you in guide how to use this Bootloader. Figure 3 Bootloader Project Folders 3.2.     Bootloader Configuration The most of the Bootloader configuration settings are collected in Config.h file.   If the modified Bootloader will use any derivative specific registers, the mc9s12zvl128.h and mc9s12zvl128.c files should be replaced with appropriate files from CodeWarrior folders: "c:\Freescale\CW MCU v10.7\MCU\lib\wizard_data\S12Z\DataBase\device\include\.." and "c:\Freescale\CW MCU v10.7\MCU\lib\wizard_data\S12Z\DataBase\device\src\.."  And followed by modification of derivative.h file.   The Config.h contains settings for: Bootloader feature configuration Clock settings SCI module settings Dispatcher definitions MCU derivative configuration and addresses Flash Configuration Field configuration   The Bootloader-persistent.prm and Bootloader-rewritable.prm linker files contain definitions of Flash and RAM ranges for Bootloader. The appropriate linker file is selected by Build Configuration. Figure 4 Build Configuration   3.2.1.     Bootloader features SECURE_MCU: The MCU may be secured after Bootloader loading (default 0 = MCU unsecured) USE_BACKDOOR_KEY: The Flash Configuration Field may already contain Backdoor Key for temporary unsecure of MCU (default 0 = backdoor key 0xFFFF FFFF FFFF FFFF). WRITE_EEPROM: When enabled, the Bootloader menu offers an option for erasing EEPROM and program option will be able to program both Flash and EEPROM. BOOTLODER_REWRITABLE: When enabled, the Bootloader code is automatically loaded into RAM and allow unprotect, erase and program Bootloader Flash area. This variable is already defined differently in used Build Configurations. That allows us to keep BOOTLODER_REWRITABLE value and selected linker file synchronized.   3.2.2.     Serial Channel The current S12Z MCU derivatives offer up to 2 SCI channels. The SCI_MODULE defines whether SCI0 or SCI1 will be used for Bootloader communication (default SCI1). The DEFAULT_BAUDRATE specifies default SCI baud rate for initial Bootloader menu display (default Baud9600: 9600bps). The baud rate can be changed via the Bootloader’s menu to 38400, 57600, or 115200 bps. The S12Z MCU derivatives offer routing options for SCI0, SCI1, and other peripherals channels. The BL_MODRR0 value defines MODRR0 value loaded by Bootloader code after a reset.    Note: The MODRR0 values may be written just once in normal mode and cannot be changed until next MCU reset.   3.2.3.     Configure Dispatcher code The default Dispatcher condition is based on the testing value of pin with push button. The PUSH_BOTTON defines tested port and pin (default PTP_PTP1) while PB_ACTIVE_LEVEL defines active logic level – when the push button is pressed (default 0 = push button to GND with pull-up). The BL_REQUEST_ADD defines tested address (default 0x100000) while BL_REQUEST_VALUE defines active value for bootloader request key. When the memory content fits to the BL_REQUEST_VALUE, Bootloader code is executed (default "BOOT" in ASCII = 0x424F4F54).   3.2.4.     Configure Derivative and addresses The FLASH_START_ADD, EEPROM_START_ADD, EEPROM_END_ADD defines MCU derivative memory ranges. The BOOTLOADER_START_ADD value is automatically obtained from linker file (ROM segment start). The Bootloader automatically move User Application reset vector to the APPLICATION_RESET_VEC_ADD address (default BOOTLOADER_START_ADD-4 = placed to the end of User Application flash area)   3.2.5.     Configure Flash Configuration Field The bytes from BACKDOOR_KEY_0 to BACKDOOR_KEY_7 defines Backdoor Comparison Key (default "UNSECURE" = 0x554E534543555245 in ASCII). The bytes PROTECTION_OVERRIDE_KEY_H and PROTECTION_OVERRIDE_KEY_L defines Protection Override Comparison Key (default "AB" = 0x4142 in ASCII). The Bootloader code should be protected against unwanted erase/rewrite operations. Trying to alter data in any protected area in the P-Flash memory will result in a protection violation error and the FPVIOL bit will be set in the FSTAT register. Flash protection scheme allows protecting 2, 4, 8 or 16KB from upper range of Flash memory. The BL_FPROT defines FPROT value automatically loaded from Flash Configuration Field after reset (default 0xD7 = upper 8kB of P-Flash protected.). The BL_DFPROT defines DFPROT value automatically loaded from Flash Configuration Field after reset (default 0xFF = EEPROM unprotected). The initial configuration of COP watchdog and GDU (S12ZVM derivatives) is given by FOPT register value. The BL_FOPT defines FPROT value automatically loaded from Flash Configuration Field after reset (default 0xFF = COP is not active after reset).   3.2.6.     Bootloader linker file Since the preprocessor functionality is no longer supported directly in prm linker file, the Bootloader use two versions of linker file: Bootloader-persistent.prm Bootloader-rewritable.prm The linker file selection is managed by two Build Configurations (Figure 4 Build Configuration).   3.3     Operation The Bootloader handles reset vector. After reset, the Bootloader’s Dispatcher routine is called. As a first step, the Dispatcher initialize stack and reads the push button pin status. If the value of the pin is equal to the PB_ACTIVE_LEVEL, the Bootloader starts its operation. If the value of this pin is not equal to the PB_ACTIVE_LEVEL, the User Application’s reset vector is tested. If the reset vector of the User Application is not available (long word at address APPLICATION_RESET_VEC_ADD is in erased state = 0xFFFFFFFF) then the Bootloader is called anyway. The User Application is called only when User Application reset vector is already programmed and the condition for Bootloader enter is not true. The user can rewrite this code to start the Bootloader or User Application upon another condition. Note: Since this code is executed prior Bootloader/application startup code, the dispatcher code shouldn’t use any uninitialized global variables.   3.4.     Interrupt vector In the case when the User Application using interrupts, it is necessary to relocate the interrupt vector table using the IVBR register. The Bootloader resides in the upper 4/8/16kB fixed block at the address defined by linker prm file. This area is had to be protected (configured in Config.h), so the User Application cannot rewrite a default location of the interrupt vector table at 0xFFFE10-0xFFFFFF. The advantage of this solution is that the Bootloader cannot be affected by a power failure that could occur when rewriting User Application interrupt and reset vectors. The Bootloader automatically moves User Application’s reset vector from address 0xFFFFFD to the  APPLICATION_RESET_VEC_ADD address = typically the end of User Application’s flash area. Since this moving is managed by the Bootloader, the whole phrase (by default from (BOOTLOADER_START_ADD-8) to BOOTLOADER_START_ADD) must be excluded from User Application’s linker usage and the same sector (512B) shouldn’t be used for User Application’s interrupt vector table.   4.  User Guide This section describes the step-by-step procedure to use the Bootloader.   4.1.     Setup procedure for the Bootloader Open the Simple_Serial_Bootloader_for_S12Z project in CodeWarrior Development Studio for MCU. The Bootloader was tested in current versions v10.7. Select the Build Configuration as shown in Figure 4 Build Configuration. The Persistent Bootloader code option allows just update a User Application. The Bootloader Rewritable code option linker allows updating both User Application and Bootloader itself. Optionally edit appropriate linker file Optionally edit the Config.h header file per your target environment (required features, clocks, channels, derivative addresses, backdoor, and protection override keys). Optionally edit the c file with conditions for select User Application/Bootloader code execution.   4.2.     Bootloader Guide   1. Compile the project and download the Bootloader to the MCU via BDM device. Note: The correct derivative should be selected in debug configuration for successful complete MCU Flash erase and programming (Figure 5 Select derivative for Bootloader download). Figure 5 Select derivative for Bootloader download     2. Open the Microsoft HyperTerminal or any other serial terminal utility (e.g. Realterm, Tera Term,…). Set the baud rate 9600 bps, 1 start bit, 8 data bits, 1 stop bit, and flow control Xon / Xoff.   3. Make sure there is a serial (USB to Serial) cable connection between the PC and the board.   4. Hold the PUSH_BOTTON pin low and reset the MCU.   5. The Bootloader is started and the following response is received in HyperTerminal. See Figure 6 Initial screen.   Figure 6 Initial screen   6. Type “a” to erase the flash memory. This is not necessary the first time because the flash has been already erased by the BDM device.   7. Type “b” to program the flash.   8. Now send the desired S-record as a text file — See Figure 7 Send Text File. Browse for S-record which is downloaded to the MCU. For testing purposes, use demo S-records that are attached to this application note. The S-records must have a specified format. Refer to chapter 3 How to write a User Application and to chapter 4.4 How to convert S-Record that will be downloaded by the Bootloader. Figure 7 Send Text File     9. Confirm the dialog and the S-record are downloaded to the MCU. One printed star (*) means that one line of S-record has been programmed. See Figure 8 Download User Application. Figure 8 Download User Application   Note: If User Application contains any EEPROM data, please erase EEPROM by typing “h” prior the step 7. Note: If you want to reprogram Bootloader code, please use subsequently options “e” (it will ask you for entering protection override key), step “f” and step “g” instead steps 6 and 7.   4.3.     How to write a User Application You must ensure that the User Application does not interfere with Bootloader area defined by Bootloader linker file.   1. Create a new User Application project in CodeWarrior Development Studio for MCU.   2. Open the User Application project.prm file   3. Trim the high address of the segment ROM from the original to the (BOOTLOADER_START_ADD-8). For example, to the address 0xFFDFF7. This is because the area 0xFFDFF8–0xFFFFFF is occupied by the Bootloader and the area at address 0xFFDFF8–0xFFDFFF will be used for the User Application reset vector. If interrupts are used:   4. Trim the low address of the segment ROM from the original to (the original address + 0x200). This area will be used for the relocated interrupt vector table. Note: You may use any other Flash sector in User Application memory for that purpose except the last one (already used for the User Application reset vector). Note: The generated CodeWarrior project doesn’t show warning about memory overlapping between linker and user object placement. This warning is disabled by default (Linker option -WmsgSd1912).      5. Create a vector table as shown in the attached demo applications and set the IVBR register accordingly. The IVBR sets the interrupt vector table base address. It contains 15 most significant bits from 24bit vector table address.   4.4.     How to convert S-Record that will be downloaded by the Bootloader The default S12Z MCU project generated by CW10 does not generate a file with s-records automatically.   1. Check option for generating S-Record file in User Application project settings per Figure 9 Generate S-Record file The <YourProjectName>.sx file will be generated when you will build your project. Figure 9 Generate S-Record file For the simplifying, the Bootloader parser, only s-records with specific format are accepted. All records must be aligned to 32 bytes and the length of records must be 32 bytes.   2. Copy SRecCvt directory with SRecCvt.exe tool from Bootloader/Application Example project to your User Application project   3. Exter command “${ProjDirPath}/SRecCvt/sreccvt.exe -hc12 -m 100000 FFFFFF 32 -o ..\FLASH\\${BuildArtifactFileBaseName}.s19 ..\FLASH\\${BuildArtifactFileBaseName}.sx” as post build step into User Application project settings per Figure 10 Adding Post-build step. Figure 10 Adding Post-build step This command will load S-Records from your <YourProjectName>.sx file and create new <YourProjectName>.s19 file with reformatted S-Records when you build your project. Note: The complete SRecCvt utility may be downloaded from NXP web pages. Unfortunately, the graphical user interface doesn’t support directly S12Z derivatives. Therefore we use this tool in command line mode.   4.5.     How to merge the User Application and Bootloader The User Application can be developed independently, that is without the Bootloader. The User Application can be loaded into the microcontroller and can be debugged directly via the BDM device. However, for production purposes, it is worth merging the User Application and Bootloader together, so it can be downloaded into the microcontroller all at once as a single S-Record file. This is a recommended procedure:   1. Open the User Application that was created as per chapter 3, "How to write a User Application" in the CodeWarrior Development Studio for MCU.   2. Replace a User Application reset vector in Project.prm file from default address to the address (BOOTLOADER_START_ADD-3), so the Bootloader can use this vector for start User Application. For example: //VECTOR 0 _Startup VECTOR ADDRESS 0xFFDFFD _Startup   3. Copy the ready-mades19 file to ..\user_application_project\FLASH directory. Note: the s-record file can be renamed for example to the bootloader.s19.   4. Link this file to the User Application be using command at the beginning of Project.prm: HEXFILE Simple_Serial_Bootloader_for_S12Z.s19   5. Build the project. The final S-Record is ready to be downloaded into the microcontroller by the BDM interface.   5.  Testing The Bootloader and example application were tested on evaluation boards: DEVKIT-ZVL128 S12ZVMC256EVB S12ZVM32EVB S12ZVM-MINIBRD   6.  Content of Zip file All mentioned projects and utilities can be found in a zip file associated with this application note: Simple_Serial_Bootloader_for_S12Z — Bootloader project for S12Z microcontrollers. Application_Example_for_SSBZ — Projects that show how to write User Applications. Converted_srecords — S-Records was taken from Bootloader and Application Example that has been converted by the SRecCvt utility (*.s19 file extension). These S-Record files can be downloaded into the MCU by the Bootloader. SRecCvt — Utility for S-Record files converting.   7.  Reference AN4258 AN4258SW: Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Technology Rev 0. February 2011. S12Z Protection Override S12Z constant, variable, code allocation in CodeWarrior S12Z Interrupt catcher for unexpected interrupts S12Z Flash example code S12Z EEPROM example code   I hope it help you. Please let me know when you find any error or if something missing in this document.   Radek Sestak
記事全体を表示
Example code pack for S12X contains simple code examples that show how to initialize and how to use MCU module/feature.   List of examples: S12XE_PLL - include S12XE_iPLL_Calculator XDP512 - ECT measuring of period - CW45 XDP512-CAN – pack of several example codes include CAN baud rate calculator XDT256 - ECT Pulse Width - CW47 XEP100 - ATD + GPIO - CW47 XEP100 - ATD and PIT - CW47 XEP100 - ATD Continuous conversion with interrupt - CW4 XEP100 - ATD multichannel - CW46 XEP100 - ATD Single conversion - CW46 XEP100 - CAN0 - CAN1 - CW45 XEP100 - ECT 500us interval - CW47 XEP100 - ECT 500us period - CW47 XEP100 - ECT as PWM - CW47 XEP100 - PWM 8bit - CW45 XEP100 - SCI default - CW47 XEP100-SCI_change_Baudrate-CW51 XEP100-SPI-CW51.ZIP XEP100-SPI-Master-Slave XS128 - PIT - CW47 XS128 - PIT 10ms+15ms and priority - CW47 XS128 - PWM 16bit - CW47     Note: More examples for S12XE could be downloaded here: LAMA's S12XE unofficial examples
記事全体を表示
Here is the example code demonstrating erase/write/read of internal Flash module integrated into MagniV devices such as S12ZVM, S12ZVC, S12ZVL etc.   Find detailed description in the project's main.c file.   The example project was created in CodeWarrior IDE v10.6.4 and tested on TRK-S12ZVL board.
記事全体を表示
Here is the example code demonstrating erase/write/read of internal EEPROM module integrated into MagniV devices such as S12ZVM, S12ZVC, S12ZVL etc.   Find detailed description in the project's main.c file.   The example project was created in CodeWarrior IDE v10.6.4 and tested on TRK-S12ZVL board.
記事全体を表示
The ADC measurement is always relative – relative to your voltage reference. The most of the applications don't allow to use accurate and expensive voltage reference. In that case, VDDA is used as the reference for ADC measurement. Since the operational VSUP range starts from 3.5V and accuracy of the voltage regulator is limited, we should use internal bandgap reference for compensating ADC voltage results. The bandgap voltage VBG has a narrow variation over temperature and external voltage supply. The example shows how to compensate ADC results by additional bandgap voltage measurement.
記事全体を表示
CAN setup calculator for S12(X) and MagniV devices.   I would like to share my CAN setup calculator I've been using for a few years. I’ll be glad if anyone who sees any discrepancy in calculation or values would contact me with comment or idea for improvement. Even I think the sheet is intuitive I’ll provide a few notes. 1) Entering input values a) fosc – defines frequency of input clocks for CAN peripheral. It can be either oscillator clock or bus clock in dependence what is used in application. Note: Because of CAN clock requirements I suggest to use oscillator clock as a source clock for CAN peripheral to meet oscillator precision parameter. The recommendation is based on the fact of that the PLL is usually used for bus clock generation and the PLL unlock parameter is usually out of clock specification. Especially un-lock parameter which can be observed and processed by PLL lock interrupt. Only for example, S12ZVC defines:   b) Physical Interface Tx+ Rx propagation delay – The parameter can be calculated from the data presented in the data sheet for given CAN transceiver. A few values are presented in the top of the sheet.   c) Required sample point - A good general rule is to set the sample point above 80%. Based on the experiences of the automotive industry, the selected sample point should be near the 80% value.   2) Output values   The results field show calculations for all combinations. The simplification, I use, is the max SJW is always used.   Lines containing correct values for bitrate setup are highlighted with orange color. The only thing which is not checked is sample point. You should check calculated “Sample point calculated” whether it corresponds to your requirements. There are two correct values of CANBTR0 and CANBTR1 for required bitrate but the bottom orange line meets exactly our requirement for sample point.
記事全体を表示
Hello all, sharing the latest version of MagniV Power Dissipation Calculator started by Carlos Vazquez and Anita Maliverney. With this excel sheet is possible estimate the power dissipated for any MCU of S12ZVM, S12ZVL, S12ZC family, considering: supply voltages, digital modules, gate drive unit, charge pump, communication transceivers, etc.   A few features where added, any additional comment or suggestion is appreciated. Regards.
記事全体を表示
The bold blue links below provide direct download of SW example packs for MagniV devices based on S12Z core.   S12ZVC Getting Started Exercises (REV 1.0) This file contains four hands-on exercise where you can find basic setup code to enable a quick development in different areas. The file includes CodeWarrior projects demonstrating usage of peripheral modules such as: - Digital-to-Analog Converter (DAC), - Controller Area Network (CAN), - Pulse Width Modulation (PWM), - Timer (TIM).   Getting started with S12ZVL32 - S12 MagniV Example Codes (REV 0) The MC9S12ZVC device integrates a battery level (12V) voltage regulator and supply voltage monitoring. This zipped file includes four CodeWarrior examples demonstrating - Overcurrent protection on EVDD pin, - low power STOP mode with API timer and wake-up feature, - Pulse Width Modulation (PWM) - Serial Peripheral Interface (SPI) communication.   Many of these examples can be used on various MCU families across the MagniV product line. Check the appropriate device guide for list of modules and its versions.
記事全体を表示
The S12Z MCU has linear address space therefore constant, variable, code placement is easier in compare with older S12 or S12X MCUs. But still, there are several ways and potential issues.   The object placement is made by Smart Linker. The linker configuration is defined by settings in project *.prm file and also by linker command line options (menu - Project – Properties – C/C++ Build – Settings – S12Z Linker). The detail information about linker options may be found in MCU_Build_Tools_Utilities.pdf with default path: "c:\Freescale\CW MCU v10.7\MCU\Help\PDF\MCU_Build_Tools_Utilities.pdf"   We may define memory segments in *.prm linker file. The default prm file contains segments for RAM, EEPROM, and ROM (Flash). The sizes of these segments typically reflect our MCU derivative physical memory map, but we may redefine that and use more virtual segments per our needs. The physical/virtual segments definition in prm linker file is located at: SEGMENTS // segments definition END‍‍‍‍‍‍   The general data placement may be divided into two main approaches: Manual – the programmer will specify fix address for some of the data Automatic – the placement will be driven automatically by Smart Linker   Manual placement The first option is an exact specification of specific content at a specific address. This may be managed for a small amount of data by FILL linker command in *.prm linker parameter file. For example: SEGMENTS //… ROM_CONST       = READ_ONLY   0xFE0000 TO 0xFE0000 FILL 0x5A;  //insert 0x5A value at address 0xFE0000 //… END‍‍‍‍‍‍‍‍‍‍ Such placement isn’t very comfortable, but it might be simply used for some configuration data out of project code. Note: you may use more than one bytes (e.g. FILL 0x0A 0x34). If segment size is bigger than a number of specified bytes, the bytes will be used as a pattern for filling whole target segment. Note: The potential linker placement will overlap such defined data.   The next option is using address specification by an @ qualifier directly in C code. For example: unsigned const int rom_const @0xFE0100 = 0x5AA5;‍‍ This may be used also for more complex types than simple byte – typically arrays,...   Since such type of placement is still manual, the linker parameters must be configured for avoiding possible overlapping. Be aware! The default CW project has disabled memory overlapping warnings. So, we must exclude target memory area from linker using. For example, in the *.prm file: SEGMENTS //… ROM_1           = READ_ONLY   0xFE0000 TO 0xFE00FF //ROM_CONST  = READ_ONLY   0xFE0100 TO 0xFE0101;            //we use the 0xFE0100 byte for rom_const ROM_2           = READ_ONLY   0xFE0102 TO 0xFFFDFF //… END‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note: We use qualifiers for define memory access type. READ_ONLY is used for Flash, READ_WRITE for RAM and NO_INIT for RAM where we do not want to initialize data after reset. Sections placed in an NO_INIT segment should not contain any initialized variables (variable defined as int c = 8).   Note: The manual placement may be also implemented by assembler code. For example: XDEF MyVariable MyVariable: equ $1100‍‍‍‍ However, also in this case, we must exclude target memory area from linker use like in the case of @ qualifier for avoiding memory overlapping.   Automatic placement by linker The PLACEMENT block allows us to physically place each section from the application in a specific memory area (segment). The sections specified in a PLACEMENT block may be linker-predefined sections (like DEFAULT_ROM, DEFAULT_RAM, COPY, SSTACK,…) or user sections specified in one of the source file building the application (like MY_RAM,…). PLACEMENT // section(s) INTO segment(s); MY_CODE INTO ROM_1; END‍‍‍‍‍‍‍‍ Note: Since the linker is case sensitive, the name of the section names specified in the PLACEMENT block must be valid predefined or user-defined section names. Note: There is quite mess in ELF/Freescale section/segment terminology. Please take this information as simplified as possible. Please look at MCU_Build_Tools_Utilities.pdf for more details about predefined segments/sections. Note: We may place a various number of sections into a various number of segments. The “,” is used as section/segment delimiter. Note: In general, the placement order is given by simple list order (first specified section will be allocated from first specified segment, after that next section …). But, there are still few limitations for sections list order. The error is generated in the case of wrong list order – for example: ERROR L1122: only checksum section may be behind .copy in the section list.   The default variable/constant/code placement may be changed by #pragma commands. Note: Most of these pragma commands are not limited to the single file. Therefore, we should keep it in complementary pairs. An example of placing code into specific section: #pragma CODE_SEG MY_CODE void f(void) { //… } #pragma CODE_SEG DEFAULT‍‍‍‍‍‍‍‍‍‍‍‍ The #pragma DATA_SEG modifies variable placement. For example: #pragma DATA_SEG MY_RAM unsigned int counter; //… #pragma DATA_SEG DEFAULT‍‍‍‍‍‍‍‍   The #pragma CONT_SEG modifies variable placement. For example: #pragma CONT_SEG MY_ROM const unsigned int my_parameter; //… #pragma CONT_SEG DEFAULT‍‍‍‍‍‍‍‍   Note: The shorter option for directly allocating variables in a named segment, rather than using a #pragma may be used. For example: unsigned int counter@"MY_RAM";‍‍ However, even in such case, the #pragma command like #pragma DATA_SEG MY_RAM must be used at least once prior that variable declaration.   Note: The S12Z compiler/linker allows to use also already predefined sections like DEFAULT_ROM, DEFAULT_RAM or ROM_VAR as target sections in #pragma commands (not possible in the case of older S12(X) compiler/linker).     More details about #pragma commands may be found in MCU_S12Z_Compiler.pdf with default path: "c:\Freescale\CW MCU v10.7\MCU\Help\PDF\MCU_S12Z_Compiler.pdf" Data alignment Sometimes we need to keep allocated data aligned. This is for example typical requirement for ADC command and result list where DMA is used for transfer data between ADC module and memory. The simplest method is using alignment attribute. For example: volatile unsigned long adc0_cmdlist[NR_A_CH] __attribute__ ((aligned (4))); //max 256 bytes = 64 commands per 4-byte entries volatile unsigned int adc0_results[NR_A_CH] __attribute__ ((aligned (4)));  //max 128 bytes = 64 results per 2-byte entries‍‍‍‍ I hope it helps you. Best regards Radek
記事全体を表示
This example simulates ECC issue by cumulative write into the same EEPROM area without an erasing.   The EEPROM erase operation set all bits into log1. The EEPROM program operation may keep bit cells in log1 state or change it into log0 state, but not in opposite way.   The S12Z MCU EEPROM is protected by 22-Bit ECC Scheme. Every word (16bits) is protected by additional 6 bits with ECC checksum. The ECC values are not accessible for users. Every EEPROM reading triggers also ECC check by internal logic. The single bit error in user data may be corrected by ECC checksum. The double bit error cannot be corrected.   The ECC protection is implemented also at flash controller commands and results are signalling by MGSTAT bits.   The first case simulates Single-bit ECC error during reading. The MGSTAT bits after the second write are 0b10 due to fact that just 1 bit is different during write verification (correctable error)   The second case simulates Single-bit ECC error during reading. The MGSTAT bits after the second write are 0b11 due to fact that more than 1 bits are different during write verification (non-correctable error)   The third case simulates Double-bit ECC error during reading. The MGSTAT bits after the second write are 0b11 due to fact that more than 1 bits are different during write verification (non-correctable error)       The EEPROM patterns are selected for highlighted described behavior and they don't have any real meaning.   The cumulative write is not allowed for normal operation!!! The code from this example should be used only for design testing - not in production!!!   Please, see the prm file. Address range 0x100000-0x100001 is excluded from default EEPROM and is used as user EEPROM memory The size of EEPROM sectors is 2 bytes. The EEPROM_Program() function may program up to 4 words in single flash command.   Note: The EEPROM_Program() function was updated - erase verification is skipped     I hope it helps you. Radek
記事全体を表示
Customers are sometimes asking for reference schematics, so here is a batch of minimal configurations for main representatives of S12(X) family. Attached is also document that should answer most common questions. Hope this will help. Lukas
記事全体を表示
Abstract The paper describes basic scaling procedure of a six-step BLDC motor control application with focus on S12ZVM MCU devices.  Abstract Introduction BLDC six-step control Speed scaling Timing Commutation periods Speed calculation Application note links Calculation accuracy Real applications Resources Introduction Based on the various questions regarding the BLDC speed calculation, I've decided to write this document to make the scale calculation clear. Please use it for your reference and comment in case there is something to be explained in more details. BLDC six-step control This document is linked with the six-step control of BLDC motors, known for the trapezoidal back-EMF shaped voltage. The key is to create a torque using DC current in two phases while the third phase is not connected. As the rotor is moving, the phases are switched (commutated) to keep the stator flux ahead the rotor flux. The principles are well described in many application notes, such as AN4718 or AN4704. The instant of the commutations can be driven by Hall sensors or by the back-EMF signal monitoring (so-called "sensorless"). For field-oriented control, please refer to the PMSM control discussed in AN5135 or AN5327. Speed scaling It's more benefitial to describe in details the sensorless algorithm over the hall-sensor-based control. However, the approach is almost the same. Timing The motor speed is calculated based on the zero-cross detection of BEMF voltage on a non-active phase. These zero-cross events times are measured by capturing a timer (TIM0CNT) register at the time the ADC routine detects a zero-cross (or when the Hall sensor commutation event occurs). That means, the time is scaled by the timer TIM0 settings. There is no general guidance how to set up the timer. However, the timer should be set to cover some reasonable number of ticks between two commutations (which is linked to the speed precission at high speeds) and should be able to cover two commutations "far away" from each other at very low speeds, without the timer overflow. A good practice would be: at least 100 timer ticks between two commutations maximum 16bit = 65535 ticks between two commutations The same aproach can be followed using the Hall-sensor events. Commutation periods In the application, zero-cross (or hall-sensor) periods are captured with periodZC_F_PhA, periodZC_R_PhA, etc. or periodZC[6], defined as tU16 (16 bit unsigned). The periods are captured using a timer, as mentioned above. In electric motor theory, we recognize "electrical" and "mechanical" speed. The "electrical" speed is linked with the rotational field. The mechanical speed is connected directly with the rotor speed. The relation between these two speeds is determined by number of poles or pole-pairs: (1)   mechanical speed = electrical speed / number of pole-pairs = electrical speed / ( number of poles / 2 ) In the following text, 3-phase BLDC motor is discussed. Speed calculation To calculate one "electrical" revolution of a motor = 6 commutations (or 6 zero-crosses), all the 6 commutation time periods shall be summed. For that case, the resulting "period6ZC" is defined, formated as tU32 (or unsigned long) to prevent an overflow if all six 16-bit zero-cross periods are summed. If you sum all the 6 zero-cross periods, you'll get the number of timer ticks per single "electric" revolution. That means, if the motor is 2-pole motor ( = 1 pole-pair motor), it would be the time per single "mechanical" revolution of the rotor. In thsi case: (2)   mechanical speed = electrical speed; You can easily get the time per mechanical revolution for higher-pole motor simply by multipling it by number of pole-pairs. (3)   time per mechanical revolution = period6ZC * number of pole-pairs  The period per 6 zero-crosses "period6ZC" is calculated within the control loop, usually in the 1 ms timer interrupt routine. Since the speed (rotor frequency) is just an inverted time period, we can use following code line to calculate the actualSpeed: (4) actualSpeed = SPEED_CALC_NUMERATOR / period6ZC; Now, how to read it's scale and what is the SPEED_CALC_NUMERATOR? Let's assume the "actualSpeed" is tFrac32 (1.31 formated signed 32bit number). It would mean the maximal fraction number is 1.0, which is represented by its integer value 2^31 = 2,147,483,648. Why to use 32-bit number over 16-bit is obvious - since the period6ZC is 32-bit value, the result should be of the same resolution or width. The task is to find the right SPEED_CALC_NUMERATOR. Let's consider the S12ZVM device and the timer TIM0 used to capture the zero-cross events times. The prescaler is set to 16 (TIM0TSCR2_PR = 4) and the bus clock is 12.5MHz, the timer tick is 12.5MHz / 16 = 781.25 kHz, in time scale it is 1.28us. Let's assume the maximum mechanical speed of the motor is 10,000 RPM and the motor has 6-pole-pairs. That would give us (5)   (10,000 RPM) / (60 seconds) = 166.67 revolutions per second, (6)   166.67*(6 pole-pairs) = 1000 electrical revolutions per second, so (7)   1000 * (6 commutations) = 6000 commutations/zero-crosses per second. (8)   That would make 1/6000 = 166.67us per one commutation. (9)   Ticks per one period at max speed = 166.67 us / 1.28us = 130.28 With our 1.28us timer, we can catch upto 130 periods at maximal speed. For maximal speed of the motor 10,000 RPM, we can simply rearrange the "actualSpeed" calulation shown in (4) into (13) and (14), assuming that: (10)   actualSpeed = FRAC32(1.0) = 2,147,483,648 (11)   period6ZC = 6 periods * 130 = 780 (rounded down, since the value is still an integer) In case of S12ZVM device, it is more convenient to use 16-bit (tFrac16) calculations than 32-bit. Hence, we can do a trick with the scaling to use 32-bit actualSpeed to prevent an overflow use the same 32-bit number as 16-bit number just by scaling it correctly benefit from the 16bit calculation, which is good enough and fast enough at the same time The trick is hidden in the casting of the actualSpeed from Frac32 to Frac16: (12)   speedErr = requiredSpeed - (tFrac16) actualSpeed; That means, only the lower 15 bits are considered the speed (assuming the actualSpeed will never exceed 32767 so the 16th "sign" bit will always be zero). For maximum speed and the SPEED_CALC_NUMERATOR determination, the "actualSpeed" should be 32767 (which is the range of signed tFrac16). Equation (4) can be used to calculate the SPEED_CALC_NUMERATOR as follows: (13)   32767 = SPEED_CALC_NUMERATOR / 780 (14)   SPEED_CALC_NUMERATOR  = 780 * 32,767 = 25,558,260 Thus  #define SPEED_CALC_NUMERATOR 25558260 Using the equation (4), the speed for the minimum period6ZC would be: (15)   actualSpeed = SPEED_CALC_NUMERATOR / period6ZC = 25,558,260 / 780 = 32,767; Masking that value by lower 15 bits and casting it to tFrac16 would give us 1.0. Since the speed scale has been determined by the maximum speed of the motor 10,000 RPM, we can calculate the real speed simply by: (16)   RealScaleSpeedRPM = (tFrac16)actualSpeed / 32,767 * MAX_SPEED = (tFrac16)actualSpeed / 32,767 * 10,000. Application note links In the application note AN4704, there are several macro constants used to control the application. These constants should be calculated using following definitions, with a little help of the SPEED_SCALE - floating point representation of the real scale of the speed. #define SPEED_SCALE 10000.0  // Used for correct calculation of the following: #define REQUIRED_RUN_SPEED FRAC16(2000.0/SPEED_SCALE) // 2000 rpm #define MIN_SPEED FRAC16(500.0/SPEED_SCALE) // 500 rpm minimal speed for Down button control (should be min 10% of nominal motor speed) #define MAX_SPEED FRAC16(5000.0/SPEED_SCALE) // 5 krpm maximum speed for Up button control #define SPEED_STEP FRAC16(100.0/SPEED_SCALE) // 100 rpm, Up/Down step for button controls   If the application uses FreeMASTER to display or control, the scales shall be updated in the FreeMASTER project as well. The new FM scales for AN4704 are: Variable name Variable watch settings requiredSpeed Real type transformation: Linear: a = SPEED_SCALE = 10,000; b = 0 actualSpeed Signed int, Size = 4 Show as: REAL Bit fields maks with: word (0xffff) Real type transformation: Linear: a = SPEED_SCALE / 32767.0 = 0.3051851; b = 0  Calculation accuracy Now, let's have a look on the speed resolution (or accuracy): At the full speed, if one period changes by 1 tick, then you'll get the period6ZC from 780 to 781 at max speed, which makes 12.8041 RPM difference. The higher the SPEED_SCALE is, the higher the error is. If the assumption would be a change in all of the 6 periods (thus the period6ZC would change from 780 to 786), the resulting change to the speed would be 76.336 RPM. That makes the speed error 10,000 RPM +- 76, which is 0.76%. In terms of accuracy, it makes sense to set the maximum speed (or the SPEED_SCALE) to the maximal speed of the application instead of copying some high number from the datasheet of the motor. Well, the max speed of the application should not exceed the max speed of the motor, but it doesn't help if the speed scale is unnecessarily high. Real applications In real applications, the calculated speed (actualSpeed) reflects all the deviations and changes of the period6ZC. Therefore, it is a good practice to do some kind of filtering of the period6ZC, either by averaging or using a low-pass filter. In case of one or more zero-crosses are lost, there should a mechanism to process and detect if the motor is stalled (mechanical speed loses lock with the commutation) or if it is just a disturbance to the signal. The stall detection or the Hall-signal fault/damage detection is one of the challenges towards high quality application. Resources S12ZVM MCU - NXP main S12ZVM page AutoMCDevKits - NXP Automotive Motor Control Development Solutions AN4718 - 3-Phase BLDC Hall Sensor Application Using S12ZVM AN4704 - 3-phase Sensorless BLDC Motor Control Kit with the S12 MagniV MC9S12ZVM AN5201 - Integrating the LIN driver with BLDC sensorless motor controller In the S12ZVM128 device AN5330 - Migration Guide for S12ZVM Devices
記事全体を表示
The example demonstrates the COP watchdog reset on MC9S12ZVL32 microcontroller. The code can be used on any MagniV device based on S12Z core. The example project is created in CodeWarrior v10.6 (Eclipse IDE). The SW code has been tested on TRK-S12ZVL board.   * Brief description: The Phase Locked Loop (PLL) is set by default to PEI mode, so the bus clock is 6.25MHz based on 1MHz internal RC oscillator (IRC1M). The RGB LED (red) is used to indicate MCU runs after reset. When the RGB colour changes to green, the COP time-out period has started. After the period times out, the COP generates a reset and COPRF flag is set. After the reset, based on COPRF flag, the Blue LED is turned on indicating previous reset has been generated by COP watchdog. The COP time-out period is set to maximum (CPMUCOP register, bits CR[2:0]=7). The number of COPCLK cycles to time-out is 2^24 = 16777216. The COPCLK is based on IRCCLK (by default) with 1MHz clock frequency. The maximum COP time-out period in this case is approximately 16.78 seconds. - On the TRK-S12ZVL board:   Port P is used to drive RGB LED. Anode is connected to VDDX, a cathode to port  pin. Port P can be set as output (DDRP=0xFF) and logic zero on output enables LED.   - Reference documentation: MC9S12ZVL Family Reference Manual & Datasheet TRK-S12ZVL Board schematics
記事全体を表示