S12 / MagniVマイクロコントローラ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12 / MagniV Microcontrollers Knowledge Base

ラベル
  • General 44

ディスカッション

ソート順:
This example simulates ECC issue by cumulative write into the same EEPROM area without an erasing.   The EEPROM erase operation set all bits into log1. The EEPROM program operation may keep bit cells in log1 state or change it into log0 state, but not in opposite way.   The S12Z MCU EEPROM is protected by 22-Bit ECC Scheme. Every word (16bits) is protected by additional 6 bits with ECC checksum. The ECC values are not accessible for users. Every EEPROM reading triggers also ECC check by internal logic. The single bit error in user data may be corrected by ECC checksum. The double bit error cannot be corrected.   The ECC protection is implemented also at flash controller commands and results are signalling by MGSTAT bits.   The first case simulates Single-bit ECC error during reading. The MGSTAT bits after the second write are 0b10 due to fact that just 1 bit is different during write verification (correctable error)   The second case simulates Single-bit ECC error during reading. The MGSTAT bits after the second write are 0b11 due to fact that more than 1 bits are different during write verification (non-correctable error)   The third case simulates Double-bit ECC error during reading. The MGSTAT bits after the second write are 0b11 due to fact that more than 1 bits are different during write verification (non-correctable error)       The EEPROM patterns are selected for highlighted described behavior and they don't have any real meaning.   The cumulative write is not allowed for normal operation!!! The code from this example should be used only for design testing - not in production!!!   Please, see the prm file. Address range 0x100000-0x100001 is excluded from default EEPROM and is used as user EEPROM memory The size of EEPROM sectors is 2 bytes. The EEPROM_Program() function may program up to 4 words in single flash command.   Note: The EEPROM_Program() function was updated - erase verification is skipped     I hope it helps you. Radek
記事全体を表示
Customers are sometimes asking for reference schematics, so here is a batch of minimal configurations for main representatives of S12(X) family. Attached is also document that should answer most common questions. Hope this will help. Lukas
記事全体を表示
Example code pack for S12G contains simple code examples how to initialize and how to use MCU module/feature. List of examples: G128-API_wakeup_from_Stop_Mode G128-Clock and COP examples G128-Interrupt_catcher-CW51 G128-LIN-CW51 G128-PLL_PEEmode-CW51 G128-Security-CW51 G240-API+STOP-CW51 G240-API-CW51 G240-ATD+GPIO-CW51 G240-ATD-Continuous_conversion_with_interrupt-CW51 G240-ATD-Multichannel_single_conversion-CW51 G240-ATD-Single_conversion-CW51 G240-Checksum-CW51 G240-Flash-CW51 G240-PLL-PBE_mode-CW51 G240-PLL-PEE_mode-CW51 G240-PLL-PEI_mode-CW51 G240-TIM_50us_interval-CW51 G240-TIM_50us_period-CW51 GN32-EEPROM-EW-CW51 GN32-LIN-CW51 GN32-PWM16b_GPIO GN32-PWM_8bit-CW51 GN32-SCI_SPI_Gateway-CW51 GN32-SCI_wake_up_from_stop-CW51   Oct-22-2013 Update: I added G128-CAN-CW51, G240-SPI-MC33810-CW51, G240-SPI-Slave examples. I added PLL calculator. I fixed error in GN32-EEPROM-EW-CW51 example code.   Aug-21-2015 Update: Updated G240-Flash-CW51 example code. Removed image files and object code from projects (9MB->2MB size)
記事全体を表示
In the attached zip file you can find three software examples demonstrating clock module and PLL configuration on MagniV device MC9S12ZVM. The examples are made in CodeWarrior IDE v10.6 (Eclipse). The main.c source file of each project provides detailed description, comments and important notes.   The source code can be used with other devices within MagniV family based on S12Z core such as S12ZVL, S12ZVC, S12ZVH/Y, but the precaution must be considered about the max bus frequency of the device.   p.s. Revision 2: SYNR, REFDIV and POSTDIV values changed in PLL initialization to achieve highest PLL locking time.
記事全体を表示
This short video demonstrates a path through NXP website to the CodeWarrior v5.1 download link. On the final place other downloads are available such as service packs, updates, patches etc. Login to NXP site is required.
記事全体を表示
For debug purposes, it is possible to read and write the user data and the ECC value directly from/to the SRAM memory. For these debug accesses a register interface is available.   By the debug access and writing incorrect data + ECC values into the system memory,  the single and double bit ECC errors may be simulated for checking the software error handling.   The debug registers may be modified only in a special mode.   The tested address 0x3000 is excluded from linker use - see prm linker file.   I hope it helps you. Radek
記事全体を表示
The ADC measurement is always relative – relative to your voltage reference. The most of the applications don't allow to use accurate and expensive voltage reference. In that case, VDDA is used as the reference for ADC measurement. Since the operational VSUP range starts from 3.5V and accuracy of the voltage regulator is limited, we should use internal bandgap reference for compensating ADC voltage results. The bandgap voltage VBG has a narrow variation over temperature and external voltage supply. The example shows how to compensate ADC results by additional bandgap voltage measurement.
記事全体を表示
Hello all, sharing the latest version of MagniV Power Dissipation Calculator started by Carlos Vazquez and Anita Maliverney. With this excel sheet is possible estimate the power dissipated for any MCU of S12ZVM, S12ZVL, S12ZC family, considering: supply voltages, digital modules, gate drive unit, charge pump, communication transceivers, etc.   A few features where added, any additional comment or suggestion is appreciated. Regards.
記事全体を表示
Work with pushbuttons and 7 segment display. Write assembly (ASM) and C programs for the HCS12, as well as to work with the pushbuttons and 7-segment display on the Dragon12-JR board.  The programs find the largest and smallest numbers from an arbitrary list of eight 8-bit unsigned numbers and displays them on the 7-segment display as outlined in the following.   1. Write a program to do the following, in both ASM and C. Do not use MINA, MINM, MAXA, and MAXM instructions.            a. Load an array of eight 8-bit unsigned numbers into RAM.            b. Find the largest of these numbers and store it.            c. Find the smallest of these numbers and store it.            d. Wait for the pushbuttons (S1 or S2) to be pressed.            e. The first time S1 is pressed, display the high nibble of the largest number; the second time S1 is pressed, display the low nibble of the largest number.                For example, if the largest number is 0x3F, the 7-segment display should show “3” the first time S1 is pressed and “F” the second time it is pressed.            f. Do the same for S2, except use the smallest number.  2. Explain why debouncing is used with switches. Optional: Implement software debouncing for switch used above.   Hints: These are unsigned numbers that your program will be searching through.  Make sure you are using the unsigned branch instructions in your ASM code. Your TA will be changing the numbers in your array to make sure it works for arbitrary 8-bit values. Please make sure the array is somewhere near the top of your program file. For interfacing to LEDs, 7 segment Displays, and pushbuttons see the schematic and manual of your development board. The type of the 7-segment LED on the Dragon12-JR board is common anode. All cathodes are driven individually by an output port and all anodes are internally connected together. The Dragon12-JR board uses port H to drive 7-segment cathodes. Skeleton files are provided to help you complete the asseignment. The 7-segment display communicates with the board via Port H whose address is $0260 (PTH).  Its data direction (input or output) is controlled by writing to Data Direction H register whose address is $0262 (DDRH). In order for PTH to be output (i.e. displaying something), you must set DDRH to $FF first (all bits high, all bits output).  The skeleton code does this for you this time. Almost every I/O port on the board works similarly to PTH; that is, you must set the direction of data on a corresponding data direction register before writing to or reading from it. The two pushbuttons (S1 and S2) are connected to PM6 and PM7. S1à PM6, S2à PM7 A subroutine that displays the low nibble of register A is included with the skeleton ASM code. Just store a value in register A and issue jsr seg7_out to display the low nibble of A. You are required to understand how it works and to write a similar routine for the C version of your code.   This document was generated from the following discussion: Professional Way to solve this HCS12 Dragon12-JR,Work with pushbottons and 7 segment display
記事全体を表示
Here are the two utilities which can be used to calculate the following:   - PLL filter component values on HCS12 devices such as MC9S12DP256   - PLL register values on S12(X) devices such as S12XE, S12XF, S12XS, S12P and S12HY.   Both utilities come with appropriate user manuals in PDF.
記事全体を表示
Have you ever wondered what is the difference between the electric motors included in those two Development Kit with S12 MagniV?     MTRCKTSBNZVM128: 3-phase Sensorless BLDC Development Kit with S12 MagniV S12ZVM MTRCKTSPNZVM128: 3-phase Sensorless PMSM Development Kit with S12 MagniV MC9S12ZVML128 MCU   Well frankly writing none. They include the same motor model 45ZWN24-90       . So the motors are same from physics perspective, only the flux distribution in an air gap is different. It is sinusoidal for PMSM whereas it is trapezoidal for BLDC motor. The powerstage is same for both but what is different however is the control strategy. The Linix motor equipped with the DevKits is in fact somewhere between PMSM and BLDC, The flux is not sinusoidal nor trapezoidal.   Further information and motor parameters can be found at manufacturer product pages:                          http://www.linixmotor.com/3-3-Tool-Motor.html
記事全体を表示
TIC example code, v.1.1 * The SW: * demonstrates FLASH programming as a part of application * uses adjusted routines from AN2720 * writes a few words into FLASH locations Pages FE and E0~EF may be used for data storage.   Other pages are used for program storage (see PRM file)      * tested on: HCS12X STARTER KIT * OSCCLK = 16MHz, BUSCLK = 8MHz * Reference to documentation: MC9S12XDP512V2 Rev.2.17 Original Attachment has been moved to: XDP512-FLASH-E_W-CW47.ZIP
記事全体を表示
The example code shows how to invoke single or double bit RAM ECC error at S12Z devices.   Some basic overview about S12Z ECC codes may be found in thread AM/FLASH ECC Error handling .
記事全体を表示
The example code demonstrates MCU low power modes: STOP and WAIT. For detailed description see main.c file of the project. * - tested on X-VLG-S12ZVC board * - BUSCLK = 6.25MHz based on internal oscillator clock IRCCLK = 1MHz.The PLL set by default in PEI mode. * - Reference documentation: MC9S12ZVCRMV1.pdf (REV 1.9) VLG-MC9S12ZVC-SCH.pdf (Document Number SCH-28038, SPF-28038)
記事全体を表示
This example: 1. write unprotected P-Flash area 2. protect target P-Flash area 3. tries to write protected P-Flash area 4. call Protection Override command for temporary modify P-Flash protection 5. write into temporary unprotected P-Flash area 6. restore original P-Flash protection scheme The part of P-Flash memory used in this example for writing tests (0xFF8000..0xFF8FFFUL) is excluded from linker using. Please look at prm linker file for more details.   The flash_array constant with Protection Override Comparison Key is not directly referenced in the code, therefore we must enter the constant name into ENTRIES section in prm linker file for avoiding stripping it out as unused. Please look at P-Flash Protection Register (FPROT) chapter in the reference manual for more details about P-Flash protection. The key for Protection Override should be rather received from external source and used as PFLASH_Protection_Override() parameter. The correct Protection Override key is here hard-coded (err = PFLASH_Protection_Override(0xCAFE, 0xF...) for example code simplifying.   I hope it helps you. Radek
記事全体を表示
The package contains of AN5327_SW ported to S12ZVML-MINIBRD hardware. Just minor changes are introduced, such as removing a button control, moving the LED light to another pin and using internal oscillator. This is just a working version, it is NOT an official release!!! AN5327_SW_CW11_MINIBRD.ZIP CodeWarrior 11.0 and AMMCLib 1.1.13 or higher is required to run this example. If you are not sure about the AMMCLib version, please download the general AN5327_SW from the www.nxp.com/automcdevkits first, install it and then unzip and use the example above.
記事全体を表示
Here is a SW example demonstrating measurement of the bandgap voltage featured on a microcontroller. The bandgap voltage is routed to an internal ATD channel. ATD converter measures the input voltage and stores it to a variable located in Flash memory. The SW example project is made in CodeWarrior v5.1 for MC9S12XEP100 device.
記事全体を表示
Dear reader,   There is extended information provided in the attached document. it contains detailed description "how-to", example design, detailed memory maps and code examples.   Also tested example projects created under CodeWarrior are attached.   I believe the document as well as SW examples will help you in the design and avoid mistakes we have met under our work in the S12(X) support team.   Yours sincerely,   Ladislav
記事全体を表示
Interrupt catcher example code catches all unexpected interrupts. It can be used for debugging or directly in the application software. The Machine Exception routine is used here as example of expected interrupt.   A few notes: 1. For each expected interrupt you must remove a code line for given interrupt     from the part of the code "A Set of unimplemented interrupts" and     create your own service routine as it is, for example, made     for interrupt 5 void Machine_Exception_ISR(void)   2. All interrupt vectors have 32bit size, however, addresses have only 24bit,     therefore the most significant byte in interrupt vector is not used.     Definitions with the keyword "interrupt XX" where XX represents vector     order in the interrupt vector is used to define interrupt service function.      3. Interrupt number 0 is assigned to POR reset vector,                      1 is assigned to Unimplemented page1 op-code trap vector                      2 is assigned to Unimplemented page2 op-code trap vector                      3  ...                      4  ...     Interrupt number = (0x1FC-Vector Address)/4. See Table 1-11. Interrupt     Vector Locations at RM(page 62-65).     For Example: Interrupt number of SCI0 = (0x1FC-0x19C)/4 = 0x18 = 24.     So you can use either form                interrupt VectorNumber_Vsci0 void SCI0_isr(void)     or                interrupt 24 void SCI0_isr(void)     or                interrupt ((0x1FC-0x19C)/4) void SCI0_isr(void)       Note: VectorNumber_Vsci0 is defined in mc9s12zvl32.h      
記事全体を表示
The bold blue links below provide direct download of SW example packs for MagniV devices based on S12Z core.   S12ZVC Getting Started Exercises (REV 1.0) This file contains four hands-on exercise where you can find basic setup code to enable a quick development in different areas. The file includes CodeWarrior projects demonstrating usage of peripheral modules such as: - Digital-to-Analog Converter (DAC), - Controller Area Network (CAN), - Pulse Width Modulation (PWM), - Timer (TIM).   Getting started with S12ZVL32 - S12 MagniV Example Codes (REV 0) The MC9S12ZVC device integrates a battery level (12V) voltage regulator and supply voltage monitoring. This zipped file includes four CodeWarrior examples demonstrating - Overcurrent protection on EVDD pin, - low power STOP mode with API timer and wake-up feature, - Pulse Width Modulation (PWM) - Serial Peripheral Interface (SPI) communication.   Many of these examples can be used on various MCU families across the MagniV product line. Check the appropriate device guide for list of modules and its versions.
記事全体を表示