Trouble implementing ios app using Taplinx SDK Hi, i'm trying to follow UG10045.pdf - Starting development with TapLinx iOS SDK. Below is excerpt from that guide: 3.4 Implementing the delegate method for APDU communication To communicate with the TapLinx iOS Library and the Tag (or Card), a delegate method which is created inside the MIFAREApduHandler must be implemented in your class. Below is the delegate method. However i do not understand where i should implement that TapLinxApduHandlerProtocol, on what class? Where/how should i pass my class to something in Taplinx SDK to indicate where i implemented that hander? Is there a ios sample app like for Android? It would be very helpful. In case there is no such app, could someone share a code sample with full sdk initialization on ios? Re: Trouble implementing ios app using Taplinx SDK Hello @DamianD
Since your problem involves the level of code debugging, we do not have such a test environment as yours, so your problem needs to be debugged by you, say sorry for that. Re: Trouble implementing ios app using Taplinx SDK hi @KaiLi - unfortunately there is only swiftsourceinfo file inside Project folder and it is of no use to me. When i add libTapLinxLibrary.a to xcode app project (and set up search paths) during compilation i get error: /Users/xxx/Projects/xcodeproj/facilityapp/SampleTaplinxApp/SampleTaplinxApp/ContentView.swift:9:8 Compiled module was created by a different version of the compiler '5.10.0.13'; rebuild 'TapLinxLibrary' and try again: /Users/xxx/Projects/xcodeproj/facilityapp/SampleTaplinxApp/TapLinxLibrary2/TapLinxLibrary.swiftmodule/arm64-apple-ios.swiftmodule\ Could you hint me at what to do? Re: Trouble implementing ios app using Taplinx SDK thanks, i will give it a try and let you know Re: Trouble implementing ios app using Taplinx SDK Hello @DamianD
Unfortunately, there is not the dedicated sample for ios, but I think there should be something in SDK could refer to, like
sdk_TapLinx_Library_iOS\TapLinxv1.0.1\TapLinxiOSSDK\TapLinxiOSSDK\TapLinxLibrary\TapLinxLibrary.swiftmodule\Project. Please try it.
查看全文