Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Dear NXP Support Team, I am encountering issues while attempting to read the internal temperature sensor on the S32K324 microcontroller using ADC hardware instance 0, channel 49. My VREF voltage is configured to 3.3V (0x35), but the temperature readings I am obtaining do not match my expected values.     Could you please provide any guidance or reference materials to help me resolve this issue and achieve accurate temperature readings?   Regards, Ranjith kumar Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Hi@Ranjith_kumar I don't quite understand what your new question is? In my previous reply, I have provided you with a test demo, and I haven't seen any of your projects. Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Dear Senlent, I followed the steps you mentioned in the shared video to read the internal temperature sensor on the S32K324 controller. However, I am not obtaining stable or expected temperature values. As I mentioned in my previous post, I am reading the raw ADC values from the internal temperature sensor, but the temperature readings show sudden spikes and are not constant. For reference, I am also using an external temperature sensor near the controller, which shows a stable temperature range of 32 to 35°C. In contrast, the internal temperature sensor readings are showing negative and fluctuating values. I have attached a video demonstrating the issue and the software I developed for this purpose. Could you please help me verify whether the values I am getting are correct or if there might be an issue with my approach? Any guidance or example code to correctly read and interpret the internal temperature sensor data would be greatly appreciated. Thank you for your support. Regards, Ranjith kumar Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Hi@Ranjith_kumar From your video, it seems that you didn't even read the raw value of the internal temperature sensor. I made a very basic example for your reference, the hardware is S32K344, the RTD is 3.0.0+P07. Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Dear Senlent, As per your suggestion and referring to the provided link, I have attempted to read the internal temperature sensor on the NXP S32K324 controller using RTD 3.0.0. However, the values I am obtaining do not match our expected results. Could you please share any example code or reference implementation that demonstrates the correct procedure for reading and converting the internal temperature sensor data? Additionally, I would appreciate your guidance on how to determine appropriate threshold temperature values for our application. I have attached the relevant document for your reference. Kindly assist me in resolving this issue. Thank you for your support. Best regards, Ranjith kumar Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Hi@Ranjith_kumar There is a similar demo in this link for your reference https://community.nxp.com/t5/S32K/S32K344-Temperature-Sensor/m-p/1876707#M35929 If you still have questions, please provide me with a basic project and I will help you check it
記事全体を表示
How to know whether any data is written or not to the specific eFuse address in S32G Hi. I have been implementing to write any data to the specific eFuse address in S32G. /* Write Shadow OCOTP_GP6_127_96 */ 1 . Ocotp_Ip_WriteShadowRegister(instance_Cfg0, OCOTP_GP6_127_96_SHADOW_REGISTER, DATA_TEST_0); 2. result = Ocotp_Ip_WriteEFuse(instance_Cfg0, OCOTP_GP6_127_96, DATA_TEST_0, false, true); after 2. step, How to know whether any data is written or not to the specific eFuse address if  the value is RP (ReadProtect)+WP (WriteProtect)+OP (OverRideProtect)in S32G? Re: How to know whether any data is written or not to the specific eFuse address in S32G Hi. This issue is resolved. Thank you for your support. BRs. Re: How to know whether any data is written or not to the specific eFuse address in S32G Hi I write 20 to it when the data of specific fuse address is empty. The value is 20 when  read the data of specific fuse address. I write 21 to the same fuse address. The value is not 21 when read data for the same fuse address. So it seems that crc error happens. Do you think what is problem? What does mean that Each eFuse bit cannot be cleared if set to 1? Re: How to know whether any data is written or not to the specific eFuse address in S32G hi,EddiePark Thank you for your reply. Will the problem still occur if you only write DATA_TEST_0 or DATA_TEST_1. What is the value that you set DATA_TEST_1. Each eFuse bit cannot be cleared if set to 1. BR Joey Re: How to know whether any data is written or not to the specific eFuse address in S32G Hi. Thank you for your response. In current, I have one issue for eFuse. The below code works normally in case any data is written the specific eFuse address which is empty,  But crc error happens in case the data of specific eFuse address is updated and I cannot read the data of specific address,   LockBit is 0x00(Neither Fuse or Shadow are locked for Read, Write and Override) please let me know what is problem. Ocotp_Ip_ReadEFuse(instance_Cfg0, OCOTP_LOCK_CUSTOMER_LOCK_BITS, &u32Data);   /* Write Shadow OCOTP_GP6_127_96 */ Ocotp_Ip_WriteShadowRegister(instance_Cfg0, OCOTP_GP6_127_96_SHADOW_REGISTER, DATA_TEST_0); /* Write Shadow OCOTP_GP6_159_128 */ Ocotp_Ip_WriteShadowRegister(instance_Cfg0, OCOTP_GP6_159_128_SHADOW_REGISTER, DATA_TEST_1);   ocotpStatus = Ocotp_Ip_WriteEFuse(instance_Cfg0, OCOTP_GP6_127_96, DATA_TEST_0, false, true); if(STATUS_OCOTP_IP_SUCCESS != ocotpStatus){ gCDDExecuted = CDD_INIT_OCOTP_FAILURE; }   ocotpStatus = Ocotp_Ip_WriteEFuse(instance_Cfg0, OCOTP_GP6_159_128, DATA_TEST_1, false, true); if(STATUS_OCOTP_IP_SUCCESS != ocotpStatus){ gCDDExecuted = CDD_INIT_OCOTP_FAILURE; } ocotpStatus = Ocotp_Ip_CalculateAndWriteCrcValue(instance_Cfg0, CRC0_EFUSE_ADD, u32DataIsTestedCRC, (uint32)2U); if(STATUS_OCOTP_IP_SUCCESS != ocotpStatus){ gCDDExecuted = CDD_INIT_OCOTP_FAILURE; }   /*Update value CRC0 eFuse to CRC0 Shadow register. If MCU reset, you dont need this step*/ Ocotp_Ip_ReadEFuse(instance_Cfg0, CRC0_EFUSE_ADD, &u32Data); Ocotp_Ip_WriteShadowRegister(instance_Cfg0, CRC0_SHADOW_REGISTER, u32Data);   /* Test CRC */ ocotpStatus = Ocotp_Ip_CrcTest(instance_Cfg0, CRC0_EFUSE_ADD, OCOTP_GP6_127_96, OCOTP_GP6_159_128); Re: How to know whether any data is written or not to the specific eFuse address in S32G hi,EddiePark Thank you for contacting us. According to the S32G2RM.pdf and the Ocotp_Ip_WriteEFuse function, you can check ADDR_SYS and WRDATA_SYS register to know whether any data has been written to the specific eFuse address. In addition , you can configure LockBit to use eFuse/shadow lock bit function by referring to S32G2_Fuse_Map_Tables.xlsx. BR Joey
記事全体を表示
FRDM-MXCN947ボードでイーサネットとカメラを同時に使用する MCXNx4x では、SmartDMA を使用してカメラ インターフェースを実装できます。 MCXNx4x データシートによると、イーサネット と SmartDMA の Pinmux 割り当てが競合します。このため、イーサネットとカメラを同時に使用することはできないと考えました。 ただし、FRDM-MCXN947 ボード ユーザー マニュアル (UM12018) には次のよう記載されています。 > カメラの使用中にイーサネット機能が必要な場合は、別の回避策があります SJ16 および SJ26 ジャンパーをデフォルトの位置から移動することです。 イーサネットとカメラを同時に使用する方法はありますか? 開発ボード MCX N Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board こんにちは@dubian1shu 書類の内容を再確認したところ、書類の記載内容に問題があることが確認できました。 文書には適時変更を加えます。 SmartDMA (EZH_CAMERA) と イーサネット (ENET)は同時に使用できますが、カメラが使用するには共有されていないピンを見つける必要があります。 こちらの記事を参考にCAN。 MCX N947:イーサネットとカメラ機能の同時実装 - NXPコミュニティ これがお役に立てれば幸いです。 BR 下がる Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 確認して返信してくれてありがとう@Harry_Zhang SmartDMA は P1_X と P3_X をサポートしているので、MCXNx4x は SmartDMA と イーサネット 機能を同時に使用 CAN と理解しています。 しかし、FRDM-MCXN947 を使用して SmartDMA および イーサネット 機能を使用することはできますか? FRDM-MCXN947 の J9 (カメラ ヘッダー) には、イーサネット ピンと競合する 7 つのピンがあります。FRDM-MCXN947 ボードのユーザー マニュアル (UM12018) に記載されている P1_4 の解決策では、そのうちの 1 つだけが解決され、他の 6 つの競合については触れられていません。 たとえば、P1_5、P1_13、および P1_15 は SmartDMA と イーサネット 間で競合します。回路図ドキュメント (SCH-90818) から見る限り、この競合を解決する解決策はないようです。 FRDM-MCXN947でSmartDMA(EZH_CAMERA)とイーサネット(ENET)を同時に使用する方法はありますか? Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board こんにちは@dubian1shu MCXNx4xのデータシートを確認したところ、確かにイーサネットとSmartDMAが競合するピンがいくつかあります。ただし、イーサネットとSmartDMAを同時に使用したい場合は、イーサネットとSmartDMAが競合しないピンを選択できます。 たとえば、SmartDMA ピンとして P3_X を選択し、イーサネット ピンとして P1_X を選択できます。 FRDM-MCXN947 ボード ユーザー マニュアル (UM12018) を参照してジャンパーを移動します。 これがお役に立てれば幸いです。 BR 下がる
記事全体を表示
CST 4.0.1 的 Openssl 版本 您好, 我从恩智浦下载了CST 4.0.1(代码签名工具),在查看文档文件夹中的文档(特别是UG10106)时,我看到了第3.1.1 节、其中提到 CST 支持Ubuntu 22.04,需要OpenSSL 3.2.0。 不过,我当前的 Ubuntu 22.04 系统使用的是OpenSSL 3.0.2已安装。我担心升级到 OpenSSL 3.2.0可能会破坏现有的系统依赖关系。使用 CST 真的需要升级 OpenSSL 吗?如果是这样,有什么最安全的方法可以在不影响我的系统的情况下做到这一点? 我还附上了 UG10106 的屏幕截图以供参考。 谢谢! Kartheek Re: Openssl Version for CST 4.0.1 您好@kartheek! 感谢您联系恩智浦支持中心! CST 工具的推荐版本是 OpenSSL 3.2.0。 遗憾的是,我们尚未测试 OpenSSL 3.0.2 版本。如果该工具不能按预期运行,则应尝试安装用户指南中推荐的版本。 此致 查维拉
記事全体を表示
在 S32K358 上配置 AUTOSAR 4.7.0 中的接收中断 大家好, 我们目前正在将我们的项目从 RTD 迁移到 AUTOSAR 4.7.0(SW 版本 3)。 发送和接收均配置为中断模式。 在 RTD 设置中,每个报文对象都有自己的缓冲区。当收到消息时,将触发信号接收 IRQ 功能,通过使用消息对象编号,可以访问和处理相应的缓冲区。 现在,在 AUTOSAR 中,我不知道如何正确配置接收中断处理。 如何在 AUTOSAR 中为接收中断分配或访问消息对象缓冲区? 是否有实现或配置接收 ISR 回调(例如通过 CanIf 或 CanDrv)的推荐方法? 此工作流程有任何示例或文档参考吗? 我查看了多个示例,但没有找到一个能说明接收中断处理的示例。 如有任何提示或配置示例,敬请垂询! Re: Configuring Reception Interrupts in AUTOSAR 4.7.0 on S32K358 你好,我是@thorben_kamp、 我猜您说的 SW 版本 3 指的是 S32K3 RTD v3.0.0 ASR21-11。 RTD 代码包为 S32K358 CAN 通信提供了 AUTOSAR 示例例程: 不过,它被配置为环回操作,这意味着输出引脚上看不到信号。您需要配置输出引脚(S32K3X8EVB 中 CAN0 的 PTA6/7),并将 CAN 实例模式从环回改为正常/用户模式。 您还需要根据硬件配置初始化 CAN 收发器。 这里发布了一个基于中断 MCAL 的 S32K3X4EVB-T172 示例:[RTD600 MCAL & IP] S32K3X4EVB-T172 FlexCAN 示例中断 /轮询——恩智浦社区。它基于 S32K344,但可以使用相同的主程序。请记住,该示例只是展示了最基本的配置,完全不符合 AUTOSAR 标准。 致以最诚挚的问候, Julián
記事全体を表示
缺少编译器 S32 Studio 我在 S32 Studio 3.6.4 中找不到编译器用于 S32K3x8 EVB。 arm-none-eabi-gcc " @board /siul2_port_ip_cfg.args "-MMD-MP-MF "板/siul2_port_IP_CFG.D "-MT " board/siul2_port_IP_CFG.O "-o " board/siul2_port_IP_CFG.O "".。/板/siul2_port_IP_CFG.C " make:*** [generate/src/subdir.mk:26: generate/src/Igf_Port_Ip_Cfg.o] ***.错误 127 /bin/sh:第 1 行:arm-none-eabi-gcc:找不到命令 make:*** [generate/src/subdir.mk:26: generate/src/OsIf_Cfg.o] ***.错误 127 /bin/sh:第 1 行:arm-none-eabi-gcc:找不到命令 make: *** [板/subdir.mk: 23:板/tspc_port_IP_CFG.O] 错误 127 /bin/sh:第 1 行:arm-none-eabi-gcc:找不到命令 make: *** [板/subdir.mk: 23:板/siul2_port_IP_CFG.O] 错误 127 Re: Missing compiler S32 Studio 你好,@Greavesinator85、 您使用的是哪个 RTD 版本?您的项目中似乎没有选择工具链。 示例项目也会出现这种情况吗?创建项目时,是否选择了"Create new S32DS application project" 选项? 您可以尝试在项目属性中手动添加工具链路径,但我建议您创建一个新项目,以避免与此相关的任何其他配置问题。 致以最诚挚的问候, Julián
記事全体を表示
MC9S12ZVM128 SRAM 双位 ECC 处理 我们正在使用 MC9S12ZVM128,想知道如何处理 SRAM 中的双位 ECC 错误。具体来说,系统是否可以通过使用以下方法执行软件重启来恢复正常运行 CPMUCOP = 0x01; CPMUARMCOP = 0x00;? Re: MC9S12ZVM128 SRAM double bit ECC handling 你好,喇嘛 感谢您的答复。这个问题我们现在已经很清楚了,我相信我们可以结束这个话题。 BR, Mark Re: MC9S12ZVM128 SRAM double bit ECC handling 您好, 让我来概括一下。 在 POR 期间,SRAM 将被初始化。如果检测到双位 ECC 错误: 内存访问受阻。 已通知启动器模块。 7.3.4内存初始化 ... 为避免出现虚假的 ECC 错误报告,允许在首次写入前进行读取的内存操作(如非对齐访问的读取-修改-写入操作)要求在执行首次读取-修改-写入访问之前,内存必须包含有效的 ECC 值。ECC 模块提供在开机阶段将整个内存内容初始化为零的逻辑。在初始化过程中,SRAM 的访问被禁用,RDY 状态位被清零。如果初始化过程完成,则可以访问 SRAM,并设置 RDY 状态位。 POR(上电复位) 它的作用:POR 是通过重新启动电源或由专用 POR 信号触发的全面硬件 RESET。 对 ECC 错误的影响 -SRAM 已清除:所有易失性存储器都丢失,包括损坏的数据。 -ECC 逻辑已 RESET:所有 ECC 错误标志或状态位都被清除。 -寄存器RESET为默认值:所有配置寄存器返回其默认状态。 - 影响:除非从闪存或外部资源重新加载相同的损坏数据,否则系统将重新启动,双位 ECC 错误将不会继续存在。 ________________________________________ COP(计算机正常运行)RESET 它的作用:当软件无法及时维修时,看门狗定时器会触发 COP RESET。 对 ECC 错误的影响 - SRAM 未清除 - ECC 错误持续存在:如果损坏的数据仍在 SRAM 中,ECC 逻辑可能会在重启后再次检测到相同的双位错误。 -寄存器可能保留值:某些寄存器可能会保留其值,具体取决于RESET配置。 ________________________________________ 建议 如果您想保证消除 ECC 错误状态,请使用 POR RESET。如果您正在调试软件故障或从软件故障中恢复,并希望保留内存以供分析,则 RESET COP 可能更合适。 因此,最好确保在 POR 之后检查并处理 RDY,而不使用 RAM。 如果 COP 重新启动了系统,则尝试写入该字,并检查 ECC 错误是否确定。 此致 拉吉斯拉夫
記事全体を表示
NXPの日本語技術記事をまとめた「コンテンツ・マップ」を公開 (日本語ブログ) 2025年よりNXP Japanから日本語の技術記事をたくさんユーザーに届けよう!との想いの下、これまでに多数の技術記事(Tech Blog)を公開してまいりました。 これらの情報をより体系的にご活用いただけるよう「コンテンツ・マップ」(PDF)を公開しています。 *2026/5/11更新 計94個のコンテンツ 図1.「コンテンツ・マップ」イメージ図(中身は逐次更新します) コンテンツ・マップとは? 本コンテンツ・マップは、NXP製品に関する技術情報をカテゴリ別に整理したもので、Yocto Linux、EdgeAI、Security、PMIC、Interface、NXPへの技術質問方法など、幅広い分野にわたる記事を網羅しています。各記事へのリンクも掲載しており、目的の情報にスムーズにアクセスできる構成となっています。 ・読みたいコンテンツの右端をクリックいただきますと、該当記事に飛ぶことができます。 図2.記事へのリンク   「Yocto Linux」、「エッジAI」、「I3C, I 2 C」、「セキュリティ」、「Zephyr」などのトピックについては、実装例やトラブルシューティングのヒントを含む実践的な内容が充実しています。これらは、開発現場での課題解決や新規プロジェクトの立ち上げ時に役立つ情報として、多くの技術者の皆様に活用いただいております。 コンテンツもメイントピック毎に色分けしており、ユーザーの状況に合わせたコンテンツを選択いただけます。 ・基礎コンテンツ:  一般知識、基礎知識、プロトコルの解説など ・手順コンテンツ:  実際に動かしてみる、環境構築など ・応用コンテンツ:  深い技術知識、デバッグ手法、応用手順など *難易度も目安として★の数で表示しています。      図3.カテゴリ分け 今後について 今後もコンテンツ・マップを本ページに公開・更新することを検討しております。より多くの方々にNXPの技術情報を活用いただけるよう努めてまいります。技術者の皆様はもちろん、教育機関や学生の方々にも参考になる内容となっておりますので、ぜひご覧ください。ブックマークも是非♪ 更新時には、SNSでもご案内いたします。            現在コンテンツ・マップに掲載の「今後のプラン」は、ほんの一部であり、他にも作成予定のコンテンツが多数ございますため、今後の更新にもご期待ください。 2025年よりNXP Japanから日本語の技術記事をたくさんユーザーに届けようとの想いの下、これまでに多数の技術記事(Tech Blog)を公開してまいりました。これらの情報をより体系的にご活用いただけるよう「コンテンツ・マップ」(PDF)を公開しています。 実装例やトラブルシューティングのヒントを含む実践的な内容が充実しており、開発現場での課題解決や新規プロジェクトの立ち上げ時に役立つ情報として、多くの技術者の皆様に活用いただいております。 (読了:5分) introduction 日本語ブログ
記事全体を表示
MakerFaire 上的炫酷科技 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 创客嘉年华,我们来了! 本周末我们将在圣马特奥分享一些超酷的项目,九月份我们将去纽约。 经过大量工作,我们的团队已经整合了一些基于 Kinetis mcus、i.MX 6 处理器、Freedom 开发平台构建的超酷项目,以及以UDOO 、 Riotboard.org为特色的热门社区项目,诺维娜、 CuBox-i 、 Wandboard.org 、Wunderbar 、ZumoBots 等。以下是我们计划的一些事情。 谁不喜欢闪烁、耀眼的灯光?PJRC的工作人员制作了一个 LED 显示屏(准确地说是 4320 个),全部由一块Teensy3.1板控制,该板大约有一块口香糖那么大。Paul 制作了一些特殊的 Teensyduino 草图库,利用 Kinetis K20 MCU 的直接内存访问引擎 (DMA) 功能来实现此演示中显示的视频和音频。Paul 不仅管理了困难的 LED 时序,而且还为 SDCard 接口的所有视频提供服务。我们是否提到过它也可以播放音频?! https://community.nxp.com/docs/DOC-100844 一旦您从标志上获得足够的光线,您就可以使用我们破解的 Wii-Fi(是的,它是 WII + WiFi)Nerf Swarmfire 测试您的技能。添加一些伺服器、一些重新布线和一个定制的 WiFi 遥控器,然后……立即享受乐趣!为了实现这一点,我们在 Nerf 本身(底座)上使用两个 FRDM-KL64F,并使用一个作为无线遥控器。基板处理来自遥控器的数据并相应地控制伺服器。 此视频已被删除。 (在 “我的视频” 中查看) 遥控板的行为有点像 Wii,用户必须移动遥控器,然后板载加速度计将其转换为运动,然后通过 WiFi 传递到基本控制器。最重要的是,我们只需要 3D 打印一个塑料控制器就可以将所有东西放进去。 https://community.nxp.com/docs/DOC-100845 这些是基于我的 Kinetis MCU 的演示。现在让我们来谈谈多媒体,也就是 i.MX 应用处理器。 当你到达该地区时,一定要和马里奥打个招呼。马里奥是一个自制的安卓机器人,拥有语音识别和Twitter连接功能。马里奥的心脏是一个运行 Android 4.3 的 UDOO Quad 加上一个 Arduino Motor Shield,它可以控制 2 个伺服器(马里奥的手臂)和 4 个转动 4 个轮子(马里奥的腿)的电机。为了展示他可爱的脸,马里奥有一个 7 英寸 LVDS 显示屏,而他的嘴是一个小扬声器。为了让他说话,我们利用了 Google API 的语音识别和文本转语音功能,赋予他生命。我们还使用了 Twitter API,通过 Twitter 控制马里奥,让他可以阅读推文,还可以通过简单的鸣叫向马里奥发送指令。
記事全体を表示
通过 Volume Curve 保护您的 LPC55Sxx 器件从原型设计到生产 确保在整个产品生命周期内保护宝贵的知识产权,可以帮助您安心并防止业务收入损失。该网络研讨会将概述恩智浦 LPC5500 MCU 系列提供的安全功能以及如何在制造过程中利用这些功能。EPS Global 是一家全球性的 IC 编程和安全配置服务提供商,它将讨论这些安全功能为 IP 保护带来的价值,并概述 LPC5500 MCU 系列可用的制造流程,以在产品的整个生命周期(从设计到整个制造供应链)提供端到端的安全性。 演讲者: 恩智浦生态系统产品营销人员 Clark Jarvis Brian Colgan,EPS Global 现场应用工程师 Arm® 处理器 LPC微控制器
記事全体を表示
ポータブルRFクッキングアプリケーションの設計上の課題 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 調理器具の設計では、家庭の有線電気システムから必要な電力や、安全性と動作温度を維持するために必要な性能について十分に考慮されています。NXPのソリッドステートRF調理チームは、バッテリー電源で動作することができるソリッドステートRFエネルギーを使用してポータブル食品加熱器具を開発しました。このセッションでは、持ち運び可能な外出先で食品を加熱するためのエネルギーを供給するための主要な課題とアプローチについて説明します。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 調理器具の設計では、家庭の有線電気システムから必要な電力や、安全性と動作温度を維持するために必要な性能について十分に考慮されています。NXPのソリッドステートRF調理チームは、バッテリー電源で動作することができるソリッドステートRFエネルギーを使用してポータブル食品加熱器具を開発しました。このセッションでは、持ち運び可能な外出先で食品を加熱するためのエネルギーを供給するための主要な課題とアプローチについて説明します。
記事全体を表示
ESC技术报告.pdf <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 飞思卡尔杯技术报告 韩国ESC团队 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 飞思卡尔杯技术报告 韩国ESC团队
記事全体を表示
AMF-ACC-T1647 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 以太网已成为汽车通信领域最受讨论的技术之一。本演示将概述汽车以太网的标准。并解决在不同应用程序中实施该技术所面临的挑战。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 以太网已成为汽车通信领域最受讨论的技术之一。本演示将概述汽车以太网的标准。并解决在不同应用程序中实施该技术所面临的挑战。
記事全体を表示
AMF-ACC-T1213 - DwFデトロイト <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> <meta http-equiv="Content-Type" content="text/html; charset=utf-8" />
記事全体を表示
AMF-ACC-T1645 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在仍然执行微控制器应用程序的同时,在闪存中编写第二个应用程序代码映像,然后切换到新的代码映像的需求正在增加。提供了飞思卡尔微控制器架构的示例实现,以演示如何通过应用程序执行进行并发编程并随后重新映射到新的应用程序代码映像。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在仍然执行微控制器应用程序的同时,在闪存中编写第二个应用程序代码映像,然后切换到新的代码映像的需求正在增加。提供了飞思卡尔微控制器架构的示例实现,以演示如何通过应用程序执行进行并发编程并随后重新映射到新的应用程序代码映像。
記事全体を表示
一种检测不精确硬故障源的方法 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本文档与Dragos Musoiu合作创建 尝试调试基于 ARM Cortex M4 的微控制器 MKW24D512 上的硬故障,我们没有找到太多关于处理不精确硬故障的文档。我们从 Erich Styger 的帖子“调试 ARM Cortex-M 上的硬故障”开始调查。基于此,我们使用Erich的代码来查找硬故障源,但无法找到导致硬故障的指令,因为围绕保存的PC执行的指令看起来是正确的。 之后,我们检查了硬故障状态寄存器,从 ARM Cortex M4 处理器的系统控制块中,我们发现 FORCED 位被设置了。ARM Cortex M4 文档提到,该位表示强制硬故障,由可配置优先级的故障升级产生,由于优先级或被禁用而无法处理。当该位设置为 1 时,HardFault 处理程序必须读取其他故障状态寄存器来查找故障原因。我们检查了其他故障寄存器,发现 ARM Cortex M4 处理器的系统控制块中的可配置故障状态寄存器(总线故障状态寄存器)中的 IMPRECISERR 位被设置。根据 ARM Cortex M4 文档,如果设置了此位,则发生数据总线错误,但堆栈帧中的返回地址与导致错误的指令无关。当处理器将此位设置为 1 时,它不会将故障地址写入 BFAR。所以这就解释了为什么我们没有按照 Erich 的指示找到导致硬故障的指令。此外,这是一个异步错误。因此,如果检测到当前进程的优先级高于 BusFault 优先级,则 BusFault 变为待处理状态,并且只有当处理器从所有更高优先级的进程返回时才会变为活动状态。 Cortex M4 处理器具有写入缓冲区功能,当对可缓冲内存区域进行写入时,处理器可以在传输完成之前继续执行下一条指令。这对于性能来说非常好,但可能会导致调试不精确的总线故障时出现一些复杂性。 通过更好地研究文档,我们发现 ARM Cortex M4 辅助控制寄存器中的 DISDEFWBUF 位在设置为 1 时会禁用默认内存映射访问期间的写入缓冲区使用。这会导致所有 BusFault 都成为精确的 BusFault,但会降低性能,因为任何存储到内存的操作都必须在处理器执行下一条指令之前完成。这样,处理器将不会继续执行下一条指令,直到写入操作完成,因此启用该位并使用 Erich 的代码,保存的 PC 指向导致硬故障的指令。 在其他情况下,如果总线故障是由中断处理程序中执行的指令触发的,且其优先级高于总线故障处理程序,则设置 DISDEFWBUF 在调试过程中很有用,因为即使出现精确错误,BFAR 寄存器值仍然有效。
記事全体を表示
汽车模拟和传感器概述,包括 BCC 和高压传感器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Eric Wu 主讲 2015 年 3 月 19 日,天安 MCU 和汽车解决方案大会 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Eric Wu 主讲 2015 年 3 月 19 日,天安 MCU 和汽车解决方案大会 传感器
記事全体を表示
Ara240 DNPU Hands-On Training Welcome to the Ara240 DNPU Training! This page provides access to training materials, presentations, demos, recordings, and supporting resources related to the Ara240 DNPU. While live Q&A support will be available during the training period, all content will remain accessible for future reference and self-paced learning. Required Hardware The following boards are supported: FRDM i.MX 95 Pro FRDM i.MX 95 FRDM i.MX 8M Plus Ara240 DNPU Ara240 16GB M.2 Module microSD >= 64GB storage USB-C debug cable Internet (Ethernet) HDMI Monitor 100 W power supply (Anker Charger is recommended) USB mouse USB keyword 1080p USB Camera Required Software The required Linux image can be found at: Embedded Linux for i.MX Applications Processors | NXP Semiconductors Instructions Step1. Watch introduction DNPU Training Introduction Ara 240 Software Components Presentation  Step2. Check the Hardware and Software Pre-requisites Getting Started Guide with FRDM-IMX8MPLUS Step3. Run the rest of the Software demo packages After completing the pre-work, each lab has its own guide document and a video guide you can use as support material in case you have any question at any step: Lab1: Running a GStreamer Pipeline for 8 Video Streams with YOLOv8n on Ara240 DNPU Ara Vision Multi-Stream YOLOv8 Object Detection Lab2: Running Unimodal Large Language Models on Ara240 DNPU LLM Edge Studio Lab3: Interacting with Vision-Language Models on Ara240 DNPU VLM Edge Studio Lab4: Enabling REST-Based LLM and VLM Inference on Ara240 DNPU eIQ AAF Connector Lab5: Running the Smart Device Gateway server on Ara240 DNPU  Smart Device Gateway  Additional Resources Take advantage of the resources below to deepen your knowledge and support your development efforts: Ara Software Development Kit (ARA SDK) Ara240 DNPU Six Pack Ara240 Discrete Neural Processing Unit (DNPU) Ara240 16GB M.2 Module FRDM i.MX 95 Pro FRDM i.MX 8M Plus ARA240 DNPU Hands-On Training
記事全体を表示
S32K314 RTD (MCAL) - OsIf クリティカルセクションが原因で発生した高優先度 ISR デッドロック S32K314 RTD (MCAL) - OsIf クリティカルセクションが原因で発生した高優先度 ISR デッドロック こんにちは、 私は以下のプラットフォームでアプリケーションを開発しています: MCU:NXP S32K314 RTD 7.0.0(AUTOSAR・マカル) FreeRTOS 7.0.0 S32 Design Studio 3.6.4 開発中に、優先度の高い割り込みに関連するデッドロックに遭遇しました。私の理解が正しいかどうか、また推奨される解決策があるかどうかをお伺いしたいと思います。 バックグランド FreeRTOSでは、configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITYよりも高い優先度を持つISRは、FreeRTOS APIを呼び出してはならないと規定されています。 しかし、多くのRTD MCAL APIは、内部的に以下の呼び出しチェーンを通じてFreeRTOSのクリティカルセクションAPIを実行していることがわかりました。 MCAL API ↓ SchM_Enter_xxx() ↓ OsIf_SuspendAllInterrupts() ↓ SuspendAllInterrupts() ↓ OsIf_Interrupts_SuspendAllInterrupts() ↓ taskENTER_CRITICAL_FROM_ISR() そして、 MCAL API ↓ SchM_Exit_xxx() ↓ OsIf_ResumeAllInterrupts() ↓ ResumeAllInterrupts() ↓ OsIf_Interrupts_ResumeAllInterrupts() ↓ taskEXIT_CRITICAL_FROM_ISR() この挙動は、DIOやGPTのような単純なペリフェラルレジスタアクセスのみを行うAPIでも存在します。 問題 MCAL API が高優先度 ISR (configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY より高い優先度) から呼び出されると、taskENTER_CRITICAL_FROM_ISR() の内部呼び出しによって FreeRTOS の割り込みマスキング状態が不整合になります。 その結果、taskEXIT_CRITICAL_FROM_ISR() が戻った後、BASEPRI が正しく復元されず、SysTick や PendSV などの優先度の低い割り込みがマスクされたままになります。 xPortSysTickHandler() が実行されなくなるため、スケジューラは最終的に停止します。 以下のようなAPIを使用して、この問題を再現することができました。 Dio_FlipChannel() GPT(PIT)割り込みプロセッシング SchMの排他領域を使用するその他のMCAL API 現在の回避策 RTDで生成されたソースコードを直接変更することを避けるため、GNUリンカーの--wrapオプションを使用して以下の関数をラップしました。 OsIf_Interrupts_SuspendAllInterrupts() OsIf_Interrupts_ResumeAllInterrupts() ラッパーは現在の割り込み優先度をチェックします。 添付のWrapperExample.cを参照してください。 現在のISRの優先度がconfigLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITYよりも高い場合、元の関数はスキップされます。 そうでない場合は、元の実装を呼び出します。 この回避策は、生成されたRTDソースを変更せずにデッドロックを解消するようです。 質問 この挙動はRTD MCALのデザイン上当然のことですか? 高優先度のISRからDIO、GPT、CAN、または他のMCAL APIを呼び出すのは推奨されますか? NXPは、ウォッチドッグサービスやGPIOトグルなどの高優先度リアルタイム機能に対して専用ドライバ(複雑デバイスドライバ)の実装を推奨していますか? GNUリンカーの--wrapオプションを使用してOsIf_Interrupts_SuspendAllInterrupts()とOsIf_Interrupts_ResumeAllInterrupts()をラップすることは、許容できる回避策でしょうか? 生成されたRTDソースコードを変更する必要のない、この問題に対する公式または推奨される解決策はありますか? 何かアドバイスやご提案があれば、大変ありがたく思います。 よろしくお願いします。 Re: S32K314 RTD (MCAL) - High Priority ISR Deadlock Caused by OsIf Critical Sections こんにちは、 @tobara さん、 このケースは現在、RTD開発チームからの意見提出を待っています。 BR、ダニエル Re: S32K314 RTD (MCAL) - High Priority ISR Deadlock Caused by OsIf Critical Sections こんにちは、 ご質問に対する回答は以下のとおりです。 この挙動はRTD MCALの設計上当然のことですか?回答:はい、これはCAT1割り込み(つまり優先度がMAX SYSCALLより高い割り込み)からOSのAPIを呼び出すために起こります。MAX_SYSCALL以上の割り込みの手当は、RTOSの影響を受けずに最小限のレイテンシで作業を行うためです。RTOSによって生じるレイテンシを避けたいなら、最終的にRTOSを使うAPIを呼び出すべきではありません。 高優先度のISRからDIO、GPT、CAN、または他のMCAL APIを呼び出すのは推奨されますか? 回答:いいえ、最初の回答で述べた理由により、MAX_SYSCALより大きくすることはできません。 NXPは、ウォッチドッグサービスやGPIOトグルなどの高優先度リアルタイム機能に対して専用ドライバ(複雑デバイスドライバ)の実装を推奨していますか? 回答: RTD SchM、OSIf API、RTOSによる遅延に耐えられるなら、既存のドライバーを使い、MAX_SYSCALLより低い割り込みから呼び出しすればいいです。優先度アップの効果は引き続き得られますが、チケットに記載されている問題は解消されません。 GNUリンカーの--wrapオプションを使用してOsIf_Interrupts_SuspendAllInterrupts()とOsIf_Interrupts_ResumeAllInterrupts()をラップすることは、許容できる回避策でしょうか? 回答:いいえ、簡単な分析によると、この回避策は一方向のみを保護するものです。デッドロックは回避できるかもしれないが、優先度の高いISR(> MAX_SYSCALL)とレジスタ/リソースを共有する優先度の低いISRを保護するものではない。この実装は共有レジスタやグローバル変数に競合条件を導入することができます。 生成された RTD ソース コードを変更する必要のない、この問題に対する公式または推奨される解決策はありますか?回答 (ただし、RTD チームによる確認が必要です) : IRQ > MAX_SYSCALL から RTD / RTOS API を呼び出さないでください。現在のRTD->OSIF->RTOSのレイテンシに耐えられるなら、優先度の高いIRQをMAX_SYSCALLより低く設定すればいいです。 すべての回答はRTDチームによる確認が必要です。私はRTOSの観点から回答しています。 Re: S32K314 RTD (MCAL) - High Priority ISR Deadlock Caused by OsIf Critical Sections 詳細なご説明をありがとうございました。 私は今、NXP RTD/MCALの以下の設計制約を理解しました。 RTD/MCAL API は、優先度の高い ISR ( configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITYよりも優先度の高い割り込み) から呼び出してはなりません。 --wrapを使う ことでデッドロックを防ぐことはできますが、RTDクリティカルセクションをバイパスすると、リソースやレジスタが高優先度コンテキストと低優先度コンテキスト間で共有される際に競合条件が発生する可能性があります。 いくつか追加の質問があります。 アプリケーションが高優先度のISR(AUTOSARカテゴリー1 ISR)でのプロセッシングを必要とする場合、推奨されるソフトウェアアーキテクチャは何ですか?このような機能は、常に複雑なデバイスドライバ(CDD)として実装されるべきでしょうか、それとも専用の低レベルドライバーとして実装されるべきでしょうか? もしGPIOポートやタイマーチャネルが単一の高優先度ISRのみで、他のタスクやISRからは一切アクセスされない場合、レースコンディションに関する懸念はラップ回避策にも適用されます か? 現在のRTD/MCALは、高優先度ISRからのAPI利用をサポートしておらず、したがって高リアルタイム機能はCDDまたは専用ドライバで実装しなければならないと理解してよいでしょうか? 自動車分野以外の組み込みソフトウェアの経験から言うと、ハードウェア抽象化層はしばしばオペレーティングシステムに依存しないように設計されています。そのため、単純なGPIOおよびタイマーAPIが内部的にRTOSのクリティカルセクションAPIを呼び出していることに気づいて驚きました。 参考までに、この問題を避けるために実装したGPTドライバー(CpuPit.h/c)を添付しました。 RTDチームからのご意見やご提案をいただければ幸いです。 改めてサポートありがとうございます。
記事全体を表示
Regarding the CAN issue of s32k344 The compiler I am currently using is s32ds3.4, RTD2.0.0. Among them, CAN FD function is enabled for can0-can5, and ENABLE RX FIFO function is enabled for can0. The implemented function is that can1 sends 64bit data to can0, can4 sends 64bit data to can2, and can3 sends 64bit data to can5. However, why can can0 and can5 receive data normally but can2 cannot receive data? When I set can4 to Loop-back mode, can4 can also receive data normally. The hardware connection is achieved by connecting CANH of can1 to CANH of can0, CANL of can1 to CANL of can0, CANH of can4 to CANH of can2, CANL of can4 to CANL of can2, CANH of can5 to CANH of can3, and CANL of can5 to CANL of can3 using DuPont wires. Here is my code 回复: Regarding the CAN issue of s32k344 I found a problem. The pin configuration is incorrect
記事全体を表示