FXTH87 flash operation functions Why nothing changed after calling function TPMS_FLASH_ERASE() and TPMS_FLASH_WRITE() ? What's wrong with code below ? fosc = 8MHz, fbus = 4MHz FCDIV = 21; // Fclk = 4MHz / (21+1) = 181.18KHz - 150KHz~200KHz //---------------------------------------------------------------------------------- const BYTE CParaAddr[] @ 0xD200u = { 0x44, 0x55, 0x66, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, }; ...... FCDIV = 21; SendDebugContent(CParaAddr[0], CParaAddr[1], CParaAddr[2]); // receive data are { 44 55 66 } mRfData1 = TPMS_FLASH_ERASE((WORD)CParaAddr); // the function return 0x00, ERASE succeed ? mCommonBuffer[0] = 0x77; mCommonBuffer[1] = 0x88; mCommonBuffer[2] = 0x99; TPMS_FLASH_WRITE_1A((WORD)CParaAddr, &mCommonBuffer[0], 10); SendDebugContent(CParaAddr[0], CParaAddr[1], CParaAddr[2]); Re: FXTH87 flash operation functions Resolved. CParaAddr is defined as const array. SendDebugContent(CParaAddr[0], CParaAddr[1], CParaAddr[2]); The compiler give three const to the function as parameters directly, instead of accessing the const array again. Re: FXTH87 flash operation functions the 2nd time calling SendDebugContent(CParaAddr[0], CParaAddr[1], CParaAddr[2]); receive data is still { 44 55 66 }, nothing changed
View full article