Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
如何将 KMZ80 的输出信号设置为 SENT 样式? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我被告知,恩智浦交付的 KMZ80 芯片默认为 AD 信号样式,如果客户想使用 SENT 信号样式,我们必须自己校准芯片,对吗? 我们能否直接购买 SENT 信号样式的 KMZ80?我没有从 KMZ80 产品数据手册(rev.3)中找到有关输出信号格式设置方法的有用相关描述-- 2019 年 4 月 26 日)。 磁力传感器 Re: How to set output signal of KMZ80 to SENT style? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> > 请联系 [email protected] 好的,我稍后再联系。 Re: How to set output signal of KMZ80 to SENT style? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 谢谢,现在我注意到了。 Re: How to set output signal of KMZ80 to SENT style? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 马亮,你好、 感谢您使用 KMZ80,您需要一个编程套件来对传感器寄存器进行编程,以便切换到 SENT 输出模式,请联系[email protected]获取套件。 编号 文廷 Re: How to set output signal of KMZ80 to SENT style? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,梁、 正如您在数据手册(第 8 章)中所注意到的,KMZ80 在引脚 OUT/DATA 上提供符合 SAE J2716 SENT 标准的数字输出信号(如果寄存器 SYS_SETTING 中的第 12 位设置为逻辑 1)。 测得的角度 α 被线性转换成一个值,并在 SENT 帧中进行数字编码。为此,可提供正或负的角斜率特性。 顺祝商祺! 托马斯
查看全文
FXLS90322 問題 1. 2軸センサデータ取得: 2軸データの取得において、デフォルトの12ビットデータバイト、8ビットチェックを使用しました。SPI通信を使用した場合、図によると、32ビットデータパケットは後続の17ビットデータ(9ビットノイズ、8ビットCRC)を削除するはずでしたが、実際のシミュレーションでは後続の12ビットを削除しており、データは正常でした。また、図は下記のセンサ応答フォーマットと一致していません。これはどのように理解すればよいでしょうか? 2.トリム感度 トリム感度は固定ですか?例えば、FXLS90322のトリム感度は33.0161(12ビット、LSB/g)ですか?もし固定であれば、11.2.24.1の項の式で計算された感度は実際の感度と一致しません。   Re: FXLS90322 probelm こんにちは、ウェンフェンさん 1.この質問は私にはよく分かりません。以下の点を明確にしていただく必要があります。 データ取得にレジスタ読み取りおよびセンサデータ要求コマンドを使用していますか? センサデータ要求を使用している場合、提供される 12 ビット (下の 2 番目の図で黄色で強調表示) は、3 番目の 図の赤い円と一致します。12 ビット解像度構成では、「オプションの SD 解像度」ビットはすべて 0 になります。 2. TrimSensitivity はバリアントによって固定されており、中 g デバイスの場合は 12 ビットで 33.0161 LSB/g です。その他の解像度 (10 ビット、16 ビットなど) の場合は、表 218 で定義されているように TrimSensitivity をスケーリングする必要があります。 お役に立てれば幸いです。 BR、トーマス
查看全文
FXLS8471Q replacement from NXP Hi. FXLS8471 is in EOL status. It lent us an excellent service with nice performance for my application. It is a difficult time to search for a replacement. I understand that. Are there any updates of possible replacement of FXLS8471Q ?  What I need is  an 14bit (may be 12bit with very low noise), +/-2g @ < 100 Hz, in full production status. One year has gone since EOL notification and we still can not find a replacement or similar part from NXP brand. Any comments or plans will be appreciated. Thank you! Accelerometers Re: FXLS8471Q replacement from NXP Hi Adelon, a) what happens with signal to noise ratio in our specific application; [A] The signal to noise ratio will be about four times worse, than the FXLS8471 14 bit+, +/-2g accelerometer you have used before. I presume you will use only +/-2g from the +/-8g span and the resolution is for the full +/-8g span. Unfortunately in the MMA8491Q maximum g span cannot be changed. I apologize for inconvenience and that we cannot offer you a better solution. b) how about those 20.000 pieces and their lead time until NXP issues a new 14 bit+, +/-2g, in full production. [A] The Chiron with 14-bit resolution is only planned, but is not approved yet. Currently we don't know if the Chiron or any other accelerometer will have +/-2g span and when there will be a new 14 bit+, +/-2g, in full production. I apologize for inconvenience.  With Best Regards, Jozef Re: FXLS8471Q replacement from NXP Thank you for your answer.   In our case, as we need a +/-2g span, we should study oversampling MMA8491Q (14 bits, +/-8 g, 1 mg/LSB) to 16 bits in order to obtain 0,24 mg/LSB and see: a) what happens with signal to noise ratio in our specific application; b) how about those 20.000 pieces and their lead time until NXP issues a new 14 bit+, +/-2g, in full production. Any way I think MMA8491Q might surely result in an acceptable provisional replacement for many FXLS8471 users Regards! Re: FXLS8471Q replacement from NXP Hi Adelon, I apologize, that the FXLS8962 is not available anymore. It supposed to be available. It seems its sold out earlier than we thought. But has 12-bit resolution, so it wouldn't help you anyway. Unfortunately currently we do not have a 14-bit 3-axis accelerometer, in Active stage of life in our portfolio, but I have checked the distributor pages and Mouser has 108 of MMA8491QR1 (End Of Life) in stock and another 20 000 can be ordered.  https://www.nxp.com/products/sensors/accelerometers:ACCELEROMETERS https://www.mouser.com/ProductDetail/NXP/MMA8491QR1?qs=sGAEpiMZZMsI%2FesINBwTt%252B%2F5LLuZJZqJmOeUnz8EUgg%3D Also Arrow has 7 pieces of MMA8491QR1 in stock. Perhaps they will have more pieces to order.  https://www.arrow.com/en/products/mma8491qr1/nxp-semiconductors?q=MMA8491QR1 I hope it will help you and I apologize for inconvenience. With Best Regards, Jozef Re: FXLS8471Q replacement from NXP Josef: I don't think it is neither exact nor fair to mark this answer as a solution to this situation.  Recommended parts in your answer are obsolete (FXLS8962 is non stocked, last time buy listed) and/or non stocked anywhere and all of them have less resolution than the 14 bits FXLS8471. Please tell me if I am missing something that could lead an NXP faithful follower to a solution, among NXP portfolio. Re: FXLS8471Q replacement from NXP Hi Adelon, it is unfortunate situation right now. Although we have replacements for the discontinued parts, the factories are not able to product enough chips to cover the demand. I apologize for inconvenience.  Regarding the Chiron accelerometer, you need to contact your local NXP Authorized distributor directly (https://www.nxp.com/support/sample-buy/distributor-network:DISTRIBUTORS). With Best Regards, Jozef Re: FXLS8471Q replacement from NXP Thank you Jozef for your answer.  I have studied those alternatives you suggested. However I can not find any of them to be purchasable  or with a certain delivery lead time.  Can you please help with some commercial part number of those "Chiron-NPI" line of 14 bit accelerometers? Re: FXLS8471Q replacement from NXP Hi Adelon, the discontinuation of the FXLS8471. The replacement is FXLS8462 which will be later replaced with pin and software compatible FXLS8964/67/74 family of accelerometers. With Best Regards, Jozef
查看全文
MPXV5100GP Long term accuracy Hello, Our client has been using a MPXV5100GP in a product for several years with good success. We are wondering if NXP collects any long term accuracy data? We have read the NXP docs concerning reliability testing at the factory which attempt to infer long term reliability. The product is only used intermittently (not continuous duty) and the max pressure is usually well under 100 kPa. It also typically used indoors so the typical operating temperature is around 25 degrees C. If you have any data or can refer us to any data, please let us know. Thanks, Bart J Pressure Sensors Re: MPXV5100GP Long term accuracy Hello Bart, You can create a standard request (we call it "case") here. My colleagues who are in charge of the NDA process will assist you and then I can send you the FIT data. But keep in mind it is just a statistic about device's reliability, it does not say anything about long term accuracy. Best regards, Tomas Re: MPXV5100GP Long term accuracy Tomas, Yes, lets move ahead on this. What are the next steps on my end? Do I first sign an NDA from you or do I just implement a "standard request" and the NDA will be an outcome of that process? Thanks again! Re: MPXV5100GP Long term accuracy Hello Bart, FIT stands for Failures In Time, you can find more details here.  Best regards, Tomas Re: MPXV5100GP Long term accuracy Tomas, What exactly is the FIT data? Thanks for your response. Re: MPXV5100GP Long term accuracy Hello Bart, Based on the feedback from our QA team, I would be able to share only the FIT data. However, this requires a signed NDA with NXP and entering a standard request. Best regards, Tomas Re: MPXV5100GP Long term accuracy Hello Bart, I assume our qualification testing is all we have in terms of reliability data over the life of the device which includes accuracy, but I have requested input from our QA guys. I will update this thread and let you know what they say in the next few days. Best regards, Tomas
查看全文
TSS(タッチセンシングソフトウェア)ライブラリの移行 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 専門家の皆様、 現在、冷蔵倉庫制御プロジェクトでは S12ZVC MCU が使用されています。タッチセンシングUIも必要です。 TSS ライブラリを S12ZVC に移行できるかどうか知りたいです。 移行できない場合は、インダストリアルグレードまたはオートモーティブグレードの MCU を推奨してください。MCU には CAN と ADC が必要です (ADC にプログラム ゲイン制御があれば最適です)。 よろしくお願いいたします。 キガー 磁気センサ 圧力センサ センシング・プラットフォーム タッチ・センサ Re: TSS(Touch Sensing Software) library migration <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるトーマスへ 本当にご協力ありがとうございました! Re: TSS(Touch Sensing Software) library migration <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるキガー様 TSS は新しいデザインには推奨されなくなり、S12ZVC デバイスのサポートを追加する予定はありません。ほとんどの Kinetis MCU をサポートするNXP Touch Softwareという新しいソフトウェア ライブラリがあります。Kinetis E シリーズは良い選択かもしれませんが、TSI モジュールは CAN モジュールを持たない KE1xZ でのみ使用できます。 したがって、I 2 C を介して S12ZVC に接続できる当社のスタンドアロン タッチ/近接センサー を検討することをお勧めします。 お役に立てれば幸いです。 よろしくお願いいたします。 トーマス 追伸: 私の回答が質問の解決に役立った場合は、「正解」とマークしてください。ありがとう。
查看全文
SensorFusion 7.0 の方向ドリフトの問題 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私は、9-DOF MEMS ナビゲーション デバイス ( InvenSense MPU-9250 、できれば NXP の部品を含む) を使用して、カスタム設計されたハードウェア、ソフトウェア、およびドライバでリアルタイムの方向を提供するアプリケーションを開発しています。すべてがカスタムであるため、SensorFusion 7.0 ライブラリを SDK で提供されるコア ルーチンにまで削減する必要がありました。さらに、初期化関数を直接呼び出し、ジャイロ、磁力計、加速度センサの 1 要素 FIFO にデータをロードする独自の関数を作成しました。 MPU-9250 の軸は、下の図のように定義されています。したがって、磁力計の軸を回転させて、ジャイロと加速度センサと同じにします。これは、Z 軸を反転し、X 軸と Y 軸を交換することによって行います。 また、単位が正しいことも確認しました (加速度は g、回転速度は度/秒、磁力計はマイクロテスラ)。整数と浮動小数点数の「単位あたりのカウント数」と「単位あたりのカウント数」の変換係数を適切に設定しました(少なくとも私はそう信じています)。 私はfRun_9DOF_GBY_KALMANアルゴリズムを 200 Hz で実行し、9 つの軸すべてに対して 200 Hz で新しいデータ/サンプルを 1 要素 FIFO にロードしています。デバイスを少し動かすと、 iFirstAccelMagLockフラグが 0 から 1 にスイッチすることがわかりました (これは良い兆候のようです)。 しかし、カルマンフィルタの様々な角度出力は、 fPhiPl; ///< ロール (度) fThePl; ///< ピッチ (度) fPsiPl; ///< ヨー (度) fRhoPl; ///< コンパス (度) fChiPl; ///< 垂直からの傾き (度) fDeltaPl; ///< カルマンフィルタからの事後傾斜角(度) 空間を漂っているように見え、デバイスの実際の回転には反応しません。 静止状態での長期平均を使用して、ジャイロの DC オフセットを測定してみました。それは約 0.5 度/秒なので、これを差し引いても、このドリフトと応答の欠如は解消されません。 したがって、SensorFusion 7.0 ライブラリの使用に関して次の質問があります。 ジャイロの回転方向を含む、9 つの自由度すべてについて、予想される入力軸と単位が正確に指定されている場所はどこですか?X、Y、Z 軸はジャイロ、磁気、加速度に対して一貫している必要があり、ジャイロの回転方向に対しては右手の法則が満たされる必要があると想定しています。しかし、もう一度言いますが、これはどこかに正確に文書化されているのでしょうか? アルゴリズムはジャイロ DC オフセット/ドリフトに対してどの程度敏感ですか?ハードウェアに合わせてこれを正確にゼロにする必要がありますか? メイン ループにキャリブレーション ルーチンが欠けているのでしょうか? SensorFusion (fRun_9DOF_GBY_KALMAN) は磁力計のキャリブレーションに対してどの程度敏感ですか?私の磁力計は 10 倍ずれているようですが、金属がたくさんある場所にあるため、磁場成分 (X、Y、Z) もずれているかどうかはわかりません。磁力計の読み取り値と磁場の歪みが最小限でなければ、アルゴリズムは適切に動作しないと考えられますか?コード内に硬鉄/軟鉄およびキャリブレーション ルーチンがいくつか含まれていたので、これらがキャリブレーションされていない磁力計の補正にどの程度役立つのか疑問に思っています。 iFirstAccelMagLock = 1 の場合、何を意味しますか?これは、SensorFusionが磁力計とジャイロデータが正しく連携して動作していると認識しているという意味でしょうか?それとも、ジャイロと磁力計のデータが何らかの理由で壊れていても、iFirstAccelMagLock = 1 になる可能性はあるのでしょうか?言い換えれば、この変数は正常な動作を示す指標としてどの程度信頼できるのでしょうか? 9-DOF デバイスを 200 Hz でサンプリングし、1 要素 FIFO を使用して 200 Hz でデータを SensorFusion にロードしています。私のサンプルのアナログ帯域幅は約 50 Hz または 100 Hz です (これを設定することができます)。SV_9DOF_GBY_KALMANの出力も200Hzで読み取っています。このアプローチに何か問題はありますか? これを適切に動作させるために、他に何かアドバイスはありますか? センサ・フュージョン Re: Problem with Drift in Orientation with SensorFusion 7.0 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ジョナサン、 通常、競争力のある部品のポートのサポートは提供していません (Invensense は NXP の競合です) が、いくつかの質問にお答えしたいと思います (他の方も追加の提案があれば歓迎します)。順番に: 1. ユーザー ガイドのセクション 5.3 では、ハードウェア抽象化の問題について説明します。 2. カルマン フィルタには、追跡する変数 (XY および Z) の 3 つとしてジャイロ オフセットが含まれます。デバイスが回転している限り、それらの推定値は継続的に更新されます。磁力計とジャイロの参照ベクトルは、デバイスが静止しているときに安定性を保つ必要があります。 3. 申し訳ございませんが、コードレビューは提供できません。 4. 適切な磁気校正が非常に重要です。これがないと、9 軸の良好な結果は期待できません。私たちが組み込んでいるルーチンは、一般に、センサに対して空間的に固定された硬鉄/軟鉄源の処理をかなりうまく行います。一般的な干渉を処理するためのコードもいくつか含まれていますが、それをどれだけうまく処理できるかには限界があります。 5. コードのコメントを確認すると、 iFirstAccelMagLock は初期化コードが一度だけ実行されるようにするためのブール変数であることがわかります。この値から全体的な健全性を推測しないでください。 6.MCU に十分な MIPS がある限り、あなたが概説したアプローチに問題はないと思います。 7. マニュアルを読みます。私はできる限り多くの「集合知」をそこに盛り込もうとしました。 よろしくお願いいたします。 Mike
查看全文
TSS(触摸感应软件)库迁移 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 亲爱的专家 现在一个冷库控制项目使用了 S12ZVC MCU。 它还需要触摸感应用户界面。 我想知道是否有可能将 TSS 库迁移到 S12ZVC? 如果无法迁移,请推荐工业或汽车级 MCU。MCU 必须具有 CAN 和 ADC(最好 ADC 具有程序增益控制功能)。 顺祝商祺! 基格 磁力传感器 压力传感器 传感平台 触摸传感器 Re: TSS(Touch Sensing Software) library migration <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 亲爱的托马斯 非常感谢你们的帮助! Re: TSS(Touch Sensing Software) library migration <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 亲爱的基格 不再建议将 TSS 用于新设计,也没有计划增加对 S12ZVC 设备的支持。新的软件库--恩智浦触摸软件支持大多数 Kinetis MCU。Kinetis E 系列可能是一个不错的选择,但 TSI 模块只适用于没有 CAN 模块的 KE1xZ。因此,我建议考虑使用我们的独立组网 \\(SA\\) 触摸/近距离传感器 ,它可以通过 I 2 C 连接到 S12ZVC 希望对您有所帮助。 顺祝商祺! 托马斯 PS:如果我的回答有助于解决您的问题,请标记为"正确" 。谢谢。
查看全文
NXP MPXV5050 Vacuum sensor support We have been working for a AUTOMOTIVE FILTER SENSOR project, based on MPXV5050 (NXP absolute vacuum sensor. We've deveoped our customized board using NXP MCU S9S08 Series. We have matched all the functional points required for reading pressure/ vacuum via MCU ADC & convert it to digital value. During our testing we set point as 3.276 V corresponding to 405mBar Since boards were meeting all required o/p parameters in testing conditions without potting in housing/ enclosure, Later after QC testing as OK, We Potted it with Hard-Epoxy component. After potting, we found the Reference has shifted by 30mBar. What could be the reason, Please help us with suggestions/ remedies / precautions to be taken care. Meanwhile, can you kindly connect me with any NXP PRESSURE/ VACUUM Sensor experts to Resolve the issue. Re: NXP MPXV5050 Vacuum sensor support Is there some sensor that may  I use directly with water? Re: NXP MPXV5050 Vacuum sensor support Hello Mahesh, My apologies for the delayed response. Please note that for all NXP standard pressure sensor products, any environment other than dry air, will have some impact on the reliability and lifetime of the product. NXP's silicon pressure sensors are NOT compatible with oil, gas, petrol and water or water vapors, or chemicals. A determination must be made if this impact is acceptable for the application. That means that you cannot use our pressure sensors in such applications in which the sensor may be in direct contact with diesel.  After some working hours, maybe days the device would fail. I would like refer to the following application notes that would be worth to be considered in addition to the provided information and solutions: AN3728 - Media Compatibility for IPS PRT Pressure Sensors AN1516 - Liquid Level Control Using a Pressure Sensor AN1950 - Water Level Monitoring In regard with the soldering and mounting techniques about the axial port, other than the information on the datasheet, we only have the material composition declaration report of this device that you can find on the following link: MPXV5050VC6T1 - MCD Report The AN1984  about how to handle NXP Pressure Sensors may be useful for you: I hope this information will be useful for you. If I misunderstood your question, feel free to let me know.  I will be glad to help. Have a great day. David Diaz. Re: NXP MPXV5050 Vacuum sensor support Hi David, Thanks for your support on Vacuum sensors, Meanwhile there are 2 more queries. 1. After inserting the FULLY-MOUNTED PCB in housing ... during field trial with Vehicle sensor P1 side of housing comes in contact with DIESEL...     Kindly let us know what would be the consequence/ effect on MPXV5050 Vacuum sensors. 2. Can we have specific mounting and soldering information on single port, Axial, type of sensor package. The part number is MPXV5050VC6T1. Your App notes, shared earlier, do not talk about this package. Kindly guide Regards Mahesh.V.S. Re: NXP MPXV5050 Vacuum sensor support Hi David, Thanks for your response. Customer would like to have specific mounting and soldering information on single port, Axial, type of sensor package. The part number is MPXV5050VC6T1. Your App notes, shared earlier, do not talk about this package. Thanks in Advance. Mahesh.V.S. Re: NXP MPXV5050 Vacuum sensor support Hello Rajiv, The MP3V5050VC6U is a Gauge pressure sensor, which means that, it measures the difference between the absolute pressure and the Local atmospheric pressure. P2 port is intended to be left open to the atmosphere. I strongly do not recommend covering the small hole. Have you considered using an Absolute pressure sensor? The typical voltage supply of almost all our absolute pressure sensors is 5V. Unfortunately, that range of pressure is not available. In regard with the assembly guidelines, I would like to recommend the following documents that describes several mounting techniques, offers lead forming recommendations, soldering recommendations, and suggests means of testing the MPX series of pressure sensors: 1. Mounting Techniques, lead forming, and testing of the MPX Series pressure sensors 2. Soldering Recommendations for Pressure Sensor Devices I hope this information will be useful for you. If I misunderstood your question, feel free to let me know.  I will be glad to help. Have a great day. David Diaz. PS: If my answer helps to solve your question, please mark it as "Correct". Thank you. Re: NXP MPXV5050 Vacuum sensor support Hi David two more question: 3. Is there a 5 Volt Vacuum sensor with -50 to 0 Kpa range, the current one we are using is 3.3V 4. Do you have any assembly guidelines App note for pressure sensors? Regards, Rajiv Bandodkar. Re: NXP MPXV5050 Vacuum sensor support Hi David, 1. In our application we have selected MP3V5050VC6U, and the single port is connected to the diesel filter, there will not be the occasion to reference it to atmospheric pressure. So what is the solution. 2. The P2 hole in the sensor: should it be open to atmosphere? if yes, How about contamination with dust, water, etc Regards, Rajiv Bandodkar. Re: NXP MPXV5050 Vacuum sensor support Hello Mahesh, I assume the pressure on-box after the potting compound is affecting on the pressure sensor because it is pressing down the sensor package affecting its measures and creating this offset.The temperature could be another factor. In this case, I recommend Implementing Auto-Zero for Integrated Pressure Sensors. Auto-zero is a compensation technique based on sampling the offset of the sensor at reference pressure (atmospheric pressure is a zero reference for a gauge measurement) in order to correct the sensor output for long-term offset drift or variation. I hope this information will be useful for you. If I misunderstood your question, feel free to let me know.  I will be glad to help. Have a great day. David Diaz. PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
查看全文
欢迎 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 用于 Kinetis MCU 的 Freescale 传感器融合库可从以下网址获取 http://www.freescale.com/sensorfusion. 这个社区空间为该库的用户和开发人员提供了一个集中的场所,使他们能够聚在一起解决问题、分享见解并了解有关传感器融合主题的更多信息。 我负责管理创建融合库的团队。 我们认为我们有一些特别的东西,并期待与您分享。 迈克尔-斯坦利 飞思卡尔传感器解决方案部 传感器融合
查看全文
RDKL25AGMP01 ボード <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> # RDKL25AGMP01 ボード-10 軸センサー RDKL25AGMP01 ボードを持っています。最初は 3 色 LED が点灯していましたが、1 分後に点灯しなくなりました。どうすればよいでしょうか。 ジャイロスコープ Re: RDKL25AGMP01 BOARD <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ニラジさん。 おそらくPCがボードを認識していないのだと思います。Windows 10 をお使いですか?そうであれば、Windows 10 システムの場合、ボードを Windows 10 マシンに接続すると、古いバージョンの OpenSDA ドライバが破損する可能性があります。その結果、多くのボードが Win 10 で MSD または COM ポートとして検出されなくなる可能性があります。現在の FRDM-K64F、FRDM-K22F、FRDM-KL25Z、および RD-KL25-AGMP01 ボードには、工場出荷時に古いバージョンの OpenSDA ドライバが付属しており、必須の OpenSDA アップデートが必要です。 このボードの OpenSDA を更新するには、 https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/の手順に従ってください。 これが役に立つことを願っています。 すてきな一日を、 パウリナ --------------------------------------------------------------------------------- 注記: - この投稿があなたの質問への回答である場合は、「正解としてマーク」ボタンをクリックしてください。ありがとう! - スレッドは最後の投稿から7週間フォローされます。それ以降の返信は無視されます。 後ほど関連する質問がある場合は、新しいスレッドを開いて、閉じたスレッドを参照してください。 ---------------------------------------------------------------------------------
查看全文
mystical sensor MPL3115 Hello, developers! Now i make a project " portable weather station" based on MPL3115. Primary functions: display current time, e-kompass, pressure, altitude, temperature and weather forecast. its a batterry-operated devices, and components must have minimal Supply Current. when I found a MPL3115 i been really excited, because this IC have all what i need. But now my project is has stalled. Firstly, i wrote a source code as datasheet recomendations, for set and change mode of MPL3115, read registers and display the results. i test code and sensor at LPC-812 MBED board (because i like LPCXpresso) and sensor board is powered from LPC-812 (3.3 Volt). and I got the some results (pressure, temperature and altitude). Next, i reading a AN3914 ("Modern Altimeter and Barometer System using the MPL115A") and start to adaptation this algorithm for  MPL3115. for  make a weather forecast i need to get  pressure change per 1 hour. for this, i chose a 3-hours/180 minutes interval for collected samples in FIFO every ~20 minutes. User should be able get a weather forecast at any time, so program must compare oldest and newest samples (for example, now is 11-10 AM, oldest sample was obtained at 8-00 AM, newest samples at 11-00 AM. i compare  this samples, divided and get a pressure change per 1 hour. then i make a weatern pattern and display it. next samples update will be at 11-20 AM. ) but i get a first STOP: bytes, reading from FIFO, "deleted from the front of the FIFO buffer" (page24 DS). so if I read values ​​from the buffer, I lost them. and if i make a weather pattern as in the above example at 11-10AM, at 11-20 AM i can't get the data from FIFO. next possibility for 1 hour pressure change i will get only via 1 hour!  all the collected data (from 8-20 AM to 11-20 AM) will be LOST! So. this way is not work.:smileyshocked: Ok, AN3914 have another faster way to make a weather forecast (page 6)! all i need - it's a  pressure and current altutude (MPL3115 must give all of this). i must calculate "ideal pressure" Pweather (for good sunny day) for current altitude by using the equation: Pweather = (101.3 * exp(((float)(CurrentAltitude))/(-7900))). and compare current pressure with "ideal". i wrote a code: set Altimeter mode and get a current altitude, set Barometer mode and get a current pressure, calculate and display result of weather pattern. i live in area at 56—178 meters of sea level. i start the test and get a second STOP  : sensor's PCB is on the table at room temperature (22-24 C) and does not move. source code don't change.  in the morning i have altitude=102 meters, in the dinner =32 meters, in the evening 0 meters. i turn on Debugger and see: when  I read data registers in Altimeter mode, OUT_P_MSB Register= 0xFF, so i get incorrect data from sensor . But i get correct temperature data in this reading operation (i make a cycle read 5 bytes from sensor at one procedure). So,this way does not inspire confidence... I just have to find a shaman! Because I can not find understanding with this really fine sensor. May be anybody help me? Best regards, Ellis Pressure Sensors Re: mystical sensor MPL3115 Hi Ellis, We have some code examples and other documentation available in Freescale communities, perhaps it can be useful: https://community.freescale.com/community/sensors/content?filterID=contentstatus%5Bpublished%5D~objecttype~objecttype%5Bdocument%5D&query=MPL3115A2 Regards, Jose
查看全文
NTM88 SPIポート こんにちは、 CodeWarrior に NTM88 スターター プロジェクトをロードしました。代わりに SPI インターフェースを使用してセンサ データを別のボードに送信するように変更したいと思います。SPI に関連するライブラリが見つかりません。 よろしくお願いいたします。 マーケル Re: NTM88 SPI Port ありがとうございます。 Re: NTM88 SPI Port こんにちは、マルケルさん。 SPI 経由でホスト MCU に転送されるセンサー データの例は、ユーザー ガイドを含むこのデモ パッケージで入手できます。 以下からダウンロードできます: https://www.nxp.com/products/sensors/pressure-sensors/tire-pressure-monitoring-sensors/ntm88-highly-integrated-tire-pressure-sensor:NTM88?#design-resources よろしくお願いいたします。 トーマス
查看全文
FXOS8700CQ pulse detection I am trying to get double-tap detection to work properly. I think the data sheet is a little unclear. Is the treshold values (PULSE_THSX/Y/Z) absolute values or differential values? Depending on orientation there will be a static value between -1g and +1g. The tap comes on top of that. The time steps in table 135 and 136 refers to HP_FILTER_CUTOFF[pls_hpf_en] = 0 or 1. However, the HP_FILTER_CUTOFF doesn't have a pls_hpf_en bit. It has bits pulse_hpf_byp  and pulse_lpf_en. I can't find any description what these two bits are doing. Why would you want low pass filter for pulse detection? Accelerometers Re: FXOS8700CQ pulse detection Hello Kurt, The tap/pulse detection function can be configured to run through the high-pass filter (HPF) using the pulse_hpf_byp bit. If pulse_hpf_byp = 0, the tap/pulse detection function processes high-pass filtered data, so the threshold value in PULSE_THSX/Y/Z registers should not take into account the static acceleration. If pulse_hpf_byp = 1, the tap/pulse detection function does not process high-pass filtered data (HPF is bypassed) and the threshold value needs to take into account the static acceleration. As for the pls_hpf_en bit, it is indeed an error, the correct bit is pulse_lpf_en in the HP_FILTER_CUTOFF register. When the low-pass filter is enabled (pulse_lpf_en = 1), the time step doubles. The LPF should help eliminate additional ringing after the tap signature is detected. I hope it answers your questions. Best regards, Tomas
查看全文
IMX8MP搭載OV5640オートフォーカス 現在、Android 11 (NXP BSP) を実行する i.MX8MP プロセッサを使用したプロジェクトを開発しています。ハードウェア セットアップには、MIPI-CSI インターフェースを介してコネクテッドされた、オートフォーカス サポート付きの OV5640 カメラ モジュールが含まれています。 カメラの画像撮影とプレビューは機能していますが、オートフォーカス機能に関する問題が発生しました。i.MX8MP 用の標準 Android 11 BSP は、OV5640 の AF コントロールをネイティブにサポートまたは公開していないようです。カーネル 5.10.72 と OV5640 MIPI カメラ サブデバイス ドライバ (drivers/media/i2c/ov5640.c) を使用しています。 オートフォーカス サポートを含む i.MX8MP 用の更新された OV5640 カーネル ドライバーはありますか? あらゆるガイダンス、パッチ、またはリファレンスドキュメントをいただければ幸いです。 Re: OV5640 autofocus with IMX8MP こんにちは、 残念ながら、Android BSP では、車載 Focus Ccontrol はサポートされていません。OmniVision にお問い合わせする必要があるかもしれません。アプリケーションノート「Auto FocusCamera Module Application Notes」があります。ファームウェアと AF シーケンスについて言及されていますが、ドライバに AFC 機能を自分で追加する必要があります。 よろしくお願いいたします。
查看全文
How can i initialize "Remember my decision" in SDK Component Management I am using workspaceS32DS 3.4 for S32K144. i'd like to keep existing in DSK component file. However, I checked "remember my decision" and clicked replace, previously. so i'd like to initialize checked "Remember my decision". how can i initialize? Re: How can i initialize "Remember my decision" in SDK Component Management Hello all, I found the file where the choice is stored: .metadata\.plugins\org.eclipse.core.runtime\.settings\com.nxp.s32ds.cle.uct.core.prefs The file is saved at exiting S32DS, and the two new rows look like that: sdk.component.overwrite.ask=true sdk.component.overwrite.policy=Keep existing Just delete the rows before S32DS starts to re-initialize "Remember my decision". The behavior appears to be consistent across S32DS versions - I checked it on S32DS 3.4., 3.5 and 3.6. Best regards, Pavel Re: How can i initialize "Remember my decision" in SDK Component Management The same thing happened to me recently. To reset to the default settings, the best option I've found is to go to the folder you defined as "workspace" and delete the ".metadata" directory. When you open S32DS again and it asks you for the "workspace" path, enter it again and it's solved. You'll have to reimport the project, but you'll have unchecked "Remember my decision." Re: How can i initialize "Remember my decision" in SDK Component Management Hi, Thanks for the feedback. This may not be our best solution, but we may have to recommend reinstalling the software, given there is no general "default settings" or "factory restore", that we see. If we found anything else, we will let you know. We do apologize for this. Please, let us know. Re: How can i initialize "Remember my decision" in SDK Component Management hi, i can not find your mentioned option in "Window > Preferences > S32 Configuration Tools". i checked 5 options, [Generate source folder], [Always show details before update code], [Show pin label & identifier table columns], [Automatically load last configuration on startup], [Enable Code Preview]. Did not check options are  [Create empty configuration if no Yaml is available], [Always overwrite files without asking], [Require identifier for Pins].   Re: How can i initialize "Remember my decision" in SDK Component Management Hi, Could be that your option is related to the following configuration: "Window > Preferences > S32 Configuration Tools > Allow component migrations" If it is checked, it automatically migrates to newer versions of the components. Please, let us know if this information was helpful or not.
查看全文
[Harman] [IPCF] Support for IPCF4.3 Discussion Bringing this thread to community for tracking - See attached email thread. Harman reports some errors in the bring-up process of core1 under the IPCF demo. The current assumption is that this is related to PE debugger script influencing the core during startup. With PE scripts, this is not started as expected (I can confirm that this applies outside IPCF context as well). Best, Bryan IPCF Re: [Harman] [IPCF] Support for IPCF4.3 Discussion Hi Bryan,   Since Harman is using a customized boot flow that is not supported by our reference examples and as this is not an IPCF issue or something related to RTD/platform drivers based on their feedback I will propose to involve in this topic also CESS team.   Also there is no email attached to this post.   Best regards, Daniel
查看全文
i.MX RT1042 イーサネット PHY DP83825 での初期化失敗 - PHY を初期化できません こんにちは、 私は i.MX RT1042 イーサネット を使用しており、i.MX RT1040 EVK で使用されているオンボード KSZ8081 の代わりに TI DP83825 PHY 評価ボードを使用しようとしています。 KSZ8081 と関連するジャンパーを EVK から取り外し、ジャンパー ワイヤを使用して i.MX RT1042 からの RMII 信号 (TXD [1:0]、RXD [1:0]、TX_EN、CRS_DV、MDC、MDIO、RESET、REF_CLK) を DP83825 EVM に接続しました。 MCUXpresso SDK イーサネット の例を使用していますが、次のログが表示されます。 PHYを初期化できません ソフトウェアの変更: デフォルトの NXP SDK は KSZ8081 PHY ドライバーを使用します。 DP83825 用の PHY ドライバはないので、KSZ8081 ドライバを DP8384 をベースに置き換えました。 レジスタ マップと構成値はほぼ同様であったため、DP8384 PHY ドライバーを DP83825 に移植して適応させました。 PHY アドレスと基本的な初期化シーケンスもそれに応じて更新されました。 ハードウェアに関する注意事項: RMII インターフェースが使用されます。 DP83825 EVM の XI/XO ピンは、デフォルトのオンボード水晶構成のままになります。 DP83825 EVM には使用されないオンボード MCU が含まれています。PHY は i.MX RT1042 によって直接制御されるように設計されています。 質問: PHY 初期化が失敗する原因となる可能性のある i.MX RT 固有の要件 (PHY リセットタイミング、MDIO 初期化順序、クロック構成) はありますか? i.MX RT イーサネット ドライバーは、PHY ドライバー層を超えて KSZ8081 固有の動作を想定していますか? DP83825 EVM の XI/XO オンボード水晶構成により、外部 MAC とインターフェイスするときに問題が発生する可能性がありますか? i.MX RT Ethernet で Microchip 以外の PHY (TI DP838xx) を使用するための既知の リファレンス デザイン、アプリケーション ノート、または例はありますか? これが主にソフトウェア統合の問題なのか、ハードウェア/クロッキングの問題なのかについてのアドバイスがあれば非常に助かります。 よろしくお願いします。
查看全文
I.MX9596 M7コアをubootフェーズで手動または自動でロードする方法 こんにちは、 現在、I.MX9596チップを開発しており、M7コアを正常にコンパイルできるVSCode用のMCUXPresson開発環境を構築しました。しかし、uboot フェーズで M7 コアをロードするにはどうすればよいでしょうか? 方法はわかりましたが、それをどのように実装するかはわかりません。Uboot フェーズで M7 イメージをロードするには、imx95evkrpmsg を使用してシステム マネージャー (M33) をコンパイルする必要があります。生成された M7 イメージを SD/eMMC のブート (FAT32) パーティションにコピーします。このコマンドは Uboot フェーズで使用できます。 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@Zhiming_Liu FRDMのソースコードが手元にないので、コンパイルできません。ボード上でテストできるように、コンパイル済みのイメージを提供していただけますか? ありがたい! Re: I.MX9596 M7 core how to manually or automatically load in uboot phase EVKと自作ボードの両方を試しましたが、問題は同じです。EVKボードのソースコードがないため、ご提供いただいたイメージを使用しています。何か関連があるのでしょうか? EVK: テストできるように、M33 の画像を送っていただけますか? Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@HL_G L6.12.49デモイメージから「imx-boot-variant-rpmsg-imx95-19x19-lpddr5-evk-sd.bin-flash_lpboot_sm_a55」ファイルをロードできます。現在EVKをお使いですか?それともカスタムボードですか?EVKの場合、具体的なモデルは何ですか? よろしくお願いします、 志明 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@Zhiming_Liu 私たちが使っているのはこれです。 mkimgコンパイルコマンドは次のとおりです: `make SOC=iMX95 flash_a55 LPDDR_TYPE=lpddr4x OEI=YES` Re: I.MX9596 M7 core how to manually or automatically load in uboot phase imx-sm の場合は mx95evkrpmsg を使用するほかに、 imx-mkimage を使用する場合は flash_lpboot_sm_a55 が必要です。 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは。 Yocto 環境は設定せず、imx-sm と imx-mkimage を使用して手動でコンパイルしました。 IMXBOOT_VARIANT="rpmsg" オプションに対応する 2 つのソース コードにはどのような変更が加えられますか? ありがたい! Re: I.MX9596 M7 core how to manually or automatically load in uboot phase bitbake imx-boot を使用して imx-boot を個別にコンパイルするだけで済みます。これは非常に高速です。 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase これには yocto の再コンパイルが必要ですか? 再コンパイルには数日かかります。 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@HL_G yocto の local.conf ファイルにIMXBOOT_VARIANT="rpmsg"を追加し、次の imx-boot を使用してみてください。 よろしくお願いします、 志明 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase はい、bin ファイルをロードしても同じエラーが発生します。 よろしくお願いします、 HL_G Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@HL_G .bin ファイルをロードしても同じエラーが発生しますか? よろしくお願いします、 志明 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase imx-sm ファイルには、 imx95evkrpmsg に関連する構成が含まれています。 現在、M33のコアプログラムはこの方法でコンパイルされており、 M33からM7を起動することはできません。M7のbinファイルとelfファイルはSD/eMMCのBoot(FAT32)パーティションに配置されています。プログラムはubootステージでロードされますが、2番目のステップに達するとエラーが発生し、プログラムが再起動します。 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@Zhiming_Liu M7 コアをロードするときに、以下に示すようにエラーが発生します。 エラーの後、コア A が再起動し、M7 は情報を印刷しませんでした。 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@HL_G uboot での具体的な手順: パワーオン ブート用に M7 イメージを imx-boot にコンパイルするには、ドキュメントのimx-mkimageセクションを参照してください。 https://www.nxp.com/docs/en/ユーザーガイド/UG10163.pdf ただし、imx-sm にはimx95evkrpmsg に関連する構成はありません。 https://github.com/nxp-imx/imx-sm/tree/master よろしくお願いします、 志明 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@HL_G このボードと対応するyoctoはまだテスト段階にあり、正式リリースされていないため、現時点ではテストできません。このrpmsgバリアントは、imx-smのmx95evkrpmsgとimx-mkimageのlpboot_sm_a55に相当します。これら2つの.binファイルが確実に更新されていることを再度ご確認ください。 https://github.com/nxp-imx/meta-imx/blob/walnascar-6.12.49-2.2.0/meta-imx-bsp/conf/machine/include/imx95-evk.inc よろしくお願いします、 志明 Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@Zhiming_Liu imx-mkimg コンパイル、make SOC=iMX95 LPDDR_TYPE=lpddr4x OEI=YES flash_lpboot_sm_a55 を使用して自社ボードでテストした結果を次の図に示します。 make SOC=iMX95 LPDDR_TYPE=lpddr4x OEI=YES および flash_lpboot_sm_all で imx-mkimg をコンパイルした結果を次の図に示します。 他のファームウェアはすべて同じで、ロードに失敗します。再起動してもubootは再起動するだけですが、M33は正常です。ubootが許可されていないポイントにアクセスしたのではないかと考えています。これに対処する方法や提案はありますか? ありがたい! Re: I.MX9596 M7 core how to manually or automatically load in uboot phase こんにちは@HL_G FATloadは実際にはファームウェアをアドレス0x90000000にロードします。0x90100000など、他のアドレスを試すこともできます。また、変数$loadaddrの実際の値も確認してください。 よろしくお願いします、 志明
查看全文
SJA1110 Target Power Failure from JTAG Debugger I got target power failure from my JTAG debugger.  The power rails are all good.  Can anyone help me narrow down which power rails (VDDIO_DEBUG, etc) should I focus?  Also can this failure also by caused by certain control IOs, like RST_N or RST_CORE_N, etc?  Thanks.  
查看全文
在 Linux 中,如何确定 s32r45 中的 SPT 是否以 600M 的速度运行? 在 Linux 中,如何确定 s32r45 中的 SPT 是否在 600M 下运行?谢谢。 cat /sys/kernel/debug/clk/spt_spt/clk_rate 使用上述方法,输出结果为 0,即未能成功验证 SPT 工作频率。 Re: In Linux, how to determine if the SPT in s32r45 is operating at 600M? 我想知道 SPT 是否已达到 600MHz 的最高频率,以确定 SPT 是否已达到最大计算能力。 Re: In Linux, how to determine if the SPT in s32r45 is operating at 600M? 如何检查 Linux 源代码中的 DIV0 配置? Re: In Linux, how to determine if the SPT in s32r45 is operating at 600M? 我知道 FXOSC 的 40MHz 频率乘以 ACCELPLL 的 60 倍频率可以得到 2.4GHz,但我不确定 Linux 源代码中的 DIV0 配置。您能帮忙再检查一遍吗? Re: In Linux, how to determine if the SPT in s32r45 is operating at 600M? 你好 只需参考参考手册:第 24.1.2.7 章 MC_CGM_2 时钟概述和 24.7.3.4SPT 时钟生成。 这些数字显示了 SPT 的时钟源,即 ACCEL_3_CLK。 检查 MC_CGM_2 模块,查看 AUX 0 的时钟源是否设置为: ACCEL_PLL_PHI0_CLK 或 FIRC_CLK 以及时钟分频器 DIV0 是如何设置的。 这将告诉你 SPT 时钟运行的确切频率。 由于参考手册不是公开的,我不会在这里发布任何屏幕截图。 顺祝商祺! Peter Re: In Linux, how to determine if the SPT in s32r45 is operating at 600M? 你好 我不知道如何在 Linux 代码中做到这一点,因为我以前从未做过。 但 SPT 时钟初始化后,只需从调试器中读取 DIV0 的寄存器即可。 MC_CGM_2 基地址:440C_0000h 时钟复用器 0 分频器 0 控制寄存器 (MUX_0_DC_0) 地址:440c_0308H 例如,您也可以在源代码中进行搜索: 导航至 S32R45 时钟驱动程序 drivers/nxp/s32/clk/s32r45_clk.c 搜索 MC_CGM_2 AUX0 DIV0 定义& 寄存器写入内容 顺祝商祺! Peter
查看全文