Hello, developers!
Now i make a project " portable weather station" based on MPL3115. Primary functions: display current time, e-kompass, pressure, altitude, temperature and weather forecast. its a batterry-operated devices, and components must have minimal Supply Current. when I found a MPL3115 i been really excited, because this IC have all what i need. But now my project is has stalled.
Firstly, i wrote a source code as datasheet recomendations, for set and change mode of MPL3115, read registers and display the results. i test code and sensor at LPC-812 MBED board (because i like LPCXpresso) and sensor board is powered from LPC-812 (3.3 Volt). and I got the some results (pressure, temperature and altitude).
Next, i reading a AN3914 ("Modern Altimeter and Barometer System using the MPL115A") and start to adaptation this algorithm for MPL3115.
for make a weather forecast i need to get pressure change per 1 hour. for this, i chose a 3-hours/180 minutes interval for collected samples in FIFO every ~20 minutes. User should be able get a weather forecast at any time, so program must compare oldest and newest samples (for example, now is 11-10 AM, oldest sample was obtained at 8-00 AM, newest samples at 11-00 AM. i compare this samples, divided and get a pressure change per 1 hour. then i make a weatern pattern and display it. next samples update will be at 11-20 AM. )
but i get a first STOP: bytes, reading from FIFO, "deleted from the front of the FIFO buffer" (page24 DS). so if I read values from the buffer, I lost them. and if i make a weather pattern as in the above example at 11-10AM, at 11-20 AM i can't get the data from FIFO. next possibility for 1 hour pressure change i will get only via 1 hour! all the collected data (from 8-20 AM to 11-20 AM) will be LOST!
So. this way is not work.:smileyshocked:
Ok, AN3914 have another faster way to make a weather forecast (page 6)! all i need - it's a pressure and current altutude (MPL3115 must give all of this). i must calculate "ideal pressure" Pweather (for good sunny day) for current altitude by using the equation: Pweather = (101.3 * exp(((float)(CurrentAltitude))/(-7900))). and compare current pressure with "ideal".
i wrote a code: set Altimeter mode and get a current altitude, set Barometer mode and get a current pressure, calculate and display result of weather pattern. i live in area at 56—178 meters of sea level. i start the test and get a second STOP :
sensor's PCB is on the table at room temperature (22-24 C) and does not move. source code don't change. in the morning i have altitude=102 meters, in the dinner =32 meters, in the evening 0 meters. i turn on Debugger and see: when I read data registers in Altimeter mode, OUT_P_MSB Register= 0xFF, so i get incorrect data from sensor . But i get correct temperature data in this reading operation (i make a cycle read 5 bytes from sensor at one procedure).
So,this way does not inspire confidence...![]()
I just have to find a shaman! Because I can not find understanding with this really fine sensor.
May be anybody help me?
Best regards, Ellis
Hi Ellis,
We have some code examples and other documentation available in Freescale communities, perhaps it can be useful: https://community.freescale.com/community/sensors/content?filterID=contentstatus%5Bpublished%5D~obje...
Regards,
Jose