NXP S32K118Q048 EVB LIN Stack Hi, I’m working with an NXP S32K118 EVB and trying to load a new LDF file into my LIN configuration. The stack worked fine with previous LDFs, but with the new file, I get terminal errors stating some nodes are missing configurable frames under Node Attributes. I also get a delay time too short error. The same LDF works fine in CANoe without issues. I have attached an example of error that I see in the terminal. Issue: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes. Level: Error Type: Tool problem Tool: Peripherals Origin: Peripherals Resource: Sources Information: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes. I want to know what could be possibly causing these and how to fix them. Is it an issue in Design studio, an inherent limitation in the NXP LIN stack or a problem in the file? Bear in mind, that the LIN stack is comptible with the RTD since I got one of the LIN stack examples working. Any help would be appreciated. regards, Re: NXP S32K118Q048 EVB LIN Stack Hi @yousefdessouki123,
Can you share the LDF?
Which revision of the S32k1xx LIN Stack do you use?
Thank you,
BR, Daniel
查看全文