2137593_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2137593_en-US

2137593_en-US

NXP S32K118Q048 EVB LIN Stack

Hi,

I’m working with an NXP S32K118 EVB and trying to load a new LDF file into my LIN configuration. The stack worked fine with previous LDFs, but with the new file, I get terminal errors stating some nodes are missing configurable frames under Node Attributes. I also get a delay time too short error.

The same LDF works fine in CANoe without issues.

I have attached an example of error that I see in the terminal.

Issue: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes.
Level: Error
Type: Tool problem
Tool: Peripherals
Origin: Peripherals
Resource: Sources
Information: %error Error: xxxxx.ldf line: 111 "NodeName" Frame sporadic_frame_name- Missing frame in LDF Configurable frames in Node Attributes.

 I want to know what could be possibly causing these and how to fix them. Is it an issue in Design studio, an inherent limitation in the NXP LIN stack or  a problem in the file? Bear in mind, that the LIN stack is comptible with the RTD since I got one of the LIN stack examples working.

Any help would be appreciated.

regards,

Re: NXP S32K118Q048 EVB LIN Stack

Hi @yousefdessouki123,

Can you share the LDF?

Which revision of the S32k1xx LIN Stack do you use?


Thank you,

BR, Daniel

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 08:26 AM
更新人: