Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
CAN based WakeUp Transrecevier TJA1465 Hi  I am using TJA1465 CAN SIC transceiver with partial networking for CAN Based Wake up i have configure this with 500kbs bitrate and ID 0x18ff21b1 for CAN wake up using partial networking using SPI. But transreceiver wake ups for other bitrate also which is not configured in the Partial networking data rate and filter configuration register (address 031h). why does transreciever wake up for bitrate also other than configured.  below is the sample code   static void tja1465_configure_can_wakeup_ext_dlc0(void) { uint8_t mode_stat,sys_stat; printf("CAN Wakeup Config Enter \n" ); tja1465_read(REG_MODE_STATUS, &mode_stat); printf("Mode Status (0x070) = 0x%02X (%s)\n",mode_stat, mode_str(mode_stat)); tja1465_write(0x031, 0x14); /* WUF ID = 0x18FF21B1 *//*0x18FF0180* MASK 0x0000304D*/ tja1465_write(0x020, 0xB1); tja1465_write(0x021, 0x21); tja1465_write(0x022, 0xFF); tja1465_write(0x023, 0x18); /* WUF ID mask (match full 29-bit ID) */ tja1465_write(0x024, 0x00); tja1465_write(0x025, 0x00); tja1465_write(0x026, 0x00); tja1465_write(0x027, 0x00); tja1465_write(0x028, 0x05); tja1465_write(0x029, 0x00); tja1465_write(0x02A, 0x00); tja1465_write(0x02B, 0x00); tja1465_write(0x02C, 0x00); tja1465_write(0x02D, 0x00); tja1465_write(0x02E, 0x00); tja1465_write(0x02F, 0x00); tja1465_write(0x030, 0xC8); tja1465_write(0x011, 0x00); tja1465_write( 0x060, 0xFF); tja1465_write( 0x061, 0xFF); tja1465_write( 0x062, 0x04); tja1465_write(0x032, 0x03); uint8_t pn_status_reg; tja1465_read(0x073, &pn_status_reg); tja1465_read(0x071, &sys_stat); printf("PN Status (0x073) = 0x%02X (CPNS: %s),CPNERRS :0x%02X\n", pn_status_reg, (pn_status_reg & 0x20) ? "OK" : "Error",(pn_status_reg & 0x40)); printf("System Status(0x071) = 0x%02X\n", sys_stat); tja1465_write(REG_MODE_CTRL, MODE_SLEEP); usleep(3000); tja1465_read(REG_MODE_STATUS, &mode_stat); printf("Mode Status (0x070) = 0x%02X (%s)\n", mode_stat, mode_str(mode_stat)); tja1465_read(REG_SYS_STATUS, &sys_stat); printf("System Status(0x071) = 0x%02X\n", sys_stat); printf("CAN Wakeup Config Exit \n" ); } Re: CAN based WakeUp Transrecevier TJA1465 Hello Vivekananda Good day! I'm going to run tests to find the error and I'll get back to you as soon as I have an answer. Have a great day and best of luck. Re: CAN based WakeUp Transrecevier TJA1465 Hello Vivekananda Can you clarify what they mean with below green sentence on ‘other bitrates’, is this about CAN FD frames? But transreceiver wake ups for other bitrate also which is not configured in the Partial networking data rate and filter configuration register (address 031h). If it’s indeed CAN FD frames, then after the wake-up please check if PNFDER =1. If so, try changing below yellow line to: tja1465_write(0x032, 0x07). This will set PNECC = 1 and CAN FD frames would not increase the error counter anymore, PNFDER should stay 0 and the device does not wake up. The Application Notes (AN14388, which can be downloaded on our page) are showing an example SPI sequence for a PN configuration for your reference (section 4.2, pages 23-24). Please take a look. I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck.
View full article
[RTD600 IP] S32K3X4EVB-T172 GPIOウェイクアップ このサンプル プロジェクトでは、WKPU + SIUL2 (GPIO) の基本機能を使用および構成する方法をユーザーに示します。 ------------------------------------------------------------------------------ * テストハードウェア: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS v3.5 および S32DS v3.6.x * SDKリリース: RTD 6.0.0 * デバッガ: PE Micro * ターゲット: internal_FLASH ------------------------------------------------------------------------------ このサンプル ルーチンは、GPIO 割り込みウェイクアップ用に WKPU ユニットを構成します。これは最も単純な WKPU の例です。ピン PTB19 (WKPU42) はウェイクアップ用に構成されています。 ルーチンはSW5が押されるのを待機し、緑色の LED をオフにして、次の処理を実行する Wkpu_EnterStandby() 関数に入ります。 コアクロックを FIRC に切り替えます。 WKPU インスタンスを初期化します。 WKPU42 (PTB19) を設定します。 スタンバイ(または高速スタンバイ)状態になります。 SW6を押すと、MCU が起動してリセットし、 SW5が再度押されるかどうかをポーリングします。 この例は現状のまま提供されており、保証やサポートはありません。
View full article
S32K3 FLEXIO数据异常 我在使用S32K314 RTD400的SAI0(主机)与FLEXIO模拟的I2S(从机)通讯,SAI只使用d0,MUX_DISABLE,word width为16,发现从机接收到的数据都是主机的数据循环左移一位得到的数据,比如发送0x8002,在代码里面从机得到的数据是0x5,改了很多配置都没用,最后勾选了下图中的Enable User Mode Support,数据就正常了,这是为什么 SAI配置如下 Re: S32K3 FLEXIO数据异常 Hi@Jason22 我查看了编译的结果,这个选项你勾不勾选完全不影响运行的结果。 按照你提供的工程,我勾选和不勾选Enable User Mode Support所编译生成的结果是完全一样的,这说明这不会导致你所说的问题。 Re: S32K3 FLEXIO数据异常 编译没问题,是出现没有”Mcal.h“文件嘛,如果是的话,清除工程,再次编译就没问题了(不知道这是不是IDE版本的问题,S32DS 3.6似乎没出现过这个错误)。如果不是这个错误,方便说一下编译时出现了什么问题嘛 Re: S32K3 FLEXIO数据异常 Hi@Jason22 抱歉,我看错了,这不是IDE版本的原因,是我将Enable User Mode Support看成了Enable Flexio Common Support 你能再次检查下你提供的工程吗,我无法编译成功。 Re: S32K3 FLEXIO数据异常 没有勾选"启用用户模式支持",配置还是有效的 不勾选"Enable Flexio Common Support",配置才无效,我使用的是 S32DS 3.5.14,这和 S32DS 版本有关嘛 Re: S32K3 FLEXIO数据异常 嗨@Jason22 你不勾选 "启用用户模式支持"下面的配置不是不生效了嘛 Re: S32K3 FLEXIO数据异常 我也比对了,发现也是一样,重新运行了一下程序,发现勾选后,又出现了数据循环左移的情况,但我第一次勾选的时候,数据确实是正常了,重复跑了几次也正常,不知道是什么因素导致的。 那我想询问一下,是我的配置还是代码有问题嘛,为什么从机接收到的数据刚好是主机发送的数据循环左移的结果?谢谢 主机发送的数据 从机收到的数据 Re: S32K3 FLEXIO数据异常 Hi@Jason22 逻辑分析仪自己去测一下你发出的数据是不是正确的
View full article
i.MXRT1064 カスタム ボードをデバッグできません。 こんにちは、 デバッグ モードでコードを実行しようとすると、「アドレス "0x20d102" でブレークしましたが、デバッグ情報が利用できません」というメッセージが表示されます。 私は i.MXRT1064 カスタム ボードを使用し、LinkServer LPC-Link2 を使用してプログラミングしています。 このボードは以前は問題なく動作していましたが、突然このメッセージが表示されます。 リリースモードを試してみました。リリース コードを使用してボードを正常にフラッシュすることはできますが、その後プログラムが実行されないようです。シリアル端末からもディスプレイからも出力が表示されません。 また、Secure Provisioning Tool を使用してこのボードをプログラミングしようとしましたが、まだ動作しません。 この問題に関して、どこに焦点を当てるべきか、または何か手がかりとなるものについて、どなたか助言をいただけませんか? Re: Unable to debug i.MXRT1064 custom board. こんにちは、MayLiuさん。 ご返信ありがとうございます。 以前、ご提案いただいた設定を試しましたが、デバッグしようとすると IDEs でエラー (MI コマンドの実行に失敗しました: -target-download) が表示されました。参考までに、そのエラーのスナップショットを添付しました。 前のメッセージに戻って、現在のプログラムが実行されているアドレスをチェックしたところ、コードが ROM 領域 (アドレス 0x20E35A) にあることが示されていたことを付け加えておきます。SO、何らかの理由で、コードはアプリケーション コードに到達/起動できず、ROM 内で停止します。私の仮定は正しいでしょうか?そんなシナリオがあり得るのでしょうか? Re: Unable to debug i.MXRT1064 custom board. こんにちは@nxpsachveさん、 弊社の製品にご興味をお持ちいただき、またコミュニティをご利用いただき誠にありがとうございます。 1: 「アプリケーションを RAM にリンク」を選択して再度デバッグしてみてください。 アプリケーションが RAM から正常に実行できる場合は、ボードをシリアル ダウンローダー モードに設定し、セキュア プロビジョニング ツールを使用して UART1 または USB1 でボードをプログラムしてください。   アプリケーションの実行に失敗した場合は、オシロスコープを使用してボードの電源投入シーケンスを確認することをお勧めします。   お役に立てれば幸いです。 よろしくお願いいたします。 メイリュー Re: Unable to debug i.MXRT1064 custom board. こんにちは@nxpsachveさん、 MCUXpresso IDE は BOOT 構成を変更するとは思いません。NXP RT 上のブート動作は、ハードウェア ブート構成とブート モード ピンによって決まります。 シリアル ダウンローダー モードでターゲットを検出できるため、ROM がまだ正常に実行されていることがわかります。次のステップとして、次のことが考えられます。 チップ全体の消去を実行します。 ボードを内部ブートモードに切り替え、 デバッグのためにMCUXpresso IDEに再接続してみてください。 あるいは、MCUXpresso Secure Provisioning Tool を使用してアプリケーション イメージをプログラムすることもできます。 よろしくお願いいたします。 メイリュー Re: Unable to debug i.MXRT1064 custom board. こんにちは@nxpsachveさん、 最新情報をありがとうございます。 提供された情報に基づくと、CPU は現在、アプリケーション コードではなく、Boot ROM からのコードを実行している可能性があります。   BOOT CFG と BOOT モード ピンの設定をチェックして、デバイスがユーザー フラッシュから起動するように構成されていることを確認することをお勧めします。   ボードをシリアル ダウンローダー モードに設定し、J-Link 経由で接続して、デバッガーがターゲットを検出して通信できるかどうかを確認することもできます。   よろしくお願いいたします。 マトリウ Re: Unable to debug i.MXRT1064 custom board. こんにちは、MayLiuさん。 ご提案ありがとうございます。 MCUXpresso 内に、BOOT Conf を変更したり影響を与えたりするような設定や構成があるかどうかを確認したいのですが。IDE を除外するためです。 リンク サーバーは、シリアル ダウンロード モードのときにターゲットを検出できます。
View full article
PN7160とnRF52840 こんにちは、 カスタムPCB上のnRF52840モジュール(Raytac MDBT50Q-1MV2)にI2C経由でコネクテッドされた外付けNFCリーダ/コントローラ(NXP PN7160A1HN/C100E)を使用しています。(プログラミングは、nRF52840 DKをデバッグプローブとして使用し、SWD経由で行います。) 現在のソフトウェア環境は、VS Code(Windows 11)のnRF Connect SDK(NCS)v3.2.0とZephyr RTOS v4.2.99です。目標は、PN7160(NCI-over-I2C)を使用して、RF検出を開始し、13.56MHzパッシブカードのUIDを読み取ることです。 私はPN7160を「典型的なZephyrの方法」で統合しようと試みました。 ソース/メイン.c ボード/nrf52840dk_nrf52840.オーバーレイ prj.conf I2C ピンと PN7160 GPIO (VEN/IRQ) を設定できますが、初期化が失敗します (プローブ中または最初のコマンド中の I2C -EIO/NACK)。その結果、RF 検出全体が機能せず、統合アプローチが正しいかどうかわかりません。 質問: NCS/Zephyrでは、`main.c`を変更するだけでPN7160をプログラムすることは可能ですか?+ `nrf52840dk_nrf52840.overlay` + `prj.conf`、それともPN7160には適切なカスタムドライバが必要であると予想されますか? ドライバが必要な場合、NCS でドライバを追加するための推奨アプローチは何ですか (デバイスツリー バインディング YAML + Kconfig + CMake + ドライバ ソース)。また、外部 Zephyr モジュール (zephyr/module.yml + EXTRA_ZEPHYR_MODULES) としてパッケージ化する必要がありますか?これを行う方法のサンプル コードはありますか (パブリック github リポジトリのようなものですが、見つけることができませんでした)? プローブ/最初の書き込み時に -EIO を引き起こす可能性のある、別の方法で処理する必要がある既知の NCS v3.2.0 / Zephyr 4.2.99 I2C/TWIM 動作はありますか? 他に役立つコメントがありましたら、ぜひ教えてください。 ご協力ありがとうございます!
View full article
S32K388 と MC33771B SPI BMS: MBDT、コード生成、AI 展開 NXPコミュニティの皆様、こんにちは。 実際のリチウムイオン電池パックをターゲットに、SPI通信を介してS32K388-Q289とFRDM-MC33771B-SPI-EVBを使用した統合BMSを開発しています。調査を進めるうちに、S32K3 シリーズに使用できる BMS 固有のサンプル プロジェクトとリファレンス実装が比較的少ないことに気付きました。そのため、このタイプのアプリケーションに推奨されるワークフローとサポートされているツールチェーンを確認するのは困難でした。 私の目標は、以下の内容を含む完全な組み込み BMS スタックを MCU に実装することです。 セル電圧/温度モニタリング(BCC経由) セルバランス制御 SOC / SOH推定アルゴリズム(ディープラーニングベースのアプローチを含む) MCU上でのリアルタイム操作 可能な場合はモデルベース デザインのワークフロー (そうでない場合は S32DS C プロジェクト) 最初に MATLAB/Simulink Model-Based Design Toolbox (MBDT) を使用する予定ですが、セットアップで完全なサポートが利用できない場合は、S32 Design Studio (S32DS) に進みます。 以下の質問についてご指導いただければ幸いです。 1) S32K3 BMSアプリケーション用のMBDTサポートおよびトレーニング・マテリアル BMS関連の開発(SPIベースのBCC通信、サンプリング/プロセッシング、保護ロジック、リアルタイム監視など)に特化したS32K3シリーズでMBDTを使用するための公式ドキュメント、ユーザーガイド、トレーニングコース、またはアプリケーションノートはありますか? 2) MBDTモデルとディープラーニングモデルの統合とコード生成 Simulink (MBDT) で BMS ロジックを開発し、Deep Learning Toolbox を使用して構築された SOC/SOH モデルを追加すると、次のようになります。 - これらを 1 つの統合 Simulink モデルに組み合わせることはできますか? - はいの場合、Embedded Coder を使用して統合モデルを C コード (またはその他のサポートされている組み込みコード) に自動的に生成し、S32K388 に展開できますか? 3) S32K388におけるリアルタイム推論の実現可能性 (2)のコード生成が実行可能であれば: - 展開されたモデルは、MCU 上のライブ バッテリー データ (電圧/電流/温度) を使用してリアルタイム推論 (SOC/SOH 推定) を実行できますか? - S32K388 には、推奨される制約やベスト プラクティス (固定小数点と浮動小数点、サポートされるレイヤーの種類、モデル サイズの制限、推論のタイミングに関する考慮事項など) はありますか? 4) MBDTにおけるセーフティ制約/保護ロジック セーフティのために、次のような保護ロジックを実装する必要があります。 - 過電圧/低電圧しきい値 - 過熱/低温しきい値 - 障害処理と安全状態の動作 これらの制限と保護ロジックを MBDT/Simulink に直接実装し、生成された組み込みコードに含めることは可能ですか? S32K ターゲットの参考例(BMS またはセーフティロジック)があれば、共有してください。 5) S32K388とFRDM-MC33771B-SPI-EVBおよび代替品との互換性 S32K388-Q289 は、BMS アプリケーション用に SPI 経由で MC33771B と連携するために正式にサポート/推奨されていますか? この組み合わせが推奨されない場合は、S32K3 ベースの BMS 開発用に公式にサポートされている BCC + リファレンス プラットフォーム (SPI または TPL) を提案していただけますか? 6) デバイス上でのトレーニング(オンライン学習)と推論のみのワークフロー 組み込み AI の観点から: - オンデバイス トレーニング (リアルタイムのバッテリー データを使用したオンライン学習) は S32K3 MCU でサポートまたは推奨されていますか? - または、PC でのオフライン トレーニング + MCU での推論のみというアプローチが推奨されますか? オフライントレーニングが推奨される場合、推奨されるワークフローを説明する公式リファレンスはありますか? 7) S32K388におけるAI推論のパフォーマンス/メモリガイダンス S32K3 (特に S32K388) 上で AI 推論を実行するためのベンチマークやガイドラインはありますか? - フラッシュ/RAM使用量の予想 - 典型的な推論レイテンシの範囲 - 最適化アプローチ(固定小数点、量子化、軽量アーキテクチャ) 😎 MBDT + DL 統合が推奨されない場合の推奨代替ワークフロー 完全な統合と自動コード生成が推奨/サポートされていない場合、S32K3 に AI モデルを展開するための推奨ワークフローは何ですか?例えば: - モデルを軽量なC推論コードに手動で変換する - CMSIS-NNのようなアプローチを使用する(該当する場合) - NXPミドルウェア/推奨ライブラリ/サンプル(例:eIQ)の使用 サポートありがとうございます。ドキュメントのリンク、トレーニング リファレンス、SDKs の例、ベスト プラクティスの推奨事項などがあれば、非常に役立ちます。 よろしくお願いいたします。 Re: S32K388 with MC33771B SPI BMS: MBDT, code generation, and AI deployment こんにちは@SonHyunTaek 、 プロジェクトに関する詳細な質問をコミュニティ フォーラムに投稿していただきありがとうございます。以下の回答は MBDT ソフトウェアの観点から提供されていることに注意してください。ハードウェアの観点からは、コンポーネントの組み合わせに関してより良いアプローチがある可能性があります。また、BMS の目標電圧とパック電流検知が必要かどうかを知っておくことも役立ちます。SPI 経由でコネクテッドされた単一の AFE を使用する予定なので、最大 48V の BMS システムをターゲットにしているものと想定します。 ご提案いただいたデバイスの組み合わせに関してですが、ハードウェア レベルでは、S32K3 は MC33771B と完全に互換性があります。しかし、ソフトウェアの観点から見ると、状況はより複雑になります。S32K3 用の MBDT は、MCAL レイヤーの NXP リアルタイム・ドライバ (RTD) 上にコードを生成するように構築されていますが、BMS 用の MBDT は、RTD と互換性のある BMS SDK 上にコードを生成します。BMS SDK には、Simulink からアクセスできるピン、クロック、ペリフェラルの外部構成ツールと、すぐに実行できるサンプルが含まれています。 ご注意ください: - MBDT for BMS 1.2.0 は、S32K388 をサポートしていない MBDT for S32K3 1.4.0 でのみ動作します。 - BMS SDKはRTD 3.0.0とのみ互換性があります。S32K3 1.4.0 の MBDT によって使用されます。当時、S32K388 は入手できませんでした。 - BMS 用 MBDT および S32K3 用 MBDT は、バッテリー ジャンクション ボックス機能を備えたハードウェアデザインで通常使用される MC33774、MC33775、MC33664、MC33665、MC33772C などの新しい AFE 部品のみをサポートします。 これらの制限はソフトウェア パッケージ (RTD および BMS SDK) に起因します。使用する予定の MC33771B には C SDK ドライバーが含まれていますが、S32K3 と MC33771B を接続するためのすぐに実行可能な互換性のある C ドライバーがないため、カスタム コードを使用して手動で MBDT に統合する必要があります。つまり、組み込み SW: MC33771B/MC33772B 用のバッテリー・セルコントローラ ソフトウェア ドライバでは、手動の C コーディングと MBDT への統合が必要です。これを実行する方法 (S32K1 用の MBDT に基づく) を説明した記事は、こちらにあります。 以下であなたの質問に答え、最後にいくつかの解決策を提案します。 1. MBDTのサポートとトレーニング 私たちが提供する最高のリソースは、 MBDT コミュニティページで入手できます。右側には、S32K3 用の MBDT を使用して基本的なタスクを実行する方法を説明した、モデルベース デザイン ツールボックスの初心者向けガイドがあります。さらに、バッテリー・マネジメントシステムについての洞察を提供する BMS ウェビナーもあります。 MathWorks と共同で作成した BMS に関する最新のウェビナーへのリンクは次のとおりです。 NXP S32 デバイス向けバッテリー システム開発の合理化。 2. ディープラーニングモデルの統合 MathWorks とのこれまでのコラボレーションでは、ディープラーニング ベースの充電状態 (SOC) 推定アルゴリズムを Simulink から直接展開し、PIL モードでテストすることに成功しました。はい、Embedded Coder は Simulink モデルから直接ニューラル ネットワークを生成でき、MBDT と組み合わせて S32K3 に展開できます。 関連するウェビナーへのリンクは次のとおりです。 NXP S32K3マイクロコントローラへのディープラーニングベースのSOC推定アルゴリズムの導入 3. S32K388におけるリアルタイム推論の実現可能性 はい、リアルタイム推論は実現可能です。以前の研究では、セル電圧、電流、温度を入力として使用しました。これらの値は実行時に AFE によって測定され、ニューラル ネットワークに提供されます。ベストプラクティスとして、PIL モードでの集中的なテストはパフォーマンスの評価に役立ちます。最適化手法を試して、最適な構成を特定することもできます。 4. セーフティ上の制約 セーフティ要件のロジックを Simulink に実装し、対応するコードを自動的に生成できます。MathWorks は、S32K3 で使用および展開した例を提供しています。 リチウムイオンバッテリー・マネジメントアルゴリズムの設計とテスト 5. S32K388とFRDM-MC33771B-SPI-EVBの互換性および代替品 Simulink からニューラル ネットワーク アプリケーションを直接テストするには、最新バージョンの S32K3 用 MBDT を使用します。これにより、展開の実現可能性を確認し、現時点で利用可能なすべての MCU に対してベンチマーク テストを実行できます。 ハードウェアの観点からは、いくつかのオプションがあります。 a. 提案されたソリューション(S32K358 + MC33771C)を続行する MC33771B ではなく、より新しく、SPI をサポートし、電流測定機能を備えている MC33771C から始めてください。カスタム コードを使用して MC33771C ドライバを Simulink に直接統合し、BMS 1.8.0 用の MBDT を使用できます。 b. サポートされているMCUを使用してSimulinkでBMS用のMBDTを使用する たとえば、セル監視用の MC33774/MC33775 と電流測定用の MC33772C を搭載した S32K358 (すべて SPI 経由)。このセットアップは、MBDT for BMS および MBDT for S32K3 1.4.0 で動作します。ただし、最初にニューラル ネットワークが S32K358 で実行されることをテストします。 c. AFE部品を搭載したS32K3または最新のBMA7318を使用する 注意: このCASE、BMS 用の MBDT を使用して Simulink からコードを展開することは直接サポートされていません。Simulink でアプリケーション ロジックとニューラル ネットワーク C コードを生成し、S32 Design Studio を使用して AFE と手動で統合することもできます。 6. デバイス上でのトレーニングと推論のみのワークフロー これはアプリケーションの要件によって異なります。これまでのアプローチは推論のみで、MATLAB でネットワークをトレーニングし、それを MCU に展開していました。推奨リソース: ディープラーニングを使用したバッテリー状態の推定。続いて、上記のポイント 2 で説明したウェビナーが開催されます。 7. S32K388におけるAI推論のパフォーマンスとメモリに関するガイダンス パフォーマンスはアプリケーションによって異なります。ニューラル ネットワークがすでにトレーニングされている場合は、生成されたコードを S32K3 ファミリの PIL モードでテストし、実行をプロファイルして、S32K388 がニーズを満たしているかどうかを判断します。参考までに、前述の SOC アルゴリズムは、S32K344 および S32K358 で正常にテストされました。 要約すると、Embedded Coder を使用すると、ニューラル ネットワークからコードを生成し、PIL モードでパフォーマンスをテストできます。検証後、生成されたコードを S32 Design Studio にインポートし、必要に応じて S32K388 に展開します。 お役に立てば幸いです。 マリウス
View full article
S32N55: sequence ID in gPTP bridge device when acting as a GM Hi team, I was testing the bridge device behavior in the gPTP example. I use the GrayVIP_1_0_22_0. According to the User Manual, if the bridge does not receive any Sync messages after StartupTimeoutS, it should start operating as a GM. However, I observed that in this situation, the Sequence ID in both Sync and Sync Follow-Up frames remains at 1024 and does not increase. After checking the related code, I found that when the bridge transitions to GM mode, the Sequence ID used for generating Sync messages is taken from the prSyncMachines[prDomain->u8SlaveMachineId].u16SequenceId of the slave port. If the slave port has not received any Sync messages, this value is never updated, which causes the Sequence ID in the Sync messages sent by the master port to remain unchanged. This behavior suggests that the bridge cannot function properly as a GM under this mechanism. Could you please help explain why the bridge is designed to behave this way? BR, Bridget GPTP_STACK Re: S32N55: sequence ID in gPTP bridge device when acting as a GM Hello @Bridget,  The team has picked up a case and will provide an answer as soon as possible  Best regards, Radu Re: S32N55: sequence ID in gPTP bridge device when acting as a GM Hi @Bridget, We are working to reproduce the issue and will discuss further steps in the team. I will get back to you. Thanks, Lukas Re: S32N55: sequence ID in gPTP bridge device when acting as a GM @Bridget, As it turns out, this behavior of the gPTP Bridge is intended, and in line with the 802.1as standard. The Bridge is supposed to relay Sequence ID received on master port. If the Grand Master is lost, the Sequence ID indeed stops being updated - this is one of the ways that downstream devices are able to tell when GM is lost. For a Bridge that never had a GM in the first place, the Sequence ID is random per standard. Our interpretation of random is that nothing about the Sequence ID is guaranteed, or should be assumed. A hardcoded 1024 is considered compliant to that (could be any other number). Is the Sequence ID causing issues in your application? As you have surely observed, Endpoints are perfectly capable of synchronizing to the Bridge, regardless of Sequence ID. Apologies for taking so long. Please do let me know if anything is unclear. BR, Lukas
View full article
MPC5748G devkit 的 HSM 启用问题 我在使用恩智浦 MPC5748G devkit [SPC5748GHMKU6] HSM 模块 时遇到了问题,保密协议 [网络安全参考手册 - HSM 网络安全固件标准代码包 - HSM 网络安全固件基本软件包] 全部可用。 问题是我设法通过 DCF 记录启用了 HSM,我验证它已通过 SSCM_UOPS_HSE = 1 启用, 但是对于 HADR(HSM 起始地址),SSCM_HSA_HADR = 0x00000000 这意味着没有 HSM 启动标头可用。 因此,我怀疑我的目标上是否闪存了 HSM 固件。 问 1: 如何验证我的 devkit 是否有可用的 HSM 固件? 问题 2:如果我已经有了 HSM 固件,我应该在以下 HSM 代码/数据块中看到什么? 问题 3: 如果我的目标上没有闪存固件,我该如何获取固件? 特别是我已经有 100 多件了 问题 4:如果有固件可用,在哪里可以找到 HSM 的启动地址? 我使用带有 PE micro 插件的 S32ds 集成开发环境进行闪存和调试,并使用 PKGPPC NEXUS STARTER 应用程序加载我的 DCF 记录 [UTest Algorithm]。 #MPC5748G #HSM Re: HSM Enabling Issue for MPC5748G devkit 你好@Yousry 请注意,带有 HSM 固件的设备仅提供给经批准的客户(批量非常大)。标准设备 SPC5748G... 未安装 HSM 固件。带有 HSE 固件的设备具有特殊的部件号。 如果你还没有与恩智浦的销售部门达成协议来购买此类设备,那么获得这些设备的机会就很小了。 强烈建议选择带有 HSE(硬件安全引擎)的设备。所有用户均可免费使用 HSE 固件。建议将 S32K3 系列设备作为 MPC5748G 的替代品: https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-general-purpose-mcus/s32k3-microcontrollers-for-automotive-general-purpose:S32K3 此致, Lukas Re: HSM Enabling Issue for MPC5748G devkit 你好@lukaszadrapa 我们已经订购了SPC5748GHMKU6 参考手册 " 订单信息 " 部分提到了这个,因为它已经有 HSM 了 那么你能指导我通过回答我之前问过的问题来弄清楚吗? 预先感谢 , Yousry   Re: HSM Enabling Issue for MPC5748G devkit 我不得不同意数据表令人困惑的说法。我过去曾要求澄清这一点,但一直没有得到更新。因此,虽然有 HSM 模块,但没有 HSM 固件。我上面的回答仍然有效。 此致, Lukas
View full article
チップ関連のリソースとドキュメントをダウンロードする方法 例: S32K3xx_interrupt_map.xlsx Re: 如何下载芯片的相关资源的文档 こんにちは@PQF データシートとガイダンスマニュアルは公式ウェブサイトからダウンロードできます。これらの資料はガイダンスマニュアルの添付ファイルに含まれています。 https://www.nxp.com/products/S32K3
View full article
Programming S08 MCUs via Background Debug Mode (BDM) To program an S08 microcontroller using an external debugger, you’ll need to use the single-wire Background Debug Mode (BDM). This interface relies on the on-chip Background Debug Controller (BDC) module. BDM Connector The connector used for BDM is typically a 6-pin header. You can refer to the evaluation kits below for examples of how to wire and configure it: S08PB16 and S08PLS Evaluation Kit | NXP Semiconductors S08P-Lite Evaluation Board | NXP Semiconductors Setting Up in CodeWarrior 11.1 Once the physical connection to the MCU is established: Create a new bareboard project in CodeWarrior. Select the target MCU. Choose the connection interface during project setup.   To upload your code: Go to Debug → Debug As → CodeWarrior. If multiple connection options are available, a window will prompt you to select the one configured during project creation. Additional Resources For more details on how to use Background Debug Mode, the following document can be helpful on how to use the Background Debug Mode. AN3335, Introduction to S08 Background Debug Mode - Application Notes
View full article
IMX415 相机移植 imx8mplus 您好, 我正在将索尼 IMX415 摄像头传感器移植到恩智浦 i.MX8M Plus (IMX8MP) 平台上。 在移植过程中,一些参考提到了通过 ISP 调整工具生成 XML 文件。 我的问题是 我真的需要生成 XML 文件才能让 IMX415 在 IMX8M Plus 上运行吗? 这些 XML 文件是否必须用于基本的传感器调试(通过 V4L2 / ISI 进行流式传输)? IMX8MPLUS Re: IMX415 camera porting imx8mplus 这是一个好问题。 仍然需要 xml 配置/校准文件,请参见此处: -AN13712: 800 万像素 ISP OS08A20 传感器 -AN13713: 800 万像素 ISP 新相机移植 我不知道为什么恩智浦最近删除了这个文件。 Re: IMX415 camera porting imx8mplus 我认为您需要 xml 文件。您可以先使用分辨率相同的设备,然后再进行微调。 另见: https://community.nxp.com/t5/i-MX-Processors/IMX8M-Plus-ISP/m-p/2220156/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufE1JN0JJTUJFRVZXMTA2fDIyMjAxNTZ8U1VCU0NSSVBUSU9OU3xoSw#M242307 Re: IMX415 camera porting imx8mplus 你好, ,关于 XML 文件,我还有一个疑问。 目前,我有用于相机传感器 OS08A20 的 XML 文件,能否将相同的 XML 文件用于 imx415 传感器? Re: IMX415 camera porting imx8mplus 感谢您的回复,但您说从最近的 isp-imx 项目中删除 xml 文件是什么意思?在移植新相机传感器时是否不再需要它们? Re: IMX415 camera porting imx8mplus 他们删除了近期 isp-imx 项目中的 xml 文件,但您可以从早期项目中获取这些文件: ,将 xx 替换为以前的版本: isp-imx-4.2.2.xx.0.bin 例如检查: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/isp-imx-4.2.2.18.0.bin https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/isp-imx-4.2.2.20.0.bin 等... Re: IMX415 camera porting imx8mplus 如何获取 XML 文件?如果你有任何想法,请告诉我。对于 OS08A20,我看到一个文件名为"Sensor0_Entry_os08a20.cfg" 的文件,文件中包含: name="os08a20" drv ="os08a20.drv" mode= 0 [mode.0] xml ="OS08a20_8M_10_1080p_linear.xml" dwe ="dewarp_config/sensor_dwe_bypass_1080P_config.json" [模式.1] xml ="OS08a20_8M_10_1080p_hdr.xml" dwe ="dewarp_config/sensor_dwe_bypass_1080P_config.json" [模式.2] xml ="OS08a20_8M_10_4k_linear.xml" dwe ="dewarp_config/sensor_dwe_bypass_4K_config.json" [模式.3] xml ="OS08a20_8M_10_4k_hdr.xml" dwe ="dewarp_config/sensor_dwe_bypass_4K_config.json 我的疑问是,这些 json 文件有必要吗? Re: IMX415 camera porting imx8mplus PS:还需要相应的 json 文件,因为无论如何都需要配置广角鱼眼畸变校正模块,即使你将其设置为绕过也是如此。
View full article
mke06128vqh4のuart0 こんにちは、友人の皆さん。私は MKE06Z128VQH4 マイクロコントローラを使用して設計したボードを持っており、その中でいくつかの出力と入力を使用しています。私は KBI 入力を 1 つ、タイマーを 3 つ、カウンターを 1 つ使用しています。SO、問題はありません。すでに設定を行っており、動作しています。 現在、UART0 シリアル ポートに取り組んでおり、USB-TTL シリアル アダプターを PC に接続してデータを受信または送信しています。SDKs ライブラリを使用して情報を送受信することができませんでした。MCUXpresso を使用した私の構成は画像のとおりです。 ピン: 時計には外部水晶12MHZがあります。 FLL にエラーがあるため、FEE オプションをCANません。FBELP を使用して設定を行っています。 UART0 では、割り込み受信および送信ポーリングを使用して構成を行っています。 インストールされている SDK は次のとおりです。 サンプルの SDK があります: これらの例を使用しても、UART0 を動作させることができません。何らかのガイダンスが必要です。UART0 を動作させるために数日間試行しています。 Re: uart0 in mke06128vqh4 こんにちは@Iotelctronic デモ版は変更せずにそのままご利用ください。 私の側でテストしましたが、問題は見つかりませんでした BR アリス Re: uart0 in mke06128vqh4 こんにちは、アリス!ポーリングを使用してデモでテストしましたが、機能しません。 codigo main.c: #include "pin_mux.h" #include "board.h" #include "fsl_uart.h" /******************************************************************************* * Definitions ******************************************************************************/ /* UART instance and clock */ #define DEMO_UART UART1 #define DEMO_UART_CLK_FREQ CLOCK_GetFreq(kCLOCK_BusClk) /******************************************************************************* * Prototypes ******************************************************************************/ /******************************************************************************* * Variables ******************************************************************************/ uint8_t txbuff[] = "Uart polling example\r\nBoard will send back received characters\r\n"; uint8_t rxbuff[20] = {0}; /******************************************************************************* * Code ******************************************************************************/ /*! * @brief Main function */ int main(void) { uint8_t ch; uart_config_t config; BOARD_InitBootPins(); BOARD_InitBootClocks(); config.baudRate_Bps = 115200U; config.parityMode = kUART_ParityDisabled; config.stopBitCount = kUART_OneStopBit; //config.txFifoWatermark = 0; //config.rxFifoWatermark = 1; config.enableTx = false; config.enableRx = false; // UART_GetDefaultConfig(&config); // config.baudRate_Bps = BOARD_DEBUG_UART_BAUDRATE; // config.enableTx = true; //config.enableRx = true; UART_Init(DEMO_UART, &config, DEMO_UART_CLK_FREQ); UART_WriteBlocking(DEMO_UART, txbuff, sizeof(txbuff) - 1); while (1) { UART_ReadBlocking(DEMO_UART, &ch, 1); UART_WriteBlocking(DEMO_UART, &ch, 1); } } Re: uart0 in mke06128vqh4 こんにちは@Iotelctronic 1) クロックに関しては、12 MHz 水晶が正常に機能しているかどうかを確認し、構成を確認してください。 2) KE06 は DMA をサポートしていません。 よろしくお願いします。 BR アリス Re: uart0 in mke06128vqh4 こんにちは。問題を見つけました。レジスターを使用していた SDK の例やその他のプロジェクトは機能せず、常に間違ったデータと間違った文字が送信されました。私は外部の 12 MHz 水晶を使用していますが、その水晶では正確に 115200 のボー レートを生成できません。ただし、 12 MHz 水晶をはんだ付けせずに構成を 8 MHz に変更すると、正常に動作します。私の大きな疑問は、構成を 8 MHz に変更しても 12 MHz の水晶を変更しないとなぜ機能するのかということです。私が示しているコードは.freqで行った変更です= 8000000U。これについて説明はありますか?また、MKE06Z128VQH4 マイクロコントローラには UART で使用するための DMA があるかどうかもお聞きしたいです。 /*********************************************************************************************************************** * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file * will be overwritten if the respective MCUXpresso Config Tools is used to update this file. **********************************************************************************************************************/ /* * How to setup clock using clock driver functions: * * 1. call CLOCK_SetSimSafeDivs() to set the system clock dividers in SIM to safe value. * * 2. If external oscillator is used Call CLOCK_SetXtal0Freq() to set XTAL0 frequency based on board settings and * call CLOCK_InitOsc0() to init the OSC. * * 3. Call CLOCK_BootToXxxMode()/CLOCK_SetXxxMode() to set ICS run at the target mode. * * 4. If ICSIRCLK is needed, call CLOCK_SetInternalRefClkConfig() to enable the clock. * * 5. call CLOCK_SetSimConfig() to configure the divider in sim. */ /* clang-format off */ /* TEXT BELOW IS USED AS SETTING FOR TOOLS ************************************* !!GlobalInfo product: Clocks v7.0 processor: MKE06Z128xxx4 package_id: MKE06Z128VLK4 mcu_data: ksdk2_0 processor_version: 9.0.0 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/ /* clang-format on */ #include "clock_config.h" /******************************************************************************* * Definitions ******************************************************************************/ /******************************************************************************* * Variables ******************************************************************************/ /* System clock frequency. */ extern uint32_t SystemCoreClock; /******************************************************************************* ************************ BOARD_InitBootClocks function ************************ ******************************************************************************/ void BOARD_InitBootClocks(void) { BOARD_BootClockRUN(); } /******************************************************************************* ********************** Configuration BOARD_BootClockRUN *********************** ******************************************************************************/ /* clang-format off */ /* TEXT BELOW IS USED AS SETTING FOR TOOLS ************************************* !!Configuration name: BOARD_BootClockRUN called_from_default_init: true outputs: - {id: Bus_clock.outFreq, value: 20 MHz} - {id: Core_clock.outFreq, value: 40 MHz} - {id: Flash_clock.outFreq, value: 20 MHz} - {id: ICSFF_clock.outFreq, value: 31.25 kHz} - {id: ICSIR_clock.outFreq, value: 37.5 kHz} - {id: LPO_clock.outFreq, value: 1 kHz} - {id: OSCER_clock.outFreq, value: 8 MHz} - {id: Plat_clock.outFreq, value: 40 MHz} - {id: System_clock.outFreq, value: 40 MHz} - {id: Timer_clock.outFreq, value: 20 MHz} settings: - {id: ICSMode, value: FEE} - {id: ICS.BDIV.scale, value: '1', locked: true} - {id: ICS.IREFS.sel, value: ICS.RDIV} - {id: ICS.RDIV.scale, value: '256'} - {id: ICS_C1_IRCLKEN_CFG, value: Enabled} - {id: OSC_CR_OSCEN_CFG, value: Enabled} - {id: OSC_CR_OSC_MODE_CFG, value: ModeOscLowPower} - {id: OSC_CR_RANGE_CFG, value: High} - {id: OSC_CR_RANGE_RDIV_CFG, value: High} - {id: SIM.DIV2.scale, value: '2'} - {id: SIM.DIV3.scale, value: '2', locked: true} sources: - {id: OSC.OSC.outFreq, value: 8 MHz, enabled: true} * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/ /* clang-format on */ /******************************************************************************* * Variables for BOARD_BootClockRUN configuration ******************************************************************************/ const ics_config_t icsConfig_BOARD_BootClockRUN = { .icsMode = kICS_ModeFEE, /* FEE - FLL Engaged External */ .irClkEnableMode = kICS_IrclkEnable, /* ICSIRCLK enabled, ICSIRCLK disabled in STOP mode */ .bDiv = 0x0U, /* Bus clock divider: divided by 1 */ .rDiv = 0x3U, /* FLL external reference clock divider: divided by 256 */ }; const sim_clock_config_t simConfig_BOARD_BootClockRUN = { .outDiv1 = 0x0U, /* DIV1 clock divider: divided by 1 */ .outDiv2 = 0x1U, /* DIV2 clock divider: divided by 2 */ .outDiv3 = 0x1U, /* DIV3 clock divider: divided by 2 */ .busClkPrescaler = 0x0U, /* bus clock optional prescaler */ }; const osc_config_t oscConfig_BOARD_BootClockRUN = { .freq = 8000000U, /* Oscillator frequency: 12000000Hz */ .workMode = kOSC_ModeOscLowPower, /* Oscillator low power */ .enableMode = kOSC_Enable, /* Enable external reference clock, disable external reference clock in STOP mode */ }; /******************************************************************************* * Code for BOARD_BootClockRUN configuration ******************************************************************************/ void BOARD_BootClockRUN(void) { /* Set the system clock dividers in SIM to safe value. */ CLOCK_SetSimSafeDivs(); /* Initializes OSC0 according to board configuration. */ CLOCK_InitOsc0(&oscConfig_BOARD_BootClockRUN); CLOCK_SetXtal0Freq(oscConfig_BOARD_BootClockRUN.freq); /* Set ICS to FEE mode. */ CLOCK_BootToFeeMode(icsConfig_BOARD_BootClockRUN.bDiv, icsConfig_BOARD_BootClockRUN.rDiv); /* Configure the Internal Reference clock (ICSIRCLK). */ CLOCK_SetInternalRefClkConfig(icsConfig_BOARD_BootClockRUN.irClkEnableMode); /* Set the clock configuration in SIM module. */ CLOCK_SetSimConfig(&simConfig_BOARD_BootClockRUN); /* Set SystemCoreClock variable. */ SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK; } Re: uart0 in mke06128vqh4 ありがとう、クロックの問題は水晶のはんだが12MHZではなく8MHZであることです
View full article
CAN MCX Nx4x FlexSPI ポートA とポートB を異なるデバイスで同時に使用できますか。 こんにちは、NXPさん FlexSPI を使用してハードウェアを接続し、両方のデバイスを同時にCAN使用できますか? ポートA->NORフラッシュ ポートB->PSRAM また、参考になる構成例はありますか? どうもありがとうございます MCX N Re: Can we use MCX Nx4x FlexSPI portA and portB with different device at the same time. こんにちは、ハリー。 Spark の説明によると、device_config と clk ソースをチェックする必要がありますか? 私は見た typedef 構造体 _flexspi_config { ...... #定義されている場合(FSL_FEATURE_FLEXSPI_SUPPORT_SEPERATE_RXCLKSRC_PORTB) && FSL_FEATURE_FLEXSPI_SUPPORT_SEPERATE_RXCLKSRC_PORTB flexspi_read_sample_clock_t rxSampleClockPortB; /*!< フラッシュ読み取り用のサンプルクロックsource_bの選択。*/ #endif 1.portA と PortB を使用する場合、別々の rxclksource を使用する必要がありますか? 2. FLEXSPI_SetFlashConfig() に渡される &deviceconfig をチェックする必要がありますか? Re: Can we use MCX Nx4x FlexSPI portA and portB with different device at the same time. こんにちは、ハリー。 サンプル コードでは、PortA の NOR フラッシュ ID にアクセスする方法のみが提供されており、MCX-N5XX-EVK にコネクテッドされた PSRAM を使用して PortB にアクセスするためのコードを追加しようとしています。参考までに実験結果を以下に示します。 FlexSPI 設定: ポートA->NORフラッシュ ポートB->PSRAM テストCASE1:成功 初期PortAおよびPortAフラッシュIDの読み取り(1バイト) テストCASE2: 成功 ポートBの初期値とポートBのフラッシュIDの読み取り(1バイト) テストCASE3: 失敗 最初にポートAとポートBの両方が、アドレスを使用してポートAとポートBのフラッシュID(1バイト)を個別に読み取ります。 以下に参考用のコードスニペットを示します。PortA と PortB の状況で間違いがあったか、さらに設定が必要かどうかを確認してください。 ポートAとポートBの両方のフラッシュデバイスを初期化するためのflexspi_nor_flash_initのコード変更 ポートBデバイスを読み取るためにflashXfer.deviceAddressにオフセットを追加します。 参考までに、変更されたファイルとプロジェクト全体のアーカイブを以下に示します。 Re: Can we use MCX Nx4x FlexSPI portA and portB with different device at the same time. こんにちは SDKs サンプルを参照していますが、同時に 2 つのデバイスではなく 1 つのフラッシュ デバイスにコネクテッドされています。 2 つのデバイスを同時に動作させるには、設定が足りないのではないかと思います。 参考になるサンプル構成はありますか? または、レジスタ レベルから正しい構成を実行したことをどのように確認すればよいでしょうか? よろしくお願いします。 Re: Can we use MCX Nx4x FlexSPI portA and portB with different device at the same time. こんにちは@greatshow_chen はい、NXP MCX Nx4x では、FlexSPI ポート A とポート B の両方を同時に使用して、2 つの異なるメモリ デバイスに接続CAN。 ポートA->NORフラッシュ ポートB->PSRAM 次の点を確認する必要があります。 NOR フラッシュと PSRAM は競合するピンを共有していません。 flexspi_octal_polling_transferをCAN参照します。 BR ハリー Re: Can we use MCX Nx4x FlexSPI portA and portB with different device at the same time. こんにちは、 FlexSPI を搭載した多くの NXP マイクロコントローラ (i.MX RT シリーズなど) には、2 つの独立した FlexSPI チャネル (ポート A とポート B) があります。各ポートは、異なるタイプのメモリ デバイスと通信するように構成CAN。これにより、NOR フラッシュを 1 つのポートに接続し、PSRAM を別のポートに接続できるようになります。
View full article
在Qt widget中使用glimagesink插件播放视频时软件崩溃 NXP工程师你好! 我们的开发板是i.mx8mp,内核5.10.9,Qt5,Yocto3.2.0。 开发软件的功能主要是视频播放和控制,需要将视频嵌入显示在widget里面,并且可以改变widget的大小,目前软件在ubuntu上开发是没有问题的,并且也能够正常运行,但是利用i.mx8mp的Qt交叉编译环境编译并运行到i.mx8mp上时,软件会崩溃,并报出Segmentation fault错误,经过问题定位,就是Glimagesink这个插件出现的问题,如果换成waylandsink,软件不会崩溃,但是视频会显示到widget之外 图1 Ubuntu显示效果,是正常想要的效果 图2 i.mx8mp崩溃log 图3 将glimagesink换成waylandsink后i.mx8mp显示效果 非常期待您能回复,如果提供例程或者问题调查方向,不胜感激 我们的源码放在附件中 feiyu Re: 在Qt widget中使用glimagesink插件播放视频时软件崩溃 Hi,@ Zhiming_Liu 非常感谢您的回复,目前问题已经解决,简单说就是wayland中,无法直接将waylandsink(或者glimagesink)插件绑定到Qt widget上,需要进行转换,我们最后的demo放到附件中,请参考 int main(int argc, char *argv[]) { gst_init(&argc, &argv); QApplication app(argc, argv); app.connect(&app, SIGNAL(lastWindowClosed()), &app, SLOT(quit())); qDebug() << "qt platform name: " << QGuiApplication::platformName(); // prepare the pipeline GstElement *pipeline = gst_parse_launch("videotestsrc ! waylandsink", NULL); // prepare the ui PlayerWindow *window = new PlayerWindow(pipeline); window->resize(640, 480); window->show(); GstElement *vsink = gst_element_factory_make("waylandsink", "wsink"); g_object_set(GST_OBJECT(pipeline), "video-sink", vsink, NULL); // connect to interesting signals GstBus *bus = gst_element_get_bus(pipeline); gst_bus_add_watch(bus, &PlayerWindow::postGstMessage, window); gst_bus_set_sync_handler(bus, bus_sync_handler, window, NULL); gst_object_unref(bus); // run the pipeline GstStateChangeReturn sret = gst_element_set_state(pipeline, GST_STATE_PLAYING); if (sret == GST_STATE_CHANGE_FAILURE) { gst_element_set_state(pipeline, GST_STATE_NULL); gst_object_unref(pipeline); // Exit application QTimer::singleShot(0, QApplication::activeWindow(), SLOT(quit())); } int ret = app.exec(); window->hide(); delete window; gst_element_set_state(pipeline, GST_STATE_NULL); gst_object_unref(pipeline); return ret; } Re: 在Qt widget中使用glimagesink插件播放视频时软件崩溃 Hi 能否再提供一下编译生成的二进制文件以及测试方法,我这边编译toolchain需要一点时间,我先在demo image上面试一下。 Best Regards Zhiming Re: 在Qt widget中使用glimagesink插件播放视频时软件崩溃 你好 感谢答复,才发现忘了上传附件,现在追加 feiyu Re: 在Qt widget中使用glimagesink插件播放视频时软件崩溃 Hi 请上传一下测试源码 Best Regards Zhiming
View full article
S32G VNP RDB2 Rev.E 上的 LLCE CAN 传输问题 尊敬的恩智浦社区成员: 当我尝试通过 S32G2 LLCE 模块的 BCAN0 发送 CAN 帧时,我遇到了一个问题。我正在使用演示板 S32G-VNP-RDB2 Rev.E。 我已经通过模拟器看到,当我弹出 BLROUT FIFO 以获取 Tx 传输表的索引时,一切都运行良好,之后我将消息填充到共享内存中,然后通过 BLRIN FIFO 发回索引。 问题是 CAN 总线上没有任何反应。因此,弹出索引 15 后,BLROUT 返回 0xFFFFFFFF。 为了启用 BCAN,我们需要设置什么配置吗? 仅供参考,固件对我发送的命令响应良好,并且我已正确配置 SIUL2 来配置 LLCE_CAN_0 的 Tx 和 Rx 引脚。 我们还观察到,当我们驱动 LLCE_CAN0_TXD 信号时,BCAN0(U17)的收发器并没有改变 LLCECAN0H 和 LLCECAN0L 的逻辑电平。我们还检查了信号LLCE_CAN01_EN处于高逻辑电平。 感谢您的支持。 顺祝商祺! 回复:@Re: S32G VNP RDB2 Rev.E 上的 LLCE CAN 传输问题 是的,我错了,我实际上有2个节点,第二个是CAN日志工具。 此致,
View full article
MIMXRT1021 内部 RTC 振荡器的特性 我正在使用看门狗,我发现它的源时钟是 RTC 时钟。 我没有使用晶体或外部 RTC 时钟源,因此只能依靠内部环形振荡器。 对环形振荡器特性的规定不一致: 在《硬件用户指南》中,它被指定为"...片上 40 kHz 振荡器。公差为 ±50%" (表 4) 在技术数据表的第 4.1.4 节中也有类似的规格说明但是在第 4.2.4.2 节中它说 " 这个方块的频率范围约为 10—45 kHz。" 选择看门狗超时时间有时是一种微妙的平衡行动,必须容许源时钟容差 +/-50%。 我的问题是 1.实际名义振荡频率是多少?如果不是 32 千赫,为什么不是? 2.如果标称频率不是 32kHz,那不就意味着看门狗超时已经出错了吗? 3.它随温度有何变化?热的时候是加速还是减速? 4.+/-50% 是否包括温度变化? 谢谢! 亚历克斯 i.MX RT102x Re: MIMXRT1021 characteristics of internal RTC oscillator 你好@alex_conway,很抱歉这么晚才回复你。 很抱歉造成您的困惑。我想说的是,我之前与你们分享的数据确实是用于生产的: 32kHz +/- 50% -40C 至 105C。 BR Habib Re: MIMXRT1021 characteristics of internal RTC oscillator 嗨,哈比卜 数据表中的所有信息均经过生产测试。 哪个数据表中包含哪些信息?请您回到我的原帖: "在《硬件用户指南》中,它被指定为"...片上 40 kHz 振荡器。公差为 ±50%" (表 4) 在技术数据表的第 4.1.4 节中也有类似的规格说明但是在第 4.2.4.2 节中它说 " 这个方块的频率范围约为 10—45 kHz。" 其中没有任何一项注明在 -40C 至 105C 温度范围内的频率为 32kHz +/- 50% ,也没有任何一项在表格中列出,而这是制造商通常会遵守的规格。 谢谢! 亚历克斯 Re: MIMXRT1021 characteristics of internal RTC oscillator 你好,@alex_conway、 所以,为了明确起见,您是说 +/-50% 包括所有可能的变化,包括初始值和从 -40C 到 105C 的温度? 是。初始值和温度都包含在这个百分比中 是否在生产中进行了测试?- 即所有芯片是否都经过 -40C 至 105C 的测试,以确保振荡器频率在 +/-50% 或 32kHz 范围内? 数据表中的所有信息均经过生产测试。 BR Habib Re: MIMXRT1021 characteristics of internal RTC oscillator Hiabib, 所以,为了清楚起见,您是说 +/-50% 包括所有可能的变化,包括初始值和从 -40C 到 105C 的温度? 是否在生产中进行了测试?- 即所有芯片是否都经过 -40C 至 105C 的测试,以确保振荡器频率在 +/-50% 或 32kHz 范围内? 谢谢 Alex Re: MIMXRT1021 characteristics of internal RTC oscillator 您好@alex_conway, 正在回答您的问题: 既然您声明标称频率为 32kHz,那么无论振荡器运行在什么频率下,看门狗超时时间是否都以标称的 32.786kHz 为参考? WDOG 的时钟频率来自振荡器。如果振荡器的工作频率低于 32 kHz,这一偏差将直接影响 WDOG 的定时。 因此,内部振荡器有助于加快启动速度并提供防篡改保护,但不应成为 32 kHz 时钟的唯一来源。 +/-50% 中有多少是初始值公差,多少是温度变化? 正如我在上一篇文章中提到的,温度导致的频率偏差受多种因素影响,可能无法预测。不过,在 -40°C 至 105°C 的工作温度范围内,变化将保持在 ±50% 之内。 BR 哈比卜 Re: MIMXRT1021 characteristics of internal RTC oscillator 嗨,哈比卜 感谢您的回答,我有几个后续问题: 既然您声明标称频率为 32kHz,那么无论振荡器运行在什么频率下,看门狗超时时间是否都以标称的 32.786kHz 为参考? +/ -50% 中有多少是初始值容差,有多少是温度变化? 谢谢! 亚历克斯 Re: MIMXRT1021 characteristics of internal RTC oscillator 你好,@alex_conway、 对不起,我的回复晚了。回答您的问题 1.实际名义振荡频率是多少?如果不是 32 千赫,为什么不是? 标称频率为 32 kHz,但根据工艺变化和温度条件,其变化幅度可达 ±50% 。 2.如果标称频率不是 32kHz,那不就意味着看门狗超时已经出错了吗? 您能否提供更多细节,说明您目前是如何测试 WDOG 超时的? 3.它是如何随温度变化的? 温度导致的频率偏差受多种因素影响,可能无法预测。不过,在 -40°C 至 105°C 的工作温度范围内,变化将保持在 ±50% 之内。 4.+/-50% 是否包括温度变化? 是的,±50% 公差考虑了温度变化以及工艺变化。 BR Habib Re: MIMXRT1021 characteristics of internal RTC oscillator 你好 Habib, 我没用 RT1020-EVK,我的板没有 RTC 时钟或水晶。RTC_XTALI 引脚连接至接地,RTC_XTALO 引脚开路。 谢谢 Alex Re: MIMXRT1021 characteristics of internal RTC oscillator 你好,@alex_conway、 我在内部询问,以便获得更多有关标称值和温度对该振荡器影响的信息。感谢您的耐心等待。 与此同时,我还有一个问题:能否请您详细介绍一下目前是如何测试 WDOG 超时的?如果您使用 RT1020-EVK,请注意它包含一个 32kHz 的外部振荡器,这意味着它不依赖于内部振荡器: BR Habib
View full article
当前的 FSS 版本"S32N_FSS_FW_R21-11_1.8.1" 是否支持 S32N53? 你好,团队、 客户 HKMC 将从 S32N55 移至 S32N53。 所以我的问题是 当前的 FSS 版本"S32N_FSS_FW_R21-11_1.8.1" 是否支持 S32N53? 如果不是,什么时候会版本支持 S32N53 的 FSS? 顺祝商祺! 谢谢您! HSE_FW 优先级:高 Re: Does current FSS version "S32N_FSS_FW_R21-11_1.8.1" support S32N53? 你好,谭生、 我们计划在本月(7月底)发布的版本中提供支持; 谢谢! 辛杜
View full article
MIPI-CSI-2 とベイヤーパターンカメラ (RAW10) を使用した i.MX93 こんにちは、 カスタムの i.MX93 ベースのボードを持っています。提供されている CSI-2 インターフェースを使用して、ベイヤーパターン カメラ (IMX327) で RAW10 データを転送したいと考えています。 デバイスツリーの設定とプレスリリース、製品ニュース-ctlの設定はSO far正しいのですが、パイプラインを開始するとdwc-mipi-csi2からIRQストームが発生し、「 IPIインターフェース致命的イベント情報」カウンタが増加します。INT_ST_IPI_FATALレジスタの値は0x2aで、IPI FIFOオーバーフローを示しています。IPIがIRQを1つも持っていないため、ISIにデータをプッシュしていないのではないかと考えています。 https://community.nxp.com/t5/i-MX-Processors/About-settings-to-operate-ov5640camera-on-i-MX93EVK/mp/1716885/highlight/true#M212016を参照何らかの特別な設定があるようです。これらの値をRAW10に適合させようとしましたが、CAMERA_MUX[DATA_TYPE]の値0x31(ユーザー定義16)について疑問がありました。CSI-2 データ型 RAW10 の場合、これが 0x2b ではなくユーザー定義であるのはなぜですか? IPI エラーの原因は何でしょうか?この問題をさらにデバッグするにはどうすればよいでしょうか? 感謝と敬意を表します。 アレクサンダー Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) アップデートはありますか?Omnivision 9732でも同じ問題が発生しています Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは@brian14さん、 i.MX93 と RAW10/12 Bayer データを出力するカメラ センサでも同じ問題が発生しています。 何かアイデアや提案はありますか? よろしくお願いします。 Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは、 連絡あった?もう1ヶ月が経ちました。 ありがとう、アレクサンダー Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは、 このトピックに関して何かニュースはありますか? ありがとう、そしてよろしく。 アレクサンダー Re: i.MX93 using MIPI-CSI-2 with a Bayer Pattern camera (RAW10) こんにちは@steinaさん、 NXP サポートにお問い合わせいただきありがとうございます。 このCASEについては社内チームで検討し、できるだけ早くお問い合わせいたします。 すてきな一日を!
View full article
S32K144: Integration of FlexCAN inside lin_master_s32k144 (S32DS.ARM2.2) Good morning: Currently using the S32K144EVB board to prepare a system demo, where we must manage 1 classical CAN-HS network (500k) and 3 LINs. (19200, multiple slaves in each LIN)  k144EVB board will behave as LIN master for the 3 LINs, that's why as starting point I've selected the LIN_master_S32K144 example. LINStACK is working fine and now I've started to check the integration of the CAN communication into the project. Reviewing S32K144 documentation and examples, i see that the K144 has 2 different ways to manage the CAN communication... either via FIFO or either via MBs... Unclear the benefits of one over the other...  for a system where i must receive 4-5 CAN messages, process some of the content data and transmit periodically 1 or 2 CAN messages: 1) which configuration is easier/better to use, considering that my LIN master will operate at full capacity?FIFO or MB? 2) do we expect any registers/clock/interrupts conflicts between NXP linstack and the FlexCAN integration? 3) is there any example available already with such an integration (LIN-MASTER + CAN-HS)? Re: S32K144: Integration of FlexCAN inside lin_master_s32k144 (S32DS.ARM2.2) Hi@rricart There's no relationship between LIN and CAN; they are two independent peripheral modules. For the S32K1 FlexCAN, the CAN FIFO does not support CAN FD, so you need to consider whether need to support CAN FD or not. If your project doesn't require CAN FD feature, either the MB or the FIFO will fine. You can refer to the demo provided in this link, which categorizes the different ways to use FlexCan and provides a simple test demo. https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753
View full article
S32G3:热关机 嗨,团队 硬件:基于 S32G3。 读取 1 区温度(A-core)时。当温度达到 "64 摄氏度 "时,硬件将重新启动。 下面是 Linux 系统的信息。连续读取三个区域的温度值,问题发生时的值如下。 64350(0 区) 64350(1 区) 62850(2 区) kernel[435]:[ 7919.187233] thermalthermal_zone1: a53_cores:达到临界温度,正在关闭 内核[435]:[ 7919.187252] 重新启动:硬件保护关闭(温度过高) 在 Linux DTS 中配置的警戒温度为 80 度,临界温度为 100 度,尽管我们配置了 100 度,但在 64 度时仍可观察到重启。 Re: S32G3: Thermal Shutdown 你好,@yellapu_anishkh 感谢您的回复。 自 BSP39 以来,有几个与 TMU 相关的问题,其中一些已在 BSP40 中修复,而另一些已在以后的版本中修复,如果可能的话,我建议在 BSP42 上对其进行测试 BR 切宁 Re: S32G3: Thermal Shutdown 您好, 我看到了该驱动程序的一个提交 (c5697686c8d19ff1edbce015fa5562ba2a2065e6)。评论中提到了它,但 Jira ID (ALB-10663) 并不匹配。请您确认一次。 Re: S32G3: Thermal Shutdown 你好,@yellapu_anishkh 感谢您的回复。 我检查了源代码,建议尽可能在 BSP42(或更新版本)下对您的情况进行测试,因为从这个版本开始应用了一些错误修复,从现有信息来看,您提到的错误也得到了修复。 BR 切宁 Re: S32G3: Thermal Shutdown 您好, 在 BSP39 上可以观察到这种情况,BSP39 版本说明中提到了以下问题。 我查看了从 BSP39 到 BSP44 的版本说明,发现当前的错误尚未修复。能否请您确认一下,是否已经修复? Re: S32G3: Thermal Shutdown 你好,@yellapu_anishkh 谢谢您的帖子。 我知道你可以在基于 S32G3 的定制板上对其进行测试,对吗?我能知道你在使用哪个版本的电路板支持包吗?一旦确认,我会首先检查内核代码。 BR 切宁
View full article