Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Textarea bug issue I created several Textarea components. When I used the keyboard to input in one of them and then clicked "Finish", the keyboard would automatically switch to another Textarea for further operations. How to solve this problem? The video is placed at https://github.com/monkeyhorse/guiguider.git Re: Textarea bug issue Hi @monkeyhorse, Thanks for the clarification. I see this issue seems to occur during simulation. Does it only occur when simulating? Or also when running the GUI on a board? Re: Textarea bug issue @EdwinHz Yes, I use the latest version. Re: Textarea bug issue Hi @monkeyhorse, Thanks for the update. What version of GUI Guider/LVGL are you using? Are they the latest (GUI Guider 1.9.1 with LVGL 9.2.1)? Re: Textarea bug issue Now I have discovered that the creation sequence of the Textarea in setup_scr_screen.c is the cause of this problem, but I still don't know how to solve it.
View full article
Target applications of CoolFlux DSP in S32K39-37-36 Company: DAEJIN SEMICONDUCTORS Contact Name: Heedong Lee Device: S32K39-37-36 Hi team, As far as customer and I understand, S32K39-37-36 were designed for safe EV control applications:     - Motor control (3- or 6-phase motor, Si IGBT/SiC/GaN transistors)     - Power conversion (DCDC, OBC)     - Battery management system (BMS) control     - Vehicle control unit (VCU) or domain control Particularly, CoolFlux DSP is built to implement FIR filtering capability for motor resolver application (in S32K39-36), postprocessing raw data from the SDADCs and provide the final samples according to the configured sampling rate. However, customer wants to know what other roles the CoolFlux DSP can play in the following applications:      - Power conversion (DCDC, OBC)      - Battery management system (BMS) control      - Vehicle control unit (VCU) or domain control Also, if SDADC is not used in the application, what other operations could CoolFlux DSP perform? Thank you in advance for your help. Have a nice day! Best Regards, Leonardo COOLFLUX Priority: HIGH Re: Target applications of CoolFlux DSP in S32K39-37-36 "CF" means CoolFlux, Petr Re: Target applications of CoolFlux DSP in S32K39-37-36 Thanks for your feedback. What does "CF" means in the acronym "CFSDADC" please? Re: Target applications of CoolFlux DSP in S32K39-37-36 Hello, as mention in the thread the main (and only) use case of the CoolFlux DSP is the motor control application. No other use case support was requested during the development phase. In case of other/new use cases an analysis would need to be performed to find out if the FW as is can support any other use case. Or there would be some changes required or different version of th e FW with different functionality would be needed. Regarding the second question. Instead of the SDADC input stream the CFSDADC FW can work with DMA-WRITE buffer and clock threshold scheduling mode. I am not sure if RTD driver has support for this at this point though. In general the CFSDADC FW supports following processing of input data (Either SDADC of DMA-WRITE buffer). Up-samping, FIR filtering, Decimation, Adjustment (gain or offset), IIR filtering. Best regards. Jindřich.
View full article
S32DS3.6.1 安装 S32K5 RTD0.4.4 P02 嗨,团队、 根据 S32k5 RTD0.4.4 P02 版本说明,模块配置为 S32DS 3.6.1。 在 S32DS 3.6.1 上安装 S32k5 RTD0.4.4 P02 时会产生以下错误。   您能指导我如何安装吗? 谢谢您! BR、 双 RTD S32DS Re: S32DS3.6.1 install S32K5 RTD0.4.4 P02 您好, 感谢您的支持。 是的,在安装 S32K5 RTD 之前我已经安装了 S32K5 代码包。问题就如弗洛林之前所说,当我移除 S32DesignStudio 时,K5 RTD P02 可以正确安装。 BR、 双 Re: S32DS3.6.1 install S32K5 RTD0.4.4 P02 嗨,弗罗林 感谢您的支持。 是的,你的变通方法在我的电脑上可行。屏幕不是客户的,是我的 S32DS 的屏幕。我已经确认它没有被截断。以下屏幕是我的 S32DS 软件网站。(安装 K5 RTD 后,我已读取 S32DesignStudio 网站)。 我连接的是公司网络,不知道网速如何。 BR、 双 Re: S32DS3.6.1 install S32K5 RTD0.4.4 P02 您好, 我认为客户的屏幕截图被截断了。如果缺少依赖项,则无法继续安装。全屏截图应该是这样的 从错误信息来看,似乎是网络问题,平台更新没有正确下载。我在内部进行了验证,结果没有任何问题。 作为一种变通方法,由于您并不真正需要 3.6.2升级时,可以进入扩展和更新 -> 管理网站 -> 找到一行: S32DesignStudio -https://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.6 并单击删除,然后重试。 安装后,你可以通过手动添加或单击 "恢复默认设置 "将其还原,这将删除你添加的任何自定义更新站点,并恢复初始默认站点。 这不是一种解决方案,而是一种变通办法。理想情况下,我们需要更多有关您的连接和网速的信息,以便确定这是否会影响流量。 另外,请注意,我们有 S32Design Studio 3.6.2 版本。安装程序向后兼容所有 3.6.x以前的版本。 亲切的问候, Florin Re: S32DS3.6.1 install S32K5 RTD0.4.4 P02 嗨,双、 在安装 S32K5 RTD 之前,请确保安装 S32K5 软件包。如果您的账户中没有 K5 代码包,您可以将其添加到 are.nxp.com 目录中。
View full article
iMX8MPlus + 88W8987 + PDn pin I am trying to reboot the 8987 module in android 10 using the PDn pin on the iMX8MPlus     # unload modules $ rmmod -f moal $ rmmod -f mlan     [  987.206583] wlan: Unloading MWLAN driver [  987.211780] wlan: Driver unloaded     #unbind MMC controller $ echo "30b50000.mmc" > /sys/bus/platform/drivers/sdhci-esdhc-imx/unbind   [  988.124586] mmc1: card 0001 removed   # set PDn to LOW   $ echo "30b50000.mmc" > /sys/bus/platform/drivers/sdhci-esdhc-imx/bind   [  998.119429] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA       # set PDn to HIGH   [ 1010.224255] mmc1: new ultra high speed SDR104 SDIO card at address 0001     # Load modules $ insmod /vendor/lib/modules/mlan.ko $ insmod /vendor/lib/modules/moal.ko mod_para=wifi_mod_para.conf       [ 1027.098443] wlan: Loading MWLAN driver [ 1027.103256] wlan: Register to Bus Driver... [ 1027.120295] vendor=0x02DF device=0x9149 class=0 function=1 [ 1027.126578] Attach moal handle ops, card interface type: 0x105 [ 1027.133282] SD8987: init module param from usr cfg [ 1027.138829] card_type: SD8987, config block: 0 [ 1027.143989] cfg80211_wext=0xf [ 1027.147669] sta_name=wlan [ 1027.151001] uap_name=wlan [ 1027.154341] wfd_name=p2p [ 1027.157589] max_vir_bss=1 [ 1027.160926] cal_data_cfg=none [ 1027.164611] ps_mode = 2 [ 1027.167844] auto_ds = 2 [ 1027.171028] host_mlme=enable [ 1027.174629] fw_name=sdiouart8987_combo_v0.bin [ 1027.179833] SDIO: max_segs=128 max_seg_size=65472 [ 1027.185353] rx_work=1 cpu_num=4 [ 1027.189296] Attach mlan adapter operations.card_type is 0x105. [ 1027.204869] wlan: Enable TX SG mode [ 1027.209100] wlan: Enable RX SG mode [ 1027.216328] Request firmware: sdiouart8987_combo_v0.bin [ 1028.066187] Wlan: FW download over, firmwarelen=603832 downloaded 603832 [ 1030.080214] Fail to poll firmware status: firmwarestat=0xf005 [ 1030.086693] FW failed to be active in time! [ 1030.091600] wlan_dnld_fw fail ret=0xffffffff [ 1030.096656] WLAN: Fail download FW with nowwait: 0 [ 1030.102459] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 00 02 03 00 [ 1030.109401] SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 00 00 [ 1030.116157] SDIO Func1: (0x8) 00 (0x58) 00 (0x5c) 0d (0x5d) 00 (0x60) 01 (0x61) 00 (0x62) 00 (0x64) 10 (0x65) 01 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00 [ 1030.130949] SDIO Func1 (0xe8-0xf2): 05 f0 00 00 00 00 00 00 24 14 70 [ 1030.241168] SDIO Func1 (0xe8-0xf2): 05 f0 00 00 00 00 00 00 24 14 70 [ 1030.248445] woal_request_fw failed [ 1030.252557] Firmware Init Failed [ 1030.260510] Free module params [ 1030.264292] woal_add_card failed [ 1030.268383] wlan_sdio: probe of mmc1:0001:1 failed with error -1 [ 1030.275567] wlan: Register to Bus Driver Done [ 1030.280673] wlan: Driver loaded successfully       # cat /sys/kernel/debug/mmc1/ios clock:          208000000 Hz vdd:            21 (3.3 ~ 3.4 V) bus mode:       2 (push-pull) chip select:    0 (don't care) power mode:     2 (on) bus width:      2 (4 bits) timing spec:    6 (sd uhs SDR104) signal voltage: 1 (1.80 V) driver type:    0 (driver type B)   wifi 8987 + imx8m plus   &usdhc2 { assigned-clocks = <&clk IMX8MP_CLK_USDHC2>; assigned-clock-rates = <400000000>; pinctrl-names = "default", "state_100mhz", "state_200mhz"; pinctrl-0 = <&pinctrl_usdhc2>; pinctrl-1 = <&pinctrl_usdhc2_100mhz>; pinctrl-2 = <&pinctrl_usdhc2_200mhz>; bus-width = <4>; pm-ignore-notify; keep-power-in-suspend; fsl,sdio-async-interrupt-enabled; status = "okay"; }; Re: iMX8MPlus + 88W8987 + PDn pin Hello, The following hardware conditions will cause the error code in your log, please take a look in each point. 1. SDIO communication is abnormal 2. The 32.768K clock of the Wi-Fi chip is not used 3. The power supply current of the Wi-Fi chip is not enough (when downloading FW, the peak current requirement is relatively large, and the total power supply current of 3.3V must be greater than 1.5A). Best regards.
View full article
S32 Design Studio for Power Architecture for WINDOWS 11 Hi, I am looking for the supported windows operating system for latest "S32 Design Studio for Power Architecture" and its download site. Thanks Gokulraj Re: S32 Design Studio for Power Architecture for WINDOWS 11 Hi,  S32DS for PA is no more developed. Latest version is S32DS for PA v2.1. It is not tested on WIN 11, but can be used with it. You can download it here - https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-ide/s32-design-studio-for-power-architecture:S32DS-PA 
View full article
[Lear] [S32K311] 需要对 MCAL RTD V4.0.0 P19 版本中的汇编器选项进行澄清 你好,团队、 李尔写道 ----------------------------------------------------------------------------- 我只想总结一下,并跟进我在这封电子邮件中提出的最初问题: 我们确定了 MCAL RTD V4.0.0 P19 版本说明中提到的汇编器选项--fpu vfpv5-SP,但在 IAR V8.50.10 文档中找不到它。您澄清了 RTD 团队实际上使用的是--fpu FPv5-SP。 我的问题是 :从李尔的角度来看,我们应该使用哪个选项——MCAL版本说明中指定的选项(--fpu v fpv5-SP),还是恩智浦团队采用的选项(--fpu fpv5-SP )? ----------------------------------------------------------------------------------------- BR Stefano 优先级:高 RTD Re: [Lear][S32K311] Clarification required on Assembler Option in MCAL RTD V4.0.0 P19 Release 你好,我是@StefanoGattazzo、 正如你在版本说明中看到的那样,编译器选项是 "--fpu=fpv5-SP ",汇编器选项是 "--fpu vfpv5-SP "。因此,他们在使用时应遵循正确的选项类型。 "--fpu=FPv5-SP" 和"--fpu VFPv5-SP" 已在"IAR C/C++ Development Guide" 文档中注明。 顺祝商祺! 丹
View full article
Error when using EB to configure FS23 driver _0-1753439081159.png _1-1753439111221.png _2-1753439144529.png Hello, I am configuring the FS2303 driver and the EB gives me an error message as in figure one. But I have added the notification function in Figure 2. At the same time, I don't know how the error in Figure 3 is generated. I am using Autosar 4.4. Version 2.0 of S32K3 mcal driver and Autosar 4.7 version 1.0 for FS23 MCAL Driver. I would like to ask if the above issue is a problem caused by incompatibility between the two versions? Re: 使用EB配置FS23驱动时报错 Okay, thanks for the reply. Re: 使用EB配置FS23驱动时报错 Hi@夏超 从release note里面来看,你所使用的版本确实是不兼容的。我将这两个版本所对应的版本截图给你看。 FS23 SBC AUTOSAR R21-11 Version 1.0.0 Senlent_0-1753669563921.png FS23 SBC Autosar 4.4 version 0.8.0 Senlent_1-1753669688281.png
View full article
S32G274ardb2 IPCF、BSP40 + IPCF_4.9.0_D2310 错误 恩智浦团队, 我在 S32G274ardb2 硬件上使用 BSP40 + IPCF_4.9.0_D2310。 我版本了 "ipc-shm-uio.ko"& " ipc-shm-sample.ko " 使用 yocto 版本系统。 我按照" 回复 中提到的步骤进行了操作: 恩智浦 S32G274A RDB2 的问题 - IPCF - 恩智浦社区 ". 但在执行 insmod ipc-shm-sample.ko 文件时,我得到了错误信息"无法保留本地 shm 区域" 。 ramjeey_0-1753444077208.png 我已经版本了 .ko文件使用 yocto 编译系统时我获得 " " 版本魔法 " 错误当我构建 .ko 的时候出现错误文件,并在 UM 上手动插入 .ko文件 root@s32g274ardb2:/lib/modules/5.15.145-rt73+g3a3fafb13baa+p0/extra# dmesg | grep uio [ 0.802110] hse-uio 40210000.mu0b:未找到固件 [ 243.511859] ipc_shm_uio:版本神奇 '5.15.145-rt73SMP preempt mod_unload aarch64 "应为 "5.15.145-rt73+g3a3fafb13baa+p0SMP 抢占 mod_unload aarch64' [ 2131.570066] ipc_shm_uio:版本魔幻 '5.15.145-rt73SMP preempt mod_unload aarch64 "应为 "5.15.145-rt73+g3a3fafb13baa+p0SMP 抢占 mod_unload aarch64' [ 8467.474097] ipc_shm_uio: version magic '5.15.145+g3a3fafb13baa+p0-rt73-dirtySMP preempt mod_unload aarch64 "应为 "5.15.145-rt73+g3a3fafb13baa+p0SMP 抢占 我的 u-启动 环境设置如下 setenv d ecache 关闭 mw.q 0x34100000 0x0 0x40000 s aveen v 启动 在这里通知我没跑," IPCF_Example_S32G274A_M7_0.bin " 在 m7-Core 上。 请求您的帮助。 Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err 你好,@ramjeey 从你分享的日志来看,IPCF 运行正常,没有问题。 对于最后一次测试,我建议您尝试手动删除使用过的 ko 文件,然后插入 ko 文件并再次运行测试,以检查是否还有问题。 BR 切宁 Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err 你好@chenyin_h 感谢您的答复。 您说得对,要加载 IPCF .koA53 核心上的文件,M7 核心上的应用程序应首先运行。以下所有输出均与 S32G274ardb2 NXP 硬件上的 BSP38 + IPCF_4.9.0_D2310 有关。 ipc-shm-dev.ko & ipc-shm-sample.koipc-shm-dev .ko& ipc-shm-sample.ko 此外,我在版本 .elf 时使用 yocto 编译系统构建了 ipc-shm-sample_uio.elf文件,我在 os_uio/ipc-os.c中做了修改 #define IPC_UIO_MODULE_NAME"ipc_shm_uio" #define IPC_UIO_MODULE_PATH"/lib/modules/5.15.119-rt65-yocto-standard/extra/ipc-shm-uio.ko" 我可以执行 ipc-shm-sample_uio.elf 并得到以下输出。 elf-execution.PNG 我已经使用 UM 步骤手动版本了 ipc-shm-sample.ko & ipc-shm-sample_uio.elf,在加载 insmod 时出现了以下错误 ipc-shm-sample.ko root@s32g274ardb2:~/IPCF# insmod ipc-shm-sample.ko insmod:ER[ 424.031982] ipc_shm_sample: version magic '5.15.119-rt65-yocto-standardSMP 抢占 mod_unload aarch64 "应为 "5.15.119-rt65SMP 抢占 mod_unload aa' ROR:无法插入模块 ipc-shm-sample.ko:无效模块格式 以上"版本魔术" 只需将 5.15.119-rt65-yocto-standard 移动/重命名为 5.15.119-rt65 即可解决。 extra# ./ipc-shm-sample_uio.elf 输入数字 [1283.925001] ipc_shm_uio:加载树外模块会污染内核。 要发送的消息数:5 ipc-shm-us-app:ch 0 > > 19 字节:发送消息:5 ipc-shm-us-app:ch 1 > > 32 字节:#0 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#0Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#1 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#1Message 来自 Cortex M7!@ ipc-shm-us-app:ch 1 > > 32 字节:#2 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#2Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#3 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#3Message 来自 Cortex M7!@ ipc-shm-us-app:ch 1 > > 32 字节:#4 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#4Message 来自 Cortex M7!@ ipc-shm-us-app:ch 0 < < 19 字节:回复的消息:5 输入要发送的消息数量:10 ipc-shm-us-app:ch 0 > > 20 字节:发送消息:10 ipc-shm-us-app:ch 1 > > 32 字节:#0 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#0Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#1 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#1Message 来自 Cortex M7!@ ipc-shm-us-app:ch 1 > > 32 字节:#2 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#2Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#3 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#3Message 来自 Cortex M7!@ ipc-shm-us-app:ch 1 > > 32 字节:#4 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#4Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#5 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#5Message 来自 Cortex M7!@ ipc-shm-us-app:ch 1 > > 32 字节:#6 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#6Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#7 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#7Message 来自 Cortex M7!@ ipc-shm-us-app:ch 1 > > 32 字节:#8 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#8Message 来自 Cortex M7!@ ipc-shm-us-app:ch 2 > > 32 字节:#9 HELLO WORLD!来自用户 ipc-shm-us-app:ch 2 < < 24 字节:#9Message 来自 Cortex M7!@ ipc-shm-us-app:ch 0 < < 20 字节:回复的消息:10 输入要发送的消息数量:1 ipc-shm-us-app:ch 0 > > 19 字节:发送消息:1 ipc-shm-us-app:ch 1 > > 32 字节:#0 HELLO WORLD!来自用户 ipc-shm-us-app:ch 1 < < 24 字节:#0Message 来自 Cortex M7!@ ipc-shm-us-app:ch 0 < < 19 字节:回复的消息:1 输入要发送的消息数量:^cSegmention fault /extra #。 /ipc-shm-sample_uio.elf ipc-shm-uio.lib:ipc_os_init ():无法加载 /lib/modules/5.15.119-rt65+ge18f05316cd9/extra/ ipc-shm-uio.ko 模块要再次执行 ipc-shm-sample_uio.elf, 我需要重新启动硬件并重新执行所有启动命令。 请注意,我只有在构建 .ko 时才会遇到这个问题。&.elf文件。 谨致 Ramjee Yadav Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err 你好,@ramjeey 感谢您的回复。 您能否检查一下 IPCF_Example_S32G274A_M7_0 目录中的 description.txt 所描述的步骤? 在插入 Linux 模块之前,可能需要先运行 M7 应用程序。 如果按照文件中显示的步骤仍发现问题,请随时更新记录,我们将帮助进一步调查。 BR 切宁 Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err 我甚至在 S32G274ardb2 硬件上使用 BSP38 + IPCF_4.9.0_D2310 A-53 内核进行了尝试。 我仍然得到同样的错误信息 root@s32g274ardb2:~/IPCF# lsmod sja1110 20480 0 root@s32g274ardb2:~/IPCF# lsmod ipc-shm-dev.ko 使用方法: lsmod root@s32g274ardb2:~/IPCF# insmod ipc-shm-dev.ko root@s32g274ardb2:~/IPCF# root@s32g274ardb2:~/IPCF# lsmod ipc_shm_dev 40960 0 sja1110 20480 0 root@s32g274ardb2:~/IPCF# insmod ipc-shm-sample.ko insmod:ERROR:无法插入模块 ipc-shm-sample.ko:无法分配内存 BSP38-IPCF-Err.PNG 请求提供如何解决 Er. 请注意,我没有在 m7-Core 上刷新 " IPCF_Example_S32G274A_M7_0.bin " 或任何二进制文件。 Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err 你好,@ramjeey 谢谢您的帖子。 我们正在研究 IPCF 4.9.0 版本说明并查看以下信息: chenyin_h_0-1753672391839.png 请问您使用 BSP38+IPCF4.9 测试过吗? BR 切宁
View full article
S32G274ardb2 IPCF、BSP40 + IPCF_4.9.0_D2310 エラー こんにちは、NXPチーム S32G274ardb2 ハードウェアで BSP40 + IPCF_4.9.0_D2310 を使用しています。 「ipc-shm-uio.ko」を構築しました& "ipc-shm-sample.ko" は yocto ビルド システムを使用します。 返信「 Re: NXP S32G274A RDB2 の問題 - IPCF - NXP コミュニティ」に記載されている手順に従いました。 しかし、insmod ipc-shm-sample.ko ファイルを実行しているときに、「ローカル shm 領域を予約できません」というエラーが発生します。 ramjeey_0-1753444077208.png 私は.koを構築しました.ko をビルドしたときに「バージョンマジック」エラーが発生したため、yocto ビルドシステムを使用してファイルをビルドしました。ファイルを手動でUMの手順に従い、.koを挿入していましたファイル。 root@s32g274ardb2:/lib/modules/5.15.145-rt73+g3a3fafb13baa+p0/extra# dmesg | grep uio [ 0.802110] hse-uio 40210000.mu0b:ファームウェアが見つかりません [ 243.511859] ipc_shm_uio: バージョンマジック '5.15.145-rt73SMP preempt mod_unload aarch64' は '5.15.145-rt73+g3a3fafb13baa+p0 であるべきであるSMP プリエンプト mod_unload aarch64' [ 2131.570066] ipc_shm_uio: バージョンマジック '5.15.145-rt73SMP preempt mod_unload aarch64' は '5.15.145-rt73+g3a3fafb13baa+p0 であるべきであるSMP プリエンプト mod_unload aarch64' [ 8467.474097] ipc_shm_uio: バージョンマジック '5.15.145+g3a3fafb13baa+p0-rt73-dirtySMP preempt mod_unload aarch64' は '5.15.145-rt73+g3a3fafb13baa+p0 であるべきであるSMPプリエンプトm' u-boot envを以下のように設定しました setenv デキャッシュオフ mw.q 0x34100000 0x0 0x40000 保存環境 ブート ここで、M7 コア上で「 IPCF_Example_S32G274A_M7_0.bin 」を実行していないことに注意してください。 あなたの助けを要請します。 Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err こんにちは、 @ramjeey 共有していただいたログによると、IPCF は問題なく正常に動作しています。 最後のテストでは、使用した ko ファイルを手動で削除し、ko ファイルを挿入して再度テストを実行し、まだ問題が残っているかどうかを確認することをお勧めします。 BR チェイン Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err こんにちは@chenyin_h ご返信ありがとうございます。 IPCF .koをロードするには、正解です。A53 コア側のファイル、M7 コア上のアプリケーションが最初に実行される必要があります。以下のすべての出力は、S32G274ardb2 NXP ハードウェア上の BSP38 + IPCF_4.9.0_D2310 に関するものです。 ipc-shm-dev.ko & ipc-shm-sample.koipc-shm-dev.ko および ipc-shm-sample.ko さらに、.elfをビルディングしながら、Yoctoビルディングシステムを使用してipc-shm-sample_uio.elfをビルディングしました。ファイル os_uio/ ipc-os.cに変更を加えました #IPC_UIO_MODULE_NAME "ipc_shm_uio" を定義します #define IPC_UIO_MODULE_PATH "/lib/modules/5.15.119-rt65-yocto-standard/extra/ipc-shm-uio.ko" ipc-shm-sample_uio.elf を実行すると、以下の出力が得られました。 elf-execution.PNG UMの手順を使用してipc-shm-sample.koとipc-shm-sample_uio.elfを手動でビルドしましたが、insmod ipc-shm-sample.koをロード中に以下のエラーが発生していました。 root@s32g274ardb2:~/IPCF# insmod ipc-shm-sample.ko insmod: ER[ 424.031982] ipc_shm_sample: バージョン マジック '5.15.119-rt65-yocto-standardSMP preempt mod_unload aarch64' は '5.15.119-rt65' であるべきであるSMP プリエンプト mod_unload aa' ROR: モジュール ipc-shm-sample.ko を挿入できませんでした:無効なモジュール形式 上記の「バージョンマジック」は、5.15.119-rt65-yocto-standard を 5.15.119-rt65 に移動/名前変更するだけで解決されました。 追加# ./ipc-shm-sample_uio.elf 入力番号 [ 1283.925001] ipc_shm_uio: ツリー外のモジュールをロードするとカーネルが汚染されます。 送信するメッセージの数: 5 ipc-shm-us-app: ch 0 >> 19 バイト: 送信メッセージ: 5 ipc-shm-us-app: ch 1 >> 32 バイト: #0 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #0Cortex M7▒からのメッセージ!@ ipc-shm-us-app: ch 2 >> 32 バイト: #1 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #1Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 1 >> 32 バイト: #2 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #2Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 2 >> 32 バイト: #3 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #3Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 1 >> 32 バイト: #4 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #4Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 0 << 19 バイト: 返信メッセージ: 5 送信するメッセージの数を入力してください: 10 ipc-shm-us-app: ch 0 >> 20 バイト: 送信メッセージ: 10 ipc-shm-us-app: ch 1 >> 32 バイト: #0 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #0Cortex M7▒からのメッセージ!@ ipc-shm-us-app: ch 2 >> 32 バイト: #1 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #1Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 1 >> 32 バイト: #2 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #2Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 2 >> 32 バイト: #3 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #3Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 1 >> 32 バイト: #4 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #4Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 2 >> 32 バイト: #5 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #5Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 1 >> 32 バイト: #6 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #6Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 2 >> 32 バイト: #7 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #7Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 1 >> 32 バイト: #8 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #8Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 2 >> 32 バイト: #9 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 2 << 24 バイト: #9Cortex M7 からのメッセージ▒!@ ipc-shm-us-app: ch 0 << 20 バイト: 返信メッセージ: 10 送信するメッセージの数を入力してください: 1 ipc-shm-us-app: ch 0 >> 19 バイト: 送信メッセージ: 1 ipc-shm-us-app: ch 1 >> 32 バイト: #0 HELLO WORLD!ユーザーから ipc-shm-us-app: ch 1 << 24 バイト: #0Cortex M7▒からのメッセージ!@ ipc-shm-us-app: ch 0 << 19 バイト: 返信メッセージ: 1 送信するメッセージの数を入力してください: ^Cセグメンテーションエラー /extra# ./ipc-shm-sample_uio.elf ipc-shm-uio-lib: ipc_os_init(): /lib/modules/5.15.119-rt65+ge18f05316cd9/extra/ipc-shm-uio.ko モジュールをロードできません ipc-shm-sample_uio.elfを再度実行するには、ハードウェアを再起動し、すべてのブート コマンドを再度実行する必要があります。 この問題は、.koをビルディングしている場合にのみ発生することをお知らせします。&.elfファイルを手動で作成します。 よろしくお願いいたします。 ラムジー・ヤダブ Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err こんにちは、 @ramjeey ご返信ありがとうございます。 IPCF_Example_S32G274A_M7_0 ディレクトリの description.txt に記載されている手順を確認していただけますか? Linux モジュールを挿入する前に、まず M7 アプリケーションを実行する必要がある場合があります。 ドキュメントに記載されている手順に従っても問題がまだ解決しない場合は、ログ全体を添えてチケットを更新してください。さらに詳しく調査いたします。 BR チェイン Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err 私も、S32G274ardb2 ハードウェア上の BSP38 + IPCF_4.9.0_D2310 A-53 コアで試しました。 それでも同じエラーが発生します root@s32g274ardb2:~/IPCF# lsmod モジュールサイズ使用 sja1110 20480 0 root@s32g274ardb2:~/IPCF# lsmod ipc-shm-dev.ko 使用法: lsmod root@s32g274ardb2:~/IPCF# insmod ipc-shm-dev.ko ルート@s32g274ardb2:~/IPCF# root@s32g274ardb2:~/IPCF# lsmod モジュールサイズ使用 ipc_shm_dev 40960 0 sja1110 20480 0 root@s32g274ardb2:~/IPCF# insmod ipc-shm-sample.ko insmod: エラー: モジュール ipc-shm-sample.ko を挿入できませんでした:メモリを割り当てられません BSP38-IPCF-Err.PNG エラーを解決する方法についてアドバイスをお願いします。 ここで、M7 コアに「 IPCF_Example_S32G274A_M7_0.bin 」または任意のバイナリをフラッシュしていないことをお知らせします。 Re: S32G274ardb2 IPCF, BSP40 + IPCF_4.9.0_D2310 Err こんにちは、 @ramjeey ご投稿ありがとうございます。 IPCF 4.9.0 リリース ノートを調べたところ、次の情報が確認されました。 chenyin_h_0-1753672391839.png BSP38+IPCF4.9 でテストしたかどうかを教えていただけますか? それはあなたの側では正しいですか? BR チェイン
View full article
内核驱动程序编译数据(mcx/gpu-viv)问题 这与其说是一个问题,不如说是对未来内核升级的希望。 作为一项政策,我们不希望在内核中写入任何身份信息。 有一个有用的版本选项 KBUILD_BUILD_HOST,可以应用它来指定我们选择的开发主机名。 浏览我们的内核和模块二进制文件的版本后发现,源代码的 mxc/gpu-viv 部分会生成自己的 HOST 变量,而不是使用内核选项。 我知道整个内核源代码包非常庞大,对于正在运行/成熟的东西来说,资源微乎其微,但我希望可以在 Kbuild 中修改这个 " 功能 " 以使用 KBUILD_BUILD_HOST 或者干脆将其删除。 对我来说,很难说楼宇主机名对驱动程序有什么价值。它仅在 mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.c 中使用。 Re: Problem With Kernel Driver Compiled-In Data (mcx/gpu-viv) 您好, ,感谢您的意见,我们将把您的意见转达给软件团队进行评估。 致以最崇高的敬意/问候, Aldo。
View full article
Can I use LVGL8.2.0 with Chinese input method, that is, the keyboard widget to input Chinese, I use LVGL8.2.0 LVGL8.2.0, use the keyboard widget to do Chinese input, I am using LVGL8.2.0, and the gui guider is using version 1.4.1; can I do it? Re: LVGL8.2.0能用中文输入法吗,就是键盘部件输入中文,我用的是LVGL8.2.0 Hello @HJJHJJ. I checked the GUI Guider v1.9.1 Release Notes. You can see that gui guider v1.4.0 and v1.4.1 support Chinese input keyboard. Celeste_Liu_0-1753951983542.png However, older versions are not sure about stability and are difficult to support if there is a problem. We recommend you to upgrade your LVGL version and use the latest version of Gui Guider v1.9.1. BRs. Celeste
View full article
VKAM voltage Output of MC33FS6523CAE Hi, How to choose this part numbers? The part number I have chosen is MC33FS6523CAE Alternator Regulator Re: VKAM voltage Output of MC33FS6523CAE MC33FS6523CAE This should be defaulted to OFF and needs to be turned on via SPI. guoweisun_0-1754272315777.png
View full article
Memmory configuration for IMX93 1GB Hi i need to modify dts to adapt to 1GB ddr i have modified and its working but when i tried to run an ai example it crashes and wont run. can anyone confirm if my dts is correct. if possible can you give examples of 1GB 512MB and 256MB reserved-memory { #address-cells = <2>; #size-cells = <2>; ranges; linux,cma { compatible = "shared-dma-pool"; reusable; alloc-ranges = <0 0x80000000 0 0x20000000>; size = <0 0x8000000>; linux,cma-default; }; ethosu_mem: ethosu_region@A0000000 { compatible = "shared-dma-pool"; reusable; reg = <0x0 0xA0000000 0x0 0x800000>; }; vdev0vring0: vdev0vring0@92000000 { reg = <0 0x92000000 0 0x8000>; no-map; }; vdev0vring1: vdev0vring1@92008000 { reg = <0 0x92008000 0 0x8000>; no-map; }; vdev1vring0: vdev1vring0@92010000 { reg = <0 0x92010000 0 0x8000>; no-map; }; vdev1vring1: vdev1vring1@92018000 { reg = <0 0x92018000 0 0x8000>; no-map; }; rsc_table: rsc-table@2021e000 { reg = <0 0x2021e000 0 0x1000>; no-map; }; vdevbuffer: vdevbuffer@92020000 { compatible = "shared-dma-pool"; reg = <0 0x92020000 0 0x100000>; no-map; }; ele_reserved: ele-reserved@92120000 { compatible = "shared-dma-pool"; reg = <0 0x92120000 0 0x100000>; no-map; }; };  @imx93 Linux Yocto Project Re: Memmory configuration for IMX93 1GB Hello, I do not see issues in your configuration. These settings are application dependent. So you need to estimate how many buffers is required for peripherals. If you application is crashing could be because CMA pool too small. Also please confirm if reserved regions don’t exceed physical RAM. Best regards. Re: Memmory configuration for IMX93 1GB @JorgeCas thanks for the answer. i have generated the ddr files and modified everything accordingly can you just let me know if the dts is correct if not provide an example. Re: Memmory configuration for IMX93 1GB Hello, What you need to configure in your board to use 1GB of RAM is the next: • Generate the 1GByte timing.c file in Config Tool. • ccange the DRAM size to 1GB. uboot-imx/include/configs/imx93_evk.h Here an example: Screenshot 2025-08-04 110203.png Best regards.
View full article
MIMXRT1062DVL6B MCU D/C:2048+ 33% 引脚开路故障 其中约三分之一有缺陷。两块板都有同样的问题:打开引脚。# 1.jpg
View full article
カーネル6.12へのアップグレード後のHDMIディスプレイの問題 こんにちは 6.12 カーネルにアップグレードした後、i.MX 8M PLus からの HDMI 出力に関して (おそらくドライバ関連で) 問題が発生した方は他にもいらっしゃいますか? 本日、SSH 接続を介して 2 台の Debix Model A モデルを 6.12 カーネルにネイティブ アップグレードし、HDMI モニターを接続してみました。両方のボードで、ボードの最初の起動時に数秒間 Debix スプラッシュ スクリーンが正しく表示されますが、その後、グラフィカル ユーザー インターフェースのない点滅する水平カーソルに切り替わります。どちらのボードも、SSH およびシリアル コンソール経由で引き続き利用できます (長期的には、ネイティブ ビルドではなくクロス コンパイルに移行する予定です)。 この問題が発生した 2 番目のボードでは、リセット直前は GUI が正しく表示されていましたが、リセット後は GUI が消えてしまいました。この問題は、sudo reboot を実行したとき、ボードのリセット ボタンを使用したとき、およびボードの電源を切断して再接続したときも同じでした。 最近は SSH 経由でボード上で作業していますが、今日はカメラ モジュールをテストするために HDMI モニターをコネクテッドしました。 HDMI モニターに必要なドライバに問題があるのかどうかわかりません。友人は、i.MX 8M Plus で使用されている Vivante IP Core ドライバ etnaviv に問題がある可能性があると示唆しました。これには、オープンソース コードに含まれていない独自のドライバが関係します。 意思 グラフィックスとディスプレイ i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M ミニ | i.MX 8M ナノ Re: HDMI Display Problem Following Upgrade to 6.12 Kernel こんにちは@Bio_TICFSL どうもありがとうございます。 これは私の責任です。私は NXP の Ubuntu ディストリビューションを使用していましたが、Ubuntu ディストリビューションが更新されなくなったことに気付かずにカーネルをアップグレードしようとしました。現在は NXP の Debian ディストリビューションに移行していますが、NXP は Debian ディストリビューションを長期的に更新し続けることを計画しているのでしょうか? ご協力ありがとうございました 意思 Re: HDMI Display Problem Following Upgrade to 6.12 Kernel こんにちは、 これはどの i.MX8 プロセッサですか? どのボードですか? これは EVK では発生しません。 よろしくお願いします。
View full article
i.MX93 Linux 的随机 MAC 地址 在我们的开发/自动测试环境中,我们根据目标硬件 MAC 地址分配固定 IP 地址。不幸的是,我刚刚发现 i.MX93 FRDM 板在每次启动时都会随机分配其 MAC 地址。 有没有办法将板配置为在每次启动时都提供一致的 MAC 地址? 标记@david_dicarlo以提高知名度。 Re: Random MAC Addresses with i.MX93 Linux 你好@dpearson: 加上 xiaochong 的好评,将 FRDM-IMX93 设置为固定 MAC 地址的另一个选择是编程 i.mx93 Fusemap bankNum 39 字 3、字 4 和字 5。i.mx93 Fusemap 位于名为 的参考手册附件中。 此致 丹尼尔 Re: Random MAC Addresses with i.MX93 Linux 在 u-boot 中。您可以使用 $setenv ethaddr xx:xx:xx:xx:xx:xx $saveenv
View full article
在 MCU MKW38 系列上实现 Eeprom 仿真 你好,恩智浦,我有一些关于 MCU MKW38 的 Eeprom 仿真功能的问题、 1。MKW38 系列有年度申请吗,我们正在寻找与以下应用笔记类似的资源: https://device.report/m/251d6f3329899e5dd1b87578434ee5e64a3084ed273449540c3ce62b51de8b25.pdf 我们特别希望了解 mkw38 系列的以下详细信息 : EEPROM数据大小代码 FlexNVM分区代码 现在我可以通过在下面设置这个宏来设置 EEPROM 的大小 4096 字节: #define EEPROM_DATA_SET_SIZE_CODE (0x32U) #define FLEXNVM_PARTITION_CODE (0x4U) 但是,我仍然不知道在 MKW38 上用作 EEPROM 仿真备份的 FlexNVM 的实际大小。现有文档仅涵盖 S32K 系列产品。虽然这可能与 MKW38 有关,但我们需要有关该 MCU 的 FlexNVM 配置的明确而具体的信息。 2.目前我使用的是 SDK_2.x_FRDM-KW383.5.0 版本、 使用 frdmkw38_ble_shell_freertos 框架和此内存布局设置: BANGYUD_0-1755058584369.png 在使用frdmkw38_ble_shell_freertos模块时,能否利用64 KB 的 FlexNVM作为备份存储器,使用4 KB数据的EEPROM 仿真? 3.如果可能的话,你能否澄清一下专门用作 EEPROM 仿真备份的 flexNVM 内存的起始地址(而不仅仅是 FlexNVM 区域的通用起始地址)? 4。如果这不可能,请与我们联系原因并提供详细解释。 谢谢! Re: Implement Eeprom Emulation on MCU MKW38 series 你好 希望你一切顺利。 尽管没有适用于该设备的特定AN文档,但我建议查看flexnvm_eeprom SDK示例,因为它演示了如何使用闪存驱动程序来操作EEPROM。 你可以在 MKW39/38/37 参考手册第 4.6.1.1 节 " 闪存大小 " 中找到有关闪存映射配置的更多信息,包括 EEPROM 备份分区。其中,FlexNVM 别名内存范围为 0x0004_0000 至 0x0007_FFFF。 有关如何配置 EEPROM 备份区域的详细信息,请参阅参考手册中的第 30.3.4.3 节 " flexNVM 分区代码 ",其中指定了如何编程 DEPROM 寄存器设置。 顺祝商祺! 安娜-索菲亚
View full article
sgtl5000 数据表模棱两可 你好 我对以下文件有疑问: 文件编号SGTL5000 Rev. 7, 1/2022 表 18(第 32 页)描述了 CHIP_CLK_CTRL 寄存器(addr=0x4)的位域。 该表的"定义" 列指出,MCLK_FREQ 字段取决于某个名为"Fs" 的值,该值在文件中没有任何定义。 我猜测(但不确定,请确认),当 RATE_MODE=0 时,"Fs"=SYS_FS。 我的问题是:当 RATE_MODE 字段未设置为 0 时,"Fs" ? 我设置了 RATE_MODE=2,但输出波形没有任何变化。 如何使用 RATE_MODE> 0 功能? 谢谢! DSC Re: sgtl5000 datasheet ambiguity 你好,亚历克斯 我不是音频工程师,但我手头有一台 evk,可以用来尝试设置。在 evk 上有一个 12.288Mhz 振荡器连接到 SYS_MCLK。我连接的是 48khz 采样率和 16 位信号源。由于手头没有 8k 采样率的信号源 ,我将 SYS_FS 设置为 48khz,并使用 256*FS,因为我的振荡频率为 12.288MHZ(48khz*256),我将 I2S0_MODE 设置为(DSP 模式 A/B),rate_mode 设置为 00(在这种情况下为 48khz),我测得 I2S 信号 I2S_LRCLK 为 48khz。 我认为 I2S_LRCLK 是 SYS_FS * rate_mode 分频器。对于 8khz,就像你的 48k*1/6。 Re: sgtl5000 datasheet ambiguity 感谢您的回复。假设我设置 1.SYS_FS=2 (48kHz) 2.RATE_MODE=3 (48kHz 的 1/6),以获得"有效" Fs=8KHz I2S_LRCLK 时钟频率应如何设置? 谢谢、 Re: sgtl5000 datasheet ambiguity 你好 我之所以引用该文档,是因为它显示了CHIP_CLK_CTRL寄存器中8kHz采样率的配置示例,如前所述,没有必要在编解码器中使用DSP模式,并且在应用笔记中忽略了与DSP_MODE相关的其他配置。 SYS_MCLK 频率应介于 8MHz 和 27MHz 之间。这样就可以将内部系统采样率设置为 48 KHz,并使用 RATE_MODE 作为预分频器来获得 8 KHz 采样率。 顺祝商祺! Re: sgtl5000 datasheet ambiguity 1. 2. 明白。 3.那么如何在不使用 I2S DSP 模式的情况下在从机模式下设置 Fs=8000Hz 呢? Re: sgtl5000 datasheet ambiguity 你好 1.不,您可以在没有 DSP 模式的情况下实现该配置。 2.我指的是速率模式预分频器之后的工作采样率。 顺祝商祺! Re: sgtl5000 datasheet ambiguity 您好,您是想说只有当 I2S 处于"DSP 模式" 时,Fs=8000Hz 才有可能吗? 另外,在"effective Fs" 下是什么意思? 致敬 Re: sgtl5000 datasheet ambiguity 你好 你说得对,最低工作频率是 8MHz。 如果您在工作频率范围内,它将使用内部 PLL 来推导音频时钟。MCLK_FREQ 和 SCLKFREQ 基于有效的 Fs,但实际的 SYS_MCLK 输入仍必须大于 8MHz,因此需要提供一个基于未修改 SYS_FS 的时钟。 您可以在应用笔记中使用此配置作为示例: I2S DSP 模式 本文件展示了如何使用 RATE_MODE 从更高的 SYS_FS(如 48 kHz)中导出 8 kHz。 顺祝商祺! Re: sgtl5000 datasheet ambiguity 谢谢。我已经尝试过这种设置,但遗憾的是没有用。 另外,数据手册(第 1 页和第 10 页)指出,SYS_MCLK 时钟的频率范围仅为 8MHz 至 27MHz。在您建议的设置中,频率为 4.096MHz。这会是问题的原因吗? 我看到本论坛已经讨论过射程问题。例如 https://community.nxp.com/t5/Other-NXP-Products/SGTL5000-minimum-SYS-MCLK-frequency/m-p/1393679/highlight/true#M12897 同时,数据表显示 Fs=8000Hz 是可以达到的。 所以问题仍然存在: Regards Re: sgtl5000 datasheet ambiguity 谢谢。我已经尝试过这种设置,但遗憾的是没有用。 另外,数据手册(第 1 页和第 10 页)指出,SYS_MCLK 时钟的频率范围仅为 8MHz 至 27MHz。在您建议的设置中,时钟频率为 4.096MHz。这会是出现问题的原因吗? 我看到本论坛已经讨论过射程问题。例如 https://community.nxp.com/t5/Other-NXP-Products/SGTL5000-minimum-SYS-MCLK-frequency/m-p/1393679/highlight/true#M12897 同时,数据表显示 Fs=8000Hz 是可以达到的。 所以问题仍然存在:怎么做? 此致 Re: sgtl5000 datasheet ambiguity 你好 我对延误表示歉意。 1. 如果您需要在同步从机模式下将编解码器安装为 8000Hz 采样率,则正确的配置为 8kHz*512=4.096MHz因为速率模式影响的是采样率,而不是原始 SYS_FS。 2. 就 SCLK 而言,由于速率模式将 SYS_FS 除以 4,因此位时钟必须为 512 kHz。 顺祝商祺! Re: sgtl5000 datasheet ambiguity 8 月 29 日,我收到了关于该主题新回复的电子邮件通知。然而,我在这里看不到。请提供帮助 Re: sgtl5000 datasheet ambiguity 您好,我明白您的意思 - 这是从您的数据表中摘录的,没有必要在此重复。我看了数据表,觉得模棱两可。因此,为了简化问题,请回答我的问题。 为方便起见,我将它们再次粘贴在这里: 假设我想在同步(从)模式下将编解码器安装到 8000Hz 的采样率。 我设置 SYS_FS=0(32kHz)和 RATE_MODE=2(Fs=SYS_RATE/4=32kHz/4=8000Hz)。 (1) 如果我选择 MCLK_FREQ=2 设置 (512*Fs),是否应提供 (a) 32kHz*512 = 16.384MHz 或 (b) 8kHz*512=4.096MHz 作为主时钟? (2) 如果我选择 SCLKFREQ=0 (64Fs) 设置,我应该提供 (a) 2.048MHz 还是 (b) 512kHz 的比特时钟? 我希望,如果你知道自己想说什么,就不难回答类似 "例如 "这样的问题。(1)a和(2)b。如果你认为选项(a)或非(b)都不正确,那么请告知我的示例的正确值。 你们的数据表模棱两可,所以我才会提出这样的问题! 感谢您的帮助 Re: sgtl5000 datasheet ambiguity 你好 在同步模式下,SCLK 位时钟的频率直接 ,取决于 SYS_MCLK 输入时钟的频率。根据 MCLK_FREQ 位的设置,计算公式如下: 。 MCLK_FREQ = 0 时,SCLK = SYS_MCLK/8 (256Fs) MCLK_FREQ = 1 时,SCLK = SYS_MCLK/12 (384Fs) MCLK_FREQ = 2 时,SCLK = SYS_MCLK/16 (512Fs) 然后,根据 SCLKFREQ 位的设置,Fs 频率可计算为 SCLK/32 或 SCLK/64。 顺祝商祺! Re: sgtl5000 datasheet ambiguity 请您澄清一下。 假设我想将编解码器安装到 8000Hz 采样率。 在从属模式下,我设置 SYS_FS=0(32kHz)和 RATE_MODE=2(Fs=SYS_RATE/4=32kHz/4=8000Hz)。 如果选择 MCLK_FREQ=2 (512*Fs),我应该提供 32kHz*512=16.384MHz 还是 8kHz*512=4.096MHz 作为主时钟? 关于 SCLKFREQ 也有同样的问题。如果选择 SCLKFREQ=0 (64Fs),应该提供 2.048MHz 还是 512kHz 的比特时钟? 谢谢! Re: sgtl5000 datasheet ambiguity 你好 是的,您需要在 SGTL5000 处于从属模式时进行配置。 在从模式下,它从主模式接收 BCLK 和 LRCLK,但需要正确设置 CHIP_CLK_CTRL 中的 SYS_FS 和 MCLK_FREQ 字段,以确保内部定时和路由。 顺祝商祺! Re: sgtl5000 datasheet ambiguity 这也适用于从属模式吗? Re: sgtl5000 datasheet ambiguity 你好 对于 PLL 模式,SYS_FS / RATE_MODE = Fs 等式只有在 SCLKFREQ 设置为 64Fs 时才有效(SCLKFREQ=0)。 顺祝商祺!
View full article
在 MCUXpresso IDE 中使用固件测试 PNEV5190 时,闪存下载不起作用。 你好 完成 PNEV5190 的外部连接设置后,我正在测试连接到 MCXN947 板的 PNEV5190 板。在测试过程中,有时会出现闪存下载过程中擦除不起作用的问题。 因此,我检查了硬件,电压正常,但 PN5190 或 K82F CPU 的晶振没有输出时钟。 此外,连接 USB 时,它会显示 " 正在连接启动加载程序 " 然后在设备管理器中,它会一直像 RESET CPU 一样运行。对于 J-Link 来说,它会被正确地捕获在设备管理器中。下面是连接到 PNEV5190 USB 时的 LED 状态图。 hangyoKim_0-1755847114916.png 上述情况是否可视为 PNEV5190 的故障? 或者我应该将其视为 K82F CPU 故障? 此外,如果有办法解决这个问题,请告诉我。 顺祝商祺! Re: When testing PNEV5190 with firmware in MCUXpresso IDE, flash download does not work. 您好@hangyoKim,日安! 感谢您对我们的产品感兴趣。 我想请您提供更多详细资料,说明截至目前所采取的程序。请说明您在将 PNEV5190 连接到外部主机时进行了哪些设置或修改? 我还想问一下,您的设置想要达到什么目的,您是如何进行测试的? 请确认,您尝试闪存的固件是什么?你试图在哪个 IC 上闪存?为此你采取了哪些步骤?您是否使用 MCUXpresso IDE? 您说时钟不是从晶振发出的,是指 SPI 时钟吗?如果没有,您是如何进行测试的?请注意,SPI 时钟必须由主机 MCU 产生,而不是由 PN5190 产生。 请注意,只有在使用 OpenSDA 接口闪存板载 k82 时,才需要使用 j20 端口通过 USB 连接 PNEV5190。 还要考虑的是,要通过 SPI 接口连接外部主机,必须对主板进行一些硬件修改,请参阅 PN5190 EMV L1 软件移植至 IMX1170 应用说明的第 2 节 ,其中您将找到相关详细信息,可用作使用 MCXN947 主机 MCU 的起点 。 致以最诚挚的问候, Daniel
View full article
MIMXRT1170-EVK,未检测到 USB0 端口 大家好, 我正在尝试调试 MIMXRT1170-EVK,但一切看起来都很好,有些板上没有检测到 USB。请问,这将是这起事件的根本原因吗? Re: MIMXRT1170-EVK, USB0 port not Detecting 你好@PushkarSutharStryker、 请查看应用笔记 AN13206: AN13206:修改采用基于LPC4322的调试探头的i.MX RT10xx板上的调试固件 | 恩智浦半导体 顺祝商祺! MayLiu Re: MIMXRT1170-EVK, USB0 port not Detecting 你好,Mayliul、 我们正在按照您的指示做同样的事情。 U24A (LPC4322JET100) 的固件有没有可能在工作过程中损坏或更改。我们是否有可能重新对 MCU 进行编程? 当我们检查了EVK上的物理(电连接)是否正确时,U24A IC的电压也正确。电脑只检测不到 USB0。我们也在尝试使用其他 EVK,但效果很好。 这是硬件故障还是 U24A MCU 程序问题? 此致, 普什卡-苏塔尔 Re: MIMXRT1170-EVK, USB0 port not Detecting 你好@PushkarSutharStryker、 感谢您提供的最新信息。 1: 如果您想编译和调试 MIMXRT1170-EVK 项目,我认为 IDE 是 MCUXPresso IDE。 i.MX RT1170 评估套件入门|恩智浦半导体 请点击此链接,并确保 SW1:0010(内部启动)。 2: 如果电源来自 USB0,则需要设置 J38 连接 5-6。 3.你想使用这个工具吗 " McuxPress 安全配置工具 " 下载你的代码,如果是,你需要设置 SW 1:0001(串行下载器模式)。 顺祝商祺! MayLiu Re: MIMXRT1170-EVK, USB0 port not Detecting 我们正在使用 MIMXRT1170-EVK,正在尝试使用 USB0 将板与电脑连接起来。 在少数板中,USB 端口无法检测。以下是同一板的更多详细信息。 1.部件号: - IMXRT1170-EVK。 2.USB0 端口。 3.电源来自 USB0。 4.示意图附后。 5。IDE:-McuXpress 安全配置工具。 Re: MIMXRT1170-EVK, USB0 port not Detecting 你好@PushkarSuthar、 非常感谢您关注我们的产品并使用我们的社区。 1:请检查 SDK 版本、MIMXRT1170-EVK 或 MIMXRT1170-EVKB 开发板版本以及 IDE 版本是否兼容。 2: 请提供有关您问题的更多详细信息。 敬上 MayLiu
View full article