2144079_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2144079_en-US

2144079_en-US

Can I use LVGL8.2.0 with Chinese input method, that is, the keyboard widget to input Chinese, I use LVGL8.2.0

LVGL8.2.0, use the keyboard widget to do Chinese input, I am using LVGL8.2.0, and the gui guider is using version 1.4.1; can I do it?

Re: LVGL8.2.0能用中文输入法吗,就是键盘部件输入中文,我用的是LVGL8.2.0

Hello @HJJHJJ.

I checked the GUI Guider v1.9.1 Release Notes.

You can see that gui guider v1.4.0 and v1.4.1 support Chinese input keyboard.

Celeste_Liu_0-1753951983542.pngCeleste_Liu_0-1753951983542.png

However, older versions are not sure about stability and are difficult to support if there is a problem. We recommend you to upgrade your LVGL version and use the latest version of Gui Guider v1.9.1.

BRs.

Celeste

Tags (1)
No ratings
Version history
Last update:
‎11-20-2025 03:56 PM
Updated by: