Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
MMA6900KQ Hello, I am looking for an accelerometer sensor for measuring the longitudinal and lateral acceleration of the vehicle. One of the key requirements is that the data measured with the accelerometer has no delay or little delay compared to the true value of the acceleration. Which product in your catalog do you advise me ? I was looking at MMA6900KQ, do you think it could fit ? Re: MMA6900KQ Hi, I think that the MMA6900KQ would work without a problem, but other solution with a different approach could be using an analog output accelerometer for which you can use an external ADC that adjust to the required conversion speed. My recommended analog output accelerometer would be the FXLN83xx family devices, you can find details in the following link: https://www.nxp.com/products/sensors/motion-sensors/accelerometers-for-iot/nxp-analog-accelerometers:FXLN83xxQ?lang=en&lang_cd=en& Have a great day, Jose ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: MMA6900KQ Hello Jose, Sincerely thank you for your quick reply to me. I want to state the fact that I used the FXLS8471Q accelerometer chip before, but the sampled data always has a large delay compared with the real value, which can't meet my requirements. I have asked about the chip delay problem in the community, but it has not been resolved. So I plan to switch to MMA6900KQ, I hope it can meet my key requirements that the data measured with the accelerometer has no delay or little delay compared to the true value of the acceleration. Best wishes, Impression Re: MMA6900KQ Hi, MMA6900KQ would be the best solution for you application, it is a 2-axis (XY) accelerometer, which would give you the capacity to measure the longitudinal and lateral acceleration of the vehicle. Timing delay between data measured compared to the true value of the acceleration is not characterized, however, been the MMA6900KQ a Safe Assure Automotive device and because of one of its typical application is Electronic Stability Control (ESC), I personally don’t think that timing would be a problem. Have a great day, Jose ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
View full article
imx8mp isp 视频节点未指定 您好, 我正在使用 5.10.35 发行版的 imx8mplus 移植 imx290 传感器模块 我按照摄像头传感器移植指南在 vvcam 中相应地更改了驱动程序,但是当主板启动时,即使驱动程序的探测功能成功也不会创建任何视频节点。 以下是模块开始加载时的日志信息: [ 6.208014] imx290_vvcam: loading out-of-tree module taints kernel. [ 6.224028] entering th func:imx290_probe [ 6.318075] eimx290_vvcam 1-0042: supply DOVDD not found, using dummy regulator [ 6.339949] eimx290_vvcam 1-0042: supply DVDD not found, using dummy regulator [ 6.349485] eimx290_vvcam 1-0042:未找到 AVDD 电源,使用假稳压器 [ 6.382951] imx8_media_dev:模块来自暂存目录,质量未知,已警告您。 [ 6.443331] enter viv_isp_init_module [ 6.448757] enter isp_hw_probe [ 6.453073] enter viv_dwe_init_module [ 6.456791] vvcam isp driver registered [ 6.457080] enter dwe_hw_probe [ 6.461686] imx-sdma 30e10000.dma-controller:固件已找到。 [6.466027] vvcam 广角鱼眼畸变校正 驱动程序已探测 [6.470277] imx-sdma 30bd0000.dma-controller: 固件已找到。 [ 6.479325] imx-sdma 30bd0000.dma-controller:已加载固件 4.6 [ 6.839512] caam 算法已在 /proc/crypto [ 6.896947] caam 30900000.crypto:caam pkc 算法已在 /proc/crypto 中注册 [ 6.896962] caam 30900000.crypto:注册 rng-caam [6.898300] 设备 caam-keygen 随机注册 [6.921808]:随机完成 crng 初始化 [6.921819]:由于速率限制错过了 7 条随机警告 [7.309550] ext4-FS (mmcblk2p2):使用有序数据模式挂载的文件系统。 选项:(null) [ 7.383698] RTL8211F 千兆以太网 30be0000.ethernet-1:01:附加 PHY 驱动程序 [RTL8211F 千兆以太网] (mii_bus: phy_addr=30be0000。) [7.475098] imx-dwmac 30bf0000.ethernet eth1:PHY [stmmac-1:01] 驱动程序 [RTL8211F 千兆以太网] (irq=poll) [7.487079] imx-dwmac 30bf0000.ethernet eth1:不支持功能安全功能 [7.487093] imx-dwmac 30bf0000.ethernet eth1:支持 IEEE 1588-2008 高级时间戳 [7.487093] imx-dwmac 30bf0000.ethernet eth1:支持 IEEE 1588-2008 高级时间戳 [7.487093] imx-dwmac] imx-dwmac 30bf0000.ethernet eth1:注册的 PTP 时钟 [7.487510] imx-dwmac 30bf0000.ethernet eth1:配置 phy/rgmii-id 链接模式 [7.519467] 8021q:在设备 eth1 的硬件过滤器中添加 VLAN 0 [8.143730] 审计:type=1006 审计 ( 1616581522. 276:2):pid=639 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 [ 8.192190] initilizing media entity pads of the camera subdev= 0 后的 returnvalue [ 8.196776] 异步注册摄像机 subdev= 0 后的 returnvalue [ 8.204482] 进入 func:imx290_retrieve_capture_properties [ 8.211560] 检测到 imx290。 当我使用 lsmod: 检查时,它正在创建以下模块,但没有加载 vvcam_video 模块 使用的模块大小 vvcam_isp 65536 0 vvcam_dwe 28672 0 imx8_media_dev 20480 0 imx290_vvcam 147456 0 当我尝试删除 imx8_media_dev 模块并再次进行 modprobe 时 imx290_vvcam 147456 1 这使得模块得到了使用,但仍然没有创建视频节点。 当我 modprobe vvcam_video 时,它正在加载,但没有再次被使用,因为 vvcam_video 40960 0 请帮我解决这个问题。 在此先表示感谢、 穆凯什-库马尔 Re: imx8mp isp video node not cteated 我们正在为 imx415 摄像头传感器开发 vvcam 摄像头驱动程序。您能为相机传感器开发驱动程序吗? Re: imx8mp isp video node not cteated 你好@quercuspau、 现在 ISP 运行良好。我已经没有问题了。至于其他信息,很抱歉我不能透露。 顺祝商祺! K. Re: imx8mp isp video node not cteated 你好@khang_letruong、 据我所知,你设法在互联网服务提供商处运行了摄像头,你捕获的照片看起来有多好?我还在一些帖子中读到,您与恩智浦相机协助公司签订了合同,但在收到 xml 和 drv 文件后,您在图像校准参数方面仍遇到一些问题。你能解决这些问题吗?请问,协助公司调整相机参数的费用是多少? BR Re: imx8mp isp video node not cteated 你好,@quercuspau、 老实说,与 Basler 摄像机相比,ov2775 和 os08a20 是两个很好的公开范例。 您可能需要根据自定义传感器连接的 I2C 总线/节点(及其属性,例如 gpio、地址)、mipi-csi2 节点(及其属性,例如通道数...)来调整设备树。 BR, K Re: imx8mp isp video node not cteated 嗨,@mukesh_kumar、 也许你指的是上层(isp-imx 中的 ISI 层)来生成供 isp_media_server 使用的 .drv,以及用于加载必要的内核模块和传感器本身校准配置的脚本。不过,这与本票最初的主题不同:在成功探测您的内核模块 imx290_vvcam 之后创建 /dev/videoX。 我发现你提到的链接中的讨论足以实现上层,包括你的 imx290 的 .drv。 BR、 K. Re: imx8mp isp video node not cteated 你好@khang_letruong 感谢您的回复, ,我已经查看了运行脚本,要想添加对 imx290 的支持,需要一个 .drv文件和 .xml文件 我在https://community.nxp.com/t5/i-MX-Processors/ISP-working-in-i-MX8M-Plus/m-p/1307705的讨论中尝试为 imx290 生成一个版本 但当我发出命令 ./build-isp-all 版本完整版 它正在部分构建,但没有生成任何 .drv文件,尽管所需文件已添加到 isi/drv/ 文件夹。 感谢并致意 穆克什 Re: imx8mp isp video node not cteated 嗨,@mukesh_kumar和@khang_letruong 如果我理解正确的话,你使用 ov2775 模块作为参考,并使用 imx290 驱动程序寄存器配置对其进行了调整。设备树摄像头方面没有预期的变化。在 imx290 中使用与 ov2775 相同的 xml 和 drv 可以吗? 此致 Re: imx8mp isp video node not cteated 你好@quercuspau 根据传感器移植指南,vvcam 中应该有支持 isp 的传感器,但 vvcam 中没有 imx290 驱动程序。 谢谢、 穆克什 Re: imx8mp isp video node not cteated 很好! Re: imx8mp isp video node not cteated 您好, 是否不能在 isp 中使用已有的 imx290 驱动程序? 我打算将同一个传感器与 imx8mp 和 ISP 一起使用。不过,我还没有开始 BR Re: imx8mp isp video node not cteated 你好@mukesh_kumar、 首先,确保 vvcam 内核驱动程序(从 imx290_vvcam.c 生成的 mx290_vvcam.ko例如)在 isp-imx 框架内执行 run.sh 脚本时会正确加载。您还可以对其进行修改,以添加 imx290 传感器。 然后确保在dmesg 中找到以下一行(即管道 I2C 传感器 -> mipi-csi2 --> isp 在 dts 中链接良好): [ 7.884122] mx8-img-md: created link [imx290 1-001a] => [mxc-mipi-csi2.0] 与 ov2775 或其他函数类似,您可以在下面的探测函数代码段中检查所有 V4L2 函数是否都成功返回: sd = &sensor->subdev; v4l2_i2c_subdev_init(sd, client, &ov2775_subdev_ops); sd->flags |= V4L2_SUBDEV_FL_HAS_DEVNODE; sd->entity.function = MEDIA_ENT_F_CAM_SENSOR; sensor->pads[OV2775_SENS_PAD_SOURCE].flags = MEDIA_PAD_FL_SOURCE; retval = media_entity_pads_init(&sd->entity, OV2775_SENS_PADS_NUM, sensor->pads); sd->entity.ops = &ov2775_sd_media_ops; if (retval < 0) goto probe_err_power_down; retval = v4l2_async_register_subdev_sensor_common(sd); if (retval < 0) { dev_err(&client->dev,"%s--Async register failed, ret=%d\n", __func__,retval); goto probe_err_entity_cleanup; } Br, K Re: imx8mp isp video node not cteated 你好@khang_letruong 感谢您回复查询, 我使用的是 isp_0 节点,并在设备树源代码中启用了相同的功能,如下所示 &cameradev { status ="okay"; }; &isi_0 { status ="disable"; }; &isp_0 { status ="okay"; }; &dewarp { status ="okay"; }; 我不明白在 basler 案例中是哪个模块/服务调用了 vvcam_video 模块,而在我之前的回复中提到的 ov2775 和 imx290 中却没有发生。 感谢并致意 穆克什 Re: imx8mp isp video node not cteated 嗨,@mukesh_kumar、 也许您忘记在 dts 中启用&isp_0 节点或&isp_1 节点。 敬上, K. Re: imx8mp isp video node not cteated 你好、 我参考了 ov2775_mipi_v3.c文件。 我观察到当我在启动 vvcam_isp 65536 1 vvcam_dwe 28672 1 vvcam_video 40960 1 vvcam_video 40960 1 imx8_media_dev 20480 0 basler_c amera_driver_vvcam 20480 0 0 它正在加载模块 ----> vvcam_video、vvcam_isp、vvcam_dwe,即使没有连接摄像头,也在使用这些模块。 如果我在启动时加载 imx8mp-evk-ov2775.dtb 文件, 它正在加载模块---> 在没有设备的情况下,甚至没有连接摄像机 vvcam_isp 65536 0 vvcam_dwe 28672 0 imx8_media_dev 20480 0 os08a20 32768 0 即使没有摄像头,我也无法理解在basler dtb的情况下哪个触发了加载vvcam_video。 请帮我理解这一点,因为就我而言,我无法在启动时加载vvcam_video模块。 此外,在 imx290 模块加载之前,imx8_media_dev 模块也在加载,如何才能让 imx8_media_dev 在我的模块探测成功后加载? 我试着在 /etc/ 文件夹下创建一个文件模块,并将顺序保持为 imx290,然后是 imx8_media_dev,但没有成功。 谁能帮我解决这两个问题? 谢谢, Mukesh kumar。 Re: imx8mp isp video node not cteated 哦,感谢您的回复, 您能否分享一下您对 ISP 调整过程的了解,有哪些要求,如何设置环境等。 再次感谢@khang_letruong 的回复。 Vishnu S Re: imx8mp isp video node not cteated 您好@SiddavatamVishnu、 请问这个问题是问我吗?如果是,我的回答是肯定的,我可以为 IMX415 开发驱动程序。 谢谢,并致以最崇高的敬意、 Khang
View full article
S32G3 QSPI 报告 FR[AIBSEF] 错误 专家你好 我们收到来自 IAST 的问题,他们报告 M7 应用程序报告了FR[AIBSEF] 错误。他们使用的是 RTD4.0.2。 根据 S32G3 RM 的说法,当 AHB 突发大小大于 bufxCR [ADATSZ] 中的预取大小时,AIBSEF 就会被触发,我检查过他们的 BUF3CR [ADATSZ] 是 0x80,这是 QSPI 支持的最大大小(1024 字节)。您知道如何检查 S32G 寄存器中的 HBUSRT 大小吗?能否请您也就此问题发表一些意见? 我还在 S32G RM 中发现了另一个令人困惑的地方,即 AHB 读取不支持 WRAP* 事务,这是否意味着 G3 实际上不支持 HBUSRT?如果是,FR[AIBSEF]的根本原因是什么? 优先级:中等 RTD Re: S32G3 QSPI reported FR[AIBSEF] error 嗨,@Arthur_shi、 我在 QSPI 中没有看到设置 HBURST 和 HSIZE 的地方。但是从我的角度来看,最大突发量 = 16,最大 Hsize = 64 位 = 8 字节。因此,AHB 事务的最大突发总大小 = 16 x 8 = 128,不能大于 1024。我没有看到驱动程序处理 FR[AIBSEF] 位。请将 AIBSEF 位出现时 QSPI 的所有寄存器和 QSPI 配置文件发给我,我将试着查看是否能发现任何问题。 顺祝商祺! Nhi Re: S32G3 QSPI reported FR[AIBSEF] error 这是从客户处收到的寄存器 Re: S32G3 QSPI reported FR[AIBSEF] error 从你的图像来看,AHB 缓冲区的配置如下: 遵循 RM 中的主 ID 表: 如果用户使用 M7,似乎所有事务都会被路由到缓冲区 3,因为主 ID 与其他缓冲区不匹配。但缓冲区 3 的配置是 1024,所以我不明白为什么他们能得到这个位。 但是,我认为他们可以尝试更改缓冲区配置,以查看与缓冲区0、1、2匹配的缓冲区大小为0且序列ID表示16字节的数据。 如果他们使用多个内核,请尝试将每个主 ID 路由到不同的缓冲区。例如CM7_0 至缓冲区 0,CM7_1 至缓冲区 1,... 在执行新的 AHB 事务之前,请尝试检查这些位是否被提升。 Re: S32G3 QSPI reported FR[AIBSEF] error 我们收到客户的反馈,在阻止 A53 内核访问后,问题消失了,因此问题可能是由 A53 内核的投机访问引起的,我不知道为什么这种访问会导致AIBSEF 错误。我想确认的另一个问题是: S32G3 QSPI 支持 AHB 突发功能吗?正如我在之前的评论中提到的、 在 RM 中,QSPI 不支持 AHB warp 功能,但也有一节介绍了 AHB burst 功能,这让我很困惑?能否请您帮忙确认一下这项功能? Re: S32G3 QSPI reported FR[AIBSEF] error 从 RM 中,我了解到 AHB 支持 2 种类型:WRAP 和 INCR。但 S32G3 只支持 INCR。 HBurst 和 Hsize 无法在 QSPI 中配置。它们在 Core 文档中定义,并在启动时配置。 在客户的案例中,他们为核心 A53 配置了核心主 ID 0、1、2,分别为缓冲区 0、缓冲区 1、缓冲区 2,缓冲区大小为 0,因此用于与突发大小进行比较的数据大小是在序列 Id 中配置的数据。就他们而言,我看到序列中的数据大小为16字节,如果启动时配置的突发大小大于此值,则可能会发生此问题。
View full article
MCX Lab Educational Materials MCX Lab: Educational Materials for Lecturers and Students 1. Getting started with FRDM-MCXN947 The Getting Started with FRDM-MCXN947 introduces FRDM‑MCXN947 development board and MCUXpresso Software & Tools: MCUXpresso SDK and IDE installation and first steps FRDM-MCXN947 board overview Implementation of a basic LED and button project using MCUXpresso Configuration Tools 2. Basic laboratory assignments for FRDM-MCXN947  The Basic Lab Assignments for FRDM-MCXN947 contains a full laboratory guide structured into five progressively advanced tasks, each teaching students how to use various peripherals of the NXP MCXN947 microcontroller and FRDM-MCXN947 and FRDM-TEACH boards: Toggle of LED controlled by buttons using polling Toggle of LED controlled by buttons using interrupts Measurement of analog voltage from potentiometer Implementation of a simple command interpreter using connected to PC terminal Measurement of frequency and duty cycle of a square wave signal Each task contains implementation instructions using low‑level (register‑based) and high‑level (SDK) programming. 3. Introduction to AI/ML for embedded systems The Introduction to AI/ML for Embedded Systems provides an overview of how AI and Machine Learning concepts and practical hands-on, including: Fundamentals of AI/ML, how models are trained and used for inference, and benefits of AI/ML processing in the embedded systems NXP’s eIQ machine learning software environment, which supports dataset preparation, model training, optimization, quantization, conversion, and deployment NXP's eIQ Neutron Neural Processing Unit (NPU), available on MCXN947 MCU Practical example and hands-on steps to demonstrate how to train, convert, and integrate a CIFAR‑10 model into an embedded application 4. Getting started with Zephyr The FRDM-MCXN947 board is supported in Zephyr, an open-source, modular Real-Time Operating System (RTOS) hosted by the Linux Foundation for resource-constrained IoT and embedded devices. See Zephyr documentation for FRDM-MCXN947 board.  The Zephyr RTOS is supported in MCUXpresso for Visual Studio Code. Use Zephyr getting started with FRDM-MCXN947 laboratory guide to learn how to create, configure and debug your first project.
View full article
MCX Lab Expansion Boards MCX Lab: Expansion Boards   The MCX Lab is supported by multiple NXP-designed expansion boards that can be connected to FRDM-MCXN947 board. The expansion boards are useful for introductory labs, featuring combination of buttons, joystick, DIP switch, rotary encoder, LED ring, potentiometer, IR sensors, OLED display, and more. FRDM-TEACH The FRDM-TEACH provides combination of buttons, switches, LEDs, potentiometer, rotary encoder, RTC and square wave generator: 4x buttons 2x4 DIP switches 5x Jumpers LED bar with 10x LEDs RGB LED External GPIO circuit with LEDs Real-time circuit Square wave generator Temperature sensor Potentiometer Rotary encoder with pushbutton Arduino compatible connectors The FRDM-TEACH is used in Basic laboratory assignments for FRDM-MCXN947. See MCX Lab Educational Materials page for more. MCXN947-SHD-OLED The MCXN947-SHD-OLED provides combination of buttons, switches, LEDs, OLED, potentiometer, rotary encoder and multiple sensors: 4x buttons 8x DIP switches 5 position tactile switch 8x LEDs in ring configuration OLED 128 x 64 display Potentiometer Rotary encoder Light sensor Humidity and temperature sensor Thermistor IR receiver Arduino compatible connectors LCD-PAR-S035 The LCD-PAR-S035 is a 3.5” 480x320 IPS TFT LCD module with wide viewing angle and 5-point capacitive touch functionality that we recommend to use with the FRDM-MCXN947 board. See also LCD-PAR-S035 homepage. Expansion Board Hub Explore the Expansion Board Hub for more modules with sensors, actuators, interfaces, displays, wireless modules etc.
View full article
MCSPTE1AK116 (S32K116 + GD3000) - 在两个相同的套件上使用相同的固件:一个电机旋转,另一个不旋转。 你好, 我有两个相同的 MCSPTE1AK116 BLDC 电机套件。我在相同的条件下对两个套件进行了相同项目和固件的闪存/调试,但实际上只有一个套件能使电机旋转。 硬件/设置 套件:2 × MCSPTE1AK116(S32K116 + MC34GD3000 前置驱动器) 电机:套件中默认的 BLDC 电机 电源:12 V 电源(相同型号/相同接线)。 连接: 原有线路,无硬件改动 调试:OpenSDA + PEmicro (S32DS) 软件 示例/项目:(例如,BLDC_6 步/6 步无传感器或基于霍尔的系统) 版本:调试 固件:确认两块板上的二进制文件相同(相同的 .elf/.srec) 复制步骤 连接 12 V 和 USB(OpenSDA) 为每个套件闪存/调试相同的项目 启动电机(按钮或自动启动,取决于固件) 两种套件的结果不同 观察到的行为 套件 A:电机正常旋转 套件 B:我能听到开关/PWM "驱动 "声,但电机不转动 线路无明显区别,重复操作结果相同 我的尝试 多次重新刷新,验证了相同的项目设置 验证 S32DS 中的调试配置 (如果适用)交换电源线/电机线/相线:[如果已更换,请添加] 问题 / 接下来要检查什么? 在固件完全相同的情况下,一台 MCSPTE1AK116 设备能正常工作,而另一台却不能,最可能的根本原因是什么? GD3000 故障/状态寄存器? 欠压/过流保护? 驱动程序 EN/RST 或 SPI 启动问题? 由于硬件的不同,ADC/PDB 触发信号或 PWM/FTM 配置的行为可能会有所不同? 哪些寄存器/变量是确定故障套件是进入故障状态还是关闭功率级的最佳 "第一道检查"? 例如,FaultStatusLatched、FaultStatus、驱动器状态、GD3000 状态寄存器 (SR0/SR1)、直流总线 ADC 读数等。 MCSPTE1AK116 上是否有已知的常见硬件问题(跳线/连接器/功率级)会导致 "开关噪声但不旋转"? 如果你告诉我什么最有用,我可以提供额外的日志/测量结果(FreeMASTER 变量、GD3000 SR0/SR1、直流总线电压/电流 ADC 值、PWM/相位输出的示波器捕获)。 谢谢。 Re: MCSPTE1AK116 (S32K116 + GD3000) – Same firmware on two identical kits: one motor spins, the othe 你好@shin_JH 由于两个工具包使用相同的示例代码,而只有一个显示了问题,因此应用程序本身不太可能是根本原因。BLDC_6Step 示例已确认可在其他套件上运行。 下一步是使用逻辑分析仪或类似测量工具比较两种设置的硬件信号。请检查两个套件的以下内容: 从 S32K116 到 MC34GD3000 的 SPI 通信 MCU 产生的 PWM 信号 电机相位端子上的输出信号 霍尔传感器信号(霍尔 A、B 和 C) ADC 测量 您注意到这两种套件有什么不同吗? 另外,您是否尝试过在两种设置之间交换硬件?例如 将工作套件中的 DEVKIT-MOTORGD 与非工作套件一起使用 将工作套件中的电机与非工作套件一起使用 BR、VaneB
View full article
FS32K142の電源の問題 NXPの専門家の皆様 このデザインで使用される MCU は FS32K142HFT0MLF です。 私の質問は、このデバイスは3.3V電源、つまりVDD = +3.3Vで駆動できるかどうかです。? ご返信をお待ちしております。 よろしくお願いいたします。 遠い Re: Power supply issue with FS32K142 こんにちは@Julián_AragónM ご返信をいただき嬉しく思います。 あなたの答えは私の質問への答えでした。どうもありがとうございます。 よろしくお願いいたします。 遠い Re: Power supply issue with FS32K142 こんにちは@FAR1234さん、 はい。S32K1は3.3Vで動作できます。2.7 V ~ 5.5 V の動作電源電圧範囲をサポートします。つまり、設計要件に応じて 3.3 V または 5 V で動作できます。 3.3 V での 5.3 DC 電気仕様については、S32K1xx データシートの 5.3 章を参照してください。 よろしくお願いします、 ジュリアン
View full article
溦【xins4698】腾龙新公司注册游戏账号网址是多少 溦【xins4698】腾龙新公司注册游戏账号网址是多少 LPC Marketing LPC51Uxx LPC546xx LPC54xxx LPC55xx LPC800
View full article
MC33HB2000 你们好 我开始使用这个驱动器我做了一个印刷电路板,如果我使用数字输入,效果很好。我曾尝试使用 SPI 通信,但没有成功,所以来这里问几个问题。首先我使用的是 STM32 系列,我的问题是: - 即使要使用 SPI,是否也需要将 ENBL 引脚置 1? - 时钟极性有效高度是否正确? - 时钟相位第 1 个边沿正确吗? - 我在数据表上读到的最大频率是 10MHz,但在数据表的另一部分,我读到的最大频率是 10Mhz,那么正确的频率是多少? -如果我想读取寄存器我需要发送 0x00 来读取设备标识符 0x2000 以获取读取状态等如果我想写就设置位 15 对吗? 是的,我在发送数据前将 CS 调至低电平。 很抱歉提出这些问题 谢谢 塞尔吉奥 Re: MC33HB2000 非常感谢你们的帮助,我今晚回家后就试试。 昨天,我在网上找到了这份文件。 Re: MC33HB2000 亲爱的塞尔吉奥 欢迎您祝您愉快 致以最崇高的敬意 约瑟夫 Re: MC33HB2000 你好,塞尔吉奥、 - 即使要使用 SPI,是否也需要将 ENBL 引脚置 1? [A] 是,ENBL 引脚都必须为逻辑高电平。 - 时钟极性高电平有效对吗? [答] 正确。SCLK 线路为高电平有效,CPOL=0。 - 时钟相位第 1 个边沿正确吗? [A] 这是不正确的。数据在 SCLK 下降沿(第 2 个边沿)采样,CPHA=1。由此推断 SPI 模式为 1。 - 我在数据表上读到的最大频率是 10MHz,但在数据表的另一部分,我读到的最大频率是 10Mhz,那么正确的频率是多少? [A] 是,HB2000 SPI 最大工作频率为 10 MHz。 -如果我想读取寄存器我需要发送 0x00 来读取设备标识符 0x2000 以获取读取状态等如果我想写就设置位 15 对吗? [A] 请查看所附的 SPI HBridge SW 驱动程序。随附一份编程指南文件。 致以最崇高的敬意 约瑟夫 Re: MC33HB2000 感谢您的支持,现在工作得很好。 塞尔吉奥
View full article
S32N55 OTA 解决方案 专家们好 我想讨论一下 S32N55 的 OTA 解决方案。 目前,还没有可用的解决方案来演示 S32N55 的 OTA 用例。与 S32G 相比,由于引入了 FSS 内核,架构发生了变化。我的主要问题是 目前有没有推荐的 A/B 交换解决方案?A/B 交换功能应由 FSS 内核还是 CRS 等应用内核实现? 我注意到 FSS 固件中打算加入治疗功能,但目前还处于 WIP 阶段。你能否分享一下治疗过程的工作流程以及触发治疗的条件? 在比较 S32N 和 S32G 时,我发现 S32N 包括一个备用 IVT。RM 提到,IVT 备份用于 OTA 更新。我想了解 OTA 流程是如何运作的。S32G/Z/E 可以在没有备用 IVT 的情况下执行 OTA,那么 S32N 是否有需要备用 IVT 的特殊性? 感谢您的支持! BRs, 挂 FSS_FW Re: S32N55 OTA solution 你好@RaduBraga、 客户为香港按揭证券有限公司 感谢您的支持。 挂 Re: S32N55 OTA solution 您好@Hang_Zhang, 团队已受理此案,并将尽快给予答复。另外,指出这一点的顾客是谁? 致以最崇高的敬意, Radu Re: S32N55 OTA solution 您好@Hang_Zhang, 来自 Stefan Ungureanu 的意见: " 需要系统架构师提供意见 - 据我所知,FSS BootRom(S32N 芯片内不可更改的代码)会在主镜像验证失败时加载备份镜像。这对 NXP 资产有效: IVT:包含指向所有可启动映像的指针 。 DCD/ST-DCD:设备配置数据。 FSS FW:基础子系统固件。 HSE 固件:硬件安全引擎固件。 SYS 映像:保存用于安全启动的哈希值和配置。 PaCo:资源分配分区合同 Codef:群组定义,包括图像偏移量和启动顺序。 不清楚应用核心是如何完成的。 愈合将作为单独的插件模块 (fss_healing) 成为 fss_firmware 的一部分。事实上,这项工作正在进行中,计划于 2026 年 5 月左右完成。有两个主要的触发条件: a) 如果 fss_healing 检测到从备份加载的映像(由 bootroM 或 Fss 加载),它会将备份复制到主服务器以保持系统的完整性和映像兼容性。 b) 成功完成OTA后,将触发应用程序核心通过HSE在备份映像上复制主映像。 更多细节可以在这个治疗文档中找到:He al ing_component_v2.0.docx 非最终版本,未经同意不得共享。 所有备份映像都是可选的,包括备份 IVT。如果用户想更新 IVT,但更新过程中出现问题,系统应能从备份(如果有)中加载 IVT。否则,它将保持 RESET 模式。(需要建筑师确认)" Re: S32N55 OTA solution 你好 、 治疗文件是彗星专用的。 愈合文件中的信息不得与其他客户共享。 1.Comet 有一个定制的 HSE,可提供特定服务;普通市场上没有这些服务。 2.大部分功能都是根据他们的流程定制的。可能会误导一些客户,使其强行执行编程过程步骤。我们不想强加于人。需要灵活处理其他客户完成的其他 OTA 流程步骤(例如:Vector)。
View full article
使用 MBDT 实现 S32K344 低电源模式 你好 我正在使用 MATLAB/Simulink 基于模型的设计工具 (MBDT) 开发 S32K344 MCU,需要有关实现低电源模式的指导。 我无法找到一个明确的、端到端的程序: 使用 MBDT 配置低电源模式(运行/停止/待机或等效模式) S32 配置工具中的必要设置(PMC、MC_ME、时钟、唤醒源) 从 Simulink/Stateflow 触发电源模式转换 在基于 MBDT 的项目中正确处理唤醒源 如果有 S32K344 + MBDT 低功耗电源管理单元的参考示例、应用笔记或推荐的工作流程,请分享。 感谢您的支持。 Re: S32K344 Low Power Mode Implementation Using MBDT 你好 我创建了一篇文章,介绍如何使用 Model Based Design Toolbox for S32K3 v1.8.0 将 S32K344 设为待机模式。 请查看 如何使用 NXP MBDT 在 S32K3 上 实现 待机模式 :使用 NXP MBDT 在 S32K3 上实现待机模式 ,了解更多信息。此外,我还附上了一个示例模型,您可以试一试。你可能需要修改用于唤醒板的引脚和 LED 使用的引脚。 如果您需要其他方法来唤醒板,也可以查看以下文章:S32K3 低功耗管理 AN 和演示。 顺祝商祺! 索林-班奇拉
View full article
i.MX93 JTAG 调试 我想在 i.MX93 上使用 openocd 进行 JTAG 调试,但处理器似乎处于边界扫描模式(IDCODE 0x0892801d 而不是 0x5ba02477)。 要切换到 DEBUG 模式,我需要做什么? 是否有 openocd 配置文件? 洛塔尔-瓦斯曼 Re: i.MX93 JTAG debugging 你好@刘志明 你能给我发一个 FRDM i.MX93 开发板必要的 OpenOCD 文件吗?我想要板文件和 SoC 文件以及我想要的任何其他文件 FRDM-i.MX93 Re: i.MX93 JTAG debugging 你好,Zhiming_Liu、 能把它们也发给我吗? 此致, 克里斯蒂安 Re: i.MX93 JTAG debugging 您能与我分享 openocd 补丁吗? Re: i.MX93 JTAG debugging 你好 Zhiming_Liu、 能把它们也发给我吗? 此致, 罗伯托 Re: i.MX93 JTAG debugging 这个补丁公开过吗?有地方能搞到这本书吗? Re: i.MX93 JTAG debugging 你好,请把补丁也发给我。 在 imx93 产品页面上提供下载,或者向 openocd 项目发送拉取请求,不是更简单吗? Re: i.MX93 JTAG debugging 你好 Zhiming_Liu、 请分享 openocd 的补丁。 此致, Re: i.MX93 JTAG debugging 你好,Zhiming_Liu、 请把 openocd 的补丁也发给我。 非常感谢、 JS Re: i.MX93 JTAG debugging 你好@刘志明 您能把@torus1000的补丁也发给我吗? Re: i.MX93 JTAG debugging 你好,Zhiming_Liu、 请分享 openocd 的补丁。 此致, VR。 Re: i.MX93 JTAG debugging 我没有收到任何带有附件的电子邮件。只有本主题的通知邮件。 Re: i.MX93 JTAG debugging 你好@lw1 我已通过电子邮件发送了附件。 Re: i.MX93 JTAG debugging 什么附件? Re: i.MX93 JTAG debugging 你好@lw1 您需要修补 openocd 引用电子邮件中的附件
View full article
i.MX 8X-imx_v8_defconfig-针对大小、启动时间、常见漏洞与后门 风险进行了优化 你好,我们在哪里可以找到针对大小、启动时间、常见漏洞与后门风险进行了优化的缺陷配置示例? 最理想的是 i.MX 8X,但如果不适合 IMX 或一般的嵌入式 Linux? https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/configs/imx_v8_defconfig 有很多 i.MX 8X 嵌入式 Linux 设备通常不会使用的东西都有 y 吗? 谢谢 Peter i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus Re: i.MX 8X - imx_v8_defconfig - optimised for size, boot time, CVE risk 您好, 感谢您对恩智浦半导体产品的关注, 实际上,i.MX 处理器 defconfigs 有很多驱动程序和模块,因为内核将用于所有 Yocto 映像,包括它们的所有设备树和二进制演示以及以它们为特色的概念验证。 每次发布之间都会承保 常见漏洞与后门 风险,因此此建议将与分支机构有关,请使用最新的版本。 对于大小和启动时间,你可以从 imx_v8_defconfig 开始,删除应用程序不需要的驱动程序,这主要是反复试验,取决于应用程序。 此致
View full article
如何将 PLS UDE 调试器插件安装到 S32 Design Studio 中 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 适用于 Power 架构的 S32 Design Studio (S32DS) 支持PLS UDE Eclipse 插件,可直接在 S32DS Eclipse IDE 中通过PLS 探针调试 S32DS 项目。 所有版本的 S32DS for Power 都支持此功能。   该插件支持以下功能: 无缝集成 Eclipse IDE 中的 Universal Debug Engine 的完整功能 UDE 提供 Eclipse IDE 的自身视角,并将 UDE 工作区集成到 Eclipse 工作区中 代码断点可以通过 C/C++ 编辑器或 UDE 特定函数设置 有关该插件的更多详细信息,请阅读PLS 网站下载部分的“UDE Eclipse 数据表”。   安装说明 首先确保您的计算机上安装了 PLS UDE 调试器。接下来我们进行eclipse插件的安装。   1. 转到菜单“帮助”->“安装新软件”,然后单击“添加...”按钮并在 PLS UDE 安装文件夹中搜索名为“ UDEEclipse4Integration.zip ”的存档文件 2. 选择通用调试引擎组件,点击“下一步”     3.最后继续安装。系统将要求您确认未签名内容的安装。UDE插件安装后需要重新启动。     使用 UDE 创建新项目 您应该能够通过 S32DS 新项目向导创建一个新的 S32DS 项目,其中现在提供 PLS UDE 调试器支持。 UDE插件启用一组新的UDE eclipse调试配置来管理(创建、删除、调整) 使用新项目创建的 UDE 调试配置需要进行一些更改,然后才能继续调试。 1. 点击“ 新建工作区”按钮,在“ \.ude” 文件夹下输入新的 UDE 工作区名称 2.创建一个新的UDE Target配置文件。 单击“创建配置”按钮并选择“使用默认目标配置”和目标 MCU。(本例中为 MPC5744P)。 将配置文件保存到项目文件夹中,例如 “ \Project_Settings\Debugger\nxp_mpc5744p_cut2_debug_jtag.cfg” 运行调试器会打开 UDE 特定的调试 eclipse 视图,您可以在其中受益于许多高级调试功能,包括跟踪、脚本…… 享受使用 S32DS 中的 PLS UDE Eclipse 插件进行调试! 第三方(高级)插件
View full article
Kinetis KV5x Cortex-M7マイクロコントローラおよびGD3000モータ・プリドライバによるUAV速度制御 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Demo このデモでは、強力なKinetis KV46マイクロコントローラを使用した無人航空機(UAV)が、4つのGD3000ブラシレスDCプリドライバを制御して、プロペラを駆動する4つのモータを回転させます。   特長 KV5x 240MHz ARM Cortex-M7 MCU、高速ADCおよびタイマ搭載、4つのBLDCモーターすべてを制御する GD3000 BDLCモータプリドライバは、低Q MOSFETを駆動する高速スイッチングを特長としています 市場で唯一のシングルMCUソリューション – 部品点数とBOMコストの削減と優れた性能   注目のNXP製品 KV5x|Kinetis KV5xコネクテッド・コントロール・マイクロコントローラ |NXPの 3相ブラシレスモータープリドライバー|NXPの   リンクス Kinetis KV5xマイクロコントローラとGD3000モーター・プリドライバを使用したUAVの速度制御を搭載するクアドロコプターのデモ オートモーティブ インダストリアル
View full article
KW36 - 32kHz RTC 外部振荡器的微调 简介 FRDM-KW36 包含一个带有 32 kHz 晶振的 RTC 模块。该模块可在超低功耗模式下为 MCU 生成 32 kHz 时钟源。该振荡器包含一组用作 C LOAD 的可编程电容器。改变这些电容器的值可以改变振荡器提供的频率。 该可配置电容值范围为 0 pF(电容器组禁用)至 30 pF,步长为 2 pF 。这些值是通过组合已启用的电容器获得的。可用值为 2 pF 、4 pF 、8 pF和 16 pF 。 这四个电容可以任意组合。建议如果外部电容可用,则禁用这些内部电容(清除 RTC 控制寄存器 SFR 中的 SC2P、SC4P、SCS8 和 SC16 位)。 要调整振荡器提供的频率,首先必须能够测量频率。使用频率计数器是理想选择,因为它比示波器提供更精确的测量。您还需要输出振荡器频率。要输出振荡器频率,以任意蓝牙演示应用程序为例,您应该执行以下操作: 调整频率示例 此示例将利用连接软件堆栈中的心率传感器演示(freertos 版本),并假设开发人员具备从 SDK 到 IDE 导入或打开项目的知识。 从您的 SDK 打开或克隆心率传感器项目。 在工作区的 board 文件夹中找到 board.c 和 board.h 文件。 在 board.h 上声明一个 void 函数文件如下所示。此功能将用于将 RTC 时钟复用到 PTB3 并能够测量频率。 /* Function to mux PTB3 to RTC_CLKOUT */ void BOARD_EnableRtcClkOut (void);‍‍ 开发board.c里面的BOARD_EnableRtcClkOut函数文件如下。 void BOARD_EnableRtcClkOut(void) { /* Enable PORTB clock gating */ CLOCK_EnableClock(kCLOCK_PortB); /* Mux the RTC_CLKOUT to PTB3 */ PORT_SetPinMux(PORTB, 3u, kPORT_MuxAlt7); /* Select the 32kHz reference for RTC_CLKOUT signal */ SIM->SOPT1 |= SIM_SOPT1_OSC32KOUT(1); } 在 BOARD_BootClockRUN(board.c 文件)之后,在 hardware_init 函数中调用 BOARD_EnableRtcClkOut 函数。 找到clock_config.c工作区板文件夹中的文件。 在文件顶部添加以下定义。 #define RTC_OSC_CAP_LOAD_0 0x0U /*!< RTC oscillator, capacitance 0pF */ #define RTC_OSC_CAP_LOAD_2 0x2000U /*!< RTC oscillator, capacitance 2pF */ #define RTC_OSC_CAP_LOAD_4 0x1000U /*!< RTC oscillator, capacitance 4pF */ #define RTC_OSC_CAP_LOAD_6 0x3000U /*!< RTC oscillator, capacitance 6pF */ #define RTC_OSC_CAP_LOAD_8 0x800U /*!< RTC oscillator, capacitance 8pF */ #define RTC_OSC_CAP_LOAD_10 0x2800U /*!< RTC oscillator, capacitance 10pF */ #define RTC_OSC_CAP_LOAD_12 0x1800U /*!< RTC oscillator, capacitance 12pF */ #define RTC_OSC_CAP_LOAD_14 0x3800U /*!< RTC oscillator, capacitance 14pF */ #define RTC_OSC_CAP_LOAD_16 0x400U /*!< RTC oscillator, capacitance 16pF */ #define RTC_OSC_CAP_LOAD_18 0x2400U /*!< RTC oscillator, capacitance 18pF */ #define RTC_OSC_CAP_LOAD_20 0x1400U /*!< RTC oscillator, capacitance 20pF */ #define RTC_OSC_CAP_LOAD_22 0x3400U /*!< RTC oscillator, capacitance 22pF */ #define RTC_OSC_CAP_LOAD_24 0xC00U /*!< RTC oscillator, capacitance 24pF */ #define RTC_OSC_CAP_LOAD_26 0x2C00U /*!< RTC oscillator, capacitance 26pF */ #define RTC_OSC_CAP_LOAD_28 0x1C00U /*!< RTC oscillator, capacitance 28pF */ #define RTC_OSC_CAP_LOAD_30 0x3C00U /*!< RTC oscillator, capacitance 30pF */ 在 BOARD_BootClockRUN 函数中搜索 CLOCK_CONFIG_EnableRtcOsc 调用函数(也在 clock_config.c 中)文件),并通过上述任何定义来编辑参数。 最后,在“preinclude.h”中禁用低功耗选项和 LED 支持位于项目源文件夹中的文件: #define cPWR_UsePowerDownMode 0 #define gLEDSupported_d 0 此时,您可以在 PTB3 中测量并使用频率计数器进行频率调整。每次对电路板进行编程时,都需要执行 POR 以获得正确的测量结果。下表是从 FRDM-KW36 板 rev B 获得的,可以用作调整频率的参考。请注意,电容不仅由启用的内部电容组成,还包括封装、键合线、键合焊盘和 PCB 走线中的寄生电容。因此,虽然下面给出的参考测量值应该接近实际值,但您也应该使用电路板进行测量,以确保频率根据您的电路板和布局进行调整。 启用电容器 负载 电容定义 频率 - 0pF RTC_OSC_CAP_LOAD_0(银行禁用) 32772.980Hz SC2P 2pF RTC_OSC_CAP_LOAD_2 32771.330Hz SC4P 4pF RTC_OSC_CAP_LOAD_4 32770.050Hz SC2P, SC4P 6pF RTC_OSC_CAP_LOAD_6 32769.122Hz SC8P 8pF RTC_OSC_CAP_LOAD_8 32768.289Hz SC2P, SC8P 10 pF RTC_OSC_CAP_LOAD_10 32767.701Hz SC4P, SC8P 12pF RTC_OSC_CAP_LOAD_12 32767.182Hz SC2P, SC4P, SC8P 14pF RTC_OSC_CAP_LOAD_14 32766.766Hz SC16P 16pF RTC_OSC_CAP_LOAD_16 32766.338Hz SC2P, SC16P 18pF RTC_OSC_CAP_LOAD_18 32766.038Hz SC4P, SC16P 20pF RTC_OSC_CAP_LOAD_20 32765.762Hz SC2P, SC4P, SC16P 22pF RTC_OSC_CAP_LOAD_22 32765.532Hz SC8P, SC16P 24pF RTC_OSC_CAP_LOAD_24 32765.297Hz SC2P, SC8P, SC16P 26pF RTC_OSC_CAP_LOAD_26 32765.117Hz SC4P, SC8P, SC16P 28pF RTC_OSC_CAP_LOAD_28 32764.940Hz SC2P, SC4P, SC8P, SC16P 30 pF RTC_OSC_CAP_LOAD_30 32764.764Hz BLE软件 千瓦 KW35 | 36
View full article
iWave Systems 的 i.MX6 Q7 开发套件 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> i.MX6 Q7 开发套件       该开发平台采用Q7 兼容 i.MX6 SOM ,该 SOM 基于飞思卡尔的 i.MX 6 系列 1.2GHz 多媒体处理器和通用 Q7 兼容开发板。该平台可用于汽车、工业和医疗等垂直领域的任何高端应用的快速原型设计。该主板采用 120mmx120mm 尺寸的纳米 ITX 外形,配备了所有必要的板载连接器,以验证完整的 i.MX6 CPU 功能。   优势 由于工业温度等级和紧凑(120 x 120 - Nano ITX)外形尺寸,组装简单、成本低且坚固耐用 由于板载标准接口(uSD、USB 和内存),集成简单且成本低廉 最低功耗。典型功耗      亮点 非常适合快速开发 缩短产品开发生命周期 可以在很短的时间内完成快速定制 适用于验证任何 R1.20 Q7 兼容模块      特性 显示屏: 7 英寸 800x480 TFT LCD、VGA 端口/电视输出、HDMI 端口*、LVD 显示连接器* 触摸屏:电阻式触摸屏 电容式触摸屏* 视频输入:摄像头接口*、TV IN* 音频:外部音频编解码器、耳机/麦克风插孔 PCIe: PCIe Mini Card*, PCIex1 Port* USB: USB2.0 设备 - Mini AB 连接器,USB2.0 主机 2 个端口 - A 型连接器 串行: UART - DB9 连接器 存储: SATA 端口 1 - 7P 连接器*、SATA 端口 2 - 22P 连接器*、标准 SD 插槽 通信: 10/100Mbps 以太网 - RJ45 插孔、802.11b/g/n Wi-Fi 模块*、CAN 端口 - DB9 连接器* 电源: 12V DC 输入,板载 RTC 纽扣电池 尺寸规格: 120 x 120 - Nano ITX 支持温度: 0 至 60 oC      目标应用 工业/医疗 绿色能源控制器 平板电脑、高端 PDA、安全设备、 工业设备控制、汽车车载信息娱乐系统 医疗 HMI、自助服务终端、POS 机、通用嵌入式系统     点击此处了解 iWave 的 i.MX 6 Q7 开发套件的更多详细信息 概述
View full article
MCUXpresso 11.9 の ConfigTools が使い物にならないほど遅い こんにちは、 MCUXpresso 11.9 を使用して、i.MXRT1170 EVKB ボードで開発しています。 最初はうまく機能していましたが、今では使い物にならないほど遅くなっています。 参考までに、2つのアイテムを変更すると、プロセスエクスプローラーで次の負荷図が生成されました 時間範囲は約 10 分で、CPU 負荷は数分間 12.5% (1 つのコアが完全に使い果たされる) です。 最初のアクションはlittlefsの構成を変更することであり、2番目のアクションは、構成ツールが開いている間にプロジェクトを切り替えることでした(->6〜7分間のCPU負荷がいっぱいになり、UIが応答しません)。 これを回避するために何ができるでしょうか? 以下の私のインストールのバージョンの詳細を参照してください。 よろしくお願いいたします。 Rainer バイナリ パス: C:\nxp\MCUXpressoIDE_11.9.0_2144\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.9.0.202312111712\binaries\ ツール パス: C:\nxp\MCUXpressoIDE_11.9.0_2144\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.9.0.202307121226\tools\ ウィザードのパス: C:\nxp\MCUXpressoIDE_11.9.0_2144\ide\plugins\com.nxp.mcuxpresso.tools.wizards_11.9.0.202307121226\Wizards\ LinkServer バイナリ パス: C:\nxp\LinkServer_1.4.85\binaries 製品:MCUXpresso IDE バージョン: MCUXpresso IDE v11.9.0 [ビルド 2144] [2024-01-05] オペレーティングシステム:Windows 10 VM: OpenJDK 64 ビット サーバー VM (64 ビット) Plugins and versions: - com.crt.advproject (11.9.0.202401050803) - com.crt.config (11.9.0.202401050803) - com.crt.ctrlcenter (11.9.0.202401050803) - com.crt.quickstart (11.9.0.202401050803) - com.crt.utils (11.9.0.202401050803) - com.crt.vendor.arm.generic (11.9.0.202307121226) - com.crt.vendor.nxp.ctnxxx (11.9.0.202307121226) - com.crt.vendor.nxp.generic (11.9.0.202307121226) - com.crt.vendor.nxp.lpc11 (11.9.0.202307121226) - com.crt.vendor.nxp.lpc13 (11.9.0.202307121226) - com.crt.vendor.nxp.lpc17 (11.9.0.202307121226) - com.crt.vendor.nxp.lpc18 (11.9.0.202307121226) - com.crt.vendor.nxp.lpc43 (11.9.0.202307121226) - com.crt.vendor.nxp.nhs3xxx (11.9.0.202307121226) - com.crt.vendor.nxp.niobe (11.9.0.202307121226) - com.crt.vendor.nxp.pn7xxxxx (11.9.0.202307121226) - com.nxp.gnudocs (11.9.0.202401050803) - com.nxp.kex.standalone (1.0.0.202401041031) - com.nxp.lpcxpresso.installation.docs (11.9.0.202307121226) - com.nxp.lpcxpresso.instructiontrace.docs (11.9.0.202307121226) - com.nxp.lpcxpresso.powermeasurement.docs (11.9.0.202307121226) - com.nxp.lpcxpresso.swotrace.docs (11.9.0.202307121226) - com.nxp.lpcxpresso.userguide.docs (11.9.0.202307121226) - com.nxp.mcuxpresso.addons.docsupport (11.9.0.202401050803) - com.nxp.mcuxpresso.addons.gnuscript.editor (11.9.0.202401050803) - com.nxp.mcuxpresso.addons.gnuscript.editor.ide (11.9.0.202307121226) - com.nxp.mcuxpresso.addons.gnuscript.editor.ui (11.9.0.202307260707) - com.nxp.mcuxpresso.addons.imageinfo (11.9.0.202401050803) - com.nxp.mcuxpresso.addons.peripheralsview (11.9.0.202401050803) - com.nxp.mcuxpresso.addons.sdkbuilder (11.9.0.202401050803) - com.nxp.mcuxpresso.azurertos.docs (11.9.0.202307121226) - com.nxp.mcuxpresso.core.common (11.9.0.202311011411) - com.nxp.mcuxpresso.core.datamodels (11.9.0.202401050803) - com.nxp.mcuxpresso.core.datamodels.develop (11.9.0.202307121226) - com.nxp.mcuxpresso.core.datamodels.interfaces (11.9.0.202401050803) - com.nxp.mcuxpresso.core.datamodels.resources (11.9.0.202307121226) - com.nxp.mcuxpresso.core.datamodels.ui (11.9.0.202401050803) - com.nxp.mcuxpresso.core.debug (11.9.0.202401050803) - com.nxp.mcuxpresso.core.debug.support.linkserver (11.9.0.202401050803) - com.nxp.mcuxpresso.core.debug.support.pe (11.9.0.202401050803) - com.nxp.mcuxpresso.core.debug.support.segger (11.9.0.202401050803) - com.nxp.mcuxpresso.core.headless (11.9.0.202401050803) - com.nxp.mcuxpresso.datamodels.generic (11.9.0.202308300815) - com.nxp.mcuxpresso.datamodels.generic.ui (11.9.0.202401050803) - com.nxp.mcuxpresso.freertos.docs (11.9.0.202307121226) - com.nxp.mcuxpresso.ide (11.9.0.202401051634) - com.nxp.mcuxpresso.ide.theme (11.9.0.202401050803) - com.nxp.mcuxpresso.ide.welcome (11.9.0.202311191811) - com.nxp.mcuxpresso.mqxrtos.docs (11.9.0.202307121226) - com.nxp.mcuxpresso.powerprofile.docs (11.9.0.202307121226) - com.nxp.mcuxpresso.romtable (11.9.0.202401050803) - com.nxp.mcuxpresso.sdkcli.docs (11.9.0.202307121226) - com.nxp.mcuxpresso.swo.core (11.9.0.202401050803) - com.nxp.mcuxpresso.swo.ui (11.9.0.202401050803) - com.nxp.mcuxpresso.tad.azurertos (11.9.0.202401050803) - com.nxp.mcuxpresso.tad.common (11.9.0.202311161535) - com.nxp.mcuxpresso.tad.freertos (11.9.0.202401050803) - com.nxp.mcuxpresso.tad.zephyrrtos (11.9.0.202401050803) - com.nxp.mcuxpresso.tools.bin.win32 (11.9.0.202312111712) - com.nxp.mcuxpresso.tools.win32 (11.9.0.202307121226) - com.nxp.mcuxpresso.tools.wizards (11.9.0.202307121226) - com.nxp.mcuxpresso.trace.core (11.9.0.202401051536) - com.nxp.mcuxpresso.trace.core.linkserver (11.9.0.202307261153) - com.nxp.mcuxpresso.trace.ui (11.9.0.202401050803) - com.nxp.mcuxpresso.zephyrrtos.docs (11.9.0.202307121226) - com.nxp.swtools.clocks (13.0.0.202401041031) - com.nxp.swtools.clocks.model (13.0.0.202401041031) - com.nxp.swtools.clocks.swt (12.0.0.202401041031) - com.nxp.swtools.common.ui.utils (1.5.0.202401041031) - com.nxp.swtools.common.ui.utils.swt (1.2.0.202401041031) - com.nxp.swtools.common.utils (1.2.0.202401041031) - com.nxp.swtools.configuration (1.7.0.202401041031) - com.nxp.swtools.core (15.0.0.202401041031) - com.nxp.swtools.core.service (15.0.0.202401041031) - com.nxp.swtools.dashboard (1.0.0.202401041031) - com.nxp.swtools.databinding (1.4.0.202401041031) - com.nxp.swtools.dcd.model (2.0.0.202401041031) - com.nxp.swtools.dcdx (4.0.0.202401041031) - com.nxp.swtools.dcdx.swt (1.0.0.202401041031) - com.nxp.swtools.derivative (1.0.0.202401041031) - com.nxp.swtools.derivative.rcp (1.0.0.202401041031) - com.nxp.swtools.doc.mcux.ide (1.0.0.202401041031) - com.nxp.swtools.docannotations (1.0.0.202401041031) - com.nxp.swtools.eclipse (1.1.0.202401041031) - com.nxp.swtools.expert (1.1.0.202401041031) - com.nxp.swtools.framework (4.1.0.202401041031) - com.nxp.swtools.icons (1.0.0.202401041031) - com.nxp.swtools.icons.standard (1.0.0.202401041031) - com.nxp.swtools.mcuxpressoide.adapter (1.0.0.202401041031) - com.nxp.swtools.mcuxpressoide.addons (1.0.0.202401041031) - com.nxp.swtools.mux (15.0.0.202401041031) - com.nxp.swtools.mux.swt (13.0.0.202401041031) - com.nxp.swtools.periphs (14.0.0.202401041031) - com.nxp.swtools.periphs.controller (14.0.0.202401041031) - com.nxp.swtools.periphs.gui (14.0.0.202401041031) - com.nxp.swtools.periphs.gui.swt (14.0.0.202401041031) - com.nxp.swtools.periphs.model (14.0.0.202401041031) - com.nxp.swtools.plu (3.0.0.202401041031) - com.nxp.swtools.rcp.analytics (1.0.0.202401041031) - com.nxp.swtools.resourcetables (14.0.0.202401041031) - com.nxp.swtools.sdkmanifest (1.0.0.202401041031) - com.nxp.swtools.sdkproject (5.0.0.202401041031) - com.nxp.swtools.sharedconfiguration (1.2.0.202401041031) - com.nxp.swtools.snippets (1.0.0.202401041031) - com.nxp.swtools.tee.controller (6.0.0.202401041031) - com.nxp.swtools.tee.gui (6.0.0.202401041031) - com.nxp.swtools.tee.model (6.0.0.202401041031) - com.nxp.swtools.tutorial (1.0.0.202401041031) - com.nxp.swtools.ui.inspector (13.0.0.202401041031) - com.nxp.swtools.ui.inspector.graphical (14.0.0.202401041031) - com.nxp.swtools.ui.targetcpu (14.0.0.202401041031) - com.nxp.swtools.ui.views (13.0.0.202401041031) - com.nxp.swtools.utils (1.1.0.202401041031) - com.nxp.swtools.utils.swt (1.1.0.202401041031) - com.nxp.swtools.validation (1.2.0.202401041031) - com.nxp.mcuxpresso.sdk.sdk_2.x_lpcxpresso54s018m (2.15.0.201911251446) Re:MCUXpresso 11.9のConfigToolsが使い物にならないほど遅い ありがとうレオ、 投稿して数分後に見つけました。今は正常に動作します。 よろしくお願いいたします。 Rainer Re:MCUXpresso 11.9のConfigToolsが使い物にならないほど遅い Hi, 私たちの製品に興味を持ち、コミュニティをご利用いただき、誠にありがとうございます。 Config Tools のパフォーマンスに関する問題はすでに報告されており、バージョン 11.9.1 で修正されています。MCUXpresso v11.9.1をご利用ください。 お役に立てば幸いです。 よい一日を!
View full article
Eink 显示面板的抖动实现 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Eink D 的 抖动 实现 显示面板 作者:Daiyu Ko,飞思卡尔 去抖 a.数字图像处理中的抖动 抖动 是 计算机图形学 中使用的一种技术,用于在具有有限 调色板 ( 颜色量化 )的图像中创建 颜色 深度的错觉。在抖动图像中,调色板中不可用的颜色通过可用调色板内的彩色像素的扩散来近似。人眼将漫射视为其中颜色的混合(参见色彩视觉)。抖动图像,特别是颜色相对较少的图像,通常可以通过特征颗粒感或斑点外观来区分。 图 1.原始照片;注意细节的平滑度 http://en.wikipedia.org/wiki/File:Dithering_example_undithered_web_palette.png 图 2. 使用 Web 安全色板 且未应用抖动效果的 原始图像 。请注意大片平坦区域和细节损失。 http://en.wikipedia.org/wiki/File:Dithering_example_dithered_web_palette.png 图 3.使用带有Floyd–Steinberg 抖动的网页安全调色板的原始图像。 请注意,即使使用相同的调色板,抖动的应用也能更好地表示原始图像 b.应用 显示硬件,包括早期的计算机 视频适配器 和许多用于 移动电话 和廉价 数码相机 的现代 液晶显示器 ,显示的色彩范围比更先进的显示器要小得多。抖动的一个常见应用是更准确地显示包含比硬件能够显示的更大颜色范围的图形。例如,可以使用抖动来在一次只能显示 256 种颜色的视频硬件上显示包含数百万种颜色的摄影图像。256 种可用颜色将用于生成原始图像的抖动近似值。如果不进行抖动,原始图像中的颜色可能会被简单地“四舍五入”为最接近的可用颜色,从而导致新图像无法很好地表现原始图像。抖动利用了人眼倾向于“混合”两种彼此靠近的颜色的倾向。 对于Eink面板,由于它只是灰度图像,我们可以使用抖动算法将灰度级别降低到仅为黑/白,但仍然可以获得更好的视觉效果。 c.算法m 有几种 用于执行抖动的 算法 。最早且至今仍最流行的算法之一是 1975 年开发的 Floyd-Steinberg 抖动 算法。该算法的优势之一是它通过 误差扩散 过程最大限度地减少视觉伪影;与简单的抖动算法相比,误差扩散算法通常能够生成更接近原始图像的图像。 (原来的) THRESHOLD 拜耳(订购)                                     示例(误差扩散): 误差扩散抖动是一种将量化误差扩散到相邻像素的反馈过程。 Floyd-Steinberg抖动仅将误差扩散至相邻像素。这会产生非常细粒度的抖动。 贾维斯、朱迪斯和宁克抖动还会将误差扩散到更远一步的像素。抖动效果更粗糙,但视觉伪影更少。它比Floyd-Steinberg抖动速度慢,因为它将误差分布在 12 个相邻像素中,而不是 Floyd-Steinberg 的 4 个相邻像素中。 Stucki抖动基于上述抖动,但速度略快。其输出往往干净利落。 弗洛伊德-斯坦伯格 Jarvis,   Judice & Ninke 施图基                         误差扩散抖动(续): Sierra 抖动基于 Jarvis 抖动,但速度更快,同时产生类似的结果。 精简版滤镜是 Sierra 的一种算法,比 Floyd–Steinberg 算法简单得多、速度快得多,同时仍能产生相似的(根据 Sierra 的说法,更好)结果。 Atkinson 抖动技术 由 Apple 程序员 Bill Atkinson 开发 , 类似于 Jarvis 抖动和 Sierra 抖动,但速度更快。另一个 区别在于,它不会扩散全部量化误差,而只会扩散四分之三。Atkinson 抖动技术往往能很好地保留细节,但非常亮和暗的区域可能会出现过度曝光。 塞拉 Sierra Lite 阿特金森                         2. Eink显示面板特点 a.分辨率低 Eink仅提供几种显示分辨率模式      杜                  (1 位,黑/白)      GC4                (2位,灰度)      GC16              (4位,灰度)      A2                   (1 位、黑/白、快速更新模式) b.更新时间慢 适用于 800x600 面板尺寸(每帧)      DU                  300ms                              GC4                450毫秒 GC16              600毫秒 A2                   125毫秒 3.3 .对Eink显示面板进行抖动处理的效果 a.低分辨率,视觉质量更好 通过对原始灰度图像进行抖动,我们可以获得更好的视觉效果。即使图像变成黑白图像,通过抖动算法,您仍然会得到灰度图像的感觉。 b.使用Eink 的动画波形更快地更新 由于 DU/A2 模式可以比灰度模式更快地更新Eink面板,通过抖动,我们不仅可以获得更好的视觉效果,而且还可以使用 DU/A2 快速更新模式来显示动画甚至普通视频文件。 4.4 .我们当前的抖动实现 a.选择简单有效的算法 考虑到Eink面板的特点,我们比较了几种抖动算法,决定采用Atkinson抖动算法。它很简单,而且效果更好,特别是对于Eink黑白展示柜。 b.做了大量优化,不会对更新时间造成太大影响 由于Atkinson抖动算法简单,我们还可以投入大量精力进行优化,以减少抖动处理时间并使其在实际应用中切实可行。 c.当前算法性能和结果 目前,采用Atkinson抖动算法,我们的处理时间约为70毫秒。 5. 5.可用性 a.我们采用相同的抖动算法实现了 Y8->Y1 和 Y8->Y4 抖动。 b.使用 i.MX6SL Linux 3.0.35 版本发布实现到我们的 EPDC 驱动程序中。 c.也在我们的Eink演示视频中实现 6. 6.参考文献 a.部分抖动介绍摘自www.wikipedia.org 图形与显示 i.MX6SL Linux 回复:Eink 显示面板的抖动实现 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 是否启用了 Atkinson 锐化滤镜? 使用 HyperDither 实现优质抖动图像 回复:Eink 显示面板的抖动实现 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 这在 i.MX7 中有改变或改进吗?
View full article
i.MX8ULP 从 m33 访问 pbridge2 Hello, 查看 imx8ulp 参考手册中的 i.MX 8ULP 架构图,我们可以看到 PBridge2 是实时域内的 DSP 域的一部分。 我知道 M33 核心没有直接连接到 DSP 域,但我看到交叉开关(XBAR_RTD 和 XBAR_DSP)是连接的;是否可以从 M33 核心访问 DSP 设备? 当我尝试在 DPS 域中使用 LPSPI2 时,尽管按照 examples/evkmimx8ulp/dsp_examples/hello_world_usart 设置了时钟,但 M33 核心还是会挂起/崩溃;因此我假设如果它完全可以访问,那么就必须进行一些操作来映射 cm33 OS 中的 pbridge2 区域。 这里的动机是,imx8ulp 的 IO 比我们之前使用的 SoC 少得多,并且我们希望使用来自 CM33 核心的 LPSPI2 和 LPUART2(均连接到 DSP 域中的 pbridge2) 谢谢! Dominique 回复:i.MX8ULP 从 m33 访问 pbridge2 对于其他关注此事的人来说,在查看此示例后,我们能够访问LPSPI1: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Test-LPUART2-DSP-domain-on-i-MX8ULP-M33/ta-p/2084372 (回顾我的差异,我猜我错过了对 Fusion_Init() 的调用?我们还花了很长时间才弄清楚如何正确挂起(深度睡眠),执行 Fusion_Deinit() 以及在恢复后重置 trdc,但最终一切都解决了) 谢谢! 回复:i.MX8ULP 从 m33 访问 pbridge2 谢谢〜我会再试一次! 回复:i.MX8ULP 从 m33 访问 pbridge2 是的,GPIO(PTA~PTC)都可以从 CM33 中使用;您只需要将 pinmux 设置为 GPIO。 回复:i.MX8ULP 从 m33 访问 pbridge2 好的,谢谢!我想测试 LPUART2 环回,所以我尝试将 RX 和 TX 作为 gpio 环路进行测试。但它不起作用。我想确认即使LPUART2 在 DSP 域中,CM33 也可以控制引脚,对吗? 回复:i.MX8ULP 从 m33 访问 pbridge2 我们放弃了这个,并为 SPI 实现了 gpio 位破解,而不是使用 LPSPI2。我仍然相信理论上这是可能的,但我只是不明白为什么 TRDC 配置不起作用。 如果您找到解决方案,我最终仍然会感兴趣,因为位拆解比 LPSPI 更慢/效率更低,但这不是目前的优先事项。 谢谢! 回复:i.MX8ULP 从 m33 访问 pbridge2 你好!你现在能驱动 Pbrigde2 外设吗? 我在void BOARD_SetTrdcGlobalConfig()中添加了一些配置,但结果是 LPUART2[ PCC_REG( kCLOCK_Lpuart2) ] 的寄存器为 0。这意味着外围设备不存在…… 回复:i.MX8ULP 从 m33 访问 pbridge2 Hi @daisukemizobuch  正如我在另一个案例中所说的那样,我们无法控制 dsp 核心之外的模块资源。 此致 志明 回复:i.MX8ULP 从 m33 访问 pbridge2 嗨@Zhiming_Liu ; 谢谢。期待您的回复。 此致 米佐 回复:i.MX8ULP 从 m33 访问 pbridge2 Hi @daisukemizobuch  @martinetd  让我花点时间来测试一下。 此致 志明 回复:i.MX8ULP 从 m33 访问 pbridge2 嗨@Zhiming_Liu ; 这方面有新的消息吗?如果您有任何新信息,我将非常感激。 此致 米佐 回复:i.MX8ULP 从 m33 访问 pbridge2 嗨@Zhiming_Liu ; 谢谢您的回复,很抱歉回复得这么慢。 我不确定我们是否同意我在这里所做的事情。 dsp_pdm_sai 示例 (examples/evkmimx8ulp/dsp_examples/pdm_sai) 当然控制 PDM,但它是从 dsp/main_dsp.c 控制的它运行在DSP核上,启动DSP核之后M33核不做任何事情。 我正在尝试直接从 M33 核心访问 DSP 外设,而无需启动 DSP 核心(我没有使用 XCC 修改或构建 DSP 图像的许可证,因此使用邮箱从 M33 控制 DSP 核心也不是解决方案)。 dsp pdm_sai 示例也完全没有从通用板配置修改 TRDC (MRC/MBC)。 我尝试向 TRDC Mbc 添加更多块,但没有成功。我尝试查看 trdc 示例(examples/evkmimx8ulp/driver_examples/trdc),看起来访问 PCC2->PCC_LPSPI2(0x2810_2034)时没有出现故障,但如果该寄存器为 0,LPSPI2 就无法工作。 我已附上我在 trdc 示例中尝试过的补丁,这是我按照您的建议设置 MDC 后(针对 PCC2 块)打印 PCC2->PCC_LPSPI2(以及用于健全性检查的 LPSPI1)得到的输出 TRDC example start other init XXXXXXX LPSPI1 80000000 @ 280300fc ; LPSPI2 0 @ 28102034 Set the MRC selected memory region not accessiable Violent MRC access at address: 0x40000000 The MRC selected region is accessiable now Set the MBC selected memory block not accessiable Violent MBC access at address: 0x28800000 The MBC selected block is accessiable now TRDC example Success 如果您能给我指明正确的方向,我将不胜感激。 谢谢! Dominique 回复:i.MX8ULP 从 m33 访问 pbridge2 Hi 请添加另一个 mbcidx 来映射 pcc2。dsp_pdm_sai 是一个很好的例子,展示了如何从 M33 控制 pdm(dsp 域)。 mbcBlockConfig.memoryBlockIdx = 2U;//PCC2 TRDC_MbcSetMemoryBlockConfig(TRDC, &mbcBlockConfig); 此致 志明 回复:i.MX8ULP 从 m33 访问 pbridge2 谢谢你的域名,我错过了。 不幸的是,当我尝试通过 LPSPI2 发送消息时,m33 核心仍然挂起。 我仔细查看了它挂起的位置, LPSPI_MasterTransferReadDataInFifoNoBuf()挂起,因为LPSPI_GetStatusFlags(LPSPI2)从未从 0 改变。 先说一下,在LPSPI_MasterTransferBlocking()的开头,我正在使用的示例(examples/evkmimx8ulp/driver_examples/lpspi/polling_b2b_transfer/master)已经调用了LPSPI_MasterInit() ,所以 LPSPI2->CR 应该是 1(启用),但事实并非如此;即使在LPSPI_Enable(base, true)之后它仍然保持在 0 所以我不确定我的问题是否出在 TRDC/MBC 上(如果是 MBC,我预计对 LPSPI2 寄存器的任何访问都会挂起或重置控制器,但事实并非如此——或者它只是忽略任何写入的内容,如果访问设置不正确,则始终返回 0?) 再往前追溯,PCC2 内存映射似乎没有映射? 手册说 PCC2 基地址:2810_2000h / PCC_LPSPI2 偏移量为 34h,如果存在(PR 位),则应至少包含 8000_0000h,但它为 0。(同时,2803_00FCh 处的 PCC_LPSPI1 此时包含 9200_0000h) 另一方面,我也没有看到任何明确映射 PCC0(2803_0000h)的东西,所以我不确定这里需要什么。 您觉得怎么样?我是否遗漏了 TRDC 设置之前(或之后)的其他内容? 谢谢! 回复:i.MX8ULP 从 m33 访问 pbridge2 Hi board.h 中有 TRDC_M33_DOMAIN_ID,你可以使用它。 /* non secure state can access LPSPI2(T-MBC3) for M33 */ mbcBlockConfig.memoryAccessControlSelect = TRDC_MBC_ACCESS_CONTROL_POLICY_ALL_INDEX; mbcBlockConfig.nseEnable = true; mbcBlockConfig.mbcIdx = 3U; mbcBlockConfig.domainIdx = TRDC_M33_DOMAIN_ID; mbcBlockConfig.slaveMemoryIdx = 0U; mbcBlockConfig.memoryBlockIdx = 13; TRDC_MbcSetMemoryBlockConfig(TRDC, &mbcBlockConfig); 参考 pdm_sai dsp 演示,我们需要从 PBRIDGE2 内存映射中获取 memoryBlockIdx。对于LPSPI2,memoryBlockIdx应该是13 此致 志明 回复:i.MX8ULP 从 m33 访问 pbridge2 抱歉重复更新,补丁实际上已附加... 回复:i.MX8ULP 从 m33 访问 pbridge2 你好@Zhiming_Liu 谢谢您的回复! 查看参考手册,就我而言,我想从 m33 访问 pbridge2 设备,因此我发现 MBC3 控制 Pbridge2 的 18 个 4k 块; (我不太确定TRDC_GetMbcHardwareConfig(TRDC, &mbcHwConfig, 3, 0) (以及更高的从属设备)是否都返回mbcHwConfig.blockNum=0;所以也许我遗漏了一些先决条件?但话又说回来,它不需要域名,所以我认为我没有正确理解这一点......) 忽略上述内容并根据手册,我尝试将对 TRDC_MBC_ACCESS_CONTROL_POLICY_ALL_INDEX + nseEnabled 的访问权限设置为所有域(域 0-7、从属 0、块 0-2),虽然这似乎没有失败,但也无济于事,我的 m33 程序在访问 LPSPI2 时仍然会挂起/崩溃 (我还删除了在 board.c 中找到的对 MBC3 的任何其他引用;并且还根据 dsp 示例在 Pcc2 上选择一个时钟,以便 pbridge2 进行设置) 我已附加适用于https://github.com/NXPmicro/mcux-sdk的差异b565979c2155efc49ffcc8cdaa1f932e19a4d0e5 和https://github.com/nxp-mcuxpresso/mcux-sdk-examplesfc18ff0c12ba90fe71714eaa4244717efa18c61c 你知道缺少了什么吗? 回复:i.MX8ULP 从 m33 访问 pbridge2 Hi 您需要在BOARD_SetTrdcGlobalConfig 中设置 MBC 策略,引用 pbridge1,使用 domainIdx 来控制哪个域可以访问它。   ..... /* for DMA1, USB0, USB1, ENET, UDSHC0, USDHC1, UDSHC2, CAMM Master(default domain id is 1), default TRDC * configuration */ /* non secure state can access Pbridge1(MBC2_MEM1) for DMA1, USB0, USB1, ENET, UDSHC0, USDHC1, UDSHC2, CAMM * Master */ mbcBlockConfig.memoryAccessControlSelect = TRDC_MBC_ACCESS_CONTROL_POLICY_ALL_INDEX; mbcBlockConfig.nseEnable = true; /* non secure state can access the block for DMA1, USB0, USB1, ENET, UDSHC0, USDHC1, UDSHC2, CAMM Master */ mbcBlockConfig.mbcIdx = 2U; /* MBC2 */ mbcBlockConfig.domainIdx = 1U; /* MBC2_DOM1 */ mbcBlockConfig.slaveMemoryIdx = 1U; /* MBC2_DOM1_MEM1 */ TRDC_GetMbcHardwareConfig(TRDC, &mbcHwConfig, mbcBlockConfig.mbcIdx, mbcBlockConfig.slaveMemoryIdx); for (n = 0U; n < mbcHwConfig.blockNum; n++) { mbcBlockConfig.memoryBlockIdx = n; /* MBC2_DOM1_MEM1_BLK_CFG_Wx */ TRDC_MbcSetMemoryBlockConfig(TRDC, &mbcBlockConfig); } .... /* non secure state can access PCC1(PBridge1 slot 17) and ADC1(PBridge1 slot 34) for cortex-A35 */ mbcBlockConfig.memoryAccessControlSelect = TRDC_MBC_ACCESS_CONTROL_POLICY_ALL_INDEX; mbcBlockConfig.nseEnable = true; /* non secure state can access the block for cortex-A35 */ mbcBlockConfig.mbcIdx = 2U; /* MBC2 */ mbcBlockConfig.domainIdx = 7U; /* MBC2_DOM7 */ mbcBlockConfig.slaveMemoryIdx = 1U; /* MBC2_DOM7_MEM1 */ mbcBlockConfig.memoryBlockIdx = 17U; /* MBC2_DOM7_MEM1_BLK_CFG_W17 */ TRDC_MbcSetMemoryBlockConfig(TRDC, &mbcBlockConfig); mbcBlockConfig.memoryBlockIdx = 34U; /* MBC2_DOM7_MEM1_BLK_CFG_W34 */ TRDC_MbcSetMemoryBlockConfig(TRDC, &mbcBlockConfig); .... 此致 志明
View full article