2301257_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2301257_en-US

2301257_en-US

MCX Lab Expansion Boards

MCX Lab: Expansion Boards

 

The MCX Lab is supported by multiple NXP-designed expansion boards that can be connected to FRDM-MCXN947 board. The expansion boards are useful for introductory labs, featuring combination of buttons, joystick, DIP switch, rotary encoder, LED ring, potentiometer, IR sensors, OLED display, and more.

FRDM-TEACH


The FRDM-TEACH provides combination of buttons, switches, LEDs, potentiometer, rotary encoder, RTC and square wave generator:

  • 4x buttons
  • 2x4 DIP switches
  • 5x Jumpers
  • LED bar with 10x LEDs
  • RGB LED
  • External GPIO circuit with LEDs
  • Real-time circuit
  • Square wave generator
  • Temperature sensor
  • Potentiometer
  • Rotary encoder with pushbutton
  • Arduino compatible connectors
Lukas_Heczko_0-1769514045075.png Lukas_Heczko_1-1769514070515.png

The FRDM-TEACH is used in Basic laboratory assignments for FRDM-MCXN947. See MCX Lab Educational Materials page for more.

MCXN947-SHD-OLED


The MCXN947-SHD-OLED provides combination of buttons, switches, LEDs, OLED, potentiometer, rotary encoder and multiple sensors:

  • 4x buttons
  • 8x DIP switches
  • 5 position tactile switch
  • 8x LEDs in ring configuration
  • OLED 128 x 64 display
  • Potentiometer
  • Rotary encoder
  • Light sensor
  • Humidity and temperature sensor
  • Thermistor
  • IR receiver
  • Arduino compatible connectors
Lukas_Heczko_1-1769511255109.pngLukas_Heczko_2-1769511262647.png

LCD-PAR-S035


The LCD-PAR-S035 is a 3.5” 480x320 IPS TFT LCD module with wide viewing angle and 5-point capacitive touch functionality that we recommend to use with the FRDM-MCXN947 board.

See also LCD-PAR-S035 homepage.


Lukas_Heczko_3-1769514364128.png


Expansion Board Hub


Explore the Expansion Board Hub for more modules with sensors, actuators, interfaces, displays, wireless modules etc.

Tags (1)
No ratings
Version history
Last update:
‎01-27-2026 09:05 AM
Updated by: