Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
使用 JLINK 编程后 LPC1778 无法连接 你好使用 J-Link 调试器对 LPC1778 芯片编程后,无法连接目标芯片。我拥有的两个不同的电路板上也发生了同样的故障。 我确认问题不是由程序代码引起的。我编程的数据是全芯片随机值,使用不同的编程工具对完全相同的随机数据集进行编程不会产生这种连接问题。 初始连接和编程过程正常完成,没有任何错误提示。在对主板进行编程后重新通电后,与硬件的所有通信都将失败。连接日志如下: 正在连接... -通过 USB 连接到探头/编程器设备 0 -探测器/编程器固件:J-Link V9 编译于 2021 年 5 月 7 日 16:26:12 -探针/编程器 S/N:69401860-设备 " LPC1778 " 已选择。 - 目标接口速度:4000 kHz(固定) - VTarget = 3.283V - 连接 CPU 失败。正在RESET下尝试连接。 - 错误:连接失败。 无法与目标建立连接。 一般故障排除指南:https://kb.segger.com/J-Link_Troubleshooting - ERROR:连接失败 此外,我使用逻辑分析器捕获波形,SWD 接口的 DP 端口工作正常,而所有 AP 访问都会导致 ACK FAULT 响应。 LPC17xx Re: LPC1778 can't connect after programming by JLINK 你好@边浩鹏1 请先在您的开发板上下载并运行一个简单的 “Hello World” 项目,而不是使用随机值,然后测试调试是否正常运行。 如果调试仍然无法正常工作,请参考带有 CMSIS DAP 探头的 LPC1769 LPCXpresso 板来检查您的原理图设计 | NXP 半导体 如果问题仍然存在,请随时与我联系。 BR 爱丽丝
View full article
MCXN947: how assign CMC0 to secure privileged mode The RM indicates it should be set to Secure and Privileged and that I can use the AHBSC register to do this. The SRM says the AHBSC register does not affect the privilege status of the CMC0 register So how do I examine/ change the security level if this register? MCXN Re: MCXN947: how assign CMC0 to secure privileged mode Hi @ClarkS  There is a training session on how to configure TrustZone. Please refer to it here: TrustZone configuration training Learn how to create a secure/nonsecure application and debug on a secure Cortex M33 NXP device.   Thank you.   BR Alice Re: MCXN947: how assign CMC0 to secure privileged mode Thank you for this, Alice. I didn’t know of this article. I’ll study it.  Re: MCXN947: how assign CMC0 to secure privileged mode Turns out this was just a collection of slides from an old presentation. I did not see any reference to the CMC peripheral.  The slides did remind me to check the Config Tools app so I downloaded the most recent version. Inspection of the Tee tool did not find the CMC0 register at all.  So how do I determine the security level of  this peripheral and especially the SRS and SSRS registers.  Also the RM should probably be updated since the note in it to use the AHBSC register to configure its permissions appears to be incorrect. Re: MCXN947: how assign CMC0 to secure privileged mode Hello @ClarkS  There is some confusion in the documentation. I have escalated it to  internall team and will share any updates with you. Thank you.   BR Alice Re: MCXN947: how assign CMC0 to secure privileged mode Thank you, Alice. Looks like it defaults to SECURE / PRIVILEGED like I hoped it was. I appreciate getting the SRM updated! Re: MCXN947: how assign CMC0 to secure privileged mode Hi @ClarkS  Thanks for your patience.  CMC access permission is controlled by AHBSC AIPS_BRIDGE_GROUP0_MEM_RULE1[1:0]. This will be fixed in the next version of RM. Thank you. BR Alice Thank you. 
View full article
FreeMASTER S32K344-WB用のSimulinkモデルを作成し、LEDを1秒ごとに点滅させるようにしました。その後、ELFファイルをFreeMASTERにインポートし、J-Linkを介して波形を監視しました。しかし、 「Go」をクリックした後、FreeMASTERオシロスコープの信号レベルは平坦な線のままで、変化しませんでした。基板上の物理的なリセットボタンを押すと、LEDは正常に点滅し始めたが、FreeMASTERの波形表示は一時停止した。MCUがLEDを連続的に点滅させながら正常に動作している状態で、FreeMASTERオシロスコープで波形を観測するには、どのように設定すればよいでしょうか? Re: freemaster こんにちは、 まず、返信が遅くなり申し訳ありません。 FreeMASTERがすでに基板に接続されている状態で評価ボードをリセットした場合、FreeMASTER接続を停止して再起動しなければなりません。そうしないと、詰まってしまうでしょう。 あなたが実現したいことを実現する一つの方法は、LEDの状態をデータストアメモリに保存することです。NOT演算を適用し(LOW→HIGHとHIGH→LOWの間で変更するため)、その値をDio_WriteChannelに渡します。こうすることで、データストアメモリを揮発性または外部にマークしてFreeMASTERプロジェクトに読み込めます。 DIOチャネルの読み書き操作を行いたいなら、ピンをINOUTに設定する必要があります(S32CTのPinsタブ)。 よろしくお願いします、 ソリン・バンシラ
View full article
IMX8MP 内联 ECC 亲爱的恩智浦技术支持团队 我目前正在尝试在 IMX8MP 上使用 Inline ECC 功能(按照 AN13566.pdf 和https://community.nxp.com/t5/NXP-Tech-Blog/xxx中的步骤操作)。 ). 根据 IMX8MPRM.pdf 第 9.2.5.1.20.3 节、我尝试将 ecc_region_parity_lock 设置为解锁。 我修改了 lpddr4_timing.c 的内容,将 0x3d400074 寄存器的值设置为 0x780。 struct dram_cfg_param ddr_ddrc_cfg[] = { {0x3d400304, 0x1}, {0x3d400030, 0x1}, {0x3d400000, 0xa3080020}, {0x3d400020, 0x1323}, {0x3d400024, 0x1e84800}, {0x3d400064, 0x7a0118}, {0x3d400070, 0x070277D4}, {0x3d400074, 0x780}, ...... 但是,通过 memtool 工具读取的寄存器值是 0x790。 root@imx8mp-lpddr4-evk:~# /unit_tests/memtool 0x3d400074 1 E Reading 0x1 count starting at address 0x3D400074 0x3D400074: 00000790 我想知道如何正确配置这个寄存器。 提前感谢您的支持。 Re: IMX8MP Inline ECC 感谢您的支持 Re: IMX8MP Inline ECC 你好@James33 请分享您修改后的 RPA 文件。 B.R Re: IMX8MP Inline ECC Hi @James33  你是自己手动修改的寄存器的值吗? B.R Re: IMX8MP Inline ECC 你好 Re: IMX8MP Inline ECC lpddr4_timing.c 文件由 DDR 工具生成( * 代码由 DDR 工具 v4.0.0_10-1eade933a 生成)。该寄存器的默认值为 0x790。根据 AN13566 第 3.2.3 节的描述、我想访问 ECC 奇偶校验区,因此手动将其改为 0x780,但没有成功。 /* * Copyright 2026 NXP * * SPDX-License-Identifier: BSD-3-Clause * * Code generated with DDR Tool v4.0.0_10-1eade933a. * DDR PHY FW2020.06 * Part number: NXP LPDDR4 EVK board's default DDR part */ #include #include /* Initialize DDRC registers */ struct dram_cfg_param ddr_ddrc_cfg[] = { {0x3d400304, 0x1}, {0x3d400030, 0x1}, {0x3d400000, 0xa3080020}, {0x3d400020, 0x1323}, {0x3d400024, 0x1e84800}, {0x3d400064, 0x7a0118}, {0x3d400070, 0x7027fd4}, {0x3d400074, 0x790}, {0x3d4000d0, 0xc00307a3}, {0x3d4000d4, 0xc50000}, {0x3d4000dc, 0xf4003f}, {0x3d4000e0, 0x330000}, {0x3d4000e8, 0x660048}, {0x3d4000ec, 0x160048}, {0x3d400100, 0x2028222a}, {0x3d400104, 0x8083f}, {0x3d40010c, 0xe0e000}, {0x3d400110, 0x12040a12}, {0x3d400114, 0x2050f0f}, {0x3d400118, 0x1010009}, {0x3d40011c, 0x502}, {0x3d400130, 0x20800}, {0x3d400134, 0xe100002}, {0x3d400138, 0x120}, {0x3d400144, 0xc80064}, {0x3d400180, 0x3e8001e}, {0x3d400184, 0x3207a12}, {0x3d400188, 0x0}, {0x3d400190, 0x49f820e}, {0x3d400194, 0x80303}, {0x3d4001b4, 0x1f0e}, {0x3d4001a0, 0xe0400018}, {0x3d4001a4, 0xdf00e4}, {0x3d4001a8, 0x80000000}, {0x3d4001b0, 0x11}, {0x3d4001c0, 0x1}, {0x3d4001c4, 0x1}, {0x3d4000f4, 0x799}, {0x3d400108, 0x9121b1c}, {0x3d400200, 0x14}, {0x3d400208, 0x0}, {0x3d40020c, 0x14141400}, {0x3d400210, 0x1f1f}, {0x3d400204, 0x50505}, {0x3d400214, 0x4040404}, {0x3d400218, 0x4040404}, {0x3d40021c, 0xf0f}, {0x3d400250, 0x1705}, {0x3d400254, 0x2c}, {0x3d40025c, 0x4000030}, {0x3d400264, 0x900093e7}, {0x3d40026c, 0x2005574}, {0x3d400400, 0x111}, {0x3d400404, 0x72ff}, {0x3d400408, 0x72ff}, {0x3d400494, 0x2100e07}, {0x3d400498, 0x620096}, {0x3d40049c, 0x1100e07}, {0x3d4004a0, 0xc8012c}, {0x3d402020, 0x1021}, {0x3d402024, 0x30d400}, {0x3d402050, 0x20d000}, {0x3d402064, 0xc001c}, {0x3d4020dc, 0x840000}, {0x3d4020e0, 0x330000}, {0x3d4020e8, 0x660048}, {0x3d4020ec, 0x160048}, {0x3d402100, 0xa040305}, {0x3d402104, 0x30407}, {0x3d402108, 0x203060b}, {0x3d40210c, 0x505000}, {0x3d402110, 0x2040202}, {0x3d402114, 0x2030202}, {0x3d402118, 0x1010004}, {0x3d40211c, 0x302}, {0x3d402130, 0x20300}, {0x3d402134, 0xa100002}, {0x3d402138, 0x1d}, {0x3d402144, 0x14000a}, {0x3d402180, 0x640004}, {0x3d402190, 0x3818200}, {0x3d402194, 0x80303}, {0x3d4021b4, 0x100}, {0x3d4020f4, 0x599}, {0x3d403020, 0x1021}, {0x3d403024, 0xc3500}, {0x3d403050, 0x20d000}, {0x3d403064, 0x30007}, {0x3d4030dc, 0x840000}, {0x3d4030e0, 0x330000}, {0x3d4030e8, 0x660048}, {0x3d4030ec, 0x160048}, {0x3d403100, 0xa010102}, {0x3d403104, 0x30404}, {0x3d403108, 0x203060b}, {0x3d40310c, 0x505000}, {0x3d403110, 0x2040202}, {0x3d403114, 0x2030202}, {0x3d403118, 0x1010004}, {0x3d40311c, 0x302}, {0x3d403130, 0x20300}, {0x3d403134, 0xa100002}, {0x3d403138, 0x8}, {0x3d403144, 0x50003}, {0x3d403180, 0x190004}, {0x3d403190, 0x3818200}, {0x3d403194, 0x80303}, {0x3d4031b4, 0x100}, {0x3d4030f4, 0x599}, {0x3d400028, 0x0}, }; 谢谢您的答复。 Re: IMX8MP Inline ECC Hello!!
View full article
BMA7318ファームウェアドライバ 当社は、BESS市場向けに高電圧BMS(バッテリー管理システム)とバッテリーパックを開発しています。ソフトウェア開発やBMS7318を使用したその他のサンプルコードのために、BMA7318ファームウェアドライバはどこでダウンロードできますか?NXPとは既に秘密保持契約を結んでいますか? Re: BMA7318 Firmware Drivers こんにちは、トーマスさん。 BMA7318ドライバはBMS SDKの「Lite SDK」バージョンに含まれているようです。しかし、「ダウンロード」を見てもLite SDKが見当たりません。 Re: BMA7318 Firmware Drivers こんにちは、 BMA7318のファームウェアドライバおよびサンプルソフトウェアについては、BMS SW SDKを参照してください。このSDKには、BMA7xxxシリーズを含むすべてのBCCデバイス向けの製品グレードのドライバとリファレンス実装が含まれています。 https://www.nxp.com/design/design-center/software/embedded-software/nxp-battery-management-software-development-kit-and-toolchain:BMS-SW   BRs、トーマス   Re: BMA7318 Firmware Drivers こんにちは、トーマスさん。 試してみましたが、そのリンクをクリックすると私のプロフィールページに移動します。成功しませんでした。 ありがとうございます ナガ Re: BMA7318 Firmware Drivers こんにちは、 NXPソフトウェアアカウントをご利用の場合は、以下のリンクからダウンロードしてみてください。 BMS Light SDK AUTOSAR 4.4 R21-11 バージョン 0.8.0 CD02 BRs、トーマス
View full article
i.MXRT1052 VDD_SOC_IN電圧 1V1 当社は、i.MX RT1052クロスオーバーMCUを使用した独自の基板を開発しました。基板に12Vを印加すると、MCUのDCDC_INピンとVDD_SNVS_INピンには3.3Vが到達しますが、DCDC_LPピンには1.1Vが生成されません。また、MCUにファームウェアをダウンロードすることもできません。なぜこのようなことが起きているのか? DCDC_LPピンで1.1Vを生成するにはどうすればよいでしょうか? 回路図とブート設定ファイルを添付しました。 Re: i.MXRT1052 VDD_SOC_IN voltage 1V1 LDOまたはDCDCを追加する必要があるかもしれません。i.MX RT1050評価キットを参照してください。 デモ用デザインですか、それとも顧客プロジェクト用デザインですか? Re: i.MXRT1052 VDD_SOC_IN voltage 1V1 こんにちは、 @bhaveshtirex さん。 NXP MIMXRTシリーズにご関心をお寄せいただきありがとうございます! 回路図を確認しましたが、大きな問題は見つかりませんでした。しかし、どうやらオンチップのDC-DCコンバータが実際には有効になっていないようで、そのためコアに電力が供給されていないようです。 電源投入シーケンスがデータシートの仕様、およびRMの該当セクションに準拠していることを確認してください。 よろしくお願いします、 ギャビン
View full article
VS Code拡張機能のアップデートによりRTOSビューアが壊れました こんにちは、 これまでは、vscode ツール バージョン 1.9.20 (旧バージョン) を使用しており、freertos スレッド (RT1189) の状態を確認するためにhttps://marketplace.visualstudio.com/items?itemName=mcu-debug.rtos-viewsを使用していました。アップデート後、ツールが動作しなくなり、「 RTOS検出が完了しませんでした。次回の停止時に再開されます。」と表示されるだけです。何か解決策はありますか? よろしくお願いします。 Re: VS code extension update broke RTOS viewer こんにちは、 VS Code 用の MCUXpresso には、以前から独自の RTOS ビューアが搭載されています。https://mcuxpresso.nxp.com/mcux-vscode/latest//html/RTOS-Details.htmlをご確認ください。 また、以前の変更点として、拡張機能がMicrosoft C/C++デバッグアダプタからCortex-Debugに基づく独自のデバッグアダプタに移行しました。そのため、新しいデバッグ構成を作成する必要があります。これにより、当社のデバッグアダプタに基づく構成が自動的に作成されます(タイプとして「mcuxpresso-debug」が表示されます)。 追記:Seggerデバッグプローブを使用している場合は、RTOSの**サポート**を有効にするために特別な**イネーブルメント**が必要になりますのでご注意ください( https://mcuxpresso.nxp.com/mcux-vscode/latest//html/Debug-Views.html#enabling-rtos-awarenessを参照)。 よろしくお願いいたします。 クリスティアン Re: VS code extension update broke RTOS viewer はい、解決しました。デバッグモードで-Ogフラグを付けてコンパイルしていたのですが、それを-O0に変更したらビューアが動作するようになりました。しかし、Ogが標準的な編集・デバッグプロセスのデフォルトとなるべきなので、このツールには改善が必要だと思います。 これとは関係ないのですが、デバッグコンソールにもこの警告が表示されます。 「警告: ' \Main.cpp' をホストエンコーディング (CP1252) から UTF-32 に変換できませんでした。」 通常はこのようなことは起こらないはずです。バグ報告を提出してください。 よろしくお願いします。 Re: VS code extension update broke RTOS viewer ありがとうございます 実際には、このメッセージはMCUXpresso RTOSビュー自体から発信されています(私は別のプラグインを誤って参照していました)。 launch.json とカスタムデバイススクリプトを添付しました (Linkserver 26.3.123 の MIMXRT1180-EVK.json と同じです)。しかし、「接続スクリプト」は「RT1180_reset.scp」です。 当社のアプリはハイパーラム上で動作し、SDK 2.16を使用しています。Freertosの変数は正しく設定されています。 アプリのステップデバッグはできますが、RTOSの詳細ビューには依然として「 RTOS検出が完了しませんでした。次の停止時に再開されます。」と表示されます。 よろしくお願いします。 Re: VS code extension update broke RTOS viewer @cristiantepusこの件について何か進展はありますか? Re: VS code extension update broke RTOS viewer 今日、MCUXpresso RTOSビューアがリリースモードでは動作せず、何も表示されないことに気づきました。 しかし、 https://marketplace.visualstudio.com/items?itemName =mcu-debug.rtos-views -Og およびリリースモードでは動作しますが、現在の mcuxpresso vscode プラグインでは動作しません (無効になります)。それを元に戻す方法はありますか? Re: VS code extension update broke RTOS viewer こんにちは、 @arunkumar_g さん。 弊社が提供するRTOS詳細ビューは、ELFファイル内にいくつかのシンボルが存在することを前提としています(例:「 FreeRTOSDebugConfig」、「 pxCurrentTCB」、「 uxCurrentNumberOfTasks」など多数あります。「 RTOS検出が完了しませんでした。次の停止時に再開されます。」というメッセージでは何が問題だったのかが分からないという点には同意します。この点をより明確にするよう努めます。 「デバッグ」と「リリース」で得られた結果についてですが、これはコンパイラ/リンカの最適化の結果だと考えられます。必要なシンボルが削除されているため、利用者はそれらを見つけることができません。この場合、RTOSの詳細ビューが機能しないだけでなく、低レベルのGDB Thread認識(LinkServer、J-Link、PEmicro)でも、コールスタックビューでFreeRTOSタスクを表示およびデバッグできなくなります。この場合、デバッグモードとリリースモードの両方で必要なシンボルが存在するようにコードを更新することをお勧めするしかありません。ドキュメントとツールからの情報を更新し、必要な記号が不足しているためにビューにデータが表示されないことを明確にします。 また、このケースではMCUデバッグRTOSビューが動作しているとおっしゃっていましたが、そうかもしれません。しかし、私が最後に確認した時点では、バージョン管理(バージョンは「 FreeRTOSDebugConfig」を調べることで確認できます)は一切サポートされていませんでした。また、FreeRTOSのデータ構造はRTOSのバージョンに固有のものであることにもご注意ください。MCUデバッグビューを有効にするには、サポート対象リストに「mcuxpresso-debug」デバッグアダプタ(MCUXpresso固有)を追加する方法をメンテナーに問い合わせてください。 古いSDK 2.16をベースにしたプロジェクトを使用しているとのことですので、CMakeとKconfigをベースにした最新のMCUXpresso SDKに切り替えることをお勧めします。   いくつかの便利なリンク: - RTOSの詳細: RTOSの詳細 — MCUXpresso for VS Code 26.04ドキュメント - MCUXpresso SDK: MCUXpresso SDK ドキュメント — MCUXpresso SDK ドキュメント   ありがとうございます エイドリアン
View full article
S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hello, I am working on a customer project with the S32N55 platform and I am facing an issue when calling SetAttribute with HSE_OTP_FOEM_ADKP_ATTR_ID for the first time. --- [Environment] - Platform: S32N55 EVB (Silicon B0) - GrayVIP: 1.0.24 - FSS FW SDK: 1.13.0+ - Current Lifecycle: OEM_OPEN (confirmed via GetAttribute) - ADKP: never provisioned (first attempt) - HSE Timeout: CRYPTO_43_HSE_TIMEOUT_DURATION_U32 = 1,000,000,000 --- [Issue] When calling SetAttribute with HSE_OTP_FOEM_ADKP_ATTR_ID, HSE never returns a response in synchronous mode. Mu_Ip_IsResponseReady() never returns TRUE, resulting in a timeout regardless of the timeout value. Other SetAttribute calls (e.g. HSE_OTP_GO_SECURE_ATTR_ID) work correctly with the same synchronous mechanism. --- [Code] hseSrvDescriptor_t xLocalDesc = {0}; hseSetAttrSrv_t* pSetAttrReq; xLocalDesc.srvId = HSE_SRV_ID_SET_ATTR; pSetAttrReq = &(xLocalDesc.hseSrv.setAttrReq); pSetAttrReq->attrId = HSE_OTP_FOEM_ADKP_ATTR_ID; pSetAttrReq->attrLen = sizeof(hseAttrOtpFoemAdkp_t); /* 32 bytes */ pSetAttrReq->pAttr = Hse_Ip_ToAHBAddress((HOST_ADDR)pAdkpBuf); xHseIpReq.eReqType = HSE_IP_REQTYPE_SYNC; xHseIpReq.u32Timeout = CRYPTO_43_HSE_TIMEOUT_DURATION_U32; hseResp = Hse_Ip_ServiceRequest(u8MuInst, u8MuCh, &xHseIpReq, (hseSrvDescriptor_t *)Hse_Ip_ToAHBAddress( (HOST_ADDR)&g_hseShared.axHseSrvDesc[u8MuInst][u8MuCh])); /* HSE never responds - Mu_Ip_IsResponseReady() always returns FALSE */ --- [Pre-conditions verified before calling SetAttribute] 1. LC is OEM_OPEN (confirmed via GetAttribute) 2. ADKP has never been provisioned on this device 3. ADKP buffer is located in non-cacheable shared memory 4. Address is translated via Hse_Ip_ToAHBAddress() --- [Observation 1 - Async mode] Looking at the GrayVIP reference implementation (Fss_Firmware_ProgSecureFuseADK), SetAttribute for ADKP is called using an asynchronous mechanism with WaitEvent: RetVal = Fss_Sem_SetHseAttribute(&setAttr); if (E_OK == hseResponse) { WaitEvent(FSS_SEM_HSESETATTR_EVENT_NAME); RetVal = Fss_Sem_GetHseAsynResponse(); } This suggests that OTP write operations may require async mode on S32N55 HSE2. --- [Observation 2 - VGPIO Fuse Power Enable] In GrayVIP, Fss_Firmware_FuseProgramming() enables fuse programming power via VGPIO before writing Boot Config fuses: VGPIO_Type *pVgpio = (VGPIO_Type *)FUSE_VDD_EN_PORT_ADDRESS; pVgpio->OV[FUSE_VDD_EN_BANK].PMOS = (1 << FUSE_VDD_EN_PIN); pVgpio->OV[FUSE_VDD_EN_BANK].OE |= (1 << FUSE_VDD_EN_PIN); pVgpio->OV[FUSE_VDD_EN_BANK].OVS = (1 << FUSE_VDD_EN_PIN); However, Fss_Firmware_ProgSecureFuseADK() (ADKP write) does not explicitly call this power enable sequence. It is unclear whether: 1. HSE2 handles fuse power internally for OTP attribute writes, or 2. VGPIO fuse power enable is also required before SetAttribute(ADKP). Additionally, GrayVIP does not include a fuse power disable sequence after the write. We are concerned about whether leaving VGPIO fuse power enabled after the OTP write could cause unintended fuse writes or security issues. --- [Questions] 1. Is synchronous mode (HSE_IP_REQTYPE_SYNC) supported for SetAttribute(ADKP), or is async mode mandatory for OTP write operations on S32N55 HSE2? 2. Is VGPIO fuse programming power enable required before calling SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID)? 3. If VGPIO fuse power enable is required, what is the correct procedure to disable it after the OTP write is complete? 4. Are there any additional prerequisites before calling SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) that may not be documented? This is a critical blocker for our customer project delivery. Any guidance would be greatly appreciated. Thank you. Re: S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hello again @EddiePark, Please find my answers to your questions below: Is synchronous mode (HSE_IP_REQTYPE_SYNC) supported for SetAttribute(ADKP), or is async mode mandatory for OTP write operations on S32N55 HSE2? For What I can understand from the FSS firmware , it is not, as you can see, the Wait and Clear functions calls you mentioned are guarded by the conditional compilation #ifdef FSS_SEM_HSESETATTR_EVENT_NAME. This way you ensure you continue once the request has been processed. Is VGPIO fuse programming power enable required before calling SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID)? No it is not, there are two kinds of one time programmable words handled by the HSE2, one is called fusebox and its handled by the  hseSrvProgFuse_t service, this one requires the VDD_EFUSE to be powered, which is controlled by a GPIO pin and a transistor in the S32N55 RDB. The other kind is usually called just OTP, these do not require the VDD_EFUSE to be powered on, that is why you don't need the GPIO to be turned on. You can check the power domains I am referring to in the reference manual, in particular in Figure 35. FSS power domains [page 241, S32N55 Reference Manual, Rev. 2, 2025-06-30]  If VGPIO fuse power enable is required, what is the correct procedure to disable it after the OTP write is complete? Depends on the board, in the S32N55 RDB it is controlled by the GPIO you see in the code, however, in a custom board that can be a jumper o an 0ohm resistor. Therefore in the RDB you can just turn off the pin and VDD_EFUSE will be powered off, you can also control it with J18, when having a jumper in that connector, VDD_EFUSE will be always ON, independently of the GPIO state. Are there any additional prerequisites before calling SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) that may not be documented? I was not able to find any information that might suggest an unknown prerequisite. Have you been able to use any other HSE2 service successfully?  Please let me know if you have any other question. Note that, as mentioned in the other post, the S32N55 is still a pre-production and thus, my expertise on this topic is not yet at the highest level. With that said, I will try to help you as much as I can. Re: S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hello, We are trying to program the ADKP (Application Debug Key/Password) via HSE2 SetAttribute service on S32N55, but we are not getting any response from HSE2. --- ## Environment - Platform: S32N55 EVB - GrayVIP version: SW32N5_GRAYVIP_1_0_22_0 - FSS FW version: S32N_FSS_FW_R21-11_1.10.0 - EB Tresos version: 29.0.0 - Called from: FSS M7 core, inside Fss_FW_Init_Task() --- ## What We Tried ### Attempt 1: Synchronous mode (HSE_IP_REQTYPE_SYNC) ```c xLocalDesc.srvId = HSE_SRV_ID_SET_ATTR; pSetAttrReq->attrId = HSE_OTP_FOEM_ADKP_ATTR_ID; pSetAttrReq->attrLen = 32U; /* hseAttrOtpFoemKey_t size */ pSetAttrReq->pAttr = Hse_Ip_ToAHBAddress((HOST_ADDR)pAttr); RetVal = Sherpa_Cdd_Execute(&xLocalDesc); /* Sync */ ``` Result: Timeout - no response from HSE2 ### Attempt 2: Asynchronous mode (HSE_IP_REQTYPE_ASYNC_IRQ) ```c g_xSherpaHseIpReq.eReqType = HSE_IP_REQTYPE_ASYNC_IRQ; g_xSherpaHseIpReq.pfCallback = &Sherpa_Cdd_HseCallback; /* Poll bDone flag set by IRQ callback */ while ((FALSE == g_xSherpaCallbackParam.bDone) && (u32Timeout > 0U)) { u32Timeout--; } ``` Result: Timeout - bDone never set to TRUE (callback never called) ### Attempt 3: With VGPIO VDD_EFUSE Power Enable ```c /* Enable VDD_EFUSE via VGPIO */ pVgpio->OV[BANK].PMOS = (1U << PIN); pVgpio->OV[BANK].OE |= (1U << PIN); pVgpio->OV[BANK].OVS = (1U << PIN); ``` Result: ShutdownHook called (bus error on VGPIO register access) --- ## Current Implementation ```c Std_ReturnType SecureDebug_SetADKP(const uint8_t* pDebugKey) { /* 1. Check LC == OEM_OPEN */ eRetVal = Sherpa_Cdd_GetAttribute(HSE_OTP_LIFECYCLE_ATTR_ID, ...); if (HSE_LC_OEM_OPEN != *pLcInSharedMem) { break; } /* 2. Check if ADKP already programmed */ eRetVal = Sherpa_Cdd_GetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID, ...); if (E_OK == eRetVal) { /* Already programmed */ break; } /* 3. Copy 32-byte key to non-cacheable shared buffer */ memcpy(pAdkpInSharedMem, pDebugKey, HSE_OTP_FOEM_KEY_SIZE); __DMB(); __DSB(); /* 4. SetAttribute */ eRetVal = Sherpa_Cdd_SetAttribute( HSE_OTP_FOEM_ADKP_ATTR_ID, HSE_OTP_FOEM_KEY_SIZE, /* 32 bytes */ (void*)pAdkpInSharedMem); } ``` --- ## Questions 1. According to HSE2 Firmware Reference Manual Figure 12, if Input size == 16, HSE treats it as a plain AES-128 key. If Input size != 16, HSE treats it as a key handle. Is the ADKP size for S32N55 HSE2 16 bytes (AES-128) or 32 bytes? 2. Is VDD_EFUSE power (J18 jumper or VGPIO) required for HSE_OTP_FOEM_ADKP_ATTR_ID SetAttribute? (Previous NXP response said it is NOT required for OTP type, only for fusebox type) 3. Is Secure ADKP Provisioning (via RAM key slot + key handle) the recommended approach for S32N55 HSE2? ```c /* Import AES-128 key to RAM slot */ SecureStorage_CipherKey_Import(RAM_SLOT, pDebugKey, 16U); /* SetAttribute with key handle */ Sherpa_Cdd_SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID, sizeof(hseKeyHandle_t), &keyHandle); ``` 4. Is there a prerequisite step (e.g. ADKP_MASTER fuse setting) before programming ADKP that we might be missing? 5. What is the correct MU instance to use for HSE_OTP_FOEM_ADKP_ATTR_ID SetAttribute on S32N55? Re: S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hello @EddiePark, I will need to contact the internal team for a more specialized support about this. I will get back to you once I have an update from them. Thanks in advance for your patience. Re: S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hello @EddiePark, I have received feedback, amazingly fast I must point out. In the release notes for for S32N5 HSE Firmware 1.0.24.0, the following is mentioned: HSE is going in shutdown while setting/getting key related OTP fuse like SRKH/ODAK, ADKP, MCK using SET/GET ATTR for OTP fuse. So, if you are using a version older than 1.0.24.0 this might be the reason for the issue. Please note that I needed to refresh my licenses for the S32N HSE FW to access version 1.0.24.0, so if you cannot already see that version (or newer) in your account you may need to contact your NXP representative to activate it. Please retest with a version 1.0.24.0 or newer and let me know if the behavior changed. Re: S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hi Thank you for your early response. I will test using HSE_FW_S32N5_1_0_24_0. I will get back to you for the result of test Re: S32N55 HSE2 - SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) No Response in Synchronous Mode Hello, Thank you for your previous response regarding HSE_FW_S32N5_1_0_24_0. We have retested with HSE_FW_S32N5_1_0_24_0 and would like to share our results and ask one additional question. --- ## Update 1: ADKP Provisioning Result After upgrading to HSE_FW_S32N5_1_0_24_0, the ADKP provisioning is now working correctly. We confirmed the ADKP is successfully programmed by calling GetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID), which returns E_OK with a SHA3_384 reference value. The previous timeout/shutdown issue (reported in the release notes as a bug in versions older than 1.0.24.0) is now resolved. --- ## Update 2: Call Location We found that the call location also matters. The SetAttribute(HSE_OTP_FOEM_ADKP_ATTR_ID) must be called AFTER Fss_Btm_PlatformApi_SetFssCohortState(FSS_BTM_COHORT_RUNNING). Calling it earlier (e.g. immediately after Crypto_43_HSE_Init) resulted in no response from HSE2. --- ## Question: VDD_EFUSE Power Enable Requirement In our previous NXP Community post, it was stated that: "OTP attributes (HSE_OTP_FOEM_ADKP_ATTR_ID) do NOT require VDD_EFUSE power, unlike fusebox operations (hseSrvProgFuse_t)." However, we would like to reconfirm this, as we attempted to enable VDD_EFUSE via VGPIO and encountered a ShutdownHook (bus error): ```c VGPIO_Type *pVgpio = (VGPIO_Type *)SECURE_DEBUG_FUSE_VDD_ADDR; pVgpio->OV[SECURE_DEBUG_FUSE_VDD_BANK].PMOS = (1U << SECURE_DEBUG_FUSE_VDD_PIN); pVgpio->OV[SECURE_DEBUG_FUSE_VDD_BANK].OE |= (1U << SECURE_DEBUG_FUSE_VDD_PIN); pVgpio->OV[SECURE_DEBUG_FUSE_VDD_BANK].OVS = (1U << SECURE_DEBUG_FUSE_VDD_PIN); ``` Questions: 1. Is VDD_EFUSE power (J18 jumper or VGPIO) truly NOT required for HSE_OTP_FOEM_ADKP_ATTR_ID SetAttribute on S32N55? 2. If VDD_EFUSE is not required, why does ADKP provisioning only work after Fss_Btm_PlatformApi_SetFssCohortState()? Is this a timing/initialization dependency rather than a power supply issue? 3. What is the correct VGPIO address and pin configuration for VDD_EFUSE control on S32N55 EVB, in case it is needed for other OTP operations (e.g. MCK, SRKH)? Thank you.
View full article
S32K1 EEPROM RTD こんにちは、 Eep_Ftfc_Example_S32K144 を使用すると正常に動作する理由がわかりません。 しかし、消去および書き込みコードを削除して、以前に保存されたデータを読み取ろうとすると、「FTFC_EEP_IP_STATUS_BLOCK_INCONSISTENT」というエラーで失敗します。 「デバイスのパーティションを保持する」と「この範囲を保持する」の両方を0x10000000から0x1000ffffに設定しました。 したがって、第2ラウンドのコードは次のとおりです。 /* クロックの初期化 */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* コード0x4のEERAM用に以前にパーティション化されていない場合のみパーティション化する */ Eep_DepartParitition(T_EEEPROM_SIZE); /* Eepドライバを初期化します */ Ftfc_Eep_Ip_Init(&EepFtfcCfg_VS_0); // /* 消去値を書き込むことでメモリを消去します */ // for(i=0; i // // retJobResultType = Ftfc_Eep_Ip_Erase(EEP_ERASE_START_ADD + i, FTFC_EEP_IP_PAGE_LONGWORD, FALSE); // if(FTFC_EEP_IP_STATUS_OK != retJobResultType) // // Exit_Example(FALSE); // 0 を返す; // } // } // // /* 1つ以上の完全なEEPROMページをEEPROMデバイスに書き込みます */ // for(i=0; i // // retJobResultType = Ftfc_Eep_Ip_Write(EEP_ERASE_START_ADD + i, dataWrTestPatt + i, FTFC_EEP_IP_PAGE_LONGWORD, FALSE); // if(FTFC_EEP_IP_STATUS_OK != retJobResultType) // // Exit_Example(FALSE); // 0 を返す; // } // } /* EEPROMメモリ領域とアプリケーションデータバッファを比較します */ for(i=0; i ヤージュ retJobResultType = Ftfc_Eep_Ip_Compare(EEP_ERASE_START_ADD + i, dataWrTestPatt + i, FTFC_EEP_IP_PAGE_LONGWORD); if(FTFC_EEP_IP_STATUS_OK != retJobResultType) ヤージュ Exit_Example(FALSE); 0を返す。 } } 事前に感謝いたします。 Re: S32K1 EEprom RTD 「FTFC_EEP_IP_STATUS_BLOCK_INCONSISTENT」はブロックアドレスのアライメントが原因で発生する可能性があります。初期パーティション時に「Preserve this Range from 0x10000000 to 0x1000ffff」以外にEEPROMアドレス設定に関する詳細情報を提供していただけますか? Re: S32K1 EEprom RTD データフラッシュとEEPROMの設定に使用するFlexNVMパーティションコードを共有してください。どの部分がEEPROMとして1000000から1000FFFFの間に設定されているかを知る必要があるかもしれません。設定によっては、EEPROMデータを読み取る必要がある場合もあります。 詳細については、AN11983「S32K1xx EEPROM機能の使用」を参照してください。 Re: S32K1 EEprom RTD こんにちは、 @ck182 さん。 FlexNVMでEEEが有効になると、FlexNVM(バックアップ)はアプリケーションコアから直接アクセスできなくなります。その時点では、EEPROMとしてのFlexRAMのみがアクセス可能です。 FlexNVMがEEP_FTFC_LOAD_AT_RESET_ENABLEDでパーティション分割されている場合、リセット後にバックアップフラッシュの内容が自動的にFlexRAM(EEPROM)にコピーされ、EEERDYフラグが設定されます。 main()関数の冒頭で、以下の点をご確認ください。 EEERDY == 1、 DEPARTには有効なパーティションコードが含まれており、 FlexRAM(EEPROM)に有効なデータが存在しますか? よろしくお願いいたします。 ダニエル Re: S32K1 EEprom RTD こんにちは、 db16122さん。 ご返信ありがとうございます。 ck182_0-1777878996851.pngck182_0-1777878996851.png 元のサンプル「Eep_Ftfc_Ip_Example_S32K144」から何も変更していません。 また、このコードを実行すると、次の点に気づきました。 retJobResultType = Ftfc_Eep_Ip_Write(EEP_ERASE_START_ADD + i, dataWrTestPatt + i, FTFC_EEP_IP_PAGE_LONGWORD, FALSE); この例では、RAMのアドレス0x14000000に書き込みが行われていますが、これは正しいものの、Flexメモリには「何か」が書き込まれません。 「somethings」はRAMだけでなく、アドレス0x10000000から始まるFlexメモリにも書き込まれるはずですが、変化が見られません。 自分が何が悪いのか理解できません 私はDS3.4とRDT 1.01を使用しています。 よろしくお願いします。 Re: S32K1 EEprom RTD @danielmartynekさん、返信が遅くなって申し訳ありません。他の仕事のため、Rtd EEPROMの作業を中断しました。 問題は解決しました。 すべてのコードとS32K144のサンプルは正しく動作しますが、問題はPEmicroデバッガーが毎回一括消去を実行することです。 そこで、Algortimの代わりにSector Erase Alrgortim pflash_dflahs_eeprom使ってみたら、今はうまくいきました。 私はpflash_dflahs_eepromアルゴリズムを維持し、FlexNMVメモリを保持することも試みましたが、この解決策は機能しませんでした。 あなたにとって正しいですか? 事前に感謝申し上げます。また、返信が長くなってしまい申し訳ありません。 Re: S32K1 EEprom RTD こんにちは、 @ck182 さん。 なるほど、情報提供ありがとうございます。 これらはPE Micro独自のアルゴリズムです。 PE Microサポートまでご連絡ください。 BR、ダニエル
View full article
清除 GPIO ISR 大家好, 我们尝试按照 IMXRT1176 参考手册从 CM7 内核获取 GPIO_DISP_B2_00 引脚的访问权限。 gpio_pin_config_t config = { kGPIO_DigitalInput, 0, kGPIO_IntRisingEdge, }; SETUP(IOMUXC_GPIO_DISP_B2_00_GPIO_MUX5_IO01, 1, AD_PULL_UP + AD_SLEW_SLOW); GPIO_PinInit(GPIO5, 1,&config ); 这发生在启动过程中的引脚复用器中。在应用程序的某处,我们会编写代码来初始化该 gpio 的中断: GPIO_PortClearInterruptFlags(GPIO5, 0xFFFFFFFF); GPIO_PortEnableInterrupts(GPIO5, 1<< 1); NVIC_SetPriority(GPIO5_Combined_0_15_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY); EnableIRQ(GPIO5_Combined_0_15_IRQn); volatile uint32_t a = GPIO_PortGetInterruptFlags(GPIO5); PRINTF (" %lu\ r\n ", a); 此代码打印: 4 294 901 757 这是 0x FFFE FFFD — >--> 0b1111 1111 1111 1110 1111 1111 1111 1101 如你所见,引脚 1 位看起来像 0。 因此,我们可以假设 RESET 对其产生了影响。 但是我不明白的是,为什么其他位设置为 1,为什么第 17 位设置为 0? 参考手册指出 1402/6259: ```当在 GPIO 输入上检测到活动状态(由 相应的 ICR 位确定)并正在等待服务时,将钳位该寄存器的第 n 位 中断状态(高电平有效)。寄存器 的值与 IMR 寄存器的值无关。 检测到激活状态后,相应位将保持设置状态,直至软件清除。 通过将1写入相应的位位置 ```来清除状态标志, 因此我假设所有值都应为0作为默认RESET状态。其他 GPIO 也遵循类似的模式,在 ISR 寄存器中设置了许多位。 谁能告诉我,我在这里误解了什么?感谢您的帮助 🙂 致以最崇高的敬意, Jakub Re: Clearing GPIO ISR 你好@jslota13245、 误解在于,GPIO ISR RESET 值仅描述 RESET 后立即的寄存器状态。它不能保证稍后在启动期间会读取什么软件。ISR 是一个锁存状态寄存器:一旦检测到配置的条件,该位将保持设置状态,直到软件将其清除,这与 IMR 无关。要确定当前启用了哪些中断源,我们可以使用GPIOx->ISR& GPIOx->IMR; 对于 RT1170,恩智浦还记录了勘误表 ERR050643:DISP_B2 引脚在初始上电期间可以看到短暂的内部上拉脉冲,因此在应用程序读取 ISR 之前,GPIO_DISP_B2_00 可能合法地处于待定状态。因此,启动后的非零ISR并不意味着重置失败。 致以最诚挚的问候, Gavin Re: Clearing GPIO ISR 亲爱的@Gavin_Jia, ,非常感谢你的详细答复。 1) 确认一下,您可能已经注意到了,在我之前发送的示例代码中,我们明确向状态寄存器写入 0xffffff ffff 以清除它,我们做了一些无操作循环,操作后我们几乎立即尝试读取它,并在 GPIO->ISR 中得到非零值。这意味着在清零/读取调用之间,硬件已在大部分引脚上注册了中断条件,这很难让人相信,因为我们根本没有使用它们。这发生在 GPIO 初始化的早期启动之后。So what you're suggesting is there is some hardware noise that may cause this behaviour when we write 0xffffffff to GPIO->ISR? 2) By the way, reading forums i found this thread: https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/GPIO-ISR-and-Clearing-ISR/m-p/1059441 答案如下: ''在您的情况下,您需要注意未配置为中断操作的位的中断状态将读作待处理。因此,你不能像 那样只检查中断状态,我想知道这是否是真的,因为这与观察到的行为有些吻合。但是我在参考手册中找不到任何关于它的信息。 再次感谢您的支持! 最美好的祝愿, Jakub
View full article
使用 Simulink 模型模块异常的 MBDT 工具箱 现在使用 S32k3 的 MBDT 工具,顶层模型包含 MBDT 工具箱模块,顶层模块包含 Simulink 模型模块。使用子系统是正常的。该模型加载了包含纯算法的 SLX 模型,但有两个问题: (1) 在每个算法模型下,都会生成 MBDT 工具箱驱动的 *. c *. h *. o,但理论上讲,纯算法模块没有这些? (2) 在 S32 ds 中编译一次所有生成的代码,并报告图中所示的错误(make:* * No rule to make target'D:/Work/APP.Merge/test260409/s32k3xx_dious32ct_Cnfig/../slprj/ert/_stharedutils/rtwshare d ', needed by' s32k3xx_dious32ct.精灵停止) " make-j8 all " 以退出代码 2 终止。版本可能不完整。),原因何在?
View full article
LX2160A 電源インテグリティ (PI) 解析 専門家の皆様へ 現在、LX2160Aを使用したPCB設計を進めており、電源インテグリティ(PI)解析を実施する予定です。 適切な分析条件を設定するために、以下の項目についてご指導いただけますでしょうか? 1. 各電源レールにおける推奨目標インピーダンス 2. 解析における想定最大過渡電流(di/dt)条件 また、推奨されるPI分析ツールや手法があれば、ぜひご教示いただければ幸いです。 サポートありがとうございます。ご返信をお待ちしております。 よろしくお願いいたします。 Re: LX2160A Power Integrity (PI) analysis 1. 電源レール概要(LX2160A) LX2160Aは、コアロジック、SRAM/PLL、SerDes、DDR、およびI/O用に複数の独立した電源レールを使用します。正確なレールリストと公称電圧は、 LX2160Aのデータシートおよびリファレンスデザインに定義されており、それらが正式な情報として扱われるべきです。 典型的なキーレール(名称は回路図によって異なります): レール機能 標準定格電圧 備考 コア(VDD) 約0.75~0.85V di/dtが最も高く、PIにとって最も重要 プラットフォーム/キャッシュ(VDD_PLAT) 約0.9V 大容量オンダイSRAM、垂下現象に敏感 SerDesアナログ 約1.0V ノイズに敏感で、di/dtが低い SerDes Digital 約0.9V 適度な切り替え活動 DDR VDD 1.2 V JEDEC主導の外部メモリが主流 DDR VPP 2.5V 低電流 入出力(VDD_IO) 1.8V / 3.3V PIの臨界値が最も低い 2. 推奨ターゲットインピーダンス(Z_TARGET) LX2160Aは明示的なZターゲット値を公表していないため、標準的な電圧リップルに基づく方法を使用する。 Ztarget=ΔVallowableΔImaxZ_{target} = \frac{\Delta V_{allowable}}{\Delta I_{max}} Z t a r g e t = Δ I m a x Δ V a l l o w a b l e NXPは一般的に、Layerscapeデバイスのコア型電源レールにおけるリップル率を3~5%以下にすることを推奨しています(設計チェックリストおよびリファレンスボードに基づく)。[static.chipdip.ru] 、[community.nxp.com] 実用的な目標インピーダンス値 レール 許容リップル 推定ΔI 推奨Z_TARGET コア(VDD) ±3%(約25mV) 8~12歳 2~3 mΩ プラットフォーム/SRAM ±3%(約30mV) 4~6 A 5~8 mΩ SerDes Digital ±5% 1~2 A 25~40 mΩ SerDesアナログ ±5% <1 A >50 mΩ DDR VDD JEDEC 3~5 A 20~30 mΩ 入出力レール ±5~10% <2 A >50 mΩ ✅ 重要なポイント: コアレールとSRAMレールのみが、低ミリオーム範囲まで非常に積極的なPDN設計を必要とする。 3. 過渡電流/di/dtに関する仮定 コアレール(重要) PIシミュレーションにおける最悪ケースの過渡現象に関する仮定は、一般的に以下のとおりです。 ΔIステップ:5~8A エッジレート:1~5ナノ秒 di/dt : 1~5 A/ns これらは以下を表しています。 複数のCortex-A72コアの同時切り替え キャッシュ+データパスアクセラレータの動作(DPAA2、DCE、SEC) これは、NXPのリファレンスボードや設計チェックリストにおけるバルク+高周波デカップリングのサイズ決定方法と一致しています。[static.chipdip.ru] 、[community.nxp.com] その他のレール レール ΔIの仮定 di/dt プラットフォーム/SRAM 2~4 A 0.5~1 A/ns SerDes Digital 0.5~1 A 0.1~0.3回答 DDR VDD JEDECによって管理されるバースト より遅い、レギュレーター主導 I/O <0.5 A 非常に低い 4. 分析対象周波数範囲 LX2160Aの場合、PI解析では以下の項目を対象とする必要があります。 DC → 100 MHz (最小) オンダイL/C効果のため、コアレールには最大300~500MHzが推奨されます。 約1MHz以下: ✅ VRMとバルクコンデンサが大部分を占める 1~100MHz: ✅ ボードレベルのMLCCとプレーン 100 MHz: ✅ オンパッケージ+オンダイ静電容量(利用可能な場合はパッケージSパラメータを使用してモデル化) 5. デカップリング戦略(参照ベース) NXPのリファレンスデザインは、3層構造のアプローチを示しています。 バルク コアレールあたり47~330μFのポリマーまたはタンタル 中周波MLCC 1~10 µF、X7R、パッケージ外周全体に分布 高周波MLCC BGA直下に0.01~0.1μF この方法は、LayerscapeのRDBレイアウトと整合性があります。[static.chipdip.ru] 6. 推奨PIツール LX2160AクラスのSoCでうまく機能する、広く使われているツール: シミュレーション ケイデンス シグリティ パワーSI Ansys SIwave Keysight PIPro Altium PDNアナライザー(初期段階のチェック) 測定(ポストシリコン) VNAを用いたPDNインピーダンス測定(2ポートシャントスルー方式) BGAブレークアウトテストポイントにおける高帯域幅プロービング 7.方法論の概要(ベストプラクティス) Z_TARGETベースのPDN設計から始めましょう スイープインピーダンスプロット(対数-対数)を作成する Z_TARGET以下の反共鳴ピークを除去する 検証方法: 最悪の場合の現在のステップ 負荷過渡シミュレーション 可能であればRDBの挙動と相関関係を分析する 8. NXP固有の推奨事項 NXPは、社内でPDNサイジングに使用される電力使用事例やレール電流に関するガイダンスを含むAN5407 – LX2160A/LX2162A設計チェックリストを確認することを強く推奨します。[community.nxp.com] NXPプレミアムサポートをご利用の場合は、以下のリクエストも可能です。 鉄道ごとの最悪シナリオの電流表 パッケージPDNモデル(利用可能な場合)
View full article
デジタル信号の電圧変換ってどうやればいいの? (日本語ブログ) 0. 目次 0. 目次 1. 電圧レベル・トランスレータって? 2. デジタル信号 2.1 様々なデジタル信号 2.2 CMOSとTTL:単純な電圧のHIGHとLOWによる論理レベルの信号 2.3 入出力電圧の規定:VOH / VOL と VIH / VIL 2.3.1 出力電圧の規定:VOHとVOL 2.3.2 入力電圧の規定:VIHとVIL 2.3.3 VOH / VOL と VIH / VIL の関係 3. 基本的な電圧レベル変換の方法:片方向信号の変換 3.1 チップの電源電圧が違っても変換の必要がない例 コラム:TTLのVIH(min) = 2.0V,VIL(max) = 0.8Vはどうやって決まっている? 3.2 変換が必要な例 3.2.1 オープンドレイン出力による変換 3.2.2 標準ロジック(汎用ロジック)チップを用いた変換 4. 自動方向切り替えが必要な双方向信号の変換 4.1 単体MOSトランジスタによる双方向変換 4.2 専用品による双方向変換 4.2.1 I²C信号電圧変換チップ 4.2.2 高速化を図った双方向オープンドレイン信号電圧変換チップ 4.2.3 双方向プッシュプル信号電圧変換チップ 4.2.4 I3C信号電圧変換チップ 4.2.5 バッファによる変換 5. まとめ 5.1 ブログ内で紹介した方式/品番の比較 6. 参考資料 1. 電圧レベル・トランスレータって? デジタル回路同士をつなぐとき,単純に信号線を直結すればいい… ということはなくて,「論理レベルの電圧」が合わないと,動作しなかったり,不安定になったり,最悪の場合チップを壊してしまうことがあります. そんなときに便利に使えるのが電圧レベル・トランスレータ(Voltage Level Translator.電圧レベル・シフタとも呼ぶ)です. 電圧レベル・トランスレータは,異なる電源電圧のデジタル回路間で信号をやり取りできるようにする回路です. 例えば,次のようなケースで必要になります. 3.3V マイコン ↔︎ 5V センサ の接続 1.8V FPGA ↔︎ 3.3V 周辺デバイス の接続 図1:信号電圧の違い   このブログでは,デジタル回路で使われる論理回路の種類(*TTL,*LVTTL,*CMOS)の電圧レベルの違いから,それを判断する上で重要なV OH /V OL /V IH /V IL の意味について解説します.さらに様々な変換の方法の中から,どのような電圧レベル・トランスレータを選べばよいかを解説します. さらにこのブログでは信号の方向を自動で検出して変換を行う電圧レベル・トランスレータの具体例を見ていきます. NXPではSDカード/SIMカード向けや,*GTL↔︎TTLレベル変換のような特定用途向け電圧レベル・トランスレータもラインナップしていますが,このブログは汎用またはシリアル・バス用途をターゲットにした製品の解説となります. *TTL(Transistor-Transistor Logic) *LVTTL(Low Voltage Transistor-Transistor Logic) *CMOS(Complementary Metal-Oxide-Semiconductor) *GTL(Gunning Transceiver Logic) 2. デジタル信号   2.1 様々なデジタル信号 いわゆる「デジタル信号」は論理レベルの1と0を電気的に表現したものです.この論理レベルの1と0を扱う回路設計方法には歴史的に様々なものがあります.論理レベルを単純な電圧のHIGHとLOWで表現するものや,電圧の差を利用してHIGH/LOWを表現するものなど. 単純なHIGH/LOWを5V/0Vで表すTTL.さらにそのTTLを低電圧化し3.3V/0Vで表すLVTTLなどバイポーラ・トランジスタ回路を基準に電圧レベルが決められたもの. 同様にバイポーラ・トランジスタを使いながらも負電源を使い低振幅で差動で動作論理レベルを実装し,高速化が図られたECL.基準電圧を設けて低振幅のシングルエンド信号でHIGH/LOWを伝達するGTLなど... また単純なHIGH/LOWでの表現でも低消費電力化を目的に開発された4000シリーズと呼ばれるCMOS汎用ロジックでは,HIGHレベルとして3V〜18Vを使うことができました. https://en.wikipedia.org/wiki/Logic_family このブログでは,上記のような様々な論理レベルの中でも,単純なHIGHとLOWの電圧で論理を表現するTTL(LVTTL)とCMOSの電圧レベルの扱いについて解説します. その他の信号変換には専用チップが用いられるため,ここでは扱いません. このほか近年では半導体技術の微細化・高速化・低消費電力化が進むとともに,電源に使われる電圧は低くなってきています.このため信号電圧差を橋渡しする電圧レベル・トランスレータは特に重要になってきています. 図2:信号波形 - 電圧の高低(HIGH/LOW)で論理レベルを表す   2.2 CMOSとTTL:単純な電圧のHIGHとLOWによる論理レベルの信号 デジタル回路に使われる単純な電圧のHIGHとLOWによる論理レベルの信号には,HIGHを電源電圧で,LOWを0Vとするものが一般的です.電源電圧が異なってもHIGH/LOWの電圧レベルが同じであれば,そのまま信号をやり取りすることができます. たとえばTTL(LVTTL)は入力される信号が2.0V以上であればHIGH,0.8V以下であればLOWと解釈します.このような取り決めがあるため,TTL信号であれば互いに電源電圧が異なってもHIGH/LOWの電圧レベルは変わりません. いっぽう,CMOSは電源電圧の半分の電圧を基準にしてHIGH/LOWを定義します.このためCMOSは電源電圧が異なるとHIGH/LOWの電圧レベルも変わります. 図3:入力信号電圧の規定   2.3 入出力電圧の規定:V OH  / V OL  と V IH  / V IL デジタル回路ではHIGHとLOWとして出力される電圧と,入力される信号をHIGHとLOWに判断する電圧が規定されています.これらは使用する各チップの仕様で規定されているため,データシートで確認する必要があります. V OH  : HIGHレベル出力電圧 (HIGH-level output voltage) V OL  : LOWレベル出力電圧 (LOW-level output voltage) V IH  : HIGHレベル入力電圧 (HIGH-level input voltage) V IL  : LOWレベル入力電圧 (LOW-level input voltage) 2.3.1 出力電圧の規定:V OH とV OL 出力ではHIGH/LOWを出力する際の電流を考えておかねばなりません.電流は負荷により増減します. HIGH出力での最大流出電流時に保証できる電圧をV OH (min),LOW出力での最大流入電流時に保証できる電圧をV OL (max)と呼びます. V OH (min)は回路出力段の上側のトランジスタがONになったときに出力される電圧です.このトランジスタには「ON抵抗」と呼ばれる抵抗分があります. トランジスタから流れ出る電流が大きい場合,"トランジスタの抵抗分 x そこに流れる電流"で電圧が発生.すると出力はその電圧分だけ電源電圧から下がってしまいV OH が低くなってしまいます.このため,あらかじめ想定される最大流出電流のときに保証できる最小の電圧がV OH (min)となります. 図4:デジタル信号出力回路(プッシュプル)   図5:HIGH出力電圧は負荷によって変化する   V OL はこの逆となります.回路出力段の下側のトランジスタがONになったとき,流れ込む電流が大きいと,上記と同様にトランジスタのON抵抗によって発生する電圧によって,出力は0Vより上がってしまいます.これを考慮し,あらかじめ想定される最大流入電流のときに保証できる最大の電圧がV OL (max)となります. 図6:LOW出力電圧も負荷によって変化する   2.3.2 入力電圧の規定:V IH とV IL 入力にはHIGHとLOWを判断するための電圧レベルがあります.V IH (min)とV IL (max)です.電圧がV IH (min)以上であればHIGHと判断され,V IL (max)以下であればLOWと判断されます. CMOS入力では電源電圧の1/2がHIGHとLOWの基準となりますが,これをそのままV IH (min)とV IL (max)とはしていません.これはチップごとのバラツキなどによって閾値が上下するためです.また,遅く立ち上がる信号に乗ったノイズなどによるグリッチが出力に現れることを軽減するため,入力にはヒステリシスを持たせることが一般的です.このような理由によりV IH (min)とV IL (max)はある程度の電圧差を設けて規定されます. 2.3.3 V OH  / V OL  と V IH  / V IL  の関係 正常な信号のやり取りを行うには,出力と入力の関係は下式を満たす必要があります. HIGHレベル: V OH (min) > V IH (min) LOWレベル: V OL (max) < V IL (max) この関係が守られていれば,出力側の回路は,次の入力側の回路に対してHIGH/LOWを正しく伝えることができます.さらにこの互いの電圧差である「V OH (min) - V IH (min)」や「V IL (max) - V OL (max)」は「ノイズ・マージン」となり,ノイズ耐性を高く保つための目安になります. 図7:V OH (min) / V OL (max) と V IH (min) / V IL (max) 3. 基本的な電圧レベル変換の方法:片方向信号の変換   3.1 チップの電源電圧が違っても変換の必要がない例 『「V OH (min) > V IH (min)」かつ「V OL (max) < V IL (max)」』の関係が成り立つ場合には基本的には電圧レベル変換は必要ありません.たとえばTTLとLVTTLはそれぞれのチップに使われる電源電圧は違うものの,入出力電圧の規定は同一です. TTL(5V)とLVTTL(3.3V)ではどちらも,V OH (min)は2.4V,V OL (max)は0.4Vです.V IH (min)/V IL (max)も,どちらも2.0V/0.8Vなので問題なく互いに接続できます. ただし出力電圧が入力側チップの電源電圧よりも高い場合には注意が必要です.出力側が5V,入力側が3.3V電源を使うチップである場合には,入力側は「5Vトレラント入力」に対応していなければなりません. 5Vトレラント入力とは,5VのHIGH信号を3.3Vの電源電圧で動作するチップの入力に接続しても問題なく動作する入力のことです.一般的なチップの入力には静電気対策のためのESD保護回路が入っていますが,このESD保護回路が次の図のような回路で構成されていると5Vを入力した際に入力から3.3Vの電源に電流が逆流してしまい,チップを破壊してしまうことがあります.このような問題を起こさないための対策が取られた入力が5Vトレラント入力です.トレラント入力にはESD保護がないわけではなく,電源電圧より高い信号が入力されても問題がないような構造を持つESD保護回路が組み込まれています. 図7のようなESD保護ダイオードは,入力側チップの電源が切られている時にも問題を引き起こします.チップごとに個別に電源のON/OFF管理を行うようなシステムの場合,入力側チップがOFFになっているにも関わらず出力側の信号が電源に回り込み,入力側チップを動作させてしまうことがあります. 図7:ESD保護ダイオード - 非トレラント入力 コラム:TTLのV IH (min) = 2.0V,V IL (max) = 0.8Vはどうやって決まっている? CMOSの入力閾値が電源電圧の中点(VCC/2)を基準にしているのに対し,TTLのV IH (min)/V IL (max)は2.0V/0.8Vという,電源電圧(5V)に対して特に綺麗な比率ではない値になっています.これには,TTLの入力段がバイポーラ・トランジスタで構成されていることが関係しています. 標準TTLロジックIC:SN7400(2入力NAND)の内部回路例 『最新汎用ロジック・デバイス規格表 1988』(CQ出版)に掲載されていたもの 標準的なTTLゲートの入力段は,多重エミッタの入力トランジスタと,その後段のフェーズスプリッタ・トランジスタが直列に重なった構造をしています.ゲートが実際に反応し始める「スイッチング・スレッショルド」は,この2段に重なったPN接合の順方向電圧で決まります.シリコンのPN接合1個あたりの順方向電圧はおよそ0.6〜0.7Vなので,2段重なると合計でおよそ1.3〜1.5V付近がTTLゲートの実質的なスイッチング・スレッショルドとなります. ただしこの約1.4Vという値はあくまで「典型値(typical)」であり,個体差や温度などのバラツキによってロットごと・条件ごとに変動します.そこでデータシート上の規定値であるV IH (min)とV IL (max)は,この約1.4Vの典型値に対して上下に十分なマージンを取り,「ここまで下がれば確実にLOWと判定できる(V IL (max)=0.8V)」「ここまで上がれば確実にHIGHと判定できる(V IH (min)=2.0V)」という,保証値として規定されています. さらにこの値は単独で決められているわけではなく,2.3.3節で説明したV OH /V OL との関係も踏まえて設計されています.標準TTLでは出力段の構成により,HIGH出力は電源電圧にはならず,少し低い(上記回路例では130Ωの抵抗,トランジスタとダイオードで発生する電圧分だけ低い)電圧になります(VOH(min)=2.4V).これとVOL(max)=0.4Vを組み合わせると, HIGH側ノイズ・マージン:V OH (min) − V IH (min) = 2.4 − 2.0 = 0.4V LOW側ノイズ・マージン:V IL (max) − V OL (max) = 0.8 − 0.4 = 0.4V のように,上下対称に0.4Vのノイズ・マージンが確保されるよう設計されています.つまりTTLの2.0V/0.8Vという「電源電圧に対して半端」に見える数字は,バイポーラ・トランジスタの接合電圧という物理的な実体と,ノイズ・マージン設計という2つの要請から導かれた,合理的な値だったということになります. SN7420(4入力NAND)の入力ピン3つをHIGH,1つに100kHzの三角波を入力(ch1)した様子 無負荷状態の出力(ch2)だがHIGHのとき4V未満の出力となっている(Vcc=5V) なお,本コラムで紹介した回路は無印(74LS00や74HC00のようにLS/HCなどの付かないもの.英語では“バニラTTL”と呼ばれることもある)標準TTLの例ですが,V IH /V IL の規定が同じ理由(入力段のバイポーラ接合特性)は74LSなど他のTTLファミリにも共通しています.   3.2 変換が必要な例   TTLやLVTTLでは電圧レベルが揃っているため上記のような接続が可能ですが,電源電圧の違うCMOSチップ同士や,CMOSとTTLチップの接続では論理レベルが合わない場合が多く発生します.前述の『「V OH (min) > V IH (min)」かつ「V OL (max) < V IL (max)」』の関係が成り立たない,またはその差が小さくなってしまい,ノイズ・マージンが取れないような状況がそれにあたります. この問題を解決するのが電圧レベル・トランスレータです. 図9:論理レベルが合わない例(1):充分なHIGH電圧が入力されない   図10:論理レベルが合わない例(2):充分なLOW電圧が入力されない     3.2.1 オープンドレイン出力による変換 電圧レベル変換チップを用いなくても,簡単に電圧レベル合わせを行う方法はあります. 信号の方向が出力側チップ→入力側チップで固定され切り替わることがないのなら.HIGH側の出力をオープンドレイン出力にすることで,入力側の電圧に合わせる方法です.オープンドレインはデジタル回路の出力段の上側のトランジスタがない構成のもので,入力側チップの電源電圧に接続されたプルアップ抵抗によってHIGHの電圧を得ます. 図11:デジタル信号出力回路(オープンドレイン)   オープンドレインは単純で安価な方法ですが,いくつかの注意点があります. まず出力側がオープンドレイン出力が可能なものである必要があります.多くのマイコンのGPIOピンなどでは設定によってこの出力が可能です. まず出力側がオープンドレイン出力が可能なものである必要があります.多くのマイコンのGPIOピンなどでは設定によってこの出力が可能です.もしオープンドレイン出力に設定できないプッシュプル出力固定など場合には,外付けのトランジスタなどを使ってオープンドレイン出力に変換する必要があります. さらにプルアップ抵抗の選択も重要です. プルアップはHIGHの電圧を得るために必要な抵抗ですが,抵抗値が小さすぎるとLOW出力時に流れる電流が大きく(負荷が大きい状態に)なり,消費電力が増える上にV OL の上昇を招いてしまいます. 逆に大きすぎると配線とピンによる容量の影響を受け,LOWからHIGHへの立ち上がりが遅くなってしまい,通信速度の低下が起こります. 3.2.2 標準ロジック(汎用ロジック)チップを用いた変換 単純な電圧レベル変換であれば標準ロジックを用いる方法もあります.たとえばNexperia社の74AVCH4T245は4ビットの双方向レベル変換を行うことができるCMOS汎用ロジックチップです. このチップでは0.8V〜3.6Vの信号を変換することができ,信号の方向をDIRピンによって切り替えることもできます.信号速度は変換を行う電圧にも依存しますが,100M〜380Mbps程度に対応可能です. 図12:標準ロジックの例 - 74AVCH4T245 このチップを用いると高速な信号の双方向電圧変換が可能ですが,方向の制御は外部からの信号によって行わなければなりません.このような制御はパラレル・バスのREAD/WRITEのような信号によって可能ですが,プロトコルによって通信方向が切り替わるシリアル・バスのような通信には適用が困難です. 図13:標準ロジックの例.信号の方向を外部から指定しなくてはならない 4. 自動方向切り替えが必要な双方向信号の変換 これまでに紹介した"オープンドレイン出力"や"標準ロジックチップを用いた電圧変換方法"では,主に一方向のみの変換を行うもの,あるいは外部信号による方向の切り替えが必要なものでした. I²C,I3Cのような信号の方向がダイナミックに変化するような通信には,方向が自動で検出して切り替わる「双方向の電圧レベル変換」が必要です.このような信号の方向を外部から制御するのは難しく,前述のようなバッファ・チップで実現するのは困難です. さらにI²Cはオープンドレイン信号であるため,オープンドレインの標準ロジック・バッファを互いに違う向きに接続するようなことができません.図14はその例です.オープンドレイン・バッファを互いに反対方向に接続しています.バッファの両側がHIGHの時は問題ありませんが,どちらかが一旦LOWになると,バッファは互いの入力をLOWに引っ張ったままとなり,HIGHに戻すことができなくなります. 図14:通常のオープンドレイン・バッファでは双方向通信を自動切替できない   4.1 単体MOSトランジスタによる双方向変換   これまでI²Cの信号電圧変換には,単純な回路が用いられることがありました.その最も簡単なMOSトランジスタを使った方法をその例として挙げます. 図15:MOSトランジスタを使った変換の例   図15はI²Cの仕様書version2.1(2000年)から引用したもので,3.3Vと5Vの信号を2本の信号にそれぞれ1個のMOSトランジスタ(TR1, TR2)を用いる例です.このような単純なトランジスタ単体での変換例は,後述する問題点があるため現在のI²Cの仕様書からは削除されていますが,原理を理解するために紹介します. SDAとSCLと呼ばれるI²Cの信号線は,どちらもオープンドレイン出力の双方向信号となっています.3.3V側と5V側にそれぞれプルアップ抵抗が接続されています. この回路では3.3V側,5V側の信号がHIGHである場合,このトランジスタのゲート(g)とソース(s)間は同電位となるため,ソース(s)とドレイン(d)OFF状態となって互いの接続が切れた状態に置かれます.この状態で3.3VがLOWに変化すると,3.3V側のトランジスタ(のsとdの間)がONになり,5V側の信号もLOWになります. 3.3V側がHIGHで5V側がLOWに変化した場合には,まず3.3V側から5V側への寄生ダイオード(ボディ・ダイオード)がONになります.ダイオードがONになるとソース(s)の電圧が降下.その結果トランジスタがONになり,3.3V側の信号もLOWになります. このようにトランジスタをスイッチとして使う非常に単純な仕組みで電圧レベル変換ができるのですが,ここには問題もあります.トランジスタのバラツキが信号変換の閾値に影響すること.さらに今日ではより低い信号電圧を扱うことが増えてきており,たとえば信号電圧が1V程度では,このような回路では十分なゲート(g)とソース(s)間電圧(Vgs)が得られないため動作させることができません. 追記:図15と同じ回路は,NXPから半導体ディスクリート/ロジック製品事業が分社化されて誕生したNexperia社のアプリケーションノートAN10441「Level shifting techniques in I²C-bus design」として今も公開されています.I²C仕様書とは別に2007年に初版(Rev.01)のアプリケーションノートが発行され,2020年にNexperiaブランドへ改訂(Rev.2)されています. 4.2 専用品による双方向変換   「電圧レベル・トランスレータ専用IC」を用いることで,I²C, I3Cのような双方向通信を行うバスの電圧レベル変換を容易に行うことができます. 4.2.1 I²C信号電圧変換チップ PCA9306,NVT20xxシリーズ(NVT2001/02, NVT2003/06, NVT2008/10)は双方向信号の変換に特化した電圧レベル・トランスレータです.これらのチップでは複数の信号線(複数ビットの信号線)をまとめて扱うことができます.これらはI²C信号の電圧変換チップとされていますが,信号の仕様が合えば他の目的(SPIやその他のプッシュプル信号など)にも使うことができます. PCA9306,NVT20xxシリーズは同じ内部構造を持ち,プルアップ抵抗は,変換する電圧差が1V以上であれば電圧の高い側だけに接続すれば良いようになっています. 図16はその内部構造と外部チップの接続を示したものです(アプリケーションノートAN11127:「Bidirectional voltage level translators NVT20xx and PCA9306」のFig.2から抜粋).このチップ内部には信号線数(ビット数)+1個のMOSトランジスタが内蔵されています.各トランジスタはソースとドレインが可換の構造となっています. 信号を伝達するための経路のトランジスタはパス・トランジスタと呼ばれ,残りの1個はリファレンス・トランジスタと呼ばれます. 図16:NVT20xx(PCA9306) - チップ動作の解説図   回路を見てみると,リファレンス・トランジスタのゲートとドレイン間はショートされており,200kΩの抵抗を介して高い電圧側の電源に接続されています.リファレンス・トランジスタの残りの端子:ソースは低電圧側の電源に接続されています.このような接続により,リファレンス・トランジスタは1個のダイオードとなっており,このゲート電圧は低電圧側の電源よりもダイオード1個分高い電圧となります. 残りのパス・トランジスタはドレイン側が高い電圧側の信号線と1kΩのプルアップ抵抗に,ソース側は低い電圧側の信号線,さらにゲートはリファレンス・トランジスタのゲートに接続されています.パス・トランジスタの高い側,低い側の信号がどちらもHIGHになっている時,高い側は1kΩによってプルアップされた電圧となります. パス・トランジスタはいわゆる「ソースフォロワ」と呼ばれる回路を構成しています.低い電圧側の端子(ソース端子)は,ゲートに印加されている電圧よりトランジスタをONにするために必要なVgs分だけ低い電圧が現れます.つまり低電圧側の電源と同じ電圧となります.トランジスタはONでもOFFでもない半分ONの状態(線形領域での動作)になっています. この状態で,高または低のどちら側かの信号がLOWになると,ゲートと信号端子の電圧差によりトランジスタがON(完全にONとなった飽和領域での動作)になり,反対側の端子もLOWになります. このシリーズで扱える信号速度は,プルアップと信号線の容量の影響を受けます.データシートでは,PCA9306は2MHzまで.NVT20xxシリーズでは192Ωのプルアップ抵抗を使用し,容量50pFの条件で最大33MHzまでの信号速度に対応可能とされています.1MHz程度の信号であれば,プルアップ抵抗や容量をあまり気にしなくても(通常I²Cで使うような範囲内を想定)で問題なく動作します.しかしこのチップをプッシュプルのより高速な信号を扱う場合には特製の把握と慎重な部品選択が必要になります. このタイプの電圧レベル・トランスレータ動作の詳細は,「PCA9306の中身と動作」の記事で紹介されています. 4.2.2 高速化を図った双方向オープンドレイン信号電圧変換チップ 高速化を図った双方向オープンドレイン信号変換チップとして,NTS030xシリーズ(NTS0302JK, NTS0304E)を紹介します. このチップは2ビットまたは4ビットの双方向信号変換を行うことができ,オープンドレイン信号であれば2Mbps(1MHz),プッシュプル信号であれば20Mbps(10MHz)の信号に対応可能です.   図17:NTS030x - チップ内部ブロック図   図17はNTS030xの信号1ビット分の内部構造です. 図ではT3のトランジスタがパス・トランジスタとなっており,ゲート端子バイアス電圧がかけられているので,AとBと書かれた信号のどちらかがLOWとなった時にONとなります. AとBの両方がHIGHの時はT3がOFFになり,AとBはそれぞれの電源に比較的大きいプルアップ抵抗(10kΩ)で接続されているのでそれぞれの電圧となります. このチップにはT3のほかにT1とT2が存在しています.このT1とT2は「エッジレート・アクセラレータ」と呼ぶ機能のために使われます.このうちの片方,T1に注目しこの動作を解説します. T1はA側に置かれ,ソース端子はA信号に,ドレイン端子はA側電源に接続されています.ゲート端子はこれを制御する「ONE-SHOT AND SLEW RATE CONTROL」と書かれたブロックに接続されています. 「ONE-SHOT AND SLEW RATE CONTROL」ブロックは反対側のB信号に接続されていて,B側の信号のLOWからHIGHへの変化を検出.これを検出した時に一時的にT1をONにして,プルアップの10kΩ抵抗をバイパスして電流を流す事により,A側の信号のHIGHへの変化を加速します.このように信号の立ち上がりを速くすることで,より高速な信号を扱うことができるようにしています. ちなみに,このT1をONにする際のスルーレートは制御されていて,急な電流増加によるリンギング発生を抑えることも考慮されています. もういっぽうのT2はこの同じ仕組みが逆方向に作られており,B側信号にも適用されるようになっています. このNTSシリーズにはもう一つの使いやすい点があります. ここまで説明したMOSトランジスタ単体やPCA9306/NVT20xxの場合,どちらかの電源がOFFになった場合,他方の信号をLOWにしてしまうという問題がありました.NTS030xではこの問題を解決するために,両方の電源がONになっていない場合は,互いに影響が出ないように信号ピンをハイ・インピーダンス状態とするよう動作します.このような機能を使うことにより,システムの電源を部分的にON/OFF制御するような使い方が可能になります. NTS030xシリーズと同等品で,より高速の信号に対応するためスルーレート制御機能の無いNTS010xシリーズ(NTS0102, NTS0104)も用意されています. なお,NTS0304Eには,すぐに簡単な動作検証ができるように評価基板:NTS0304EUK-ARDが用意されています.NTS0304EUK-ARD基板の概要と動かし方はこちらの動画「NTS0304EUK-ARDの動かし方」をご参考ください. 4.2.3 双方向プッシュプル信号電圧変換チップ さらにこのNTS030xシリーズをプッシュプル信号だけで使う場合のより高速なオプションとしてNTB010xシリーズ(NTB0102, NTB0104)があります. HIGHまたはLOWで安定した状態では4kΩを通して信号を駆動.NTS030xシリーズ同様のワンショット機能をHIGHとLOW側の両側に持たせ,いずれかの端子で信号の変化があった場合にこれを用いて,反対側信号を変化させる機構を持っています. このような機構により,信号方向の自動検出機能を持ちながら70〜80Mbpsの速度の信号電圧変換が可能です.   図17:NTB010x - チップ内部ブロック図 4.2.4 I3C信号電圧変換チップ I3Cはオープンドレインとプッシュプルを切り替えながら通信を行う仕様を持ち,オープンドレインではI²Cと互換〜4MHzの周波数.プッシュプル時は12.5MHzのクロックが使われます.信号の電圧は通常1V〜3.3Vの範囲で使われるため,電圧差がある場合には,信号仕様に合わせた動作をする電圧レベル・トランスレータが必要になります. 図18はP3A1604の1ビット分の内部ブロック図です.このチップでは図の通り,LOW→HIGHだけでなくHIGH→LOWの変化を加速する仕組みとON/OFFの切り替えができるプルアップ抵抗が内蔵されています.   図18:P3A1604 - チップ内部ブロック図 P3A1604は4ビット用のI3C電圧レベル・トランスレータ.この他にも2ビット用のP3A9606も用意されています.   4.2.5 バッファによる変換 もう一つの双方向信号の変換方法として,専用品のバッファを使う方法があります. バッファの本来の目的は,駆動能力の増強や接続している信号線の容量の分離などですが,電圧の変換に対応した製品も存在します. 双方向のオープンドレイン信号を相互にバッファするには,このブログの中で説明したように単純なバッファでは実現できません.そのため双方向オープンドレイン信号用として様々な工夫がされたバッファ製品が用意されています. バッファについての詳細はまた次の機会に解説する予定です. 5. まとめ 電圧レベル・トランスレータは,異なる電源電圧を持つデジタル回路間で安全かつ確実に信号をやり取りするために不可欠な部品です.TTLやLVTTL,CMOSなど論理レベルの規定や,VOH/VOL/VIH/VILの関係を理解することで,適切な接続や変換方法を選択できます. 片方向の変換にはオープンドレイン出力や標準ロジックIC,双方向の変換にはMOSトランジスタや専用IC(PCA9306/NVT/NTS/NTB/P3Aシリーズなど)が利用できます. 特にI²CやI3Cなど双方向通信が必要なバスでは,信号方向の自動検出機能を持つ電圧レベル・トランスレータが有効です. また,近年の半導体技術の進化により,低電圧化・高速化が進み,より厳密な電圧レベル管理が求められるようになっています.電圧レベル変換の方法や選択肢は多岐にわたりますが,信号仕様や速度,システムの電源管理など用途に応じて最適な方法・部品を選ぶことが重要です. 5.1 ブログ内で紹介した方式/品番の比較 方式/品番 用途 ビット数 方向切替 オープンドレイン対応 低電圧側[V] 高電圧側[V] ビットレート[bps] オープンドレイン出力での変換 汎用 1 片方向 - - - - 標準ロジック(例:74AVCH4T245) 汎用(パラレルバスなど) 4 + 4 外部制御 非対応 0.8 ~ 3.6 0.8 ~ 3.6 100M ~ 380M 単体MOSトランジスタによる双方向変換 I²C, 汎用 1 自動 対応 トランジスタの仕様による ~ 1M PCA9306 I²C, 汎用 2 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M (2MHz.条件による) NVT2001 I²C, 汎用 1 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M(2MHz@オープンドレイン), 66M(33MHz@最適化条件による) NVT2002 I²C, 汎用 2 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M(2MHz@オープンドレイン), 66M(33MHz@最適化条件による) NVT2003 I²C, 汎用 3 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M(2MHz@オープンドレイン), 66M(33MHz@最適化条件による) NVT2006 I²C, 汎用 6 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M(2MHz@オープンドレイン), 66M(33MHz@最適化条件による) NVT2008 I²C, 汎用 8 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M(2MHz@オープンドレイン), 66M(33MHz@最適化条件による) NVT2010 I²C, 汎用 10 自動 対応 1.0 ~ 3.6 1.8 ~ 5.5 4M(2MHz@オープンドレイン), 66M(33MHz@最適化条件による) NTS0302JK I²C, SPI, 汎用 2 自動 対応 0.95 ~ 3.6 1.65 ~ 5.5 2M @オープンドレイン, 20M @プッシュプル NTS0304E I²C, SPI, 汎用 4 自動 対応 0.95 ~ 3.6 1.65 ~ 5.5 2M @オープンドレイン, 20M @プッシュプル NTS0102 I²C, SPI, 汎用 2 自動 対応 1.65 ~ 3.6 2.3 ~ 5.5 50M @プッシュプル NTS0104 I²C, SPI, 汎用 4 自動 対応 1.65 ~ 3.6 2.3 ~ 5.5 50M @プッシュプル NTB0102 SPI, 汎用 2 自動 非対応 1.2 ~ 3.6 1.65 ~ 5.5 70M ~ 80M NTB0104 SPI, 汎用 4 自動 非対応 1.2 ~ 3.6 1.65 ~ 5.5 70M ~ 80M P3A9606 I3C, I²C, SPI, 汎用 2 自動 対応 0.72 ~ 1.98 0.72 ~ 1.98 (12.5MHz) P3A1604 I3C, I²C, SPI, 汎用 4 自動 対応 0.72 ~ 1.98 1.62 ~ 3.63 6.8M @オープンドレイン, 40M @プッシュプル 表1:ブログ内で紹介した方式/品番の比較   6. 参考資料 製品紹介ページ:電圧レベル変換器 NXP システム・マネジメントI2C, I3C, SPIセレクタ・ガイド I2C バス仕様およびユーザーマニュアル (Rev5.0 日本語版) I2C バス仕様およびユーザーマニュアル (Rev7.0 英語版) NXPコミュニティ・ブログ:I3Cバスの概要 ~次のシリアルバス~ 日本語ウェビナー動画:『【今知っておくべき】次世代インターフェース「I3C」の基礎』  Qiita @teddokano:PCA9306の中身と動作 変更履歴: 2025-08-28:初版 2025-08-28:NTS0304EUK-ARDの紹介と動画公開ブログへのリンクを追記 2026-04-10:表1の低電圧側[V],高電圧側[V]の訂正 2026-06-20:第3.1節「コラム:TTLのVIH(min) = 2.0V,VIL(max) = 0.8Vはどうやって決まっている?」を追加.標準TTLロジックIC:SN7400(2入力NAND)の内部回路例,SN7420の出力波形を追加 2026-07-10:第4.1節に,図15の回路がNexperia社アプリケーションノートAN10441としても公開されている旨を追記 ========================= 本投稿の「Comment」欄にコメントをいただいても、現在返信に対応しておりません。 お手数をおかけしますが、お問い合わせの際には「NXPへの技術質問 - 問い合わせ方法 (日本語ブログ)」をご参照ください。 (既に弊社NXP代理店、もしくはNXPとお付き合いのある方は、直接担当者へご質問いただいてもかまいません。) このブログでは,デジタル回路で使われる論理回路の種類(*TTL,*LVTTL,*CMOS)の電圧レベルの違いから,それを判断する上で重要なV OH /V OL /V IH /V IL の意味について解説します. さらに様々な変換の方法の中から,どのような電圧レベル・トランスレータを選べばよいかを解説します. 特に特別な扱いが必要となる,双方向オープンドレイン信号の変換について詳しく見てみます Interface introduction 日本語ブログ
View full article
[ABUSE] Post By: @RishavKaaraTech / Board: TapLinx-SDK / Reported by: wfxasz wfxasz has reported the post RFIDDiscover tool acquired but how to use it posted by @RishavKaaraTech for the following reasons: Reason: Plagiarism Details: http://www.xe-none.com/topic/10431">purchase augmentin duonasa store check http://fictioneer.org/content/augmentin-cheap-bacterial-infections-rx">how to purchase augmentin https://slp.millingtonpubliclibrary.org/content/augmentin-want-purchase">buy augmentin cheap medication 35009 https://arendville.ru/augmentin-cheap-bacterial-infections-rx">effect augmentin 1000mg price cost http://surfing.4fan.cz/node/231">get not expensive augmentin cod https://mail.reflexologie-cerilly.fr/hi/node/4413">augmentin 375 mg cheap price http://ru.ph-ed-plus.nspu.ru/article/18606">300 mg purchase augmentin https://cadel.ru/forum/augmentin-buy-american-express">to buy augmentin american express https://hr-life.ru/node/53929">buy augmentin free shipping oklahoma https://www.thebiketube.com/cube-jia">pharmacy cavumox augmentin tablet discount https://nsssp-prod-backend.parallelpublicworks.com/node/6702">cheap augmentin jcb western union https://www.rapidservice.com.ec/es/content/1-carga-liviana-977">cavumox 625mg augmentin capsules pharmacy http://wsb2.pl/content/augmentin-buy-online-synermox-order">how to purchase augmentin https://www.thebiketube.com/cube-jia">buy augmentin privately p5dug https://www.tripmayntra.com/augmentin-can-i-purchase-fedex">no script augmentin clavamox legally https://jeunescathos-bxl.org/fr/content/augmentin-purchase-duonasa-store-check">can i purchase augmentin store https://direct.needshub.com/node/28362">augmentin target price http://lsdsng.com/node/4331">can i order augmentin https://www.cableman.ru/node/86272">cheap augmentin tab no doctors https://mail.reflexologie-cerilly.fr/hi/node/4413">purchase augmentin without prescription online https://www.jobwebby.ilovemarkso.com/domainasname-anthony-gmbh/augmentin-no-script-clavamox-legally">wpwlm buy augmentin uk only https://ufa-help.ru/content/augmentin-buy-md-aligne">how to buy augmentin https://www.internationalhumanistparty.org/es/content/augmentin-order-shop">augmentin order samples mastercard website https://wibride.com/your-couple-name-3437">roselle augmentin buy on flintshire http://www.le-cercle-des-sourires.fr/article/augmentin-cheapest-pill-saturday-shipping">pharmacy cavumox augmentin tablet discount http://www.xe-none.com/topic/10431">cost of augmentin xr https://slp.millingtonpubliclibrary.org/content/augmentin-want-purchase">pharmacy tech online augmentin https://hetnieuweteamwerken.be/forums/forum/augmentin-cheap-bacterial-infections-rx">where can i buy augmentin https://www.aairlab.com/IDev/?q=node/372">how to purchase augmentin https://www.ziveknihy.sk/autor/augmentin-buy-cheap-medication-35009">cheap augmentin fedex g6oii http://surfing.4fan.cz/node/231">pharmacy tech online augmentin https://www.flohmy.ch/en/node/4426">300 mg purchase augmentin https://satto.vtranet.com/binh-luan-493">where can i buy augmentin http://fictioneer.org/content/augmentin-cheap-bacterial-infections-rx">roselle augmentin buy on flintshire http://www.xe-none.com/topic/10431">where to order next augmentin https://www.danduo168.com/en/artworks/692/augmentin-1000mg-pharmacy-group">order augmentin store https://enki.ua/advert/17096">augmentin 1000mg pharmacy group https://hr-life.ru/node/53929">want to purchase augmentin https://www.worldcolleges.info/node/29890">pharmacy tech online augmentin https://www.geofak85.ru/augmentin-how-buy">purchase augmentin duonasa store check Post link: https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/RFIDDiscover-tool-acquired-but-how-to-use-it/m-p/2164324#M205 Post author: @RishavKaaraTech | Email Author Reported by: wfxasz | Email Reporter The reported post has 3 replies.
View full article
MC9S12ZVM_AMMCLIB_RTM_1.1.17 NXPテクニカルサポートエンジニア様 こんにちは! 私はMC9S12ZVMシリーズのMCUをベースにしたモーター制御アプリケーション(EPSパワーステアリング)を開発しています。 私の現在のプロジェクトは、古いフルバージョンのライブラリであるMC9S12ZVM_AMMCLIB_RTM_1.1.17に完全に依存しています。 問題の説明: 新バージョン(1.1.35/ 1.1.43)これらはすべて簡略化されたソースコードバージョンであり、gflib.h は含まれていません。gmclib.h、gdflib.hおよび標準のSWLIBS型定義。 私のプロジェクトでは、GFLIB、GDFLIB、GMCLIB、tFrac16、tU8、tBoolなどの構造体を多用していますが、これらは1.1.17の完全プリコンパイル版でのみ正常にコンパイルできます。 過去のバージョンは公式サイトから直接ダウンロードできなくなったため、プロジェクトのビルドに失敗します。 リクエストコンテンツ: MC9S12ZVM_AMMCLIB_RTM_1.1.17 の公式オリジナルインストールパッケージのダウンロードリンクを提供してください。量産プロジェクトのメンテナンスは非常に緊急を要する。 サポートありがとうございます! Re: MC9S12ZVM_AMMCLIB_RTM_1.1.17 こんにちは、トムさん。 AMMCLibの現在のバージョン(1.1.43)下位互換性があり、旧バージョン1.1.17で利用可能だったすべてのヘッダーファイルと型定義が含まれています。私はhttps://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SWS12Z-MMCL1Dから MC9S12ZVM AMMCLib パッケージをダウンロードし、必要なファイルがすべて揃っていることを確認しました。添付のファイルリストを参照してください。
View full article
i.MX95 EVK(19x19):M7 内核上的 CAN1 不工作 我正试图在 i.MX95 19x19 EVK的M7 内核上使用CAN1来接收/发送 CAN 报文。 我使用的是带有 M7 内核的 i.MX95 EVK (19x19),Yocto Linux 在 A 内核上运行,CAN 路由SW9:3 设置为 ON。 我在 M7 内核上使用了 FlexCAN SDK 示例。通过系统管理器,我使用"mm 0x443c01e0 0x6"和"mm 0x443c01e4 0x6"授予 M7 访问这些引脚的权限,但仍然不起作用。 如何在 i.MX95 的 M7 内核上正确启用 FlexCAN1?是否需要其他配置? Re: i.MX95 EVK (19x19): CAN1 on M7 core not working 确保 M7 真正拥有 FlexCAN1 外设 在 i.MX95 上,每个外设默认都归 SCMI/System Manager 所有。 您必须明确授予 FlexCAN1 寄存器 PER:CAN1(AIPSTZ/外设 ID) FlexCAN1 信息 RAM CAN1_MR(独立外设范围) CAN1 I/O 焊盘 与CAN1_TX和CAN1_RX相对应的 GPIO_IOxx 引脚 您的命令 毫米 0x443c01e0 0x6 毫米 0x443c01e4 0x6 只能修改引脚模式, 不能授予 M7权限。 您必须通过 SCFW(系统控制器固件)申请所有权。 在 Cortex-M7 SDK 示例中,可通过以下方式实现: sc_err_t err; err = sc_rm_get_partition(&ptn); err = sc_rm_assign_resource(ptn, SC_R_CAN_1); err = sc_rm_assign_resource(ptn, SC_R_CAN_1_MEM); 显示更多线条 如果缺少这一步,CAN1 寄存器看似 "工作",但实际上什么也没发生。
View full article
S32DS 2.1 如何扩展许可证 如何扩展(或更新)S32DS 许可证?我试着重新安装。但我在办理许可证时被拦住了。 Re: S32DS 2.1 How to extend license 你好,nxp团队,我的 S32DS v2.2许可证即到期了,如何更新?激活代码为1F6D-7D64-6C38-A53C 烦请帮忙延期,谢谢。 Re: S32DS 2.1 How to extend license 是的,它很有效。 但当我点击返回按钮时,却没有成功。 问题解决,安装成功。 谢谢! Re: S32DS 2.1 How to extend license 你好,@kuhruhm、 我发现问题出在旧许可证没有退还。 现在应该修好了。 请尝试使用许可证进行安装。 谢谢!顺祝商祺!  -梅胡尔-帕特尔 Re: S32DS 2.1 How to extend license 我以管理员身份重新尝试。但一切都没有改变。 但停止了在线许可,也没有创建日志。 我的许可证有效期为 2023 年 10 月 1 日 权利到期日为 2027 年 10 月 3 日 这是否意味着我的许可证已激活? Re: S32DS 2.1 How to extend license 你好,@kuhruhm、 正如我在你的日志中看到的以下错误,我认为问题出在安装时没有以管理员模式运行或没有足够的权限。 您的 Windows 用户账户必须是安装指南中提到的管理员组的成员。https://www.nxp.com/docs/en/user-guide/S32DSPAIG.pdf 安装 S32 Design Studio 时不应使用 "以管理员身份运行 "选项。如果在 Windows 权限方面出现错误,那么您很可能没有安装所需的权限。 如果在以管理员模式运行时遇到问题,请联系 IT 部门寻求帮助。 如果您能够进一步移动,请与我们联系。 谢谢!顺祝商祺! - Mehul Patel Re: S32DS 2.1 How to extend license 我的 S32DS 是 2.1 版 我试图在新电脑上安装。 我停止了在线许可,也停止了任务管理器。 c:\NXP\S32DS_Power_v2.1\_S32Power Architecture Design Studio Version 2.1_installation\Logs\ 没有文件。 Re: S32DS 2.1 How to extend license 你好,@kuhruhm、 请分享 .NET Framework 4.0 中的 S32DS 安装日志: C:\NXP\S32DS.3.5\_S32Design Studio for S32 Platform 3.5_安装/日志 谢谢。 顺祝商祺!  - Mehul Patel
View full article
IMX8mp gstreamer vpuenc_h264 set profile and level We are using an IMX8mp on a custom board and are using the NXP Yocto hardknott as the base platform. We are compressing/encoding a camera stream to H264/MP4 using the hardware H264 encoders vpuenc_h264 plugin. A basic example is like: gst-launch-1.0 -v videotestsrc num-buffers=100 ! video/x-raw,width=720,height=576,framerate=25/1 ! vpuenc_h264 ! video/x-h264,profile=main ! h264parse ! mp4mux fragment-duration=10 ! filesink location=/tmp/Video1.mp4 However it appears that the vpuenc_h264 igores the profile= and level= stream parameters. Looking at the imx-gst1.0-plugin code there appears to be no ability to set the H264 profile. Is there any ability to set the H264 hardware encoders profile using gstreamer parameters ? I have seen some things on the Internet that appear to suggest you have to hardcode this setting into the VPU's hardware registers, is this the case ? I note that an alternative (communit?) gstreamer1.0-plugins-imx plugin appears to have support for profile and level. I assume this cannot be used with the softwatre modules/kernel in the NXP fsl-nxp-bsp-hardknott Yocto build ? Re: IMX8mp gstreamer vpuenc_h264 set profile and level Thanks for the corroborating observations. I was similarly seeing v4l2-ctl -d /dev/video1 --all  being deceptive about these encoder parameters, falsely implying they could be changed and that "high" is the default profile Re: IMX8mp gstreamer vpuenc_h264 set profile and level Ok, thanks for the pointer. Information for other users from what I have gathered searching the Internet and looking at the code as there is, typically, lack of NXP documentation available: The H264 encoding profile is hard coded in vpu_wrapper to Baseline. You can change this to Mainline for example (rebuilding vpu_wrapper) and the H264 streams are marked as Mainline. If the actual compression is any different I don't know. The level is set by vpu_wrapper based on the resolution of the video. Not sure if this has any affect other than tagging the H264 stream with this level. It looks like older versions of vpu_wrapper had a bug setting this level incorrectly. If you don't specify a bitrate, at least at the gstreamer vpuenc_h264 level then the resulting stream will have a very low bit rate and thus be very low quality (at least with our video streams (generally static picture with occasional movements)). If not setting the bitrate ends up with the H264 encoder using some variable bitrate algorithm I don't know. Feedback to NXP: There needs to be documentation on the profile, level and bitrate of the H264 encoder, maybe in "i.MX Linux Reference Manual" or other places on this. The NXP gstreamer vpuenc_h264 code should mention this in the code when listing information on the module with gst-inspect-1.0 as a lot of end users will be working at this level. Re: IMX8mp gstreamer vpuenc_h264 set profile and level Hi @TerryBarnaby1, I hope you are doing well   Please find the information related to the same in the below thread. https://community.nxp.com/t5/ i-MX-Processors/Encoding-H- 264-amp-H-265-using-vpu- wrapper-h/m-p/1347610   I hope this information helps you.   Thanks & Regards, Dhruvit Vasavada Re: IMX8mp gstreamer vpuenc_h264 set profile and level in a similar vein, the device seems to falsely advertise force_key_frame (V4L2_BUF_FLAG_KEYFRAME) being possible, when in reality it seems to be completely ignored by the VPU when I send it Re: IMX8mp gstreamer vpuenc_h264 set profile and level Relatedly, I just found another case where NXP lies to us: video_peak_bitrate is completely ignored!
View full article
ADC-DMAはS32K358では動作しません。例 こんにちは、 現在、MBDT 1.8上でXS32K3X8EVB-Q289を使用しており、提供されているADC-DMAのサンプルを試しています。 私が抱えている問題は、以前のチケットで述べたものと同じです。 https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work/mp/2117066#M10292 アプリケーションの動作をFreemaster上で確認したところ、ADC_POT0の値はADCによって一度だけ更新されることがわかりました。ポテンショメータの位置を変更してボードをリセットすると、ADC_POT0の新しい値が設定されますが、それ以上更新されません。 S32DSでデバッグモードに入り、Adc_StartGroupConversion呼び出しにブレークポイントを設定すると、式タブでADC_POT0の値がポテンショメータの位置に応じて変化することが確認できます。 プログラムをブレークポイントなしで実行すると、freemaster の ADC_POT0 の値が更新されません。 この動作は、何らかの理由で ADC_POT0 の値を更新できない freemaster に関連していると考えましたが、ハードウェア割り込みコールバックの最初の行にブレークポイントを設定しても、デバッグモードで Resume を実行しても ADC_POT0 の値が更新されません。 また、ADC値が10000より大きい場合にRGBLED0_BLUEを反転させるという単純なIf文をSimulinkに追加しようとしました。これは、想定されるフリーマスターの問題を回避するためのものですが、この場合はどちらも機能しませんでした...つまり、フリーマスターが問題の原因ではありません。 アイデアが尽きてしまいました。どなたかこの問題について助けていただけませんか? 更新済みのプロジェクトファイルを添付します。 ありがとうございます サイモン  
View full article
MCU1 掩码版本详细信息 您好,NXP团队: 你能否与我们联系 S32K MCU 使用的是哪种类型的 MASK 版本,比如 ROM、Flash 还是 OTP 类型? Re: MCU1 Mask version Details 你好@JANANI_NIVETIDA S32K MCU 使用嵌入式闪存作为程序存储器。它们没有掩膜 ROM 或掩膜 OTP 版本(只有用于内部微调/设置的小 OTP 区域)。 此致, Lukas
View full article