Inquiry: S32N55 system power mode APIs Hello Team,
I learned that the FSS supports 2 APIs which can be used to set the system power mode.
A1, Scmi_SystemPowerRequestProtocolMessageAttributesSynch
A2, Scmi_PowerRequestSystemModeSynch
And A1 can be used to set the cohort mode and state as well. However, there are dedicated cohort APIs to set cohort state, for example: Scmi_BtmWarmResetCohortSynch, Scmi_BtmSuspendCohortSynch.
It seems that the functionality of A1 API overlaps with the other 2 types of APIs.
My question is: What is the A1 API used for? Or what kind of scenario is the A1 API used under?
Best regards,
Tangsheng.
FSS_FW Priority: MEDIUM Re: Inquiry: S32N55 system power mode APIs Thanks Marius, explain the confusion very clearly. Re: Inquiry: S32N55 system power mode APIs Hi @Tangsheng_Zhou ,
The Power Domain protocol and the Boot protocol were the original protocols added for Tunis; for various reasons, this was well adapted to the Tunis usecases but not fully compatible with the SCMI spec; as a result, alongside adding support for Luxor platform we added also the System Power protocol, which is the ARM SCMI compliant one -> hence the overlap.
In terms of implementation and future support:
- APIs like Scmi_SystemPowerStateSetSynch( ) are implemented as wrappers over the Btm_* APIs, both are going to be supported and both are going to do the exact same thing; Autosar/Tunis users can use the existing Btm APIs, while Linux is expected to use the new SystemPower APIs.
APIs from PowerDomain protocols like Scmi_PowerRequestSystemModeSynch are going to be deprecated and anyway everyone is recommended to use the new, SCMI compatible API of SystemPower.
Internally we have ticket for tracking the UserManual updates and clarifications. FSF-29425
Thanks,
Marius
記事全体を表示