RT1176 SFPD QSPI IS25LP064D-JKLE I am attempting to flash a custom RT1176 board that implements FlexSPI1 in the same manner as the eval board, except I have supplied flash VCC with 3.3V to support the IS25LP064D-JKLE I am trying to use. I have attached my flexspi_nor_config.c and memory setup. I am using the default flexspi_nor_polling_transfer_cm7. When I debug with Link Application to RAM Enabled, it returns "Program data - read out data value incorrect !" (line 125). I have yet to figure out what the issue is in my configuration. I am currently using an MCU Link MR, but also have access to a Jlink. My custom board has DIP Switches, and I have bootmode 1 set to 1 and bootmode 0 set to 0. Re: RT1176 SFPD QSPI IS25LP064D-JKLE Hi @AnteoJ ,
Thanks for your interest in NXP MIMXRT series!
The flash used by the RT1020-EVK happens to be ISSI_IS25LP064A, so you can find the corresponding flexspi_nor_config.c in its SDK . Please check this first.
Also, when replacing the flash you can first pass the tests of the built-in templates in SEC/MCUBootUtility, which are able to shield your own flash from LUT issues.
Best regards, Gavin Re: RT1176 SFPD QSPI IS25LP064D-JKLE I have gone through and replaced values for my specific flash according to the datasheet although I still run into a IMPRECISERR and UNDEFINSTR when I start up debug. I am not sure if there are additional parameters that need to be adjusted. Here is my code so far: /* * Copyright 2018-2022 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #include "evkbmimxrt1170_flexspi_nor_config.h" /* Component ID definition, used by tools. */ #ifndef FSL_COMPONENT_ID #define FSL_COMPONENT_ID "platform.drivers.xip_board" #endif /******************************************************************************* * Code ******************************************************************************/ #if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1) #if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__) __attribute__((section(".boot_hdr.conf"), used)) #elif defined(__ICCARM__) #pragma location = ".boot_hdr.conf" #endif #define FLASH_DUMMY_CYCLES 0x03 #define FLASH_DUMMY_VALUE 0x03 const flexspi_nor_config_t qspiflash_config = { .memConfig = { .tag = FLEXSPI_CFG_BLK_TAG, .version = FLEXSPI_CFG_BLK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally, .csHoldTime = 3u, .csSetupTime = 3u, // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock .controllerMiscOption = 0x10, .deviceType = kFlexSpiDeviceType_SerialNOR, .sflashPadType = kSerialFlash_4Pads, .serialClkFreq = kFlexSpiSerialClk_60MHz, .sflashA1Size = 8u * 1024u * 1024u, /* Enable flash configuration feature */ .configCmdEnable = 1u, .configModeType[0] = kDeviceConfigCmdType_Generic, /* Set configuration command sequences */ .configCmdSeqs[0] = { .seqNum = 1, .seqId = 12, .reserved = 0, }, /* Prepare setting value for Read Register in flash */ .configCmdArgs[0] = (FLASH_DUMMY_VALUE << 4), .lookupTable = { // Read LUTs [0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x20), [1] = FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, FLASH_DUMMY_CYCLES, READ_SDR, FLEXSPI_4PAD, 0x04), // Read Status LUTs [4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05, READ_SDR, FLEXSPI_1PAD, 0x04), // Write Enable LUTs [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP, FLEXSPI_1PAD, 0x0), // Erase Sector LUTs [4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x20, RADDR_SDR, FLEXSPI_1PAD, 0x18), // Erase Block LUTs [4 * 8 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD8, RADDR_SDR, FLEXSPI_1PAD, 0x18), // Pape Program LUTs [4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x02, RADDR_SDR, FLEXSPI_1PAD, 0x18), [4 * 9 + 1] = FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_1PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0), // Erase Chip LUTs [4 * 11 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x60, STOP, FLEXSPI_1PAD, 0x0), // Set Read Register LUTs [4 * 12 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC0, WRITE_SDR, FLEXSPI_1PAD, 0x01), [4 * 12 + 1] = FLEXSPI_LUT_SEQ(STOP, FLEXSPI_1PAD, 0x00, 0, 0, 0), }, }, .pageSize = 256u, .sectorSize = 4u * 1024u, .ipcmdSerialClkFreq = 0x1, .blockSize = 64u * 1024u, .isUniformBlockSize = false, }; #endif /* XIP_BOOT_HEADER_ENABLE */
查看全文