Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
デンバーのモバイルアプリ開発会社はどこでエンド・ツー・エンド・サービスを提供していますか? デンバーでエンドツーエンドのサービスを提供する モバイルアプリ開発会社 をお探しなら、 JPLoft は検討する価値があります。16+年の経験と1,250+件のプロジェクトを手がけ、JPLoftはUI/UXデザイン、iOSおよびAndroid開発、AI統合、テスト、展開、リリース後のサポートを含む完全なモバイルアプリ開発ソリューションを提供しています。 同社はスタートアップや企業がビジネスニーズに合わせたスケーラブルで使いやすいモバイルアプリの開発を支援しています。  
View full article
i.MX 8M Plus Custom Board: ums and fastboot commands fail with "USB init failed: -22" in U-Boot 2024 I am experiencing an issue bringing up USB peripheral functions (ums and fastboot) on a custom hardware platform based on the i.MX 8M Plus running U-Boot v2024.04 (built via Yocto). When trying to export the eMMC as mass storage or invoke fastboot, the controller fails to initialize and throws an invalid argument error (-22):   u-boot=> ums 0 mmc 2 UMS: LUN 0, dev mmc 2, hwpart 0, sector 0x0, count 0x3a3e000 Couldn't init USB controller. u-boot=> fastboot 0 USB init failed: -22 Environment & Setup Context: U-Boot Version: 2024.04 (PV="2024.04" confirmed via BitBake environment check). Hardware: Custom board. Unlike the reference i.MX 8M Plus EVK, this design does not feature a standard Type-C Port Controller (TCPC) chip on the I2C bus. Current Software Adjustments: We currently include a patch to bypass errors inside board/freescale/imx8mp_evk/imx8mp_evk.c so the bootloader does not completely abort initialization when the TCPC functions fail to locate the I2C device. The Problem: Even with the boot abort bypassed, the USB stack rejects the initialization commands with error code -22 (EINVAL). We want to verify whether this failure is directly related to how the missing TCPC state handles dynamic role assignment, or if there is a fundamental driver model / device tree framework configuration mismatch required for USB peripheral operation on custom i.MX 8M Plus layouts when deviating from the reference EVK design. Questions: What are the common structural or configuration causes for the -22 (EINVAL) error when invoking fastboot or ums on an i.MX 8M Plus platform under U-Boot 2024.04? How should a custom board without the reference EVK's Type-C setup correctly configure its board file or device tree properties to safely enable standalone USB device/peripheral functionality? Any insights or debugging pointers would be appreciated 
View full article
IMX93 Metering Application I am currently working on an energy metrology project and would like to port the metrology libraries from the TWR-KM35Z75M platform to an i.MX 93-based board, where the Cortex-M33 core will be used for the metrology application. I would appreciate guidance on the following: Recommended approach for porting the metrology libraries to the i.MX 93 M33 core. Any hardware or software dependencies that need to be considered. Availability of reference designs, application notes, or migration guides. Existing examples of metrology implementations on the i.MX 93 platform. Best practices for interfacing ADC data acquisition and maintaining metrology accuracy on the new platform. Any implementation steps, references, or experiences from similar migrations would be greatly appreciated. Thank you. Power Re: IMX93 Metering Application It seems all of your questions are already being tracked in https://nxp.lightning.force.com/lightning/r/Case/500Te00000gKfLQIA0/view Most require confirmation from our internal team. Please follow the updates there. Thanks.
View full article
IMX93 メーターアプリケーション 現在、エネルギー計測プロジェクトに取り組んでおり、 TWR-KM35Z75M プラットフォームの計測ライブラリを i.MX 93ベースのボードに移植し、 Cortex-M33コア を計測応用に使う予定です。 以下の点についてご指導いただければ幸いです。 計測ライブラリをi.MX 93 M33コアに移植するための推奨アプローチ。 考慮すべきハードウェアやソフトウェアの依存関係について。 リファレンス・デザイン、アプリケーションノート、または移行ガイドの入手可能性。 i.MX 93プラットフォーム上の計測実装の既存例。 ADCデータ取得のインターフェースおよび新プラットフォームでの計測精度維持のベストプラクティス。 同様の移行に関する実装手順、参考資料、または経験談などがあれば、大変ありがたいです。 よろしくお願いします。 パワー Re: IMX93 Metering Application ご質問はすべて、 https://nxp.lightning.force.com/lightning/r/Case/500Te00000gKfLQIA0/viewで既に追跡されているようです。 ほとんどの場合、社内チームによる確認が必要です。最新情報はそちらでご確認ください。 ありがとうございます。
View full article
i.MX 8M Plusカスタムボード:U-Boot 2024でumsおよびfastbootコマンドが「USB初期化失敗:-22」で失敗する i.MX 8M Plusをベースにしたカスタムハードウェアプラットフォーム(U-Boot v2024.04(Yocto経由で構築)でUSBペリフェラル機能(UMSやfastboot)を起動する際に問題が発生しています。 eMMCをマスストレージとしてエクスポートしたりfastbootを呼び出しようとすると、コントローラーが初期化に失敗し、無効な引数エラー(-22)を出します:   u-boot=> ums 0 mmc 2 UMS: LUN 0、開発 MMC 2、hwpart 0、セクター 0x0、カウント 0x3a3e000 USBコントローラを起動できませんでした。 u-boot=> fastboot 0 USB初期化失敗: -22 環境とセットアップのコンテキスト: U-Boot バージョン: 2024.04 (PV="2024.04"BitBake環境チェックで確認済み。 ハードウェア:カスタム基板。8M Plus EVK i.MX 参照モデルとは異なり、この設計には標準的なType-Cポートコントローラ(TCPC)チップがI2Cバスに搭載されていません。 現在のソフトウェア調整: 現在、board/freescale/imx8mp_evk/imx8mp_evk.c内のエラーを回避するためのパッチを含んでいますそのため、TCPC機能がI2Cデバイスを特定できなくても、ブートローダーは初期化を完全に中止しません。 問題: ブート中止を回避した場合でも、USBスタックは初期化コマンドをエラーコード-22(EINVAL)で拒否します。 この失敗が、欠損したTCPC状態が動的役割割り当てをどのように処理するかに直接関係しているのか、あるいはカスタム i.MX 8M Plusレイアウト上のUSBペリフェラル動作に必要な根本的なドライバーモデルやデバイスツリーフレームワークの設定ミスマッチが、参照EVKデザインから逸脱した場合に必要かどうかを確認したいと考えています。 質問: U-Boot 2024.04の下で i.MX 8M Plusプラットフォーム上でfastbootやumsを呼び出す際に-22(EINVAL)エラーが起こる一般的な構造的または構成原因は何ですか? リファレンスEVKのType-Cセットアップを使わないカスタムボードは、ボードファイルやデバイスツリーのプロパティを正しく設定して、スタンドアロンのUSBデバイスやペリフェラル機能を安全に有効化させるにはどうすればよいのでしょうか? 何かご意見やデバッグのヒントがあれば幸いです。
View full article
Which Denver mobile app development company offers end-to-end services? If you're looking for a mobile app development company in Denver that offers end-to-end services, JPLoft is worth considering. With 16+ years of experience and 1,250+ projects delivered, JPLoft provides complete mobile app development solutions, including UI/UX design, iOS and Android development, AI integration, testing, deployment, and post-launch support. The company helps startups and enterprises build scalable, user-friendly mobile apps tailored to their business needs.  
View full article
Recommendation for NXP i.MX Processor for 1080p RTSP IP Camera Hi everyone, Could anyone suggest the lowest cost NXP i.MX processor that can handle a 1080p RTSP IP camera stream? My requirements are:     1 RTSP IP camera input    2 1080p resolution    3 Around 25–30 FPS    4 Looking for the lowest-cost i.MX processor/board that can handle this reliably The main goal is to receive and process/display a  1080p RTSP camera stream at the lowest possible hardware cost. If anyone has tested a low-cost i.MX processor for a similar use case, please share your recommendation and experience. Thanks! Re: Recommendation for NXP i.MX Processor for 1080p RTSP IP Camera Hello, For a pure receive/display application using an IP Camera, you can consider i.MX8MM since includes a dedicated hardware VPU capable of 1080p60 decode. Best regards.
View full article
Correct snvs_cfg values for TAMPER_OUT0/TAMPER_IN4 active tamper loop on i.MX8DXL EVK (J20) Hi, I'm validating the external active-tamper loop on the i.MX8DXL EVK (MCIMX8DXL-WEVK) via U-Boot. From the board schematic, I've confirmed J20 (TAMPER header, 1x3) is wired as: - Pin 1 = TAMPER_IN4 (net SNVS.TAMPER_IN4, ball AJ13) - Pin 2 = GND - Pin 3 = TAMPER_OUT0 (net SNVS.TAMPER_OUT0, ball AP22) These are dedicated SNVS pins, not shared with SAI2/SAI3 like TAMPER_OUT1-4/IN0-3. Available U-Boot commands: tamper_pin_cfg, snvs_cfg (with sub-registers hp.lock, hp.secvio_intcfg, hp.secvio_ctl, lp.lock, lp.secvio_ctl, lp.tamper_filt_cfg, lp.tamper_det_cfg, lp.tamper_det_cfg2, lp.tamper_filt1_cfg, lp.tamper_filt2_cfg, lp.act_tamper1_cfg through lp.act_tamper5_cfg, lp.act_tamper_ctl, lp.act_tamper_clk_ctl, lp.act_tamper_routing_ctl1, lp.act_tamper_routing_ctl2), snvs_sec_status, snvs_clear_status. Since TAMPER_OUT0/TAMPER_IN4 form an active tamper pair, my questions: 1. Which lp.act_tamperN_cfg channel (1-5) corresponds to TAMPER_OUT0? 2. What values for lp.act_tamper_routing_ctl1/routing_ctl2 route TAMPER_OUT0's pattern to be checked against TAMPER_IN4? 3. What value for lp.act_tamper_clk_ctl enables the pattern clock for this channel? 4. What value for lp.act_tamper_ctl globally enables active tamper detection for this channel? Goal: closing a jumper across J20 pins 1-3 should read as secure in snvs_sec_status, and opening it should trigger a violation. Is there a reference test procedure or app note for external active tamper validation on i.MX8DXL? Thanks!
View full article
将自定义模型从 S32K3xx MBDT 1.5.0 迁移到 1.8.0,硬件设置错误 您好,NXP支持团队, 我们需要您的帮助,将现有的 Simulink 模型从 S32K3xx 的基于模型的设计工具箱 1.5.0 版迁移到 1.8.0 版。 我们的模型集成了我们自定义的 IOC 工具箱,之前一直使用 MBDT 1.5.0 版本。升级到 1.8.0 版本后,在使用 MATLAB/Simulink R2024b 时,我们的工程师在打开模型的硬件设置时遇到了错误。 重现步骤如下: 1. 安装适用于 S32K3xx 的 MBDT 版本 1.8.0。 2. 打开我们现有的演示模型,IOC_DemoPrj.slx。 3. 选择硬件 → 硬件设置。 “配置参数”对话框无法打开,并显示以下错误: 输出参数“out”(以及其他可能的参数)未赋值 在执行“mbd_s32k3.nxp.target.get_target_memory_entries”时 功能。 对话框中还提到了 getTargetHardwareDetailWidgets.p。请查看附件截图以获取完整信息。 我们已就此问题联系了 MathWorks 技术支持,案例编号为 #09014041。他们建议我们咨询 NXP,因为 MBDT 插件是由 NXP 开发的;根本原因尚未得到确认。 请问您能否帮我们解决以下问题? 1. 迁移流程:将模型从 MBDT 1.5.0 迁移到 1.8.0 的支持流程是什么?是否有迁移指南或转换工具可用,我们是否可以直接升级? 2. 错误诊断:get_target_memory_entries 错误是已知问题吗?是否有适用的补丁或解决方法? 3. 现有配置:该型号的硬件、目标内存或外设配置是否需要转换或重新生成?如果需要,在无法打开硬件设置的情况下,我们应该如何执行此操作? 4. 自定义 IOC 工具箱:这些版本之间的哪些更改可能需要更新我们的自定义模块、模型回调或构建集成?请指出相关的接口和建议的更改。 5. 诊断信息:您需要哪些模型文件、配置文件、日志和安装详细信息来确定这是迁移问题、安装/路径问题还是自定义工具箱集成问题? 我们的目标是保留现有的 IOC 功能,并进行必要的更改,以便使用 MBDT 1.8.0 成功配置、构建和运行模型。 谢谢。
View full article
セーフティ機構 SM1。INTERCONNECT_EDC _GASKET SM1を有効にする必要があります。INTERCONNECT_EDC_GASKET私のプロジェクトのためのセーフティ機構です。コードを生成するためにAUTOSAR RTD 3.0.0とS32 Design Studio(S32DS)ツールを使っています。 以下の点を明確にしていただけますか? 1. S32DS内にこのセーフティ機構を有効にするオプションはありますか?もしあれば、どうやって有効にするか教えていただけますか? 2. S32DSでこのオプションが利用できない場合、有効にするための推奨される方法は何ですか?可能であれば、サンプルコードを共有してください。 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、@sandeepSingh18606 さん。 S32K3XXはセーフティ ペリフェラル ドライバを使いましょう。 https://www.nxp.com/docs/en/product-brief/S32K-SPDPB.pdf ドライバはS32K3xx Standard SWパッケージに含まれています: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D S32K3 Safety Peripheral ドライバ バージョン 1.0.3 は RTD 3.0.0 と互換性があります。 eMCEMドライバでは、利用可能なすべての故障を有効化できます。 danielmartynek_1-1789975567252.png SPDパッケージにはEB Tresosのデモが1枚含まれています。 S32DS には、利用可能な SPD の例が 1 つだけあります (SPD 1.0.6、RTD 7.0.0): https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-BIST-eMCEM-SPD106-v2-0-S32DS365-RTD700/ta-p/2373113 よろしくお願いいたします。 ダニエル Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET SPDは無料ではなく、パッケージ購入が必要だと思います。 SM1メカニズムはNXPによって実装されているため、ユーザーはこれを有効にするだけで済みます。しかし、NXP RTDはこの機能をサポートしていません。 SPDパッケージがない場合、推奨されるアプローチは何でしょうか? Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、@sandeepSingh18606 さん。 セーフティ ペリフェラル ドライバ (SPD) は無料で利用可能で、RTDの拡張版です。一方、Safety Software Framework(SAF)は有料のプレミアムソフトウェアです。 以下のドキュメントを参照してください: https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF よろしくお願いいたします。 ダニエル Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、@sandeepSingh18606 さん。 リストに載っていないのに、どうやってインストールしたのですか? まず、お使いのRTDリリースと互換性のあるバージョンが必要です。 SPDのリリースノートによると: SPD v1.0.3:このSPDバージョンはS32K3リアルタイムドライバーバージョン3.0.0と互換性がありますおよび 3.0.0P07。 SPD v1.0.4:このSPDバージョンはS32K3リアルタイムドライバーバージョン4.0.0およびS32K3リアルタイムドライバーバージョン3.0.0と互換性がありますP07(S32K324_MAPBGA257派生機種向けのTresosバージョン)。 最新バージョンであるv1.0.5およびv1.0.6は、より新しいRTDリリースとのみ互換性があります。 例えば、更新サイトのZIPパッケージをダウンロードしてください:S32K3_SPD_1.0.3_DS_updatesite.zip その後、S32 Design Studioの拡張機能の下で更新サイトを追加します。 ありがとうございました。 BR、ダニエル Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET それは「前の項目」タブにありますが、あなたのアカウントではそのタブが非アクティブになっているようです。 管理を担当しているチームに確認してみます。 できるだけ早くご連絡いたします。 よろしくお願いいたします。 ダニエル Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、ダニエルさん。 現在、RTS 3.0.0を使用しています。ご提案いただいたように、SPD v1.0.3が必要なのですが、NXPのウェブサイトでこのバージョンを見つけることができません。 どこで見つけられるか、直接リンクを教えていただけませんか? Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、ダニエルさん。 確認ありがとうございます。 S32 Design StudioでSPDドライバーをインストールしようとしましたが、インストール後もS32DSの拡張機能やアップデートで見つかりません。 以下は、現在私のシステムにインストールされているRTDのスクリーンショットです。 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、サンディープさん。 今すぐアカウントをご確認ください。 お知らせ下さい。 ありがとうございます。 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET こんにちは、ダニエルさん。 今は以前のバージョンにアクセスできるようになりました。サポートありがとうございます。
View full article
LPC54608 内部温度传感器 我尝试按照 LPC54608 用户手册中的说明配置内部温度传感器的 ADC,但我无法读取正确的值。我还使用了数据表中给出的斜率和偏移量值。 Re: LPC54608 Internal temperature sensor Hello 能否请您确认一下,您是否以ADC的示例作为基准?如果是,请指出是哪一种; 您是否已将输入 ADC 通道 0 和输入选择寄存器配置为 3,以便选择温度传感器? 更多详细信息,请参阅LPC546xx 用户手册[UM10912]中的第 44.6.2 章。 如果您能提供更多关于您如何配置ADC温度传感器的详细信息,那就太好了。 根据LPC546xx 产品数据手册第 7.22 章, “上电后,温度传感器的输出必须稳定下来才能用作精确的ADC输入。为了使ADC能够精确测量温度传感器的值,必须将ADC配置为单通道突发模式。九次(或更多次)转换突发信号的最后一个值可以提供精确的结果。”因此,可能是您的温度传感器尚未稳定,或者您需要在单通道突发模式下进行更多转换。 您还应该考虑优化ADC外部电路,以最大限度地减少与外部环境相关的ADC误差。 本应用笔记可以帮助您了解如何在应用中提高模拟数字变流器的精度。 此致敬礼,路易斯 Re: LPC54608 Internal temperature sensor 我的配置方式如下: 1. 清除 ADC、VREFP、VDDA、TS、ANA 并等待 20 微秒 2. ADC 时钟使能,AHBCLKCTRL0。 3. 使用 PRESETCTRL0 寄存器清除 ADC0 外设复位。 4. 在 INSEL 中设置温度通道 5. 启用ADC,并使用ctrl寄存器中的CLKDIV将时钟频率设置为15MHz。 5. 设置同步模式,12 位分辨率,BYPASS = 0,TSAMP = 0 6. 然后在 SEQA_CTRL 中配置序列 A,CHANNELS = 1,TRIGGER = 0,TRIGPOL = 0,SYNCBYPASS = 0,BURST = 0,SINGLESTEP = 0,LOWPRIO = 0,MODE = 0,SEQA_ENA = 1 7. 设置 CALIB = 1 并等待 CALIB = 0 8. 然后通过 START 位开始转换,读取结果 但每次结果都一样,并且 DATA VALID 没有被设置。
View full article
LPC54608 Internal temperature sensor I tried to configure ADC for internal temperature sensor as given in LPC54608 user manual, but i couldn't read correct values. I used the slope, offset values given in data sheet also. Re: LPC54608 Internal temperature sensor Hello Could you help us confirm if you have used an example for the ADC as a base? If so, indicate which; Have you configured the input ADC Channel 0 and Input Select Register as 3 so you can select temperature sensor? For more detailed information, kindly refer to Chapter 44.6.2 in LPC546xx User manual[UM10912] If you could bring more details about, how did you configure the ADC temperature sensor, please. According to LPC546xx Product data sheet Chapter 7.22, "After power-up, the temperature sensor output must be allowed to settle to its stable value before it can be used as an accurate ADC input. For an accurate measurement of the temperature sensor by the ADC, the ADC must be configured in single-channel burst mode. The last value of a nine-conversion (or more) burst provides an accurate result." Therefore, it could be that your Temperature sensor is not settle yet or you need to make more conversions in single channel burst mode. You also should consider optimize the ADC external circuit to minimize the ADC error related to external environment. This Application Note can help you in How to Increase the Analog-to-Digital Converter Accuracy in an Application Best Regards, Luis Re: LPC54608 Internal temperature sensor I have configured in the following manner: 1. Cleared ADC, VREFP, VDDA, TS, ANA & wait for 20us 2. ADC clock enable, AHBCLKCTRL0. 3. Clear the ADC0 peripheral reset using the PRESETCTRL0 register 4. set temperature channel in INSEL 5. Enable ADC & set clock to 15MHz using CLKDIV in ctrl register 5. Set Synchronous mode , 12-bit resolution, BYPASS = 0, TSAMP = 0 6. then configures sequence A in SEQA_CTRL, CHANNELS = 1, TRIGGER = 0, TRIGPOL = 0, SYNCBYPASS = 0, BURST = 0, SINGLESTEP = 0, LOWPRIO = 0, MODE = 0, SEQA_ENA = 1 7. SET CALIB = 1 & waited till CALIB = 0 8. then started conversion by START bit, read result but result is same everytime & DATA VALID is not setting.
View full article
LPC54608 内部温度センサー ユーザーマニュアルに記載されているように内部温度センサ用にADCを設定しようLPC54608が、正しい値を読み取ることができませんでした。データシートに記載されている傾きとオフセットの値も使用しました。 Re: LPC54608 Internal temperature sensor Hello ADCの例をベースに使ったことがあるか確認していただけますか?もしそうなら、どの作品かを示してください。 入力ADCチャネル0と入力選択レジスタを3に設定して温度センサーを選択できるようにしましたか? 詳細については、LPC546xxユーザーマニュアルの第44.6.2章[UM10912]をご参照ください。 もしADC温度センサーをどのように設定したのか、もう少し詳しく教えていただければ教えてください。 LPC546xx製品データシート第7.22章によると、 「電源アップ後、温度センサの出力は安定した値に落ち着くまで待たなければ、正確なADC入力として使用できません。ADCによる温度センサの正確な測定のためには、ADCをシングルチャネルバーストモードに設定する必要があります。9回以上の変換バーストの最後の値が正確な結果を提供します。」したがって、温度センサがまだ安定していないか、単一チャネルバーストモードでさらに変換が必要な可能性があります。 また、外部環境に関連するADC誤差を最小限に抑えるために、ADC外部回路の最適化も検討すべきです。 この応用ノートは、アプリケーションにおけるアナログ-デジタル変換器の精度を高める方法に役立ちます 敬具、ルイス Re: LPC54608 Internal temperature sensor 私は以下のように設定しました。 1. ADC、VREFP、VDDA、TS、ANAをクリアし、20μs待機します。 2. ADCクロック有効化、AHBCLKCTRL0。 3. PRESETCTRL0レジスタを使ってADC0ペリフェラルリセットをクリアする 4. INSELで温度チャネルを設定する 5. ADCを有効にし、制御レジスタのCLKDIVを使用してクロックを15MHzに設定します。 5. 同期モード、12ビット分解能、BYPASS = 0、TSAMP = 0 に設定します。 6. 次にシーケンスAをSEQA_CTRLで構成します。チャネル = 1、TRIGGER = 0、TRIGPOL = 0、SYNCBYPASS = 0、BURST = 0、SINGLESTEP = 0、LOWPRIO = 0、MODE = 0、SEQA_ENA = 1 7. CALIB = 1 に設定し、CALIB = 0 になるまで待機する 8. 次にSTARTビットで変換を開始し、結果を読み取る しかし、結果は毎回同じで、DATA VALID は設定されていません。
View full article
功能安全 SM1.INTERCONNECT_EDC_GASKET 我的项目中需要启用 SM1.INTERCONNECT_EDC_GASKET 安全机制。我使用的是 AUTOSAR RTD 3.0.0 和 S32 Design Studio (S32DS) 工具来生成代码。 请您澄清以下问题: 1. S32DS 中是否有启用此功能安全机制的选项?如果有,能否指导我如何启用? 2. 如果S32DS中没有此选项,那么启用它的推荐方法是什么?如果可以,请提供示例代码。 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 你好@sandeepSingh18606 , 为 S32K3xx 使用功能安全外围设备驱动程序。 https://www.nxp.com/docs/en/product-brief/S32K-SPDPB.pdf 驱动程序包含在 S32K3xx 标准软件包中: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D S32K3 功能安全外围设备驱动程序版本 1.0.3 与 RTD 3.0.0 兼容。 在 eMCEM 驱动程序中,可以启用所有可用的故障。 danielmartynek_1-1789975567252.png SPD 软件包包含一个 EB Tresos 演示程序。 对于 S32DS,目前只有一个 SPD 示例可用(SPD 1.0.6,RTD 7.0.0): https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-BIST-eMCEM-SPD106-v2-0-S32DS365-RTD700/ta-p/2373113 此致, 丹尼尔 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 你好@sandeepSingh18606 , 功能安全外围驱动器 (SPD) 可免费使用,它是 RTD 的扩展。而功能安全软件框架(SAF)是一款付费高级软件。 请参阅以下文档: https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF 此致, 丹尼尔 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 我认为SPD不是免费的,需要购买套餐才能使用。 由于 SM1 机制由 NXP 实现,用户只需启用它即可。但是,NXP RTD 不支持此功能。 如果没有 SPD 软件包,推荐的方法是什么? Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 你好@sandeepSingh18606 , 如果列表中没有列出安装方法,你是如何安装的? 首先,你需要一个与你的RTD版本兼容的版本。 根据西雅图警察局发布的公告: SPD v1.0.3:此SPD版本与S32K3实时驱动程序3.0.0版兼容。以及 3.0.0P07。 SPD v1.0.4:此SPD版本与S32K3实时驱动程序4.0.0版和S32K3实时驱动程序3.0.0版兼容。P07(Tresos 版本,适用于 S32K324_MAPBGA257 衍生产品)。 较新的版本 v1.0.5 和 v1.0.6 仅与较新的 RTD 版本兼容。 下载更新站点 ZIP 包,例如:S32K3_SPD_1.0.3_DS_updatesite.zip 然后,在 S32 设计工作室的“扩展”下添加更新站点。 谢谢! BR,丹尼尔 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 嗨,丹尼尔, 谢谢你的确认。 我尝试在 S32 Design Studio 中安装 SPD 驱动程序,但即使安装后,我仍然无法在 S32DS 扩展和更新下找到它们。 以下是我的系统上当前安装的RTD的屏幕截图: Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 您可以在“上一页”选项卡中找到它,但该选项卡在您的帐户中似乎处于非活动状态。 我需要向负责管理这个项目的团队确认一下。 我会尽快回复您。 此致, 丹尼尔 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 嗨,丹尼尔, 我目前使用的是 RTS 3.0.0。根据您的建议,我需要 SPD v1.0.3,但我无法在 NXP 网站上找到此版本。 请问您能否告知我可以在哪里找到它,或者提供一个直接链接? Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 你好,桑迪普, 请立即查看您的账户。 请告诉我。 谢谢 Re: Safety Mechanism SM1.INTERCONNECT_EDC _GASKET 嗨,丹尼尔, 我现在可以访问之前的版本了。谢谢支持。
View full article
カスタムモデルをS32K3xx MBDT 1.5.0から1.8.0へ移行中ハードウェア設定エラー NXPサポートチームの皆さん、こんにちは。 既存のSimulinkモデルをModel-Based Design Toolbox for S32K3xxバージョン1.5.0からバージョン1.8.0へ移行する際のご協力をお願いしています。 当社のモデルはカスタムIOCツールボックスを組み込み、以前はMBDT 1.5.0で動作していました。MATLAB/Simulink R2024bを使用して1.8.0にアップグレードした後、エンジニアはモデルのハードウェア設定を開く際にエラーに直面しました。 再現手順は以下のとおりです。 1. S32K3xxバージョン1.8.0用のMBDTをインストールする。 2. 既存のデモモデル、IOC_DemoPrj.slxを開きます。 3. ハードウェア→ハードウェア設定を選択します。 設定パラメータダイアログが開かず、次のエラーが表示されます。 出力引数「out」(およびその他の引数)に値が割り当てられていません 「mbd_s32k3.nxp.target.get_target_memory_entries」を使用した実行において 関数。 このダイアログには、getTargetHardwareDetailWidgets.p への参照も含まれています。メッセージ全文については、添付のスクリーンショットをご覧ください。 私たちはCASE #09014041でMathWorksのテクニカルサポートに連絡しました。彼らはMBDTアドオンがNXPが開発しているため、NXPに相談するよう勧めました。根本原因はまだ確認されていません。 以下の点についてご協力いただけますか? 1. 移行手順:MBDT 1.5.0から1.8.0へのモデル移行にはどのような手順が適用されていますか?移行ガイドや変換ユーティリティが利用可能で、直接アップグレードは可能ですか? 2. エラー診断:このget_target_memory_entriesエラーは既知の問題ですか?適用可能なパッチや回避策はありますか? 3. 既存構成:モデルのハードウェア、ターゲットメモリ、またはペリフェラルの設定は変換または再生が必要ですか?もしそうなら、ハードウェア設定が開けない場合、どのように実行すればよいでしょうか? 4. カスタムIOCツールボックス:これらのバージョン間で、カスタムブロックの更新、モデルコールバック、ビルド統合が必要な変更点は?関連するインターフェースと推奨変更点をご確認ください。 5. 診断情報:移行、インストール/パス、カスタムツールボックス統合の問題かを判断するために、どのようなモデルファイル、設定ファイル、ログ、インストールの詳細が必要ですか? 私たちの目標は、既存のIOC機能を維持しつつ、MBDT 1.8.0でモデルを成功裏に設定・構築・実行するために必要な変更を行うことです。 ありがとう。
View full article
更正 i.MX8DXL EVK (J20) 上 TAMPER_OUT0/TAMPER_IN4 活动防篡改循环的 snvs_cfg 值 您好, 我正在通过 U-Boot 验证 i.MX8DXL EVK (MCIMX8DXL-WEVK) 上的外部主动篡改循环。 根据电路板原理图,我已经确认 J20(防篡改接头,1x3)的接线方式如下: - 引脚 1 = TAMPER_IN4(网络 SNVS.TAMPER_IN4,焊球 AJ13) - 引脚 2 = 接地 - 引脚 3 = TAMPER_OUT0(网络 SNVS.TAMPER_OUT0,引脚 AP22) 这些是专用的 SNVS 引脚,不像 TAMPER_OUT1-4/IN0-3 那样与 SAI2/SAI3 共享。 可用的 U-Boot 命令:tamper_pin_cfg、snvs_cfg(及其子寄存器 hp.lock、hp.secvio_intcfg、hp.secvio_ctl、lp.lock、lp.secvio_ctl、lp.tamper_filt_cfg、lp.tamper_det_cfg、lp.tamper_det_cfg2、lp.tamper_filt1_cfg、lp.tamper_filt2_cfg、lp.act_tamper1_cfg 至 lp.act_tamper5_cfg、lp.act_tamper_ctl、lp.act_tamper_clk_ctl、lp.act_tamper_routing_ctl1、lp.act_tamper_routing_ctl2)、snvs_sec_status、snvs_clear_status。 由于 TAMPER_OUT0/TAMPER_IN4 构成一个有效的防篡改对,我的问题是: 1. lp.act_tamperN_cfg 通道(1-5)中,哪个对应于 TAMPER_OUT0? 2. 要检查 lp.act_tamper_routing_ctl1/routing_ctl2 路由 TAMPER_OUT0 的模式与 TAMPER_IN4 的匹配度,需要检查哪些值? 3. 要使该通道启用模式时钟,lp.act_tamper_clk_ctl 的值是多少? 4. lp.act_tamper_ctl 的全局值是多少才能启用此通道的主动篡改检测? 目标:将跳线连接到 J20 引脚 1-3 时,snvs_sec_status 应显示为安全状态;断开跳线时,应触发违规。 i.MX8DXL 是否有针对外部主动防篡改验证的参考测试程序或应用说明? 谢谢您!
View full article
about imx6q ddr stresstest I am running a DDR stress test on the i.mX6Q and need to know which Excel file to use. I have obtained `MX6Q_SabreSD_DDR3_register_programming_aid_v2.5.xlsx`; does this appear to be the correct file? I am currently using Samsung K4B4G16 256M×16 chips (4 chips totaling 2GB), but the test fails to complete, returning the error "No chip select is enabled." How can I resolve this issue? Thanks. Re: about imx6q ddr stresstest Hi @GavinChen  This RPA table is right for i.MX6Q. please share your RPA able. B.R
View full article
1080p RTSP IPカメラ用のNXP i.MX プロセッサの推奨 こんにちは、皆さん 1080p RTSP IPカメラストリームを処理できる、最も安価なNXP i.MX プロセッサーを誰か教えてもらえますか? 私の要望は以下の通りです。 1つのRTSP IPカメラ入力 2 1080p解像度 3 約25~30 FPS 4 この問題を安定して扱える、最も低コストで i.MX プロセッサ/ボードを探しています 主な目的は、可能な限り低いハードウェアコストで1080pのRTSPカメラストリームを受信し、処理/表示することです。 もし同じようなケースで低コストの i.MX プロセッサを試したことがある方がいれば、ぜひおすすめや体験を共有してください。 よろしくお願いします! Re: Recommendation for NXP i.MX Processor for 1080p RTSP IP Camera こんにちは、 IPカメラを使った純粋な受信・表示アプリケーションとしては、i.MX8MMを検討してください。なぜなら、1080p60デコード対応の専用ハードウェアVPUが含まれているからです。 よろしくお願いいたします。
View full article
关于 imx6q DDR 压力测试 我正在对 i.mX6Q 进行 DDR 压力测试,需要知道应该使用哪个 Excel 文件。 我已获取到 `MX6Q_SabreSD_DDR3_register_programming_aid_v2.5.xlsx` 文件;请问这是否是正确的文件? 我目前使用的是三星 K4B4G16 256M×16 芯片(4 颗芯片共 2GB),但测试未能完成,并返回错误“未启用芯片选择”。 我该如何解决这个问题? 谢谢。 Re: about imx6q ddr stresstest 嗨@GavinChen 此 RPA 表适用于 i.MX6Q。 请分享您的RPA能力。 B.R
View full article
Migrating custom model from S32K3xx MBDT 1.5.0 to 1.8.0, Hardware Settings error Hi NXP Support Team, We need your assistance migrating an existing Simulink model from Model-Based Design Toolbox for S32K3xx version 1.5.0 to version 1.8.0. Our model incorporates our custom IOC toolbox and previously worked with MBDT 1.5.0. After upgrading to 1.8.0 while using MATLAB/Simulink R2024b, our engineer encounters an error when opening the model’s Hardware Settings. The steps to reproduce are: 1. Install MBDT for S32K3xx version 1.8.0. 2. Open our existing demo model, IOC_DemoPrj.slx. 3. Select HARDWARE → Hardware Settings. The Configuration Parameters dialog fails to open and displays this error: Output argument "out" (and possibly others) not assigned a value in the execution with "mbd_s32k3.nxp.target.get_target_memory_entries" function. The dialog also references getTargetHardwareDetailWidgets.p. Please see the attached screenshot for the full message. We contacted MathWorks Technical Support under case #09014041. They advised us to consult NXP because the MBDT add-on is developed by NXP; the root cause has not yet been confirmed. Could you please help us with the following? 1. Migration procedure: What is the supported process for migrating a model from MBDT 1.5.0 to 1.8.0? Is a migration guide or conversion utility available, and can we upgrade directly? 2. Error diagnosis: Is this get_target_memory_entries error a known issue? Are there any applicable patches or workarounds? 3. Existing configuration: Does the model’s hardware, target memory, or peripheral configuration need conversion or regeneration? If so, how should we perform this when Hardware Settings cannot open? 4. Custom IOC toolbox: Which changes between these versions could require updates to our custom blocks, model callbacks, or build integration? Please identify the relevant interfaces and recommended changes. 5. Diagnostic information: What model files, configuration files, logs, and installation details would you need to determine whether this is a migration, installation/path, or custom toolbox integration issue? Our goal is to retain the existing IOC functionality and make the changes necessary to configure, build, and run the model successfully with MBDT 1.8.0. Thanks.
View full article