2416166_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2416166_en-US

2416166_en-US

Migrating custom model from S32K3xx MBDT 1.5.0 to 1.8.0, Hardware Settings error

Hi NXP Support Team,


We need your assistance migrating an existing Simulink model from Model-Based Design Toolbox for S32K3xx version 1.5.0 to version 1.8.0.
Our model incorporates our custom IOC toolbox and previously worked with MBDT 1.5.0. After upgrading to 1.8.0 while using MATLAB/Simulink R2024b, our engineer encounters an error when opening the model’s Hardware Settings.


The steps to reproduce are:

1. Install MBDT for S32K3xx version 1.8.0.
2. Open our existing demo model, IOC_DemoPrj.slx.
3. Select HARDWARE → Hardware Settings.
The Configuration Parameters dialog fails to open and displays this error:
Output argument "out" (and possibly others) not assigned a value
in the execution with "mbd_s32k3.nxp.target.get_target_memory_entries"
function.

The dialog also references getTargetHardwareDetailWidgets.p. Please see the attached screenshot for the full message.


We contacted MathWorks Technical Support under case #09014041. They advised us to consult NXP because the MBDT add-on is developed by NXP; the root cause has not yet been confirmed.


Could you please help us with the following?
1. Migration procedure: What is the supported process for migrating a model from MBDT 1.5.0 to 1.8.0? Is a migration guide or conversion utility available, and can we upgrade directly?
2. Error diagnosis: Is this get_target_memory_entries error a known issue? Are there any applicable patches or workarounds?
3. Existing configuration: Does the model’s hardware, target memory, or peripheral configuration need conversion or regeneration? If so, how should we perform this when Hardware Settings cannot open?
4. Custom IOC toolbox: Which changes between these versions could require updates to our custom blocks, model callbacks, or build integration? Please identify the relevant interfaces and recommended changes.
5. Diagnostic information: What model files, configuration files, logs, and installation details would you need to determine whether this is a migration, installation/path, or custom toolbox integration issue?
Our goal is to retain the existing IOC functionality and make the changes necessary to configure, build, and run the model successfully with MBDT 1.8.0.

Thanks.

Tags (1)
No ratings
Version history
Last update:
Friday
Updated by: