Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
GUIDER 2.0 インターフェース最適化に関する提案 こんにちは: 1. イベントのスケール変更後、接続矢印の位置が正しくなく、ずれが生じます。 2. このイベント内のコンテンツ(他の要素を含む)は、中国語の文字をサポートしたり、マウスカーソルを重ねたときに中国語の説明を表示したりできますか? 回复: GUI GUIDER 2.0界面优化建议 こんにちは、 @ALVANさん 貴重なご提案をありがとうございます。いただいたご意見は、GUIガイドチームに伝え、さらに検討・検討していただきます。   BR ハリー
View full article
S32K5 supports various peripheral parameters I'd like to know which peripherals the S32K5 supports, and how many ports each peripheral has. Re: S32K5支持的各项外设参数 Hello @TAlice, All of the currently available information is provided in the K5's product page: S32K5 Auto General-Purpose MCUs | NXP Semiconductors. When S32K5 is publicly launched, specific peripheral information will be available. If you require further details, please contact your NXP distributor or assigned sales. Best regards, Julián
View full article
Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot builds Hi, we are using NXP Android Automotive 16.0.0_1.3.0 with kernel 6.12 and the prebuilt revisions documented by NXP: platform/prebuilts/clang/host/linux-x86 66acdd82ee62e4aaa4248f03191c59dfed9db193 kernel/prebuilts/build-tools 3c5e4f14b451ec85167c38b917d2459687abd7f4 platform/prebuilts/rust 5156e7f81ae254c79ee736e44c960e75ad685c67 platform/prebuilts/clang-tools 17329f6590e2872dcf04a0c96a176be089470cd9 These are the revisions listed in the NXP Android Automotive User's Guide for this release. The build works with these revisions, but our container vulnerability scan reports several HIGH and CRITICAL findings inside the supplied Android prebuilts. For example, the Clang prebuilts contain embedded Go standard libraries. For clang-r536225/bin/clang, the scan reports: Total: 22 HIGH: 21 CRITICAL: 1 Go stdlib version: v1.23.2 Example: CVE-2025-68121 crypto/tls - incorrect certificate validation The same finding pattern also appears in clang++ and clang-tidy, and in the newer clang-r547379 binaries where the embedded Go version is v1.23.4. The NXP-pinned kernel/prebuilts/build-tools also contains affected soong_zip binaries with the same Go-stdlib finding pattern. The Rust prebuilts also contain findings in shipped Cargo lock files, for example: thin-vec 0.2.13 CVE-2026-6654 fixed in 0.2.16 hashbrown 0.15.0 GHSA-wwq9-3cpr-mm53 fixed in 0.15.1 We do not want to replace the documented revisions with arbitrary newer AOSP commits, because these prebuilts are part of the NXP kernel/U-Boot build environment and we want to preserve compatibility with Android Automotive 16.0.0_1.3.0 / kernel 6.12. Are there newer NXP-recommended or known-compatible commit IDs for these prebuilts? In particular, we are looking for updated revisions for: platform/prebuilts/clang/host/linux-x86 kernel/prebuilts/build-tools platform/prebuilts/rust platform/prebuilts/clang-tools   Has NXP, or anyone in the community, already updated these revisions and verified that the following still work? Ideally, we would also like confirmation that a complete Android Automotive build still works with the updated prebuilts. We would prefer to update the affected prebuilts instead of permanently suppressing the security findings. I have attached the failed vulnerability scan log for reference. It contains the complete findings for the affected Clang, kernel build-tools and Rust prebuilts, including detected embedded versions and available fixed versions. Thanks. Android Re: Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot bu Hello, I'm reviewing your issue, I'll keep you updated.  Regards. Re: Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot bu Hello,  Internal team has shared below reply.   We have not any newer recommended/know-compatible commit IDs for  platform/prebuilts/clang/host/linux-x86 kernel/prebuilts/build-tools platform/prebuilts/rust platform/prebuilts/clang-tools and for Android 16.0 automotive 1.3.0 release version.   Android 16.0 automotive 1.3.0 has been released on May-21 2026, since then there have been no updates for this release. We do not update Android automotive releases; we are working on the next Android automotive release => Android 16.0 automotive 2.1.0 based on Linux kernel 6.18.y & with updated Linux kernel build tools. External release date of AA16.0 2.1.0 is on Oct-13 2026.
View full article
T1042NXE BSDL 文件 您好,我正在寻找该组件的BSDL文件: T1042NXE7PQB BGA780 你能把文件发给我吗? 谢谢! Re: T1042NXE BSDL file 你好, 您的元器件T1042NXE7PQB的 BSDL 文件包含在T1040/T1042 组合 BSDL 文件(文件名: T1040_and_T1042_1.1.bsdl )中。这个文件同时适用于 T1040 和 T1042 处理器。 如何下载 该文件可直接在 NXP 产品页面的“设计资源”→“设计文件”→“模型”下找到: T1040/42 的 BSDL 文件 — 下载(需要账号) 文件代码: T1040-T1042-BSDL 修订版:R1A(2019年2月20日) 大小:110.13 KB 此致 Re: T1042NXE BSDL file 你好, 谢谢你的回答。
View full article
LX2080A Linux 开发支持 – Yocto 和 Buildroot 你好, 我正在使用 NXP LX2080A 平台,并希望开发一个嵌入式 Linux 系统。 我想了解恩智浦为LX2080A提供的Linux开发支持。 Yocto是否获得官方支持?如果可以,我可以在哪里找到 NXP Yocto 电路板支持包。/层? Buildroot 是否正式支持 LX2080A? NXP是否有推荐的用于Linux开发的BSP/SDK? 请分享相关文档、源代码库或指南。 谢谢! Re: LX2080A Linux Development Support – Yocto and Buildroot 请参阅https://www.nxp.com/webapp/Download?colCode=LX2160ARDBGSG ,第 11 页。 通过将 SW3[1:3] 从 111 改为 110,该板将作为 LX2080A 平台启动。 任何所需的 RCW、ATF 或其他软件修改将取决于您的具体硬件设计,并且可能与参考 LX2160ARDB 实现有所不同。 谢谢。 Re: LX2080A Linux Development Support – Yocto and Buildroot 你好, 谢谢你提供的信息。 我想澄清一下关于LX2080A的一点。 如果我们使用 LX2160A-RDB 软件和参考配置在 LX2080A 上启用 Linux,是否需要对 RCW(重置配置字)或 ATF(TF-A)配置进行任何更改以支持 LX2080A? 具体来说,LX2160A-RDB 使用的 RCW 和 ATF 配置是否可以用于 LX2080A,还是需要对 LX2080A 进行修改? 谢谢。 Re: LX2080A Linux Development Support – Yocto and Buildroot LX2080A 属于 LX2 系列,而 LX2 系列普遍支持 Linux 软件。LX2160A-RDB 通常用作软件启用的参考硬件平台。 对于 Linux 开发,支持 Layerscape Yocto BSP (LDP Yocto)。源代码和图层可从以下网址获取: https://github.com/nxp-qoriq/yocto-sdk/tree/walnascar 请参考:UG10374 和 UG10381。 NXP 的官方 Linux 支持基于 Layerscape LDP / Yocto 版本。我们没有为 LX2080A 提供专用的 Buildroot 电路板支持包 版本。 Layerscape LDP 页面提供以下最新软件版本、文档和支持的设备信息: https://www.nxp.com/design/design-center/software/embedded-software/cross-platform-embedded/layerscape-linux-distribution-poc:LAYERSCAPE-SDK 谢谢!
View full article
How to escalate a problem with AT&T? Facing an AT&T problem that keeps going unresolved? AT&T Escalation Support Team
View full article
Android オートモーティブ 16.0.0_1.3.0向けのセキュリティアップデート済みプリビルドで、カーネルやU-Bootビルドを壊さずに提供されました こんにちは、 NXPの Android オートモーティブ 16.0.0_1.3.0をカーネル6.12 と、NXPが文書化したプリビルドのリビジョンを使用しています。 プラットフォーム/Prebuilts/Clang/Host/Linux-x86 66acdd82ee62e4AAAA4248F03191C59DFED9DB193 カーネル/prebuilts/build-tools 3c5e4f14b451ec85167c38b917d2459687abd7f4 プラットフォーム/prebuilts/rust 5156e7f81ae254c79ee736e44C960e75AD685C67 プラットフォーム/prebuilts/clang-tools 17329f6590e2872dcf04a0c96a176be089470cd9 これらは本リリースのNXP Android Automotiveユーザーガイドに記載された改訂版です。 ビルドはこれらのリビジョンで動作しますが、当社のコンテナ脆弱性スキャンでは、 提供されたAndroidプリビルト内でいくつかのHIGHかつCRITICALな発見が報告されています。 例えば、Clangのプリビルド版にはGoの標準ライブラリが組み込まれています。clang-r536225/bin/clang のスキャン結果は以下のとおりです。 合計: 22 高: 21 重大: 1 Go stdlib バージョン: v1.23.2 例: CVE-2025-68121 crypto/tls - 証明書の検証が正しく行われていない 同様の検出パターンは、clang++ および clang-tidy、そして組み込みの Go バージョンが v1.23.4 である新しい clang-r547379 バイナリでも見られます。 NXPが固定しているkernel/prebuilts/build-toolsにも、同じGo-stdlib検出パターンを持つ、影響を受けるsoong_zipバイナリが含まれています。 Rustのプリビルド版には、出荷されるCargoロックファイルに含まれる発見事項も含まれています。例えば、以下のとおりです。 thin-vec 0.2.13 CVE-2026-6654 は 0.2.16 で修正されました。 hashbrown 0.15.0 GHSA-wwq9-3cpr-mm53 は 0.15.1 で修正されました。 これらのプリビルドはNXPカーネル/U-Bootビルド環境の一部であり、 Android Automotive 16.0.0_1.3.0 / カーネル6.12との互換性を維持したいため、ドキュメント化されたリビジョンを任意の新しいAOSPコミットで置き換えるつもりはありません。 これらのプリビルド製品に対応する、NXPが推奨する、または互換性が確認されている新しいコミットIDはありますか? 特に、以下の項目に関する最新の改訂版を求めています。 platform/prebuilts/clang/host/linux-x86 カーネル/prebuilts/build-tools platform/prebuilts/rust platform/prebuilts/clang-tools   NXP社、あるいはコミュニティの誰かが、これらの改訂版を既に更新し、以下の内容が引き続き正常に動作することを確認しましたか? 理想的には、更新されたプリビルト車と完全なAndroid Automotiveビルドがまだ動作するかどうかの確認も望んでいます。 セキュリティ調査結果を恒久的に抑制するよりも、影響を受けたプリビルトを更新したいと考えています。 参考までに、失敗した脆弱性スキャンログを添付しました。これには、影響を受けるClang、カーネルビルドツール、およびRustのプリビルド版に関する完全な調査結果が含まれており、検出された組み込みバージョンと利用可能な修正バージョンも含まれています。 ありがとうございます。 Android Re: Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot bu こんにちは、 ご指摘いただいた件について調査中です。進捗状況は随時ご連絡いたします。 よろしくお願いします。 Re: Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot bu こんにちは、 社内チームから以下の回答が寄せられました。 推奨/互換性のある新しいコミット ID はありません。 プラットフォーム/プリビルト/CLANG/ホスト/Linux-x86 kernel/prebuilts/build-tools プラットフォーム/プレビルド/錆 プラットフォーム/プレビルド/クラングツール そしてAndroid 16.0のオートモーティブ向け1.3.0リリースバージョンです。   Android 16.0 オートモーティブ 1.3.0は2026年5月21日にリリースされましたが、それ以降はアップデートはありません。Androidオートモーティブのアップデートは行っていません。次回のAndroid オートモーティブ リリースに取り組んでいます => Android 16.0 automotive 2.1.0Linuxカーネル6.18.yをベースにし、最新のLinuxカーネルビルドツールを用いています。 AA16.0 2.1.0の外部リリース日は2026年10月13日です。
View full article
UTEST書き込みデータ処理 こんにちは Utestにデータを書き込むには、データの消去が必要ですか? UTEST_program.jpegUTEST_program.jpeg AN13388では、UTESTセクターにデータを書き込むプロセスは、他のブロックにプログラムを書き込むプロセスと同じであると述べられている。 しかし、UTESTは一度しか実行されないプログラムなので、書き込み前に消去する必要があるのでしょうか? リカ 回复: UTEST写数据流程 また、UTESTのどの部分をDEBUGデバッグを使って変更できるのかも知りたいです。 Re: UTEST写数据流程 最初に消去しないでください。UTESTセクターはOTP(ワンタイムプログラマブル)です。 Example_S32K344_decouple_RTD400_Ip_C40_DS35には、参考としてUTESTのサンプルが含まれています。 申し訳ありませんが、「UTEST中にDEBUGで変更できる領域」の意味が分かりませんでした。デバッグ中にレジスタを操作して、標準のフラッシュプログラムシーケンス(AN13388で説明されているのと同じプロセス)を実行するという意味でしょうか?S32K3XXRM.pdf Rev12の「表837」を参照してください。「ライフサイクルとビット構成に基づくデバッグアクセス」という表現は、ライフサイクルのさまざまな段階におけるデバッグ権限について言及しています。これは、あなたが言及している内容でしょうか? 添付ファイルS32K3xx_DCF_clients.xlsxからS32K3XXRM.pdfにあるUTESTメモリマップテーブルの「アクセス権限」列と「プログラム作成者」列は、アクセス権限を示しています。また、異なるライフサイクルごとに異なる色で読み取り/書き込み権限が示されています。 Re: UTEST写数据流程 はい、デバッグ中に、レジスタ操作による標準フラッシュプログラムシーケンスを実行することで、CUST_DEL LCステージのUTESTの内容を変更することは可能ですか?1から0へのいくつかの位置をクリアしたいのです。 Re: UTEST写数据流程 utest nvm ユーザー空間プログラミングの回答を参照してください。 Re: UTEST写数据流程 はい、どうもありがとうございました。
View full article
LX2080A Linux開発サポート – YoctoおよびBuildroot こんにちは、 私はNXPのLX2080Aプラットフォームを使っており、組み込みLinuxシステムを開発したいと考えています。 NXPが提供しているLinux開発サポートについて知りたいLX2080A。 Yoctoは公式にサポートされていますか?もしそうなら、NXP Yocto BSPやレイヤーはどこで手に入りますか? BuildrootはLX2080Aで正式にサポートされていますか? Linux開発におすすめのNXPのBSP/SDKはありますか? 関連するドキュメント、ソースリポジトリ、またはガイドを共有してください。 よろしくお願いします。 Re: LX2080A Linux Development Support – Yocto and Buildroot https://www.nxp.com/webapp/Download?colCode=LX2160ARDBGSGの11ページを参照してください。 SW3[1:3]を111から110に変更することで、ボードはLX2080Aプラットフォームとして起動します。 必要なRCW、ATF、その他のソフトウェア変更は、あなたのハードウェア設計によって異なり、リファレンスLX2160ARDB実装とは異なる場合があります。 ありがとうございます。 Re: LX2080A Linux Development Support – Yocto and Buildroot こんにちは、 情報ありがとうございます。 LX2080Aに関して、一点だけ明確にしておきたいと思います。 LX2080A上でLX2160A-RDBソフトウェアとLinuxイネーブルメントのリファレンス構成を使用する場合、LX2080AをサポートするためにRCW(リセット設定ワード)やATF(TF-A)の設定に変更が必要ですか? 具体的には、LX2160A-RDBに使われているRCWとATFの設定をLX2080Aにも使えるのか、それともLX2080A向けに変更する必要があるのか? ありがとうございます。 Re: LX2080A Linux Development Support – Yocto and Buildroot このLX2080AはLX2ファミリに属し、LinuxソフトウェアのサポートはLX2ファミリ全体で共通しています。LX2160A-RDBは通常、ソフトウェア実現のためのリファレンスハードウェアプラットフォームとして使用されます。 Linux開発にはLayerscape Yocto BSP(LDP Yocto)がサポートされています。ソースコードとレイヤーは、 https://github.com/nxp-qoriq/yocto-sdk/tree/walnascarから入手できます。 UG10374およびUG10381を参照してください。 NXPの公式LinuxイネーブルメントはLayerscapeのLDP / Yoctoリリースに基づいています。LX2080A専用のBuildroot BSPリリースは提供しておりません。 Layerscape LDPページには、最新のソフトウェアリリース、ドキュメント、サポートデバイス情報が以下に掲載されています。 https://www.nxp.com/design/design-center/software/embedded-software/cross-platform-embedded/layerscape-linux-distribution-poc:LAYERSCAPE-SDK よろしくお願いします。
View full article
如何升级AT&T的问题? 遇到始终无法解决的AT&T问题?请联系AT&T升级支持团队。
View full article
UTEST写数据流程 您好 请问往Utest中写入数据需要擦除吗 UTEST_program.jpegUTEST_program.jpeg The AN13388 said the process to write a data in the UTEST Sectorr is the same process used to program in other blocks. 但是UTEST属于一次性编程,写入前需要擦除吗? Lika 回复: UTEST写数据流程 同时我想知道UTEST哪些区域可以通过DEBUG调试修改 Re: UTEST写数据流程 不要先擦除,UTEST Sector 属于OTP (One Time Programmable)。 Example_S32K344_decouple_RTD400_Ip_C40_DS35 这里有写UTEST的例程可供你参考。 抱歉我没明白“UTEST哪些区域可以通过DEBUG调试修改”。请问你是指调试的时候通过操作寄存器执行标准的 Flash Program 序列(与 AN13388 中描述的流程相同)?S32K3XXRM.pdf Rev12 的"Table 837. Debug access based on LifeCycle and bit configurations" 有提到不同LifeCycle阶段的调试权限,请问你是指这个? S32K3XXRM.pdf的附件S32K3xx_DCF_clients.xlsx 的 UTEST Memory Map 表格Accessibility、Programmed by列有写明权限。另外不同的颜色表示不同LifeCycle时候的读写权限。 Re: UTEST写数据流程 对的,调试的时候通过操作寄存器执行标准的Flash Program序列可以在CUST_DEL LC阶段修改UTEST内容吗,我想将一些位置的1清0 Re: UTEST写数据流程 请参考 utest nvm user space programming 里的答复。 Re: UTEST写数据流程 好的,非常感谢
View full article
AT&Tで問題をエスカレートさせるにはどうすればよいですか? 解決されていない AT&T の問題に直面していますか? AT&T エスカレーションサポートチーム
View full article
PCF2123TS-1,118の外観バリエーションに関するお問い合わせ NXPチーム様:PCF2123TS-1,118チップ2リールの入荷検査中に、2種類の異なる外観タイプを発見しました。タイプ1:表面が光沢があり、ピン1のインジケータが小さく、側面のテクスチャは光沢があり、わずかに湾曲しています。タイプ2:表面が粗く、ピン1のインジケータが大きく、側面のテクスチャは粗く、直線的です。これらの違いは正常な状態でしょうか?ご回答をお待ちしております。よろしくお願いいたします。劉
View full article
如果我使用的是树莓派 Pico 2W,如何在 Arduino IDE 中查看 Serial.prints 的输出? 我花了很多时间试图弄明白这件事,但最终一无所获。我尝试运行一个简单的代码,让内置 LED 闪烁,同时在 Serial.print 中打印“hello”。LED 指示灯闪烁,但 pico 没有在串口监视器中输出任何内容。我发现 pico 在上传后会断开连接,然后重新连接,但连接的是不同的端口。我猜我的板是从 COM 5/4 重新连接到 COM 11,但是如果我尝试进入“工具”->“端口”->“COM 11”,LED 指示灯停止闪烁,IDE 显示错误信息,我的笔记本电脑发出类似板断开连接又重新连接的声音。我能做些什么吗?我考虑过从 Arduino IDE 切换到 VS Code,但是没有关于如何在 Windows 上进行切换的教程,而 GPT 也没有教会我太多东西。 Kinetis W系列MCU
View full article
How can I see the Serial.prints in Arduino IDE if I am using a raspberry pi pico 2w? I spent a lot of hours trying to figure this out and I didn't manage to do anything. I tried to run a simple code that makes the built in LED blink while also writing "hello" at Serial.print. The LED blinks, but the pico does't print anything in the serial monitor. I found out the pico disconnects after the upload and then reconnects again, but on a different port. I guess mine reconnects from com 5/4 to com 11 but if I try to go to Tools -> Port -> COM 11 the LED stops blinking, the IDE shows me an error message and my laptop makes the sound as if the board was disconnected and connected again. Is there something I can do about this? I took into consideration switching from arduino ide to vs code, but there are no tutorials on how to do that for windows and GPT didn't teach me much. Kinetis W Series MCUs
View full article
Raspberry Pi Pico 2Wを使っている場合、Arduino IDEでSerial.printsを見るにはどうすればいいですか? 何時間もかけて解決しようと試みましたが、結局何もできませんでした。内蔵LEDを点滅させながら、Serial.printに「hello」と書き込む簡単なコードを実行してみました。LEDは点滅するが、ピコはシリアルモニターに何も出力しない。アップロード後にピコが切断され、その後別のポートで再接続されることが分かりました。私のはcom 5/4からcom 11に再接続されるようですが、Tools -> Port -> COM11に行こうとするとLEDが点滅し、IDEにエラーメッセージが表示され、ノートPCは基板が外されて再接続されたかのような音を出します。これについて何かできることはありますか?Arduino IDEからVS Codeに切り替えることも考えましたが、Windows用のチュートリアルがなく、GPTもあまり教えてくれませんでした。 Kinetis Wシリーズ・マイクロコントローラ
View full article
Inquiry on PCF2123TS-1,118 Appearance Variation Dear NXP team: During incoming inspection of two reels of PCF2123TS-1,118 chips, we discovered two different appearance types: Type 1: Glossy surface, smaller pin 1 indicator; glossy and slightly curved side texture. Type 2: Rough surface, larger pin 1 indicator; rough and straight side texture. Are these differences normal? We look forward to your reply. Thank you! Sincerely, Ms. Liu
View full article
Inquiry on PCF2123TS-1,118 Appearance Variation 尊敬的恩智浦团队:在对两卷PCF2123TS-1,118芯片进行来料检验时,我们发现了两种不同的外观类型:类型1:表面光亮,引脚1指示器较小;侧面纹理光亮且略微弯曲。类型2:表面粗糙,引脚1指示器较大;侧面纹理粗糙且平直。请问这些差异是否属于正常现象?期待您的回复。谢谢!此致,刘小姐
View full article
如何获取适用于 S32K3 的“HSE-B 固件参考手册 V2.2”? 您好,NXP团队, 我正在开发一个基于 S32K312 的项目,需要使用 HSE(硬件安全引擎)来实现安全启动/密钥管理/加密服务。 我正在寻找名为“HSE-B固件参考手册V2.2”的文档,但在NXP的公开网站上找不到。 非常感谢您的支持! 顺祝商祺! Re: How to get access to "HSE-B Firmware Reference Manual V2.2" for S32K3? 嗨@SpringAutumn 所有 HSE 文件均受保密协议约束,仅可通过安全文件获取。如果您还没有访问安全文件的权限,请按照“安全访问权限 | NXP Semiconductors”页面上概述的步骤申请相应的权限。 另外,请注意,HSE-B 固件参考手册的最新版本为 2.8 版。 BR,VaneB
View full article
LX2160ARDB:DDR验证 您好, 我们已将 LSDK 中的 RCW 文件 (rcw_2200_750_2900_19_5_2.bin) 加载到 SD 卡中,在 DDR 配置面板中,读取 SPD完成后,出现“不支持的原始卡版本。请手动将 CLK 设置为 DQS 偏移值。” 如何在QCVS工具中对LX2160ARDB执行DDR验证 Priyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.png Re: LX2160ARDB: DDR validation 嗨,六月卢, 感谢您的支持 对于 USB 接口,该命令的结果是: (bin)51% findcc cwtaps 0 (箱)51% 以及以太网连接 (bin)51% findcc cwtaps FSL07E3D5 (10.1.66.150):CodeWarrior TAP v2 Cortex-10探针尖端 启动加载程序 v1.0.1 操作系统版本 1.0.5 1 目前我们能否使用以太网连接进行 DDR 验证? Re: LX2160ARDB: DDR validation (bin)52% 显示 cc 0:USB 开路失败 未配置任何命令变流器。 这表明无法通过 USB 连接检测到 CWTAP。 请检查 USB 连接线连接情况,并确保主机能够正确识别 CWTAP。 另外,请运行以下命令并分享结果: (bin)6% findcc cwtaps 谢谢。 Re: LX2160ARDB: DDR validation 嗨,六月卢, CodeWarrior 版本- Priyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.png (bin)49% log v CCS Linux 版本 503.0.0.220812-p0 详细日志记录 (bin)50% 全部删除 (bin)51% 配置 cc cwtap (bin)52% 显示 cc 0:USB 开路失败 未配置任何命令变流器。 (箱)53% (bin)53% 源 IDcode.tcl 正在扫描通过 USB 连接的可用 TAP…… 未找到通过 USB 连接的 TAP ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ + + 可用的远程连接 + +1 - CodeWarriorTAP - +2 - GigabitTAP - + + x - 不进行任何更改地退出脚本 + ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ 指定连接方式: 无法读取“CONNECTION()”:数组中不存在此元素 (箱)54% (箱)54% 能够通过以太网连接并 ping 通目标设备。即使将 CodeWarrior 更新到 v11.5.12 版本后,读取 SPD 仍然显示“不支持的原始卡版本。请手动设置 CLK 到 DQS 偏移值。” 谢谢 Re: LX2160ARDB: DDR validation 请从“帮助”→“关于 CodeWarrior Development Studio for QorIQ LS Series (ARM v8 ISA)”确认 CodeWarrior 版本。 请按照“CCS Windows Release Build 503.0.0.220812-p0.txt”中的说明验证连接状态。 我们建议先测试 USB 连接,然后再测试以太网连接。 IP地址似乎已更改。请问您是否可以成功 ping 通目标设备? Re: LX2160ARDB: DDR validation 嗨,六月卢, 我们使用的是 CodeWarrior 11.5.0,DIMM 是 LX2160ARDB 主板原装的内存条。 CodeWarrior 已更新,存档为com.freescale.armv8.11.5.12.GA.Lin.updatesite.221209.zip适用于 v11.5.12 现在无法检测到JTAG Priyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.png 谢谢 Re: LX2160ARDB: DDR validation 我按照你的步骤操作,成功读取了SPD数据。 请问您使用的是哪个版本的CodeWarrior?是 CodeWarrior 11.5.12 吗? 另外,这个内存条是原装的吗? 谢谢。 Re: LX2160ARDB: DDR validation 嗨,六月卢, 通过 FlexSPI 启动后,使用 tftpboot 在 u-boot 中加载 RCW 文件,并执行如下 mmc 写入命令。 => tftpboot 0x90000000 rcw_2200_750_2900_19_5_2.bin -> mmc 设备 0;mmc 写入 0x90000000 8 1 => qixis_reset sd(执行此命令期间,D19 被打开和关闭) 对于 DDR 配置,从 SPD 读取时显示“不支持的原始卡版本。请手动将 CLK 设置为 DQS 偏移值。” Re: LX2160ARDB: DDR validation 如何将 LSDK 中的 RCW 文件(rcw_2200_750_2900_19_5_2.bin)加载到 SD 卡中? D19 是否已开启和关闭? 您可以参考以下关于使用 QCVS 工具对 LX2160ARDB 进行 DDR 验证的信息: QCVS_DDR_用户指南 谢谢! Re: LX2160ARDB: DDR validation (bin)50% 全部删除 (bin)51% 配置 cc cwtap:10.1.66.150 (bin)52% 显示 cc (bin)53% 源 IDcode.tcl 如果您能找到与“CCS Windows 版本 503.0.0.220812-p0.txt”相同的 LX2160A。 您可以使用以太网连接,IP 地址为:10.1.66.150 进行 DDR 验证。 谢谢! Re: LX2160ARDB: DDR validation 这是截图成功的结果。 June_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.png 我使用 USB 连接到 CWTAP。您需要为探测器设置正确的 IP 地址。 您能否成功运行“诊断连接”? June_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.png Re: LX2160ARDB: DDR validation 嗨,六月卢, 通过以太网连接,并能找到文本文件中提供的 LX2160A。 Priyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.png 但读取 SPD 时,DDR 配置窗口中显示“不支持的原始卡版本。请手动设置 CLK 到 DQS 偏移值。” 如何验证SPD值是否读取成功? Re: LX2160ARDB: DDR validation 连接诊断成功 Priyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.png 读取 SPD 后,DDR 配置如下所示 Priyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.png 请问DDR验证是否已成功启动? 我遇到的问题是, “开始验证”按钮已启用,但验证开始后立即被取消了。 Re: LX2160ARDB: DDR validation 嗨,六月卢, 按照用户指南,我再次创建了一个项目来进行DDR配置,并已完成SPD读取,如下所示。 Priyaa_0-1788498272408.pngPriyaa_0-1788498272408.pngPriyaa_0-1788498272408.pngPriyaa_0-1788498272408.png DIMM 模块插入 RDB 的 J14、J17 连接器中。 Re: LX2160ARDB: DDR validation 嗨,六月卢, 将开关(SW1)切换到 SD 卡模式(RCW 源存在)后,我们就能进行验证了。 感谢大家的支持。 Re: LX2160ARDB: DDR validation 你的屏幕截图似乎和我的不一样,缺少“返回”和“取消”按钮。 您是否已按照QCVS_DDR_User_Guide 1.1.1 进行操作?使用DDR配置工具吗? 谢谢! Re: LX2160ARDB: DDR validation 看起来你已经成功读取了 SPD,虽然截图和我这边看到的略有不同。 请将 SW1[1:4] 设置为 1001 以从 eMMC 启动,其中 RCW 源已配置为 DDR 验证。 另外,请确认“目标连接”是否显示为已连接,请参见屏幕截图。 确认后,即可进行 DDR 验证。 June_Lu_0-1788504721222.png Re: LX2160ARDB: DDR validation 嗨,六月卢, 要从 SD 卡启动 LX2160ARDB,是否需要在 u-boot 源代码中修改 DDR 寄存器值,还是直接从 DIMM 的 SPD 读取? 请帮忙澄清一下……谢谢。 Re: LX2160ARDB: DDR validation 对于带有 DIMM 插槽的标准 LX2160ARDB,DDR 寄存器通过读取已安装 DIMM 的 SPD 进行自动配置——此过程由 TF-A BL2 阶段 (ddr_init.c) 处理,而非 U-Boot。只有在 LX2160ARDB 上使用自定义 DIMM 时才需要修改 ATF 源代码。 如果还有其他问题,请另开新帖,以便我们更好地跟踪,因为这个案例已经很久没有更新了。 谢谢。
View full article