2412394_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2412394_en-US

2412394_en-US

Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot builds

Hi,

we are using NXP Android Automotive 16.0.0_1.3.0 with kernel 6.12 and the prebuilt revisions documented by NXP:

platform/prebuilts/clang/host/linux-x86 66acdd82ee62e4aaa4248f03191c59dfed9db193 kernel/prebuilts/build-tools 3c5e4f14b451ec85167c38b917d2459687abd7f4 platform/prebuilts/rust 5156e7f81ae254c79ee736e44c960e75ad685c67 platform/prebuilts/clang-tools 17329f6590e2872dcf04a0c96a176be089470cd9

These are the revisions listed in the NXP Android Automotive User's Guide for this release.

The build works with these revisions, but our container vulnerability scan reports several HIGH and CRITICAL findings inside the supplied Android prebuilts.

For example, the Clang prebuilts contain embedded Go standard libraries. For clang-r536225/bin/clang, the scan reports:

Total: 22 HIGH: 21 CRITICAL: 1 Go stdlib version: v1.23.2 Example: CVE-2025-68121 crypto/tls - incorrect certificate validation

The same finding pattern also appears in clang++ and clang-tidy, and in the newer clang-r547379 binaries where the embedded Go version is v1.23.4.

The NXP-pinned kernel/prebuilts/build-tools also contains affected soong_zip binaries with the same Go-stdlib finding pattern.

The Rust prebuilts also contain findings in shipped Cargo lock files, for example:

thin-vec 0.2.13 CVE-2026-6654 fixed in 0.2.16 hashbrown 0.15.0 GHSA-wwq9-3cpr-mm53 fixed in 0.15.1


We do not want to replace the documented revisions with arbitrary newer AOSP commits, because these prebuilts are part of the NXP kernel/U-Boot build environment and we want to preserve compatibility with Android Automotive 16.0.0_1.3.0 / kernel 6.12.

Are there newer NXP-recommended or known-compatible commit IDs for these prebuilts?

In particular, we are looking for updated revisions for:

platform/prebuilts/clang/host/linux-x86 kernel/prebuilts/build-tools platform/prebuilts/rust platform/prebuilts/clang-tools

 

Has NXP, or anyone in the community, already updated these revisions and verified that the following still work?

Ideally, we would also like confirmation that a complete Android Automotive build still works with the updated prebuilts.

We would prefer to update the affected prebuilts instead of permanently suppressing the security findings.

I have attached the failed vulnerability scan log for reference. It contains the complete findings for the affected Clang, kernel build-tools and Rust prebuilts, including detected embedded versions and available fixed versions.

Thanks.

AndroidRe: Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot bu

Hello,

I'm reviewing your issue, I'll keep you updated. 

Regards.

Re: Security-updated prebuilts for Android Automotive 16.0.0_1.3.0 without breaking kernel/U-Boot bu

Hello, 


Internal team has shared below reply.
 


We have not any newer recommended/know-compatible commit IDs for 


  • platform/prebuilts/clang/host/linux-x86

  • kernel/prebuilts/build-tools

  • platform/prebuilts/rust

  • platform/prebuilts/clang-tools

and for Android 16.0 automotive 1.3.0 release version.
 
Android 16.0 automotive 1.3.0 has been released on May-21 2026, since then there have been no updates for this release. We do not update Android automotive releases; we are working on the next Android automotive release => Android 16.0 automotive 2.1.0 based on Linux kernel 6.18.y & with updated Linux kernel build tools.
External release date of AA16.0 2.1.0 is on Oct-13 2026.

Tags (1)
No ratings
Version history
Last update:
2 weeks ago
Updated by: